Hello, all
I'm trying to build the Sai_47478A_440_100 example in S32DS 3.4 for S32K344, but I am encountering the following issues.
1. .mex File Load Error in Peripheral Mode
When I select the project from the Peripheral tab, I get the following error:
"error during opening configuration sai_~.mex
processor s32k344, platformsdk_s32k3 version is not supported by current version of the tool"s32ds3.4_error_loading_mex.png
I'm using S32DS 3.4 and have installed SW32K3_RTD_4.4_1.0.0.
How can I properly load the .mex file in Peripheral Mode?
The goal is to integrate this code into RTD 5.0.0 in S32DS 3.5
If anyone has faced a similar issue, I would appreciate any guidance on resolving this.
Thank you!
The Sai_47478A_440_100 project is configured by EBTresos instead of S32 Configuration Tool(S32DS).
You need to import the C:\NXP\S32K344_Whiteboard_Example_RTM_1.0.0\S32K344_Whiteboard_Example_RTM_1.0.0\SAI\Sai_47478A_440_100\Tresos_Project\Sai_47478A_440_100 by using EBTresos.
Here is the configuration of LPI2C0:
Sai_47478A_440_100 Tresos_Project i2c.png
Sorry, I'm afraid you need to refer to EBTresos Project to migrate the project to RTD 5.0.0 in S32DS.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------