Hello everyone,
I'm tryng to build the imx-boot image by using imx-mkimage, following the steps I found for i.MX 93 A1 in Linux Users Guide (from 39/166 to 40/166):
https://www.nxp.com/doc/IMX_LINUX_USERS_GUIDE
I succesfully build u-boot.bin and u-boot-spl.bin (GitHub - nxp-imx/uboot-imx at lf_v2023.04) and I and I copied them in imx-mkimage/iMX93 (source: GitHub - nxp-imx/imx-mkimage: i.MX Mkimage Bootloader Tool 6.6.3_1.0.0).
In the same folder I put bl31.bin, generated from GitHub - nxp-imx/imx-atf: i.MX ARM Trusted firmware together with mx93a1-ahab-container.img (u-boot/doc/board/nxp/imx93_11x11_evk.rst at master · u-boot/u-boot · GitHub) . So the final content of the folder is this:
When it comes to run the command:
make SOC=iMX93 flash_singleboot
The output gives the following error:
Can anyone help me with this issue? I can't figure out what is going on.
Thanks, in advance,
Bob
Thank you, now it works!
Regards,
Bob
Hi,
This is another issue missing DDR firmware.
Follow the steps as below.
wget https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/firmware-imx-8.23.bin
chmod +x firmware-imx-8.23.bin
./firmware-imx-8.23.bin
copy missing ddr firmware from -> firmware-imx-8.23/firmware/ddr/synopsys/
Regards
Harvey
Hello,
I tried to do the gitclone command as you suggested:
git clone https://github.com/nxp-imx/imx-mkimage.git
The download terminated succesfully, then I moved all the necessary files into iMX93 folder. Then I execute:
make SOC=iMX93 flash_singleboot
this command returns:
How can i go ahead?
Regards,
Bob
This seems to be a problem with your git.
or did you download the imx-mkimage in git clone?
Regards
Harvey
Hello @Harvey021 ,
Thanks for responding,
I tried the command you suggested and this is the output:
Can you tell me what I have to do next?
Thanks,
Bob
It seems that the commit number has not been generated. please make sure your download. Have a run "git rev-parse --short=8 HEAD >> src/build_info.h" to see what it is.
Regards
Harvey