Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
NHS3100 app_demo_dp_url 更新された NDEF メッセージ こんにちは。app_demo_dp_urlをベースラインとして使用し、センサーの読み取り値で更新しています。センサーの読み取りには約200ms(積分時間)かかります。NDEFメッセージを更新し、更新されたメッセージが存在することをリーダー(スマートフォン)に「通知」するにはどうすればよいですか? 測定時間が50msを超えると、電話はタグの適切な読み取りを停止し、「空のタグ」を返します。よろしくお願いいたします
View full article
About 32K3 MCAL RTD version control I wanna ask something about the S32K3 RTD version number. I find that the code of module MEM_43_INFLS in version S32K3_RTD_3_0_0_P07_D2306_ASR_REL_4_7_REV_0000_20230629 and version S32K3_RTD_3_0_0_D2303_ASR_REL_4_7_REV_0000_20230331 are different in case. So I just wanna know what "P07" means in RTD version number. Thanks! Re: About 32K3 MCAL RTD version control Hi @ZMY666777, S32K3_RTD_3_0_0_P07_D2306 is Patch 07 for S32K3_RTD_3_0_0_D2303. Refer to the release notes of S32K3_RTD_3_0_0_P07_D2306. The driver is updated in the patch. Regards, Daniel
View full article
LPC54616 LINブレークジェネレーション LPC54616ユーザーマニュアルに記載されているLINのUSART0によって生成されたブレーク信号は利用できないようです。LINモードでUSART0を使用してブレーク信号を生成する方法と、USARTの初期化を設定する方法を知りたいですか? Re:LPC54616 LINブレークジェネレーション 私が言いたいのは、現在usart0を使用してlinバス機能を実行していますが、LINパケットを送信するときに問題が発生しているということです。LINパケットはブレーク信号(同期インターバル(ブレークフィールド))で始まります。この信号を正常に送信するにはどうすればよいですか?また、USART0割り込みはどのように構成できますか? Re:LPC54616 LINブレークジェネレーション こんにちは、私の名前はパベルです、そして私はあなたのケースをサポートします、あなたはフレームの開始または停止を意味しましたか?もう少し詳しく教えていただけますか? よろしくお願いいたします パベル
View full article
TI AM62x 上的 88W9098 我正在尝试编译 nxp-imx/mwifiex repo 以用于 ARM64 AM62x-Board,并遵循以下说明: https://community.nxp.com/t5/Wireless-Connectivity/Wifi-Driver-Build-for-Generic-ARM64/td-p/1598321 驱动程序编译没有问题,我将 moal.ko 和 mlan.ko 放在 /lib/modules/[...]/extra 文件夹中,以及 .conf以及固件/nxp文件夹中的.bin。 当我尝试加载模块时,出现以下错误: modprobe moal mod_para=nxp/wifi_mod_para.conf [108.554822] moal:未知符号 cfg80211_sched_scan_results(错误-2) [108.561485] moal:未知符号 cfg80211_mgmt_tx_status_ext(错误-2) [108.568052] moal:未知符号 cfg80211_rx_assoc_resp(错误-2) [108.574271] moal:未知符号regulatory_set_wiphy_regd_sync(错误-2) [108.581153] moal:未知符号 cfg80211_scan_done(错误-2) [108.586943] moal:未知符号 cfg80211_sched_scan_stopped(错误-2) [108.593461] moal:未知符号 cfg80211_remain_on_channel_expired(错误-2) [108.600515] moal:未知符号 cfg80211_cac_event(错误-2) [108.606188] moal:未知符号 cfg80211_register_netdevice(错误-2) [108.612695] moal:未知符号regulatory_hint(错误-2) [108.618160]moal:未知符号cfg80211_new_sta(错误-2) [108.623655] moal:未知符号 cfg80211_disconnected(错误-2) [108.629651] moal:未知符号 wiphy_new_nm(错误-2) [108.634794] moal:未知符号 cfg80211_ready_on_channel(错误-2) [108.641077]moal:未知符号cfg80211_classify8021d(错误-2) [108.647089] moal:未知符号 cfg80211_rx_mlme_mgmt(错误-2) [108.653038] moal:未知符号 wiphy_register(错误-2) [108.658365] moal:未知符号 __cfg80211_alloc_reply_skb(错误-2) [108.664735] moal:未知符号 __cfg80211_alloc_event_skb(错误-2) [108.671107]moal:未知符号cfg80211_put_bss(错误-2) [108.676602]moal:未知符号cfg80211_roamed(错误-2) [108.682002] moal:未知符号 cfg80211_ch_switch_notify(错误-2) [108.688296] moal:未知符号 ieee80211_get_channel_khz(错误-2) [108.694565] moal:未知符号 __cfg80211_radar_event(错误-2) [108.700582] moal:未知符号 cfg80211_tdls_oper_request(错误-2) [108.706961]moal:未知符号cfg80211_find_elem_match(错误-2) [108.713148] moal:未知符号 __cfg80211_send_event_skb(错误-2) [108.719472] moal:未知符号 cfg80211_michael_mic_failure(错误-2) [108.726012] moal:未知符号 wiphy_apply_custom_regulatory(错误-2) [108.732657]moal:未知符号cfg80211_del_sta_sinfo(错误-2) [108.738678] moal:未知符号 wiphy_unregister(错误-2) [108.744218] moal:未知符号 cfg80211_get_bss(错误-2) [108.749740] moal:未知符号 ieee80211_freq_khz_to_channel(错误-2) [108.756357] moal:未知符号 cfg80211_pmksa_candidate_notify(错误-2) [108.763144] moal:未知符号 cfg80211_vendor_cmd_reply(错误-2) [108.769416] moal:未知符号 cfg80211_cqm_beacon_loss_notify(错误-2) [108.776286] moal:未知符号 cfg80211_unregister_wdev(错误-2) [108.782482] moal:未知符号 cfg80211_rx_mgmt_ext(错误-2) [108.788361] moal:未知符号 ieee80211_channel_to_freq_khz(错误-2) [108.794986]moal:未知符号ieee80211_hdrlen(错误-2) [108.800499]moal:未知符号cfg80211_report_wowlan_wakeup(错误-2) [108.807111] moal:未知符号 cfg80211_ft_event(错误-2) [108.812721] moal:未知符号 cfg80211_inform_bss_data(错误-2) [108.818951]moal:未知符号ieee80211_bss_get_elem(错误-2) [108.824983] moal:未知符号 cfg80211_connect_done(错误-2) [108.830903] moal:未知符号 cfg80211_unlink_bss(错误-2) [108.836660] moal:未知符号 wiphy_free(错误-2) [108.841648] moal:未知符号 cfg80211_cqm_rssi_notify(错误-2) [108.847851] moal:未知符号 cfg80211_auth_timeout(错误-2) modprobe:错误:无法插入“moal”:模块中未知符号或未知参数(参见 dmesg) 有什么提示可以告诉我如何解决这个问题吗?对于编译,我使用 Yocto SDK、tmp/work/[...]/build 中的 KERNELDIR(内核构建文件,类似于 NXP-BSP 中的构建文件)和 mwifiex 中最近的分支(lf-6.1.55_2.2.0 用于 linux-ti-staging 6.1.46) 回复:TI AM62x 上的 88W9098 当然,我会关闭这个。 此致, 多米尼克 回复:TI AM62x 上的 88W9098 你好@Christine_Li , 我忙于其他任务,所以没有注意到假期 😉 88W9098 仍然无法工作,但这可能是因为 SDIO 部分配置错误。 在存在 cfg80211.ko 的情况下驱动程序已成功加载,但由于某种原因它未安装在映像中。如果我成功了或者遇到其他困难,我会及时通知你! 此致, 多米尼克
View full article
Boot logs for debugging S32G399A-RDB3 Dear NXP fellows, I am currently debugging our custom design board based on the S32G399A-RDB3 model. For some reason, the PFE0 interface (connected through SGMII to the SerDes and the SJA1110 switch is not working as expected). I would like to compare some configurations. So, if possible, using the BSP41.0 and the default configuration (out-of-the box) for all the components, can you provide me the boot log of the board? Besides, can you run the following commands and provide me the output? During U-Boot: mii info pri hwconfig //After boot and root login: ifconfig -a dmesg | grep pfe0 dmesg | grep sja1110 ethtool pfe0 ethtool pfe1 ip link show pfe0 //Without any ethernet cable connected) ip link show pfe0 //With Ethernet cable connected at port P2 or P3) ifconfig pfe0 ping //With Ethernet cable connected at port P2 or P3) That would be a valuable resource for my investigation. Thank you very much, Best regards, Guilherme Re: Boot logs for debugging S32G399A-RDB3 Hello, @chenyin_h  Ok, thank you very much for your feedback. Best regards, Guilherme Re: Boot logs for debugging S32G399A-RDB3 Hello, @GuilhermeS32G3 1. If by default no cable connected to the PFE0 interface(P2 or P4), the prints are as following: pfe0: flags=4163 mtu 1500 inet6 fe80::204:9fff:febe:ef00 prefixlen 64 scopeid 0x20 ether 00:04:9f:be:ef:00 txqueuelen 1000 (Ethernet) RX packets 0 bytes 0 (0.0 B) 2. Regarding to the sja1110_switch.bin, yes, it is correct from your assumption. For SJA1110 related images, they both are generated from the SJA1110 SDK, from S32G forum perspective, the only document related with this topic is the one you mentioned, for the information that beyond this document is not included in our supporting scope. I do apologize. BR Chenyin Re: Boot logs for debugging S32G399A-RDB3 Hello @chenyin_h , Thank you for the log, it was certainly helpful. Yes, I also have this issue with mii info resetting the board from my side. Actually it happens when I use the default configuration, but when I modify the device tree files, it doesn't happen. From your ifconfig output: pfe0: flags=4163 mtu 1500 inet 10.192.209.48 netmask 255.255.255.0 broadcast 10.192.209.255 inet6 fe80::204:9fff:febe:ef00 prefixlen 64 scopeid 0x20 ether 00:04:9f:be:ef:00 txqueuelen 1000 (Ethernet) RX packets 7 bytes 1454 (1.4 KiB) RX errors 0 dropped 0 overruns 0 frame 0 TX packets 21 bytes 2248 (2.1 KiB) TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0 device memory 0x46000000-46ffffff Can you confirm that the proper behavior of pfe0 when configured as SGMII is to have non-zero RX packets and TX packets even when no ethernet cable is connected? I also found that this behavior: [ 7.765177] sja1110 spi5.1: Could not get GPIO from device tree [ 7.765196] sja1110 spi5.1: [sja1110_post_probe_upload_worker] Trying to initialize switch [ 7.766772] sja1110 spi5.1: Direct firmware load for sja1110_switch.bin failed with error -2 [ 7.766785] sja1110 spi5.1: request_firmware failed with -2 [ 7.766790] sja1110 spi5.0: [sja1110_post_probe_upload_worker] Trying to initialize uC [ 7.766822] sja1110 spi5.0: Direct firmware load for sja1110_uc.bin failed with error -2 [ 7.766828] sja1110 spi5.0: request_firmware failed with -2 Is due to the position of the J189 jumpers. In the default configuration it just loads the default firmware. When both sides are in state short, then it successfully reads the firmware files from lib/firmware/ folder, as described here. But another question is: How can I get the file sja1110_switch.bin? Following the Ethernet Enablement Guide, I am able to reconfigure the SJA1110 switch, but it only explains how to generate the flash_image.bin file that corresponds to sja1110_uc.bin. How about the other configuration file? How is it generated? Thank you again, Best regards, Guilherme Re: Boot logs for debugging S32G399A-RDB3 Hello, @GuilhermeS32G3  You are welcome and thanks for your post. All right, please find the attached log for your reference with BSP41 running on RDB3. Some comments below: mii command seems work incorrect on the current BSP, the command will trigger the board to reset. Ping test is not included in the log, but it works well from my side. BR Chenyin Re: Boot logs for debugging S32G399A-RDB3 If it is not asking too much, could you please also include the output of the command mdio list from U-boot? Thank you
View full article
88W9098 on TI AM62x I'm trying to compile the nxp-imx/mwifiex repo for use with an ARM64 AM62x-Board and followed this instructions: https://community.nxp.com/t5/Wireless-Connectivity/Wifi-Driver-Build-for-Generic-ARM64/td-p/1598321 The driver compiles without problems and I placed the moal.ko & mlan.ko in the /lib/modules/[...]/extra folder as well as the .conf and .bin in the firmware/nxp folder. When I try to load the module, I get following errors: modprobe moal mod_para=nxp/wifi_mod_para.conf [ 108.554822] moal: Unknown symbol cfg80211_sched_scan_results (err -2) [ 108.561485] moal: Unknown symbol cfg80211_mgmt_tx_status_ext (err -2) [ 108.568052] moal: Unknown symbol cfg80211_rx_assoc_resp (err -2) [ 108.574271] moal: Unknown symbol regulatory_set_wiphy_regd_sync (err -2) [ 108.581153] moal: Unknown symbol cfg80211_scan_done (err -2) [ 108.586943] moal: Unknown symbol cfg80211_sched_scan_stopped (err -2) [ 108.593461] moal: Unknown symbol cfg80211_remain_on_channel_expired (err -2) [ 108.600515] moal: Unknown symbol cfg80211_cac_event (err -2) [ 108.606188] moal: Unknown symbol cfg80211_register_netdevice (err -2) [ 108.612695] moal: Unknown symbol regulatory_hint (err -2) [ 108.618160] moal: Unknown symbol cfg80211_new_sta (err -2) [ 108.623655] moal: Unknown symbol cfg80211_disconnected (err -2) [ 108.629651] moal: Unknown symbol wiphy_new_nm (err -2) [ 108.634794] moal: Unknown symbol cfg80211_ready_on_channel (err -2) [ 108.641077] moal: Unknown symbol cfg80211_classify8021d (err -2) [ 108.647089] moal: Unknown symbol cfg80211_rx_mlme_mgmt (err -2) [ 108.653038] moal: Unknown symbol wiphy_register (err -2) [ 108.658365] moal: Unknown symbol __cfg80211_alloc_reply_skb (err -2) [ 108.664735] moal: Unknown symbol __cfg80211_alloc_event_skb (err -2) [ 108.671107] moal: Unknown symbol cfg80211_put_bss (err -2) [ 108.676602] moal: Unknown symbol cfg80211_roamed (err -2) [ 108.682002] moal: Unknown symbol cfg80211_ch_switch_notify (err -2) [ 108.688296] moal: Unknown symbol ieee80211_get_channel_khz (err -2) [ 108.694565] moal: Unknown symbol __cfg80211_radar_event (err -2) [ 108.700582] moal: Unknown symbol cfg80211_tdls_oper_request (err -2) [ 108.706961] moal: Unknown symbol cfg80211_find_elem_match (err -2) [ 108.713148] moal: Unknown symbol __cfg80211_send_event_skb (err -2) [ 108.719472] moal: Unknown symbol cfg80211_michael_mic_failure (err -2) [ 108.726012] moal: Unknown symbol wiphy_apply_custom_regulatory (err -2) [ 108.732657] moal: Unknown symbol cfg80211_del_sta_sinfo (err -2) [ 108.738678] moal: Unknown symbol wiphy_unregister (err -2) [ 108.744218] moal: Unknown symbol cfg80211_get_bss (err -2) [ 108.749740] moal: Unknown symbol ieee80211_freq_khz_to_channel (err -2) [ 108.756357] moal: Unknown symbol cfg80211_pmksa_candidate_notify (err -2) [ 108.763144] moal: Unknown symbol cfg80211_vendor_cmd_reply (err -2) [ 108.769416] moal: Unknown symbol cfg80211_cqm_beacon_loss_notify (err -2) [ 108.776286] moal: Unknown symbol cfg80211_unregister_wdev (err -2) [ 108.782482] moal: Unknown symbol cfg80211_rx_mgmt_ext (err -2) [ 108.788361] moal: Unknown symbol ieee80211_channel_to_freq_khz (err -2) [ 108.794986] moal: Unknown symbol ieee80211_hdrlen (err -2) [ 108.800499] moal: Unknown symbol cfg80211_report_wowlan_wakeup (err -2) [ 108.807111] moal: Unknown symbol cfg80211_ft_event (err -2) [ 108.812721] moal: Unknown symbol cfg80211_inform_bss_data (err -2) [ 108.818951] moal: Unknown symbol ieee80211_bss_get_elem (err -2) [ 108.824983] moal: Unknown symbol cfg80211_connect_done (err -2) [ 108.830903] moal: Unknown symbol cfg80211_unlink_bss (err -2) [ 108.836660] moal: Unknown symbol wiphy_free (err -2) [ 108.841648] moal: Unknown symbol cfg80211_cqm_rssi_notify (err -2) [ 108.847851] moal: Unknown symbol cfg80211_auth_timeout (err -2) modprobe: ERROR: could not insert 'moal': Unknown symbol in module, or unknown parameter (see dmesg) Any hints how I can solve this? For compilation I use the Yocto SDK, the KERNELDIR in tmp/work/[...]/build (kernel buildfiles, analog to the build files in the NXP-BSP) and the nearest branch in mwifiex (lf-6.1.55_2.2.0 for use with linux-ti-staging 6.1.46) Re: 88W9098 on TI AM62x Of course, I will close this one. Best regards, Dominik Re: 88W9098 on TI AM62x Hi, @dpog  Thanks for your feedback. If you need more time, would you mind help to close this current case, and after you verified, then create a new case to us? It would be appreciated if you could create a new case after you verified still have issue or have other new questions. Best regards, Christine. Re: 88W9098 on TI AM62x Hi @Christine_Li, I was occupied by other tasks, so i didn't notice the holiday 😉 The 88W9098 still doesn't work, but thats probably because of a misconfiguration on the SDIO part. The driver is being loaded successfully with cfg80211.ko present, for some reason it was not installed in the image. I will keep you posted if I succeed or face other dificulties! Best regards, Dominik Re: 88W9098 on TI AM62x Hi, @dpog  Does the 88W9098 work on your side? I am back from the public holiday, please do not hesitate to let me know if still need support. And also provide me your detailed current status and related dmesg logs. Best regards, Christine. Re: 88W9098 on TI AM62x Hi, @dpog  Thanks for creating case to us. From your logs, I think you need also to compile cfg802.11.ko based on your host platform. You can search how to cross compile cfg80211.ko on Linux to fix this error. Usually, you can configure it through make menuconfig during compiling Linux kernel BSP. Also, if after you compiled cfg80211.ko, you still meet any failure, please provide me your full dmesg logs for further debugging. And for your information, we will start our Mid-Autumn public holiday from tomorrow and come back to office until 18th/Sep. So please allow me replying delay for this case. Sorry for the inconvenience to you. ​ Best regards, Christine.​
View full article
The ENET1 module does not function unless the Peripheral control register (MC_ME_PCTL6) is enabled 工程文件:lwip_mpc5748g 开发板型号:2018 NXP B.V. MPC5748G-GW 按照 MPC5748G-GW-RDB_ExampleCodes-UserGuide中的步骤来进行ENET1的开发 但是当前连PING也不通过,通过论坛里的一些相关回答,尝试了在PC上增加ARP表,但是仍然PING不通,此时在翻阅文档时发现有标注错误问题,但是通过查看寄存器说明,不是很理解这里说的enable是指做出什么样的设置。 MPC5748G-GW-RDB 
View full article
Automatic Power-On Behavior for i.MX8MP with overtemperature I am using a congatec SMARC module with a imx8mp processor. To clarify our requirements: When the temperature sensor on the SMARC module reaches 105°C, the system powers off. Currently, the system requires a manual power cycle to restart. I would like to modify this behaviour so that the system automatically powers back on when the temperature falls below the trigger threshold. We found references suggesting that this behaviour could be modified in the SCFW (System Controller Firmware). However, the SCFW firmware is not used for the i.MX8MP processor. The boot sequence for the i.MX8MP is as follows: BootROM → SPL → BL31 (ATF - ARM Trusted Firmware) → OP-TEE (Optional) → BL33 (U-Boot) → Linux kernel. Based on our understanding, potential areas to address this behaviour include: a) Modifying BL31 (ATF).          Adjusting settings within the SNVS (Secure Non-Volatile Storage). b) Configuring the PMIC PCA9450C present on the SMARC module to enable auto-power-on. If the PMIC configuration is the correct path, could you provide documentation or details on configuring the PCA9450C for automatic power-on? Or, do you have a better solution? Evaluation Board Re: Automatic Power-On Behavior for i.MX8MP with overtemperature I ended up setting a wake up alarm, and adding a service to set it up just before the shutdown. So each time the system would be triggered a power off etc. the alarm will be triggered. Better than nothing. echo +120 > /sys/class/rtc/rtc1/wakealarm   Re: Automatic Power-On Behavior for i.MX8MP with overtemperature dear Marco_Savo, to modify the BL31 is not an option. your second option is not posible due you have to assert the PMIC_ON_REQ in order to start the power-on sequence it hasn't an auto power-on. You could use a FPGA to assert the PMIC_ON_REQ signal.
View full article
TI AM62x の 88W9098 ARM64 AM62x-Boardで使用するためにnxp-imx / mwifiexリポジトリをコンパイルしようとしており、次の手順に従いました https://community.nxp.com/t5/Wireless-Connectivity/Wifi-Driver-Build-for-Generic-ARM64/td-p/1598321 ドライバは問題なくコンパイルされ、私は moal.ko と mlan.ko を /lib/modules/[...]/extra フォルダと .confそして.bin firmware/nxpフォルダにあります。 モジュールをロードしようとすると、次のエラーが表示されます。 modprobe moal mod_para=nxp/wifi_mod_para.conf [ 108.554822] moal: 不明な記号 cfg80211_sched_scan_results (err -2) [ 108.561485] moal: 不明な記号 cfg80211_mgmt_tx_status_ext (err -2) [ 108.568052] moal: 不明な記号 cfg80211_rx_assoc_resp (err -2) [ 108.574271] moal: 不明な記号 regulatory_set_wiphy_regd_sync (エラー-2) [ 108.581153] moal: 不明な記号 cfg80211_scan_done (err -2) [ 108.586943] moal: 不明な記号 cfg80211_sched_scan_stopped (err -2) [ 108.593461] moal: 不明な記号 cfg80211_remain_on_channel_expired (err -2) [ 108.600515] moal: 不明な記号 cfg80211_cac_event (err -2) [ 108.606188] moal: 不明な記号 cfg80211_register_netdevice (err -2) [ 108.612695] moal: 不明な記号 regulatory_hint (err -2) [ 108.618160] moal: 不明な記号 cfg80211_new_sta (err -2) [ 108.623655] moal: 不明な記号 cfg80211_disconnected (err -2) [ 108.629651] moal: 不明な記号 wiphy_new_nm (err -2) [ 108.634794] moal: 不明な記号 cfg80211_ready_on_channel (err -2) [ 108.641077] moal: 不明な記号 cfg80211_classify8021d (err -2) [ 108.647089] moal: 不明な記号 cfg80211_rx_mlme_mgmt (err -2) [ 108.653038] moal: 不明な記号 wiphy_register (err -2) [ 108.658365] moal: 不明な記号 __cfg80211_alloc_reply_skb (err -2) [ 108.664735] moal: 不明な記号 __cfg80211_alloc_event_skb (err -2) [ 108.671107] moal: 不明な記号 cfg80211_put_bss (err -2) [ 108.676602] moal: 不明な記号 cfg80211_roamed (err -2) [ 108.682002] moal: 不明な記号 cfg80211_ch_switch_notify (err -2) [ 108.688296] moal: 不明な記号 ieee80211_get_channel_khz (err -2) [ 108.694565] moal: 不明な記号 __cfg80211_radar_event (err -2) [ 108.700582] moal: 不明な記号 cfg80211_tdls_oper_request (err -2) [ 108.706961] moal: 不明な記号 cfg80211_find_elem_match (err -2) [ 108.713148] moal: 不明な記号 __cfg80211_send_event_skb (err -2) [ 108.719472] moal: 不明な記号 cfg80211_michael_mic_failure (err -2) [ 108.726012] moal: 不明な記号 wiphy_apply_custom_regulatory (err -2) [ 108.732657] moal: 不明な記号 cfg80211_del_sta_sinfo (err -2) [ 108.738678] moal: 不明な記号 wiphy_unregister (err -2) [ 108.744218] moal: 不明な記号 cfg80211_get_bss (エラー-2) [ 108.749740] moal: 不明な記号 ieee80211_freq_khz_to_channel (err -2) [ 108.756357] moal: 不明な記号 cfg80211_pmksa_candidate_notify (err -2) [ 108.763144] moal: 不明な記号 cfg80211_vendor_cmd_reply (err -2) [ 108.769416] moal: 不明な記号 cfg80211_cqm_beacon_loss_notify (err -2) [ 108.776286] moal: 不明な記号 cfg80211_unregister_wdev (err -2) [ 108.782482] moal: 不明な記号 cfg80211_rx_mgmt_ext (エラー-2) [ 108.788361] moal: 不明な記号 ieee80211_channel_to_freq_khz (err -2) [ 108.794986] moal: 不明な記号 ieee80211_hdrlen (err -2) [ 108.800499] moal: 不明な記号 cfg80211_report_wowlan_wakeup (err -2) [ 108.807111] moal: 不明な記号 cfg80211_ft_event (err -2) [ 108.812721] moal: 不明な記号 cfg80211_inform_bss_data (err -2) [ 108.818951] moal: 不明な記号 ieee80211_bss_get_elem (err -2) [ 108.824983] moal: 不明な記号 cfg80211_connect_done (err -2) [ 108.830903] moal: 不明な記号 cfg80211_unlink_bss (err -2) [ 108.836660] moal: 不明な記号 wiphy_free (err -2) [ 108.841648] moal: 不明な記号 cfg80211_cqm_rssi_notify (err -2) [ 108.847851] moal: 不明な記号 cfg80211_auth_timeout (err -2) modprobe: エラー: 'moal' を挿入できませんでした: モジュール内の不明なシンボル、または不明なパラメータ (dmesg を参照) これをどのように解決できるかのヒントはありますか?コンパイルには、Yocto SDK、tmp/work/のKERNELDIRを使用します[...]/build (カーネルビルドファイル、NXP-BSP のビルドファイルに類似) と mwifiex の最も近いブランチ (linux-ti-staging 6.1.46 で使用するための lf-6.1.55_2.2.0) 日時:TI AM62xの88W9098 もちろん、これは閉じます。 よろしくお願いいたします ドミニク 日時:TI AM62xの88W9098 こんにちは @Christine_Li、 他の仕事で忙しかったので、休日に気づかなかった 😉 88W9098 はまだ動作しませんが、これはおそらく SDIO 部分の設定ミスが原因です。 ドライバーは cfg80211.ko が存在する状態で正常に読み込まれていますが、何らかの理由でイメージにインストールされていません。私が成功した場合、または他の困難に直面した場合は、あなたを投稿し続けます! よろしくお願いいたします ドミニク
View full article
MIMXRT1170SDK 中的 CONFIG_WIFI_SMOKE_TESTS 有什么用途? 我正在尝试了解 SDK (2_16_100) MIMXRT1170-EVKB 中的 wifi_examples/wifi_cli 示例。谁能告诉我 CONFIG_WIFI_SMOKE_TESTS 的用途是什么?我看到这会将以太网接口拉入 wifi_cli 构建中,但我不太明白其目的是什么。 有什么想法吗? 回复:MIMXRT1170SDK 中的 CONFIG_WIFI_SMOKE_TESTS 有什么用途? 再试一次... 有关于此的最新消息吗? 回复:MIMXRT1170SDK 中的 CONFIG_WIFI_SMOKE_TESTS 有什么用途? 谢谢。我一直在看代码,但很难弄清楚这个宏的用途。 目前我正在使用 Embedded Artists 2EL M.2 模块(WIFI_IW612_BOARD_MURATA_2EL_M2);但这可能会改变。 回复:MIMXRT1170SDK 中的 CONFIG_WIFI_SMOKE_TESTS 有什么用途? 有最新消息吗?
View full article
MK60F12 - Unable to lock JTAG by securing flash through FSEC I'm trying to lock the JTAG on the MK60F12 by through the Flash Configuration loaded from program flash at 0x400 at startup. However, no matter what I put in the SEC field of flash configuration FSEC (0b00, 0b01 or 0b11), the FTFL_FSEC register always loads with 0b10 (unsecured). I tried changing other fields of FSEC (KEYEN, MEEN, etc.) and that works, but FSEC is always 0b10. I'm using the SEGGER J-Link JTAG programmer. Would anybody have any clue to why I'm not able to secure FSEC? Kinetis K Series MCUs Re: MK60F12 - Unable to lock JTAG by securing flash through FSEC Hi @LRawlyk  Thank you for reaching out! Let me provide my first recommendation, so you could double check.  In the device selection, please try to select the Allow security option option for your part. Here is an example for the Segger J-Link commander. I do not know about the tools that you are using, but please ensure to select that option, per my experience, with this it will allow you to manipulate FSEC.  Just beware of the MEEN, the if the mass erase is not enabled, you won't be able to write a new image with the FSEC enabled again. I hope this could help you!  Diego
View full article
What is the purpose of CONFIG_WIFI_SMOKE_TESTS in the MIMXRT1170SDK? I'm trying to get to know the wifi_examples/wifi_cli example in the SDK (2_16_100) MIMXRT1170-EVKB.  Can anyone tell me what the purpose of the CONFIG_WIFI_SMOKE_TESTS is for?  I see that this pulls in the Ethernet interface into the wifi_cli build, but I don't quite follow what the purpose is. Any thoughts? Re: What is the purpose of CONFIG_WIFI_SMOKE_TESTS in the MIMXRT1170SDK? Hi, This macro is for internal use only. Please ignore it. Regards, Daniel Re: What is the purpose of CONFIG_WIFI_SMOKE_TESTS in the MIMXRT1170SDK? Trying again... Any updates on this? Re: What is the purpose of CONFIG_WIFI_SMOKE_TESTS in the MIMXRT1170SDK? Thanks. I've been looking at the code, but it's just tough to figure out what that macro is for. Right now I'm using the Embedded Artists 2EL M.2 module (WIFI_IW612_BOARD_MURATA_2EL_M2); but that may change. Re: What is the purpose of CONFIG_WIFI_SMOKE_TESTS in the MIMXRT1170SDK? Hi, I am still checking this. I going to ask internally. Please let me know the Wi-fi chipset you are using. Regards, Daniel Re: What is the purpose of CONFIG_WIFI_SMOKE_TESTS in the MIMXRT1170SDK? Any update on this? Re: What is the purpose of CONFIG_WIFI_SMOKE_TESTS in the MIMXRT1170SDK? Let me check. Regards, Daniel.
View full article
MK60F12 - FSEC を介してフラッシュを固定することで JTAG をロックできない 私は、起動時に0x400でプログラムフラッシュからロードされたフラッシュ設定を介して、MK60F12のJTAGをロックしようとしています。 ただし、フラッシュ構成FSEC(0b00、0b01、または0b11)のSECフィールドに何を入れても、FTFL_FSECレジスタは常に0b10(保護されていない)でロードされます。 FSECの他のフィールド(KEYEN、MEENなど)を変更してみましたが、それは機能しますが、FSECは常に0b10です。 SEGGER J-Link JTAGプログラマを使用しています。 誰かが私がFSECを保護できない理由についての手がかりを持っていますか? Kinetis KシリーズMCU
View full article
MK60F12 - 无法通过 FSEC 保护闪存来锁定 JTAG 我正在尝试通过在启动时从 0x400 的程序闪存中加载的闪存配置来锁定 MK60F12 上的 JTAG。 但是,无论我在闪存配置 FSEC 的 SEC 字段中输入什么(0b00、0b01 或 0b11),FTFL_FSEC 寄存器总是加载 0b10(不安全)。 我尝试更改 FSEC 的其他字段(KEYEN、MEEN 等),并且可行,但 FSEC 始终为 0b10。 我正在使用 SEGGER J-Link JTAG 编程器。 有人知道为什么我无法获得 FSEC 吗? Kinetis K系列MCU
View full article
MIMXRT1170SDK CONFIG_WIFI_SMOKE_TESTSの目的は何ですか? 私はSDK(2_16_100)MIMXRT1170-EVKBのwifi_examples / wifi_cliの例を知ろうとしています。誰かがCONFIG_WIFI_SMOKE_TESTSの目的を教えてもらえますか?これにより、イーサネットインターフェイスがwifi_cliビルドに引き込まれることがわかりますが、目的が何であるかはよくわかりません。 何か考えはありますか? Re:MIMXRT1170SDKでのCONFIG_WIFI_SMOKE_TESTSの目的は何ですか? 再試行しています... これに関する最新情報はありますか? Re:MIMXRT1170SDKでのCONFIG_WIFI_SMOKE_TESTSの目的は何ですか? 感謝。私はコードを見てきましたが、そのマクロが何のためにあるのかを理解するのは難しいです。 現在、Embedded Artists 2EL M.2モジュール(WIFI_IW612_BOARD_MURATA_2EL_M2)を使用しています。しかし、それは変わるかもしれません。 Re:MIMXRT1170SDKでのCONFIG_WIFI_SMOKE_TESTSの目的は何ですか? これに関する最新情報はありますか?
View full article
[I.MX93] eMMC design : pull-up & pull-down resistor Dear NXP Community, I am currently working on the eMMC PCBA design for the I.MX93 and noticed some differences between the NXP EVK design and our initial design. I would like to seek clarification on this matter. Based on the eMMC design guidelines I reviewed, it appears that pull-up resistors are generally required for CMD and DAT0-DAT7, and a pull-down resistor is needed for DS. However, upon referencing your design in the SPF-94611_B1.pdf, I noticed that these additional external resistors are not present in the eMMC circuitry. Could you kindly confirm if the absence of these external resistors is due to the presence of internal pull-up or pull-down resistors for DAT0-DAT7 and CMD within the I.MX93? If this understanding is correct, could you also advise whether configuring the internal pull-up or pull-down settings appropriately in the software will be sufficient to meet the design requirements? Thank you for your support, and I look forward to your guidance! Best regards, Howard  Re: [I.MX93] eMMC design : pull-up & pull-down resistor Hi @Chou! Thank you for contacting NXP Support! in iMX93-EVK board we configure the internal pull up resistors in those pins,. but I recommend to put external pull-up resistors to guarantee the logical state. This is a reference schematic The pull-up resistors are configured in u-boot device tree and maintain the configuration on Linux device tree Best Regards! Chavira
View full article
Clk2Cs parameter on Tresor issue Hello everyone, I'm trying to create a SPI code for S32K344 microcontroller using Tresos. On RTD I was able to create without error (.mex file), but when I try to do the same configuration on Tresos, I got error. The error shows that 1.0E-4 is out of range. But in the description it allow from 30ns up to 0.01s. Can someone help me to fix this problem, please? Thanks, MVR Re: Clk2Cs parameter on Tresor issue Hi MVR, I checked the file. This is an old implementation, so it's different with the RTD currently. Basically, the code not report any errors. It will set the minimum value (as 0) if you put delay time lower than minimum range, and set maximum value (as 255) if you put delay time higer than the maximum range. When you put the delay time as 0, the code will immediately return 1, then the bestSckPcs will be 0 -> Register CCR_SCKPCR = 0 In case you put the value not 0 but lower than minimum range, the for loop will return with sckpcs = 1, due to the abs() function will increase when sckpcs increase. Then the return value still 1, and bestSckPcs = 0 then. As your case, when you put the value higher than maximum range, the abs() will lowest when sckpcs = 256. So the DeviceInfo of CCR will be 255, as your current code. So from my opinion, for the current RTD driver, the errors is better (for customer), and you can set the maximum value of range for the 255 value of register CCR As i said, you can see the tool automatically calculate the maximum range, also you can calculate it easily as my previous done one. Thank you, Nam. Re: Clk2Cs parameter on Tresor issue Re: Clk2Cs parameter on Tresor issue Hello @NamLee  I will test with the new version.  Sure, follow attached the .c that you requested.  It is located in "C:\NXP\S32DS.3.4\eclipse\mcu_data\components\PlatformSDK_S32K3_2022_07\Spi" Thank you!! MVR Re: Clk2Cs parameter on Tresor issue Hi MVR, - Yes. Seems like your version is old one. Can you help me to test with RTD_updatesite 4.0.0 in your side? - Yes, for the 255 as maximum delay time you should put it as maximum in EB Tresos. The value range will be reported in the tool, so you can follow the range basically. One more point, in the 2.0.1 that you're using, can you help me to share the file Lpspi_Ip_PBcfg.c? It should be located in Spi component of PlatformSDK in C:\NXP\S32DS.3.5\eclipse\mcu_data\components\PlatformSDK_S32K3\Spi\Lpspi_Ip_PBcfg.c I wanna check the implementation of the SpiTimeClkCs. Thank you, Nam. Re: Clk2Cs parameter on Tresor issue Hello @NamLee  I'm using SW32K3_RTD_4.4_2.0.1_DS_updatesite_D2207. The problem is that when I define  1.0E-6, my application doesn't work... But when I define  1.0E-5 like the picture, it works but the SSCK is 255... As I could understand with this old version, when selected a value out of range it is automatically set 255, right? So in the new version, which value should I set for my application works? Should be 1/40M x (255 + 1) = 6.4E-6? I still doesn't have the hardware to test, but as soon as I receive back the hardware, I will test again. Thanks, MVR. Re: Clk2Cs parameter on Tresor issue Hi MVR, In my tested RTM 4.0.0, the error will be reported as i explained. I thought you're using RTD 4.0.0 also? Which is RTD_updatesite version that you're using right now? I'm using SW32K3_S32M27x_RTD_R21-11_4.0.0_D2311_DS_updatesite One more point, please help me to check the implementation of SpiTimeClk2Cs code gen. It should be located in file C:\NXP\S32DS.3.5\eclipse\mcu_data\components\PlatformSDK_S32K3\Spi\Lpspi_Ip_PBcfg.c I think you're using an old version, and the design at that time as i said, when you put a value higher than maximum then the register value will be set as 255, as in possible range. The number stands for delay time required between Clock and Cs signal. E.g: in my test, PCSSCK is 39 -> the delay time is 1/40M x (39 + 1) = 1.0E-6 With Busclock for LPSPI2 is 40M Hz. So in 4.0.0, if you wanna keep the maximum delay time (as current sequence) then you just put the maximum value for those nodes (as 6.4E-6) My point is, this is correct implementation in current design driver. Thank you, Nam. Re: Clk2Cs parameter on Tresor issue Hey @NamLee , The SDK that I'm using is "S32K3_RTD_2_0_1_D2207_ASR_REL_4_4_REV_0000_20220707". So maybe this version has this problem, right? So in the end, what value do these "255" represent? I know that this is the maximum value, but how is the reverse calculation so I can find out the correct value to configure in Tresos? Thanks, MVR Re: Clk2Cs parameter on Tresor issue Hi MVR, I checked with RTD K3 4.0.0 RTM The flow quite the same, when the SpiTimeClkCs value as input for GenerateExternalDeviceInfo function And we have the same flow of generate value, as when the time is too high or too low, than the error be loged out. In DS, when i set value Clk2Cs as 1.0E-5, the error reported. Because the range is maximum as 6.4E-6 (as calculation before) Same flow with Cs2Clk. when i put it as 1.0E-6, value is in range and no errors reported. To confirm about this, the generated values are matching with expectation 1> The SCKDIV is 78 -> as Scaler is 78 as calculation before. I'm using SLOW_CLK as 40M Hz for LPSPI2 channel 2> PCSSCK is 39 -> the delay time is 1/40M x (39 + 1) = 1.0E-6 3> SCKPCS is 0 as initialized value of Device.OptimalSCKPCS, only error log be updated. From my view, there's no problem with driver in both EB Tresos and DS tool. Thank you, Nam. Re: Clk2Cs parameter on Tresor issue Hello @NamLee, It makes sense, as soon as possible I will try with 6.4E-6. Now I don't have more the hardware because it is being used in other place. But when I get back it I will test. Also I will try to measure it.  Thank you! MVR Re: Clk2Cs parameter on Tresor issue Hi MVR, Thank you so much for your detailed answers. It's not a configure tool issue because the value of node still in range, but invalid corresponding to the Clock and Baudrate. Maybe in EB Tresos enable the feature Verify configuration everytime you change a node. It'll report errors before you hit generate. But it doesn't matter. The root cause is the delay time is longer than maximum range. I saw the value of CCR register, specially LPSPI_CCR_SCKPCS: - The SCKDIV is 78, which confirm that the calculation of ScalerValue is correct here. Your configuration is fine. - The SCKPCS/PCSSCK/DBT field is 255. Which is maximum of the range. From my guess, in DS, if the configured delay value is higher than the possible delay time amount, then the code gen will set 255 as maximum value for those delay times. I'll check the DS driver and code gen about this point. In additionally, can you set the value of SpiTimeClk2Cs in EB to 6.4E-6? I suppose the generated code will be the same (with the code from DS), and all sequences will run normally. Please help me to try this workaround. I'll also try in DS. Thank you, Nam. Re: Clk2Cs parameter on Tresor issue Only complementing (I can't edit what I sent): - Do you use DesiredBaudrateConfig and apply another Baudrate different with 500K? This might change the value of PrescalerValue. R: I didn't use "DesiredBaudrateConfig" and also I didn't try to apply another baudrate. Re: Clk2Cs parameter on Tresor issue Hello @NamLee , thank you by your support. First of all, I'm facing error before to generate the code on Tresos: Note: - I attached the SPI and MCU modules configuration. And answering your questions: - Do you use DesiredBaudrateConfig and apply another Baudrate different with 500K? This might change the value of PrescalerValue. R: I didn't use. - In case you enable DualClock mode, the BusClock will be BusClockAlternate R: I didn't enabled this option - Do you use the same package RTD 4.0.0 HF01 in DS? R: Yes and also I tested with the lastest version "4.00 HF02_D2407", which I get the same error. - In DS when you configure the value of Clk2Cs, can you give me the range of this node (in DS) in this time? R: Is it your request? -> - In generated code, can you give me value of LPSPI_CCR_SCKPCS? R: Configuration that works (Generated by DS tool): Configuration that doesn't work for me (generated by Tresos, with 😞 Thanks, MVR Re: Clk2Cs parameter on Tresor issue Hi MVR, I'm Nam from NXP RTD, i'm in charge of topic from Daniel so i comment directly here to discuss easier. I saw the error came from Generate code, not Configure tool. The Configuration not report error, but the Generate value is not in range of delay time in PrescaledClock About the value of TimeClk2Cs, it's the value of delay time in SCKPCS field, in range of 1~255 clock cycle which calculated with Prescaler as the field in TCR register. The clock be calculated from Bus clock (which is 40M Hz if you not choosing Dual Clock of SPI), and the PrescalerValue is 2^(Prescaler) which calculated here: With Busclock as 40M and DesiredBaudrate as 500K, the devide value should be 80, which mean the PrescalerValue is 1 (as 2^0) and the SckDiv will be 78. I tried to enable the DesiredBaudrateConfig with corresponding values, confirmed it's correct. So with PrescalerValue as 1, the PrescaledClock will equal with BusClock which is 40M Hz, and the Delaytime will have to in range of 2.5E-8 ~ 6.4E-6 As my view, i don't see problem with EB Config in my side, compare with RM of SPI. I'm doubting about your configuration in DS (.mex file) in 2 points: - Do you use DesiredBaudrateConfig and apply another Baudrate different with 500K? This might change the value of PrescalerValue. - Your clock of SPI be changed somewhere. Normally, the BusClock will be the reference clock which configured in this node, refered to Mcu In case you enable DualClock mode, the BusClock will be BusClockAlternate You should not enable the AlternateClockRef node. Can you help me check these 2 points? I have few questions with your DS tool configuration:  - Do you use the same package RTD 4.0.0 HF01 in DS? - In DS when you configure the value of Clk2Cs, can you give me the range of this node (in DS) in this time? - In generated code, can you give me value of LPSPI_CCR_SCKPCS? Thank you, Nam. Re: Clk2Cs parameter on Tresor issue Hello @MVR, No need for a new thread. But this case is currently pending on the RTD team, and it might take some time before it is analyzed by them and even longer to update the SW if needed. Re: Clk2Cs parameter on Tresor issue Hello @danielmartynek  Should I open a new topic? Thank you. MVR Re: Clk2Cs parameter on Tresor issue Hi @MVR, It has been reported to the RTD development team. I will update the thread once I have some feedback. BR, Daniel Re: Clk2Cs parameter on Tresor issue Can someone help me, please? I closed the ticket but I found a new issue. Re: Clk2Cs parameter on Tresor issue Take a look the error: And this is the clock configured: Re: Clk2Cs parameter on Tresor issue Hello @danielmartynek  It makes sense. But I set the same configuration (clock and baudrate) that I set on RTD (.mex file) but I can't define the same range, do you know why? I'm trying to set 1.0E-5 in LPSPI_1, using 4.0E7 of clock (AIPS_SLOW_CLK) and 500000.0 of baudate. Why on S32DS tool it works but on Tresos it doesn't work? Thanks. Re: Clk2Cs parameter on Tresor issue I see now, I can reproduce it. The range that the tool reports depends on the selected clock and baudrate. So, if you change the baudrate, you should see that the range moves. The delay is configurable in the CCR register and it depends on TCR[PRESCALE]. Regards, Daniel Re: Clk2Cs parameter on Tresor issue I'm using 29 as well. That's strange... Re: Clk2Cs parameter on Tresor issue Hi @MVR, What EB Tresos version do you use? I can set 1.0E-4 in Tresos 29. I imported this example: ...\SW32K3_S32M27x_RTD_R21-11_4.0.0_HF01\eclipse\plugins\Spi_TS_T40D34M40I0R0\examples\EBT\S32K3XX\Spi_Transfer_S32K344 Regards, Daniel Re: Clk2Cs parameter on Tresor issue Some other notes: RTD configuration (here it works): I'm using this version of AUTOSAR MCAL:
View full article
s32k3 secure debug interface? Hi Nxp,     i've set S32K312  LC to OEM_PROD and secure debug is active.  i only got jlink now and have some question : 1. to open the secure debug,  is interface JTAG / SWD both available or ONLY JTAG? 2. is there any scripts for jlink to authurize secure debug?   Re: s32k3 secure debug interface? thanks, use pylink to implement CR auth works. Re: s32k3 secure debug interface? Hi @victory  1. To open secure debugging, are JTAG/SWD or JTAG ONLY interfaces available? Both JTAG and SWD interfaces are available. 2. Is there any script for jlink to enable secure debugging? I am afraid J-Link does not support secure debugging of applications with password authentication or with challenge/response authentication. BR, VaneB
View full article
S32k142中的默认启动模式和启动引脚 我正在研究S32k142 MCU。我希望启动模式是从Flash启动。 S32k14x MCU 中的默认启动模式是什么?而且我在引脚排列中没有找到任何启动引脚,启动模式配置是如何完成的? 谢谢, 杰万
View full article
尝试使用 EGL_image_external 进行渲染时出现 GPU 错误 在 iMX.8QuadMax 上运行,我正在尝试部署一个 Gstreamer 管道,该管道解码 HEVC 帧,然后将其传递给“glupload”,这是一个能够生成 EGL_image 支持的 GL 纹理的 Gstreamer 元素。 根据其调试和日志输出,glupload 在从 DMA 缓冲区创建 EGL 图像时似乎设置了正确的参数。 但是,当我尝试在 GLES 中渲染解码后的帧并从 EGL_image 支持的纹理中进行采样时,出现错误: [ 1] ES30: 验证过程中出现一些绘制错误并被跳过 此外,在从纹理中采样的过程中,偶尔会出现 SEGFAULT。调用堆栈是: #0 0x0000fffff5a48e68 在 ?? () 中来自 /usr/lib/libGAL.so #1 0x0000fffff59edcb4 在 gcoSURF_DisableTileStatus () 中来自 /usr/lib/libGAL.so #2 0x0000fffff5a036e8 在 gco3D_SetTarget () 中来自 /usr/lib/libGAL.so 我可以得到一些帮助来找出问题所在吗? 回复:尝试使用 EGL_image_external 进行渲染时出现 GPU 错误 我解决了这个问题。Gstreamer 插件使用它们自己的 GL 上下文而不是共享我的渲染上下文,因此我获得的纹理 ID 尽管在渲染上下文中是有效的纹理 ID,但实际上并不是相同的对象。因此,尝试将这些纹理采样为 EGLImage 外部支持纹理是错误的。 回复:尝试使用 EGL_image_external 进行渲染时出现 GPU 错误 我真的不认为这是一个内存空间限制。纹理为 200x200 RGBA。我正在播放的视频流中有 3 帧。总共只有 160KB。 我已阅读 Gstreamer 指南。它主要讨论使用 gst-launch 构建管道,但在这里没有帮助。 “验证过程中某些绘制出现错误并被跳过”是什么意思?我如何获得有关实际*错误*的更多详细信息? 我也尝试了 VIV_DEBUG=-MSG_LEVEL:WARNING,但没有打印任何新内容。
View full article