1954589_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1954589_en-US

1954589_en-US

s32k3 secure debug interface?

Hi Nxp,

    i've set S32K312  LC to OEM_PROD and secure debug is active.  i only got jlink now and have some question :

1. to open the secure debug,  is interface JTAG / SWD both available or ONLY JTAG?

2. is there any scripts for jlink to authurize secure debug?  

Re: s32k3 secure debug interface?thanks, use pylink to implement CR auth works.Re: s32k3 secure debug interface?

Hi @victory 

1. To open secure debugging, are JTAG/SWD or JTAG ONLY interfaces available? Both JTAG and SWD interfaces are available.

2. Is there any script for jlink to enable secure debugging? I am afraid J-Link does not support secure debugging of applications with password authentication or with challenge/response authentication.


BR, VaneB

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 08:45 PM
Updated by: