Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
S32DS3.5 GBK S32DS3.6.2UTF-8 使用 S32DS3.5 时、我使用的是 GBK 编码。但是,当我用 S32DS3.6.2 打开该文件时,却发现它并没有运行、我发现中文评论是乱码。结果发现 S32DS3.6.2 不支持 GBK 编码。问题来了:如何解决中文评论乱码的问题?为什么最新的 IDE 3.6.2不支持 GBK? Re: S32DS3.5 GBK S32DS3.6.2 UTF-8 你好、 能否请您提供一些受影响的文件以供测试?
記事全体を表示
Read mifare plus EV2 cards on ios Hello, good day. I am working on a project that uses MIFARE Plus EV2 cards in security level 3 for reading and writing operations. For Android, I have been able to successfully perform authentication and reading using the TapLinx library. However, for iOS, I have not been able to find if such a library exists. I see it mentioned in the documentation at development center, but I cannot locate it. Furthermore, I am unsure whether I can develop my own implementation using APDUs because, from what I understand, the CMAC calculation for this type of card  and security level is not publicly available. Code examples Example code Offline version Re: Read mifare plus EV2 cards on ios Hello @KennethBarrera Hope you are doing well. For iOS, you can refer to UG10045 Starting development with TapLinx iOS SDK, and TapLinx Software Development Kit (TLLIBSDK) that can be downloaded from TapLinx SDK > Downloads section. MIFARE Plus EV2 requires support for its native command set or ISO/IEC 7816-4 wrapping. As you mention, documentation about command set and structure is secured under NDA and must be requested through the Secure Files. Regards, Eduardo.
記事全体を表示
android want not create Android Directory Path Hi, everyone here. During Android porting, I am asking for the following reasons. os: android 13 cpu:imx8mini When you insert an SD card or USB memory on Android, the directory below is automatically created • Environment.DIRECTORY_ALARMS: Save audio file for alarm (/mnt/sdcard/Alarms) • Environment.DIRECTORY_DCIM : Save photos taken with camera (/mnt/sdcard/DCIM) • Environment.DIRECTORY_DOWNLOADS: Save the downloaded file (/mnt/sdcard/Download) • Environment.DIRECTORY_MUSIC : 음악 파일 저장 (/mnt/sdcard/Music) • Environment.DIRECTORY_MOVIES : 영상 파일 저장 (/mnt/sdcard/Movies) • Environment.DIRECTORY_NOTIFICATORS: Store audio files for use as notification sounds (/mnt/sdcard/Notifications) • Environment.DIRECTORY_PICTURES : 그림 파일 저장 (/mnt/sdcard/Pictures) • Environment.DIRECTORY_PODCASTS: save podcast file (/mnt/sdcard/Podcasts) Is there a way to prevent this directory from happening Re: android want not create Android Directory Path Hello, The directory is create by the android, is necessary but you can change with android studio, and change the permission and loaders. Regards
記事全体を表示
32.12 Recovery mode And Functional Reset Hi There, I read a lot of posts and about It. I can disable Reset by modify DCM-DCRWP1 or (more unsafe) trigger IPMC_RGM->FREC= 0xF before each functional reset. But I read  from RM 32.12 Recovery mode that also, for example "SBAF does not boot the application" or other cases listed causes the VTOR = 2040_0100 address. I notice in this case PC = 0x2040_012E and stack pointer SP= 0x2040_200 that are all wrong and they are in the middle of my sram Memory! and also PC loops on 0x2040_012e endless! I don't know if I need to fill any VT code on  2040_0100 but all is stucked ! HSE is skipped and sbaf loads directly my application code. can you help Me ? Best Regards  Fabio  Re: 32.12 Recovery mode And Functional Reset Hi @FabioG  This is called JTAG based recovery mode. You are not supposed to load own code to the RAM, the wfi and endless loop is written there by SBAF. The purpose of this recovery mode is to put the device to some defined state when user is allowed to attach a debugger and take appropriate actions (like re-program application, check the content of flash, change configuration or whatever). If you want to execute own code automatically in this situation, you can use HSE and its Secure Recovery Mode. See HSE firmware reference manual for details. Or something similar - if you want to execute specific code when your application is corrupted, see: https://community.nxp.com/t5/S32K/How-to-enable-the-rollback-function-of-Hse-AB-SWAP-on-S32K3/m-p/2146151/highlight/true#M51578 Regards, Lukas
記事全体を表示
android 无法创建 Android 目录路径 嗨,大家好。 在 Android 移植过程中,我出于以下原因提出请求。 操作系统:安卓 13 CPU:imx8mini 在安卓系统上插入 SD 卡或 USB 存储器时,会自动创建以下目录 - Environment.DIRECTORY_ALARMS:保存警报音频文件(/mnt/sdcard/Alarms) - Environment.DIRECTORY_DCIM:保存相机拍摄的照片(/mnt/sdcard/DCIM) - Environment.DIRECTORY_DOWNLOADS:保存下载的文件 (/mnt/sdcard/Download) - Environment.DIRECTORY_MUSIC : 音乐 (/mnt/sdcard/Music) - Environment.DIRECTORY_MOVIES : 영상 파일 저장 (/mnt/sdcard/Movies) - Environment.DIRECTORY_NOTIFICATORS:存储用作通知声音的音频文件 (/mnt/sdcard/Notifications) - Environment.DIRECTORY_PICTURES : 그림 파일 저장 (/mnt/sdcard/Pictures) - Environment.DIRECTORY_PODCASTS:保存播客文件 (/mnt/sdcard/Podcasts) 是否有办法防止该目录发生这种情况 Re: android want not create Android Directory Path 你好 目录由 android 创建,这是必要的,但您可以使用 android studio 进行更改,并更改权限和加载器。 此致
記事全体を表示
S32G3 SAF - eMCEM 反应超时周期 你好,团队、 我目前正在开发恩智浦的 S32G3 功能安全框架。在为 eMCEM 映射 NMI 故障时,我提出了一个与本地恢复超时周期有关的问题。 我正在开发 ASIL-C 汽车系统,其 FTTI 为 50 ms。 SAF 手册中提到的默认超时为NCF 恢复超时寄存器 = 65535 [48MHz IRC ticks] (1365 [us])。 在这种情况下,TImeout Period 应该是什么?需要根据哪些参数来决定?请提出建议并帮我确定超时时间。 提前感谢! Re: S32G3 SAF - eMCEM Reaction Timeout Period 你好@SHIVRAJ、 这只是个人建议,您需要在正确的条件下验证产品的性能。 考虑到少于 50 毫秒都是正确的,我将使用 2,000,000 ticks,即在 48MHz 时钟下,恢复超时略多于 41 毫秒。 请注意,这个值取决于您决定如何处理故障以及如何恢复故障。 如果这些信息有用,请告诉我。 Re: S32G3 SAF - eMCEM Reaction Timeout Period 你好@alejandro_e、 非常感谢你们的帮助。 是的,我们已经推出了特定产品的功能安全要求,例如FTTI、故障处理机制、操作模式、安全状态、最大电压和电流额定值等。 定义的 FTTI 为 50 毫秒,我们确定的 FHTI 小于 FTTI (<50 毫秒)。 期待您对超时时间的回复。 提前感谢! Re: S32G3 SAF - eMCEM Reaction Timeout Period 你好@SHIVRAJ、 感谢您联系我们,很抱歉这么晚才回复您。关于你的问题,我的专业领域不是功能安全话题,但我也许能帮助你。但首先我需要知道你的产品是否有功能安全要求,特别是非关键故障的恢复时间。 感谢您提供的信息
記事全体を表示
ECSPI_SCLK signal integrity Hi,  I'm using the i.MX8M mini. I measured the waveform of SCLK and MISO at the i.MX end.  The SCLK is output by i.MX as the master, but there are distortions such as glitches on the rising edge. When capturing data form MISO, does the i.MX8 use this SCLK waveform? Is my unerstanding correct that the internal circuit driving the data acquisition uses a clean singal that is isolated by buffers, and is not affected by external reflections? CH1 (Yellow) : SCLK CH2 (Blue): MISO Thanks, Re: ECSPI_SCLK signal integrity  Dear janxie, Thank you for your reply. I understand that we currently don't have the internal design diagram, so we cannot resolve my question at this time. Best Regards, Re: ECSPI_SCLK signal integrity refer to the RM, I only find this diagram, though I don't have internal design diagram, but the ecspi design can provide the clean signal to the SCLK,  if all of your boards get the jitter, should check the HW design or measurement tools, if only one or two boards have this issue, maybe you can do the AB test to confirm if this issue is related to the chip  Re: ECSPI_SCLK signal integrity Dear janxie, Thank you for your reply. I understand that ECSPI uses SCLK signal for Shift register. And SCLK wavefore is important for Slave device. I'd like to know the i.MX inside diagram. Figure 1. is  my understanding. Do you mean that Figure 2 is correct?       Thanks, Re: ECSPI_SCLK signal integrity 1)When capturing data form MISO, does the i.MX8 use this SCLK waveform? >yes, refer to the reference manual, The ECSPI master uses the Chip Select (SS) signal to enable an external SPI device, and  uses the SCLK signal to transfer data in and out of the Shift register. 2)Is my unerstanding correct that the internal circuit driving the data acquisition uses a clean singal that is isolated by buffers, and is not affected by external reflections? > the signal integrity issues present at the pin would be affected by external, so you need to double check your HW design
記事全体を表示
使用相同 ID 时无法收到确认 我们目前在设置中使用相同的 ID,但没有收到任何确认。我们已经验证了该ID的配置正确并按预期重复使用,但是响应/ACK 未通过。
記事全体を表示
32.12 リカバリモードと機能リセット こんにちは、 私はそれに関するたくさんの投稿を読みました。 DCM-DCRWP1 を変更するか、(より危険ですが) 各機能リセットの前に IPMC_RGM->FREC= 0xF をトリガーすることで、リセットを無効にすることができます。 しかし、RM 32.12 リカバリ モードから読み取ったところ、たとえば「SBAF がアプリケーションを起動しない」など、リストされている他のCASEでも、VTOR = 2040_0100 アドレスが発生することがわかりました。 このCASE、PC = 0x2040_012E とスタック ポインター SP= 0x2040_200 がすべて間違っており、SRAM メモリの中央にあることに気付きました。また、PC は 0x2040_012e で無限にループします。 2040_0100 に VT コードを入力する必要があるかどうかはわかりませんが、すべてが停止しています。 HSE はスキップされ、sbaf がアプリケーション コードを直接ロードします。 手伝ってもらえますか ? よろしくお願いします ファビオ Re: 32.12 Recovery mode And Functional Reset こんにちは@FabioG これは JTAG ベースのリカバリ モードと呼ばれます。独自のコードを RAM にロードすることは想定されていません。WFI と無限ループは SBAF によってそこに書き込まれます。このリカバリ モードの目的は、ユーザーがデバッガーを接続して適切なアクション (アプリケーションの再プログラム、フラッシュの内容の確認、構成の変更など) を実行できる場合に、デバイスを何らかの定義済みの状態にすることです。 このような状況で独自のコードを自動的に実行したい場合は、HSE とそのセキュア リカバリ モードをCAN。詳細については、HSE ファームウェア リファレンス マニュアルを参照してください。 または同様に、アプリケーションが破損したときに特定のコードを実行する場合は、以下を参照してください。 https://community.nxp.com/t5/S32K/S32K3 で Hse-AB-SWAP のロールバック機能を有効にする方法/mp/2146151/highlight/true#M51578 よろしくお願いいたします。 ルーカス
記事全体を表示
iOSでMifare Plus EV2カードを読み取る こんにちは、おはようございます。 私は、読み取りおよび書き込み操作にセキュリティ レベル 3 の MIFARE Plus EV2 カードを使用するプロジェクトに取り組んでいます。Android の場合、TapLinx ライブラリを使用して認証と読み取りを正常に実行できました。しかし、iOS の場合、そのようなライブラリが存在するかどうかはわかりませんでした。開発センターのドキュメントに記載されていますが、見つけることができません。 さらに、私の理解では、このタイプのカードとセキュリティ レベルの CMAC 計算は公開されていないため、APDU を使用して独自の実装を開発できるかどうかはわかりません。 コード・サンプル サンプル・コード オフライン版 Re: Read mifare plus EV2 cards on ios こんにちは@KennethBarrera あなたの調子が良いといいのですが。 iOS の場合は、 UG10045「TapLinx iOS SDK を使用した開発の開始」およびTapLinx SDK > ダウンロード セクションからダウンロードできる TapLinx ソフトウェア開発キット (TLLIBSDK) を参照できます。 MIFARE Plus EV2 には、ネイティブ コマンド セットまたは ISO/IEC 7816-4 ラッピングのサポートが必要です。ご指摘のとおり、コマンド セットと構造に関するドキュメントは NDA に基づいて保護されており、セキュア ファイルを通じてリクエストする必要があります。 よろしくお願いいたします。 エドゥアルド。
記事全体を表示
S32DS3.5 GBK S32DS3.6.2 UTF-8 When using S32DS3.5, I used the GBK encoding. However, when I opened the file with S32DS3.6.2, I found that the Chinese comments were garbled. It turned out that S32DS3.6.2 does not support GBK encoding. So here comes the problem: how should I solve the issue of garbled Chinese comments? And why does the latest IDE 3.6.2 not support GBK? Re: S32DS3.5 GBK S32DS3.6.2 UTF-8 Hi,  can you please share some affected file for testing? 
記事全体を表示
S32K3 MBDT Simulink 外部模式 ADC 配置 我正在尝试使用 Simulink 上的 S32K3 MBDT 工具箱配置 ADC。 请推荐基于 PWM 触发信号进行配置的最简单方法,并能够使用外部模式在 Simulink 范围内查看结果。 MBDT 工具箱库中的示例使用外部 Freemaster 进行显示。此外,它们似乎使用多个缓冲区和配置块来启用 freemaster。 我希望了解配置 ADC 块的基本工作流程,以减少与外部环境的交互。 Re: S32K3 MBDT Simulink External Mode ADC configuration 你好,@shashwats、 感谢您对 S32K3 基于模型的设计工具箱的关注。 我强烈推荐这篇文章 (使用 ADC 和 PWM 控制 LED 强度) 是关于 ADC 和 PWM 配置的绝佳介绍。它通过清晰的解释、详细的视觉效果和实用的指导,一步步引导您完成整个过程,是设置基本 ADC 配置的完美起点。 欢迎浏览 MRCANHUB 系列中的其他文章--它们提供了关于外设配置的全面概述,可以拓宽您对该主题的理解: - 与 MR-CANHUBK344 上的数字输入/输出互动 - 通过 UART 发送数据并使用 FreeMASTER 监控信号 -通过 CAN 总线通信 与我们联系您的进度, 顺祝商祺! 德拉古
記事全体を表示
求新产品SPC5675KFK0MMS2R与替代原产品SPC5675KFF0VMS2R的参数区别 老产品SPC5675KFF0VMS2R已经停产,官网提供的信替代型号SPC5675KFK0MMS2R与原产品的具体区别,还求提供说明,谢谢 Re: 求新产品SPC5675KFK0MMS2R与替代原产品SPC5675KFF0VMS2R的参数区别 你好 旧版 SPC5675KFF0VMS2R 已停产。我希望能详细解释一下替换型号 SPC5675KFK0MMS2R 与原始型号之间的区别,如官方网站所提供的那样。谢谢。 我想知道新的 SPC5675KFK0MMS2R 和原来的 SPC5675KFF0VMS2R 在参数上有什么不同。 区别如下: K0 与 F0-出厂时不同但设备切割效果相同(修订版) M vs V - 不同温度范围 您可以在第 9 版数据表中找到这些信息。 顺祝商祺! Peter
記事全体を表示
MIMXRT1024 and ERR011164 - ADC_ETC with DMA Hello, is the workaround for ERR011164 usable when using more than 1 trigger chain? How to tell which DMA request to clear in DMA_CTRL of ADC_ETC? Is there any other way to use ADC and ADC_ETC with DMA? I tried to use PIT + ADC_ETC and read ADC results of ADC1 and ADC2 with DMA based on ADC DMA requests. It looks like ADC_ETC is clearing the DMA requests of ADC when it clears the COCO bits. This causes some ADC results to be lost when there are ADC1 and ADC2 conversions completed at a same time. One DMA is performed, but other DMA request is lost. I have ADC1 and ADC2 synced together by ADC_ETC triggers 0 and 4 to achieve sampling of voltage and current based on PIT. Any way to solve this? i.MXRT 102x Re: MIMXRT1024 and ERR011164 - ADC_ETC with DMA Hi, As the above answer, if you encounter this issue, refer to the workable solution. And, NXP cannot provide an SDK or proposed solution as the mentioned Errata . Here is a similar case for reference. Re: MIMXRT1024 and ERR011164 - ADC_ETC with DMA I think this doesn't really answer the question: Is the workaround for ERR011164 usable when using more than 1 trigger chain? If yes, then how? How to tell which DMA request to clear in DMA_CTRL of ADC_ETC? Re: MIMXRT1024 and ERR011164 - ADC_ETC with DMA Hi, Yes, this Errata of RT1024CE shows this ERR as the following. ERR011164 ADC: ADC_ETC fails to clear the ADC_ETC request signals  automatically after receiving DMA ack. Description: If enable ADC_ETC to trigger DMA transfer, the DMA transfer data send ack out. It does not clear the request signals automatically and continue to trigger DMA. Projected Impact: This issue can lead to DMA failure when working with ADC_ETC. Workarounds: Configuring two DMA channels for ADC_ETC data transfer. The first DMA channel with low priority triggered by ADC_ETC request is to transfer ADC_ETC data. The second DMA channel with high priority links to the first channel is to clear request of ADC_ETC by writing DMA_CTRL register. Both channel’s priority need to be higher than any channel used by other peripherals. This solution is result in DMA to transfer ADC_ETC data twice for one request signal and application need handle the redundant data properly. Proposed Solution: No fix scheduled Software Status: Software workaround is not in SDK.
記事全体を表示
新製品 SPC5675KFK0MMS2R と代替製品 SPC5675KFF0VMS2R のパラメータの違いを教えてください。 旧製品SPC5675KFF0VMS2Rは販売終了となりました。代替製品SPC5675KFK0MMS2R(公式サイトに掲載)と旧製品の違いについて教えていただけますか?よろしくお願いいたします。 Re: 求新产品SPC5675KFK0MMS2R与替代原产品SPC5675KFF0VMS2R的参数区别 こんにちは、 古いSPC5675KFF0VMS2Rは製造中止になりました。公式サイトに記載されている交換モデル SPC5675KFK0MMS2R と元のモデルの違いについて詳しく説明していただければ幸いです。ありがとう。 新しい SPC5675KFK0MMS2R とオリジナルの SPC5675KFF0VMS2R のパラメータの違いを知りたいです。 違いは次のとおりです。 K0 vs F0 - 工場は異なるが同じデバイスカット(リビジョン) M vs V - 異なる温度範囲 これらの情報はデータシート rev 9 に記載されています。 よろしくお願いいたします。 ピーター
記事全体を表示
ECSPI_SCLK 信号完整性 你好、 我使用的是 i.MX8M mini。 我测量了 i.MX 端 SCLK 和 MISO 的波形。 SCLK由i.MX作为主输出,但上升沿存在诸如故障之类的失真。 从 MISO 捕获数据时,i.MX8 是否使用这个 SCLK 波形? 我的理解是否正确,即驱动数据采集的内部电路使用的是通过缓冲器隔离的干净单声道,不会受到外部反射的影响? CH1(黄色) :SCLK CH2(蓝色):MISO 谢谢! Re: ECSPI_SCLK signal integrity 亲爱的 janxie, 感谢您的回复。 据我所知,我们目前还没有内部设计图,所以暂时无法解决我的问题。 致以最崇高的敬意 Re: ECSPI_SCLK signal integrity 参考 RM,我只能找到这个图表,尽管我没有内部设计图,但是 ecspi 的设计可以向 SCLK 提供干净的信号,如果你的所有板都出现抖动,应该检查硬件设计或测量工具,如果只有一两块板有这个问题,也许你可以做 AB 测试来确认这个问题是否与芯片有关 Re: ECSPI_SCLK signal integrity 亲爱的 janxie、 谢谢您的答复。 我知道ECSPI使用SCLK信号作为移位寄存器。 而且 SCLK 波峰对从机设备很重要。 我想知道 i.MX 内部图。 图 1.这是我的理解。 你是说图 2 正确吗? 的影响 影响 谢谢、 Re: ECSPI_SCLK signal integrity 1) 从 MISO 捕获数据时,i.MX8 是否使用这个 SCLK 波形? > 是的,参考参考手册,ECSPI主站使用芯片选择(SS)信号来启用外部SPI设备,并使用SCLK信号将数据传入和传出移位寄存器。 2)我的理解是否正确,即驱动数据采集的内部电路使用的是通过缓冲器隔离的纯净信号,不会受到外部反射的影响? > 引脚上存在的信号完整性问题会受到外部影响,因此您需要仔细检查您的硬件设计
記事全体を表示
MIMXRT1024 和 ERR011164 - 带 DMA 的 ADC_ETC 你好,使用 1 个以上的触发链时,ERR011164 的解决方法是否可用?如何确定要清除 ADC_ETC 的 DMA_CTRL 中的哪个 DMA 请求? 是否有其他方法将 ADC 和 ADC_ETC 与 DMA 结合使用? 我尝试使用 PIT + ADC_ETC,并根据 ADC DMA 请求通过 DMA 读取 ADC1 和 ADC2 的 ADC 结果。看起来 ADC_ETC 在清除 COCO 位时,正在清除 ADC 的 DMA 请求。当 ADC1 和 ADC2 转换同时完成时,这会导致一些 ADC 结果丢失。执行了一个 DMA,但丢失了其他 DMA 请求。 我通过 ADC_ETC 触发信号 0 和 4 将 ADC1 和 ADC2 同步在一起,以实现基于 PIT 的电压和电流采样。 有办法解决这个问题吗? i.MX RT102x Re: MIMXRT1024 and ERR011164 - ADC_ETC with DMA 您好, 如上所述,如果您遇到这个问题,请参考可行的解决方案。而且,恩智浦无法提供 SDK 或上述勘误表中建议的解决方案。 这是一个类似的案例供参考。 Re: MIMXRT1024 and ERR011164 - ADC_ETC with DMA 我认为这并不能真正回答问题: 使用 1 个以上的触发信号链时,ERR011164 的解决方法是否可用?如果是,那怎么办? 如何在 ADC_ETC 的 DMA_CTRL 中分辨出要清除哪个 DMA 请求? Re: MIMXRT1024 and ERR011164 - ADC_ETC with DMA 您好, 是的,RT1024CE 的勘误表显示该 ERR 如下。 ERR011164 ADC: ADC_ETC fails to clear ADC_ETC 请求信号 automatically 在收到 DMA ack 后。 描述 : 如果启用 ADC_ETC 来触发 DMA 传输,则 DMA 传输的数据会发回去。它不会自动清除请求信号并继续触发 DMA 触发信号 。 预计影响: 使用 ADC_ETC 时,此问题可能导致 DMA 故障。 变通办法 : 为 ADC_ETC 数据传输配置两个 DMA 通道。由 ADC_ETC low 请求触发信号的第一个 优先级为 的 DMA 通道是传输 ADC_ETC 数据。 第二个 high priority 带有指向第一个频道的 链接的 DMA 频道是通过写入 DMA_CTRL 寄存器来清除 ADC_ETC 的请求 。两个通道的优先级都必须高于其他 外设使用的任何信道。 该解决方案导致 DMA 为一个请求信号传输两次 ADC_ETC 数据,应用程序需要正确处理 冗余数据。 建议的解决方案:未计划修复 软件状态:软件解决方法不在 SDK 中。
記事全体を表示
S32G3 SAF - eMCEM 反応タイムアウト期間 こんにちは、チームの皆さん 現在、NXP の S32G3 向けセーフティ Framework に取り組んでいます。eMCEM の NMI 障害をマッピングしているときに、ローカル リカバリのタイムアウト期間に関するクエリがありました。 私は FTTI が 50 ミリ秒の ASIL-C オートモーティブシステムに取り組んでいます。 SAF マニュアルに記載されているデフォルトのタイムアウトは次のとおりです: NCF リカバリ タイムアウト レジスタ = 65535 [48MHz IRC ティック] (1365 [us])。 こののタイムアウト期間はどのくらいにすべきでしょうか?どのようなパラメータに基づいて決定する必要がありますか?タイムアウト期間の決定についてご提案とご協力をお願いします。 よろしくお願いいたします! Re: S32G3 SAF - eMCEM Reaction Timeout Period こんにちは@SHIVRAJ 、 これはあくまで個人的な推奨事項であり、正しい条件下で製品のパフォーマンスを検証する必要があります。 50 ミリ秒未満であれば正しいと考えると、2,000,000 ティックを使用します。これは、48 MHz クロックの場合、回復タイムアウトに 41 ミリ秒強になります。 この値は、障害をどのように処理し、どのように回復するかによって異なることに注意してください。 この情報が役に立ったかどうかお知らせください。 Re: S32G3 SAF - eMCEM Reaction Timeout Period こんにちは@alejandro_e 、 この件に関してご協力いただき、誠にありがとうございます。 はい、FTTI、障害処理メカニズム、動作モード、セーフティ状態、最大電圧および電流定格などの製品固有のセーフティ要件はすでに導出されています。 定義された FTTI は 50 ミリ秒であり、私たちが決定した FHTI は FTTI 未満 (<50 ミリ秒) です。 タイムアウト期間に関するご返答をお待ちしております。 よろしくお願いいたします! Re: S32G3 SAF - eMCEM Reaction Timeout Period こんにちは@SHIVRAJ 、 お問い合わせいただきありがとうございます。返信が遅くなり申し訳ございません。あなたの質問について、私の専門分野はセーフティトピックではありませんが、お役に立てるかもしれません。しかし、まず、製品にセーフティ要件、特に重大でない障害の回復時間に関する要件があるかどうかを知る必要があります。 情報ありがとうございます
記事全体を表示
S32K3 MBDT Simulink外部モードADC構成 Simulink 上の S32K3 MBDT ツールボックスを使用して ADC を構成しようとしています。 PWM トリガーに基づいてこれを設定し、外部モードを使用して Simulink スコープで結果を表示できるようにする最も簡単な方法を提案してください。 MBDT ツールボックス ライブラリに含まれる例では、表示に外部の Freemaster を使用します。また、フリーマスターを有効にするために複数のバッファや構成ブロックを使用しているようです。 外部環境との相互作用を最小限に抑えて ADC ブロックを構成するための基本的なワークフローを理解したいと思います。 Re: S32K3 MBDT Simulink External Mode ADC configuration こんにちは、 @shashwats さん、 S32K3 向けモデルベース デザイン ツールボックスにご興味をお持ちいただきありがとうございます。 ADC と PWM の構成に関する優れた入門書として、この記事 ( ADC と PWM による LED 輝度の制御) を強くお勧めします。わかりやすい説明、詳細なビジュアル、実用的なガイダンスを使用して、プロセスを段階的に説明します。基本的な ADC 構成をセットアップするための出発点として最適です。 MRCANHUB シリーズの他の記事もぜひご覧ください。ペリフェラルの構成に関する優れた概要が提供されており、トピックの理解を深めることができます。 - MR-CANHUBK344のデジタル入力/出力の操作 - UART経由でデータを送信し、FreeMASTERで信号を監視 - CANバスを介した通信 進捗状況をお知らせください。 よろしくお願いいたします。 ドラゴス
記事全体を表示
在 i.MX95 中从 CA55 启动 我想知道如果不可能的话,是否可以在 i.MX95 中将 A55 而不是 M33 配置为启动核心,需要做什么解决方法 Re: Booting from CA55 in i.MX95 i.MX95 还在试生产阶段,我已经查过了: 默认情况下,不支持直接从 Cortex-A55 (CA55) 启动。 在i.MX95架构中,Cortex-M33被设计为默认的启动内核。Cortex-M33 ROM 执行硬件初始化,并从由引导模式引脚或熔丝选择的主引导设备加载映像。
記事全体を表示