Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
mcxn947 加密区域可以指定范围么,程序内部如何访问flash加密区 Can encryption and signing be applied to a specified range of flash space? How does the program's own read/write behavior within the encrypted flash region differ from before (is the data read back ciphertext? is the data written plaintext?)? During OTA upgrades, how can the architecture be made to match the chip's encryption/decryption without conflicts? Re: mcxn947 加密区域可以指定范围么,程序内部如何访问flash加密区 Hello, To be clear first: once encryption is enabled, when a program running on the chip writes to flash, the data it writes is plaintext, but what is ultimately stored in flash is ciphertext; when the ciphertext in flash is read by a program running on the chip, it comes out as plaintext. Correct Based on above viewpoint : Then, the SB file read by your Secure Provisioning software is ciphertext, and what is sent over serial ISP to the chip’s factory ISP ROM bootloader must also be ciphertext (otherwise there would be a logical flaw). The factory ISP ROM bootloader decrypts the ciphertext received over serial into plaintext, and then writes the plaintext data into flash, but ultimately the data stored in flash is encrypted again, becoming ciphertext. In other words, during ISP programming, the factory ISP ROM bootloader first decrypts and then encrypts, going through a decrypt-then-encrypt round trip. Let me put more light into this: yes SB file is encrypted and must be decrypted by ROM before writing to Flash. But SB file is encrypted completely independently, to protect the firmware between the OEM and manufacturing facility. Programming flash, either internal or external, is different story and either is not used at all or is used with different algorithm, initial vector, etc. Regards, Libor Re: mcxn947 加密区域可以指定范围么,程序内部如何访问flash加密区 To be clear first: once encryption is enabled, when a program running on the chip writes to flash, the data it writes is plaintext, but what is ultimately stored in flash is ciphertext; when the ciphertext in flash is read by a program running on the chip, it comes out as plaintext.   Based on above  viewpoint : Then, the SB file read by your Secure Provisioning software is ciphertext, and what is sent over serial ISP to the chip’s factory ISP ROM bootloader must also be ciphertext (otherwise there would be a logical flaw). The factory ISP ROM bootloader decrypts the ciphertext received over serial into plaintext, and then writes the plaintext data into flash, but ultimately the data stored in flash is encrypted again, becoming ciphertext. In other words, during ISP programming, the factory ISP ROM bootloader first decrypts and then encrypts, going through a decrypt-then-encrypt round trip.                           Re: mcxn947 加密区域可以指定范围么,程序内部如何访问flash加密区 Hi, For MCXN devices: Can encryption and signing be applied to a specified range of flash space? SEC tool: - signs whole application - encryption region is configured once in the product lifetime, you need to make a reserve for future updates (increased size of app) How does the program's own read/write behavior within the encrypted flash region differ from before (is the data read back ciphertext? is the data written plaintext?)? Encryption/decryption is on-the-fly. App reading from flash does not need to care, it is transparent. About writing to encrypted flash region from the application itself, you need to investigate, I'm not sure if there are any caveats. During OTA upgrades, how can the architecture be made to match the chip's encryption/decryption without conflicts? As mentioned above, you need to specify reasonable size of memory region for encryption. If you application exceeds the encrypted region, OTA will work, only the part of the app that will be outside of encrypted area will still work, only your IP won't be protected by the encryption. Regards, Libor
記事全体を表示
Re: S32G274A LLCE CAN 当前自研板运行在多核模式下,1个A53核是用来和其他设备网络通信任务的,还有几个A53跑的是一些总线通信的驱动,每个类型的总线单独使用一个A53核。现在出现了一个问题是当前给LLCE CAN配置的恢复操作是设置LLCE CAN的模式先stop再start,在实际运行的场景大部分可以恢复通信的,但是有的时候会频繁的执行总线恢复以至于到影响其他的A53正常运行(网络通信任务中断)。想问的是LLCE CAN有那些方法可以总线恢复,还有是为什么LLCE CAN已经单独放置一个核运行还会影响到其他的核。以下是版本信息:S32G_LLCE_1_0_9;SW32G_RTD_4.4_4.0.2_P04_D2312 Re: S32G274A LLCE CAN Hello, @JACK_Q  您好 麻烦您详细介绍一下您的软硬件测试环境: 1. 在您的系统中,是M核和A核端同时使用吗?M7核运行什么任务?基于哪些软件包? 2. A53端从您的描述来看,每个核都有自己的任务,请问是运行的什么软件?是否是Linux BSP? BR Chenyin
記事全体を表示
Falconモードでセキュアブートを有効にする(カーネルバージョン6.12.49)|| iMX8MP_EVK チームの皆さん、こんにちは。 Falcon ModeでSecure Boot を有効にするのを手伝ってもらえます か? meta-imx-fastboot GitHubリポジトリ の助けを借りて、Falcon Modeの実現に成功しました 。しかし、meta-imx-fastbootの実装では 、Falcon Modeのブートフロー中に 意図的に OP-TEE が削除されていることがわかりました。 OP-TEEも私のユースケースに必要なので、NXPフォーラムで質問をしました。@elena_popa OP-TEEを保持・有効化するソリューションを提供してくれました。参考のためにフォーラム のリンク を添付しました。 現在、Secure Bootを有効にする際に問題に直面しています 現在のカーネルバージョンでファルコンモード付きのセキュアブートに関するドキュメントが見つからなかったためです。 環境詳細: ボード: i.MX8M Plus EVK(i.MX8MP EVK) カーネルバージョン: 6.12.49 Yocto Environment: Yocto拠点のNXP BSP ブートモード:ファルコンモード 要件:ファルコンモード + OP-TEE + セキュアブート Yocto Project Re: Enable Secure Boot in Falcon Mode (6.12.49 - Kernel Version) || iMX8MP_EVK こんにちは、 どのエラーが出ているのか教えていただけますか? よろしくお願いいたします。
記事全体を表示
mcxn947加密区域可以指定范围,程序内部如何访问flash加密区域 能否对指定范围的闪存空间进行加密和签名? 程序在加密闪存区域内的读/写行为与之前有何不同(读取回的数据是密文吗?写入的数据是明文吗?)? 在 OTA 升级过程中,如何使架构与芯片的加密/解密相匹配而不发生冲突? Re: mcxn947 加密区域可以指定范围么,程序内部如何访问flash加密区 你好, 首先要明确一点:一旦启用加密,当芯片上运行的程序向闪存写入数据时,写入的数据是明文,但最终存储在闪存中的是密文;当芯片上运行的程序读取闪存中的密文时,读取出来的却是明文。 正常 基于以上观点: 然后,您的安全配置软件读取的 SB 文件是密文,通过串行 ISP 发送到芯片的工厂 ISP ROM 引导加载程序的内容也必须是密文(否则就会出现逻辑缺陷)。工厂 ISP ROM 引导加载程序将通过串口接收的密文解密为明文,然后将明文数据写入闪存,但最终存储在闪存中的数据又会被加密,变成密文。 换句话说,在 ISP 编程期间,工厂 ISP ROM 引导加载程序首先进行解密,然后再进行加密,经历一个解密再加密的往返过程。 让我再详细解释一下: 是的,SB 文件已加密,必须先由 ROM 解密才能写入 Flash。但SB文件是完全独立加密的,以保护OEM厂商和制造工厂之间的固件安全。 对闪存(无论是内部闪存还是外部闪存)进行编程是另一回事,要么根本不使用闪存,要么使用不同的算法、初始向量等。 此致, 伦敦银行间同业拆借利率 (Libor) Re: mcxn947 加密区域可以指定范围么,程序内部如何访问flash加密区 首先要明确一点:一旦启用加密,当芯片上运行的程序向闪存写入数据时,写入的数据是明文,但最终存储在闪存中的是密文;当芯片上运行的程序读取闪存中的密文时,读取出来的却是明文。   基于以上观点: 然后,您的安全配置软件读取的 SB 文件是密文,通过串行 ISP 发送到芯片的工厂 ISP ROM 引导加载程序的内容也必须是密文(否则就会出现逻辑缺陷)。工厂 ISP ROM 引导加载程序将通过串口接收的密文解密为明文,然后将明文数据写入闪存,但最终存储在闪存中的数据又会被加密,变成密文。 换句话说,在 ISP 编程期间,工厂 ISP ROM 引导加载程序首先进行解密,然后再进行加密,经历一个解密再加密的往返过程。                           Re: mcxn947 加密区域可以指定范围么,程序内部如何访问flash加密区 您好, 对于 MCXN 设备: 能否对指定范围的闪存空间进行加密和签名? 高效密码学标准\(SEC\)工具: - 签署整个申请 - 加密区域在产品生命周期内只需配置一次,您需要预留空间以备将来更新(应用程序体积增大)之需。 程序在加密闪存区域内的读/写行为与之前有何不同(读取回的数据是密文吗?写入的数据是明文吗?)? 加密/解密是即时进行的。应用程序从闪存读取数据无需关心,它是透明的。关于从应用程序本身写入加密闪存区域的问题,你需要进行调查,我不确定是否存在任何注意事项。 在 OTA 升级过程中,如何使架构与芯片的加密/解密相匹配而不发生冲突? 如上所述,您需要指定合理大小的加密内存区域。如果您的应用程序超出加密区域,OTA 更新仍可运行,但只有应用程序超出加密区域的部分仍可运行,您的 IP 地址将不再受加密保护。 此致, 伦敦银行间同业拆借利率 (Libor)
記事全体を表示
S32K1_S32M24X 和 S32K1 RTD 封装有什么区别? 我正在为S32K116进行开发。 我在检查 S32DS 扩展和更新时注意到,我安装了两个 S32K1 软件包: “S32K1_S32M24X 实时驱动程序 AUTOSAR R21-11 版本 3.0.0”QLP06” 和 S32K1 实时驱动程序 AUTOSAR R21-11 版本 3.0.0QLP06“ 两者之间有什么区别? 如果他们也对我的情况这样做,我应该保留哪个/卸载哪个? 我尝试移除其中一个(S32K1),但之后我的项目就无法加载它们的 .mex 文件了。文件不再存在。 Re: Difference between S32K1_S32M24X and S32K1 RTD packages? 嗨@daniel_meier 虽然这些软件包看起来可能很相似,但它们彼此之间以及与 S32DS 之间存在依赖关系,因此不应被视为可以彼此独立使用的独立组件。 因此,我们建议重新安装该软件包,并保持两个软件包都已安装,以确保项目功能正常。 BR,VaneB
記事全体を表示
FreeMaster Lite NODE Redに新しいノードを統合することは不可能です 親愛なるみんな FreeMaster Liteを使用してNode-REDにウィジェットを統合したいと考えています。NXPのトレーニング終了後 FreeMASTER Lite 1.1 + Node-RED統合 https://www.nxp.com/design/design-center/training/TIP-FREEMASTER-LITE-NODE-RED (@ minute 0:40)ウィジェットは設定 -> 管理パレットにアクセスすることで追加されるべきであることが示されています。しかし、最新のFreeMaster LiteインストールにはPalett管理オプションがなく、NXPのサイトからダウンロードしたばかりです どんなサポートでも感謝します パオロ Re: Impossible to integrare new node in FreeMaster Lite NODE Red こんにちは、@pberna67 さん。 FreeMASTER Lite バージョン1.5.1を使用しているか確認していただけますか: 2.png2.png2.png また、Node-REDのバージョンは4.0.9です。 1.png1.png1.png クリーンインストールをして「パレット管理」オプションにアクセスできました。 ちょっと確認しますが、ユーザーフォルダから「.node_red」フォルダを削除(または名前変更)して、古いNode-REDの設定が最新のインストールに干渉していないか確認してみてはどうでしょうか。 それでも解決しない場合は、追加の詳細を教えてもらえますか: FreeMASTER Liteは、スタンドアロンインストーラーから実行していますか、それともFreeMASTER 3.2本体に同梱されているインストーラーから実行していますか? お使いのホストOSは何ですか? 外部にNode-REDをインストールしていますか? 敬具、 イウリアン Re: Impossible to integrare new node in FreeMaster Lite NODE Red 親愛なるイウリアン 迅速なご回答ありがとうございます! 私が使用しているFreeMASTERは、FreeMASTER Liteバージョン1.5.1であることを確認します。 pberna67_0-1790026466167.pngpberna67_0-1790026466167.png Node-REDのバージョンは4.09です。 pberna67_1-1790026600039.pngpberna67_1-1790026600039.png FreeMASTER Liteは、スタンドアロンインストーラーから実行していますか、それともFreeMASTER 3.2本体に同梱されているインストーラーから実行していますか? インストールしたパッケージは以下の通りです: pberna67_2-1790027196038.pngpberna67_2-1790027196038.png それ以前にFreeMASTERパッケージは一切インストールされていませんでした。 お使いのホストOSは何ですか? まだWindows 10です 外部にNode-REDをインストールしていますか? いいえ、していません よろしくお願いします。 パオロ Re: Impossible to integrare new node in FreeMaster Lite NODE Red こんにちは、@pberna67 さん。 Node-REDのドキュメントを確認しましたが、NPMがインストールされていない場合に起こる動作のようです。パレット管理機能は、依存関係のダウンロードとインストールにNPMツールを使用しています。 NPMは別途インストールする必要があります。Node-REDコミュニティにはこのトピックについて詳しく説明しているスレッドがあります: https://discourse.nodered.org/t/why-isn't-manage-palette-showing-up/27219/9 お役に立てば幸いです。 イウリアン Re: Impossible to integrare new node in FreeMaster Lite NODE Red 親愛なるイウリアン どこにもnpmプログラムがインストールされているのが見当たりません。node-redパッケージもインストールする必要がありますか?それともすべてインストールすればいいのですが、 ? Node-REDの一部は動作するのに、一部は動作しないというのは奇妙です。あなたが示したスレッドには、追加コンポーネントNPMのインストール方法が示されていません。他に何かアイデアはありますか? 宣言されています: https://www.nxp.com/design/design-center/software/development-software/freemaster-run-time-debugging-tool:FREEMASTER FreeMasterはグラフィカルユーザーインターフェース(GUI)ガイド 設計ツールとの連携機能を備えています。FreeMasterのGUIビルダーに関する事例や、その他の統合に関する詳細情報はありますか? よろしくお願いいたします パオロ
記事全体を表示
无法在 FreeMaster Lite NODE Red 中集成新节点 各位 我想使用 FreeMaster Lite 将小部件集成到 NodeRed 中。参加完 NXP 名为“ FreeMASTER Lite 1.1 + Node-RED 集成 https://www.nxp.com/design/design-center/training/TIP-FREEMASTER-LITE-NODE-RED (@ 分钟 0:40)应通过访问“设置”->“管理调色板”来添加该小部件。但是,从 NXP 网站下载的最新版 FreeMaster Lite 中并没有“管理调色板”选项。 感谢大家的支持 Paolo Re: Impossible to integrare new node in FreeMaster Lite NODE Red 嗨@pberna67 , 请确认您运行的是 FreeMASTER Lite 1.5.1 版本: 2.png2.png2.png Node-RED 版本为 4.0.9: 1.png1.png1.png 我进行了全新安装,并且可以访问“管理调色板”选项。 快速检查一下——您可以尝试从用户文件夹中删除(或重命名)`.node_red`文件夹,以确保任何旧的Node-RED设置不会干扰最新的安装。 如果以上信息仍无法解答您的问题,能否提供更多详细信息? 您是通过独立安装程序运行 FreeMASTER Lite,还是通过与主 FreeMASTER 3.2 捆绑的安装程序运行 FreeMASTER Lite? 你的主机操作系统是什么? 你们是否有任何外部 Node-RED 安装? 亲切的问候, 尤利安 Re: Impossible to integrare new node in FreeMaster Lite NODE Red 亲爱的尤利安 谢谢你的快速回复! 我确认我运行的 FreeMASTER 版本是 FreeMASTER Lite 1.5.1: pberna67_0-1790026466167.pngpberna67_0-1790026466167.png Node-RED 版本为 4.09 pberna67_1-1790026600039.pngpberna67_1-1790026600039.png 您是通过独立安装程序运行 FreeMASTER Lite,还是通过与主 FreeMASTER 3.2 捆绑的安装程序运行 FreeMASTER Lite ? 我只安装了以下软件包: pberna67_2-1790027196038.pngpberna67_2-1790027196038.png 之前没有安装过 FreeMASTER 软件包。 你的主机操作系统是什么? 仍然是 Windows 10 你们是否有任何外部 Node-RED 安装? 不,我没有。 谢谢! Paolo Re: Impossible to integrare new node in FreeMaster Lite NODE Red 嗨@pberna67 , 我查阅了Node-RED的文档,如果系统上没有安装NPM,这似乎是预期行为。管理调色板功能依赖于 NPM 工具进行依赖项的下载和安装。 NPM 需要单独安装。Node-RED 社区里有一个帖子更详细地解释了这个问题: https://discourse.nodered.org/t/why-isnt-manage-palette-showing-up/27219/9 希望对您有所帮助。 尤利安 Re: Impossible to integrare new node in FreeMaster Lite NODE Red 亲爱的尤利安 我没有看到任何地方安装了 npm 程序。我还需要安装 node-red 包吗?还是所有东西都应该由其他程序自动安装? ? 奇怪的是,Node-RED 的一部分可以正常工作,但另一部分却不行。您提到的帖子中没有说明如何安装额外的元器件 NPM。还有其他想法吗? 声明如下: https://www.nxp.com/design/design-center/software/development-software/freemaster-run-time-debugging-tool:FREEMASTER FreeMaster 与图形用户界面 (GUI) 导星器设计工具集成。您是否有关于FreeMaster中GUI构建器集成的示例或更多细节? 问候 保罗
記事全体を表示
Re: S32G274A LLCE CAN The current self-developed board runs in multi-core mode. One A53 core is used for network communication tasks with other devices, and several other A53 cores run bus communication drivers, with each type of bus using a separate A53 core. A problem has arisen: the current LLCE CAN recovery operation is configured to stop and then start the LLCE CAN mode. In most actual scenarios, communication can be restored, but sometimes bus recovery is executed frequently, affecting the normal operation of other A53 cores (network communication tasks are interrupted). The questions are: what methods are available for LLCE CAN bus recovery, and why does having LLCE CAN running on a separate core still affect other cores? The version information is: S32G_LLCE_1_0_9; SW32G_RTD_4.4_4.0.2_P04_D2312 Re: S32G274A LLCE CAN Hello, @JACK_Q Hello Could you please provide a detailed description of your software and hardware testing environment? 1. In your system, are the M-core and A-core used simultaneously? What tasks does the M7 core run? Which software packages does it rely on? 2. From your description, each core on the A53 side has its own task. What software is it running? Is it a Linux BSP? BR Chenyin
記事全体を表示
S32K1_S32M24XとS32K1のRTDパッケージの違いは何ですか? 私はS32K116向けに開発を行っています。 S32DS拡張機能とdUpdatesを使っているときに、2つのS32K1パッケージがインストールされていることに気づきました: 「S32K1_S32M24X リアルタイム・ドライバ AUTOSAR R21-11 バージョン 3.0.0QLP06" および 「S32K1 リアルタイム・ドライバ AUTOSAR R21-11 バージョン 3.0.0」QLP06" この2つの違いは何ですか? もし私のケースでも同じように対応するなら、どちらを残しておくべきか、アンインストールすべきでしょうか? そのうちの1つ(S32K1)を削除してみましたが、そうするとプロジェクトが.mexファイルを読み込めなくなってしまいました。もうファイルはありません。 Re: Difference between S32K1_S32M24X and S32K1 RTD packages? こんにちは、 @daniel_meier さん。 パッケージは似ているように見えますが、互いに依存関係があり、互いに独立して使用できる独立したコンポーネントとして扱うことを意図していません。 したがって、プロジェクトの適切な機能を確保するために、パッケージを再インストールし、両方のパッケージを同時にインストールしておくことをお勧めします。 BR、VaneB
記事全体を表示
Impossible to integrare new node in FreeMaster Lite NODE Red Dear All I would like to integrate widgets in NodeRed usinf FreeMaster Lite. Following the NXP training titled FreeMASTER Lite 1.1 + Node-RED Integration https://www.nxp.com/design/design-center/training/TIP-FREEMASTER-LITE-NODE-RED It is shown that (@ minute 0:40) the widget shuld be added accessing to Setting -> Managing Palette . But Managing Palett option is not available in the latest installation of FreeMaster Lite, just downloaded from NXP site Thanks for any support Paolo Re: Impossible to integrare new node in FreeMaster Lite NODE Red Hi @pberna67, Could you confirm that you are running FreeMASTER Lite version 1.5.1: 2.png2.png2.png and that the Node-RED version is 4.0.9: 1.png1.png1.png I did a clean install and could access the `Manage palette` option.  A quick check - could you try removing (or renaming) the `.node_red` folder from your user folder to make sure that any older Node-RED settings do not interfere with the latest installation. If that does not help you could you provide additional details: Are you running FreeMASTER Lite from the stand-alone installer or the one bundled with the main FreeMASTER 3.2 ? What is you host OS system ? Do you have any external Node-RED installations ? Kind regards, Iulian  Re: Impossible to integrare new node in FreeMaster Lite NODE Red Dear Iulian  Thanks for your quick answer ! I confirm that the FrieeMaster I'm  running is FreeMASTER Lite version 1.5.1: pberna67_0-1790026466167.pngpberna67_0-1790026466167.png Node RED version is 4.09 pberna67_1-1790026600039.pngpberna67_1-1790026600039.png Are you running FreeMASTER Lite from the stand-alone installer or the one bundled with the main FreeMASTER 3.2 ? I've installed only the following package: pberna67_2-1790027196038.pngpberna67_2-1790027196038.png There were NO previous FreeMASTER package installed. What is you host OS system ? Still Windows 10 Do you have any external Node-RED installations ? No, I haven't Thanks Paolo Re: Impossible to integrare new node in FreeMaster Lite NODE Red Hi @pberna67, I checked Node-RED documentation and it seems to be an expected behavior if NPM is not installed on the system. Manage Palette functionality relies in NPM tool for dependencies download and installation. NPM should be installed separately. There is a thread on Node-RED community explaining this topic in more details: https://discourse.nodered.org/t/why-isnt-manage-palette-showing-up/27219/9 Hope it helps, Iulian Re: Impossible to integrare new node in FreeMaster Lite NODE Red Dear  Iulian I don't see any npm program installed anywhere. Do I need to install node-red package too , or everything should be installed by  ? It is strange that part of node-red works and part no. In the thread you have indicated is not shown how to install the additional component NPM. Any additional idea? It is declared: https://www.nxp.com/design/design-center/software/development-software/freemaster-run-time-debugging-tool:FREEMASTER that FreeMaster has Integration with Graphical User Interface (GUI) Guider  design tool. Do you have any examples or additional integration details of the GUI builder in FreeMaster ? Regards Paolo
記事全体を表示
Config Tools for i.MX 26.09 Now Available We are pleased to announce that Config Tools for i.MX 26.09 are now available. Downloads & links To download the installer for all platforms, please login to our download site via:  https://www.nxp.com/design/designs/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX Please refer to  Documentation  for installation and quick start guides. For further information about DDR config and validation, please go to this  blog post. Release Notes Full details on the release (features, known issues...) Version 26.09 Framework Added support for downloading all boards associated with a processor when downloading the processor. DDR tool Added support for i.MX 937 Added DDR3 support for i.MX 8MP FRDM board Added support for i.MX93W FRDM and EVK boards at 3600 MT/s Enabled PMIC PF9453 support for i.MX 91 Minor improvements, enhancements, and bug fixes SerDes tool Added support for i.MX 952 System Manager Multiple validation ID issues are resolved. DDR tool – NXP-validated memory configurations for multiple vendors is available System Manager – extended CLI support for a headless setting      
記事全体を表示
MCUXpresso Config Tools 26.09 Now Available We are pleased to announce that MCUXpresso Config Tools 26.09 are now available. Downloads Also via installer in MCUXpresso for VS Code https://marketplace.visualstudio.com/items?itemName=NXPSemiconductors.mcuxpresso In order to use it with other toolchains, download the installer for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/config Please refer to https://docs.mcuxpresso.nxp.com/config/latest/ for installation and quick start guides. For online version, login into MCUXpresso site: MCUXpresso WEB Release Notes Full details at https://docs.mcuxpresso.nxp.com/config/latest/ Version 26.09 Framework Support public releases of “preliminary” EAR/PRC processor data. Added support for downloading all boards associated with a processor when downloading the processor.
記事全体を表示
Introduction DNPU Training Introduction DNPU Training   Explore the evolution of AI at the edge, from perception AI and generative AI to the emerging era of Agentic AI. This session introduces NXP’s discrete NPU strategy and examines how neural networks, transformer models, and AI agents enable intelligent decision-making for industrial, healthcare, and automation applications. Participants will gain an understanding of the technologies driving the next generation of intelligent edge systems.   This video is currently being processed. Please try again in a few minutes. (view in My Videos) ARA240 DNPU Hands-On Training
記事全体を表示
Ara240 DNPU Hands-On Training Welcome to the Ara240 DNPU Training! This page provides access to training materials, presentations, demos, recordings, and supporting resources related to the Ara240 DNPU. While live Q&A support will be available during the training period, all content will remain accessible for future reference and self-paced learning. Required Hardware The following boards are supported: FRDM i.MX 95 Pro FRDM i.MX 95 FRDM i.MX 8M Plus Ara240 DNPU Ara240 16GB M.2 Module microSD >= 64GB storage USB-C debug cable Internet (Ethernet) HDMI Monitor 100 W power supply (Anker Charger is recommended) USB mouse USB keyword 1080p USB Camera Instructions Step1. Watch introduction DNPU Training Introduction Step2. Check the Hardware and Software Pre-requisites Getting Started Guide with FRDM-IMX8MPLUS Step3. Run the rest of the Software demo packages After completing the pre-work, each lab has its own guide document and a video guide you can use as support material in case you have any question at any step: Lab1: Running a GStreamer Pipeline for 8 Video Streams with YOLOv8n on Ara240 DNPU Ara Vision Multi-Stream YOLOv8 Object Detection Lab2: Running Unimodal Large Language Models on Ara240 DNPU LLM Edge Studio Lab3: Interacting with Vision-Language Models on Ara240 DNPU VLM Edge Studio Lab4: Enabling REST-Based LLM and VLM Inference on Ara240 DNPU eIQ AAF Connector Lab5: Running the Smart Device Gateway server on Ara240 DNPU  Smart Device Gateway  Additional Resources Take advantage of the resources below to deepen your knowledge and support your development efforts: Ara Software Development Kit (ARA SDK) Ara240 DNPU Six Pack Ara240 Discrete Neural Processing Unit (DNPU) Ara240 16GB M.2 Module FRDM i.MX 95 Pro FRDM i.MX 8M Plus ARA240 DNPU Hands-On Training
記事全体を表示
Transformed and Quantized your model with NPU of the MX8Mplus     Introduction In this article, we will explain in this article which steps you have to take to transform and quantize your model with different TensorFlow versions. We are only looking into post training quantization. We are using the MX8MPlus EVK run our model that have a dedicated neural network accelerator IP from VeriSilicon (Vivante VIP8000). Press enter or click to view image in full size i.mx8MPlus block diagram from NXP Is the neural processing unit (NPU) from NXP need a fully int8 quantized model we have to look into full int8 quantization of a TensorFlow lite or PyTorch model. Both libraries are supported with the eIQ library from NXP. Here we will only look into the TensorFlow variant. The general overview on how to do post training quantization can be found on the TensorFlow website.  The operations for floating point are more complex than for integer (arithmetic’s, avoiding overflow). This results in the ability to use only the much simpler and smaller arithmetic units instead of the larger floating-point units. ​ ​The physical space needed for float32 operation much larger than for int8. This results in:​ Lower power consumption, ​ Less heat development, ​ The ability to join more calculation units decreasing inference time. Prerequisite To create the code on your PC first, we recommend using Anaconda with a virtual environment running Python 3.6, TensorFlow 2.x, numpy, opencv-python and pandas. Post training quantization with TensorFlow Version 2.x If you created and trained a model via tf.keras there are three similar ways of quantizing the model. First Method — Quantizing a Trained Model Directly The trained TensorFlow model has to be converted into a TFlite model and can be directly quantize as described in the following code block. For the trained model we exemplary use the updated tf,keras_vggface model based on the work of rcmalli . The transformation starts at line 28. from keras_vggface_TF.utils import preprocess_input from keras_vggface_TF.vggfaceTF import VGGFace converter.inference_output_type = tf.int8 import tensorflow as tf import numpy as np tfVersion=tf.version.VERSION.replace(".", "") # can be used as savename print(tf.version.VERSION) # TRAIN A MODEL pretrained_model = VGGFace(model='resnet50', include_top=False, input_shape=(224, 224, 3), pooling='avg') # pooling: None, avg or max #Create a generator for representative Dataset folderpath='./All_croped_images/' def prepare(img):          img = np.expand_dims(img,0).astype(np.float32)          img = preprocess_input(img, version=2) return img repDatagen=tf.keras.preprocessing.image.ImageDataGenerator(preprocessing_function=prepare) datagen=repDatagen.flow_from_directory(folderpath,target_size=(224,224),batch_size=1) def representative_dataset_gen():       for _ in range(10):       Img = datagen.next()       yield [img[0]] #CONVERT YOUR MODEL TO TFLITE AND QUANTIZE TO INT8 converter = tf.lite.TFLiteConverter.from_keras_model(pretrained_model) converter.optimizations = [tf.lite.Optimize.DEFAULT] converter.representative_dataset = representative_dataset_gen converter.target_spec.supported_ops = [tf.lite.OpsSet.TFLITE_BUILTINS_INT8] converter.experimental_new_converter = True converter.target_spec.supported_types = [tf.int8] converter.inference_input_type = tf.int8 quantized_tflite_model = converter.convert() #SAVE THE QUANTIZED MODEL AS TFLITE FILE open('quant_model.tflite' , "wb").write(quantized_tflite_model) After loading/training your model you first have to create a representative data set. The representative data set is used by the converter to get the max and min values to be able to estimate the scaling factor. This limits the error introduced by the quantization from float32 to intX. The error comes from the different number-space of float and int. Converting from float to int8 limits the number-space to integer values between -128 to 127. Calibrating the model on the dynamic range of the input limits this error. Here you can just loop through your images or create a generator as in our example. We used the tf.keras.preprocessing.image.ImageDataGenerator() to yield images and do the necessary prepossessing on the images. As a generator you can of course also use the tf.data.Dataset.from_tensors() or … from.tensor_slices(). Just keep in mind to do the same pre-processing on your data here as you did on the data you trained your network with (normalization, resizing, de-noising, …). This can all be packed into the preprocessing_function call of the generator (line 19). The conversion starts at line 28. A simple TensorFlow lite conversion would look like this: converter = tf.lite.TFLiteConverter.from_keras_model(pretrained_model) tflite_model = converter.convert() open('model.tflite' , "wb").write(tflite_model) The quantization part is in-between: converter = tf.lite.TFLiteConverter.from_keras_model(pretrained_model) converter.optimizations = [tf.lite.Optimize.DEFAULT] converter.representative_dataset = representative_dataset_gen converter.target_spec.supported_ops = [tf.lite.OpsSet.TFLITE_BUILTINS_INT8] converter.experimental_new_converter = True converter.target_spec.supported_types = [tf.int8] converter.inference_input_type = tf.int8 converter.inteference_output_type=tf.int8 quantized_tflite_model = converter.convert() open('quant_model.tflite' , "wb").write(quantized_tflite_model) Line 3 : optimizations other than default are deprecated. No other options are available at the moment (Year 2020). Line 4 : Here we set the representative data set. Line 5 : Here we make sure that we have a full conversion to int8. Without this option, only the weights and biases would be converted but not the activations. This is used when we only want to reduce the model size. However, our NPU needs full int8 quantization. Having the activations still in floating point would result in overall floating-point and could not run on the NPU. Line 6: Enables MLIR-based conversion instead of TOCO conversion, which enables RNN support, easier error tracking. Line 7: Sets the internal constant value to int8. The target_spec corresponds with the TFLITE_BUILTINS from line 5. Line 9 and 10: Set also the input to int8. This is fully available from TF 2.3 Now if we convert the model using TF2.3 with experimental_new_converter=True inference_input_type=tf.int8 inference_output_type=tf.int8 we receive the following model: However if we do not set the inference_input_type and inference_output_type we receive following model: So the effect is that you can determine which input data type the model accepts and returns. This can be important if you work with an embedded camera, as included with the MX8MPEVK. The mipi camera returns 8bit values, so if you want to spare a conversion to float32 int8 input can be handy. But be aware, if you use a model without prediction layers to gain e.g., embeddings, an int8 output will result in very poor performance. Here an output of float32 is recommended. This shows that each problem needs a specific solution. Second and Third Method — Quantize a Saved Model from *.h5 or *.pb Files If you already have your model, you most likely have it saved somewhere either as an Keras h5 file or a TensorFlow protocol buffer pb. We will quickly save our model using TF2.3: import tensorflow as tf f rom keras_vggface_TF.vggfaceTF import VGGFace pretrained_model = VGGFace(model='resnet50', include_top=False, input_shape=(224, 224, 3), pooling='avg') # pooling: None, avg or max # Saving as a protocol buffer !mkdir -p saved_model pretrained_model.save('saved_model/my_model') #saving as a h5 file (if your Tensorflow Version is < 2.0 use this) !mkdir -p keras_model pretrained_model.save('keras_model/my_model.h5') Following the conversion and quantization is very similar as in Method One. The only difference is how we load the model in with the converter. Either load the model and continue as in Method One. #Load the h5 model pretrained_model = tf.keras.models.load_model('my_model.h5') #Then use the converter as before converter = tf.lite.TFLiteConverter.from_keras_model(pretrained_model) Or load the h5 model directly. When using TensorFlow version 2 and above you have to use a compatible converter: # Or load the h5 model from file # TensorFlow version >2.x converter = tf.compat.v1.lite.TFLiteConverter.from_keras_model_file(saved_model_dir + h5_modelname) #works now also with TF2.x # TensorFlowversion < 2.0 converter = tf.lite.TFLiteConverter.from_keras_model_file(saved_model_dir + h5_modelname) If you load from a TensorFlow pb file use: # Or load the pb file from the modelfolder # TensorFlow version >2.x converter = tf.lite.TFLiteConverter.from_saved_model(saved_model_dir) # the folder contains the pb file and a assets and variables folder Converting with TensorFlow Versions below 2.0 If you want to convert a model written in TensorFlow version < 1.15.3 using Keras, not all options are available for TFlite conversion and quantization. The best way is to save the model with the TensorFlow version it was created in (e.g., rcmalli keras-vggface was trained in TF 1.13.2). I would suggest not using the “saving and freeze graph” method to create a pb file as the pb files differ between TF1 and TF2. The TFLiteConverter.from_saved_model does not work, creating quite a hassle to achieve quantization. I would suggest using the above mentioned method using Keras: import keras …. pretrained_model.save('my_model.h5') Then convert and quantize your model with a TensorFlow version from 1.15.3 onward. From this version on a lot of functions where added in preparation for TF2. I suggest using the latest version. This will result in the same models presented here.          
記事全体を表示
MFRC531 01T 的设备集成(软件) 我需要将 NXP Mifare 阅读器 (crypto1) MFRC531 01T 集成到系统中,并且我需要一些关于 RS232 相关协议命令的帮助,以便轮询 SID、进行身份验证和读取块/扇区。 Re: Device Integration (Software) for MFRC531 01T 你好@Menspa 遗憾的是,NXP 没有提供基于 MFRC531 的演示示例;因此,您需要参考 MFRC531 数据手册( MFRC531 标准 ISO/IEC 14443 A/B 读卡器解决方案)并使用 NXP 的 NxpNfcRdLib 库来开发您的读/写卡应用程序。
記事全体を表示
エマール・ビーチフロントの完成済み4ベッドルームアパートメントを購入するためのステップバイステップの手順 エマールビーチフロントは急速にドバイで最も人気のあるウォーターフロントの目的地の一つとなり、家族や投資家の間で4ベッドルームのアパートメントの需要が高まっています。この島のコミュニティで広々とした入居準備が整った家の購入を検討しているなら、購入プロセスの最初から最後まで理解しておくことで遅延を避け、自信を持って判断できます。 このガイドでは、エマールビーチフロントで4ベッドルームのアパートを購入するための各段階を案内し、ドバイの信頼できる不動産会社タクウェーン・アルダーからの実用的な洞察も添えています。 エマール・ビーチフロントが、すぐに住める4ベッドルームのアパートメントを求める購入者に魅力的な理由 エマールビーチフロントはドバイマリーナとパームジュメイラの間に位置し、プライベートビーチアクセス、リゾートスタイルの施設、スカイラインの眺めを提供しています。ここでの4ベッドルームのアパートは、工事を何年も待たずにより多くの居住空間を求める大家族に適しています。ユニットはすでに建設され引き渡されているため、買い手は実際の物件を検査し、迅速に入居し、賃貸を選べば早く賃貸収入を得始めることができます。 ステップ1:予算と資金調達方法を明確にする リスティングを見る前に、現実的にどれくらいの費用が出せるかを計算しましょう。エマールビーチフロントの4ベッドルームアパートはプレミアムな購入なので、リスティング価格だけでなく全体のコスト面も考慮してください。 次の点を考慮してください。 頭金の要件は、駐在員の場合通常20〜25%です 融資が必要な場合は、UAEの銀行から住宅ローンの事前承認を得てください。 ドバイ土地局の譲渡手数料は、通常、購入価格の4%です。 代理店手数料、通常2パーセント ビルディングおよび地域社会に連動した継続的なサービス料金 早期に住宅ローンの事前承認を得ることで、明確な予算上限ができ、売り手との交渉において自分の立場を強化します。 ステップ2:エマール・ビーチフロントの完成済み物件を絞り込む 予算が決まったら、ニーズに合った、すぐに住める4ベッドルームのアパートを探し始めましょう。エマールビーチフロントにはビーチビスタ、サンライズベイ、ビーチアイルなどのタワーがあるため、建物ごとに利用可能性やレイアウトは大きく異なることがあります。 Takween AlDarのような知識豊富な不動産会社と協力することで、階数、眺望、間取りの効率性、周辺施設への近さなどに基づいて選択肢を絞り込むことができ、最新の在庫状況を反映していない可能性のあるオンラインの物件情報だけに頼る必要がなくなります。 ステップ3:物件の内覧を予約する 完成済みマンションは、未完成物件の購入とは異なり、契約前に実際に物件内を見学することができます。閲覧機能を使って以下の点を確認してください。 実際の部屋のサイズとレイアウトの流れ 仕上げと装備の品質 自然光と眺望の向き 共用エリア、エレベーター、駐車場の状態 以前にその物件が使用されていた場合は、メンテナンス履歴や最近の修理状況について確認してください。 ステップ4:所有権および不動産関連書類の確認 オファーを出す前に、ドバイ土地局を通じて売主の所有権を確認し、権利証を請求してください。担当エージェントは、物件に関連する未払いの住宅ローン、管理費の滞納、または法的紛争がないかどうかも確認する必要があります。この確認手順は、後々の取引におけるトラブルを防ぐためのものです。 ステップ5:覚書を交渉し署名する 物件とドキュメントに満足したら、オファーを提出してください。合意が成立した場合、両当事者はドバイ土地局のTrakheesiシステムを通じて、一般にフォームFとして知られる覚書に署名する。この段階では、通常、購入価格の約10%にあたる手付金を支払います。この手付金は、譲渡手続きが完了するまで保管されます。 ステップ6:異議なし証明書を取得する 売り手は開発者、この場合はEmaarに対して「異議なし証明書」を請求しなければなりません。この証明書は、不動産に未払いのペイメントや制限がないことを確認し、所有権移転の道を切り開きます。プロセッシングは通常数営業日かかり、開発者に料金が支払われます。 ステップ7:ドバイ土地局で譲渡手続きを完了する 異議なし証明書を手に、買主と売主は共にドバイ土地局の事務所、または登録済みの信託センターに出向き、譲渡手続きを完了させる。この面談時に、残高、振込手数料、および適用される諸費用をお支払いいただきます。手続きが完了すると、所有権証書があなたの名義で発行され、正式にあなたがアパートの所有者となります。 ステップ8:公共料金の手続きと入居 移管後は、電気と水道のDEWAに登録し、建物に関連する地域サービスも有効化してください。アパートは準備が整い、入居も準備できているので、工事完了を待たずに引き継ぎ手続きを始め、鍵を受け取り、引っ越しの計画を立てることができます。 Takween AlDarが購入をサポートする方法 エマール・ビーチフロントの即入居可能な4ベッドルームのアパートメントを購入するには複数の手順が必要であり、経験豊富なパートナーがいればストレスとリスクを軽減できます。タクウィーン・アルダールは、物件選び、書類確認、交渉、そして所有権移転に至るまで、購入者を丁寧にサポートし、最初の内覧から最終的な引き渡しまで、透明性と円滑な手続きを保証します。 よくある質問 Q:Emaar Beachfrontで完成済みのマンションを購入するには、どれくらい時間がかかりますか? A: 資金調達やドキュメントが整っている場合、覚書の署名から権利証書の移転完了まで通常2〜4週間かかります。 Q: 外国人はエマールビーチフロントで4ベッドルームのアパートを購入できますか? A:はい、エマール・ビーチフロントは所有権が完全なフリーホールドエリアに位置しているため、あらゆる国籍の購入者が完全な外国人所有権を取得できます。 質問:物件を見学する前に、住宅ローンの事前承認は必要ですか? A:必須ではありませんが、事前承認を得ておくことで予算を把握しやすくなり、売り手にとってあなたの提案の信頼性が高まります。 質問:購入価格以外に、どのような費用を予算に組み込むべきでしょうか? A: 開発業者からはドバイ土地局の譲渡手数料4%、代理手数料2%、そして場合によってはNOCプロセッシング手数料を支払うことを覚悟してください。 Q:エマール・ビーチフロントでは、完成済みのマンションは、未完成の物件よりも良い選択肢でしょうか? A:完成済みのマンションはすぐに入居でき、購入前に内覧も可能ですが、未完成の物件は購入価格が低い場合もありますが、引き渡しまで待つ必要があります。 まとめ エマール・ビーチフロントで完成済みの4ベッドルーム・アパートメントを購入するには、現実的な予算の設定から書類の確認、ドバイ土地局での所有権移転手続きの完了まで、綿密な計画を立てることが重要なプロセスとなります。適切な指導があれば、買い手は自信を持って各ステップを進め、無駄な遅延なく新しいウォーターフロントの家に落ち着くことができます。Takween AlDarは、最初の物件探しから最終引き渡しまで、この旅のあらゆる段階でサポートいたします。
記事全体を表示
S32K312:NMI 在 Reset_Handler 执行之前触发,仅在功能(软件)复位之后触发,且仅在特定情况下触发。 设备:S32K312 工具链:Green Hills ELXR(编译器) HSE固件:s32k312_hse_fw_0.13.0_2.55.0_pb250129.bin 调试器:Lauterbach TRACE32 软件:基于AUTOSAR RTD的引导加载程序(FBL)+应用程序(APP),双镜像结构 问题概要 在部分生产单元上,CPU 在执行功能性操作后立即挂起。 (软件)RESET。同样的单位在破坏性 (上电复位)后总能正常启动。在我们的参考/已知良好设备上,不会出现卡顿现象。 证据表明,非军事事件 (NMI) 发生在任何应用程序代码执行之前。 1)在挂起点捕获的 CPU 上下文(自动堆叠的异常帧): - R0-R3 = 0x00000000,R12 = 0x00000000 - LR = 0xFFFFFFFF(重置默认值 -> 尚未执行任何 BL) - PC = 0x00416904(我们的 Reset_Handler 的第一个指令地址) - xPSR = 0x01000000 2) SCB->ICSR = 0x00000802 Chibeom_3-1785136456875.pngChibeom_3-1785136456875.pngChibeom_3-1785136456875.pngChibeom_3-1785136456875.pngChibeom_3-1785136456875.pngChibeom_3-1785136456875.png - VECTACTIVE[8:0] = 2 -> NMI 是当前活动的异常 - RETTOBASE = 1 这证实 CPU 当前正在 NMI 处理程序内部执行。 3) 我们向量表中的 NMI 偏移量条目正确指向我们自己的 默认异常处理程序,因此这是一个真正的 NMI 事件,而不是向量事件。 表格损坏。 在相同的挂起状态下检查的寄存器(全部读取为干净/非活动状态) - MC_RGM_DES = 0x00000000(非破坏性RESET) - MC_RGM_FES = 0x20000000(仅限第 29 位)(仅限“软件功能RESET”) 标志位已设置,无其他功能 RESET源已标记) - FCCU:STAT、N2AF_STATUS、A2FF_STATUS、N2FF_STATUS、NCF_S0、IRQ_STAT 全部 = 0x00000000 - CMU_FC 实例 0、3、4:SR = 0x00000000(无频率高/低故障) - PMC LVSC = 0x00000000(无 LVD/HVD 标志,已锁存或带电) - ERM (0x4025C000): 无法读取正常单元或故障单元的 ERM 值 (在我们的配置中可能采用时钟门控),因此 ERM 状态未经验证。 问题 1. 除了 FCCU / CMU_FC / PMC / MC_RGM 之外,还有其他 NMI 来源吗? 这可能会在应用程序的 Reset_Handler 执行之前触发。 第一条指令? 2. 由于 HSE 子系统独立于应用程序核心运行,因此 应用程序核心功能重置是可能的(但这不会导致) 重置 HSE)以创建状态不匹配,从而触发 NMI。 应用核心? 3. 是否有与此症状相符的 S32K312 已知勘误表(仅限 NMI) 功能性/软件重置(而非上电复位)? 任何关于需要检查的其他登记册的指导,或涵盖以下内容的任何文件 非常感谢来自 FCCU / ERM / CMU_FC / PMC 以外的 NMI 信息来源。 Re: S32K312: NMI triggered before Reset_Handler executes, only after Functional (SW) Reset, on speci 你好@Chibeom , 请您在系统处于挂起状态时读取寄存器 MU_0.MUB CSSR0 和 MU_1.MUB CSSR0,并确认其中任何一个寄存器的第 0 位(NMIC)是否已设置? 谢谢 Re: S32K312: NMI triggered before Reset_Handler executes, only after Functional (SW) Reset, on speci 嗨@danielmartynek , 感谢您指出 MU_0.MUB / MU_1.MUB CSSR0。 MU_0.MUB 和 MU_1.MUB 上的 CSSR0(位 0,NMIC)均读取 0x00000000。 单元处于挂起状态,因此 MU->NMI 请求路径 (CCR0[NMI] / CSSR0[NMIC]) 似乎并非待处理。 然而,在比较已知良好单元和一台设备之间的MU寄存器时, 故障单元(两者均在相同的挂起状态地址范围内捕获), 我们发现了一个始终存在的差异: 正常单元 故障单元 MU_0.MUB 版本 0x0300000F 0x0300000F(相同) MU_0.MUB PAR 0x20200404 0x20200404(相同) MU_0.MUB CR 0x00000000 0x00000000(相同) MU_0.MUB SR 0x00000000 0x00000002 <- MURIP 集 MU_1.MUB VER/PAR/CR:正常单元和故障单元完全相同 MU_1.MUB SR 0x00000000 0x00000002 <- MURIP 集 因此,在两个 MU 实例上,SR 位 1 (MURIP) 仅在发生故障的实例上设置。 单位,始终如一。根据参考手册,MURIP 指出: “处理器 A”已发出 MU 复位,且只能通过以下方式清除: 系统重置(非 MU 重置)。 由于 CPU 在执行任何操作之前都会在 NMI 处理程序内部冻结,因此无法执行任何操作。 应用程序代码本身无法清除此标志,因此它 必须在启动序列之前(或作为启动序列的一部分)设置。 我们非常希望您能就以下问题提供意见: 1.对于 MU_0.MUB 和 MU_1.MUB,哪个处理器是“处理器 A”(即 谁制定 MURIP?我们的头部信息仅暴露了“MUB”寄存器块。 应用程序核心可访问地址——这是否意味着 应用程序核心始终是“处理器 B”,而 HSE 是“处理器 A”。 在这些情况下呢? 2. “系统RESET”(清除 MURIP 所必需的操作)是否包含功能/软件 是RESET应用核心,还是仅进行破坏性/上电RESET?如果 MURIP 无法通过我们的功能 RESET 清除,这就能解释为什么了。 SW RESET 后该设置保持不变,但开机后则清除。 3. 独立于 NMI 问题:MURIP 标志本身是否已设置/卡住 在正常运行期间,这是预期之内的还是被认为是异常的? 4. 由于 CSSR0[NMIC] 当前读取值为 0,硬件是否有可能…… NMI 例外条目出现时是否自动清除 NMIC,还是仅通过以下方式清除: 显式软件写入(在这种情况下,NMIC=0 表示 MU->NMI通道从一开始就从未被钳位? 再次感谢您一直以来的帮助。 Re: S32K312: NMI triggered before Reset_Handler executes, only after Functional (SW) Reset, on speci 你好@Chibeom , 很抱歉耽搁了。我离开办公室两天。 1. 是的,HSE_B 核心控制 MU_0 和 MU_1 的 MUA 接口。 2. 任何系统 RESET 都应该 RESET MURIP。 3. 我认为这是一个异常情况,因为我对此了解不多。 4. 由于它是 W1C 寄存器,因此需要显式写入。 能否确保在触发功能 RESET 时 HSE_B 处于非活动状态? 另外,当应用程序卡在 NMI 处理程序中时,HSE_B 的状态是什么? 你能读取 MU_0 B 侧的标准 HSE GPR (0x4039_C028)、FSR 和 GSR 寄存器吗? 您在应用程序中使用NMI引脚吗? 此致, 丹尼尔 Re: S32K312: NMI triggered before Reset_Handler executes, only after Functional (SW) Reset, on speci 嗨,丹尼尔, 请查看附件中的三张合并后的寄存器转储截图,如下所示。 根据您的问题整理我们的研究结果。 -------------------------------------------------------- 附件 -------------------------------------------------------- 附件 1:正常设备(已启用安全调试,运行正常) Chibeom_3-1785730814252.pngChibeom_3-1785730814252.pngChibeom_3-1785730814252.pngChibeom_3-1785730814252.pngChibeom_3-1785730814252.pngChibeom_3-1785730814252.png 附件 2:故障单元,在功能 RESET 之前 已触发信号(正常运行) Chibeom_4-1785730831377.pngChibeom_4-1785730831377.pngChibeom_4-1785730831377.pngChibeom_4-1785730831377.pngChibeom_4-1785730831377.pngChibeom_4-1785730831377.png 附件3:故障单元,功能RESET后,卡在…… NMI 处理程序(挂起状态) [[ ## completed ##]] Chibeom_5-1785730838688.pngChibeom_5-1785730838688.pngChibeom_5-1785730838688.pngChibeom_5-1785730838688.pngChibeom_5-1785730838688.pngChibeom_5-1785730838688.png -------------------------------------------------------- 发现 1)功能RESET触发时的 HSE_B 活动,以及 2)HSE_B 在 NMI 处理程序中卡住时的状态: 比较附件 2(RESET前)和附件 3(RESET后, 在故障单元上(处于挂起状态),我们检查的每个寄存器都显示: 重置前后完全相同: [[ ## completed ##]] - MU_0.MUB / MU_1.MUB TSR = 0x0000000F,RSR = 0x00000000(无待处理 发送/接收通道上的消息(RESET后保持不变) - MU_0.MUB GSR = 0x00000000(不变) - MU_0.MUB FSR = 0x03600000(未更改) - HSE GPR (0x4039C028) = 0x000001C1(未更改) - MU_0.MUB / MU_1.MUB SR 位 1 (MURIP) = 0x00000002 -- 已设置 在RESET触发信号之前,并且保持设置状态,保持不变;在 RESET之后 因此,MURIP 在此次 RESET 周期之前就已经设置好了,并且 功能 RESET 本身并不会改变任何与 HSE 相关的 登记簿。 作为参考,引用,在一台运行良好的设备上,使用相同的安全调试功能 配置(附件 1),MURIP 在两个设备上均读取 0x00000000 MU_0.MUB 和 MU_1.MUB,而 HSE GPR 和 WKPU NCR 读取的是 相同的值。将值视为故障单元。 3)关于设置/卡住的 MURIP 是否属于异常情况: 明白了,谢谢确认。 4) NMI 引脚使用: 我们不使用 WKPU 路由的 NMI 路径(WKPU_IP_USED 未启用; 我们的引导加载程序中没有编译任何 WKPU 驱动程序代码。 应用程序图像)。WKPU NCR (0x402B4008) = 0x60000000 完全相同 在所有三个附件中。在所有情况下,NSR = 0x00000000。自从 我们认为,这一点在所有单位和条件下都保持不变。 涉及外部/WKPU路由的NMI源。 目前为止的调查结果概要 故障 设备上的 MURIP(MU_0.MUB 和 MU_1.MUB SR 位 1)已设置。在功能 RESET 的触发信号发出之前,该单元就已经存在,并且仍然存在。 悬挂期间保持不变。在一台性能良好的设备上,读数为0,与上述相同。 安全调试配置。这是唯一一致且可复现的结果。 我们在比较过的每个注册表中都发现了差异(FCCU, CMU_FC、PMC、WKPU 和 MU CSSR0/GSR/TSR/RSR/GPR/FSR)。 由于 MURIP 由“处理器 A”(HSE_B)设置,因此应该由……清除。 根据您的回答,“任何系统 RESET”,而且它之前已经设置过了。 我们的功能 RESET 已发出触发信号(但 RESET 本身并未显示)。要更改它),这表明 HSE_B 在早些时候发布了 MU RESET。 HSE_B 识别的“系统 RESET”从未清除过该点。 问题 1. 从健康、安全和环境 (HSE) 的角度来看,是否有办法确定什么会导致这种情况发生 首先,HSE_B(处理器 A)是否应该发出 MU RESET 指令?我们会 我想了解为什么会设置 MURIP。 2. 是否有推荐的方法来触发 HSE_B 的 RESET?被应用程序 识别为“系统 RESET”(以清除 MURIP)。除了完全断电重启之外,软件方面还有什么需要改进的地方吗? 3. 应用程序核心端的 MURIP 标志卡住是否可能与以下情况有关? 我们正在观察的是NMI,或者这更有可能是两个独立的NMI。 是否出现了与之前同一事件相同的症状? 再次感谢您一直以来的帮助。 Re: S32K312: NMI triggered before Reset_Handler executes, only after Functional (SW) Reset, on speci 你好@danielmartynek , 感谢您提供的最新信息,以及您对 MURIP / NMI 路径的升级处理。 请向您内部的健康、安全与环境(HSE)团队提出问题。我们对此表示感谢,我们会等待。 他们的意见。 与此同时,我们发现了一个可能相关的额外数据点, 所以我们希望现在就分享出来,而不是等待。 在比较UTEST Flash区域中性能良好的单元的OTP字段时 我们发现,在故障单元中,生命周期插槽存在差异。 CUST_DEL (0x1B000220-22F) 和 OEM_PROD (0x1B000230-23F) 完全相同 在好的单元和坏的单元上都编程了(所有字均为 0x55AA50AF) 故障单元。 区别在于 IN_FIELD 插槽 (0x1B000240-24F): - 良好单元:开始进行编程。 Chibeom_2-1786069927793.pngChibeom_2-1786069927793.pngChibeom_2-1786069927793.pngChibeom_2-1786069927793.pngChibeom_2-1786069927793.pngChibeom_2-1786069927793.png - 故障单元:读取为未编程 (0xFFFFFFFF) Chibeom_1-1786069910918.pngChibeom_1-1786069910918.pngChibeom_1-1786069910918.pngChibeom_1-1786069910918.pngChibeom_1-1786069910918.pngChibeom_1-1786069910918.png 我们仍在仔细核对 IN_FIELD 中的确切字节模式。 我们这边有个位置,但这个位置的好坏差异似乎很明显。 持续的。 请问您能否解释一下: 1.这是否意味着故障单元的配置发生了变化 在过渡过程中途被损坏或不完整 IN_FIELD? 2. 生命周期推进到 IN_FIELD 是否可能不完整或缺失 请解释我们一直在研究的NMI/挂起行为 线? 3. 是否有安全的方法来检查或完成此生命周期进展 对于故障单元,是否需要进行全面的生产线重启? 再次感谢您的帮助。 Re: S32K312: NMI triggered before Reset_Handler executes, only after Functional (SW) Reset, on speci 你好@Chibeom , 根据内存视图,OEM_PROD = 非活动状态,IN_FIELD = 已擦除。 请先读取DCM寄存器:RM,版本12,第 39.3.1 节 DCM 内存映射。 以及第 38.2.3 节“破坏性重置 3 (DCMROD3) 中的只读 GPR”? 您也可以使用 HSE_FW API 来获取 LC 属性? 谢谢 Re: S32K312: NMI triggered before Reset_Handler executes, only after Functional (SW) Reset, on speci 你好@Chibeom , 感谢您提供的详细寄存器转储文件。我已经将有关 MURIP 行为以及 HSE_B 和 CM7_0 之间潜在的 NMI 路径的问题上报给了我们内部的 HSE 团队,因为这似乎没有相关文档记录。等我收到他们的反馈后,我会尽快回复你。 Re: S32K312: NMI triggered before Reset_Handler executes, only after Functional (SW) Reset, on speci 你好@Chibeom , 谢谢你提供的数据。 由于 IN_FIELD 槽仍处于擦除状态,您能否尝试再次设置该属性以推进其更新? 正如我之前提到的,该案件目前正在内部讨论中。 一旦有任何新消息,我会立即更新此帖。 Re: S32K312: NMI triggered before Reset_Handler executes, only after Functional (SW) Reset, on speci 嗨@danielmartynek , 感谢您向我们指出 DCM 内存映射和 DCMROD3。我们在两台设备上捕获了 DCMSTAT (0h)、DCMLCS (8h)、DCMLCS_2 (80h) 和 DCMROD3 (208h),并根据 RM rev.9 对它们进行了解码。 ---------------------------------------------------- 捕获的值 ---------------------------------------------------- 好单位: Chibeom_0-1786500129171.pngChibeom_0-1786500129171.pngChibeom_0-1786500129171.pngChibeom_0-1786500129171.pngChibeom_0-1786500129171.pngChibeom_0-1786500129171.png - DCMSTAT (0h) = 0x00000E11 - DCMLCS (8h) = 0x00000000 - DCMLCS_2 (80h) = 0x00000000 - DCMROD3 (208h) = 0x00000000 故障单元: Chibeom_1-1786500144600.pngChibeom_1-1786500144600.pngChibeom_1-1786500144600.pngChibeom_1-1786500144600.pngChibeom_1-1786500144600.pngChibeom_1-1786500144600.png - DCMSTAT (0h) = 0x00000E03 - DCMLCS (8h) = 0x06184104 - DCMLCS_2 (80h) = 0x00000006 - DCMROD3 (208h) = 0x00400000 ---------------------------------------------------- 已解码字段(仅限故障单元,因为正常单元读取的值为全零) ---------------------------------------------------- DCMSTAT: - bit1 DCMERR = 1(DCM 完成出错)-- 正常设备的此位值为 0 - bit4 DCMLCST = 0(LC 扫描状态未“成功完成”)——正常设备的此位值为 1 DCMLCS: - 位 21-19 DCMLCC4(IN_FIELD 标记)= 011b = "区域已擦除/未擦除" - 位 15-13 DCMLCC3(OEM_PROD 标记)= 010b = "标记为非活动" - 位 27-25 DCMLCC5(预 FA 标记)= 011b = “已擦除/原始” - 所有关联的 *_ECE/*_CFE/*_CSS 位 = 0。 DCMLCS_2: - 位 3-1 DCMLCC6(FA 标记)= 011b = "已擦除/原始" DCMROD3: - bit22 LC_ERR = 1(“生命周期扫描出错”) 这与我们之前分享的 UTEST OTP 转储一致:故障单元上的 IN_FIELD 插槽读取为已擦除/全新。 ---------------------------------------------------- 故障单元上的 HSE_FW API 结果 (HseReadLifecycle) ---------------------------------------------------- HseReadLifecycle() 返回 0x10 = HSE_LC_IN_FIELD。因此,从 HSE 固件的角度来看,当前生命周期已经是 IN_FIELD。 这似乎与上面的 DCM/OTP 数据相冲突:DCM 的 DCMLCC4 字段读取 IN_FIELD 标记为“已擦除/原始”,而 UTEST OTP IN_FIELD 插槽(0x1B000240h 及之后)读取为未编程(0xFFFFFFFF),但 HSE API 报告生命周期已确认为 IN_FIELD。 我们想按原样分享这些信息,而不是得出结论,因为我们不知道 HSE 是否通过独立于 DCM 闪存标记的单独/安全存储来跟踪生命周期,或者这是否表明标记本身存在问题。 问候, 智范 Re: S32K312: NMI triggered before Reset_Handler executes, only after Functional (SW) Reset, on speci 你好@danielmartynek 我们按照建议,再次尝试在故障单元上设置 IN_FIELD 属性。 结果:HSE_SRV_RSP_NOT_ALLOWED (0xAA55A21C) 问候, 智范 Re: S32K312: NMI triggered before Reset_Handler executes, only after Functional (SW) Reset, on speci 你好@Chibeom , 可能是负责推进生命周期 (LC) 的 HSE 服务中断了,导致 LC 处于这种状态。 LC 和 LC 控制 (DCMLCC) 寄存器报告的值与 HSE_FW 相同,均为 0x77 (IN_FIELD),但 UTEST 区域的编程不正确。理论上,您可以使用调试器对 UTEST IN_FIELD 插槽进行编程,这应该可以清除 DCM 错误。 此致, 丹尼尔 Re: S32K312: NMI triggered before Reset_Handler executes, only after Functional (SW) Reset, on speci 嗨@danielmartynek 感谢您建议使用调试器对 UTEST IN_FIELD 槽进行编程。 我们检查了内部 OTP 字段参考表,发现 IN_FIELD 生命周期槽 (1B00_0240-024F) 在 LC > MCU_PROD (OEM_PROD) 后,除 HSE 外,对任何主设备均被列为写保护。由于该单元上的 HseReadLifecycle() 已经报告 IN_FIELD,因此该 LC 条件似乎已经满足。 能否解释一下,在这种保护规则下,调试器向该插槽写入数据如何才能成功?在这种情况下,要使调试器被视为允许的主设备,是否需要特定的程序、模式或身份验证步骤? 另外,您是否已经找到任何关于为什么 LC 推进到 IN_FIELD 时最初会处于这种不完整状态的原因?如果可以进行分析,我们希望了解根本原因,而不仅仅是恢复步骤。 谢谢你, 智范 Re: S32K312: NMI triggered before Reset_Handler executes, only after Functional (SW) Reset, on speci 你好@Chibeom , 谢谢你提供的信息。 目前看来,似乎没有办法恢复MCU。 一种可能性是,HSE 设置属性服务请求推进 LC 的操作被系统 RESET 中断(据我了解,LC 不是通过 IVT 中的 LCW 推进的)。 您是否阅读了 HSE 对服务请求的回复?你们会记录是否出现错误吗? 在触发服务之前,您是否验证过 HSE_STATUS_INIT_OK 是否已设置? 有多少块电路板/MCU受到此问题的影响?这种情况仅限于少数设备,还是在更多设备上都观察到了? 谢谢! 丹尼尔 Re: S32K312: NMI triggered before Reset_Handler executes, only after Functional (SW) Reset, on speci 你好@Chibeom , 请问有任何最新消息吗? 谢谢 Re: S32K312: NMI triggered before Reset_Handler executes, only after Functional (SW) Reset, on speci 嗨@danielmartynek , 很抱歉回复晚了,感谢您的提问。以下是我们的回答: 1.对于 LC 推进序列,我们读取 HSE 服务响应(来自 DebugAuth、AdvanceLifecycle 和 ReadLifecycle 调用),并使用它们来确定总体成功/失败状态。我们不记录具体是哪个调用失败了,也不记录具体的错误代码——只有总体的 OK/FAIL 结果,并且不会将其保存到任何地方。因此,我们没有关于这些设备最初进行LC推进过程中发生了什么的记录。 2. 我们的 LC 更新函数及其调用者在触发 AdvanceLifecycle 服务之前,都没有显式检查 HSE_STATUS_INIT_OK。我们在下载流程开始时检查一次 HSE_STATUS_INIT_OK,方法是读取 MU_0.MUB FSR 寄存器 (0x4038C104) 并从中导出 hseStatus_t(对 FSR 位 16-31 进行掩码/移位,如在 Hse_Ip_GetHseStatus 中所做的那样)。在流程后续的生命周期推进步骤之前,不会重复进行此检查。 为了提供更多背景信息,我们故障单元的生产设备日志显示了以下顺序:FSR 检查完成(OK)-> 应用程序下载 -> 安全调试启用 -> 失败。请注意,我们设备日志中的“安全调试启用”指的是包含 LC 推进(DebugAuth、AdvanceLifecycle 和 ReadLifecycle 一起)的整个过程——它被记录为一个单独的通过/失败步骤,因此我们无法从该日志中判断哪个子步骤实际失败了。 我们的调试设备(TRACE32)已在现有调试流程中检查了 HSE_STATUS_INIT_OK,但我们的下载/编程设备(生产线)可能没有在 LC 前进触发的序列点上持续检查此状态。 关于受影响的设备数量:目前我们有 2 块板/MCU 出现此问题。 我们还有两个后续问题: - 通过读取 FSR 寄存器并从中导出 hseStatus_t 来检查 HSE_STATUS_INIT_OK 是否是一种有效/推荐的方法? - 目前,我们在下载流程开始时通过读取寄存器来检查 HSE_STATUS_INIT_OK。在触发生命周期推进之前,是否也应该专门检查一下? 谢谢你,Chibeom Re: S32K312: NMI triggered before Reset_Handler executes, only after Functional (SW) Reset, on speci 嗨@danielmartynek , 希望你一切都好。我想查看一下这个帖子有没有什么更新。 如果您有时间,能否提供一些指导?我们将不胜感激。 谢谢你, 智范 Re: S32K312: NMI triggered before Reset_Handler executes, only after Functional (SW) Reset, on speci 你好@Chibeom , 很抱歉耽搁了——我一直在等待 HSE 团队的反馈,但还没有收到关于 NMI 的明确解释。 DCMROD3 中的 LC_ERR 标志:只有当 FCCU NCF 3 配置为生成 NMI 时,它才能触发 NMI。 关于您的问题: 是的,没错。 系统 RESET 后应检查 HSE_STATUS_INIT_OK 标志。应用程序必须等待此标志出现后才能更改系统时钟或使用任何 HSE 服务。一旦设定,就不会改变。该应用程序还可以轮询 HSE_B 内核的 WFI 标志 (PRTN0_CORE2_STAT[WFI]),以确定 HSE_B 是忙还是空闲。 关于 LC 推进中断的问题——还有一个值得调查的可能根本原因。更改生命周期会修改 UTEST 闪存的内容,而 UTEST 闪存与代码闪存块 0 位于同一个 RWW(边读边写)分区中。如果在 UTEST 写入期间有任何代码正在从块 0 执行,则会发生 RWW 错误,并可能阻止生命周期更改成功完成。为避免这种情况,应用程序必须确保在 LC 推进服务进行期间没有对 Block 0 的并发访问。请注意,缓存在大多数情况下可能会掩盖此问题,但在某些特殊情况下,特别是当应用程序使用非同步事件时,可能会导致缓存未命中,从而使问题显现出来。 此致, 丹尼尔 Re: S32K312: NMI triggered before Reset_Handler executes, only after Functional (SW) Reset, on speci 嗨@danielmartynek , 感谢您确认 HSE_STATUS_INIT_OK 的两点。 我想就您在上次回复中描述的 RWW 机制(关于 UTEST 和代码闪存块 0)跟进一下。我们参考了 AN13388(S32K3 存储器指南)表 3 对此进行了进一步研究,但对具体的冲突机制仍有疑问。 根据 AN13388 表 3,对于我们的设备 (S32K312): - 代码闪存块 0:0x0040_0000 - 0x004F_FFFF (1 MB) - 代码闪存块 1:0x0050_0000 - 0x005F_FFFF (1 MB) - UTEST:0x1B00_0000 - 0x1B00_1FFF (8 KB) UTEST 被列为一个独立的区块,与代码闪卡区块 0/1 分开。该文档对 RWW 的一般描述指出,同时读/写“仅适用于操作在不同的块中的情况”,我们理解这意味着只有当读取和写入操作针对*同一*块时才会发生冲突。 鉴于 UTEST 和代码闪存块 0 根据此地址映射是物理上独立的块,您能否解释一下,在生命周期推进期间写入 UTEST 如何会与从块 0 执行的代码产生 RWW 冲突?具体来说: 1. 尽管 UTEST 和 Code Flash Block 0 的地址范围不同,但它们是否共享用于 RWW 目的的内部闪存控制器资源(例如编程/擦除状态机或信号量)? 2. 参考手册中是否记录了其他/更具体的分区分组(除了 AN13388 中的块表之外)是我们应该参考的? 我们的应用程序代码从代码闪存块 0 运行,因此我们希望在决定修复方案之前了解其确切机制。 再次感谢您一直以来的支持。 最好的, 智范 Re: S32K312: NMI triggered before Reset_Handler executes, only after Functional (SW) Reset, on speci 你好@Chibeom , UTEST 确实在 BLOCK 0 中。 请参阅RM: 表103。闪存块配置 S32K3xx_内存映射.xlsx 此外,AN13388(S32K3 内存指南)第 3 章。闪存状态: “最多有五个街区,最少有两个街区。” Block 0 - 4,而 UTEST 位于 Block 0。 此致, 丹尼尔
記事全体を表示
2026 年最佳个人数据移除服务:独立测试与比较 ⚡快速结论 经过六个月的实际独立测试, Incogni 在 全自动移除和同类最佳价值方面 排名第一 ,约为 ~6.49 美元 /月 。 ⚡INCOGNI - 立即访问 ➤➤   DeleteMe凭借以人为本的礼宾服务方式和行业领先的 750 多家经纪人覆盖率,在 上排名第 2。这两项服务都包括持续的再监测--这是 2026 年最重要的一项功能。 ⚡DELETEME - 立即访问 ➤➤   快速对比表:2026 年最佳数据移除服务 下表根据最重要的指标对所有五项服务进行了排名:自动化水平、经纪人数据库大小、按年计费的每月大致成本,以及我们经过六个月实际测试后的总体得分。 # 服务价格/月度最佳 自动化经纪人覆盖范围 我们的评分 🥇1 INCOGNI - 立即访问 ➤➤ 编辑推荐 自动化& 价值 ~$6.49 ✔ Full 180+ ★★★★★ 5.0 🥈2 DELETEME - 立即访问 ➤➤ 顶级支持 人力清除 ~$10.75 ✔ 混合动力 750多个 ★★★★★ 4.8 3 Optery 最透明 经核实的搬迁证明 ~$3.99 ✔ Full 200+ ★★★★½ 4.5 4 灵气 一体化 隐私 + AV + VPN 捆绑软件 ~$12.00 ✔ Full 100+ ★★★★ 4.0 5 隐私小蜜蜂 高级用户 粒状控制& 深度 ~$14.99 ✔ Full 150+ ★★★★ 4.0 *价格反映年度计划的大致月费。2026 年 5 月验证。 为什么 2026 年数据删除不再是可选的 2026 年的数字隐私环境甚至与五年前截然不同。您的个人信息——家庭住址、电话号码、家庭详细信息——已经从助长垃圾邮件的滋扰演变为人工智能欺诈的关键基础设施。这不是未来的威胁,而是正在发生的事情。 从定向广告到人工智能驱动的冒名顶替 十年前,数据经纪人对你的个人资料所能做的最糟糕的事情就是把它卖给电话推销员。如今,随着先进的生成式人工智能的广泛使用,相同的配置文件已成为语音克隆和深度伪造身份盗窃的蓝图。不良分子从寻人网站上获得你的详细履历后,就能构建超个性化的网络钓鱼活动,与你认识的人发送的真实通信无异。在2026年,隐私是人身安全的直接先决条件,而不仅仅是一种偏好。 "再曝光生命周期" :为什么一次移除申请永远不够 隐私界最危险的神话也许就是提交一次退出请求就能永久解决问题。数据中介平台的架构可持续重新抓取公共记录。即使成功删除,他们的自动爬网程序也会在 60 到 90 天内重新抓取您的数据。这种循环(我们称之为 Re-exposure Lifecycle )正是 Incogni 和 DeleteMe 等服务专注于 持续自动监控 而非一次性扫描的原因。持续压制是唯一真正有效的防御手段。 我们如何对每项服务进行测试和排名 本指南中的所有排名均基于六个月的独立测试,而不是新闻稿或未经验证的用户评论。这正是我们测量的结果: 📊 长期抑制 我们追踪了已删除的个人资料是否在整整六个月的时间内一直处于删除状态,对任何允许数据在不触发新的删除周期的情况下重新出现的服务进行处罚。 🔍 扫描频率 在 2026 年,提供近乎实时或每周监测的服务的排名明显高于按季度或按月扫描的服务,而按季度或按月扫描的服务是不够的。 📁 经纪人数据库覆盖范围 我们对数据经纪商的数量和质量都进行了审核,优先考虑高流量的人员搜索网站和营销数据聚合商,而不是模糊的低风险来源。 💻 用户体验& 透明度 我们评估了仪表板的清晰度、报告的详细程度,以及关键的一点,即每项服务是否提供了可核实的、有文件证明的证据,证明清除工作确实已经完成。 INCOGNI - 立即访问 ➤➤ 回顾 2026:最佳整体数据移除服务 🥇 Incogni - 综合排名第一 编辑推荐 2026 ★★★★★ 5.0 / 5.0 ~6.49 美元/月(年度账单) 🏚由冲浪鲨提供🌎 全球覆盖范围(GDPR + CCPA)📋 180+ 经纪人🔄 持续监测 Incogni 是我们 2026 年的头号选择,也是 市场上整体最佳的个人数据删除服务 。它由Surfshark VPN背后的同一个团队创建,旨在使您在GDPR和CCPA框架下行使删除权的法律程序自动化。设置需要几分钟:您授权Incogni代表您行事,该平台会向180多个数据经纪人发送具有法律约束力的选择退出请求,然后在您的数据重新出现时进行监测并自动重新提交。 Incogni 的独特优势在于 价格、自动化深度和国际影响力。年度计划的月费约为 6.49 美元,与我们测试过的任何竞争服务相比,它都能提供更高的性价比。仪表板简洁直观,进度报告易于解读,持续的再监测循环意味着您在初次扫描后绝不会失去保护--这正是打破再曝光生命周期所需的防御。 适合人群: 任何希望以最具竞争力的价格获得全自动、无需动手、全球法律覆盖的隐私解决方案的人。 ✅优点 市场上最优惠的价格(约 6.49 美元/月) 100% 自动化 - 无需人工操作 180 多个经纪人数据库,完全符合 GDPR 全球标准 持续重新监测和自动清除 简洁、直观的仪表板,可显示实时进度 以久负盛名的 Surfshark 品牌为后盾 ❌缺点 对异常复杂的案件不提供人力支持 经纪人数量少于 DeleteMe(180 对 750+) 手动定制选项有限 DELETEME - 立即访问 ➤➤ 2026 年回顾:最适合由人工引导的支持 🥈 DeleteMe - 综合排名第二 最佳人工引导服务 ★★★★★ 4.8 / 5.0 ~10.75 美元/月(年度账单) 🏚由 Abine 提供🇺🇸 以美国为重点 + 国际性📋 750 多名经纪人👥 人工+自动混合 DeleteMe 在纯自动化领域表现出色,因此排名第二。 750 多家数据经纪商的行业领先数据库,是我们测试过的所有服务中覆盖范围最广的。更重要的是,DeleteMe在其自动化系统之上运用了人工专业知识——一支由隐私专业人员组成的专用的团队负责处理经常忽略或拒绝自动退出的固执经纪人的删除请求。 如果您的情况比较复杂--一个非常普通的名字、多个地址的历史记录或在不知名的地区目录中出现的数据--DeleteMe 的管家式方法可确保万无一失。他们详细的季度报告提供了高度的文件透明度,家庭计划选项使其对家庭来说很实用。价格较高(~10.75 美元/月)对于需要专业级监督的用户来说,这反映了所涉及的人力劳动,是非常合理的。 适合人群: 有复杂隐私需求的用户,他们希望经纪人的覆盖面尽可能广,并保证由人工专家积极管理他们的搬迁。 ✅优点 业内最大的经纪人数据库:750 多个站点 人类隐私专家处理棘手的边缘案例 详细的季度报告,并将结果记录在案 历史悠久,业绩卓著(成立于 2010 年) 家庭计划选项可降低人均成本 ❌缺点 每月费用高于 Incogni(约 10.75 美元/月) 以季度为周期进行报告,而非实时报告 界面不如 Incogni 的仪表板精简 其他推荐服务:Optery、Aura& Privacy Bee Optery - 透明度最高(排名第 3) Optery 通过无与伦比的验证标准赢得了第 3 名的位置。在提交 移除请求 之前 ,其仪表板为用户提供了指向其公开个人资料的直接链接,并且它是我们测试的唯一一项提供 基于屏幕截图的证据以 证明 每项删除都已完成的服务。它的起价约为 3.99 美元/月,也是本列表中最经济实惠的选择--对于注重预算、拒绝信口开河的用户来说,这是一个令人信服的选择。其主要局限性在于,其团队和后续行动的积极性还无法与 Incogni 或 DeleteMe 相提并论。 Aura — 最佳多合一网络安全套件(排名 #4) 对于想要将其整个数字网络安全堆栈整合到单个订阅中的用户来说,Aura是正确的答案。它的价格约为每月12美元,将自动数据删除与防病毒保护、VPN和信用监控捆绑到一个统一的平台中,特别适合家庭使用。该移除工具本身是全自动和有效的,不过其中介数据库中的 100 多个网站明显少于我们的前两个选择。 隐私蜂 - 最适合高级用户(排名第 5 位) Privacy Bee 专为痴迷于隐私的用户而打造,他们希望对其数字足迹进行精细的外科控制。它的价格约为 14.99 美元/月,是本列表中最昂贵的选项,但它提供了最深入的自定义选项--你可以优先处理特定的经纪人类别、锁定特定的数据类型,并精确配置删除计划。同样的复杂性也使它不太适合那些只想不假思索地解决问题的普通用户。 Incogni vs DeleteMe:您应该选择哪个? 这是个人数据删除中最常被问到的问题,因此这里有一个直接、简单的答案: 如果您需要最优惠的价格、完全端到端自动化、全球 GDPR 和 CCPA 覆盖范围,以及无需持续工作的仪表板,请选择 Incogni 。这对绝大多数用户来说都是正确的选择。 如果您的隐私情况确实非常复杂,需要尽可能广泛的经纪人数据库(750 多个),或者需要专业人员积极管理和验证您的案例,请选择 DeleteMe 。 这两项服务都包括持续的重新监测--这在 2026 年是不可谈判的。与手动删除或不作为相比,这两种方法都能提供更好的长期保护。 数据删除之外:建立完整的隐私战略 暗网监控和信用跟踪 数据删除可以解决一个关键的暴露载体,但它本身并不是一个完整的网络安全解决方案。暗网监控增加了重要的第二层:如果您的凭证出现在泄露中,则需要立即发出警报,而不是延迟发现。如果有人试图以你的名义开立账户或进行交易,你会立即收到通知。 密码管理和多因素身份验证 密码泄露会破坏你为保护隐私所做的一切。专用的密码管理器可确保您在每项服务中维护独特、复杂的凭据,从而消除单一密码失败的风险。在任何可用的地方启用多因素身份验证,并尽可能使用身份验证器应用程序而不是短信;基于 SMS 的 MFA 容易受到 SIM 交换攻击,适当的身份验证器应用程序可以防止这种攻击。 设备级安全:防病毒和指纹拦截器 您的本地设备是最后的边界。2026 年强大的防病毒软件不是可选的——现代恶意软件旨在以静默方式收集文件、凭据和行为数据。与此相辅相成的浏览器扩展程序可以主动屏蔽第三方跟踪器并抵制指纹识别,通过这种技术,数据经纪人可以根据浏览器配置和浏览模式建立您的详细档案,完全不使用 cookie。 2026 年您的法律权利:CCPA、GDPR 以及服务如何使用这些权利 CCPA 和不断扩大的美国隐私框架 《加州消费者隐私法》及其随后的修正案赋予了美国消费者要求数据经纪人删除其个人信息的法律强制执行的权利。截至 2026 年,对违规行为的处罚已变得更加具体,选择退出的基础设施也已成熟。 Incogni 和 DeleteMe 等服务作为法定代理人代表你行事--他们利用你的消费者权利提交具有约束力的退出请求,迫使经纪商在监管处罚的威胁下清除你的记录。 GDPR:全球数据权利标准 对于欧盟或英国的用户来说,《通用数据保护条例》仍然是最有力的隐私保护工具。GDPR 的 "删除权 "对任何处理欧盟居民数据的组织都规定了严格的义务。Incogni 由 Surfshark 背后的欧洲团队开发,专门围绕 GDPR 合规性进行架构设计,使其能够向全球范围内的经纪商提出可强制执行的删除请求,这对国际用户尤为重要。 DIY 方法:如何在不使用付费服务的情况下删除数据 零预算也可以手动删除数据,但需要投入大量时间和持续的纪律。基本流程: 在主要的寻人网站上搜索你的全名、城市和州:Spokeo、Whitepages、BeenVerified、Intelius 和 MyLife 是最优先的起始点。 找到每个网站的退出页面或"Do Not Sell My Personal Information" 页面--通常埋藏在网站页脚的 "隐私政策 "下。 完成每个退出工作流程,并保存确认电子邮件作为记录证据。 安排日历提醒,每三到四个月重复一次整个过程,因为重新刮擦会在固定的周期内撤销你的清除。 对于大多数人来说,手动删除的时间成本使得像 Incogni 这样每月约 6.49 美元的服务 成为显而易见的经济选择。也就是说,如果你的风险状况确实很低,并且你对系统化流程有耐心,那么在投资自动化之前,手动优先的方法可以作为有用的基础。 准备好从互联网上删除您的个人数据了吗? 停止暴露你的数字足迹。从我们的顶级服务开始,今天就重新掌控您的个人信息。 ↑ 比较以上所有服务 常见问题 2026 年最好的数据移除服务是什么? Incogni 是我们 2026 年排名第一的数据移除服务--因其集完全自动化、全球法律覆盖面和高级层最低价格(约 6.49 美元/月)于一身而综合排名第一。 DeleteMe 排名第二,是情况复杂、希望由专业人员管理案件的用户的更佳选择。   2026 年 Incogni 的成本是多少? Incogni 的年度计划费用约为 6.49美元/月 (约 77.88 美元/年)。也可选择按月付费,但费用较高。因此,它是目前市场上最具成本效益的高级数据删除服务。   2026 年 DeleteMe 的成本是多少? DeleteMe 的年度计划费用约为 ,每月10.75美元 (每年约 129 美元)。家庭计划可用,在涵盖多个家庭成员时,可以显著降低人均成本。   数据删除服务真的有效吗? 是的,但前提是必须包括持续的再监测。数据经纪商每隔 60 到 90 天就会重新抓取公共记录,因此一次性删除请求无效。像 Incogni 和 DeleteMe 这样的服务可以自动完成整个周期,利用 GDPR 和 CCPA 框架持续压制您的数据。我们为期 6 个月的测试证实,在所有排名靠前的服务中,暴露量都有可衡量的持续减少。   Incogni 比 DeleteMe 更好吗? 对大多数用户来说,是的,Incogni 提供了一个卓越的价值主张:完全自动化、价格更低和全球法律覆盖范围。DeleteMe 是以下用户的更佳选择:需要处理真正复杂案件的用户、需要尽可能广泛的经纪人数据库(750 多个对 180 多个)的用户,或者特别希望由专业人员验证其移除行为而不是仅仅依赖自动化的用户。   我可以免费从数据经纪商那里删除我的数据吗? 是的,大多数数据经纪商都提供免费的退出页面,而且可以免费手动删除。这样做的代价是巨大的:这个过程耗费时间,每隔几个月就必须重复一次,而且需要跟踪几十个经纪人。对于持续的自动保护, Incogni对大多数人来说是一种实用的升级。对于预算紧张的低风险个人来说,DIY 方法最适合作为免费的起点。   重新掌控您的数字足迹 2026 年的数据经纪人经济是无情的。您的个人信息不断被收集、打包和出售,如果落入坏人之手,则会成为人工智能欺诈、社会工程和身份盗窃的原材料。等待不是一种中立的选择,而是一种继续暴露的决定。 经过 6 个月的严格独立测试, Incogni 赢得了我们无条件的最高推荐:最具价值、最无缝的自动化和真正的全球覆盖。 DeleteMe 是您需要最广泛的经纪人覆盖范围和人类专业知识保证时的正确选择。这两项服务直接抵消了 "再曝光生命周期 "的影响,使一次性清除工作在几个月内就会过时。 无论您开始使用哪种服务,都可以在其基础上构建:强大的唯一密码、多因素身份验证和设备级安全性构成了 2026 年所需的完整深度防御方法。您的隐私不是一次性配置的设置,而是一种持续的实践。从今天开始 Re: Best Personal Data Removal Services of 2026: Independently Tested and Compared @Mentorstgf快速结论 经过六个月的实际独立测试, Incogni排名第一 全自动移除服务,性价比一流,价格约为 每月约 6.49 美元。 隐身模式 — 立即访问 ➤➤   DeleteMe 排名第二 以人为本的礼宾服务方式和业内领先的750多家经纪公司覆盖范围而闻名。这两项服务都包含持续再监控功能——这是 2026 年最关键的功能。 DELETEME — 立即访问 ➤➤   快速对比表:2026 年最佳数据移除服务 下表根据最重要的指标对所有五项服务进行了排名:自动化水平、经纪人数据库大小、按年计费的每月大致成本,以及我们经过六个月实际测试后的总体得分。 对于任何想要减少其在线足迹的人来说,这都是一个有用的比较——尤其值得关注的是持续监控和重新删除,而不是依赖一次性选择退出。为期六个月的测试方法也使得自动化服务和人工主导的服务之间的差异更容易理解。
記事全体を表示
secure_provisioning工具烧写sb格式加密签名文件后无法使用mcu链接调试 使用 Secure Provisioning 工具刷写 SB 格式加密签名文件后,将无法再通过 MCU-Link 进行调试。 justdomyself_0-1790073326861.png justdomyself_1-1790073357176.png 当我使用mcuexpress调试代码时,出现错误: justdomyself_2-1790073419631.png 我的开发板可以恢复到之前的状态以使用调试功能吗? Re: secure_provisioning 工具烧写 sb格式 加密签名文件后无法用mcu link debug 嗨@justdomyself > 那么,我可以使用安全提供工具来生成新的许可证,并将新的已签名和加密的 sb 格式文件写入芯片吗? 是的,安全配置工具旨在配置芯片,即安装安全资产(密钥),构建签名或加密的应用程序可启动映像并将其安装到闪存中。 Re: secure_provisioning 工具烧写 sb格式 加密签名文件后无法用mcu link debug @liborukropec非常感谢。我的问题已经解决了。 justdomyself_0-1790128360736.png 我还有个问题: 如上图所示,此擦除操作已将存储芯片上的所有数据擦除干净。 那么,我可以使用安全提供工具来生成新的许可证,并将新的已签名和加密的 sb 格式文件写入芯片吗? Re: secure_provisioning 工具烧写 sb格式 加密签名文件后无法用mcu link debug 您好, 如果将 ROM 配置为仅执行已签名映像,然后从 VSCode(或其他 IDE)编写未签名映像的应用程序,则 ROM 将拒绝运行。 此外,如果推进生命周期,则只能通过调试身份验证打开调试器(请参阅文档)。 如果您没有推进生命周期(在工具栏上),您应该能够删除 CMPA。最简单的办法是使用调试探针,然后在“写入”选项卡上使用“擦除整个芯片...”按钮。 liborukropec_0-1790086908628.png 重启电源后,您应该可以再次进行调试。 此致, 伦敦银行间同业拆借利率 (Libor)
記事全体を表示