i.MX8MP_EVK: YOCTO Compilation Error do_package() (Issue: tar & *at()) Hi, These are my yocto build parameters: Release: imx-linux-walnascar BSP Version: imx-6.12.49-2.2.0 MACHINE: imx8mpevk DISTRO: fsl-imx-xwayland I have been using this build environment successfully for the past couple of months. However, I suddenly started encountering the attached error. To troubleshoot, I completely cleaned the build environment, reinitialized the repository (repo init), synced everything again, and performed a fresh build. Unfortunately, I am still facing the same issue. Please find the attached log file for your reference. I would appreciate your help in identifying the root cause and suggesting a solution. i.MX 8M | i.MX 8M Mini | i.MX 8M Nano Re: i.MX8MP_EVK: YOCTO Compilation Error do_package() (Issue: tar & *at()) bitbake imx-image-core Re: i.MX8MP_EVK: YOCTO Compilation Error do_package() (Issue: tar & *at()) What "bitbake command" are you using?
I will do verification. Re: i.MX8MP_EVK: YOCTO Compilation Error do_package() (Issue: tar & *at()) Thank you for your response. I verified my build environment, and it already matches the configuration you recommended. Host OS: Ubuntu 22.04.5 LTS (Jammy) GNU tar version: GNU tar 1.34 $ cat /etc/os-release PRETTY_NAME="Ubuntu 22.04.5 LTS" ... $ tar --version tar (GNU tar) 1.34 However, I still encounter the same failure Re: i.MX8MP_EVK: YOCTO Compilation Error do_package() (Issue: tar & *at()) Please check the tar version, if the host is Ubuntu 24.04 and tar is 1.35
Build inside a container or VM with:
Ubuntu 22.04 LTS
GNU tar 1.34
Re: i.MX8MP_EVK: YOCTO Compilation Error do_package() (Issue: tar & *at()) Please find file below, Here i am pasting the some lines of error DEBUG: Executing python function extend_recipe_sysroot NOTE: Direct dependencies are ['/home/vvdn/LWT_Build/sources/poky/meta/recipes-devtools/binutils/binutils-cross_2.44.bb:do_populate_sysroot', '/home/vvdn/LWT_Build/sources/poky/meta/recipes-devtools/gcc/gcc-cross_14.3.bb:do_populate_sysroot', '/home/vvdn/LWT_Build/sources/poky/meta/recipes-devtools/quilt/quilt-native_0.68.bb:do_populate_sysroot', '/home/vvdn/LWT_Build/sources/poky/meta/recipes-kernel/kern-tools/kern-tools-native_git.bb:do_populate_sysroot', 'virtual:native:/home/vvdn/LWT_Build/sources/poky/meta/recipes-core/coreutils/coreutils_9.6.bb:do_populate_sysroot', 'virtual:native:/home/vvdn/LWT_Build/sources/poky/meta/recipes-devtools/bison/bison_3.8.2.bb:do_populate_sysroot', 'virtual:native:/home/vvdn/LWT_Build/sources/poky/meta/recipes-devtools/dwarfsrcfiles/dwarfsrcfiles.bb:do_populate_sysroot', 'virtual:native:/home/vvdn/LWT_Build/sources/poky/meta/recipes-devtools/flex/flex_2.6.4.bb:do_populate_sysroot', 'virtual:native:/home/vvdn/LWT_Build/sources/poky/meta/recipes-devtools/patch/patch_2.7.6.bb:do_populate_sysroot', 'virtual:native:/home/vvdn/LWT_Build/sources/poky/meta/recipes-devtools/pkgconfig/pkgconfig_git.bb:do_populate_sysroot', 'virtual:native:/home/vvdn/LWT_Build/sources/poky/meta/recipes-devtools/pseudo/pseudo_git.bb:do_populate_sysroot', 'virtual:native:/home/vvdn/LWT_Build/sources/poky/meta/recipes-devtools/rpm/rpm_4.20.0.bb:do_populate_sysroot', 'virtual:native:/home/vvdn/LWT_Build/sources/poky/meta/recipes-extended/bc/bc_1.08.1.bb:do_populate_sysroot', 'virtual:native:/home/vvdn/LWT_Build/sources/poky/meta/recipes-kernel/kmod/kmod_34.1.bb:do_populate_sysroot'] NOTE: Installed into sysroot: [] NOTE: Skipping as already exists in sysroot: ['gettext-minimal-native', 'binutils-cross-aarch64', 'cmake-native', 'gcc-cross-aarch64', 'libtool-native', 'm4-native', 'quilt-native', 'texinfo-dummy-native', 'kern-tools-native', 'linux-libc-headers', 'file-native', 'openssl-native', 'coreutils-native', 'expat-native', 'ncurses-native', 'readline-native', 'util-linux-libuuid-native', 'zlib-native', 'bison-native', 'dwarfsrcfiles-native', 'elfutils-native', 'flex-native', 'git-native', 'gnu-config-native', 'json-c-native', 'libedit-native', 'lua-native', 'make-native', 'patch-native', 'perl-native', 'pkgconfig-native', 'pseudo-native', 'python3-native', 'rpm-native', 'bc-native', 'bzip2-native', 'libarchive-native', 'libidn2-native', 'lzlib-native', 'xz-native', 'zstd-native', 'kmod-native', 'acl-native', 'attr-native', 'curl-native', 'gdbm-native', 'gmp-native', 'gnutls-native', 'libtasn1-native', 'libcap-native', 'libffi-native', 'libgcrypt-native', 'libgpg-error-native', 'libmicrohttpd-native', 'libmpc-native', 'libunistring-native', 'mpfr-native', 'nettle-native', 'p11-kit-native', 'popt-native', 'sqlite3-native'] DEBUG: Python function extend_recipe_sysroot finished DEBUG: Executing python function sstate_task_prefunc DEBUG: Python function sstate_task_prefunc finished DEBUG: Executing python function do_package DEBUG: Executing python function package_setup_pkgv DEBUG: Python function package_setup_pkgv finished DEBUG: Executing python function package_convert_pr_autoinc DEBUG: Python function package_convert_pr_autoinc finished DEBUG: Executing python function package_prepare_pkgdata NOTE: Installed into pkgdata-sysroot: [] DEBUG: Python function package_prepare_pkgdata finished DEBUG: Executing python function perform_packagecopy ERROR: Error executing a python function in exec_func_python() autogenerated: The stack trace of python calls that resulted in this exception/failure was: File: 'exec_func_python() autogenerated', lineno: 2, function: 0001: *** 0002:perform_packagecopy(d) 0003: File: '/home/vvdn/LWT_Build/sources/poky/meta/classes-global/package.bbclass', lineno: 363, function: perform_packagecopy 0359: rpath_replace (dvar, d) 0360:} 0361:perform_packagecopy[cleandirs] = "${PKGD}" 0362:perform_packagecopy[dirs] = "${PKGD}" *** 0363: 0364:python populate_packages () { 0365: oe.package.populate_packages(d) 0366:} 0367:populate_packages[dirs] = "${D}" File: '/usr/lib/python3.10/subprocess.py', lineno: 421, function: check_output 0417: else: 0418: empty = b'' 0419: kwargs['input'] = empty 0420: *** 0421: return run(*popenargs, stdout=PIPE, timeout=timeout, check=True, 0422: **kwargs).stdout 0423: 0424: 0425:class CompletedProcess(object): File: '/usr/lib/python3.10/subprocess.py', lineno: 526, function: run 0522: # We don't call process.wait() as .__exit__ does that for us. 0523: raise 0524: retcode = process.poll() 0525: if check and retcode: *** 0526: raise CalledProcessError(retcode, process.args, 0527: output=stdout, stderr=stderr) 0528: return CompletedProcess(process.args, retcode, stdout, stderr) 0529: 0530: Exception: subprocess.CalledProcessError: Command 'tar --exclude=./sysroot-only -cf - -C /home/vvdn/LWT_Build/build/tmp/work/imx8mpevk-poky-linux/linux-imx/6.12.34+git/image -p -S . | tar -xf - -C /home/vvdn/LWT_Build/build/tmp/work/imx8mpevk-poky-linux/linux-imx/6.12.34+git/package' returned non-zero exit status 2. Subprocess output: got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path lib couldn't allocate absolute path for 'lib'. tar: ./usr/lib: Cannot mkdir: Bad address got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path lib couldn't allocate absolute path for 'lib'. got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path lib couldn't allocate absolute path for 'lib'. tar: ./usr/lib: Cannot mkdir: Bad address tar: ./usr/lib/modules: Cannot mkdir: No such file or directory Re: i.MX8MP_EVK: YOCTO Compilation Error do_package() (Issue: tar & *at()) It seems that I don't have the permission to download the attachment.
Would you please resend it again? Re: i.MX8MP_EVK: YOCTO Compilation Error do_package() (Issue: tar & *at()) Hi @yipingwang Awaiting for your prompt support in further debugging. Re: i.MX8MP_EVK: YOCTO Compilation Error do_package() (Issue: tar & *at()) On your ubuntu PC, use the command "sudo apt install tar=1.34+dfsg-1build3" Re: i.MX8MP_EVK: YOCTO Compilation Error do_package() (Issue: tar & *at()) @Sanjiv_MnsDid this resolve the issue ? Re: i.MX8MP_EVK: YOCTO Compilation Error do_package() (Issue: tar & *at()) Hi @abannish Please try below commands this works for me... wget http://archive.ubuntu.com/ubuntu/pool/main/t/tar/tar_1.34+dfsg-1build3_amd64.deb sudo dpkg -i tar_1.34+dfsg-1build3_amd64.deb sudo apt-mark hold tar Re: i.MX8MP_EVK: YOCTO Compilation Error do_package() (Issue: tar & *at()) Thanks! That solved the issue also in my side! FYI, everything worked perfectly until some autoupdate from the Ubuntu service...
查看全文