Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
S32DS 3.5 activation failed – no remaining activations, request reset Hello, I am trying to activate S32 Design Studio for S32 Platform v3.5 on my new Windows PC, but activation fails with an error saying there are no remaining activations. I previously activated it on a virtual machine (Parallels on Mac), but I have already deleted that VM, so I cannot return the license from it. Could you please reset the activation count for my activation code or issue a new activation code? Product: S32 Design Studio for S32 Platform v3.5 Windows 11 I can send the full activation code via private message if needed. Thank you. Re: S32DS 3.5 activation failed – no remaining activations, request reset Hello, Please try now. It should be working. Best regards, Peter
View full article
i.MX95:推荐的 电路板支持包 / Neutron SDK 版本控制策略 (LF_6.18.20_2.0.0) 你好, 我们正在使用 i.MX95 作为平台开发汽车应用的 PoC,并希望明确推荐的 电路板支持包 和 Neutron SDK 版本策略。 我们已经阅读了 NeutronSDKUserGuide.md 中的“Neutron SDK 版本与 Yocto 电路板支持包的兼容性”表格,并了解到编译器和运行时必须来自同一个 SDK。但是,该指南并未说明推荐哪个版本。 您能帮我们理解一下吗? 1.我们应该始终在当前的 电路板支持包。 上使用最新的 Neutron SDK 版本(运行时已升级),还是应该使用该 电路板支持包。 的默认 SDK 版本? 2. 当有新的 电路板支持包。 版本发布时,建议从我们当前的 电路板支持包。 版本升级,还是应该保留当前版本,除非有必要升级? 环境 - 板:IMX95LPD5EVK-19 - 电路板支持包:LF_6.18.20_2.0.0 - Neutron SDK:eiq-neutron-sdk-linux-3.2.3 - NeutronFirmware.elf、libNeutronDriver.so 和 libneutron_delegate.so 已更新至 Neutron SDK 3.2.3 的版本。 谢谢!
View full article
Regarding Flash Programming for the FRDM-A-S32K144N I was debugging using the FRDM-A-S32K144N when the following symptoms occurred: * Unable to write to flash memory. * Since the write failure, the power LED and reset LED have remained constantly lit. I attempted recovery by performing the following steps: 1. Tried writing to the flash memory by unplugging and replugging the USB cable while holding down the reset button, aiming to catch the window before the infinite loop started. * Attempted this dozens of times but was unsuccessful. 2. Connected the USB cable while holding down the reset button to enter bootloader mode. * Flashed "BOOTUPDATEAPP_Pemicro_v111.SDA". * Then flashed "MSD-DEBUG-EVB-S32K144_PEmicro_v125.SDA". * The situation did not improve. 3. Attempted flash recovery using "Kinetis_Recovery_Utility.exe". * Unplugged and replugged the USB cable several times, but the process did not complete. I am unsure what to try next. If anyone knows how to restore the board, could you please advise me on the procedure? Re: Regarding Flash Programming for the FRDM-A-S32K144N Hi Fukuda, I don't have the newly released FRDM-A-S32K144N development board on hand, so I haven't tested it myself. If you aren't in a rush, I can help you troubleshoot the issue now, and then perform tests on my end once I receive the board—which I expect to arrive in mid-October. After plugging the cable into the J1 USB Type-C port, please take a photo of the top side of the board and share it with me. I am not sure which two LEDs you are referring to, as the SPF-96556_B.pdf document only lists D5 (Red) and D4 (Orange). If D4 is lit, it indicates that the onboard OpenSDA debugger is functioning correctly. However, if D5 is lit, it indicates that the S32K144N is in a reset state (The RESET_MCU signal may go low); please use an oscilloscope to observe the signal and check for the frequency of periodic low pulses.  Additionally, I am unsure what program was previously flashed onto the S32K144N. If it is a blank chip and the RESET_MCU signal shows periodic high-level pulses with a period of ~118µs, you can recover the MCU by executing a "mass erase" command via the SWD/JTAG debug interface. Since the onboard debugger is provided by PEMicro, it is recommended to download the latest "USB Multilink Resources Installer" from the "Support & Downloads" category of the "Multilink Debug Probes". After installation, open PEFirmwareConfig.exe located in C:\PEMicro\Multilink_Resources to check the firmware version. Select Hardware Type: Multilink ACP Embedded - OnBoard ARM Debug Interface  Then, check for available updates. It appears you have already refer to the discussion "S32K144 D2 RED LED is ON always". Please note that the Kinetis_Recovery_Utility (Version 8.17) previously provided on the PEMicro website did not work correctly; the Kinetis_Recovery_Utility (Version 1.06)—which I uploaded as an attachment in that discussion—works properly. When using the Kinetis_Recovery_Utility, It is recommended to keep the PEMicro debugger powered on and repeatedly power-cycle reset only the S32K chip. If you have an external debugger like the Multilink connected to the J3, you can repeatedly plug and unplug J1 to cycle power to the S32K144N while keeping the external Multilink active. However, if you do not have an external Multilink and are relying solely on the onboard OpenSDA debugger, the design of the FRDM-A-S32K144N presents some inconvenience. Jumper SJ10 is not as convenient as J107 on the S32K144EVB for repeatedly cycling power to the S32K144. I am not certain whether repeatedly pressing SW2 alone would allow the Kinetis_Recovery_Utility to successfully halt the S32K144N at the right moment. Best Regards, Robin Re: Regarding Flash Programming for the FRDM-A-S32K144N Hi, Robin. I apologize for the significant delay in my reply. I have attached a photo of the board to this post. Unfortunately, I do not own an oscilloscope, so I was unable to verify the frequency. I tried using PEFirmwareConfig.exe, but the FRDM-A-S32K144N did not appear in the device list; I will continue to look into this. I will also continue attempting to use the Kinetis_Recovery_Utility. I apologize for the lack of significant progress since my last post. Best Regards, Fukuda Re: Regarding Flash Programming for the FRDM-A-S32K144N Hi Fukuda, Thank you for your update, and no worries about the delayed response. I just returned from vacation. Unfortunately, the FRDM-A-S32K144N board I ordered has not arrived yet, so I am currently unable to perform any testing. Although I haven't received the FRDM-A-S32K144N yet, I tested the onboard debugger using the FRDM-A-S32K344: PEFirmwareConfig.exe successfully detects the onboard debugger, as shown in the image: Unfortunately, Kinetis_Recovery_Utility (Version 1.06)—the version capable of successfully halting the MCU—does not detect the FRDM-A-S32K344's onboard debugger. While Kinetis_Recovery_Utility (Version 8.17) does detect the FRDM-A-S32K344's onboard debugger, it fails to halt the MCU, as I mentioned previously. Please wait while I consult PEMicro technical support regarding the issues currently encountered with Kinetis_Recovery_Utility. Do you happen to have an external PEMicro debugger, such as a Multilink Debug Probe? I recall that Kinetis_Recovery_Utility (Version 1.06) can be used with external Multilink Debug Probe. Additionally, have you tried the "Emergency Kinetis Device Recovery by Full Chip Erase" feature in S32DS that I mentioned in the "S32K144 D2 RED LED is ON always" thread? Re: Regarding Flash Programming for the FRDM-A-S32K144N Also, have you tried the workaround mentioned in "Solution to FRDM-A-S32K144 and FRDM-A-S32K144N not detected during initial USB-C connection"? Even though I see the orange D4 LED is lit on your FRDM-A-S32K144N board, I still suggest trying the other workarounds. This is because the FRDM-A-S32K144N I ordered isn't expected to arrive until next week for testing. Re: Regarding Flash Programming for the FRDM-A-S32K144N I just received the FRDM-A-S32K144N and tested it. Bearing in mind the issue mentioned in "Solution to FRDM-A-S32K144 and FRDM-A-S32K144N not detected during initial USB-C connection" I used a USB-A to USB-C data cable. PEFirmwareConfig.exe did not detect any Multilink hardware. This differs from the test results for the FRDM-A-S32K344; I apologize for misleading you earlier. The D4 LED is lit orange, indicating the OpenSDA status is normal, and the device appears in Device Manager. In Kinetis_Recovery_Utility (Version 1.06), selecting "Show Hardware" and clicking "START" reveals the OpenSDA device. After selecting the OpenSDAUSB device and clicking "START," the following appears: Communication via SWD Cable Version is 119 Continuously attempting to halt processor. Please try power cycling your board until this operation is successful Success. Processor halted. Re: Regarding Flash Programming for the FRDM-A-S32K144N Hi, Robin. Thank you for your reply. Unfortunately, I do not own an external PEMicro debugger. I have also tried the "Emergency Kinetis Device Recovery by Full Chip Erase" function in S32DS multiple times, but all attempts failed. Since the FRDM-A-S32K144N is recognized by the PC, I have not tried the "Solution for when FRDM-A-S32K144 and FRDM-A-S32K144N are not detected via USB-C connection." Just to clarify, does "power ON/OFF" in the Kinetis_Recovery_Utility refer to unplugging and replugging the USB cable? Even after unplugging and replugging the USB cable, the process did not proceed past the message: "Please try power cycling your board until this operation is successful." Best Regards, Fukuda Re: Regarding Flash Programming for the FRDM-A-S32K144N I connected an external J-Link Plus to the onboard S32K144N via J3 and erased the chip using the `unlock kinetis` command in J-Link Commander. Now, observing the J9.5 RESET_MCU pin with an oscilloscope, I see a square wave signal with a period of approximately 120 µs and a high-level duration of about 660 ns. Regardless of whether I hold down SW2, the onboard OpenSDA, in conjunction with Kinetis_Recovery_Utility (Version 1.06), successfully halted the MCU: At this point, the periodic pulses on the J9.5 RESET_MCU pin stop; after closing Kinetis_Recovery_Utility, the new program can be downloaded within S32DS v3.6.11. Have you previously programmed the S32K144N? Are you using a USB-A to USB-C data cable?
View full article
i.MX95: Recommended BSP / Neutron SDK versioning strategy (LF_6.18.20_2.0.0) Hello, We are developing a PoC for an automotive application using the i.MX95 as our platform and would like to clarify the recommended BSP and Neutron SDK versioning strategy. We have read the "Neutron SDK Version Compatibility with Yocto BSP" table in NeutronSDKUserGuide.md and understand that the compiler and runtime must come from the same SDK. However, the guide does not say which version is recommended. Could you help us understand: 1. Should we always use the latest Neutron SDK version (with the runtime upgraded) on our current BSP, or should we use the SDK version that is Default for that BSP? 2. When a new BSP release becomes available, is it recommended to upgrade from our current BSP, or should we keep the current version unless an upgrade is necessary? Environment - Board: IMX95LPD5EVK-19 - BSP: LF_6.18.20_2.0.0 - Neutron SDK: eiq-neutron-sdk-linux-3.2.3 - NeutronFirmware.elf, libNeutronDriver.so, and libneutron_delegate.so have been updated to the versions from Neutron SDK 3.2.3. Thank you!
View full article
关于 FRDM-A-S32K144N 的闪存编程 我在使用 FRDM-A-S32K144N 进行调试时,出现了以下症状: 无法写入闪存。 * 自写入失败以来,电源指示灯和RESET指示灯一直亮着。 我尝试通过以下步骤进行恢复: 1. 尝试通过拔下并重新插入 USB 电缆,同时按住重置按钮,向闪存写入数据,目的是在无限循环开始之前抓住这个机会。 * 尝试了几十次,但都失败了。 2. 按住重置按钮,同时连接 USB 数据线,进入引导加载程序模式。 * 已刷写“BOOTUPDATEAPP_Pemicro_v111.SDA”。 然后刷入“MSD-DEBUG-EVB-S32K144_PEmicro_v125.SDA”。 情况并未好转。 3. 尝试使用“Kinetis_Recovery_Utility.exe”进行闪存恢复。 * 多次拔下并重新插上 USB 数据线,但该过程仍未完成。 我不知道接下来该尝试什么。 如果有人知道如何修复主板,能否请您指导一下步骤? Re: Regarding Flash Programming for the FRDM-A-S32K144N 嗨福田, 我手头没有新发布的 FRDM-A-S32K144N 开发板,所以我自己还没有测试过。如果您不着急,我现在可以帮您排查问题,然后在我收到主板后(预计10月中旬到货)再进行测试。 将数据线插入J1 USB Type-C 接口后,请拍摄主板正面的照片并与我分享。 我不确定您指的是哪两个 LED,因为 SPF-96556_B.pdf 文档只列出了D5 (红色)和D4 (橙色)。 如果D4亮起,则表示板载OpenSDA调试器运行正常。但是,如果D5亮起,则表示 S32K144N 处于 RESET 状态( RESET_MCU信号可能变为低电平);请使用示波器观察信号并检查周期性低脉冲的频率。 此外,我不确定之前在S32K144N上刷入的是什么程序。如果芯片是空白的,并且RESET_MCU信号显示周期约为 118µs 的周期性高电平脉冲,则可以通过 SWD/JTAG 调试接口执行“批量擦除”命令来恢复 MCU。 由于板载调试器由 PEMicro 提供,建议 从“ 多链路调试探针”的“支持与下载”类别 下载最新的“ USB 多链路资源安装程序” 。安装完成后,打开 位于 C:\PEMicro\Multilink_Resources 的 PEFirmwareConfig.exe 文件 以检查固件版本。选择硬件类型: Multilink ACP Embedded - OnBoard ARM Debug Interface然后,检查是否有可用更新。 看来您已经参考了“ S32K144 D2 红色 LED 始终亮着”的讨论。请注意,之前在 PEMicro 网站上提供的Kinetis_Recovery_Utility (版本8.17 )无法正常工作; Kinetis_Recovery_Utility (版本1.06 )——我已将其作为附件上传到该讨论中——运行正常。 使用Kinetis_Recovery_Utility时,建议保持 PEMicro 调试器通电,并反复对 S32K 芯片进行断电重启复位。 如果您有像Multilink这样的外部调试器连接到J3 ,您可以反复插拔J1来循环给S32K144N供电,同时保持外部Multilink处于活动状态。 但是,如果您没有外部Multilink ,并且仅依赖板载OpenSDA调试器,则 FRDM-A-S32K144N的设计会带来一些不便。对于S32K144EVB来说,跳线SJ10不如J107方便,可以反复循环给 S32K144 供电。我不确定单独反复按下SW2是否能让Kinetis_Recovery_Utility在正确的时间成功停止 S32K144N。 此致, 罗宾 Re: Regarding Flash Programming for the FRDM-A-S32K144N 你好,罗宾。 对于回复延迟如此之久,我深表歉意。 我已将电路板的照片附在此帖中。 遗憾的是,我没有示波器,所以无法验证频率。 我尝试使用 PEFirmwareConfig.exe,但是 FRDM-A-S32K144N 没有出现在设备列表中;我会继续调查此事。 我也会继续尝试使用 Kinetis_Recovery_Utility。 很抱歉,自上次发帖以来,并没有取得实质性进展。 此致, 福田 Re: Regarding Flash Programming for the FRDM-A-S32K144N 另外,您是否尝试过“解决 FRDM-A-S32K144 和 FRDM-A-S32K144N 在初始 USB-C 连接期间无法检测到的问题”中提到的解决方法?即使我看到你的FRDM-A-S32K144N板上的橙色 D4 LED 亮起,我仍然建议你尝试其他解决方法。这是因为我订购的FRDM-A-S32K144N预计要到下周才能到货进行测试。 Re: Regarding Flash Programming for the FRDM-A-S32K144N 嗨福田, 感谢您的更新,回复延迟无需担心。 我刚度假回来。很遗憾,我订购的FRDM-A-S32K144N板还没有到货,所以我目前无法进行任何测试。 虽然我还没有收到FRDM-A-S32K144N ,但我已经使用FRDM-A-S32K344测试了板载调试器: PEFirmwareConfig.exe成功检测到板载调试器,如图所示: 遗憾的是,能够成功停止 MCU 的Kinetis_Recovery_Utility (版本 1.06)无法检测到 FRDM-A-S32K344 的板载调试器。 虽然Kinetis_Recovery_Utility (版本 8.17)确实检测到了 FRDM-A-S32K344 的板载调试器,但它无法停止 MCU,正如我之前提到的那样。 请稍候,我正在咨询 PEMicro 技术支持,了解目前Kinetis_Recovery_Utility遇到的问题。 您手头是否有外部 PEMicro 调试器,例如Multilink Debug Probe ?我记得Kinetis_Recovery_Utility (版本 1.06)可以与外部Multilink Debug Probe一起使用。 另外,您是否尝试过我在“ S32K144 D2 红色 LED 常亮”主题中提到的 S32DS 中的“ 通过完全芯片擦除进行紧急 Kinetis 设备恢复”功能? Re: Regarding Flash Programming for the FRDM-A-S32K144N 我刚收到FRDM-A-S32K144N并进行了测试。 考虑到“ FRDM-A-S32K144 和 FRDM-A-S32K144N 在初始 USB-C 连接期间无法检测到的解决方案”中提到的问题,我使用了USB-A 转 USB-C 数据线。 PEFirmwareConfig.exe未检测到任何Multilink硬件。这与FRDM-A-S32K344的测试结果不同;对于之前误导您,我深表歉意。 D4 LED 亮起橙色,表示OpenSDA状态正常,并且该设备出现在设备管理器中。 在Kinetis_Recovery_Utility (版本 1.06)中,选择“显示硬件”并单击“开始”即可显示 OpenSDA 设备。 选择OpenSDAUSB设备并单击“开始”后,将出现以下界面: 通过短波驱动进行通信 有线版本售价119美元 持续尝试停止处理器。 请尝试重启主板,直到操作成功为止。 成功。处理器已停止运行。 Re: Regarding Flash Programming for the FRDM-A-S32K144N 你好,罗宾。 感谢您的回复。 遗憾的是,我没有外置的PEMicro调试器。 我也多次尝试了 S32DS 中的“通过完全芯片擦除进行紧急 Kinetis 设备恢复”功能,但所有尝试都失败了。 由于 FRDM-A-S32K144N 已被 PC 识别,因此我没有尝试“当 FRDM-A-S32K144 和 FRDM-A-S32K144N 无法通过 USB-C 连接检测到时的解决方案”。 请确认一下,Kinetis_Recovery_Utility 中的“电源开/关”是指拔下并重新插上 USB 电缆吗? 即使拔下并重新插上 USB 电缆,该过程仍然停留在以下提示信息:“请尝试重启主板,直到操作成功。” 此致, 福田 Re: Regarding Flash Programming for the FRDM-A-S32K144N 我通过 J3 将 外部 J-Link Plus 连接到板载 S32K144N ,并使用 J-Link Commander 中的 ` unlock kinetis` 命令擦除了芯片。 现在,用示波器观察 J9.5 RESET_MCU引脚,我看到一个周期约为 120 µs、高电平持续时间约为 660 ns 的方波信号。 无论我是否按住SW2,板载OpenSDA配合Kinetis_Recovery_Utility (版本1.06)都能成功停止MCU运行: 此时,J9.5 RESET_MCU引脚上的周期性脉冲停止;关闭Kinetis_Recovery_Utility后,即可在 S32DS v3.6.11 中下载新程序。 您之前是否对S32K144N进行过编程? 你使用的是 USB-A 转 USB-C 数据线吗?
View full article
S32DS3.4安装iar插件失败 报错如下: 收集要安装的项目时发生错误,会话上下文为:(profile=DefaultProfile,phase=org.eclipse.equinox.internal.p2.engine.phases.Collect,operand=,action=)。下载工件时出现问题:osgi.bundle,com.iar.dmgr,1.1.0.202505161156。读取签名内容时出错:C:\Users\vboxuser\AppData\Local\Temp\signatureFile8984369696384064703.jar 处理文件 C:\Users\vboxuser\AppData\Local\Temp\signatureFile8984369696384064703.jar 的签名时出错 下载工件时出现问题:org.eclipse.update.feature,com.iar.dmgr.feature,1.1.0.202505161156。读取签名内容时出错:C:\Users\vboxuser\AppData\Local\Temp\signatureFile2215016743562443700.jar 处理文件 C:\Users\vboxuser\AppData\Local\Temp\signatureFile2215016743562443700.jar 的签名时出错 下载工件时出现问题:osgi.bundle,com.iar.dmgr.jna,3.4.0.202505161156。读取签名内容时出错:C:\Users\vboxuser\AppData\Local\Temp\signatureFile3084560555014788452.jar 处理文件 C:\Users\vboxuser\AppData\Local\Temp\signatureFile3084560555014788452.jar 的签名时出错 下载工件 osgi.bundle,com.iar.dmgr.ui,1.1.0.202505161156 时出现问题。读取签名内容时出错:C:\Users\vboxuser\AppData\Local\Temp\signatureFile5078090908682208579.jar 处理文件 C:\Users\vboxuser\AppData\Local\Temp\signatureFile5078090908682208579.jar 的签名时出错 回复: S32DS3.4 安装iar插件失败 HI,CHRIS 目前遇到这个问题:S32DS3.5安装IAR插件;路径是官网下的https://eclipse-update.iar.com/plugin-manager/1.0 安装重启之后在HELP下看不到IAR EMBEDED workbench plugin manager这一个选项 IAR 版本为9.32.2 回复: S32DS3.4 安装iar插件失败 s32ds v3.5可以用 插件eclipse-iar-arm-8.0 有的版本s32ds(对应不同版本eclipse),可以试试离线安装iar插件的 https://eclipse-update.iar.com/updatesites.html 回复: S32DS3.4 安装iar插件失败 3.5以上就可以了 回复: S32DS3.4 安装iar插件失败 好的 ,请教下 现在什么版本可以安装IAR插件? 回复: S32DS3.4 安装iar插件失败 前段时间我问过,iar插件升级不支持老版本的eclipse
View full article
MWCT2016 HSE 2.40.0 安全启动配置失败 - ImportPlainSymKeyReqMuChannel 环境 MCU:基于MWCT2016S的无线充电控制器 工作设置(旧版) : HSE固件版本:2.6.0 (应用程序 + 安全启动)合并十六进制。 新设置(失败) : HSE固件版本:2.40.0 (应用程序 + 安全启动)合并十六进制。 我们正在从 HSE FW v2.6.0 迁移到 HSE FW v2.40.0,同时保持相同的 Qi 密钥配置和安全启动流程。 问题陈述 使用 HSE FW v2.6.0,完整的配置序列可以成功执行: HSE 安装 擦除按键 S2TP密钥槽配置 Qi 键编程 安全启动配置 应用程序启动成功 使用HSE FW v2.40.0时,所有配置步骤均成功完成,直到启动安全启动配置。 在安全启动配置期间,以下API 失败: 在安全启动代码中导入PlainSymKeyReqMuChannel()。   返回HSE 响应: 0x55A5A399 ,对应于: #define HSE_SRV_RSP_INVALID_PARAM ((hseSrvResponse_t)0x55A5A399UL)   出现此故障后,安全启动配置无法完成,ECU 将卡在安全启动代码中。   配置顺序 工作配置(HSE 2.6.0) 00_Blank_MWCT2016_CodeFlash_DataFlash.hex 电源 RESET 01_HSE_flash.srec版本 2.6.0 电源 RESET 02_EraseKeysSW.hex 电源 RESET 03_S2TP_KeySlotsAligned.srec S2TP 软件版本:1.1.1 电源 RESET 通过 UART 写入 Qi 密钥。 电源 RESET 应用程序+安全启动.hex 电源 RESET     从 UART 日志中获取合并十六进制烧录后的 HSE 响应: HseStatus:2848 位 0:0 RFU 位 1:0 HSE_SHE_STATUS_SECURE_BOOT 位 2:0 HSE_SHE_STATUS_SECURE_BOOT_INIT 位 3:0 HSE_SHE_STATUS_SECURE_BOOT_FINISHED 位 4:0 HSE_SHE_STATUS_SECURE_BOOT_OK 位 5:1 HSE_STATUS_RNG_INIT_OK 位 6:0 HSE_STATUS_HOST_DEBUGGER_ACTIVE 位 7:0 HSE_STATUS_HSE_DEBUGGER_ACTIVE 位 8:1 HSE_STATUS_INIT_OK 位 9:1 HSE_STATUS_INSTALL_OK 位 10:0 HSE_STATUS_BOOT_OK 位 11:1 HSE_STATUS_CUST_SUPER_USER 位 12:0 HSE_STATUS_OEM_SUPER_USER 位 13:0 HSE_STATUS_FW_UPDATE_IN_PROGRESS 位 14:0 RFU 位 15:0 RFU smrCoreStatus_Get: smrCoreStatus[1]:0,smrCoreStatus[0]:0 smrStatus[1]:0,smrStatus[0]:0   代码调试日志 HSE 响应:  ImportPlainSymKeyReqMuChannel-hseResp:0x55a5aa33   LoadBootMacKey-hseResp: 0x55a5aa33    Generic_ImportKeys-hseResp:0x55a5aa33   KeyProvisioningForJTAG-status: 1   SecureBootConfiguration-hseResp: 0x55a5aa33   KeyProvisioningToHseNVM-status: 1    NON_SECURE_IVT-BLOCK1-hseResp:0x55a5aa33    SECURE_IVT-BLOCK0-hseResp:0x55a5aa33   writeDefaultData   运行安全启动配置程序 Hse-FW 版本:0.13.0.2.6.0,完整内存 使用的接口版本:0.13.0.2.6.0 HseStatus:2862 位 0:0 RFU 位 1:1 HSE_SHE_STATUS_SECURE_BOOT 位 2:1 HSE_SHE_STATUS_SECURE_BOOT_INIT 位 3:1 HSE_SHE_STATUS_SECURE_BOOT_FINISHED 位 4:0 HSE_SHE_STATUS_SECURE_BOOT_OK 位 5:1 HSE_STATUS_RNG_INIT_OK 位 6:0 HSE_STATUS_HOST_DEBUGGER_ACTIVE 位 7:0 HSE_STATUS_HSE_DEBUGGER_ACTIVE 位 8:1 HSE_STATUS_INIT_OK 位 9:1 HSE_STATUS_INSTALL_OK 位 10:0 HSE_STATUS_BOOT_OK 位 11:1 HSE_STATUS_CUST_SUPER_USER 位 12:0 HSE_STATUS_OEM_SUPER_USER 位 13:0 HSE_STATUS_FW_UPDATE_IN_PROGRESS 位 14:0 RFU 位 15:0 RFU smrCoreStatus_Get: smrCoreStatus[1]:0,smrCoreStatus[0]:0 smrStatus[1]:1,smrStatus[0]:1 配置失败 - HSE 固件 2.40.0 报告: 00_Blank_MWCT2016_CodeFlash_DataFlash.hex 电源 RESET 01_S32K344_HSE_FW_UPDATE_v2_40_0.srec 电源 RESET 02_M210WLCUMBCD00A_WSB00.31_EraseKeySW_UART_ENABLE.hex 电源 RESET 03_S2TP_2_1_0_KeySlotsAligned.srec 电源 RESET 通过 UART 写入 Qi 密钥。 电源 RESET 应用程序+安全启动.hex 电源 RESET   房屋状态:2912 位 0:0 RFU 位 1:0 HSE_SHE_STATUS_SECURE_BOOT 位 2:0 HSE_SHE_STATUS_SECURE_BOOT_INIT 位 3:0 HSE_SHE_STATUS_SECURE_BOOT_FINISHED 位 4:0 HSE_SHE_STATUS_SECURE_BOOT_OK 位 5:1 HSE_STATUS_RNG_INIT_OK 位 6:1 HSE_STATUS_HOST_DEBUGGER_ACTIVE 位 7:0 HSE_STATUS_HSE_DEBUGGER_ACTIVE 位 8:1 HSE_STATUS_INIT_OK 位 9:1 HSE_STATUS_INSTALL_OK 位 10:0 HSE_STATUS_BOOT_OK 位 11:1 HSE_STATUS_CUST_SUPER_USER 位 12:0 HSE_STATUS_OEM_SUPER_USER 位 13:0 HSE_STATUS_FW_UPDATE_IN_PROGRESS 位 14:0 RFU 位 15:0 RFU smrCoreStatus_Get: smrCoreStatus[1]:0,smrCoreStatus[0]:0 smrStatus[1]:0,smrStatus[0]:0 ImportPlainSymKeyReqMuChannel-hseResp:0x55A5A399   断电重启后: UML 软件版本:WSB00.3B_UART_ENABLE   运行安全启动配置程序 Hse-FW 版本:0.13.0.2.40.0,完整内存 使用的接口版本:0.13.0.2.40.0   HseStatus:2848 位 0:0 RFU 位 1:0 HSE_SHE_STATUS_SECURE_BOOT 位 2:0 HSE_SHE_STATUS_SECURE_BOOT_INIT 位 3:0 HSE_SHE_STATUS_SECURE_BOOT_FINISHED 位 4:0 HSE_SHE_STATUS_SECURE_BOOT_OK 位 5:1 HSE_STATUS_RNG_INIT_OK 位 6:0 HSE_STATUS_HOST_DEBUGGER_ACTIVE 位 7:0 HSE_STATUS_HSE_DEBUGGER_ACTIVE 位 8:1 HSE_STATUS_INIT_OK 位 9:1 HSE_STATUS_INSTALL_OK 位 10:0 HSE_STATUS_BOOT_OK 位 11:1 HSE_STATUS_CUST_SUPER_USER 位 12:0 HSE_STATUS_OEM_SUPER_USER 位 13:0 HSE_STATUS_FW_UPDATE_IN_PROGRESS 位 14:0 RFU 位 15:0 RFU smrCoreStatus_Get: smrCoreStatus[1]:0,smrCoreStatus[0]:0 smrStatus[1]:0,smrStatus[0]:0    导入PlainSymKeyReqMuChannel-hseResp:0x55a5a399 ECU 仅卡在安全启动模式 Re: MWCT2016 HSE 2.40.0 Secure Boot Configuration Failure- ImportPlainSymKeyReqMuChannel 嗨@ShrikantM 能否请您分享一下您的密钥目录以及在ImportPlainSymKeyReqMuChannel()函数调用中使用的参数?报告的错误表明一个或多个 HSE 请求参数无效。 BR,VaneB Re: MWCT2016 HSE 2.40.0 Secure Boot Configuration Failure- ImportPlainSymKeyReqMuChannel 嗨@VaneB , 我们使用以下主要目录: /* 包含 NVM 密钥目录条目的表 */ const hseKeyGroupCfgEntry_t aHseNvmKeyCatalog[] = { /* NvmKeyGroup_0 */ {(HSE_MU0_MASK), HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_SHE, 1U, 128U, {0U, 0U}}, /* NvmKeyGroup_1 */ {(HSE_MU0_MASK), HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_ECC_PAIR, 1U, 256U, {0U, 0U}}, /* NvmKeyGroup_2 */ {(HSE_MU0_MASK), HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_AES, 1U, 256U, {0U, 0U}}, /* 关键目录结束标记 */     {0U, 0U, 0U, 0U, 0U, {0U, 0U}} }; /* 包含 RAM 键目录条目的表 */ const hseKeyGroupCfgEntry_t aHseRamKeyCatalog[] = { /* RamKeyGroup_0 */ {(HSE_MU0_MASK), HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_SHE, 1U, 128U, {0U, 0U}}, /* 关键目录结束标记 */     {0U, 0U, 0U, 0U, 0U, {0U, 0U}} }; 对于以下函数,我们收到 HSE_SRV_RSP_INVALID_PARAM 错误 hseSrvResponse_t Generic_ImportKeys(void) { hseSrvResponse_t srvResponse = HSE_SRV_RSP_GENERAL_ERROR; /*导入与 SMR#0 关联的密钥*/     srvResponse = ImportPlainSymKeyReqMuChannel( MU0, 1U             NVM_AES128_BOOT_KEY,             HSE_KEY_TYPE_AES,             ( HSE_KF_USAGE_VERIFY ),             0U, aesEcbKeyLength, aesEcbKey, 真的             ); ASSERT(HSE_SRV_RSP_OK == srvResponse); 如果(HSE_SRV_RSP_OK != srvResponse)             跳转到出口; /* 加载 SHE 安全启动的密钥 */ srvResponse = LoadBootMacKey(); ASSERT(HSE_SRV_RSP_OK == srvResponse); 如果(HSE_SRV_RSP_OK != srvResponse)             跳转到出口; 出口: 返回 srvResponse; } 请查看附件 global_defs.h 文件。有关参数的更多详细信息。 感谢并致意 斯瓦普尼尔·加瓦德 Re: MWCT2016 HSE 2.40.0 Secure Boot Configuration Failure- ImportPlainSymKeyReqMuChannel 嗨@SwapnilGawade 感谢您分享信息。根据您的配置,我有以下几点看法: SHE 密钥组配置的所有者为 HSE_KEY_OWNER_CUST。但是,HSE 服务 API 参考手册规定,对于 SHE 密钥目录配置,SHE 密钥组的所有者必须设置为 HSE_KEY_OWNER_ANY。NVM SHE 密钥目录配置示例也证明了这一点。 传递给 ImportPlainSymKeyReqMuChannel() 的 targetKeyHandle 定义如下: #define NVM_AES128_BOOT_KEY GET_KEY_HANDLE(HSE_KEY_CATALOG_ID_NVM, 1, 1)​ 但是,根据您的 NVM 密钥目录配置,AES 密钥组是第三组 (NvmKeyGroup_2)。基于此配置,NVM_AES128_BOOT_KEY 的正确定义应该是: GET_KEY_HANDLE(HSE_KEY_CATALOG_ID_NVM, 2, 0)​ Re: MWCT2016 HSE 2.40.0 Secure Boot Configuration Failure- ImportPlainSymKeyReqMuChannel 嗨@VaneB , 根据您的建议,我已经进行了更改,但它仍然给出与HSE_SRV_RSP_INVALID_PARAM (0x55a5a399) 类似的响应。 经过调试,我们发现ImportPlainSymKeyReqMuChannel (...)-> EraseKeyReq (targetKeyHandle, HSE_ERASE_NOT_USED))-> HSE_Send (muIf, muChannelIdx, gSyncTxOption, pHseSrvDesc)-> Hse_Ip_ServiceRequest (u8MuInstance, u8MuChannel, pHseIp_Request , HSE_DTCM_ADDR(pHseSrvDesc))-> Mu_Ip_SetTxRegister (Hse_Ip_apMuBase[u8MuInstance], u8MuChannel, (uint32)pHseSrvDesc) 返回的响应为HSE_SRV_RSP_INVALID_PARAM (0x55a5a399) 。 pHseSrvDesc 的参数已添加到附件 Mu_Ip_SetTxRegister-pHseSrvDesc.xlsx 中。 感谢并致意 斯瓦普尼尔·加瓦德 Re: MWCT2016 HSE 2.40.0 Secure Boot Configuration Failure- ImportPlainSymKeyReqMuChannel 嗨@SwapnilGawade 根据您的描述,我注意到您似乎将 DemoApp 框架与 Hse_Ip 驱动程序结合使用了。我的理解正确吗?如果进行了修改,具体做了哪些修改? 另外,您是否已在项目中禁用数据缓存?这是导致 HSE_SRV_RSP_INVALID_PARAM 错误的一个常见原因。所有用于与 HSE 通信的数据对象都必须强制存储在不可缓存的内存中。 我还注意到,您将 HSE_DTCM_ADDR(pHseSrvDesc) 作为 pHseSrvDesc 参数传递给了 Hse_Ip_ServiceRequest() 函数。请参阅HSE_ReadAdkp 返回 HSE_SRV_RSP_INVALID_ADDR 的线程,我的同事在其中解释了有关将 HSE 与 DTCM 内存一起使用的一些注意事项。 您可能还想了解一下 Hse_Ip_ToAHBAddress(),当启用 TCM 支持时,它会将本地地址转换为 HSE 主机地址。在这种情况下,它或许有用。 Re: MWCT2016 HSE 2.40.0 Secure Boot Configuration Failure- ImportPlainSymKeyReqMuChannel 嗨@VaneB , 在 HSE 2.6.0 的工作环境中,我们使用了以下库: 1. RTD AUTOSAR 4.4 2.主要目录如下 /* 包含 NVM 密钥目录条目的表 */ const hseKeyGroupCfgEntry_t aHseNvmKeyCatalog[] = { /* NvmKeyGroup_0 */ {(HSE_MU0_MASK), HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_SHE, 1U, 128U, {0U, 0U}}, /* NvmKeyGroup_1 */ {(HSE_MU0_MASK), HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_ECC_PAIR, 1U, 256U, {0U, 0U}}, /* NvmKeyGroup_2 */ {(HSE_MU0_MASK), HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_AES, 1U, 256U, {0U, 0U}}, /* 关键目录结束标记 */     {0U, 0U, 0U, 0U, 0U, {0U, 0U}} }; /* 包含 RAM 键目录条目的表 */ const hseKeyGroupCfgEntry_t aHseRamKeyCatalog[] = { /* RamKeyGroup_0 */ {(HSE_MU0_MASK), HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_SHE, 1U, 128U, {0U, 0U}}, /* 关键目录结束标记 */     {0U, 0U, 0U, 0U, 0U, {0U, 0U}} }; 我们使用的是与 HSE 2.40.0相同的RTD AUTOSAR 4.4和密钥目录,但我们遇到了问题。ImportPlainSymKeyReqMuChannel(...) 函数返回 HSE 响应为HSE_SRV_RSP_INVALID_PARAM 。 此RTD AUTOSAR 4.4中不提供 Hse_Ip_ToAHBAddress() 函数。 感谢并致意 斯瓦普尼尔·加瓦德 Re: MWCT2016 HSE 2.40.0 Secure Boot Configuration Failure- ImportPlainSymKeyReqMuChannel 嗨@SwapnilGawade 如前所述,SHE 密钥组配置的所有者为 HSE_KEY_OWNER_CUST。但是,HSE 服务 API 参考手册规定,对于 SHE 密钥目录配置,SHE 密钥组的所有者必须设置为 HSE_KEY_OWNER_ANY。 你的项目中是否禁用了数据缓存?这是导致 HSE_SRV_RSP_INVALID_PARAM 错误的一个常见原因。所有用于与 HSE 通信的数据对象都必须强制存储在不可缓存的内存中。 另外,能否分享一个简单的示例,展示您导入密钥的所有步骤? Re: MWCT2016 HSE 2.40.0 Secure Boot Configuration Failure- ImportPlainSymKeyReqMuChannel 你好@VaneB , 我们已根据您的建议和应用要求修正了密钥目录日志。 如果使用S2TP 版本 1.1.0 或跳过 S2TP刷写,安全启动可以正常工作。请参考下表了解更多信息。我们怀疑S2TP ver2.1.0版本是否发生了某些变化。其中,Qi 密钥导入的 CatLog 已更改,与我们配置的以下密钥 CatLog 不匹配。 HSE 版本 S2TP 版本 结果 2.40 1.1.1 1. 安全启动功能正常 2. 25瓦充电失败 -> Qi密钥导入失败 身份验证:初始化错误:5,身份验证:初始化错误 - 证书导入/验证失败 2.40 2.1.0 1. 安全启动在导入密钥时失败,错误代码:0x55A5A399 2. 25瓦充电无需安全启动软件即可工作(独立应用程序) 3. 如果跳过 S2TP 刷写,安全启动可以正常工作。但是充电功能无法使用。 闪流 擦除软件:擦除和格式化密钥目录   ↓   电源循环   ↓   使用 S2TP 闪充 Qi 密钥   ↓   电源循环   ↓   Flash SECBoot 代码:密钥导入   ↓   闪存启动 + 应用程序代码 关键目录: /* 包含 NVM 密钥目录条目的表 */ const hseKeyGroupCfgEntry_t aHseNvmKeyCatalog[] = { /* NvmKeyGroup_0:用于隐式 SHE 函数操作 */ {(HSE_MU0_MASK), HSE_KEY_OWNER_ANY, HSE_KEY_TYPE_SHE, 12U, 128U, {0U, 0U}}, /* NvmKeyGroup_1:配置为 AES 以满足 NVM_AES128_BOOT_KEY(组 1,插槽 1)*/ {(HSE_MU0_MASK), HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_AES, 4U, 128U, {0U, 0U}}, /* NvmKeyGroup_2:扩展为 3 个插槽,用于 PROVISION_KEY0(插槽 0)和 APP_MAC_KEY(插槽 2) */ {(HSE_MU0_MASK), HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_AES, 4U, 256U, {0U, 0U}}, /* HMAC 密钥 */ { HSE_ALL_MU_MASK, HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_HMAC, 2U, HSE_KEY512_BITS, {0U, 0U} }, \ /* ECC 密钥 */ \ { HSE_ALL_MU_MASK, HSE_KEY_OWNER_CUST, WRP_KEY_TYPE_ECC_PAIR, 4U, WRP_ECC_KEY_SIZE, {0U, 0U} }, \ { HSE_ALL_MU_MASK, HSE_KEY_OWNER_CUST, WRP_KEY_TYPE_ECC_PUB, 2U, WRP_ECC_KEY_SIZE, {0U, 0U} }, \ { HSE_ALL_MU_MASK, HSE_KEY_OWNER_CUST, WRP_KEY_TYPE_ECC_PUB_EXT, 1U, WRP_ECC_KEY_SIZE, {0U, 0U} }, \     /* RSA 密钥 */ \ { HSE_ALL_MU_MASK, HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_RSA_PAIR, 2U, HSE_KEY4096_BITS, {0U, 0U}}, \ /* NvmKeyGroup_8:NVM_RSA2048_PUB_CUSTAUTH_HANDLE0 的显式 RSA 公钥组 */ {(HSE_MU0_MASK), HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_RSA_PUB, 1U, 2048U, {0U, 0U}}, /* 关键目录结束标记 */     {0U, 0U, 0U, 0U, 0U, {0U, 0U}} };   /* 包含 RAM 键目录条目的表 */ const hseKeyGroupCfgEntry_t aHseRamKeyCatalog[] = { /* RamKeyGroup_0 */ {(HSE_MU0_MASK), HSE_KEY_OWNER_ANY, HSE_KEY_TYPE_SHE, 1U, 128U, {0U, 0U}}, /* 关键目录结束标记 */     {0U, 0U, 0U, 0U, 0U, {0U, 0U}} }; 使用 S2TP 版本 2.1.0 时,SecBoot 代码中的密钥导入失败: #define NVM_AES128_BOOT_KEY                     GET_KEY_HANDLE ( HSE_KEY_CATALOG_ID_NVM , 1 , 1 ) Re: MWCT2016 HSE 2.40.0 Secure Boot Configuration Failure- ImportPlainSymKeyReqMuChannel 你好@Bhushan1312 我们先来尝试找出问题所在。我已通过私信向您发送了一个简单的演示程序,该程序会导入一个 AES-128 密钥,将其删除,然后再重新导入。虽然该示例并非基于您当前使用的 RTD 版本,但仍应作为有用的参考,引用。 请根据您的设置调整演示,并验证基本的密钥导入和删除操作是否正常工作。这将有助于我们找到一个已知的有效工作基准,并从最基本的功能开始分析问题。由此,我们可以确定是什么原因导致您的应用程序中的 HSE 返回 HSE_SRV_RSP_INVALID_PARAM。 Re: MWCT2016 HSE 2.40.0 Secure Boot Configuration Failure- ImportPlainSymKeyReqMuChannel @VaneB感谢您的支持。在NXP团队的支持下,问题已解决。 我们发现用于导入 Qi 密钥的 S2TP 软件中配置的密钥目录日志存在问题。现在已经改正了。 经过此次更改,安全启动功能运行正常,充电功能也运行正常。
View full article
EB Tresos 29 的当前许可证缺少一些功能。 你好! 最近过期的 EB Tresos Studio 29 许可证包含的功能比当前可用的许可证要多得多。 以前的: 当前的: 值得注意的是,操作系统配置器和除一个导入器之外的所有导入器都已不再可用。 是否可以获得恢复缺失功能的新许可证? Re: EB Tresos 29 features missing from current license 嗨@johrehn 本案例中没有任何缺失的功能。比较的是两种不同产品的许可证。 功能集较大的产品是 EB tresos AutoCore,而功能较少的产品是 EB tresos Studio / AUTOSAR 配置工具。 BR,VaneB
View full article
如果选择了 Microsoft Edge 选项,则不会显示板内置的欢迎页面。 各位 我已经下载了 sdk.sdk_2.x_lpcxpresso54114仅提供 FreeMASTER 示例。它运行正常,但如果我在 FreeMASTER 的选项面板中选择 Edge 支持,就会出现问题。 在这种情况下,将显示欢迎屏幕: 点击一次板内置的欢迎页面,然后等待 10 秒或更长时间……没有任何反应。10秒后再次点击(第二次点击)页面才会出现: 没有图标,而且点击链接会出现奇怪的现象(例如,点击 readme.txt 链接时会弹出保存窗口)。 反之亦然,如果您在 FreeMASTER 的选项面板中选择 Internet Explorer,结果几乎是正确的。 “readme”链接会打开内部的 readme.txt 文件,但如果您点击“演示项目文件”链接,则会打开“演示项目”文件。 出现错误提示的 MSXbox 仍然会出现。 问题是我需要使用 RPC-JSON 脚本方式支持最新的浏览器,但是你提供的和我附加的 html 文件都无法正常工作。请测试我的 .h 文件。同时,请将文件上传到您的平台。它指的是 SDK 固件中相同的变量和命令 此致 Paolo Re: Board's Built-in Welcome Page doesn't appear if Microsoft Edge option is selected 亲爱的保罗: 这三种浏览器选项都能很好地检测和加载 SDK 示例应用程序中嵌入的演示页面和项目文件。浏览器元器件的行为确实会受到本地系统设置和已安装浏览器版本的很大影响,但通常情况下我们不应该遇到您描述的问题。 freemaster 使用其自己的浏览器方案“fmstr://”来访问存储在应用程序闪存中并由 TSA 表描述的内容。当系统设置过于严格时,此方案可能会被禁用或运行异常。Edge 浏览器不显示物品图标是一个已知问题。 目前,我们先忽略浏览 HTML 页面时遇到的图标缺失和其他问题。我们先来打开存储在目标闪存中的项目文件。请尝试直接点击欢迎页面中的“FreeMASTER演示项目”项。我从你的信息中理解到以下内容: Internet Explorer:无法打开项目,显示错误消息框 Chromium:项目能正确打开吗? 微软Edge浏览器:没有任何反应 请确认我的理解是否正确。 谢谢你, 米哈尔 Re: Board's Built-in Welcome Page doesn't appear if Microsoft Edge option is selected 亲爱的米哈尔 如果我直接在欢迎页面点击“FreeMASTER演示项目” , item directly in the Welcome page, it always works, it doesn't work if I try to reach the same project clicking it 板's Built-in Welcome Page .如果我选择 Chromium(图标和链接都有效,可以访问内部资源文件)或 Edge(图标不显示,资源文件也不显示)选项,项目访问将无法正常工作(方式不同)。因此,结论是问题出在内置的欢迎页面,该页面中的图标和相关资源有时会显示,有时则不会显示。 板内置欢迎页面: Internet Explorer:无法打开项目,显示错误信息框,但可以打开内部资源(readme 文件)。 Chromium浏览器:无法打开项目,显示错误信息框,但可以打开内部资源(readme文件)。 MS Edge:没有任何反应:难以进入板内置的欢迎页面,无法打开项目,显示错误消息框,页面中缺少图标,无法打开内部资源(readme)。 问候 Paolo
View full article
i.NX RT 1060 PMIC_ON_REQ behavior Hello, I am designing a custom board using the MIMXRT1062CVJ5B. The power supplies are connected as shown in the attached figure. Could you please help clarify the following points regarding this configuration? (1) Does PMIC_ON_REQ go high immediately after VDD_SNVS_IN is applied, or is there any delay before it is asserted? (2) When POR_B is driven low, what is the state of PMIC_ON_REQ? Does it remain high or transition low? (3) When VDD_SNVS_IN power is removed, does PMIC_ON_REQ go low? Is the output voltage level guaranteed in this condition? (4) Does VDD_SNVS_IN have an undervoltage lockout (UVLO) function? If so, at what voltage threshold does it become active? (5) In the case shown as "Waveform - A", where only VCC_3V3 is turned off (0 V) while VDD_SNVS_IN remains powered, is this operating condition supported? In this scenario, POR_B transitions from high to low and then from low to high. Can the i.MX RT1062 boot correctly and operate normally after this sequence? Thank you for your support. i.MXRT 106x Re: i.NX RT 1060 PMIC_ON_REQ behavior Hi, PMIC_ON_REQ is associated with VDD_SNVS_IN and is a push-pull output. There is no specific reference in the documentation indicating a delay before it is asserted. You could test this on an EVK. For example, on the EVKC, you can measure PMIC_ON_REQ through R282 and VDD_SNVS_IN through J30. The documentation does not guarantee a logic-low or logic-high output state for PMIC_ON_REQ when POR_B is driven low or when VDD_SNVS_IN power is removed. You can refer to Section 21.3.3, Power Mode Transitions, of the i.MX RT1060 Processor Reference Manual for different scenarios and how PMIC_ON_REQ behaves in each case. There is no UVLO specification explicitly documented for VDD_SNVS_IN for the i.MX RT1060. The SNVS digital low-voltage detector described in the reference manual includes a mechanism to detect interruptions of the SNVS_LP power supply that could cause the LP control, status, and secure counter values to change. Regarding question 5, would these scenarios occur during power-up, power-down, or while the application code is running? Best Regards, Pablo Re: i.NX RT 1060 PMIC_ON_REQ behavior Hi, Thank you for your reply. The scenario described in Question 5 assumes that, during normal operation, a temporary abnormal condition occurred on VCC_3V3, causing the voltage to drop. Best regards, Tomokazu Re: i.NX RT 1060 PMIC_ON_REQ behavior Hi In Section 4.1.6 Low Power Mode Supply Currents of the i.MX RT1060 Data Sheet, a mode is described in which DCDC_IN = 0 V, VDD_HIGH_IN = 0 V, and VDD_SNVS_IN = 3.3 V. For information regarding SNVS mode, please refer to Section 5.2.4 SNVS Mode of AN12085: How to Use i.MX RT Low Power Features. For the reset signal to be considered valid, it must be asserted for at least one RTC_XTALI clock cycle, according to the values specified in Table 28 Reset Timing Parameters of the data sheet. Best Regards, Pablo
View full article
MCPを追加して、CodeXに直接接続し、コラボレーションを実現しましょう。 CodeXやその他のエージェントを直接使用してIDEを操作できるように、MCPを追加していただけませんか?現在Figmaを使用している方法では、Figmaのクォータ制限があり、あまり便利ではありません。 回复: 增加MCP,直连codex进行协作 こんにちは、 @ALVANさん ご提案ありがとうございます。いただいたご意見は、GUI Guiderチームに共有し、検討していただくよう依頼いたします。 BR ハリー
View full article
MWCT2016 HSE 2.40.0 Secure Boot Configuration Failure- ImportPlainSymKeyReqMuChannel Environment MCU: MWCT2016S based Wireless Charging Controller Working Setup (Legacy): HSE FW Version: 2.6.0 (Application + Secure Boot) merge hex. New Setup (Failing): HSE FW Version: 2.40.0 (Application + Secure Boot) merge hex. We are migrating from HSE FW v2.6.0 to HSE FW v2.40.0 while maintaining the same Qi key provisioning and Secure Boot flow. Problem Statement With HSE FW v2.6.0, the complete provisioning sequence executes successfully: HSE installation Erase Keys S2TP key slot provisioning Qi key programming Secure Boot configuration Application boots successfully With HSE FW v2.40.0, all provisioning steps complete successfully until Secure Boot configuration is started. During Secure Boot configuration the following API fails: ImportPlainSymKeyReqMuChannel() in secure boot code.   return HSE response: 0x55A5A399 which corresponds to:  #define HSE_SRV_RSP_INVALID_PARAM ((hseSrvResponse_t)0x55A5A399UL)   After this failure, Secure Boot configuration cannot be completed, and the ECU remains stuck in the Secure Boot code.   Provisioning Sequence Working Configuration (HSE 2.6.0) 00_Blank_MWCT2016_CodeFlash_DataFlash.hex Power Reset 01_HSE_flash.srec  version 2.6.0 Power Reset 02_EraseKeysSW.hex Power Reset 03_S2TP_KeySlotsAligned.srec  S2TP SW Version: 1.1.1 Power Reset Write Qi Keys via UART Power Reset Application+SecureBoot.hex Power Reset     HSE response after merge hex flashing from UART log:  HseStatus : 2848         bit 0   : 0 RFU         bit 1   : 0 HSE_SHE_STATUS_SECURE_BOOT         bit 2   : 0 HSE_SHE_STATUS_SECURE_BOOT_INIT         bit 3   : 0 HSE_SHE_STATUS_SECURE_BOOT_FINISHED         bit 4   : 0 HSE_SHE_STATUS_SECURE_BOOT_OK         bit 5   : 1 HSE_STATUS_RNG_INIT_OK         bit 6   : 0 HSE_STATUS_HOST_DEBUGGER_ACTIVE         bit 7   : 0 HSE_STATUS_HSE_DEBUGGER_ACTIVE         bit 8   : 1 HSE_STATUS_INIT_OK         bit 9   : 1 HSE_STATUS_INSTALL_OK         bit 10  : 0 HSE_STATUS_BOOT_OK         bit 11  : 1 HSE_STATUS_CUST_SUPER_USER         bit 12  : 0 HSE_STATUS_OEM_SUPER_USER         bit 13  : 0 HSE_STATUS_FW_UPDATE_IN_PROGRESS         bit 14  : 0 RFU         bit 15  : 0 RFU  smrCoreStatus_Get :  smrCoreStatus[1] : 0 , smrCoreStatus[0] : 0  smrStatus[1] : 0 , smrStatus[0] : 0   Code debug log HSE response:  ImportPlainSymKeyReqMuChannel-hseResp: 0x55a5aa33    LoadBootMacKey-hseResp: 0x55a5aa33    Generic_ImportKeys-hseResp: 0x55a5aa33    KeyProvisioningForJTAG-status: 1    SecureBootConfiguration-hseResp: 0x55a5aa33    KeyProvisioningToHseNVM-status: 1    NON_SECURE_IVT-BLOCK1-hseResp: 0x55a5aa33    SECURE_IVT-BLOCK0-hseResp: 0x55a5aa33    writeDefaultData    Running Secure Boot CFG program  Hse-FW Version : 0.13.0.2.6.0 , full mem  using interface version : 0.13.0.2.6.0  HseStatus : 2862         bit 0   : 0 RFU         bit 1   : 1 HSE_SHE_STATUS_SECURE_BOOT         bit 2   : 1 HSE_SHE_STATUS_SECURE_BOOT_INIT         bit 3   : 1 HSE_SHE_STATUS_SECURE_BOOT_FINISHED         bit 4   : 0 HSE_SHE_STATUS_SECURE_BOOT_OK         bit 5   : 1 HSE_STATUS_RNG_INIT_OK         bit 6   : 0 HSE_STATUS_HOST_DEBUGGER_ACTIVE         bit 7   : 0 HSE_STATUS_HSE_DEBUGGER_ACTIVE         bit 8   : 1 HSE_STATUS_INIT_OK         bit 9   : 1 HSE_STATUS_INSTALL_OK         bit 10  : 0 HSE_STATUS_BOOT_OK         bit 11  : 1 HSE_STATUS_CUST_SUPER_USER         bit 12  : 0 HSE_STATUS_OEM_SUPER_USER         bit 13  : 0 HSE_STATUS_FW_UPDATE_IN_PROGRESS         bit 14  : 0 RFU         bit 15  : 0 RFU  smrCoreStatus_Get :  smrCoreStatus[1] : 0 , smrCoreStatus[0] : 0  smrStatus[1] : 1 , smrStatus[0] : 1 Failing Configuration-HSE FW 2.40.0 reports: 00_Blank_MWCT2016_CodeFlash_DataFlash.hex Power Reset 01_S32K344_HSE_FW_UPDATE_v2_40_0.srec Power Reset 02_M210WLCUMBCD00A_WSB00.31_EraseKeySW_UART_ENABLE.hex Power Reset 03_S2TP_2_1_0_KeySlotsAligned.srec Power Reset Write Qi Keys via UART Power Reset Application+SecureBoot.hex Power Reset    HseStatus : 2912         bit 0   : 0 RFU         bit 1   : 0 HSE_SHE_STATUS_SECURE_BOOT         bit 2   : 0 HSE_SHE_STATUS_SECURE_BOOT_INIT         bit 3   : 0 HSE_SHE_STATUS_SECURE_BOOT_FINISHED         bit 4   : 0 HSE_SHE_STATUS_SECURE_BOOT_OK         bit 5   : 1 HSE_STATUS_RNG_INIT_OK         bit 6   : 1 HSE_STATUS_HOST_DEBUGGER_ACTIVE         bit 7   : 0 HSE_STATUS_HSE_DEBUGGER_ACTIVE         bit 8   : 1 HSE_STATUS_INIT_OK         bit 9   : 1 HSE_STATUS_INSTALL_OK         bit 10  : 0 HSE_STATUS_BOOT_OK         bit 11  : 1 HSE_STATUS_CUST_SUPER_USER         bit 12  : 0 HSE_STATUS_OEM_SUPER_USER         bit 13  : 0 HSE_STATUS_FW_UPDATE_IN_PROGRESS         bit 14  : 0 RFU         bit 15  : 0 RFU  smrCoreStatus_Get :  smrCoreStatus[1] : 0 , smrCoreStatus[0] : 0  smrStatus[1] : 0 , smrStatus[0] : 0 ImportPlainSymKeyReqMuChannel-hseResp: 0x55A5A399   after Power reset:  UML SW Version : WSB00.3B_UART_ENABLE    Running Secure Boot CFG program  Hse-FW Version : 0.13.0.2.40.0 , full mem  using interface version : 0.13.0.2.40.0    HseStatus : 2848         bit 0   : 0 RFU         bit 1   : 0 HSE_SHE_STATUS_SECURE_BOOT         bit 2   : 0 HSE_SHE_STATUS_SECURE_BOOT_INIT         bit 3   : 0 HSE_SHE_STATUS_SECURE_BOOT_FINISHED         bit 4   : 0 HSE_SHE_STATUS_SECURE_BOOT_OK         bit 5   : 1 HSE_STATUS_RNG_INIT_OK         bit 6   : 0 HSE_STATUS_HOST_DEBUGGER_ACTIVE         bit 7   : 0 HSE_STATUS_HSE_DEBUGGER_ACTIVE         bit 8   : 1 HSE_STATUS_INIT_OK         bit 9   : 1 HSE_STATUS_INSTALL_OK         bit 10  : 0 HSE_STATUS_BOOT_OK         bit 11  : 1 HSE_STATUS_CUST_SUPER_USER         bit 12  : 0 HSE_STATUS_OEM_SUPER_USER         bit 13  : 0 HSE_STATUS_FW_UPDATE_IN_PROGRESS         bit 14  : 0 RFU         bit 15  : 0 RFU  smrCoreStatus_Get :  smrCoreStatus[1] : 0 , smrCoreStatus[0] : 0  smrStatus[1] : 0 , smrStatus[0] : 0    ImportPlainSymKeyReqMuChannel-hseResp: 0x55a5a399 ECU getting stuck in secure boot only Re: MWCT2016 HSE 2.40.0 Secure Boot Configuration Failure- ImportPlainSymKeyReqMuChannel Hi @ShrikantM  Could you please share your key catalogs as well as the parameters used in the ImportPlainSymKeyReqMuChannel() function call? The reported error indicates that one or more HSE request parameters are invalid. BR, VaneB Re: MWCT2016 HSE 2.40.0 Secure Boot Configuration Failure- ImportPlainSymKeyReqMuChannel Hi @SwapnilGawade  Thank you for sharing the information. Based on your configuration, I have the following observations: The SHE key group is configured with HSE_KEY_OWNER_CUST as the owner. However, the HSE Service API Reference Manual specifies that, for an SHE key catalog configuration, the owner of an SHE key group must be set to HSE_KEY_OWNER_ANY. This is also demonstrated in the NVM SHE Key Catalog Configuration example. The targetKeyHandle passed to ImportPlainSymKeyReqMuChannel() is defined as: #define NVM_AES128_BOOT_KEY GET_KEY_HANDLE(HSE_KEY_CATALOG_ID_NVM, 1, 1)​ However, according to your NVM key catalog configuration, the AES key group is the third group (NvmKeyGroup_2). Based on this configuration, the correct definition for NVM_AES128_BOOT_KEY should be:  GET_KEY_HANDLE(HSE_KEY_CATALOG_ID_NVM, 2, 0)​ Re: MWCT2016 HSE 2.40.0 Secure Boot Configuration Failure- ImportPlainSymKeyReqMuChannel Hi @VaneB , We are using below key catalogs: /* Table containing NVM key catalog entries */ const hseKeyGroupCfgEntry_t aHseNvmKeyCatalog[] = {     /* NvmKeyGroup_0 */     {(HSE_MU0_MASK), HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_SHE, 1U, 128U, {0U, 0U}},     /* NvmKeyGroup_1 */     {(HSE_MU0_MASK), HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_ECC_PAIR, 1U, 256U, {0U, 0U}},     /* NvmKeyGroup_2 */     {(HSE_MU0_MASK), HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_AES, 1U, 256U, {0U, 0U}},     /* Marker to end the key catalog */     {0U, 0U, 0U, 0U, 0U, {0U, 0U}} }; /* Table containing RAM key catalog entries */ const hseKeyGroupCfgEntry_t aHseRamKeyCatalog[] = {     /* RamKeyGroup_0 */     {(HSE_MU0_MASK), HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_SHE, 1U, 128U, {0U, 0U}},     /* Marker to end the key catalog */     {0U, 0U, 0U, 0U, 0U, {0U, 0U}} }; For below function we receive HSE_SRV_RSP_INVALID_PARAM hseSrvResponse_t Generic_ImportKeys(void) {     hseSrvResponse_t srvResponse = HSE_SRV_RSP_GENERAL_ERROR;     /*Import key linked with SMR#0*/     srvResponse = ImportPlainSymKeyReqMuChannel(             MU0,             1U,             NVM_AES128_BOOT_KEY,             HSE_KEY_TYPE_AES,             ( HSE_KF_USAGE_VERIFY ),             0U,             aesEcbKeyLength,             aesEcbKey,             TRUE             );     ASSERT(HSE_SRV_RSP_OK == srvResponse );     if(HSE_SRV_RSP_OK != srvResponse)             goto exit;     /* load keys for SHE secure boot */     srvResponse = LoadBootMacKey();     ASSERT(HSE_SRV_RSP_OK == srvResponse );     if(HSE_SRV_RSP_OK != srvResponse)             goto exit; exit:     return srvResponse; } Please check attached global_defs.h for more details about the parameters. Thanks and Regards, Swapnil Gawade Re: MWCT2016 HSE 2.40.0 Secure Boot Configuration Failure- ImportPlainSymKeyReqMuChannel Hi @SwapnilGawade  According to your description, I noticed that you appear to have combined the DemoApp framework with the Hse_Ip drivers. Is my understanding correct? If so, what modifications have been applied? Also, have you disabled the data cache in your project? This is a common cause of the HSE_SRV_RSP_INVALID_PARAM error. All data objects used for communication with HSE must be forced to non-cacheable memory. I also noticed that you are passing HSE_DTCM_ADDR(pHseSrvDesc) as the pHseSrvDesc parameter to the Hse_Ip_ServiceRequest() function. Please refer to the thread HSE_ReadAdkp returning HSE_SRV_RSP_INVALID_ADDR, where my colleague explains some considerations regarding the use of HSE with DTCM memory. You may also want to take a look at Hse_Ip_ToAHBAddress(), which converts a local address into an HSE host address when TCM support is enabled. It could be useful in this scenario. Re: MWCT2016 HSE 2.40.0 Secure Boot Configuration Failure- ImportPlainSymKeyReqMuChannel Hi @VaneB , As per your suggestion I have done the changes, but it also gives similar response as HSE_SRV_RSP_INVALID_PARAM (0x55a5a399). After debugging we found that it, in ImportPlainSymKeyReqMuChannel(...)->EraseKeyReq(targetKeyHandle, HSE_ERASE_NOT_USED))->HSE_Send(muIf, muChannelIdx, gSyncTxOption, pHseSrvDesc)->Hse_Ip_ServiceRequest(u8MuInstance, u8MuChannel, pHseIp_Request , HSE_DTCM_ADDR(pHseSrvDesc))->Mu_Ip_SetTxRegister(Hse_Ip_apMuBase[u8MuInstance], u8MuChannel, (uint32)pHseSrvDesc) retruns response as HSE_SRV_RSP_INVALID_PARAM (0x55a5a399). The parameters of pHseSrvDesc are added in attached Mu_Ip_SetTxRegister-pHseSrvDesc.xlsx. Thanks and Regards, Swapnil Gawade Re: MWCT2016 HSE 2.40.0 Secure Boot Configuration Failure- ImportPlainSymKeyReqMuChannel Hi @SwapnilGawade  As mentioned, the SHE key group is configured with HSE_KEY_OWNER_CUST as the owner. However, the HSE Service API Reference Manual specifies that, for an SHE key catalog configuration, the owner of an SHE key group must be set to HSE_KEY_OWNER_ANY. Have you disabled the data cache in your project? This is a common cause of the HSE_SRV_RSP_INVALID_PARAM error. All data objects used for communication with HSE must be forced to non-cacheable memory. Also, would it be possible to share a simple example showing all the steps you are performing to import the key? Re: MWCT2016 HSE 2.40.0 Secure Boot Configuration Failure- ImportPlainSymKeyReqMuChannel Hi @VaneB , In working setup with HSE 2.6.0 we are using following libraries: 1. RTD AUTOSAR 4.4 2. Key catalog as below /* Table containing NVM key catalog entries */ const hseKeyGroupCfgEntry_t aHseNvmKeyCatalog[] = {     /* NvmKeyGroup_0 */     {(HSE_MU0_MASK), HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_SHE, 1U, 128U, {0U, 0U}},     /* NvmKeyGroup_1 */     {(HSE_MU0_MASK), HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_ECC_PAIR, 1U, 256U, {0U, 0U}},     /* NvmKeyGroup_2 */     {(HSE_MU0_MASK), HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_AES, 1U, 256U, {0U, 0U}},     /* Marker to end the key catalog */     {0U, 0U, 0U, 0U, 0U, {0U, 0U}} }; /* Table containing RAM key catalog entries */ const hseKeyGroupCfgEntry_t aHseRamKeyCatalog[] = {     /* RamKeyGroup_0 */     {(HSE_MU0_MASK), HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_SHE, 1U, 128U, {0U, 0U}},     /* Marker to end the key catalog */     {0U, 0U, 0U, 0U, 0U, {0U, 0U}} }; Same RTD AUTOSAR 4.4 and Key catalog we are using with HSE 2.40.0, but we are facing issue. ImportPlainSymKeyReqMuChannel(...) function returns HSE Response as HSE_SRV_RSP_INVALID_PARAM. Hse_Ip_ToAHBAddress() function is not available in this RTD AUTOSAR 4.4. Thanks and Regards, Swapnil Gawade Re: MWCT2016 HSE 2.40.0 Secure Boot Configuration Failure- ImportPlainSymKeyReqMuChannel Hello @VaneB ,  We corrected the Key CatLog as per your suggestion and application requirements. Secure boot works well if we are using S2TP ver1.1.0 or skipping S2TP flashing. Please see below table to get more idea. We doubting that something has changed with S2TP ver2.1.0 where CatLog is changed for Qi key import which is not matching with below Key CatLog which we have configured. HSE Version S2TP Version Result 2.40 1.1.1 1. Secure Boot works 2. 25 Watt charging fails -> Qi Key import fails Auth: Init Error: 5, Auth: Init Error - Certificate Import/Validate Failed 2.40 2.1.0 1. Secure Boot fails at Import Keys ERROR: 0x55A5A399 2. 25 Watt charging works without Secure Boot SW (Stand alone application) 3. Secure boot works if we skip S2TP flashing. But Charging functionality do not work Flashing Flow Erase SW: Erase and Format Key Catlog   ↓   Power Cycle   ↓   Flash Qi keys with S2TP   ↓   Power Cycle   ↓   Flash SECBoot Code: Keys Import   ↓   Flash Boot + App code Key CatLog:  /* Table containing NVM key catalog entries */ const hseKeyGroupCfgEntry_t aHseNvmKeyCatalog[] = {     /* NvmKeyGroup_0: For implicit SHE Functional operations */     {(HSE_MU0_MASK), HSE_KEY_OWNER_ANY, HSE_KEY_TYPE_SHE, 12U, 128U, {0U, 0U}},     /* NvmKeyGroup_1: Configured as AES to satisfy NVM_AES128_BOOT_KEY (Group 1, Slot 1) */     {(HSE_MU0_MASK), HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_AES, 4U, 128U, {0U, 0U}},     /* NvmKeyGroup_2: Expanded to 3 slots for PROVISION_KEY0 (Slot 0) and APP_MAC_KEY (Slot 2) */     {(HSE_MU0_MASK), HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_AES, 4U, 256U, {0U, 0U}},     /* HMAC key */ \     { HSE_ALL_MU_MASK, HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_HMAC,          2U,        HSE_KEY512_BITS, {0U, 0U} }, \     /* ECC keys */ \     { HSE_ALL_MU_MASK, HSE_KEY_OWNER_CUST, WRP_KEY_TYPE_ECC_PAIR,      4U,         WRP_ECC_KEY_SIZE, {0U, 0U} }, \     { HSE_ALL_MU_MASK, HSE_KEY_OWNER_CUST, WRP_KEY_TYPE_ECC_PUB,       2U,         WRP_ECC_KEY_SIZE, {0U, 0U} }, \     { HSE_ALL_MU_MASK, HSE_KEY_OWNER_CUST, WRP_KEY_TYPE_ECC_PUB_EXT,   1U,         WRP_ECC_KEY_SIZE, {0U, 0U} }, \     /* RSA keys */ \     { HSE_ALL_MU_MASK, HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_RSA_PAIR,      2U,         HSE_KEY4096_BITS, {0U, 0U}}, \     /* NvmKeyGroup_8: Explicit RSA Public Key Group for NVM_RSA2048_PUB_CUSTAUTH_HANDLE0 */     {(HSE_MU0_MASK), HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_RSA_PUB, 1U, 2048U, {0U, 0U}},     /* Marker to end the key catalog */     {0U, 0U, 0U, 0U, 0U, {0U, 0U}} };   /* Table containing RAM key catalog entries */ const hseKeyGroupCfgEntry_t aHseRamKeyCatalog[] = {     /* RamKeyGroup_0 */     {(HSE_MU0_MASK), HSE_KEY_OWNER_ANY, HSE_KEY_TYPE_SHE, 1U, 128U, {0U, 0U}},     /* Marker to end the key catalog */     {0U, 0U, 0U, 0U, 0U, {0U, 0U}} }; Key Import failure in SecBoot code with S2TP ver2.1.0: #define NVM_AES128_BOOT_KEY                     GET_KEY_HANDLE(HSE_KEY_CATALOG_ID_NVM, 1, 1) Re: MWCT2016 HSE 2.40.0 Secure Boot Configuration Failure- ImportPlainSymKeyReqMuChannel Hi @Bhushan1312  Let's try to isolate the issue first. I have sent you, in a private message, a simple demo that imports an AES-128 key, erases it, and then imports it again. Although the example is not based on the RTD version you are currently using, it should still serve as a useful reference. Please adapt the demo to your setup and verify whether the basic key import and erase operations work correctly. This will help us align on a known working baseline and analyze the issue starting from the most basic functionality. From there, we can identify what is causing the HSE to return HSE_SRV_RSP_INVALID_PARAM in your application. Re: MWCT2016 HSE 2.40.0 Secure Boot Configuration Failure- ImportPlainSymKeyReqMuChannel @VaneB Thank you for your kind support. The issue is been resolved with NXP team support. We identified that there was issue with Key CatLog configured in S2TP SW used to import Qi keys. Its rectified now. With this change now Secure boot working fine and also the Charging functionality works ok.
View full article
增加MCP,直连codex进行协作 是否可以新增mcp,支持直接使用codex,或者其他的agent来操作IDE,目前已有的使用figma的方式有figma额度的限制,不是很好用 回复: 增加MCP,直连codex进行协作 嗨@ALVAN 谢谢你的建议。我会将您的反馈意见转达给 GUI Guider 团队,供他们参考。 BR 哈里
View full article
i.NX RT 1060 PMIC_ON_REQの動作 こんにちは、 私はMIMXRT1062CVJ5Bを使用してカスタム基板を設計しています。電源は添付の図に示されているように接続されています。 この構成に関する以下の点について、教えていただけますか? (1)PMIC_ON_REQはVDD_SNVS_INが適用された直後にハイになりますか、それともアサートされるまでに遅延がありますか? (2)POR_Bがローに駆動されたとき、PMIC_ON_REQの状態はどうなりますか?高止まりするのか、それとも低迷に転じるのか? (3)VDD_SNVS_IN電源が切断されたとき、PMIC_ON_REQはローになりますか?この条件下で出力電圧レベルは保証されますか? (4)VDD_SNVS_INには低電圧ロックアウト(UVLO)機能がありますか?もしそうなら、どの電圧閾値で活性化しますか? (5) 「波形 - A」として示されている場合、VCC_3V3だけがオフ(0 V)でVDD_SNVS_INが電源を保持している場合、この動作条件はサポートされていますか? このシナリオでは、POR_Bは高から低へ、そして低から高へと変化します。この手順の後、i.MX RT1062は正常に起動し正常に動作しますか? 再開まで今しばらくお待ちください。 i.MXRT 106x Re: i.NX RT 1060 PMIC_ON_REQ behavior こんにちは、 PMIC_ON_REQはVDD_SNVS_INに関連付けられており、プッシュプル出力です。ドキュメントには、主張されるまでの遅延を示す具体的な言及はありません。EVKで試してみるのもいいでしょう。例えばEVKCでは、R282までの量PMIC_ON_REQ、J30までのVDD_SNVS_INを測定できます。 ドキュメントは、POR_Bが低電圧で駆動されたり電源が切断されたりしたときにPMIC_ON_REQの論理ロー(論理低)または論理高(logic-high)出力状態VDD_SNVS_IN保証していません。 セクション21.3.3を参照できます。i.MX RT1060プロセッサリファレンスマニュアルの電源モード移行、さまざまなシナリオとPMIC_ON_REQの挙動について。 i.MX RT1060のUVLO仕様はVDD_SNVS_INとして明示的に文書化されていません。リファレンスマニュアルに記載されているSNVSデジタル低電圧検波器には、SNVS_LP電源の遮断を検出し、LP制御、状態、セカンプカウンター値が変化する可能性のある機構が含まれています。 質問5についてですが、これらのシナリオは電源投入中、電源オフ中、それともアプリケーションコードが実行中で起こるのでしょうか? よろしくお願いします、 パブロ Re: i.NX RT 1060 PMIC_ON_REQ behavior こんにちは、 お返事ありがとうございます。 問5で説明されているシナリオは、通常動作中にVCC_3V3で一時的な異常状態が発生し、電圧が低下したことを前提としています。 よろしくお願いします、 友和 Re: i.NX RT 1060 PMIC_ON_REQ behavior ハイ セクション4.1.6i.MX RT1060 データシートの低電力モード電源電流は、DCDC_IN = 0 V、VDD_HIGH_IN = 0 V、VDD_SNVS_IN = 3.3 V のモードが記述されています。SNVSモードに関する情報については、AN12085「i.MX RT低消費電力機能の使用方法」のセクション5.2.4「SNVSモード」を参照してください。 リセット信号が有効とみなされるためには、データシートの表28「リセットタイミングパラメータ」に指定されている値に従って、少なくとも1つのRTC_XTALIクロックサイクルの間、信号がアサートされている必要があります。 よろしくお願いします、 パブロ
View full article
S32DS3.4 インストール済みファイルの紛失 报错如下: インストールするアイテムを収集中にエラーが発生しました。セッションコンテキストは次のとおりです:(profile=DefaultProfile、phase=org.eclipse.equinox.internal.p2.engine.phases.Collect、operand=、action=)。アーティファクトのダウンロードに関する問題: osgi.bundle、com.iar.dmgr、1.1.0.202505161156。署名済みコンテンツの読み取りエラー:C:\Users\vboxuser\AppData\Local\Temp\signatureFile8984369696384064703.jar ファイルの署名プロセッシング中にエラーが発生しました:C:\Users\vboxuser\AppData\Local\Temp\signatureFile8984369696384064703.jar アーティファクトのダウンロードに問題あり:org.eclipse.update.feature,com.iar.dmgr.feature,1.1.0.202505161156。署名付きコンテンツの読み取りエラー:C:\Users\vboxuser\AppData\Local\Temp\signatureFile2215016743562443700.jar ファイルの署名処理中にエラーが発生しました:C:\Users\vboxuser\AppData\Local\Temp\signatureFile2215016743562443700.jar アーティファクトのダウンロードに問題がありました:osgi.bundle,com.iar.dmgr.jna,3.4.0.202505161156。署名済みコンテンツの読み取りエラー:C:\Users\vboxuser\AppData\Local\Temp\signatureFile3084560555014788452.jar ファイルの署名プロセッシング中にエラーが発生しました:C:\Users\vboxuser\AppData\Local\Temp\signatureFile3084560555014788452.jar アーティファクトのダウンロードに問題ありました:osgi.bundle,com.iar.dmgr.ui,1.1.0.202505161156。署名済みコンテンツの読み取りエラー:C:\Users\vboxuser\AppData\Local\Temp\signatureFile5078090908682208579.jarファイルの署名処理中にエラーが発生しました:C:\Users\vboxuser\AppData\Local\Temp\signatureFile5078090908682208579.jar 回复: S32DS3.4 安装iar插件失败 こんにちは、クリス 現在、S32DS3.5にIARプラグインをインストールする際に問題が発生しています。インストール先は公式ウェブサイト(https://eclipse-update.iar.com/plugin-manager/1.0 )からダウンロードしたパスです。 インストールと再起動後、「IAR EMBEDED workbench plugin manager」オプションがヘルプメニューに表示されなくなります。 IARのバージョンは9.32.2です。 回复: S32DS3.4 安装iar插件失败 S32DS v3.5はeclipse-iar-arm-8.0プラグインを使用できます。 S32DSの一部のバージョン(Eclipseの異なるバージョンに対応)では、IARプラグインをオフラインでインストールしてみてください。 https://eclipse-update.iar.com/updatesites.html 回复: S32DS3.4 安装iar插件失败 3.5以上であれば問題ありません。 回复: S32DS3.4 安装iar插件失败 わかりました。IARプラグインをインストールできるバージョンを教えていただけますか? 回复: S32DS3.4 安装iar插件失败 以前問い合わせたところ、IARプラグインのアップグレードは古いバージョンのEclipseをサポートしていないことが分かりました。
View full article
EB Tresos 29の機能が現在のライセンスに含まれていません こんにちは! 最近期限切れとなったEB Tresos Studio 29のライセンスには、現在入手可能なライセンスよりもはるかに多くの機能が含まれています。 前の: 現在: 特に、OSコンフィギュレーターと、インポートツールのほとんど(1つを除く)が利用できなくなっている。 欠落していた機能が復元された新しいライセンスを取得することは可能でしょうか? Re: EB Tresos 29 features missing from current license こんにちは、 @johrehnさん この場合、欠けている特徴はありません。比較は2つの異なる製品のライセンスを比較しています。 機能セットが豊富な製品はEB tresos AutoCoreで、機能が少ないのはEB tresos Studio / AUTOSAR Configuration Toolです。 BR、VaneB
View full article
找一款已经随设备适航过的用于核心处理机的芯片(支持多核多分区,最好有图像处理功能) 最好有图像生成功能 多核多分区 随设备已经做过适航认证的 Re: 找一款已经随设备适航过的用于核心处理机的芯片(支持多核多分区,最好有图像处理功能) 您好, 根据您对具有多个分区且最好具备图像处理能力的多核中央处理器的要求,我们建议您评估以下恩智浦半导体(NXP)设备: 1. i.MX 8QuadMax 产品链接 多核:2 个 Cortex-A72、4 个 Cortex-A53 和 2 个 Cortex-M4F。 硬件分区、虚拟化和资源隔离。 集成GPU、视觉和4K视频功能。 最适合多核、分区和图像处理。 2. Layerscape LS2088A / LS2048A 产品链接 8 个或 4 个 Cortex-A72 核心。 硬件虚拟化和分区强制执行。 非常适合航空航天、航空电子和高性能处理领域。 图像处理可能需要外部GPU、FPGA或加速器。 3. i.MX 8M Plus 产品链接 2 或 4 个 Cortex-A53 核心加 Cortex-M7。 双ISP、摄像头接口和NPU最高可达2.3 TOPS。 最适合图像处理或人工智能应用场景,但其分区功能应根据您的具体应用场景进行验证。 请注意,恩智浦提供汽车认证,与航空要求有一些重叠之处,但并不提供航空认证本身。NXP 的客户已将 NXP 微处理器应用于航空航天领域。有关特定零件编号、可用技术资料和相关客户经验的详细信息,请联系您授权的 恩智浦 代理商或 恩智浦代表。 如果您没有 NXP 企业账户或代理商联系人,请提供您的公司名称、国家/地区和项目详情,以便我们确定合适的渠道。
View full article
NXP_Support_Package_S32K3 v1.8.0 与 电池管理系统 Add-On v1.2.0 的兼容性 我查看了 MATLAB 插件管理器,发现 NXP_Support_Package_S32K3 的最新版本是 1.8.0。但是,NXP_Support_Package_BMS(版本 1.2.0)与 NXP_Support_Package_S32K3 版本 1.4.0 兼容。 您建议将 NXP_Support_Package_S32K3 升级到最新版本吗?如果是这样,NXP_Support_Package_BMS 插件是否与其兼容? 示例模型 Re: Compatibility of NXP_Support_Package_S32K3 v1.8.0 with BMS Add-On v1.2.0 你好, 要开发电池管理系统应用程序,您可以使用以下工具箱: MBD for S32K3 v1.4.0 (可在 NXP 网站上找到)。 NXP_Support_Package_S32K3 v1.8.1 (在 MATLAB 插件浏览器中找到)。 MBD for 电池管理系统 v1.2.0 (可在 NXP 网站上找到)。 NXP_Support_Package_BMS v1.2.0 (可在 MATLAB 插件浏览器中找到)。 S32K3 v1.4.0 的 MBD 文件包含: S32K3 RTD驱动器 S32 配置工具 S32K3 外设模块(ADC、DIO、PWM 等)。 示例 电池管理系统 v1.2.0 的 MBD包含: 电池管理系统 SDK 电池管理系统专用模块。 示例 如您所见,这两个文件包含了开发电池管理系统应用程序所需的所有文件。 NXP_Support_Package_S32K3 v1.8.1不包含构建和部署电池管理系统应用程序所需的任何文件。它的唯一目的是帮助您安装适用于S32K3 的 MBD Toolbox的任何版本(从 v1.0.0 到 v1.8.0)。 同样, NXP_Support_Package_BMS_V1.2.0不包含构建和部署电池管理系统应用程序所需的任何文件。它的唯一目的是帮助您安装MBD Toolbox for 电池管理系统 v1.2.0 。 MBD Toolbox for S32K3 V1.4.0之后 如果已安装MBD Toolbox for 电池管理系统 v1.2.0 ,则可以卸载NXP_Support_Package_S32K3 v1.8.1和NXP_Support_Package_BMS_V1.2.0 ,因为它们不再需要了。 根据我所掌握的信息,我的理解是 电池管理系统 Add-On v1.2.0 仅与 NXP 软件包 S32K3 v1.4 兼容。 MBD Toolbox for 电池管理系统 v1.2.0仅与NXP_Support_Package_电池管理系统_V1.2.0 兼容。 NXP_Support_Package_S32K3 v1.8.1无法安装MBD Toolbox for 电池管理系统 v1.2.0。 此致, 索林·班奇拉 Re: Compatibility of NXP_Support_Package_S32K3 v1.8.0 with BMS Add-On v1.2.0 亲爱的索林: 感谢您的回复。 我已经使用 NXP 支持代码包,软件包 S32K3 v1.4 和电池管理系统插件 v1.2.0 运行了电池管理系统 。 然而,关于 NXP 软件包 S32K3 v1.8 与 电池管理系统 插件 v1.2.0 的兼容性问题,我提出的问题 仍然没有得到解答。 根据我所掌握的信息,我的理解是 电池管理系统 Add-On v1.2.0 仅与 NXP 软件包 S32K3 v1.4 兼容。  如果是这样,未来是否有计划更新 电池管理系统 插件以支持 v1.8 版本? 此致, 拉苏尔 Re: Compatibility of NXP_Support_Package_S32K3 v1.8.0 with BMS Add-On v1.2.0 你好, 要使用电池管理系统 1.2.0的基于模型的设计工具箱,必须先安装S32K3 1.4.0 的基于模型的设计工具箱。这些工具箱包含RTD/SDK驱动程序、开发中使用的工具(gcc、S32配置工具)以及示例。这些工具可以从此页面下载:基于模型的设计工具箱 (MBDT) 另一方面,在 MATLAB 插件浏览器中,您会找到NXP_Support_Package_S32K3。该工具箱仅用于帮助用户安装S32K3 的基于模型的设计工具箱。支持包可用于安装所有S32K3工具箱版本(包括 1.4.0、MBD Toolbox for 电池管理系统 需要此工具)。它不包含 RTD/SDK 驱动程序、工具或示例。 笔记!我们提供的每个支持包都只能为一个特定平台安装工具箱。对于 MBD Toolbox for BMS,您需要安装NXP_Support_Package_BMS。 总而言之,要使用基于模型的电池管理系统设计工具箱,您需要执行以下操作: 1. 安装NXP_Support_Package_S32K3。 2. 运行GettingStarted.mlx并安装S32K3 的基于模型的设计工具箱 v1.4.0。   3. 安装NXP_Support_Package_BMS 4. 运行NXP_Support_Package_BMS.m脚本,并按照安装程序中的步骤操作。 5. 打开电池管理系统工具箱内的patches文件夹,并解压文件“NXP_MBDToolbox_S32K3xx_1.4.3_patch.zip”。建议您使用 MATLAB 的文件资源管理器解压该文件,因为 Windows 系统在处理长路径时可能会存在一些限制。 6. 运行位于解压文件夹中的 NXP_MBDToolbox_S32K3xx_patch.m 脚本。 此致, 索林·班奇拉
View full article
[I.MX95] Failed to enable LVDS1 + MIPI-DSI Hello NXP technical supports, My i.mx95 env is lf-6.18.y. I am using pixel_interleaver ch0 for DSI and ch1 for LVDS port 1. Now I got a problem that MIPI-DSI doesn't work when enabling LVDS1 and MIPI-DSI at the same time in the device-tree. I used modetest to see the information, but I see nothing about DSI. But if I disabled pixel_interleaver channel@1, DSI was to be OK. How do I configure the device-tree for enabling DSI + single port LVDS? Can show me an example? Attachments are my dtso files, but I changed the file name, because your webpage doesn't allow uploading files which's name with .dtso. Thanks in advance. Re: [I.MX95] Failed to enable LVDS1 + MIPI-DSI Hello,  Please try to use the following patch: https://community.nxp.com/t5/Multi-Source-Translation-Content/2046000-en-US/ta-p/2411639  It enables MIPI-DSI plus two LVDS outputs, so enabling only LVDS1 is a valid subset. Re: [I.MX95] Failed to enable LVDS1 + MIPI-DSI Sorry my bad. Do not need to change anything, but it's a bit weird, I have to install lvds and mipi driver both, then I can see the devices information by modetest. If install only one of them, can not see anything. Sorry, I have not tried the patch yet, because I was working on other problems.
View full article
車載ネットワーキングについてどこで学べばいいですか? CANバスや車載ネットワーキング全般についてもっと学びたいです。CANバスとOBDについて理論的かつ実践的な知識の両方を得られるコースや文献を探しています。この知識を活かして、自分自身のCANバス解析ハードウェアとソフトウェアを開発したいと考えています。前もって感謝します! イーサネット Re: Where do I learn about in-vehicle networking? こんにちは、 @czhong さん、 これが私が最初に手に取った本です。 https://intrepidcs.com/products/automotive-ethernet-the-definitive-guide-2nd-edition-2022/ よろしくお願いいたします。 パベル
View full article