2417634_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2417634_en-US

2417634_en-US

[I.MX95] Failed to enable LVDS1 + MIPI-DSI

Hello NXP technical supports,

My i.mx95 env is lf-6.18.y.
I am using pixel_interleaver ch0 for DSI and ch1 for LVDS port 1.

Now I got a problem that MIPI-DSI doesn't work when enabling LVDS1 and MIPI-DSI at the same time in the device-tree. I used modetest to see the information, but I see nothing about DSI.

But if I disabled pixel_interleaver channel@1, DSI was to be OK. How do I configure the device-tree for enabling DSI + single port LVDS? Can show me an example?

Attachments are my dtso files, but I changed the file name, because your webpage doesn't allow uploading files which's name with .dtso.

Thanks in advance.


Re: [I.MX95] Failed to enable LVDS1 + MIPI-DSI

Hello, 

Please try to use the following patch:

https://community.nxp.com/t5/Multi-Source-Translation-Content/2046000-en-US/ta-p/2411639 

It enables MIPI-DSI plus two LVDS outputs, so enabling only LVDS1 is a valid subset.

Re: [I.MX95] Failed to enable LVDS1 + MIPI-DSISorry my bad. Do not need to change anything, but it's a bit weird, I have to install lvds and mipi driver both, then I can see the devices information by modetest.
If install only one of them, can not see anything.

Sorry, I have not tried the patch yet, because I was working on other problems.
Tags (1)
No ratings
Version history
Last update:
2 weeks ago
Updated by: