Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
ETH MDIO driver We are using sia1110, and now we've noticed that when both TCP client and server are running simultaneously, one of them will randomly disconnect after some time. The client can reconnect successfully by clicking the reconnect button on the host machine, but the server cannot. The same procedure does not have this problem on different platforms. Could you please explain to me the reason for this? My current idea is to use MDIO to monitor the status between the MCU and the switch, but I'm currently facing some problems. status_t Dwmac_LLD_Mii_Read_Reg(volatile DwmacReg *dwmac_reg, uint32_t phy_addr, uint32_t reg_addr, uint32_t *reg_data) {     while (dwmac_reg->MAC_MDIO_ADDRESS.B.GB != 0U) {; }       dwmac_reg->MAC_MDIO_DATA.B.RA = reg_addr;     dwmac_reg->MAC_MDIO_DATA.B.GD = 0;     dwmac_reg->MAC_MDIO_ADDRESS.B.PA = phy_addr;     dwmac_reg->MAC_MDIO_ADDRESS.B.RDA = reg_addr;     dwmac_reg->MAC_MDIO_ADDRESS.B.GOC = 2U;      dwmac_reg->MAC_MDIO_ADDRESS.B.CR = 0xB;       dwmac_reg->MAC_MDIO_ADDRESS.B.GB = 1U;       while (dwmac_reg->MAC_MDIO_ADDRESS.B.GB != 0U) {; }       *reg_data = (uint16_t) (dwmac_reg->MAC_MDIO_DATA.R & 0x0000FFFFU);     return STATUS_SUCCESS; }   Dwmac_LLD_Mii_Read_Reg(&ETHERNET_0, 0x1B, 0x2U, &reg_val); The underlying function being used here, in which reg_val remains 0 all the time.   Re: ETH MDIO driver SJA110 2.0 and Using RMII I want to use the MDIO to monitor the registers and check the status of the switch and MCU when one of the ports is disconnected. This is just one method of detection, as I'm not sure what causes the TCP server and client to fail to coexist simultaneously. Not sure which version it is. xingyun_0-1788248086523.pngxingyun_0-1788248086523.png Re: ETH MDIO driver Hello @xingyun , Before analyzing the TCP disconnection and the MDIO read function, could you please provide some additional information about your setup? Which exact SJA1110 device variant and silicon revision are you using? Which MCU or processor is connected to the SJA1110 and which interface is used between them, for example RGMII, RMII, SGMII or another interface? Could you provide a simplified connection diagram showing the MCU, SJA1110 ports and the devices running the TCP client and server? Which TCP/IP stack and stack version are you using? Which version of SJA1110 SDK/RTD is used in the project? Does the TCP client and server run on the same MCU and the same Ethernet interface or on separate devices/interfaces? Could you also clarify what exactly you intend to monitor using the MDIO read function? In particular, which device and register do PHY address 0x1B and register address 0x02 refer to in your setup? Please also share the relevant schematic section or connection details showing how the SMI interface, including the MDC and MDIO signals, is connected between the MCU and the SJA1110. We kindly ask you to provide precise details for the questions above, as this will help us establish a clear understanding of your setup and avoid any potential misunderstandings at an early stage of the analysis.   Best regards, Pavel Re: ETH MDIO driver Hello @xingyun , To further help you I need more information. Please answer to all question below: 1. Which exact SJA1110 device variant do you use? SJA1110A, B, C or D? 2. What ports on SJA1110 are connected to TCPS and to TCPC? 3. Both used ports to TCPS and to TCPC used RMII? 4. TCPS and to TCPC are connected directly to RMII or is there any PHY between them? 5. How is SJA1110 configured? Is there any SW running on SJA1110 or SJA1110 acts only as a switch? 6. What software has been used to configure SJA1110? S32 Design Studio ? Best regards, Pavel
View full article
[S32DS 3.5+RTM401] I don't know what this SHxT happened I have no idea how to descripe it...  I was modified this Project 2 days ago...  After OS announce me to update OS !?  This SHxT happened :  I am not sure it's OS's update or S32DS's problem cause these problemssessss : CY9_0-1788140744365.png It's PURE Example Project from Example : CY9_2-1788142362452.png ```  root@NB /cygdrive/c/Project/NXP/WorkPath $grep -niR "pins_siul2_driver.h" * Prj_LinMaster_144/.project:314: SDK/platform/drivers/src/pins/pins_siul2_driver.h Prj_LinMaster_144/.project:316: $%7BS32K144_SDK_4_0_1_PATH%7D/platform/drivers/src/pins/pins_siul2_driver.h pwm_pal_s32k118/.project:174: SDK/platform/drivers/src/pins/pins_siul2_driver.h pwm_pal_s32k118/.project:176: $%7BS32K118_SDK_4_0_1_PATH%7D/platform/drivers/src/pins/pins_siul2_driver.h pwm_pal_s32k144/.project:159: SDK/platform/drivers/src/pins/pins_siul2_driver.h pwm_pal_s32k144/.project:161: $%7BS32K144_SDK_4_0_1_PATH%7D/platform/drivers/src/pins/pins_siul2_driver.h ```  CY9_3-1788142580908.png $find /cygdrive/c/NXP/S32DS.3.5/ -iname "lin_common_api.[hc]" /cygdrive/c/NXP/S32DS.3.5/S32DS/software/S32SDK_S32K1XX_RTM_4.0.1/middleware/lin/coreapi/lin_common_api.c /cygdrive/c/NXP/S32DS.3.5/S32DS/software/S32SDK_S32K1XX_RTM_4.0.1/middleware/lin/include/lin_common_api.h CY9_4-1788142877104.png Press [Reload] :  CY9_5-1788142890715.png CY9_6-1788142996465.png Although UI show it's exist ,  CY9_7-1788143484147.png Actually, it's *NOT* there :  $find /cygdrive/c/Project/NXP/WorkPath -name "S32K144_64_flash.ld" ./pwm_pal_s32k144/Linker_Files.bak/S32K144_64_flash.ld but ... I add Keyword in UI , "//// 2028/08/31 : Prj_LinMaster_144 ++Mark " and search :  $find /cygdrive/c/NXP/S32DS.3.5/ -iname "S32K144_64_flash.ld" -exec grep -l "Prj_LinMaster_144" {} \; /cygdrive/c/NXP/S32DS.3.5/S32DS/software/S32SDK_S32K1XX_RTM_4.0.1/platform/devices/S32K144/linker/gcc/S32K144_64_flash.ld ... as attachment  --  My daily work report : adjusting NXP S32DS parameters .  ~_~"'  General SDKs Re: [S32DS 3.5+RTM401] I don't know what this SHxT happened S32K1 SDK RTM 4.0.1 should not be present in S32DS v3.5. Unfortunately, it is present in S32DS v3.5, which is not recommended. I reported this issue to the internal team in 2023. S32K1 SDK RTM 4.0.1 in S32DS v3.5.png If customers install the S32K1 SDK RTM 4.0.1 using S32DS Extensions and Updates in S32DS v3.5, they will encounter a missing NXP GCC issue. They need to install the version of NXP GCC for Arm Embedded Processors v6.3 mentioned in S32SDK_for_S32K1xx_RTM_4.0.1_ReleaseNotes.pdf. This is why I recommend you use S32DS v3.3 with S32K1 SDK RTM 4.0.1. When you install S32K1 SDK RTM 4.0.1 in S32DS v3.3, you will see that S32DS Extensions and Updates automatically install NXP GCC for Arm Embedded Processors v6.3. Sorry for the inconvenience we bring you! Re: [S32DS 3.5+RTM401] I don't know what this SHxT happened Ref :  https://community.nxp.com/t5/S32-Design-Studio/S32DS-3-6-1-Update-Fail/m-p/2409828/emcs_t/S2h8ZW1haWx8dG9waWNfc3Vic2NyaXB0aW9ufE1USTBNME5CM1ZRTDhBfDI0MDk4Mjh8U1VCU0NSSVBUSU9OU3xoSw#M14454  Can you install a brand new S32DS v3.5 on a new computer/virtual machine to confirm it !?  Re: [S32DS 3.5+RTM401] I don't know what this SHxT happened Hi I apologize for all the trouble caused by the compatibility issues between the old version of S32DS and the S32K1 SDK. Please tell me which version of the S32K1 SDK RTM you are currently looking to install? Let me recommend the appropriate S32DS version for you. For S32K1 SDK RTM 4.0.1, I recommend download S32DS v3.3 instead of v3.5. download S32DS v3.3.png Then installing S32K1 SDK 4.0.1 by S32DS Extensions and Updates in S32DS v3.3: install S32K1 SDK 4.0.1 in S32DSv3.3.png install S32K1 SDK 4.0.1 in S32DSv3.3 S32DS Extensions and Updates.png I am able to build the hello_world_s32k144 project without error. Best Regards, Robin 回复: [S32DS 3.5+RTM401] I don't know what this SHxT happened By the way, CY9_0-1788149348559.png HW: You guess the device name Processor: Intel(R) Core(TM) Ultra 5 225H (1.70 GHz) Installed RAM 16.0 GB (15.2 GB available) Intel® Graphics (128 MB) Storage used: 692 GB / 954 GB Device Identifier: 8E10A0E8-3FEC-40F9-A621-C4C90079B8D2 Product Identifier: 00355-63764-61077-AAOEM System type: 64-bit operating system, x64 processor. Stylus and touch input: This display does not offer stylus or touch input functionality. OS: Version: Windows 11 Professional Edition, Version 25H2 Installed on 2026/5/26 OS build 26200.9278 Featured Windows Experience Suite 1000.26100.360.0 CY9_0-1788149671285.png 回复: [S32DS 3.5+RTM401] I don't know what this SHxT happened Brand new [HelloWorld] Project from Example Projet :  [Build] directly : Build Finished. 0 errors, 0 warnings. (took 917ms) BUT...  [Project Explorer] / / [Propertites] :  CY9_0-1788147961450.png [Edit/View...]  ... After 200 years ... CY9_1-1788148473408.png --  Whole my life wasted on S32DS shXt . 
View full article
FRDM Automotive S32K358 12V supply Hi, the user manual for the FRDM Automotive S32K358 board says that the board has the option to use 12 V power supply if  C1, C9, D1 are soldered. Unfortunately the manual does not say which concrete parts to use. Can you tell me that? Best, Johannes Re: FRDM Automotive S32K358 12V supply Hi, board's schematic/BOM show components. Download board's design files https://www.nxp.com/webapp/Download?colCode=FRDM-A-S32K358-DESIGN-FILES PetrS_0-1788172336991.png BR, Petr
View full article
S32K3 低功耗问题 您好,我在调试S32K348的低功耗的时候发现现在电流只能到达3.2ma,但是断掉MCU的供电电源发现外部电路只有0.2ma,麻烦帮忙看一下,还有什么没有关闭吗,怎么让功耗更低?附件是NXP的工程 Re: S32K3 低功耗问题 db16122_0-1788252143924.pngdb16122_0-1788252143924.pngdb16122_0-1788252143924.pngdb16122_0-1788252143924.pngdb16122_0-1788252143924.pngdb16122_0-1788252143924.png 根据 S32K348 数据手册,在待机模式下,FIRC ON (24MHz)(mA) 在 25C 环境温度下的电流消耗为 1.5137 mA。 您可以查看 FIRC 状态并将其关闭。由于 CAN 总线功耗不属于 MCU 功耗,因此您可能需要控制系统级别的电流消耗。顺便问一下,你们的系统设计用途是什么?可能需要更多示意图才能更好地理解您的问题。 Re: S32K3 低功耗问题 嗨,朱利安, 我使用自行开发的板进行了测试。我测试了板的电源,具体测试方法见项目说明。在进入低功耗之前,我处理了所有使用的引脚。除了CAN芯片外,板上所有其他电源均已控制。在进入低功耗之前,我关闭了3.3V、5V和15V的控制电源,并对外部设备和引脚进行了处理。CAN芯片和MCU也进入了低功耗。正常工作时,板电流超过200mA,经过一系列操作后,电流降至3mA多一点,但这仍然不够,需要进一步降低。 Re: S32K3 低功耗问题 你好@Joker_Y , 我猜这是定制设计,对吗?S32K3 数据手册中给出的功耗值仅通过 MCU 的电源进行测量。例如,在 S32K3X8EVB-Q289 中,必须移除 J25: Julin_AragnM_0-1788190113307.pngJulin_AragnM_0-1788190113307.pngJulin_AragnM_0-1788190113307.pngJulin_AragnM_0-1788190113307.pngJulin_AragnM_0-1788190113307.pngJulin_AragnM_0-1788190113307.png 如果你只测量电源,那么测量的是整个电路板的电流消耗,而不仅仅是MCU的电流消耗。在运行模式下影响不大,但在低电源模式下肯定无法使用。 能否分享一下你们是如何衡量当前能耗的? 我建议查看S32K3 低功耗电源管理单元 AN 和演示文档。第 10.2 节提供了一些在工作台上进行低功耗测量的技巧,以及一些电流消耗的示例案例。 另外,请记住,您需要将输入引脚驱动/拉至 VSS 或 VDD,以避免漏电流。这在社区帖子中讨论过:已解决:回复:S32K324 睡眠前的三态引脚 - NXP 社区。 根据 S32K3 的数据表,测量结果约为:运行时电流 ~3mA,待机电流 ~0.05mA。 此致, 朱利安 Re: S32K3 低功耗问题 是的,也就是说MCU有3ma左右的功耗 Re: S32K3 低功耗问题 MCU整体断掉电源是不是0.2mA的电流还存在? Re: S32K3 低功耗问题 你好@Joker_Y , “我测试了电路板的电源。”由此,我假设您确实是在系统级别测量整个电路板,但这无法与 S32K3 数据手册中的值进行比较,因为 S32K3 数据手册中的值只是 MCU VDD 的测量值。 ~3.2 mA 是 MCU 处于待机状态 + CAN 收发器处于低功耗模式 + 自行开发的板可能存在的任何残余漏电流的总和。 S32K3 数据手册中公布的当前值是在 MCU 的 VDD 电源引脚上,在受控条件下(无外部负载)测量的。待机供电电流值(如@db16122所提到的)在 FIRC 开启的待机状态下约为 1.5mA。 建议的做法是在定制板上,将电流表与 MCU 的 VDD 供电线串联。这与S32K3 低功耗电源管理单元 AN 和演示的第 10.2 节中描述的方法相同。与 S32K3 EVB 相同,移除跳线J25以断开 VDD 路径,并在其位置插入仪表。请在您定制电路板的原理图上找到对应的点。 我测试了一个简单的待机项目,可以测量出 MCU 的电流消耗低至 ~65uA,这与 25°C 时的典型消耗一致。 此外,还值得检查一下您的项目和设置中是否无意中保持了任何外围时钟、功率域或振荡器处于活动状态,以及引脚(例如,您项目中的 CP_OUT)是否存在任何漏电流。 希望这能帮到您。 此致, 朱利安 Re: S32K3 低功耗问题 你好@Joker_Y , 您可以尝试[RTD701 IP] S32K3X8EVB-Q289 和 FRDM-A-S32K358 待机 RTC GPIO 唤醒 - NXP 社区。这是我用来测量当前功耗的例子。 此致, 朱利安 Re: S32K3 低功耗问题 你好,朱利安 您是否有相关的测试演示可以参考?此外,我还会测试您的建议。谢谢。 Re: S32K3 低功耗问题 您好,有相关demo可以参考吗?我是开发的一个车载项目 Re: S32K3 低功耗问题 好的,谢谢。我去查一下。
View full article
[S32DS 3.5+RTM401] このSHxTが何で起きたのか分からない どう説明すればいいのか全くわからない... このプロジェクトは2日前に修正されました。 OSがOSのアップデートを促した後で!? こんなことが起こった: OSのアップデートの問題なのか、S32DSの問題なのか、これらの問題の原因がわかりません。 CY9_0-1788140744365.png これは、Example からの純粋なサンプル プロジェクトです。 CY9_2-1788142362452.png 「`」 root@NB /cygdrive/c/Project/NXP/WorkPath $grep -niR "pins_siul2_driver.h" * Prj_LinMaster_144/.project:314: SDK/platform/drivers/src/pins/pins_siul2_driver.h Prj_LinMaster_144/.project:316: $%7BS32K144_SDK_4_0_1_PATH%7D/プラットフォーム/ドライバ/src/pins/pins_siul2_driver.h pwm_pal_s32k118/.project:174: SDK/platform/drivers/src/pins/pins_siul2_driver.h pwm_pal_s32k118/.project:176: $%7BS32K118_SDK_4_0_1_PATH%7D/プラットフォーム/ドライバ/src/pins/pins_siul2_driver.h pwm_pal_s32k144/.project:159: SDK/platform/drivers/src/pins/pins_siul2_driver.h pwm_pal_s32k144/.project:161: $%7BS32K144_SDK_4_0_1_PATH%7D/プラットフォーム/ドライバ/src/pins/pins_siul2_driver.h 「`」 CY9_3-1788142580908.png $find /cygdrive/c/NXP/S32DS.3.5/-「lin_common_api」[HC]」 /cygdrive/c/NXP/S32DS.3.5/S32DS/software/S32SDK_S32K1XX_RTM_4.0.1/middleware/lin/coreapi/lin_common_api.c /cygdrive/c/NXP/S32DS.3.5/S32DS/software/S32SDK_S32K1XX_RTM_4.0.1/middleware/lin/include/lin_common_api.h CY9_4-1788142877104.png [リロード]を押してください: CY9_5-1788142890715.png CY9_6-1788142996465.png UI上では存在すると表示されているが、 CY9_7-1788143484147.png 実際には、そこには*ありません*。 $find /cygdrive/c/Project/NXP/WorkPath -name "S32K144_64_flash.ld" ./pwm_pal_s32k144/Linker_Files.bak/S32K144_64_flash.ld しかし... UI にキーワードを追加します。「//// 2028/08/31 : Prj_LinMaster_144 ++Mark」 および検索: $find /cygdrive/c/NXP/S32DS.3.5/-iname "S32K144_64_flash.ld" -exec grep -l "Prj_LinMaster_144" {} \; /cygdrive/c/NXP/S32DS.3.5/S32DS/ソフトウェア/S32SDK_S32K1XX_RTM_4.0.1/プラットフォーム/devices/S32K144/linker/gcc/S32K144_64_flash.ld ...添付ファイルとして -- 私の日々の業務報告:NXP S32DSのパラメータ調整。~_~"' 全般 SDK Re: [S32DS 3.5+RTM401] I don't know what this SHxT happened S32K1 SDK RTM 4.0.1 は S32DS v3.5には含まれていません。残念ながら、これは推奨されないS32DS v3.5に含まれています。私は2023年にこの問題を社内チームに報告しました。 S32K1 SDK RTM 4.0.1 in S32DS v3.5.png お客様がS32DS v3.5のS32DS拡張機能とアップデートを使ってS32K1 SDK RTM 4.0.1をインストールすると、NXP GCCの問題が見つからなくなります。S32SDK_for_S32K1xx_RTM_4.0.1_ReleaseNotes.pdf で言及された NXP GCC for Arm Embedded Processors v6.3 のバージョンをインストールする必要があります。 だからこそ、 S32DS v3.3 とS32K1 SDK RTM 4.0.1を組み合わせて使うことをおすすめします。S32DS v3.3にS32K1 SDK RTM 4.0.1をインストールすると、S32DS拡張とアップデートが自動的にNXP GCC for Arm Embedded プロセッサ v6.3をインストールするのがわかります。 ご迷惑をおかけして申し訳ございません! Re: [S32DS 3.5+RTM401] I don't know what this SHxT happened 参照: https ://community.nxp.com/t5/S32-Design-Studio/S32DS-3-6-1-Update-Fail/mp/2409828/emcs_t/S2h8ZW1haWx8dG9waWNfc3Vic2NyaXB0aW9ufE1USTBNME5CM1ZRTDhBfDI0MDk4Mjh8U1VCU0NSSVBUSU9OU3xoSw#M14454 新しいコンピュータや仮想マシンに新しいS32DS v3.5をインストールして確認できますか!? Re: [S32DS 3.5+RTM401] I don't know what this SHxT happened ハイ 旧版S32DSとS32K1 SDK間の互換性問題でご迷惑をおかけし申し訳ありません。 現在インストールを検討しているS32K1 SDK RTMのバージョンを教えてください。あなたに最適なS32DSのバージョンをお勧めしましょう。 For S32K1 SDK RTM 4.0.1,S32DS v3.5ではなくv3.3をダウンロードすることをお勧めします。 S32DS v3.3.pngをダウンロード 次に、S32DSの拡張とアップデートでS32DSの32K1 SDK 4.0.1をインストールします。 インストール S32K1 SDK 4.0.1 in S32DSv3.3.png インストール S32K1 SDK 4.0.1 in S32DSv3.3 S32DS 拡張とUpdates.png hello_world_s32k144プロジェクトをエラーなくビルドできます。 よろしくお願いいたします ロビン 回复: [S32DS 3.5+RTM401] I don't know what this SHxT happened ところで、 CY9_0-1788149348559.png 宿題: デバイス名を推測してください プロセッサー:インテル(R) Core(TM) Ultra 5 225H (1.70 GHz) 搭載RAM:16.0GB(空き容量:15.2GB) インテル®グラフィックス(128MB) 使用ストレージ容量:692 GB / 954 GB デバイス識別子: 8E10A0E8-3FEC-40F9-A621-C4C90079B8D2 製品識別番号: 00355-63764-61077-AAOEM システムの種類:64ビットオペレーティングシステム、x64プロセッサ。スタイラスおよびタッチ入力:このディスプレイは、スタイラスおよびタッチ入力機能に対応していません。 OS: バージョン: Windows 11 Professional Edition、バージョン 25H2 2026年5月26日にインストールされました OSビルド26200.9278 注目のWindowsエクスペリエンススイート 1000.26100.360.0 CY9_0-1788149671285.png 回复: [S32DS 3.5+RTM401] I don't know what this SHxT happened サンプルプロジェクトからの真新しい[HelloWorld]プロジェクト: [ビルド] 直接実行:ビルド完了。エラー0件、警告0件。(所要時間917ms) しかし... [プロジェクトエクスプローラー] / / [プロパティ] : CY9_0-1788147961450.png [編集/表示...] …200年後… CY9_1-1788148473408.png -- 私の人生はS32DSのクソみたいなことに全て無駄に費やされた。
View full article
[S32DS 3.5+RTM401] 我不知道这到底是怎么回事 我不知道该如何描述它…… 我两天前修改了这个项目…… 系统竟然提示我需要更新!? 这件糟心事发生了: 我不确定是操作系统更新还是S32DS的问题导致了这些问题: CY9_0-1788140744365.png 这是一个纯粹的示例项目,来自 Example: CY9_2-1788142362452.png ``` root@NB /cygdrive/c/Project/NXP/WorkPath $grep -niR "pins_siul2_driver.h" * Prj_LinMaster_144/.project:314: SDK/platform/drivers/src/pins/pins_siul2_driver.h Prj_LinMaster_144/.project:316: $ %7BS32K144_SDK_4_0_1_PATH% 7D/platform/drivers/src/pins/pins_siul2_driver.h pwm_pal_s32k118/.project:174: SDK/platform/drivers/src/pins/pins_siul2_driver.h pwm_pal_s32k118/.project:176: $ %7BS32K118_SDK_4_0_1_PATH% 7D/platform/drivers/src/pins/pins_siul2_driver.h pwm_pal_s32k144/.project:159: SDK/platform/drivers/src/pins/pins_siul2_driver.h pwm_pal_s32k144/.project:161: $%7BS32K144_SDK_4_0_1_PATH%7D/platform/drivers/src/pins/pins_siul2_driver.h ``` CY9_3-1788142580908.png $find /cygdrive/c/NXP/S32DS.3.5/-iname "lin_common_api.[hc]" /cygdrive/c/NXP/S32DS.3.5/S32DS/software/S32SDK_S32K1XX_RTM_4.0.1/middleware/lin/coreapi/lin_common_api.c /cygdrive/c/NXP/S32DS.3.5/S32DS/software/S32SDK_S32K1XX_RTM_4.0.1/中间件/lin/include/lin_common_api.h CY9_4-1788142877104.png 按下[重新加载]键: CY9_5-1788142890715.png CY9_6-1788142996465.png 虽然用户界面显示它存在, CY9_7-1788143484147.png 实际上,它并不在那里。 $find /cygdrive/c/Project/NXP/WorkPath -name "S32K144_64_flash.ld" ./pwm_pal_s32k144/Linker_Files.bak/S32K144_64_flash.ld 但是……我在 UI 中添加关键字,“//// 2028/08/31 : Prj_LinMaster_144 ++Mark” 并搜索: $find /cygdrive/c/NXP/S32DS.3.5/-iname "S32K144_64_flash.ld" -exec grep -l "Prj_LinMaster_144" {} \; /cygdrive/c/NXP/S32DS.3.5/S32DS/software/S32SDK_S32K1XX_RTM_4.0.1/platform/devices/S32K144/linker/gcc/S32K144_64_flash.ld ……作为附件 —— 我的日常工作报告:调整NXP S32DS的参数。~_~"' 概述 SDK Re: [S32DS 3.5+RTM401] I don't know what this SHxT happened S32DS v3.5中不应包含S32K1 SDK RTM 4.0.1 。遗憾的是,它存在于S32DS v3.5中,不建议使用该版本。我于 2023 年向内部团队报告了这个问题。 S32K1 SDK RTM 4.0.1 在 S32DS v3.5 中.png 如果客户使用S32DS v3.5中的S32DS 扩展和更新安装S32K1 SDK RTM 4.0.1 ,则会遇到缺少 NXP GCC 的问题。他们需要安装 S32SDK_for_S32K1xx_RTM_4.0.1_ReleaseNotes.pdf 中提到的 NXP GCC for Arm Embedded Processors v6.3 版本。 因此,我建议您使用S32DS v3.3和S32K1 SDK RTM 4.0.1 。当您在S32DS v3.3中安装S32K1 SDK RTM 4.0.1时,您会发现S32DS 扩展和更新会自动安装NXP GCC for Arm Embedded Processors v6.3 。 给您带来的不便,我们深表歉意! Re: [S32DS 3.5+RTM401] I don't know what this SHxT happened 参考链接: https ://community.nxp.com/t5/S32-Design-Studio/S32DS-3-6-1-Update-Fail/mp/2409828/emcs_t/S2h8ZW1haWx8dG9waWNfc3Vic2NyaXB0aW9ufE1USTBNME5CM1ZRTDhBfDI0MDk4Mjh8U1VCU0NSSVBUSU9OU3xoSw#M14454 您能否在一台新电脑/虚拟机上安装全新的S32DS v3.5版本来确认一下? Re: [S32DS 3.5+RTM401] I don't know what this SHxT happened HI 对于旧版 S32DS 与 S32K1 SDK 之间的兼容性问题造成的所有麻烦,我深表歉意。 请问您目前想要安装哪个版本的S32K1 SDK RTM?让我为您推荐合适的S32DS版本。 适用于S32K1 SDK RTM 4.0.1 ,我建议下载S32DS v3.3而不是v3.5 。 下载 S32DS v3.3.png 然后通过S32DS 扩展和更新在S32DS v3.3中安装S32K1 SDK 4.0.1 : 在 S32DSv3.3.png 中安装 S32K1 SDK 4.0.1 在 S32DSv3.3 中安装 S32K1 SDK 4.0.1 S32DS 扩展和更新.png 我能够成功构建hello_world_s32k144项目,没有出现任何错误。 此致敬礼, Robin 回复: [S32DS 3.5+RTM401] I don't know what this SHxT happened BTW,  CY9_0-1788149348559.png HW :  裝置名稱 you guess 處理器 Intel(R) Core(TM) Ultra 5 225H (1.70 GHz) 已安裝記憶體(RAM) 16.0 GB (15.2 GB 可用) 圖形卡 Intel(R) Graphics (128 MB) 儲存體 已使用 692 GB/954 GB 裝置識別碼 8E10A0E8-3FEC-40F9-A621-C4C90079B8D2 產品識別碼 00355-63764-61077-AAOEM 系統類型 64 位元作業系統,x64 型處理器 手寫筆與觸控 此顯示器不提供手寫筆或觸控式輸入功能 OS :  版本 Windows 11 專業版 版本 25H2 安裝於 ‎2026/‎5/‎26 OS 組建 26200.9278 特色 Windows 功能體驗套件 1000.26100.360.0 CY9_0-1788149671285.png 回复: [S32DS 3.5+RTM401] I don't know what this SHxT happened 来自 Example Projet 的全新 [HelloWorld] 项目: [直接构建]:构建完成。0 个错误,0 个警告。(耗时 917 毫秒) 但... [项目资源管理器] / / [属性] : CY9_0-1788147961450.png [编辑/查看...] ……200年后…… CY9_1-1788148473408.png —— 我这辈子都浪费在S32DS这种垃圾上了。
View full article
Question About SD2_VSEL and SD2_RST_B Connections on i.MX95 19x19 EVK Dear NXP Support Team, While reviewing the i.MX95 19x19 CPU EVK board schematic, I noticed that the SD2_VSEL and SD2_RST_B signals are connected to the FP09 GPIO1 and GPIO2 pins. Could you please explain the purpose of these connections in more detail? In particular, I would like to understand why these two signals are connected to the GPIO pins and how they are intended to be controlled or used in the system. Best regards, Walter Re: Question About SD2_VSEL and SD2_RST_B Connections on i.MX95 19x19 EVK The intent is to let the i.MX95 uSDHC2 block control the SD-card power rails through the PF09 PMIC, rather than treating those nets as ordinary board GPIOs. SD2_VSEL → PF09 GPIO1 : this is for SD/SDIO voltage switching. The i.MX95 uSDHC VSELECT output is defined as a signal used to change the external power-supply voltage, and the controller supports voltage selection through VEND_SPEC[VSELECT] . In PF09, GPIO1 can be configured as a dedicated VSELECT input ; when enabled, GPIO1 selects LDO2 = 3.3 V when low and LDO2 = 1.8 V when high . This matches the SD3.0 requirement that the platform implement both 3.3 V and 1.8 V signaling. SD2_RST_B → PF09 GPIO2 : this is for card power/reset control. The i.MX95 RESET_B signal is described as optional, active-low, and for a removable card it can be used “instead of hardware reset to enable/disable Card power during warm reset.” PF09 GPIO2 can be configured as an LDO1EN input , where the pin enables or disables the LDO1 output by hardware. So the EVK connection gives the uSDHC2 reset/power-control signal a direct path to the PMIC-controlled SD-card supply. In practical terms, these PF09 pins are not being used as random expansion GPIOs on the EVK. They are multi-function PMIC pins wired so the SD host controller can request the correct SD-card rail behavior: Signal PF09 pin role System purpose SD2_VSEL PF09 GPIO1 in VSELECT mode Switch NVCC_SD2 /SD I/O supply between 3.3 V and 1.8 V for SD3.0 operation. SD2_RST_B PF09 GPIO2 in LDO1EN mode or equivalent card-power control role Enable/disable SD-card power, especially around reset/warm-reset behavior. So the control path is typically: uSDHC2 driver/U-Boot configures the SD host controller → uSDHC2 drives SD2_VSEL and/or SD2_RST_B → PF09 interprets those pins according to its OTP/configuration → PF09 changes the SD-related LDO state . PF09’s GPIO modes/default behavior are OTP-configurable, and its GPIO outputs can also be controlled in system-on states when configured as GPOs, but the EVK wiring is intended to use the PMIC’s dedicated SD power-management functions rather than manual bit-banging. Bottom line: SD2_VSEL and SD2_RST_B are routed to PF09 GPIO1/GPIO2 so the i.MX95 uSDHC2 interface can perform SD-card voltage switching and card power/reset control through the PMIC. Re: Question About SD2_VSEL and SD2_RST_B Connections on i.MX95 19x19 EVK Hello, Yes. Those connections are intentional SD2_VSEL and SD2_RST_B are used to let the i.MX95 USDHC2 interface control the SD-card power/reset behavior through the PF09 PMIC, rather than being ordinary GPIO signals. SD2_VSEL → PF09 GPIO1: controls the SD-card I/O voltage switching, typically between 3.3 V and 1.8 V for SD 3.0 operation. SD2_RST_B → PF09 GPIO2: provides SD-card power/reset control, particularly useful during reset or power-cycle sequences. So the intended path is essentially: i.MX95 USDHC2 → SD2_VSEL / SD2_RST_B → PF09 → SD-card power rails The Linux device tree also shows SD2_VSELECT being used by USDHC2 and SD2_RESET_B being used for SD-card power control, which confirms these are part of the normal SD-card design rather than spare GPIOs.
View full article
Support Availability for AVAS Solution on NXP Platform Dear Team, Our customer is planning to develop an AVAS (Acoustic Vehicle Alerting System) solution and would like to evaluate an NXP-based platform for this project. Could you please advise whether NXP has a supported solution for AVAS applications? If available, kindly share the recommended MCU/MPU, reference design, development platform, software support, and any relevant documentation. Your guidance will help us propose the most suitable solution to the customer. Looking forward to your response. Re: Support Availability for AVAS Solution on NXP Platform Hello, NXP does not currently offer a dedicated, off-the-shelf AVAS reference platform. However, AVAS can be implemented using the NXP S32K3 automotive MCU family, combined with an external automotive audio amplifier and speaker subsystem. S32K3 provides the necessary automotive communication interfaces, safety capabilities, and software support required for AVAS ECU development. The exact device selection depends on the required audio complexity, functional safety targets, and network architecture. An official S32K5 AVAS demo using the DSP-V subsystem is planned for 2026, enabling more advanced sound synthesis. Best regards, Peter
View full article
NXP平台上AVAS解决方案的支持可用性 亲爱的团队, 我们的客户计划开发AVAS(声学车辆警报系统)解决方案,并希望评估基于 NXP 的平台是否适用于该项目。 请问NXP是否有针对AVAS应用的支持解决方案?如有条件,请提供推荐的MCU/MPU、参考设计、开发平台、软件支持以及任何相关文档。 您的指导将有助于我们为客户提供最合适的解决方案。 期待您的回复。 Re: Support Availability for AVAS Solution on NXP Platform 你好, NXP目前没有提供专用的、现成的AVAS参考平台。然而,AVAS 可以使用 NXP S32K3 汽车 MCU 系列,结合外部汽车音频放大器和扬声器子系统来实现。S32K3 提供 AVAS ECU 开发所需的必要汽车通信接口、功能安全能力和软件支持。具体设备选择取决于所需的音频复杂度、功能安全目标和网络架构。 官方计划于 2026 年推出使用 DSP-V 子系统的 S32K5 AVAS 演示,以实现更高级的声音合成。 顺祝商祺! Peter
View full article
i.MX95 19x19 EVKにおけるSD2_VSELおよびSD2_RST_B接続に関する質問 親愛なるNXPサポートチームへ、 i.MX95 19x19 CPU EVK基板の回路図を確認していると、SD2_VSEL信号とSD2_RST_B信号がFP09のGPIO1およびGPIO2ピンに接続されていることに気づきました。 これらの接続の目的をもう少し詳しく説明していただけますか? 特に、なぜこれら2つの信号がGPIOピンに接続されているのか、そしてそれらがシステム内でどのように制御または使用されるのかを理解したいです。 よろしくお願いいたします。 ウォルター Re: Question About SD2_VSEL and SD2_RST_B Connections on i.MX95 19x19 EVK その目的は、i.MX95 uSDHC2ブロックがPF09 PMICを介してSDカードの電源レールを制御できるようにすることであり、これらのネットを通常のボードGPIOとして扱うことではありません。 SD2_VSEL → PF09 GPIO1 :これはSD/SDIO電圧の切り替え用です。i.MX95 uSDHC VSELECT出力は外部電源電圧を変化させる信号として定義されており、コントローラはVEND_SPEC[VSELECT]による電圧選択をサポートしています。PF09では、GPIO1を専用のVSELECT入力として設定できます;有効化すると、低電圧時はLDO2 = 3.3 V、高電圧時はLDO2 = 1.8 Vを選択します。これは、プラットフォームが3.3Vと1.8Vの両方の信号を実装するSD3.0の要件と一致します。 SD2_RST_B → PF09 GPIO2 : これはカードの電源/リセット制御用です。i.MX95のRESET_B信号はオプションのアクティブローと説明されており、着脱式カードの場合は「ハードウェアリセットの代わりにウォームリセット時にカード電源を有効化・無効化するために使用できます」。PF09 GPIO2はLDO1EN入力として構成でき、ピンがハードウェアによってLDO1出力を有効または無効化します。したがって、EVK接続はuSDHC2のリセット/電源制御信号をPMIC制御のSDカード供給に直接送る経路を与えます。 実際には、これらのPF09ピンはEVK上でランダム拡張GPIOとしては使用されていません。これらは多機能PMICピンで、SDホストコントローラーが正しいSDカードレールの挙動を要求できるように配線されています。 信号 PF09ピンロール システムの目的 SD2_VSEL PF09 GPIO1 を VSELECT モードで使用する SD3.0動作用に3.3Vから1.8Vの間の/SD I/O電源をスイッチNVCC_SD2。 SD2_RST_B PF09 GPIO2をLDO1ENモードまたは同等のカード電源制御ロールで使用する SDカードの電源を有効/無効にします。特にリセット/ウォームリセット動作時に役立ちます。 したがって、制御経路は通常次の通りです:uSDHC2ドライバー/U-BootがSDホストコントローラ→uSDHC2ドライブをSD2_VSEL設定し、PF09がそれらのピンをOTPや設定に従って解釈SD2_RST_B →PF09がSD関連のLDO状態を変更し→PF09のGPIOモードやデフォルト動作はOTPで設定可能で、GPO出力もGPOとして設定した場合、システムオン状態で制御可能ですが、EVK配線は手動ビットバンではなく、PMIC専用のSD電源管理機能を使用することを意図しています。 結論として、SD2_VSELとSD2_RST_BはPF09 GPIO1/GPIO2にルーティングされているため、i.MX95 uSDHC2インターフェースはPMICを通じてSDカードの電圧切り替えやカードの電源・リセット制御を行えます。 Re: Question About SD2_VSEL and SD2_RST_B Connections on i.MX95 19x19 EVK こんにちは、 はい。これらの接続は意図的なSD2_VSELであり、SD2_RST_Bはi.MX95 USDHC2インターフェースが通常のGPIO信号ではなく、PF09 PMICを通じてSDカードの電源/リセット動作を制御するために使われています。 SD2_VSEL → PF09 GPIO1: SDカードのI/O電圧の切り替えを制御します。SD 3.0動作の場合、通常は3.3Vと1.8Vの間で切り替わります。 SD2_RST_B → PF09 GPIO2: SDカードの電源/リセット制御を提供します。特にリセットまたは電源サイクルシーケンス中に役立ちます。 つまり、意図された経路は基本的に次の通りです: i.MX95 USDHC2 → SD2_VSEL / SD2_RST_B → PF09 → SDカード電源レール Linuxデバイスツリーでは、USDHC2でSD2_VSELECTが使用され、SD2_RESET_BがSDカードの電源制御に使われていることが示されており、これらは予備のGPIOではなく通常のSDカード設計の一部であることが確認されています。
View full article
S32K3 low power consumption issue Hello, I'm debugging the low-power S32K348 and found that the current is only reaching 3.2mA. However, when I disconnect the MCU's power supply, the external circuit only draws 0.2mA. Could you please take a look and see if anything is still being turned off, and how to further reduce the power consumption? Attached is the NXP project file. Re: S32K3 低功耗问题 db16122_0-1788252143924.pngdb16122_0-1788252143924.pngdb16122_0-1788252143924.pngdb16122_0-1788252143924.pngdb16122_0-1788252143924.pngdb16122_0-1788252143924.png From S32K348 datasheet , during STANDBY mode, the current consumption for FIRC ON (24MHz)(mA) is 1.5137 mA at 25C ambient temperature. You may check the FIRC status and turn it off. You may need control current consumption for system level since CAN consumption is not part of MCU power consumption. BTW, what is your system design for? More schematics may need for better understand your question. Re: S32K3 低功耗问题 Hi Julián, I conducted the test using a self-developed board. I tested the power supply of the board, as shown in the project. Before entering low power consumption, I processed all the pins used. Except for the CAN chip, all other power supplies on the board were controlled. Before entering low power consumption, I turned off the controlled power supplies of 3.3V, 5V, and 15V, and processed the peripherals and pins. The CAN also entered low power consumption, and the MCU also entered low power consumption. During normal operation, the board has a current of more than 200 mA, and after a series of operations, it only has more than 3mA, but it is not enough and still needs to be lowered. Re: S32K3 低功耗问题 Hello @Joker_Y, I suppose this is a custom design, correct? Power consumption values given in S32K3's Data Sheet are measured only through the MCU's power supply. For example, in S32K3X8EVB-Q289, you must remove J25: Julin_AragnM_0-1788190113307.pngJulin_AragnM_0-1788190113307.pngJulin_AragnM_0-1788190113307.pngJulin_AragnM_0-1788190113307.pngJulin_AragnM_0-1788190113307.pngJulin_AragnM_0-1788190113307.png If you are only measuring the power supply, this measures the current consumption of the whole board, not just consumption of the MCU. It's not so significant in run modes but it's definitely not usable for low power modes. Can you share how are you measuring current consumption?  I suggest looking at S32K3 Low Power Management AN and demos documentation. Section 10.2 provides some tips for making low-power measurements on the bench, as well as some example cases for current consumption. Also, keep in mind you need to drive/ pull input pins to either VSS or VDD to avoid leakage current. It was discussed in this community post: Solved: Re: S32K324 Tristate Pins before sleep - NXP Community. Measurements from S32K3's data sheet are ~3mA@RUN and ~0.05mA@STANDBY approximately. Best regards, Julián Re: S32K3 低功耗问题 Yes, that means the MCU has a power consumption of around 3mA. Re: S32K3 低功耗问题 If the MCU is completely powered off, will the 0.2mA current still exist? Re: S32K3 低功耗问题 Hello @Joker_Y, "I tested the power supply of the board" With this, I assume you are indeed measuring the whole board at a system-level, which cannot be compared to S32K3 datasheet values, which are MCU VDD-only measurements. The ~3.2 mA is the sum of the MCU in Standby + CAN transceiver in low-power mode + any residual leakage the self-developed board may have. The current values published in the S32K3's datasheet are measured on the MCU's VDD supply pins, under controlled conditions with no external load. The Standby supply current values (as @db16122 mentioned) are ~1.5mA in Standby with FIRC on. The recommended approach is to insert a current meter in series with the MCU's VDD supply line on your custom board. This is the same methodology described in Section 10.2 of the S32K3 Low Power Management AN and demos. Same as on the S32K3 EVB by removing jumper J25 to break the VDD path and insert a meter in its place. Please identify the equivalent point on your custom board's schematic. I've tested a simple Standby project and can measure the MCU's current consumption down to ~65uA, which is in line with the typical consumption @25°C. It also may be worth to check in your project and setup whether any peripheral clocks, power domains, or oscillators may have been left active unintentionally, as well as any leakage in pins (for example, CP_OUT in your project). Hope this helps. Best regards, Julián Re: S32K3 低功耗问题 Hello, do you have any relevant demos I can refer to? I'm developing an in-vehicle project. Re: S32K3 低功耗问题 Hi,Julián Do you have any relevant demos for your testing that you can refer to? Additionally, I will also test your suggestions. Thank you. Re: S32K3 低功耗问题 Hello @Joker_Y , You can try [RTD701 IP] S32K3X8EVB-Q289 & FRDM-A-S32K358 Standby RTC GPIO Wake-up - NXP Community. This is the example I used to measure the current consumption. Best regards, Julián Re: S32K3 低功耗问题 Okay, thank you. I'll go and research it out
View full article
FRDMオートモーティブS32K358 12V電源 こんにちは、 FRDMオートモーティブS32K358基板のユーザーマニュアルには、 C1、C9、 D1 がはんだ付け されている場合に12V電源を使用するオプションがあると記載 されています。残念ながら、マニュアルにはどのコンクリート部品を使用すべきかが記載されていません。それを教えてくれる? 最高、 ヨハネス Re: FRDM Automotive S32K358 12V supply こんにちは、 基板の回路図/部品表には構成部品が示されています。ボードのデザインファイルをダウンロードしてください https://www.nxp.com/webapp/Download?colCode=FRDM-A-S32K358-DESIGN-FILES PetrS_0-1788172336991.png BR、ペトル
View full article
FRDM Automotive S32K358 12V 电源 您好, FRDM Automotive S32K358 板的用户手册指出,如果焊接 C1、C9、 D1, 则该板可以选择使用 12V 电源 。遗憾的是,手册中没有说明应该使用哪些混凝土部件。你能告诉我吗? 最好的, 约翰内斯 Re: FRDM Automotive S32K358 12V supply 您好, 板原理图/物料清单显示了元器件。下载电路板设计文件 https://www.nxp.com/webapp/Download?colCode=FRDM-A-S32K358-DESIGN-FILES PetrS_0-1788172336991.png BR,彼得
View full article
NXPプラットフォームでのAVASソリューションのサポート利用可能性 チームの皆様へ お客様は AVAS(音響車両警報システム) ソリューションの開発を計画しており、このプロジェクトのためにNXPベースのプラットフォームを評価したいと考えています。 NXPにはAVASアプリケーションに対応しているソリューションがあるか教えていただけますか?可能であれば、推奨されるMCU/MPU、リファレンスデザイン、開発プラットフォーム、ソフトウェアサポート、関連ドキュメントの共有をお願いいたします。 皆様のご指導により、お客様に最適な解決策を提案する助けとなります。 ご回答をお待ちしております。 Re: Support Availability for AVAS Solution on NXP Platform こんにちは、 NXPは現在、専用の既製品AVASリファレンスプラットフォームを提供していません。しかし、AVASはNXP S32K3自動車用MCUファミリーと外部の自動車用オーディオアンプおよびスピーカーサブシステムを組み合わせて実装可能です。S32K3はAVAS ECU開発に必要なオートモーティブ通信インターフェース、セーフティ機能、ソフトウェアサポートを提供します。正確なデバイス選択は、必要なオーディオ複雑さ、機能安全目標、ネットワークアーキテクチャによって異なります。 2026年にはDSP-Vサブシステムを使った公式S32K5 AVASデモが予定されており、より高度なサウンド合成が可能になります。 よろしくお願いいたします。 ピーター
View full article
关于 i.MX95 19x19 EVK 上的 SD2_VSEL 和 SD2_RST_B 连接的问题 尊敬的恩智浦技术支持团队: 在查看 i.MX95 19x19 CPU EVK 板原理图时,我注意到 SD2_VSEL 和 SD2_RST_B 信号连接到 FP09 GPIO1 和 GPIO2 引脚。 请您更详细地解释一下这些连接的用途? 我尤其想了解为什么这两个信号要连接到 GPIO 引脚,以及它们在系统中是如何控制或使用的。 顺祝商祺! 沃尔特 Re: Question About SD2_VSEL and SD2_RST_B Connections on i.MX95 19x19 EVK 其目的是让 i.MX95 uSDHC2 模块通过 PF09 PMIC 控制 SD 卡电源轨,而不是将这些网络视为普通的板 GPIO。 SD2_VSEL → PF09 GPIO1 :这是用于 SD/SDIO 电压切换。i.MX95 uSDHC 的 VSELECT 输出被定义为用于改变外部电源电压的信号,控制器支持通过 VEND_SPEC[VSELECT] 进行电压选择。在 PF09 中, GPIO1 可以配置为专用 VSELECT 输入;启用时,GPIO1在低电平时选择 LDO2 = 3.3 V,在高电平时选择 LDO2 = 1.8 V。这符合 SD3.0 的要求,即平台必须同时实现 3.3 V 和 1.8 V 信号。 SD2_RST_B → PF09 GPIO2 : this is for card power/RESET control.i.MX95 的 RESET_B 信号被描述为可选的、低电平有效的,对于可拆卸卡,它可以“代替硬件 RESET,在热 RESET 期间启用/禁用卡电源”。PF09 GPIO2 可以配置为 LDO1EN 输入,该引脚通过硬件启用或禁用 LDO1 输出。因此,EVK 连接为 uSDHC2 RESET/电源控制信号提供了一条直接通往 PMIC 控制的 SD 卡电源的路径。 实际上,这些 PF09 引脚并没有在 EVK 上用作随机扩展 GPIO。它们是多功能 PMIC 引脚,连接方式使得 SD 主机控制器可以请求正确的 SD 卡导轨行为: 信号 PF09 引脚角色 系统目的 SD2_VSEL PF09 GPIO1 处于 VSELECT 模式 将 NVCC_SD2 /SD I/O 电源在 3.3 V 和 1.8 V 之间切换,以实现 SD3.0 操作。 SD2_RST_B PF09 GPIO2 处于 LDO1EN 模式或等效的卡电源控制角色 启用/禁用 SD 卡电源,尤其是在 RESET/热 RESET 行为期间。 因此,控制路径通常是: uSDHC2 驱动程序/U-Boot 配置 SD 主机控制器 → uSDHC2 驱动 SD2_VSEL 和/或 SD2_RST_B → PF09 根据其 OTP/配置解释这些引脚 → PF09 改变与 SD 相关的低压差线性稳压器(LDO)状态。PF09 的 GPIO 模式/默认行为可通过 OTP 配置,其 GPIO 输出在配置为 GPO 时也可在系统开启状态下进行控制,但 EVK 接线旨在利用 PMIC 的专用 SD 电源管理功能,而不是手动进行位操作。 结论:SD2_VSEL 和 SD2_RST_B 被路由到 PF09 GPIO1/GPIO2,以便 i.MX95 uSDHC2 接口可以通过 PMIC 执行 SD 卡电压切换和卡电源/复位控制。 Re: Question About SD2_VSEL and SD2_RST_B Connections on i.MX95 19x19 EVK 你好, 是的。这些连接是故意的,SD2_VSEL 和 SD2_RST_B 用于让 i.MX95 USDHC2 接口通过 PF09 PMIC 控制 SD 卡的电源/复位行为,而不是普通的 GPIO 信号。 SD2_VSEL → PF09 GPIO1:控制 SD 卡 I/O 电压切换,SD 3.0 操作通常在 3.3 V 和 1.8 V 之间切换。 SD2_RST_B → PF09 GPIO2:提供 SD 卡电源/RESET 控制,在 RESET 或电源循环序列期间特别有用。 所以预期的路径本质上是: i.MX95 USDHC2 → SD2_VSEL / SD2_RST_B → PF09 → SD卡电源轨 Linux 设备树还显示 SD2_VSELECT 被 USDHC2 使用,SD2_RESET_B 被用于 SD 卡电源控制,这证实了这些是正常 SD 卡设计的一部分,而不是备用 GPIO。
View full article
S32K3の低消費電力問題 こんにちは。低消費電力のS32K348をデバッグしているのですが、消費電流が3.2mAしか出ていないことがわかりました。しかし、MCUの電源を切断すると、外部回路の消費電流は0.2mAにまで低下します。何かがまだオフになっている箇所がないか、また、消費電力をさらに削減する方法を教えていただけないでしょうか?NXPプロジェクトファイルを添付します。 Re: S32K3 低功耗问题 db16122_0-1788252143924.pngdb16122_0-1788252143924.pngdb16122_0-1788252143924.pngdb16122_0-1788252143924.pngdb16122_0-1788252143924.pngdb16122_0-1788252143924.png S32K348のデータシートによると、スタンバイモード時のFIRC ON(24MHz)時の消費電流は、周囲温度25℃で1.5137mAです。 FIRCの状態を確認し、必要に応じてオフにすることができます。CAN消費はMCUの消費電力の一部ではないため、システムレベルの電流消費制御が必要になるかもしれません。ところで、あなたのシステムは何のための設計ですか?ご質問内容をより深く理解するためには、追加の回路図が必要になるかもしれません。 Re: S32K3 低功耗问题 こんにちはフリアン、 自作の基板を使ってテストを行いました。プロジェクトに示されたように、基板の電源をテストしました。低消費電力に入る前に、使用したすべてのピンを処理しました。CANチップを除き、基板上の他のすべての電源は制御されていました。低消費電力に入る前に、3.3V、5V、15Vの制御電源を切り、**ペリフェラル**とピンを処理しました。CANも低消費電力に入り、MCUも低消費電力に入りました。通常動作時はボードの電流が200mAを超え、一連の動作を経て3mAを超えますが、それでも十分ではなく低下が必要です。 Re: S32K3 低功耗问题 こんにちは、 @Joker_Y さん。 これはカスタムデザインだと思いますよね?S32K3のデータシートに記載されている消費電力値は、MCU の電源のみを通じて測定されています。例えば、S32K3X8EVB-Q289では、J25を削除する必要があります。 Julin_AragnM_0-1788190113307.pngJulin_AragnM_0-1788190113307.pngJulin_AragnM_0-1788190113307.pngJulin_AragnM_0-1788190113307.pngJulin_AragnM_0-1788190113307.pngJulin_AragnM_0-1788190113307.png 電源ユニットのみを測定する場合は、MCU全体の消費電力ではなく、基板全体の電流消費量を測定します。実行モードではそれほど重要ではありませんが、低消費電力モードでは確実に使えません。 電流消費量をどのように測定しているのか教えてもらえますか? S32K3の低消費電力パワーマネージメントANやデモのドキュメントを調べることをおすすめします。セクション10.2では、ベンチ上で低消費電力測定を行う際のいくつかのヒントや、電流消費の例例も紹介しています。 また、 漏れ電流を避けるためには、入力ピンをVSSまたはVDDのいずれかに駆動または引っ張る必要があります。このコミュニティ投稿で議論されました: 解決: スリープ前のトリステートピンS32K324件 - NXPコミュニティ 。 S32K3のデータシートによると、約3mA@RUN、約0.05mA@STANDBYとなっています。 よろしくお願いします、 ジュリアン Re: S32K3 低功耗问题 はい、つまりMCUの消費電力は約3mAということです。 Re: S32K3 低功耗问题 MCUの電源が完全にオフになった場合でも、0.2mAの電流は流れ続けるのでしょうか? Re: S32K3 低功耗问题 こんにちは、 @Joker_Y さん。 「基板の電源をテストしました」ということは、システムレベルでボード全体を測定していると仮定しますが、これはMCU VDD専用のS32K3データシートの値と比較できません。 ~3.2 mAは、スタンバイ+CANトランシーバの低消費電力モードのMCU+自社開発基板に残る残留漏れの合計です。 S32K3のデータシートに掲載されている電流値は、外部負荷のない制御条件下でMCUのVDD電源ピンで測定されます。( @db16122さんが言及したように)スタンバイ時の供給電流値は、FIRCがオンのスタンバイ状態で約1.5mAです。 推奨される方法は、カスタム基板上のMCUのVDD電源ラインに直列に電流計を挿入することです。これは S32K3低 パワーマネージメント ANおよびデモのセクション10.2で説明されている方法と同じです。S32K3 EVBと同様に、ジャン パーJ25 を外してVDD経路を断ち切り、その代わりにメーターを挿入します。お客様のカスタム基板の回路図上で、対応する箇所を特定してください。 簡単なスタンバイプロジェクトをテストしたところ、MCUの現在の消費電力を~65uAまで測定できました。これは典型的な消費電力の@25°Cと一致しています。 また、プロジェクト内で周辺クロックや電源ドメイン、発振器が意図せずアクティブになっていることや、ピンの漏れ(例えばプロジェクトのCP_OUT)がないか確認する価値があります。 これがお役に立てば幸いです。 よろしくお願いします、 ジュリアン Re: S32K3 低功耗问题 やあ、フリアン テストに関連するデモはありますか?さらに、いただいたご提案も試してみます。ありがとう。 Re: S32K3 低功耗问题 こんにちは、 @Joker_Y さん。 [RTD701 IP] S32K3X8EVB-Q289 および FRDM-A-S32K358 スタンバイRTC GPIO Wake-up - NXPコミュニティを試してみてください。これは、現在の消費量を測定するために私が使用した例です。 よろしくお願いします、 ジュリアン Re: S32K3 低功耗问题 こんにちは。参考になるデモはありますか?車載システム開発プロジェクトに取り組んでいます。 Re: S32K3 低功耗问题 はい、ありがとうございます。調べてみます
View full article
S32K344 Bare-Metal RTD Package Availability (Non-AUTOSAR) Hello NXP Team, I am new to the S32K344 platform and recently purchased an S32K344-based board. I would like to start with bare-metal development using S32 Design Studio and Real-Time Drivers (RTD), without using AUTOSAR. However, on the NXP Software Download page, I can only find packages labeled: S32K1_S32M24x Real-Time Drivers AUTOSAR R21-11 S32K1_S32M24x Real-Time Drivers AUTOSAR 4.4 I am specifically looking for: Bare-metal / non-AUTOSAR RTD package GPIO, UART, SPI, ADC examples S32K344 support S32 Design Studio integration Could you please clarify: Is there a separate RTD package available for bare-metal development on S32K344? If not, can the currently available RTD package be used in a non-AUTOSAR project? Where can I download bare-metal examples for S32K344 (GPIO, UART, SPI, etc.)? Is there any recommended getting-started guide for learning S32K344 at register level and RTD level without AUTOSAR? Re: S32K344 Bare-Metal RTD Package Availability (Non-AUTOSAR) No, there is no separate bare-metal RTD package for S32K344. The standard S32K3 RTD package is intended for both AUTOSAR and non-AUTOSAR applications. Yes, the currently available RTD package can be used in non-AUTOSAR projects. The RTD release notes explicitly state that S32K3 Real-Time Drivers can also be used in a non-AUTOSAR environment as a collection of peripheral drivers designed to simplify and accelerate application development on NXP microcontrollers. GPIO, UART, SPI, ADC and other peripheral examples are delivered as part of the RTD package and are available through the RTD installation and S32 Design Studio example projects. RTD is integrated with S32 Design Studio and supports non-AUTOSAR development workflows. For getting started, we recommend using the S32K3 Reference Manual for register-level programming together with the RTD Getting Started documentation, RTD Release Notes, and the RTD example projects included in the package. Additionally, for S32K344 you should use the S32K3_S32M27x RTD package. The S32K1 RTD packages mentioned in your post are intended for different device families.
View full article
最新 MediaPipe 面网格(478 个地标)的量化(INT8)模型可用性 我希望在 iMX 平台上高效运行 Google 的MediaPipe 人脸网格(478 点地标模型,带虹膜追踪/注意力网格) 。NXP 目前是否提供 478 点人脸地标模型的官方量化版本(例如 INT8)? 如果目前还没有发布,未来有发布计划吗? 我尝试使用 eIQ 工具包量化谷歌提供的原始模型,但精度大幅下降。当我用同样的方法量化谷歌旧版 Facemesh 模型(486 个地标点)时,却能获得不错的性能。NXP 是否也观察到了同样的问题? 还有其他人尝试过量化谷歌最新的 FaceMesh(478 Landmark)模型吗? 机器学习 Re: Availability of Quantized (INT8) Model for Latest MediaPipe Face Mesh (478 Landmarks) 你好, 目前尚不可用,但我们正在内部测试,以期实现 int8 的性能提升。 此致敬礼
View full article
S32K344 ベアメタルRTDパッケージの入手可能性(非AUTOSAR) NXPチームの皆様、こんにちは。 私はS32K344プラットフォームは初めてで、最近S32K344ベースのボードを購入しました。 まずはAUTOSARを使わずに、S32 Design Studioとリアルタイム・ドライバを使った ベアメタル開発 から始めたいと思っています。 しかし、NXPソフトウェアダウンロードページでは、以下のようなラベルのパッケージしか見つかりません。 S32K1_S32M24x リアルタイム・ドライバ AUTOSAR R21-11 S32K1_S32M24x リアルタイム・ドライバ AUTOSAR 4.4 私が特に探しているのは以下のものです。 ベアメタル/非AUTOSAR RTDパッケージ GPIO、UART、SPI、ADCの例 S32K344サポート S32 Design Studioの統合 もう少し詳しく教えていただけますか: S32K344でベアメタル開発用の別のRTDパッケージはありますか? もしそうでなければ、現在利用可能なRTDパッケージはAUTOSAR以外のプロジェクトで使用できますか? S32K344用のベアメタルの例(GPIO、UART、SPIなど)はどこでダウンロードできますか? AUTOSARなしでレジスターレベルやRTDレベルでのS32K344を学ぶためのおすすめの入門ガイドはありますか? Re: S32K344 Bare-Metal RTD Package Availability (Non-AUTOSAR) いいえ、S32K344用の別個のベアメタルRTDパッケージはありません。標準のS32K3 RTDパッケージは、AUTOSARおよび非AUTOSARの両方のアプリケーションを想定しています。 はい、現在利用可能なRTDパッケージはAUTOSAR以外のプロジェクトでも使用できます。RTDのリリースノートには、S32K3リアルタイム・ドライバは非AUTOSAR環境でも、NXPマイクロコントローラ上のアプリケーション開発を簡素化・加速するために設計された周辺ドライバの集合として使用可能であると明記されています。 GPIO、UART、SPI、ADCなどのペリフェラル例はRTDパッケージの一部として提供され、RTDインストールおよびS32 Design Studioのサンプルプロジェクトを通じて利用可能です。RTDはS32 Design Studioと統合されており、AUTOSAR以外の開発ワークフローをサポートしています。 始めるには、レジスタレベルのプログラミングにはS32K3リファレンスマニュアルと、RTDの入門ドキュメント、RTDリリースノート、パッケージに含まれるRTDサンプルプロジェクトを併用することを推奨します。 さらに、S32K344にはRTDパッケージS32K3_S32M27xを使うべきです。あなたの投稿で言及されているS32K1 RTDパッケージは、異なるデバイスファミリー向けに設計されています。
View full article
最新のMediaPipeフェイスメッシュ(478ランドマーク)における量子化(INT8)モデルの利用可能性 GoogleのMediaPipe Face Mesh(478ポイントのランドマークモデルでアイリストラッキング/Attention Mesh)を使おうと考えています iMXプラットフォーム上で効率的に対応しています。NXPは現在、478ポイントのフェイスランドマーカーモデルに対して公式の量子化版(例:INT8)を提供していますか? もし現在入手可能でなければ、FUTUREにリリース予定はありますか? eIQツールキットを使ってGoogleの元のモデルを量子化しようとしましたが、精度は大幅に低下しています。Googleの古いFacemeshモデル(486 Landmarks)も同じ方法で量子化すると、まずまずのパフォーマンスが得られます。NXPも同じ観察結果を出していますか? 他にGoogleの最新のFaceMesh(478 Landmark)モデルの量子化を試したことがある人はいますか? 機械学習 Re: Availability of Quantized (INT8) Model for Latest MediaPipe Face Mesh (478 Landmarks) こんにちは、 現時点では利用できませんが、int8の改善に向けて社内でテストを行っています。 敬具。
View full article