Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
TEF82xx 底层驱动程序构建问题 你好, 我正在尝试版本 TEF82xx API 底层驱动程序 RFP9.3.0 20240920_PROD 以运行其中包含的示例,但遇到了问题: 找不到源文件:src/plf_sys.c 这个文件确实丢失了。与其他一些文件(plf_cap.c,plf_crc.c,plf_hio.c,等等)bc_api\bc_api_src\plf\CMakeLists.txt 所要求的。我可以在哪里找到这些文件? Re: TEF82xx Low Level Drivers build issue 你好, 是的你是对的。我在 TEF82xx API 底层驱动程序 RFP9.3.0 20240920_PROD.zip 软件包中没有看到该文件。 肯定是从其他代码包,软件包里拿出来的。名称plf_sys.c指向平台——驱动程序很可能期望它来自操作系统。 摘自 TEF82xx API 底层驱动程序 RFP9.3.0 20240920_PROD\TEF82xx_API_RN_V9.3.0.pdf petervlna_0-1783494576622.png 我在文档中没有找到更多信息。 顺祝商祺! Peter Re: TEF82xx Low Level Drivers build issue 你好, 是的你是对的。我在 TEF82xx API 底层驱动程序 RFP9.3.0 20240920_PROD.zip 软件包中没有看到该文件。 肯定是从其他代码包,软件包里拿出来的。名称plf_sys.c指向平台——驱动程序很可能期望它来自操作系统。 摘自 TEF82xx API 底层驱动程序 RFP9.3.0 20240920_PROD\TEF82xx_API_RN_V9.3.0.pdf petervlna_0-1783494576622.png 我在文档中没有找到更多信息。 顺祝商祺! Peter
記事全体を表示
IMX95LPD5EVK-19CM: UUU eMMC flash of L6.18.2 fails (LIBUSB errors on Linux and Windows) Hello NXP team, I need help upgrading IMX95LPD5EVK-19CM from the factory BSP to LF_v6.18.2-1.0.0 for eIQ Neutron NPU YOLO inference. UUU eMMC flashing fails on both Linux and Windows with different libusb errors at SDPS:boot. Details below. --- ## 1. Hardware | Item | Detail | |------|--------| | Board | IMX95LPD5EVK-19CM (i.MX 95 19×19 EVK, SOM + baseboard) | | Yocto machine / hostname | imx95-a1-19x19-lpddr5-evk | | Silicon | i.MX 95 A1 | | Storage | 64 GB eMMC (factory pre-flashed Linux) | | Power | 12 V on J5, SW4 ON | | Debug | J31 USB-C → host (serial, 115200) | | Flash port | J8 USB1 OTG USB-C → host | | Camera | Logitech C920 on J7 (/dev/video13) | --- ## 2. Software versions ### Current (factory eMMC — Linux boots normally) | Component | Version | |-----------|---------| | BSP | LF6.12.34_2.1.0 | | Kernel | 6.12.34-lts-next-gbe78e49cb433 | | Boot cmdline | root=/dev/mmcblk0p2 | | Neutron delegate | v1.0.0-be8bf399 | | libneutron_delegate.so | /usr/lib/libneutron_delegate.so | | Host converter (old) | eIQ Toolkit 1.17 / neutron-converter 2.1.3 | ### Target (downloaded, not yet flashed to eMMC) | Component | Version / file | |-----------|----------------| | BSP release | LF_v6.18.2-1.0.0 (SCR-6.18.2-1.0.0) | | Kernel (expected) | 6.18.2-1.0.0 | | Image package | LF_v6.18.2-1.0.0_images_IMX95 | | Boot image | imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all | | Rootfs | imx-image-full-imx95evk.wic (~11 GB) | | Neutron delegate (expected) | v1.0.0-7399a58e | | Host converter (ready on host) | eIQ Neutron SDK 3.0.1 (converter 3.0.1+0Xd5d7918e) | Reference: NXP forum engineer (Zhiming_Liu) validated YOLOv8m on i.MX95 with L6.18.2 + eIQ Neutron SDK 3.0.1 + delegate 7399a58e. --- ## 3. Application goal USB webcam person detection with YOLO (v8n / v11n) using: - INT8 TFLite export (Ultralytics) - neutron-converter --target imx95 - tflite_runtime + libneutron_delegate.so on board On current BSP (6.12.34): - NXP forum yolov8m_full_integer_quant_converted.tflite → SEGFAULT on NPU invoke (exit 139) - Custom yolov8n_neutron.tflite → invoke OK but 0 person detections - Headless backbone on NPU → constant garbage output (~1.13); CPU split pipeline works (56–90% detections) Conclusion: need L6.18.2 BSP on eMMC before NPU models converted with SDK 3.0.1 can be validated. --- ## 4. Host setup | Host | UUU version | Path | |------|-------------|------| | Ubuntu 24.04 (x86_64) | libuuu_1.5.243-0-g230f1b1 | /usr/local/bin/uuu | | Windows 10/11 | libuuu_1.5.243-0-g230f1b1 | uuu.exe (from mfgtools uuu_1.5.243 release) | Image directory on both hosts: LF_v6.18.2-1.0.0_images_IMX95 --- ## 5. Boot switch SW7 (per IMX95LPD5EVK-19CM QSG, 1=ON 0=OFF) | Mode | SW7-1 | SW7-2 | SW7-3 | SW7-4 | |------|-------|-------|-------|-------| | Serial Download (UUU) | 1 | 0 | 0 | 1 | | eMMC boot (normal) | 1 | 0 | 1 | 0 | eMMC boot (SW7=1010) works normally. Full power cycle performed before each SW7 change. --- ## 6. Flash procedure (eMMC via UUU) Board preparation (same for Linux and Windows): - SW7 = 1001 (Serial Download) - J8 (USB1 OTG) connected to host PC (not J31) - J31 connected for optional serial console - J5 12 V power connected - Board powered ON when uuu displays "Wait for Known USB Device" Command: uuu -b emmc_all imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all imx-image-full-imx95evk.wic (Linux: sudo uuu ... | Windows: uuu.exe ... from image directory) --- ## 7. UUU errors — Linux (Ubuntu 24.04) sudo /usr/local/bin/uuu -b emmc_all \ imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all \ imx-image-full-imx95evk.wic Output: uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.243-0-g230f1b1 Success 0 Failure 1 1:6-E3C50910 1/1 [HID(W): LIBUSB_ERROR_NO_DEVICE (-4)] SDPS: boot -scanterm -f imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all ... Notes: - lsusb briefly shows NXP USB device (1fc9:015d) in SDP mode - uuu sometimes prints "New USB Device Attached" then fails at SDPS: boot - Without sudo: permission denied (errno=13) - eMMC was not modified (flash did not complete) --- ## 8. UUU errors — Windows Host: Windows 10/11, PowerShell, uuu.exe 1.5.243 Working directory: C:\Users\Hardware.Team\Downloads\LF_v6.18.2-1.0.0_images_IMX95 ### Attempt — flash_all (expected correct boot image) PS C:\Users\Hardware.Team\Downloads\LF_v6.18.2-1.0.0_images_IMX95> & '..\uuu (2).exe' -b emmc_all imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all imx-image-full-imx95evk.wic uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.243-0-g230f1b1 Success 0 Failure 1 1:3-E3C50910 1/1 [HID(W): LIBUSB_ERROR_PIPE (-9)] SDPS: boot -scanterm -f imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all ... Summary of USB errors across hosts: | Host | Boot image | libusb error | |------|------------|--------------| | Ubuntu 24.04 | flash_all | LIBUSB_ERROR_NO_DEVICE (-4) | | Windows | flash_all | LIBUSB_ERROR_PIPE (-9) | All failures occur at the same step: SDPS: boot (before eMMC write progress). --- ## 9. What works today - SW7=1010 → boots factory eMMC Linux (6.12.34) normally - SSH over eth0 works - USB webcam (/dev/video13) detected - libneutron_delegate.so present (be8bf399) - CPU-side inference validated; NPU output incorrect on current BSP --- ## 10. Questions for NXP 1. For SDPS:boot failures with uuu 1.5.243 on IMX95LPD5EVK-19CM (A1), device 1fc9:015d, SW7=1001, J8 — what causes LIBUSB_ERROR_NO_DEVICE (-4) on Linux vs LIBUSB_ERROR_PIPE (-9) / LIBUSB_ERROR_IO (-1) on Windows? 2. Are there known uuu 1.5.243 + IMX95 A1 compatibility requirements (driver, WinUSB/Zadig on Windows, udev rules on Linux)? 3. Confirm imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all + imx-image-full-imx95evk.wic is the correct pair for IMX95LPD5EVK-19CM eMMC flash (not sd-ecc unless ECC RAM). 4. Any known Neutron delegate differences between be8bf399 (6.12.34) and 7399a58e (6.18.2) affecting YOLOv8 INT8 models? 5. Is there an alternative supported method to flash L6.18.2 to eMMC if UUU USB path fails on both Linux and Windows? --- ## 11. Logs available on request - Full uuu verbose log: uuu -v -b emmc_all ... (Linux and Windows) - Host lsusb / Device Manager / dmesg when board enters SDP mode - Serial console log (factory eMMC boot — working) - Board: uname -r, strings libneutron_delegate.so, NPU test results on 6.12.34 Thank you for guidance on completing the eMMC upgrade to L6.18.2-1.0.0 for Neutron NPU development. Best regards Re: IMX95LPD5EVK-19CM: UUU eMMC flash of L6.18.2 fails (LIBUSB errors on Linux and Windows) The A1 silicon of the i.MX 95 is no longer supported from our latest BSPs, 6.12.34 seems to be last one supporting A1. There is no workaround, you can't make the latest BSP work on A1 silicon, you need to upgrade your EVK with a new daughter card. The A1 silicon card is blue, the B0 silicon card is green. I didn't test a UUU download onto an old EVK using the 6.18.2 .wic image, but I expect that it fails the same way as it fails on your side. I'll do this in the next days. You could do a test with an SD-Card, program the .wic image on your PC to an SD-Card and try to run it on your EVK with boot mode set to SD-Card. Regards, Bernhard. Re: IMX95LPD5EVK-19CM: UUU eMMC flash of L6.18.2 fails (LIBUSB errors on Linux and Windows) Hello, Thanks for response. i have another query regrading same board. I am trying to run an M7 application on IMX95LPD5EVK-19 following AN14748, but I cannot flash flash.bin with UUU. The board is detected briefly, then SDPS boot fails immediately. Hardware: IMX95LPD5BB-19 REV A1 (2024 NXP B.V.) Boot switch (SW7[1:4]): 1001 (Serial Download) Target: eMMC Host: Ubuntu Linux UUU: libuuu_1.5.243-0-g230f1b1 SDKs tried (MCUXpresso SDK Builder): SDK_26.06.00_IMX95LPD5EVK-19 SDK_2.15.000_IMX95LPD5EVK-19 Both produce the same result. Command: cd IMX95LPD5EVK/build_/tmp/deploy/images/imx95-a1-19x19-lpddr5-evk sudo uuu -b emmc flash.bin   Error: Success 0 Failure 1 1:2-E3C50910 1/ 1 [HID(W): LIBUSB_ERROR_NO_DEVICE (-4)] SDPS: boot -f flash.bin   Steps followed (per AN14748): Set SW7 = 1001 with board powered off Connect USB to host Run sudo uuu -b emmc flash.bin Power-cycle board Fails at SDPS boot every time Questions: Which MCUXpresso SDK version is validated for IMX95LPD5BB-19 REV A1 M7 flashing? Is build target imx95-a1-19x19-lpddr5-evk correct for this hardware? Any known UUU issues or extra steps beyond AN14748 for this board revision? Should I use -b emmc or -b sd first, and which USB port should be used?
記事全体を表示
S32K344 chip, failed to download using bootloader after adding eMCEM_1 module in spd Sort out the logic and rewrite: As the title suggests, when I enabled eMCEM_1 in the app code, downloading the app using the official bootloader failed. If I didn't erase the chip, I couldn't enter the boot again, and even after powering it back on, it wouldn't solve the problem. I suspect that after powering it back on, the boot jumped to the app, but the app didn't run. When I disable eMCEM_1, this issue does not occur. How can I use boot to flash the app when eMCEM_1 is enabled Re: S32K344 chip, failed to download using bootloader after adding eMCEM_1 module in spd Hi @XPW, The problem description is not entirely clear. If the application is being programmed through the bootloader, the eMCEM_1 configuration contained in the application should not affect the programming process itself, since the application is not executed during download, it is just a binary. Only after the bootloader transfers execution to the application would eMCEM/FCCU-related configuration become relevant, and at that point, it would be useful to check: FCCU status registers DCM flags, MC_RGM flags. Or whether the application actually reaches main() Based on the current description, it is unclear whether the programming operation fails, or whether programming succeeds and the issue occurs later when the application starts executing. Could you clarify the exact sequence of events? Regards, Daniel Re: S32K344 chip, failed to download using bootloader after adding eMCEM_1 module in spd After my investigation, I found that some global variables were not initialized as defined when was enabled 。 Select a portion for explanation: Firstly, when I haven't enabled the target XPW_0-1783494597992.png Clock_ip. c under RTD file XPW_1-1783494731850.png XPW_2-1783494792174.png Power_ip. c under RTD file XPW_3-1783494883662.png XPW_4-1783494909192.png Can initialize correctly。 However, when I activated it: XPW_5-1783495188492.png XPW_6-1783495223242.png Clock_ip. c under RTD file XPW_7-1783495794585.png XPW_8-1783495823066.png Power_ip. c under RTD file XPW_9-1783495866324.png XPW_10-1783495886502.png Global variable initialization failed。 May I ask if there is a better solution? Re: S32K344 chip, failed to download using bootloader after adding eMCEM_1 module in spd Hi @XPW, Based on what I see in the screenshots, the variables are initialized correctly at first. However, after the eMCEM initialization, Clock_Ip_pfkNotificationsCallback contains an invalid pointer. eMCEM does not magically change the pointer value. This looks much more like one of the following issues: Startup initialization (.data copy / .bss initialization) is not completed correctly. RAM corruption occurs before main(). Linker sections overlap. Stack corruption. Can you test it with the linker file from the SPD demo project? BR, Daniel Re: S32K344 chip, failed to download using bootloader after adding eMCEM_1 module in spd The link file has been modified for the following. XPW_0-1783992772039.png XPW_1-1783993101988.png I have defined three global variables: XPW_2-1783993317537.png I found that when is not enabled, after executing init_data-bss, XPW_3-1783993342206.png XPW_4-1783993406406.png It seems to be aligned with 4 bytes and assigned correctly. But when I enable , after executing init_data-bss XPW_5-1783994068084.png XPW_6-1783994226472.png It doesn't seem to be aligned. Re: S32K344 chip, failed to download using bootloader after adding eMCEM_1 module in spd What is the cause of this phenomenon and how should I investigate and solve it. Re: S32K344 chip, failed to download using bootloader after adding eMCEM_1 module in spd HI @XPW, Based on the screenshots, I am not convinced there is actually a problem with the variable initialization itself. variable_a is an 8-bit variable, and enabling eMCEM will introduce additional variables, which can change the layout of the .data section. Therefore, seeing the variables at different offsets is expected and does not by itself indicate corruption. I think the key question is whether the issue occurs when the application is run standalone, or only when it is programmed and started through the bootloader. Can you reproduce the issue when programming the application directly with the debugger and running it without the bootloader? If the problem only occurs after loading the application through the bootloader, then the investigation should focus on the bootloader programming process, image layout, or bootloader handover rather than the application itself. BR, Daniel
記事全体を表示
Need help verifying CAN communication on the RD33772C14VEVM board Hello, My name is Hyewoon Jang. I am currently trying to test the RD33772C14VEVM board, and I have set up my environment as follows: Software: MBDT for BMS 1.2.0 + MBDT for S32K3xx 1.4.3 (I installed version 1.4.0 first and then applied the 1.4.3 patch.) Model: MBDT for BMS → BMS_Examples → rd33772c14vevm → rd33772c14vevm_s32ct → rd33772c14vevm_s32ct.mdl Hardware: The hardware is connected as shown in the attached photo. For now, I have not connected a battery, since I would like to check the basic operation of the model first. I am only supplying 12 V power to the board. After setting up the environment as described above, I tried to download the model to the board, but the download process shows “Could not connect to target.” Therefore, I imported the generated code into S32 Design Studio 3.5 and tried to download it from there. In S32DS, the build process completes successfully. Therefore, I connected the board to Vector CANalyzer in order to check whether any CAN messages are being transmitted from the board. However, no CAN messages are displayed in CANalyzer. Since I suspected that the issue might be related to the J-Link debugger, I also tried connecting the board using TRACE32. However, the reset indicator repeatedly turns red, and TRACE32 shows the error message “target power fail.” At this point, I simply want to verify whether the board is operating properly by checking if any CAN messages are transmitted. I really would like to resolve this issue. If there are any items that I should check, I would greatly appreciate it if you could let me know. I will follow your guidance and try each step. Could you please advise me on what I should do to solve this problem? #rd33772c14vevm, #CAN, #s32k344, #JTAG, #MBDT Re: Need help verifying CAN communication on the RD33772C14VEVM board Hello, First of all, I am sorry for the late reply. From the message you sent, I suspect that the board is not properly powered. I see that you built the application in S32DS too, but the build process to do not involve to deploy the application to the board. You have to create a Debug Configuration compatible for S32K344 and deploy the .elf from there. Since you didn't connect a battery yet, I recommend you to power the board from cell emulator instead of the beefy screws found on the EVB. I am not sure that you can power up the board using the Shunt resistor (R62), please thoroughly check the schematic. In the readme for the model, it states that you can power up the board from the emulator board: Connect the power supply to the emulator board: 12V -> BH1(K30_12V_L) and GND -> BH2(GND_KL31_DOWN) Let me know if this solves your problem. Best regards, Sorin Bancila
記事全体を表示
IMX95LPD5EVK-19CM:L6.18.2のUUU eMMCフラッシュが失敗(LinuxおよびWindowsでのLIBUSBエラー) NXPチームの皆様、こんにちは。 純正BSPからIMX95LPD5EVK-19CMをeIQ Neutron NPU YOLO推論のためにLF_v6.18.2-1.0.0にアップグレードするのに助けが必要です。UUU eMMCのフラッシュは、LinuxとWindowsの両方でSDPS:bootで異なるlibusbエラーで失敗します。詳細は下記をご覧ください。 --- ## 1. ハードウェア |アイテム|詳細 | |------|--------| |ボード|IMX95LPD5EVK-19CM(i.MX 95 19×19 EVK、SOM + ベースボード) | |Yocto マシン / ホスト名 |IMX95-a1-19x19-LPDDR5-EVK | |シリコン |i.MX 95 A1 | |ストレージ |64GB eMMC(工場出荷時の事前フラッシュ済みLinux) | |パワー|J5に12V、SW4オン | |デバッグ |J31 USB-C →ホスト(シリアル番号115200) | |フラッシュポート |J8 USB1 OTG USB-C →ホスト | |カメラ |J7上のLogitech C920(/dev/video13) | --- ## 2.ソフトウェアのバージョン ### 現在(純正eMMC — Linuxは通常起動) | コンポーネント | バージョン | |-----------|---------| | BSP | LF6.12.34_2.1.0| |カーネル |6.12.34-lts-next-gbe78e49cb433 | |Boot cmdline |root=/dev/mmcblk0p2 | |Neutron delegate |v1.0.0-be8bf399 | |libneutron_delegate.so |/usr/lib/libneutron_delegate.so | |ホストコンバータ(旧) |eIQツールキット1.17 / Neutronコンバーター2.1.3| ### ターゲット(ダウンロード済み、eMMCへの書き込みはまだ完了していません) |コンポーネント |バージョン / ファイル | |-----------|----------------| |BSPリリース |LF_v6.18.2-1.0.0 (SCR-6.18.2-1.0.0) | |カーネル(期待値) |6.18.2-1.0.0 | |画像パッケージ |LF_v6.18.2-1.0.0_images_IMX95 | |ブートイメージ |imx-boot-imx95-19x19-lpddr5-evk-sd.bin flash_all| |根源 |imx-image-full-imx95evk.wic(~11 GB) | |Neutron代理(期待) |v1.0.0-7399A58E | |ホストコンバータ(ホストで準備完了) |eIQ Neutron SDK 3.0.1 (converter 3.0.1+0Xd5d7918e)| 参考:NXPフォーラムエンジニア(Zhiming_Liu)がi.MX95上でYoloV8mをL6.18.2+eIQ Neutron SDK 3.0.1+delegate 7399a58eで検証しました。 --- ## 3.アプリケーション目的 YOLO(v8n / v11n)でのUSBウェブカメラの人物検出方法: - INT8 TFLite エクスポート(Ultralytics) - Neutron コンバータ --ターゲットIMX95 - tflite_runtime + libneutron_delegate.SO 搭載 現在のBSP(6.12.34)では: - NXPフォーラム yolov8m_full_integer_quant_converted.tflite → NPU呼び出しでセグメンテーション違反 (終了コード139) - カスタム yolov8n_neutron.tflite → 呼び出しは成功しましたが、人物検出数は0です - NPU上のヘッドレスバックボーン → 常にガベージ出力(約1.13)CPU分割パイプラインは正常に動作する(検出率56~90%) 結論:SDK 3.0.1で変換されたNPUモデルを検証するには、eMMC上でL6.18.2 BSPが必要です。 --- ## 4. ホスト設定 | ホスト | UUU バージョン | パス | |------|-------------|------| | Ubuntu 24.04 (x86_64) | libuuu_1.5.243-0-g230f1b1 | /usr/local/bin/uuu | | Windows 10/11 | libuuu_1.5.243-0-g230f1b1 | uuu.exe (mfgtools uuu_1.5.243 リリースより) | 両ホスト上のイメージディレクトリ: LF_v6.18.2-1.0.0_images_IMX95 --- ## 5.ブートスイッチSW7(IMX95LPD5EVK-19CM QSGごと、1=ON 0=OFF) | モード | SW7-1 | SW7-2 | SW7-3 | SW7-4 | |------|-------|-------|-------|-------| |シリアルダウンロード (UUU) | 1 | 0 | 0 | 1 | | eMMC ブート (通常) | 1 | 0 | 1 | 0 | eMMCブート(SW7=1010)は正常に動作します。SW7の交換前には必ず、電源の完全な投入サイクルを実施してください。 --- ## 6. フラッシュ手順 (UUU 経由の eMMC) 基板準備(LinuxとWindowsでも同様): - SW7 = 1001(シリアルダウンロード) - J8(USB1 OTG)はホストPCにコネクテッド(J31ではありません) - オプションのシリアルコンソール用にJ31コネクテッド - J5 12 V電源コネクテッド - 「既知のUSBデバイスを待機中」と表示されたときにボードが電源オン コマンド: uuu -b emmc_all imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_allimx-image-full-imx95evk.wic (Linux: sudo uuu ... |ウィンドウズ:uuu.exe...画像ディレクトリより) --- ## 7.UUU errors — Linux (Ubuntu 24.04) sudo /usr/local/bin/uuu -b emmc_all \ imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all\ imx-image-full-imx95evk.wic 出力: NXP IMXチップ用uuu(Universal Update Utility)-- libuuu_1.5.243-0-g230f1b1 成功 0 失敗 1 1:6-E3C50910 1/1 [HID(W): LIBUSB_ERROR_NO_DEVICE (-4)] SDPS: boot -scanterm -f imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all... 注: - lsusb は、NXP USB デバイス (1fc9:015d) が SDP モードであることを短時間表示します。 - uuu は時々「新しい USB デバイスが接続されました」と表示した後、SDPS: ブートで失敗します - sudoなしの場合:権限が拒否されました(errno=13) - eMMCは変更されませんでした(フラッシュ書き込みが完了しませんでした) --- ## 8. UUUエラー — Windows ホスト: Windows 10/11、PowerShell、uuu.exe 1.5.243 作業ディレクトリ:C:\Users\Hardware.Team\Downloads\LF_v6.18.2-1.0.0_images_IMX95 ### 試行 — flash_all (正しいブートイメージが期待される) PS C:\Users\Hardware.Team\Downloads\LF_v6.18.2-1.0.0_images_IMX95> & '..\uuu (2).exe' -b emmc_all imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_allimx-image-full-imx95evk.wic NXP IMXチップ用uuu(Universal Update Utility)-- libuuu_1.5.243-0-g230f1b1 成功 0 失敗 1 1:3-E3C50910 1/1 [HID(W): LIBUSB_ERROR_PIPE (-9)] SDPS: boot -scanterm -f imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all... 各ホストにおけるUSBエラーの概要: | ホスト | ブートイメージ | libusb エラー | |------|------------|--------------| | Ubuntu 24.04 | flash_all | LIBUSB_ERROR_NO_DEVICE (-4) | | Windows | flash_all | LIBUSB_ERROR_PIPE (-9) | すべての障害は同じステップで発生します:SDPS:ブート(eMMC書き込み処理前)。 --- ## 9. 今日通用するもの - SW7=1010 →通常、工場出荷時のeMMC Linux(6.12.34)を起動します - eth0上のSSH作業 - USBウェブカメラ(/dev/video13)を検出 - libneutron_delegate.so present(be8bf399) - CPU側の推論検証;現在のBSPでのNPU出力が不正確です --- ## 10.NXPへの質問 1.IMX95LPD5EVK-19CM(A1)、デバイス1fc9:015d、SW7=1001、J8でuuu 1.5.243を搭載したSDPS:ブート失敗の場合、LinuxでLIBUSB_ERROR_NO_DEVICE(-4)がLIBUSB_ERROR_PIPE(-9)/LIBUSB_ERROR_IO(-1)になる原因は何ですか? 2. 既知のuuu 1.5.243はありますか?+ IMX95 A1の互換性要件(ドライバ、WindowsのWinUSB/Zadig、Linuxのudevルール)について? 3. imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all + imx-image-full-imx95evk.wic が IMX95LPD5EVK-19CM eMMC フラッシュ (ECC RAM でない限り sd-ecc ではない) の正しい組み合わせであることを確認します。 4. be8bf399(6.12.34)と7399a58e(6.18.2)の間に、YOLOv8 INT8モデルに影響を与える既知のNeutronデリゲートの違いはありますか? 5. LinuxとWindowsの両方でUUUのUSBパスが失敗した場合に、L6.18.2をeMMCにフラッシュする代替の方法はありますか? --- ## 11.ログはご要望に応じて提供いたします。 - 完全なuuuu詳細ログ:uuu -v -b emmc_all...(LinuxおよびWindows) - ボードがSDPモードに入った際のホストLSUSB / デバイスマネージャー / dmesg - シリアルコンソールログ(工場出荷時のeMMC起動 — 動作中) - ボード:uname -r、文字列libneutron_delegate.so、NPUテスト結果は1934年12月6日 Neutron NPU開発のためのeMMCアップグレードをL6.18.2-1.0.0に完成させるためのご指導ありがとうございます。 よろしくお願いいたします。 Re: IMX95LPD5EVK-19CM: UUU eMMC flash of L6.18.2 fails (LIBUSB errors on Linux and Windows) i.MX 95のA1シリコンは、最新のBSPではサポートされなくなりました。6.12.34がA1をサポートする最後のバージョンと思われます。 回避策はありません。最新のBSPをA1シリコンで動かすことはできません。EVKを新しいドーターカードでアップグレードする必要があります。A1シリコンカードは青色、B0シリコンカードは緑色です。 6.18.2の.wicファイルを使用して古いEVKにUUUダウンロードをテストしていません。画像ですが、おそらくそちら側と同じように失敗すると思います。数日中にやります。SDカードでテストして、.wicをプログラムすることもできますPC上のイメージをSDカードにコピーし、ブートモードをSDカードに設定してEVKで実行してみてください。 よろしくお願いいたします。 ベルンハルト。 Re: IMX95LPD5EVK-19CM: UUU eMMC flash of L6.18.2 fails (LIBUSB errors on Linux and Windows) こんにちは、 ご回答ありがとうございます。同じ掲示板に関して、もう一つ質問があります。 IMX95LPD5EVK-19 follow AN14748 でM7アプリケーションを実行しようとしていますが、フラッシュできません flash.binUUUと共に。ボードは短時間検出されるが、その後すぐにSDPSの起動に失敗する。 ハードウェア: IMX95LPD5BB-19 REV A1 (2024 NXP B.V.) ブートスイッチ(SW7[1:4]): 1001(シリアルダウンロード) ターゲット: eMMC ホスト: Ubuntu Linux うーん: libuuu_1.5.243-0-g230f1b1 試したSDKs(MCUXpresso SDK Builder): SDK_26.06.00_IMX95LPD5EVK-19 SDK_2.15.000_IMX95LPD5EVK-19 どちらも同じ結果を生み出す。 コマンド: cd IMX95LPD5EVK/build_/tmp/deploy/images/imx95-a1-19x19-lpddr5-evk sudo uuu -b emmc flash.bin   エラー: 成功 0 失敗 1 1:2-E3C50910 1/1 [HID(W): LIBUSB_ERROR_NO_DEVICE (-4)] SDPS: boot -f flash.bin   実施された手順(AN14748に基づく): ボードの電源をオフにした状態で、SW7を1001に設定します。 USBをホストに接続します 走る sudo uuu -b emmc flash.bin 電源サイクルボード SDPSの起動に毎回失敗する 質問: どのMCUXpresso SDKバージョンが IMX95LPD5BB-19 REV A1 M7のフラッシュに有効ですか? ビルドターゲット imx95-a1-19x19-lpddr5-evk このハードウェアには正しいですか? この基板改訂版に関して、既知のUUUに関する問題や、AN14748以外に追加の手順はありますか? 使うべきでしょうか -b emmc または -b sd まず、どのUSBポートを使用すればよいでしょうか?
記事全体を表示
TEF82xx 低レベルドライバーのビルド問題 こんにちは、 TEF82xx API Low Level ドライバ RFP9.3.0 20240920_PRODをビルドして、含まれている例を実行しようとしているのですが、問題が発生しています: ソースファイルが見つからない:src/plf_sys.c そして、このファイルは本当に見つからないのです。他のいくつかの例と同様に (plf_cap.c、plf_crc.c、plf_hio.c、bc_api\bc_api_src\plf\CMakeLists.txt で必要とされるものなど。これらのファイルはどこで見つけられますか? Re: TEF82xx Low Level Drivers build issue こんにちは、 はい、おっしゃる通りです。TEF82xx API Low Level ドライバ RFP9.3.0 20240920_PROD.zipパッケージにはそのファイルが見当たりません。 他のパッケージからのものに違いない。名前plf_sys.cプラットフォームを指している可能性が高いです。おそらくドライバはOSからのものだと想定しているのでしょう。 TEF82xx API 低レベルドライバ RFP9.3.0 20240920_PROD\TEF82xx_API_RN_V9.3.0.pdf petervlna_0-1783494576622.png ドキュメントにはそれ以上の情報は見つかっていません。 よろしくお願いいたします。 ピーター Re: TEF82xx Low Level Drivers build issue こんにちは、 はい、おっしゃる通りです。TEF82xx API Low Level ドライバ RFP9.3.0 20240920_PROD.zipパッケージにはそのファイルが見当たりません。 他のパッケージからのものに違いない。名前plf_sys.cプラットフォームを指している可能性が高いです。おそらくドライバはOSからのものだと想定しているのでしょう。 TEF82xx API 低レベルドライバ RFP9.3.0 20240920_PROD\TEF82xx_API_RN_V9.3.0.pdf petervlna_0-1783494576622.png ドキュメントにはそれ以上の情報は見つかっていません。 よろしくお願いいたします。 ピーター
記事全体を表示
有没有比较简单易用的8位微控制器/汇编语言? 我正在寻找一款可以查看实际十六进制/二进制代码的 8 位微控制器。我在大学学习 8051 汇编语言,我非常喜欢看到和理解内存中的每一条指令和值。但是这些微控制器已经过时,需要很多“破解”才能兼容。至少每次我把代码放到真正的硬件上运行时,都会有这种感觉。那么,有没有一种简单的8位汇编语言,可以配合实际的芯片,让我能够编写简单的电子项目程序呢? Re: Is there a simple 8 bit microcontroller/assembly language that is nice to work with? 你好, 恩智浦半导体有8位设备的产品目录,您可以选择S08SG|8位小封装SG MCU | 恩智浦半导体设备。 S08SG 系列是一款入门级到中端设备,具备通用功能。 CodeWarrior 工具中包含了 S08SG 设备。 CodeWarrior 工具版本 11.1 支持 Windows 11,该工具支持不同的连接方式 [P&E USB Multilink Universal / USB Multilink、P&E Cyclone、开源 BDM、P&E 全芯片仿真]。 您可以从以下链接下载该工具: CodeWarrior ® for MCUs (Eclipse IDE) v11.1 在 CW 工具中,进入调试模式时,会有一个反汇编视图部分,其中显示加载的程序,该程序以汇编语言指令与源代码混合的形式进行比较。 此致敬礼,路易斯 Re: Is there a simple 8 bit microcontroller/assembly language that is nice to work with? 以下是一些您还可以探索的 8 位控制器。 pic16lf18326-i-sl/2263047 Microchip 的 PIC16LF18326-I/SL 是一款 14 引脚 8 位微控制器,具有 16KB 闪存、1KB RAM、12 位 ADC、10 个 PWM 通道、I2C、SPI 和 UART 接口,低功耗,工作电压为 2.3V 至 5.5V。 atmega8l-8mu/258363 MICROCHIP 的 ATMEGA8L-8MU 是一款 8 位 AVR 微控制器,具有 8MHz 频率、8KB Flash、32 引脚 VQFN 封装、I2C、SPI、UART 接口,工作电压为 2.7V-5.5V。温度范围为-40°C至85°C。
記事全体を表示
需要帮助验证 RD33772C14VEVM 板上的 CAN 通信 你好, 我的名字是张惠云。 我目前正在测试RD33772C14VEVM开发板,我的测试环境设置如下: 软件: MBDT for 电池管理系统 1.2.0 + MBDT for S32K3xx 1.4.3 (我先安装了 1.4.0 版本,然后应用了 1.4.3 补丁。) 模型: MBDT for 电池管理系统 → 电池管理系统_Examples → rd33772c14vevm → rd33772c14vevm_s32ct → rd33772c14vevm_s32ct.mdl 硬件: 硬件连接方式如图所示。 目前我还没有连接电池,因为我想先检查一下模型的基本运行情况。我只给电路板提供 12V 电源。 按照上述步骤设置好环境后,我尝试将模型下载到开发板上,但下载过程显示“无法连接到目标”。 因此,我将生成的代码导入到 S32 Design Studio 3.5 中,并尝试从那里下载它。在 S32DS 中,构建过程成功完成。 因此,我将电路板连接到 Vector CANalyzer,以检查电路板是否正在发送任何 CAN 消息。但是,CANalyzer 中没有显示任何 CAN 消息。 由于我怀疑问题可能与 J-Link 调试器有关,所以我还尝试使用 TRACE32 连接电路板。但是,复位指示灯反复变红,TRACE32 显示错误信息“目标电源故障”。 此时,我只想通过检查是否有 CAN 消息发送来验证电路板是否正常工作。 我真的很想解决这个问题。 如果还有什么需要我检查的项目,请您告知,我将不胜感激。我会按照您的指导,一步一步地尝试。 请问我应该如何解决这个问题? #rd33772c14vevm,#CAN,#s32k344,#JTAG,#MBDT Re: Need help verifying CAN communication on the RD33772C14VEVM board 你好, 首先,很抱歉回复晚了。 从你发来的信息来看,我怀疑电路板没有正常通电。我看到您也在 S32DS 中构建了应用程序,但是构建过程并不涉及将应用程序部署到电路板上。您需要创建一个与 S32K344 兼容的调试配置,并部署 .elf 文件。从那里开始。 由于你还没有连接电池,我建议你使用电池模拟器为电路板供电,而不是使用 EVB 上的粗螺丝供电。我不确定您是否可以使用分流电阻(R62)为电路板供电,请仔细检查电路图。 该模型的自述文件中提到,可以通过模拟器板为电路板供电: 将电源连接到仿真板:12V > BH1(K30_12V_L) 和 GND > BH2(GND_KL31_DOWN) 请告诉我这是否解决了您的问题。 此致, 索林·班奇拉
記事全体を表示
IMX95LPD5EVK-19CM:L6.18.2 版本的 UUU eMMC 闪存出现故障(Linux 和 Windows 系统均出现 LIBUSB 错误) 您好,NXP团队, 我需要帮助将 IMX95LPD5EVK-19CM 从工厂 BSP 升级到 LF_v6.18.2-1.0.0,以便进行 eIQ Neutron NPU YOLO 推理。UUU eMMC 刷写在 Linux 和 Windows 系统上均失败,在 SDPS:启动 处出现不同的 libusb 错误。详情如下。 --- 1. 硬件 | 项目 | 详情 | |------|--------| | 板 | IMX95LPD5EVK-19CM(i.MX 95 19×19 EVK,SOM + 基板)| | Yocto 机器/主机名 | imx95-a1-19x19-lpddr5-evk | | 硅 | i.MX 95 A1 | | 存储 | 64 GB eMMC(出厂预装 Linux 系统) | | 电源 | J5 接 12V,SW4 打开 | | 调试 | J31 USB-C → 主机(串口,115200) | | 闪存端口 | J8 USB1 OTG USB-C → 主机 | | 摄像头 | 罗技 C920,J7 接口 (/dev/video13) | --- 2. 软件版本 ### 当前版本(出厂 eMMC — Linux 正常启动) | 元器件 | 版本 | |-----------|---------| | BSP | LF6.12.34_2.1.0| | 内核 | 6.12.34-lts-next-gbe78e49cb433 | | 启动命令行 | root=/dev/mmcblk0p2 | | Neutron 委托 | v1.0.0-be8bf399 | | libneutron_delegate.so | /usr/lib/libneutron_delegate.so | |主机变流器(旧)| eIQ 工具包 1.17 / 中子变流器 2.1.3| ### 目标(已下载,尚未刷写到 eMMC) | 组件 | 版本/文件 | |-----------|----------------| | BSP 版本 | LF_v6.18.2-1.0.0 (SCR-6.18.2-1.0.0) | | 内核(预期) | 6.18.2-1.0.0 | | 图像包 | LF_v6.18.2-1.0.0_images_IMX95 | | 启动镜像 | imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all| | 根文件系统 | imx-image-full-imx95evk.wic (约 11 GB) | | Neutron 委托(预期) | v1.0.0-7399a58e | | 主机变流器(主机端已准备就绪) | eIQ Neutron SDK 3.0.1(变流器 3.0.1+0Xd5d7918e)| 参考:NXP 论坛工程师 (Zhiming_Liu) 在 i.MX95 上使用 L6.18.2 + eIQ Neutron SDK 3.0.1 + delegate 7399a58e 验证了 YOLOv8m。 --- 3. 应用目标 使用 YOLO (v8n / v11n) 进行 USB 网络摄像头人脸检测: - INT8 TFLite 导出(Ultralytics) - 中子变流器 --target imx95 - 板载 tflite_runtime + libneutron_delegate.so 基于当前 BSP (6.12.34): - NXP 论坛 yolov8m_full_integer_quant_converted.tflite → NPU 调用时发生段错误(退出代码 139) - 自定义 yolov8n_neutron.tflite → 调用成功,但未检测到任何人 - 无头骨架构在 NPU 上运行 → 持续输出垃圾数据(~1.13);CPU拆分流水线工作正常(检测率56%–90%) 结论:在验证使用 SDK 3.0.1 转换的 NPU 模型之前,需要在 eMMC 上使用 L6.18.2 BSP。 --- 4. 主机设置 | 主机 | UUU 版本 | 路径 | |------|-------------|------| | Ubuntu 24.04 (x86_64) | Ubuntu 24.04 (x86_64) libuuu_1.5.243-0-g230f1b1 | /usr/local/bin/uuu | /usr/local/bin/uuu | /usr/local/bin/uuu | Windows 10/11 | libuuu_1.5.243-0-g230f1b1 | uuu.exe(来自 mfgtools uuu_1.5.243 版本) | 两台主机上的镜像目录: LF_v6.18.2-1.0.0_images_IMX95 --- ## 5. 启动开关 SW7(根据 IMX95LPD5EVK-19CM 快速入门指南,1=开,0=关) | 模式 | SW7-1 | SW7-2 | SW7-3 | SW7-4 | |------|-------|-------|-------|-------| |串行下载 (UUU) | 1 | 0 | 0 | 1 | | eMMC 启动(正常) | 1 | 0 | 1 | 0 | eMMC 启动(SW7=1010)工作正常。每次更改SW7之前,都需执行完整的电源循环。 --- ## 6. 闪存程序(通过 UUU 的 eMMC) 板准备(Linux 和 Windows 系统相同): - SW7 = 1001(序列号下载) - J8(USB1 OTG)连接到主机(不是 J31) - J31 连接可选的串行控制台 - J5 已连接 12V 电源 - 当 uuu 显示“等待已知的 USB 设备”时,板已通电 命令: uuu -b emmc_all imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_allimx-image-full-imx95evk.wic (Linux:sudo uuu ... | Windows:uuu.exe ... 从镜像目录运行) --- ## 7. UUU 错误 — Linux (Ubuntu 24.04) sudo /usr/local/bin/uuu -b emmc_all \ imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all\ imx-image-full-imx95evk.wic 输出: 适用于 NXP imx 芯片的 uuu(通用更新实用程序)-- libuuu_1.5.243-0-g230f1b1 成功 0 失败 1 1:6-E3C50910 1/1 [HID(W): LIBUSB_ERROR_NO_DEVICE (-4)] SDPS: boot -scanterm -f imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all... 笔记: - lsusb 命令短暂显示 NXP USB 设备 (1fc9:015d) 处于 SDP 模式 - uuu 有时会打印“已连接新 USB 设备”,然后在 SDPS: 启动时失败。 - 未使用 sudo:权限被拒绝(错误号=13) - eMMC 未修改(闪存未完成) --- ## 8. UUU 错误 — Windows 主机:Windows 10/11,PowerShell,uuu.exe 1.5.243 工作目录:C:\Users\Hardware.Team\Downloads\LF_v6.18.2-1.0.0_images_IMX95 ### 尝试 — flash_all(预期正确的启动映像) PS C:\Users\Hardware.Team\Downloads\LF_v6.18.2-1.0.0_images_IMX95> & '..\uuu (2).exe' -b emmc_all imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_allimx-image-full-imx95evk.wic 适用于 NXP imx 芯片的 uuu(通用更新实用程序)-- libuuu_1.5.243-0-g230f1b1 成功 0 失败 1 1:3-E3C50910 1/1 [HID(W): LIBUSB_ERROR_PIPE (-9)] SDPS: boot -scanterm -f imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all... 各主机USB错误汇总: | 主机 | 启动映像 | libusb 错误 | |------|------------|--------------| | Ubuntu 24.04 | flash_all | LIBUSB_ERROR_NO_DEVICE (-4) | | Windows | flash_all | LIBUSB_ERROR_PIPE (-9) | 所有故障都发生在同一步骤:SDPS:启动(在 eMMC 写入进度之前)。 --- 9. 如今哪些方法行之有效 - SW7=1010 → 正常启动出厂 eMMC Linux (6.12.34)。 - 通过 eth0 进行 SSH 连接正常 检测到 USB 网络摄像头 (/dev/video13) - libneutron_delegate.so 存在 (be8bf399) - CPU端推理已验证;当前电路板支持包。上的NPU输出不正确 --- 10.向恩智浦提出的问题 1.对于在 IMX95LPD5EVK-19CM (A1) 上,使用 uuu 1.5.243 版本,设备 1fc9:015d,SW7=1001,J8 时 SDPS:启动 失败的情况,Linux 上出现 LIBUSB_ERROR_NO_DEVICE (-4) 错误的原因是什么?而 Windows 上出现 LIBUSB_ERROR_PIPE (-9) / LIBUSB_ERROR_IO (-1) 错误的原因又是什么? 2. 是否有已知的 uuu 1.5.243+ IMX95 A1 兼容性要求(驱动程序、Windows 上的 WinUSB/Zadig、Linux 上的 udev 规则)? 3. 确认 imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all + imx-image-full-imx95evk.wic 是 IMX95LPD5EVK-19CM eMMC 闪存的正确配对(除非是 ECC RAM,否则不是 sd-ecc)。 4. be8bf399 (6.12.34) 和 7399a58e (6.18.2) 之间是否存在已知的中子代表差异,从而影响 YOLOv8 INT8 模型? 5. 如果在 Linux 和 Windows 系统上 UUU USB 路径均失败,是否有其他受支持的方法将 L6.18.2 刷写到 eMMC? --- 11.日志可应要求提供 - 完整的 uuu 详细日志:uuu -v -b emmc_all ...(Linux 和 Windows) - 当主板进入 SDP 模式时,运行主机 lsusb / 设备管理器 / dmesg 命令 - 串口控制台日志(工厂 eMMC 启动 — 正常) - 板:uname -r,字符串 libneutron_delegate.so,NPU 测试结果(版本 6.12.34) 感谢您对 Neutron NPU 开发中 eMMC 升级到 L6.18.2-1.0.0 的指导。 顺祝商祺! Re: IMX95LPD5EVK-19CM: UUU eMMC flash of L6.18.2 fails (LIBUSB errors on Linux and Windows) i.MX 95 的 A1 芯片已不再受我们最新的 BSP 支持,6.12.34 似乎是最后一个支持 A1 的版本。 没有变通办法,你不能让最新的 电路板支持包。 在 A1 芯片上运行,你需要用新的子卡升级你的 EVK。A1硅卡为蓝色,B0硅卡为绿色。 我没有使用 6.18.2 .wic 文件在旧款 EVK 上测试过 UUU 下载。图片显示正常,但我预计它在您那边出现的问题与之前一样。我会在接下来的几天里完成这件事。你可以用SD卡做个测试,对.wic文件进行编程。将电脑上的镜像文件复制到 SD 卡上,然后尝试在 EVK 上运行该镜像文件,并将启动模式设置为 SD 卡。 问候, 伯恩哈德。 Re: IMX95LPD5EVK-19CM: UUU eMMC flash of L6.18.2 fails (LIBUSB errors on Linux and Windows) 你好, 谢谢回复。我还有关于同一板的另一个问题。 我正在尝试运行一个 M7 应用程序 IMX95LPD5EVK-19 下列的 AN14748 ,但我无法刷机。 flash.bin 用 UUU。短暂检测到电路板后,SDPS 启动立即失败。 硬件: IMX95LPD5BB-19 修订版 A1 (2024 NXP BV) 启动开关(SW7[1:4]): 1001(序列号下载) 目标: eMMC 主持人: Ubuntu Linux UUU: libuuu_1.5.243-0-g230f1b1 尝试过的 SDK(MCUXpresso SDK Builder): SDK_26.06.00_IMX95LPD5EVK-19 SDK_2.15.000_IMX95LPD5EVK-19 两者产生的结果相同。 命令: cd IMX95LPD5EVK/build_/tmp/deploy/images/imx95-a1-19x19-lpddr5-evk sudo uuu -b emmc flash.bin   错误: 成功 0 失败 1 1:2-E3C50910 1/ 1 [HID(W): LIBUSB_ERROR_NO_DEVICE (-4)] SDPS: 启动 -f flash.bin   执行步骤(根据 AN14748): 在电路板断电的情况下,将 SW7 设置为 1001 将 USB 连接到主机 跑步 sudo uuu -b emmc flash.bin 电源循环板 每次 SDPS 启动都失败 问题: 哪个 MCUXpresso SDK 版本经过验证? IMX95LPD5BB-19 REV A1 M7 闪烁? 构建目标 imx95-a1-19x19-lpddr5-evk 对这套硬件来说合适吗? 针对此电路板版本,是否存在已知的 UUU 问题或除 AN14748 之外的额外步骤? 我应该使用 -b emmc 或者 -b sd 首先,应该使用哪个USB端口?
記事全体を表示
S32K344の開発ボードはOpenSDAではフラッシュできません。 S32K344の開発ボードはOpenSDAではフラッシュできません。 djaylou_3-1783083734014.png djaylou_2-1783083701367.png Re: The S32K344 development board cannot be flashed using OpenSDA. こんにちは、 @djaylou さん。 現在使用しているボードは、FRDM-A-S32K344、S32K3X4EVB-T172、またはS32K344-WBのどれですか?また、機器の電源が正しく供給されているか確認してもらえますか? BR、VaneB
記事全体を表示
S32K358 MBDT Referenced Model Build Failure Hi, I am using MATLAB R2024b and NXP MBDT for S32K358. I have a standalone NXP CAN communication model that builds, flashes, and runs correctly on hardware (10 Hz CAN Tx/Rx). I also have a separate BMS algorithm model (Offline_Test) containing referenced models, state machines, estimators, and fault management logic. When I integrate the BMS algorithm into the working NXP model and build, MBDT generates a separate configuration folder for a referenced model (BMS_Out_Config) and fails with: fatal error: Mcl.h: No such file or directory #include The error comes from: Controller/BMS_Out_Config/src/mbdt_board_init.c while Mcl.h is not generated in: Controller/BMS_Out_Config/RTD/include My question is: Should algorithm-only referenced models have their own hardware configuration/RTD generation? Or should they inherit the top-level hardware model configuration? Is there a recommended workflow for integrating large algorithmic referenced models into an existing S32K3 hardware project? Screenshots of the working NXP model, the BMS algorithm model, and the build error are attached. Thanks.
記事全体を表示
S32K3_RTD_7_0_0のダウンロードリンクについて NXPのHPから、以下の条件のRTDのExeをダウンロードしたく、探したのですが見つかりません。 ダウンロードリンクを教えていただけないでしょうか? 急いでいるのでご回答いただけると助かります。 S32K3_RTD_7_0_0_D2510_ASR_REL_4_9_REV_0000_20251031 こちらで探したところ、近しいものとして以下をダウンロードできたのですが 上記の条件のRTDを必要としています。 SW32K3_S32M27x_RTD_R21-11_6.0.0_QLP04_HF01_D2510.exe SW32K3_S32M27x_RTD_R23-11_7.0.0_D2511.exe SW32K3_S32M27x_RTD_R23-11_7.0.0_QLP03_D2512.exe Re: S32K3_RTD_7_0_0のダウンロードリンクについて ハイ EBTresosまたはS32DSを使用する必要がありますか? EBTresosを使用する場合は、S32K3_S32M27xリアルタイム・ドライバASR R23-11バージョン7.0.0をダウンロードしてインストールしてください(SW32K3_S32M27x_RTD_R23-11_7.0.0_D2511.exe) S32DSを使用する必要がある場合は、S32K3_S32M27xリアルタイム・ドライバASR R23-11バージョン7.0.0をダウンロードしてください(SW32K3_S32M27x_RTD_R23-11_7.0.0_D2511_DesignStudio_updatesite.zip) よろしくお願いいたします ロビン
記事全体を表示
S32K344チップ、spdにeMCEM_1モジュールを追加した後、ブートローダーを使用してダウンロードに失敗しました。 ロジックを整理して書き直します。タイトルにあるように、アプリコードでeMCEM_1を有効にすると、公式ブートローダーを使用したアプリのダウンロードが失敗しました。チップを消去しなければ、再びブート画面に入ることができず、電源を入れ直しても問題は解決しなかった。電源を入れ直した後、起動プロセスでアプリが起動したものの、アプリが起動しなかったのではないかと推測しています。eMCEM_1を無効にすると、この問題は発生しません。eMCEM_1が有効になっているときに、Bootでアプリを書き換えるにはどうすればいいですか Re: S32K344 chip, failed to download using bootloader after adding eMCEM_1 module in spd こんにちは、 @XPW さん。 問題の説明が必ずしも明確ではない。 もしアプリケーションがブートローダーを通じてプログラムされている場合、アプリケーションに含まれるeMCEM_1設定はダウンロード中に実行されるわけではなく、単なるバイナリであるため、プログラミングプロセス自体に影響を与えることはありません。 ブートローダーがアプリケーションへの実行を転送した後にのみ、eMCEM/FCCU関連の設定が重要になり、その時点で以下の点を確認することが有用です。 FCCUステータス登録簿 DCMフラグ、MC_RGMフラグ。 また、アプリケーションが実際にmain()に到達するかどうかも重要です。 現在の説明からは、プログラミング操作が失敗するのか、プログラムが成功して問題がアプリケーションの実行開始時に起こるのかは不明です。 出来事の正確な順序を説明していただけますか? よろしくお願いいたします。 ダニエル Re: S32K344 chip, failed to download using bootloader after adding eMCEM_1 module in spd 調査の結果、 が有効になった際に、一部のグローバル変数が定義どおりに初期化されていなかったことが判明しました 。 説明が必要な箇所を選択してください: まず、ターゲットを有効にしていないとき XPW_0-1783494597992.png Clock_ip.c(RTDファイル内) XPW_1-1783494731850.png XPW_2-1783494792174.png Power_ip。c は RTD ファイル内 XPW_3-1783494883662.png XPW_4-1783494909192.png Can initialize correctly。 しかし、起動したとき: XPW_5-1783495188492.png XPW_6-1783495223242.png Clock_ip.c(RTDファイル内) XPW_7-1783495794585.png XPW_8-1783495823066.png Power_ip.c は RTD ファイル内にあります。 XPW_9-1783495866324.png XPW_10-1783495886502.png グローバル変数の初期化に失敗しました。 もっと良い解決策はありますでしょうか? Re: S32K344 chip, failed to download using bootloader after adding eMCEM_1 module in spd こんにちは、 @XPW さん。 スクリーンショットを見る限り、変数は最初は正しく初期化されているようです。しかし、eMCEMの初期化後、Clock_Ip_pfkNotificationsCallbackには無効なポインタが含まれています。 eMCEMはポインターの値を魔法のように変更するわけではありません。これは、以下のいずれかの問題に非常によく似ています。 起動時の初期化 (.data copy / .bss初期化が正しく完了していません。 RAMの破損はmain()関数の前に発生します。 リンカー部分は重複している。 スタック破損。 SPDデモプロジェクトのリンカーファイルでテストできますか? BR、ダニエル Re: S32K344 chip, failed to download using bootloader after adding eMCEM_1 module in spd リンクファイルは以下のように変更されました。 XPW_0-1783992772039.png XPW_1-1783993101988.png 私は3つのグローバル変数を定義しました。 XPW_2-1783993317537.png が有効になっていない場合、init_data-bssを実行した後、 XPW_3-1783993342206.png XPW_4-1783993406406.png 4バイトに正しく整列され、適切に割り当てられているようです。 しかし、 を有効にすると、init_data-bssを実行した後、 XPW_5-1783994068084.png XPW_6-1783994226472.png 位置がずれているようです。 Re: S32K344 chip, failed to download using bootloader after adding eMCEM_1 module in spd この現象の原因は何でしょうか?また、どのように調査し、解決すればよいでしょうか? Re: S32K344 chip, failed to download using bootloader after adding eMCEM_1 module in spd こんにちは、 @XPW さん。 スクリーンショットを見る限り、変数の初期化自体に問題があるとは考えにくい。variable_aは8ビット変数であり、eMCEMを有効にすると追加の変数が導入され、.データのレイアウトが変わる可能性がありますセクション。したがって、異なるオフセットで変数が見られることは想定内のことであり、それ自体がデータの破損を示すものではありません。 重要な問題は、アプリケーションが単独で実行されたときに起こるのか、それともブートローダーでプログラムされて起動された時だけ発生するのかということです。 デバッガで直接プログラムし、ブートローダーなしで実行した場合にこの問題を再現できますか?もし問題がブートローダーを通じてアプリケーションを読み込んだ後にのみ発生する場合は、調査はアプリケーション自体ではなく、ブートローダーのプログラミングプロセス、イメージレイアウト、またはブートローダーのハンドオーバーに焦点を当てるべきです。 BR、ダニエル
記事全体を表示
使いやすい8ビットのマイクロコントローラやアセンブリ言語はありますか? 実際の16進/バイナリコードが見られる8ビットのマイクロコントローラを探しています。大学で8051アセンブリ言語を学んでいるのですが、メモリ内の命令や値の一つ一つを見て理解できることが本当に大好きです。しかし、それらのマイクロコントローラは時代遅れで互換性のために多くの「ハック」が必要です。少なくとも、自分のコードを実際のハードウェアに書き込むたびに、そんな風に感じるんです。では、シンプルな8ビットアセンブリ言語で実際のチップを使った簡単な電子工学プロジェクトをプログラムできるものはありますか? Re: Is there a simple 8 bit microcontroller/assembly language that is nice to work with? こんにちは、 NXPには 8ビットデバイスのカタログがあります。 S08SG|8ビットSmall Package SG MCUを使えます |NXPセミコンダクターズの デバイス、 S08SGファミリーは、一般的な機能を備えたエントリーレベルからミッドレンジのデバイスです。 S08SGデバイスはCodeWarriorツールに含まれています。 CodeWarriorツールバージョン11.1はWindows 11でサポートされており、このツールはさまざまな接続に対応しています[P&E USB Multilink Universal / USB Multilink、P&E Cyclone、オープンソースBDM、P&E Full chip simulation] このツールはこちらのリンクからダウンロードできます: CodeWarrior® for MCUS (Eclipse IDE) v11.1 CWツールでデバッグを入力すると、Disassemblyビューのセクションがあり、読み込まれたプログラムがアセンブリ言語命令とソースコードの混合として比較されています。 敬具、ルイス Re: Is there a simple 8 bit microcontroller/assembly language that is nice to work with? ここでは、8ビットコントローラーのいくつかも試せます pic16lf18326-i-sl/2263047  MICROCHIPのPIC16LF18326-I/SLは、14ピン8ビットマイクロコントローラで、16KBフラッシュ、1KBメモリ、12ビットADC、10PWMチャネル、I2C SPI、UARTインターフェース、低消費電力、動作電圧2.3Vから5.5Vを備えています。 atmega8l-8mu/258363 MICROCHIPのATMEGA8L 4-8MUは8ビットAVRマイクロコントローラで、8MHz周波数、8KBフラッシュ、32ピンVQFN、I2C、SPI、UARTインターフェースを備え、2.7Vから5.5Vで動作します。温度範囲は-40℃~85℃です。
記事全体を表示
VSCodeのデバッグプローブウィンドウが読み込まれない(右にスクロールする白い線が表示される)。 これはOS X、VSCバージョン26.6.57での動作です。DEBUG PROBES ウィンドウは、プローブを一切検出していません(現時点では Segger です)。これは、私がアップグレードを行う前は正常に動作していたフリーフォームプロジェクトに関するものです。何を調査すべきかについて、ご提案をいただければ幸いです。プローブはVS Code拡張機能の外部で機能しています。MCUXpresso Installerも実行しました(PEMicroサーバーのインストールでは常に回転するホイールが表示されますが、tarを~/.mcuxpressotools/pemicrogdbserverに展開することには成功しました)。(余談ですが)。 拡張機能がデバッグツールとどのように連携しようとしているのか、その内容や方法に関する情報が役立つでしょう。拡張機能の設定などでツールの場所を指定しようと試みました。 デバッグプローブビューは、debug-tracker-vscodeの依存関係によって制御されますか? 読み込み時に「プロバイダーが見つかりませんでした」というメッセージが一瞬表示されます。 buff_0-1783086903160.png Re: VSCode DEBUG PROBES window not loading (white line scrolling right). こんにちは、 @buff。 「これはアップグレードを行う前に動作していた自由形式のプロジェクト用です」とおっしゃった際、何がアップグレードされたのかを明確にしていただけますか? これで問題が解決するかどうかを確かめるために、以下のテストを行ってもらえますか? -デバッグプローブウィンドウで、 [デバッグのクリーンアップ]をクリックし、[更新]ボタンをクリックします。 MCUXpressoインストーラーを最新バージョンにアップデートしてください。パッケージ およびコンポーネントの状態、バージョン、更新 のセクションで説明されている手順に従うことができます。 - MCUXpressoインストーラーからSEGGER J-Linkソフトウェアパックを再インストールしてください。 また、現在どのデバイスを使っているのか教えていただけますか?これは当社のEVK製品の一つですか、それともカスタムボードですか? BR ハビブ Re: VSCode DEBUG PROBES window not loading (white line scrolling right). ~/.mcuxpressotools を削除したところ、少なくとも MCUXpresso インストーラーはアップデートの確認で回転しなくなりました。これから依存関係を再インストールします。 Re: VSCode DEBUG PROBES window not loading (white line scrolling right). インストーラーを使ってツールとコンポーネントをアップデートすることができました。VS Codeを再起動すると、デバッグプローブウィンドウの内容が表示されるようになりました。なお、Spotlightとシェルの両方からVSCoceを起動してみましたが、どちらも正常に動作しました。 Re: VSCode DEBUG PROBES window not loading (white line scrolling right). MCUXpressoインストーラーのバージョンはv26.03です。アップグレードしてインストールを実行した後、初めてこのことに気づきました。バージョン26.06が最新版のようですね。それをインストールして、どうなるか見てみます。 * v26.06.117をインストールして起動したところ、回転するアイコンが表示されるだけでした。私はします buff_0-1783345794175.png /アプリケーション/MCUXpressoInstaller.app/Contents/MacOS/MCUXpressoInstallerCLI経由でインストーラーを再起動しました 詳細情報については、こちらをご覧ください。デフォルト環境からMCUXpressoInstallerCLIを起動すると、この回転する動作が見られます。その後、GUI (OS X) から再起動すると、インストーラーは PEMicro を除くコンポーネントの状態 (インストール済み、アップデートが利用可能) を表示します。 -デバッグプローブウィンドウで、 [デバッグのクリーンアップ]をクリックし、[更新]ボタンをクリックします。 VSCodeのデバッグプローブウィンドウには、クリックできる項目がありません。表示されたメッセージには、そのウィンドウの「プロバイダー」が存在しないことが示されていました。このメッセージは、MCUXpressoが最初に起動したときにすべてのウィンドウに表示され、MCUXpressoの読み込みが完了すると消えます(デバッグプローブのウィンドウを除く)。MCUXpressoをVSCode拡張機能用に一気に使い直して再インストールする手かもしれません。 MCUXpressoInstallerCLI の出力に以前このような記述がありました。これは PEMicro のヒントかもしれません。 冗長:MCUXpresso for VS Codeがすでにインストールされているか確認中... 情報:MCUXpresso for VS Codeはすでにインストール済みです。バージョン:26.6.57 ^Cverbose: PEmicroがすでにインストールされているかどうか確認中... 情報:「/Users/bruff/.mcuxpressotools/pemicrogdbserver/pegdbserver_console --version」を実行します。 情報: zsh -c "source /Users/bruff/.zprofile && /Users/bruff/.mcuxpressotools/pemicrogdbserver/pegdbserver_console --version" error: コマンド /Users/bruff/.mcuxpressotools/pemicrogdbserver/pegdbserver_console コード1で終了。 stdout:「P&E GDB Server for Arm(R)デバイス、バージョン10.02.00.00 著作権 2025、P&E Microcomputer Systems Inc、無断複写・転載を禁じます ライブラリ /Users/bruff/.mcuxpressotools/pemicrogdbserver/gdi/unit_ngs_arm_internal.so を読み込み中 ...完了。 コマンドライン引数: --version stderr: "モジュール libsystem_kernel.dylib の 00007FF80629B3CA で例外 EControlC が発生しました。 コントロールCがヒットしました。 情報: PEmicro が見つかりません。 'versionReport' ハンドラーでエラーが発生しました:エラー:ブラウザウィンドウのハンドルを取得できません at new o (/アプリケーション/MCUXpressoInstaller.app/Contents/Resources/app.asar/main.js:2:312914) at o.getInstance (/アプリケーション/MCUXpressoInstaller.app/Contents/Resources/app.asar/main.js:2:313215) at r(/アプリケーション/MCUXpressoInstaller.app/Contents/Resources/app.asar/main.js:2:313676) at Rc(/アプリケーション/MCUXpressoInstaller.app/Contents/Resources/app.asar/main.js:2:519204) at async Session. (node:electron/js2c/browser_init:2:114068)
記事全体を表示
关于 S32K3_RTD_7_0_0 的下载链接 我想从 NXP 网站下载一个符合以下条件的 RTD 可执行文件,但我找不到。 请问可以提供下载链接吗? 我很赶时间,所以希望您能尽快回复。 S32K3_RTD_7_0_0_D2510_ASR_REL_4_9_REV_0000_20251031 我找到了以下类似的可下载产品,但它需要一个符合上述条件的 RTD(Ready-to-Download)。 SW32K3_S32M27x_RTD_R21-11_6.0.0_QLP04_HF01_D2510.exe SW32K3_S32M27x_RTD_R23-11_7.0.0_D2511.exe SW32K3_S32M27x_RTD_R23-11_7.0.0_QLP03_D2512.exe Re: S32K3_RTD_7_0_0のダウンロードリンクについて HI 您需要使用 EBTresos 还是 S32DS? 如果您需要使用 EBTresos,请下载并安装 S32K3_S32M27x 实时驱动程序 ASR R23-11 版本 7.0.0。(SW32K3_S32M27x_RTD_R23-11_7.0.0_D2511.exe)。 如果您需要使用 S32DS,请下载 S32K3_S32M27x 实时驱动程序 ASR R23-11 版本 7.0.0。(SW32K3_S32M27x_RTD_R23-11_7.0.0_D2511_DesignStudio_updatesite.zip)。 此致敬礼, Robin
記事全体を表示
VSCode 调试探测窗口无法加载(白色线条向右滚动)。 这是在 OS X 系统上,VSC 版本:26.6.57。DEBUG PROBES 窗口未检测到任何探针(目前是 Segger)。这是一个自由格式项目,在我进行升级之前它运行正常。我想请教一下应该检查哪些方面。这些探针在 VSCode 扩展之外运行。我还运行了 MCUXpresso 安装程序(尽管 PEMicro 服务器安装一直显示旋转的圆圈,但它确实成功地将 tar 文件解压到了 ~/.mcuxpressotools/pemicrogdbserver)。(只是顺便提一下)。 有用的信息包括该扩展程序尝试与调试工具进行哪些交互/如何交互。我已尝试在扩展程序设置等中提供工具位置。 调试探针视图是否受 debug-tracker-vscode 依赖项控制? 页面加载时会短暂显示一条消息,内容大概是找不到提供商。 buff_0-1783086903160.png Re: VSCode DEBUG PROBES window not loading (white line scrolling right). 你好@buff , 您提到“这是一个自由格式项目,在我进行升级之前运行正常”,请问您能否具体说明升级了什么? 为了确定这是否能解决问题,请您执行以下测试? -在“调试探针”窗口中,单击“清理调试” ,然后单击“刷新”按钮。 -将 MCUXpresso 安装程序更新到最新版本。您可以按照“代码包,软件包和元器件状态、版本和更新”部分中描述的步骤进行操作。 -从 MCUXpresso 安装程序重新安装 SEGGER J-Link 软件包。 另外,请问您目前使用的是哪款设备?这是我们的EVK产品之一,还是定制的电路板? BR 哈比卜 Re: VSCode DEBUG PROBES window not loading (white line scrolling right). 我使用安装程序更新了工具和元器件。重启 VSCode 后,现在可以显示“调试探针”窗口的内容。注意,我分别通过 Spotlight 和 shell 启动了 VSCoce,两种方式都成功了。 Re: VSCode DEBUG PROBES window not loading (white line scrolling right). 我删除了 ~/.mcuxpressotools 目录,MCUXpresso 安装程序至少不再循环检查更新了。我现在将重新安装依赖项。 Re: VSCode DEBUG PROBES window not loading (white line scrolling right). MCUXpresso 安装程序版本为 v26.03。我是在升级并运行安装程序后才注意到这个问题的。我看到最新版本是 v26.06,我会安装看看情况如何。 * 我安装了 v26.06.117 版本,启动后只看到旋转的图标。我会 buff_0-1783345794175.png 我通过 /Applications/MCUXpressoInstaller.app/Contents/MacOS/MCUXpressoInstallerCLI 重新启动了安装程序 获取更多信息。从我的默认环境通过 MCUXpressoInstallerCLI 启动时,我看到了这种旋转现象。当我随后从 GUI(OS X)重新启动时,安装程序会显示元器件状态(已安装、有更新可用),但 PEMicro 除外。 -在“调试探针”窗口中,单击“清理调试” ,然后单击“刷新”按钮。 在 VSCode 的“调试探针”窗口中,没有任何可以点击的内容。弹出的消息表明该窗口没有“提供程序”。首次启动时,此消息会显示在所有窗口中,然后随着 MCUXpresso 加载完成而消失(调试探针窗口除外)。我想我可以把 MCUXpresso for VSCode 扩展卸载掉,然后重新安装。 MCUXpressoInstallerCLI 输出曾经出现过这个内容,这可能是 PEMicro 的一个线索: 详细信息:正在检查 MCUXpresso for VS Code 是否已安装…… 信息:MCUXpresso for VS Code 已安装。版本:26.6.57 ^详细:正在检查 PEmicro 是否已安装... 信息:正在执行“/Users/bruff/.mcuxpressotools/pemicrogdbserver/pegdbserver_console --version” 信息:zsh -c "source /Users/bruff/.zprofile && /Users/bruff/.mcuxpressotools/pemicrogdbserver/pegdbserver_console --version" 错误:命令 /Users/bruff/.mcuxpressotools/pemicrogdbserver/pegdbserver_console 退出,返回代码为 1。 标准输出:“适用于 Arm(R) 设备的 P&E GDB 服务器,版本 10.02.00.00 版权所有 © 2025 P&E 微型计算机系统公司,保留所有权利 正在加载库 /Users/bruff/.mcuxpressotools/pemicrogdbserver/gdi/unit_ngs_arm_internal.so ... 完成。 命令行参数:--version” stderr: "模块 libsystem_kernel.dylib 中出现异常 EControlC,地址为 00007FF80629B3CA。 Ctrl+C 按下。 信息:未找到 PEmicro。 'versionReport' 处理程序中发生错误:错误:无法获取浏览器窗口句柄 在 new o (/Applications/MCUXpressoInstaller.app/Contents/Resources/app.asar/main.js:2:312914) 在 o.getInstance (/Applications/MCUXpressoInstaller.app/Contents/Resources/app.asar/main.js:2:313215) 在 r (/Applications/MCUXpressoInstaller.app/Contents/Resources/app.asar/main.js:2:313676) 在 Rc (/Applications/MCUXpressoInstaller.app/Contents/Resources/app.asar/main.js:2:519204) 在异步会话. (node:electron/js2c/browser_init:2:114068)
記事全体を表示
VSCode DEBUG PROBES window not loading (white line scrolling right). This is on OS X, VSC ver: 26.6.57.  The DEBUG PROBES window is not detecting any probes (Segger at the moment).  This is for a freeform project which was functioning before I performed an upgrade.  I am looking for suggestions as to what to examine.  The probes are functioning outside of the VSCode extension.  I also have run MCUXpresso Installer as well (though the PEMicro server install always shows a spinning wheel, it did succeed in extracting the tar into ~/.mcuxpressotools/pemicrogdbserver - just an aside). Useful info would be what/how the extension is attempting to interact with the debug tools.  I have attempted to supply tool locations in the extension settings, etc.   Is the Debug Probes view controlled by the debug-tracker-vscode dependency? There is a message visible briefly when this loads, something about no provider found. buff_0-1783086903160.png Re: VSCode DEBUG PROBES window not loading (white line scrolling right). Hello @buff, When you mentioned, "This is for a freeform project which was functioning before I performed an upgrade," could you please clarify what was upgraded? In order to try a pinpoint if this solves the issue, could you perform the following tests? -In the Debug Probes window, click Clean-up Debug and then click the Refresh button. -Update the MCUXpresso Installer to the latest available version. You can follow the steps described in the Package and Component Status, Version, and Updates section. -Reinstall the SEGGER J-Link Software Pack from the MCUXpresso Installer. Also, could you please provide me which device are you currently using? Is one of our EVKs or is a custom board? BR Habib Re: VSCode DEBUG PROBES window not loading (white line scrolling right). MCUXpresso Installer is at v26.03.  I first noticed this after upgrading and running the install.  I see v26.06 is now current, I will install that and see what's what. * I installed v26.06.117 and upon launching it, I just see the spinning icons.  I will buff_0-1783345794175.png I relaunched Installer via /Applications/MCUXpressoInstaller.app/Contents/MacOS/MCUXpressoInstallerCLI to get more info.  Launching from MCUXpressoInstallerCLI from my default environment I see this spinning behavior.  When I relaunched from the GUI (OS X) a subsequent time the installer shows component status (installed, update available) with the exception of PEMicro.   -In the Debug Probes window, click Clean-up Debug and then click the Refresh button. In the VSCode DEBUG PROBES window there is nothing to click.  The message which popped up indicated that there is no 'provider' for the window.  This message shows up in all the windows when first launched then goes away as MCUXpresso finishes loading (with the exception of the DEBUG PROBES windows).  I guess I could blow away the MCUXpresso for VSCode extension and reinstall. MCUXpressoInstallerCLI output once had this, might be hint for PEMicro: verbose: Checking if MCUXpresso for VS Code is already installed... info: MCUXpresso for VS Code already installed. Version: 26.6.57 ^Cverbose: Checking if PEmicro is already installed... info: Executing "/Users/bruff/.mcuxpressotools/pemicrogdbserver/pegdbserver_console --version" info: zsh -c "source /Users/bruff/.zprofile && /Users/bruff/.mcuxpressotools/pemicrogdbserver/pegdbserver_console --version" error: Command /Users/bruff/.mcuxpressotools/pemicrogdbserver/pegdbserver_console exited with code 1. stdout: "P&E GDB Server for Arm(R) devices, Version 10.02.00.00 Copyright 2025, P&E Microcomputer Systems Inc, All rights reserved Loading library /Users/bruff/.mcuxpressotools/pemicrogdbserver/gdi/unit_ngs_arm_internal.so ... Done. Command line arguments: --version" stderr: "Exception EControlC in module libsystem_kernel.dylib at 00007FF80629B3CA. Control-C hit." info: PEmicro not found. Error occurred in handler for 'versionReport': Error: Could not get browser window handle at new o (/Applications/MCUXpressoInstaller.app/Contents/Resources/app.asar/main.js:2:312914) at o.getInstance (/Applications/MCUXpressoInstaller.app/Contents/Resources/app.asar/main.js:2:313215) at r (/Applications/MCUXpressoInstaller.app/Contents/Resources/app.asar/main.js:2:313676) at Rc (/Applications/MCUXpressoInstaller.app/Contents/Resources/app.asar/main.js:2:519204) at async Session. (node:electron/js2c/browser_init:2:114068) Re: VSCode DEBUG PROBES window not loading (white line scrolling right). I was able to use Installer to update the tools and components.  Restarting VSCode now shows the DEBUG PROBES window contents.  Note I did launch VSCoce from both spotlight and a shell, both worked.   Re: VSCode DEBUG PROBES window not loading (white line scrolling right). I deleted ~/.mcuxpressotools and MCUXpresso Installer at least isn't spinning checking for updates.  I will re-install the dependencies now.
記事全体を表示
i.MX 943 EVK:LinuxとZephyrの間でENETCの共有ユースケースを実行 こんにちは、 私は i.MX 943 EVKボードを使っており、Linux上のCortex-A55 SMPとZephyrのCortex-M33sの間でネットワークを共有したいと考えています。 そこで興味を持ちました。i.MX Linux ユーザーズガイド(https://www.nxp.com/docs/en/user-guide/UG10163.pdf - セクション11.6.2)からのENETC共有ユースCASEです。この例では、Linux側でプロキシPFドライバーを有効にするためにRPMsg接続を設定しました。RPMsg接続のリソーステーブルのアドレスは0x208a0000で、仮想キューは0x20800000にあります。これらのアドレス([0x20800000~0x208A0FFF])はNETC OCRAM内にあります。この領域はCortex-M33 Core1(M33S)とAP(非セキュアLinux)間のRPMSG共有メモリとして使用されます。 この例では、mx94evknetc.cfgのシステムマネージャー設定ファイルを使い、Cortex-M33がネットワークにアクセスできるようにしています。この設定ファイルの関係で、A55とM33は起動時に起動する必要があるので、ターゲットのimx-mkimage flash_allを使っています。 問題は、flash_a55ターゲット(mx94rte.cfgシステムマネージャーの設定ファイル)を使うと、Linux/U-BootとZephyrはそれらのアドレスにアクセスできますが、flash_allに切り替えると(システムマネージャーの設定ファイルに関係なく)、Linux/U-BootもZephyrもそれらのアドレスにアクセスできません。Zephyrはこれらのアドレスでバスフォールトが発生します。しかし、Zephyrの代わりにシンプルなhello_worldなどのFreeRTOSプログラムを使うと、Cortex-M33sやLinux/U-Bootがそれらのアドレスにアクセスできます。 また、mx94rte.cfgシステムマネージャーファイルでflash_allターゲットを使うと、Linux/U-BootもZephyrもそのアドレスにアクセスできませんが、Cortex-M33を停止してFreeRTOS hello_worldを読み込んで再起動すると、Linux/U-BootはNETC OCRAMにアクセスできます。 ちなみに、Zephyrはflash_M33sターゲットにアクセスできません。 そこで、FreeRTOSが初期化時にZephyrができないことを知りたいです。つまり、Linux/U-BootとZephyr間でNETC OCRAMにアクセスしやすくするために、その点はflash_allターゲットで。 ゼファーバージョン:4.3 Linuxバージョン(リアルタイムエッジ版):6.18.2 Linux Re: i.MX 943 EVK : Run the ENETC shared use case between Linux and Zephyr こんにちは、 @Remantj さん。 お元気でお過ごしのことと思います。 ぜひnxp-zephyrのドキュメントをご覧ください: https://github.com/nxp-zephyr/nxp-zephyr/blob/main/boards/nxp/imx943_evk/doc/index.rst#programming-and-debugging-m33-in-netc-mix-m7_0-in-m7mix0-m7_1-in-m7mix1 System-Managerで説明されている変更があなたの場合に効果があったか教えてください。 よろしくお願いいたします。 サラス。 i.MX 943 EVK : Run the ENETC shared use case between Linux and Zephyr こんにちは、 @Manuel_Salas さん、 ご回答ありがとうございます。 あなたが指摘したドキュメントを見て、ドキュメントで行われたのと同じ方法でシステムマネージャにパッチを当ててみましたが、何も変わりませんでした。 これは予想通りのようです。なぜなら、私の問題の違いはFreeRTOSのファームウェアとZephyrのファームウェアの違いだからです。System マネージャの設定ファイルは2つのケースで同じままです。 FreeRTOSがZephyrと違うNETC OCRAMについて何をしているのかはわかりませんが、Zephyrで同じことができる方法について何かアイデアはありますか? よろしくお願いします
記事全体を表示
Newbie setting up an autosar environment xmrchen_0-1783048422915.png When downloading S32 Design Studio for ARM 2.2 – Windows/Linux, the above message appears. Hopefully, the official website can be reset so that downloads can proceed normally. Thank you. When downloading S32 Design Studio for ARM 2.2 – Windows/Linux, the above message appears. Hopefully, the official website can reset this so that the download can proceed normally. Thank you. Re: 新手搭载autosar环境 Hello, Please try it now. It should be working. Best regards, Peter S32K新手搭载autosar环境 Thank you very much, teacher. The first problem is solved. However, when installing the S32DS_ARM_Win32_v2.2.exe integrated development environment, an activation failure message appeared. The cause was found to be an expired Activation Code. Therefore, I am requesting an extension. Thank you. 新手搭载autosar环境 Thank you very much for the teacher's support. The environment has been set up.
記事全体を表示