Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
在 S32 Design Studio for Power Architecture v2.1 中,PEmicro GDB 启动失败 您好, 我正在测试的电路板是 MTRCKTSPS5744P(带有 MPC5744P MCU 的三相 PMSM 电机控制开发套件)。 不知何故,下载过程不太顺利。 点击调试按钮后,下载失败,此时会弹出此窗口。 eunwoo_lee_0-1789496057004.png 弹出一个窗口,显示此错误信息。 服务启动序列错误 PEmicro GDB 启动失败:GDB 服务器无法与目标处理器建立连接。请检查您的连接和电源。请确认调试配置中的启动设置是否准确。 控制台面板显示此消息。 来自“127.0.0.1”的连接,通过 127.0.0.1。从端口“53438”到7224的连接 PE错误:警告。部件运行时无法读取寄存器。 PE错误:警告。部件运行时无法读取内存。@0(4 字节) PE错误:警告。部件运行时无法读取内存。@0(4 字节) PE错误:警告。部件运行时无法读取寄存器。 PE错误:警告。部件运行时无法读取内存。@0(4 字节) PE错误:警告。部件运行时无法读取内存。@0(4 字节) PE错误:警告。部件运行时无法写入二进制文件。40001000 - 长度:0 - 值:二进制数据 PE错误:警告。部件运行时无法写入二进制文件。40001000 - 长度:460 - 值:二进制数据 PE错误:警告。部件运行时无法写入二进制文件。40001460 - 长度:460 - 值:二进制数据 PE错误:警告。部件运行时无法写入二进制文件。400018c0 - 长度:460 - 值:二进制数据 PE错误:警告。部件运行时无法写入二进制文件。40001d20 - 长度:2e0 - 值:二进制数据 PE错误:GDB客户端处理:发生异常:程序异常! 异常类:EIDCONNCLOSEDGRACEFULLY 消息:连接已正常关闭。 地址 0X0046EA89 通过 127.0.0.1 与“127.0.0.1”断开连接。通过端口“53438”与7224断开连接 目标设备已断开连接。 你知道有什么办法解决这个问题吗? 谢谢。 Re: PEmicro GDB Launch Failure in S32 Design Studio for Power Architecture v2.1 你好, 你知道有什么办法解决这个问题吗? 正如消息中所述,您无法在运行时写入/读取寄存器。首先在调试器中停止代码执行,然后才能修改寄存器、内存等…… MPC5744P 正在运行用户代码,P&E 探针无法停止设备,因此所有内存/寄存器访问均失败,下载操作中止。 这看起来不像是一个闪存编程问题,而更像是调试器在下载之前未能停止 MPC5744P 的运行。 例如,微控制器中是否存在启用了 SWT0 的软件? 或者这是一个没有运行任何软件的全新样本? 顺祝商祺! Peter
記事全体を表示
S32K3_RTD_6_0_0_D2506_ASR_REL_4_7_REV_0000_2025 不支持 HB200x AUTOSAR R21-11 版本 0.8.0 您好,NXP, 我尝试将 HB200x AUTOSAR 规范 SDK 集成到 S32 Design Studio 中,但收到以下错误消息: 问题:在工具链/IDE 项目中找不到 Mc33hb。该项目无法编译! 级别:错误 类型:验证 工具:工具链/IDE 项目 来源:外围设备 目标:工具链/IDE 项目:M7_0 资源:platform.driver.mc33hb 甚至包括 CDD_Mb33Hb.c 文件在 S32 Design Studio 应用程序 (v3.6.4) 中安装 SDK 时,尚未添加 CDD_Mb33Hb.h 等文件。 Re: HB200x AUTOSAR R21-11 Version 0.8.0 not supported by S32K3_RTD_6_0_0_D2506_ASR_REL_4_7_REV_0000_ 你好, 您似乎使用了错误的RTD版本。根据 HB200x AUTOSAR R21-11 0.8.0 发行说明,该软件可以基于 SW32K3_RTD_4.4_R21-11_3.0.0_D2303_DS_updatesite.zip 使用(该软件需要安装在 S32 Design Studio IDE v3.5 中)。 PetrS_0-1789471295419.pngPetrS_0-1789471295419.png BR,彼得
記事全体を表示
PEmicro GDB Launch Failure in S32 Design Studio for Power Architecture v2.1 Hi, The board I am testing is MTRCKTSPS5744P (3-Phase PMSM Motor Control Development Kit with MPC5744P MCU). For some reason, the download process doesn't go well. This window pops up after failure in downloading when I click debug button. eunwoo_lee_0-1789496057004.png An window pops up showing this error message. Error in services launch sequence PEmicro GDB Launch Failure : The GDB Server was not able to establish a connection to the target processor. Please check your connections and power. Verify that the launch settings in the Debug Configuration are accurate. Console panel displays this message. Connection from "127.0.0.1" via 127.0.0.1. Connection from port "53438" to 7224 PE-ERROR: Warning. Can't read registers while part is running. PE-ERROR: Warning. Can't read memory while part is running. @0 (4 bytes) PE-ERROR: Warning. Can't read memory while part is running. @0 (4 bytes) PE-ERROR: Warning. Can't read registers while part is running. PE-ERROR: Warning. Can't read memory while part is running. @0 (4 bytes) PE-ERROR: Warning. Can't read memory while part is running. @0 (4 bytes) PE-ERROR: Warning. Can't Write Binary while part is running. 40001000 - Length of: 0 - Value of: Binary Data PE-ERROR: Warning. Can't Write Binary while part is running. 40001000 - Length of: 460 - Value of: Binary Data PE-ERROR: Warning. Can't Write Binary while part is running. 40001460 - Length of: 460 - Value of: Binary Data PE-ERROR: Warning. Can't Write Binary while part is running. 400018c0 - Length of: 460 - Value of: Binary Data PE-ERROR: Warning. Can't Write Binary while part is running. 40001d20 - Length of: 2e0 - Value of: Binary Data PE-ERROR: GDB Client Processing : Exception Occured : PROGRAM EXCEPTION! EXCEPTION CLASS: EIDCONNCLOSEDGRACEFULLY MESSAGE: CONNECTION CLOSED GRACEFULLY. ADDRESS 0X0046EA89 Disconnected from "127.0.0.1" via 127.0.0.1. Disconnection by port "53438" from 7224 Target Disconnected. Is there any solution you know for this problem? Thanks. Re: PEmicro GDB Launch Failure in S32 Design Studio for Power Architecture v2.1 Hello, Is there any solution you know for this problem? As the message explains you cannot write/read registers on the fly. First stop the execution of the code in debugger and then you can modify the registers, memory, etc... The MPC5744P is running user code and the P&E probe is unable to halt the device, therefore all memory/register accesses fail and the download operation aborts. This looks less like a flash programming problem and more like a debugger failing to halt the MPC5744P before download. Is there for example SW with SWT0 enabled in the microcontroller? Or is it a fresh sample with no SW running? Best regards, Peter
記事全体を表示
IW612蓝牙连接几天后崩溃 你好, 一位用户向我们报告了 Murata LBES5PL2EL-923(IW612 内核)蓝牙功能的一个缺陷:通过蓝牙静态 RFCOMM/SPP 连接设备几天后,蓝牙协议栈会崩溃。 (原始报告已公开,可在以下网址以日语查看:https://armadillo.atmark-techno.com/forum/armadillo/31772)) 关于这个问题,目前已知有哪些漏洞? 软件设置: * 基于 lf-6.12.49-2.2.0 的 Linux 6.12(确切的源代码树: https://github.com/atmark-techno/linux-6.12-at/tree/6.12.105-r0 ) 这是一个蓝牙问题,但以防万一,无线驱动程序基于 mwifiex lf-6.12.49-2.2.0。 * 固件已从 imx-firmware 仓库更新至最新版本 lf-6.18.20_2.0.0 https://github.com/nxp-imx/imx-firmware/tree/lf-6.18.20_2.0.0/FwImage_IW612_SD * BlueZ 软件包(目前正在确认确切版本,抱歉我忘了问) * 该板通过 *经典蓝牙*(非 BLE)连接到单个设备,采用 RFCOMM/SPP。每隔 60 秒,应用程序发送一条消息并收到回复(简单轮询)。几天后出现命令超时,蓝牙驱动程序重启。 我附上了一个固件转储文件(崩溃后从 /sys/class/bluetooth/hci0/devcoredump/data 获取),假设它有用的话,在崩溃之前 dmesg 中没有任何消息(很抱歉,在“开始固件转储”消息之前的内容被截断了,所以没有时间戳,我的理解是崩溃发生后立即发生的)。 FW 重新装弹机制可以工作,但这需要重新连接,所以如果可能的话,最好解决这个问题。 [ 0.000000] Linux version 6.12.105-0-at (builder@71056255c5a6) (aarch64-alpine-linux-musl-cc (Alpine 15.2.0) 15.2.0, GNU ld (GNU Binutils) 2.45.1) #1-Alpine SMP PREEMPT Mon Aug 24 07:48:35 UTC 2026 [...] [ 9.321032] wlan: version = SDIW612---18.99.8.p52-MM6X18540.p33-GPL-(FP92) [...] [ 10.349326] Bluetooth: hci0: FW already running. [ 38.303160] Bluetooth: MGMT ver 1.23 [170117.376944] Bluetooth: hci0: command tx timeout Bluetooth: hci0: ==== Start FW dump === Bluetooth: hci0: ==== FW dump complete === Bluetooth: hci0: Request Firmware: nxp/uartspi_n61x_v1.bin.se Bluetooth: hci0: FW Download Complete: 412940 bytes 如有其他有助于分析的信息,请提出。 谢谢 Re: IW612 bluetooth crash after a few days 1.能否提供HCI日志,以便我们确定是哪个命令超时并生成了固件转储? 您能解释一下您这句话的意思吗?事后是否有命令可以运行,还是应该运行 hcidump 或类似命令来转储进程运行时的所有命令? 3. 要获取 Wi-Fi 驱动程序加载参数,您可以提供以下文件:/lib/firmware/nxp/wifi_mod_para.conf 我们不会使用此文件,因此这里也应该使用默认参数。我们已经将日志级别从默认值降低了,所以 dmesg 在这里也帮不上什么忙(我在之前的回复中已经发送了 dmesg 的链接)。 我会向用户确认他们在此期间是否使用无线网络。 Re: IW612 bluetooth crash after a few days 嗨, @martinetd 1.能否提供HCI日志,以便我们确定是哪个命令超时并生成了固件转储? 2.请提供基于WLAN的使用案例,在WLAN运行的情况下,检查在生成固件转储文件时WLAN是否工作正常? 3.要获取Wi-Fi驱动程序加载参数,您可以提供以下文件:/lib/firmware/nxp/wifi_mod_para.conf 或者您可以向我们提供正常的启动 dmesg 日志,其中包含 WiFi/蓝牙加载的整个过程。我们可以从 dmesg 日志中获取信息。 4.目前,我们没有比您正在使用的版本更新的公开 GitHub 固件版本: imx-firmware/FwImage_IW612_SD at lf-6.18.20_2.0.0 · nxp-imx/imx-firmware · GitHub 所以,我认为这不是一个已知问题。 我们希望获得更多与用例和 HCI 日志相关的信息,以便跟踪发生了什么或重现步骤,从而使我们能够在本地重现问题。 如果您还有其他与此问题相关的信息,请与我们分享。 顺祝商祺! Christine。 Re: IW612 bluetooth crash after a few days 嗨@Christine_Li,谢谢你的快速回复。 > 1.如果您正在使用 btnxpuart 驱动程序,请提供 btnxpuart.c 文件。 我们正在使用https://github.com/nxp-imx/linux-imx中提供的 btnxpuart。基于 lf-6.12.49-2.2.0 版本,您可以在这里找到确切的文件:https://github.com/atmark-techno/linux-6.12-at/blob/6.12.105-r0/drivers/bluetooth/btnxpuart.c > 2. 您使用的是 Wi-Fi 和蓝牙/802.15.4 组合固件吗?还是使用的是单独的固件? 我们同时使用了这两种方式:wifi 驱动程序在启动时加载组合固件,崩溃后重新加载单独的固件(因此日志中会将单独的固件命名为“单独的固件”)。 发生此次崩溃时,组合固件已加载(启动后首次崩溃),但据我了解,两种固件都会出现此问题。 > 3.请问您能否提供一下您的 Wi-Fi 和蓝牙驱动程序加载参数? 我们明确设置的唯一 wifi 参数是 drv_mode = 0x3,用于禁用我们不使用的 wifi direct 接口;我们没有设置任何蓝牙参数。如果你能告诉我如何导出确切的设置,我可以让我们的用户运行命令来获取这些信息。 > 4.请问您能否提供详细的重现步骤? 由于这是基于用户报告,我只能描述一下(RFCOMM 连接每 60 秒轮询一次,持续几天);恐怕这可能取决于芯片实际连接的子设备。 我会尝试找一个可以通过 RFCOMM ping 通的设备,并在本地重现问题,以便为您提供测试脚本(如果需要的话)。但目前我找不到任何关于固件/btnxpuart 驱动程序已知错误的发布说明,所以我想确认是否存在已知错误(也希望您能从固件转储中获取任何信息)。 谢谢 Re: IW612 bluetooth crash after a few days 嗨, @martinetd 1.您是否正在使用我们NXP的btnxpuart蓝牙驱动程序?或者您使用的是Linux开源UART驱动程序? 如果您正在使用 btnxpuart 驱动程序,请提供 btnxpuart.c 文件。 2.您使用的是Wi-Fi和蓝牙/802.15.4组合固件吗?还是使用的是单独的固件? 因为我看到你的日志如下所示,所以我怀疑你使用了单独的固件,需要和你再次确认。 hci0: Request Firmware: nxp/uartspi_n61x_v1.bin.se 3.请问您能否提供一下您的 Wi-Fi 和蓝牙驱动程序负载参数? 4.请问您能否提供详细的重现步骤? 顺祝商祺! Christine。 Re: IW612 bluetooth crash after a few days >> * BlueZ 软件包(目前正在确认确切版本,抱歉我忘了问) 如果这很重要的话,BlueZ 版本是 5.82。
記事全体を表示
ARINC615A Data loading with JTAG Access password protected When HSE firmware is not installed, SWD/JTAG access on the S32K3 can be restricted using the CUST_DB_PSWD_A field and device lifecycle configuration. Would enabling this password protection have any impact on performing an ARINC 615A software data load to the processor, assuming the update is handled by application or bootloader software rather than through the debug interface? Re: ARINC615A Data loading with JTAG Access password protected CUST_DB_PSWD_A only restricts SWD/JTAG debug access. I am not familiar with the details of your ARINC 615A implementation, but if the software load is handled entirely by your application or bootloader, I would not expect the debug password itself to have any impact. Ultimately, this is application-specific and depends on how ARINC 615A has been implemented in your system. If the update mechanism does not use the debug interface, debug access restrictions should generally be independent of the software loading process. Any additional limitations would depend on your lifecycle configuration and application security design.
記事全体を表示
参照構成パス Simulinkでハードウェアを構成する際に、参照構成のディレクトリを相対パスに変更しようとしています。 Simulink -> HW-Settings -> Hardware Implementation -> Target hardware resources -> Referenced Configuration 参照構成パス = '.\generated\referenced_config' 残念ながら、ここでは相対パスを入力することはできません。 また、MATLABスクリプトで進路を設定することもまだできません。 スクリプトはCoderTargetDataにパスを設定しているように見えますが、実際には適用されていません。 古いパスが引き続き有効になるか、空のパスが適用されます。 参照設定に対して相対パスを設定する方法はありますか?
記事全体を表示
HB200x AUTOSAR R21-11 バージョン 0.8.0 S32K3_RTD_6_0_0_D2506_ASR_REL_4_7_REV_0000_2025 がサポートしていません こんにちは、NXPさん。 HB200x AUTOSAR仕様SDKをS32 Design Studioに統合しようとしましたが、以下のエラーメッセージが表示されます。 問題点:Mc33hbはツールチェーン/IDEプロジェクトに存在しません。プロジェクトはコンパイルできません! レベル: エラー タイプ:検証 ツール:ツールチェーン/IDEプロジェクト 起源:ペリフェラル ターゲット:ツールチェーン/IDEプロジェクト:M7_0 リソース:platform.driver.mc33hb CDD_Mb33Hb.c ファイルでさえCDD_Mb33Hb.hなどは、SDKがS32 Design Studioアプリケーション(v3.6.4)にインストールされた際には追加されていませんでした。 Re: HB200x AUTOSAR R21-11 Version 0.8.0 not supported by S32K3_RTD_6_0_0_D2506_ASR_REL_4_7_REV_0000_ こんにちは、 どうやら間違ったRTDバージョンを使用しているようです。HB200x AUTOSAR R21-11 0.8.0リリースノートに基づき、このソフトウェアはSW32K3_RTD_4.4_R21-11_3.0.0_D2303_DS_updatesite.zip(S32 Design Studio IDE v3.5にインストールする必要があります)上で使用可能です。 PetrS_0-1789471295419.pngPetrS_0-1789471295419.png BR、ペトル
記事全体を表示
refence configuration path In Simulink, when configuring the hardware, I am trying to change the directory for the reference configuration to a relative path. Simulink -> HW-Settings -> Hardware Implementation -> Target hardware resources -> Referenced Configuration Reference Configuration Path = '.\generated\referenced_config' Unfortunately, it is not possible to enter a relative path here. Nor have I so far been able to set the path via a MATLAB script. Although the script appears to set the path in CoderTargetData, it is not actually applied. Either the old path remains active, or an empty path is applied. Is there a way to set a relative path for the reference configuration?
記事全体を表示
参考配置路径 在 Simulink 中配置硬件时,我尝试将参考配置的目录更改为相对路径。 Simulink -> 硬件设置 -> 硬件实现 -> 目标硬件资源 -> 参考配置 参考配置路径 = '.\generated\referenced_config' 很遗憾,这里无法输入相对路径。 到目前为止,我还没能通过 MATLAB 脚本设置路径。 虽然脚本似乎在 CoderTargetData 中设置了路径,但实际上并没有应用。 要么保持旧路径有效,要么应用一个空路径。 是否可以为参考配置设置相对路径?
記事全体を表示
IW612 bluetooth crash after a few days Hello, One of our users reported us a bug with the murata LBES5PL2EL-923 (IW612 core) bluetooth functionality, where the bluetooth stack crashes after a few days connected to a device over bluetooth static RFCOMM/SPP (The original report is public and available in Japanese at https://armadillo.atmark-techno.com/forum/armadillo/31772 ) Are there any known bugs about this? Software setup: * linux 6.12 based on lf-6.12.49-2.2.0 (exact source tree: https://github.com/atmark-techno/linux-6.12-at/tree/6.12.105-r0 ) this is a BT problem but in case it matters the wireless driver is based on mwifiex lf-6.12.49-2.2.0 * firmware updated to the latest from the imx-firmware repo at lf-6.18.20_2.0.0 https://github.com/nxp-imx/imx-firmware/tree/lf-6.18.20_2.0.0/FwImage_IW612_SD * BlueZ stack (currently confirming the exact version, sorry I forgot to ask) * the board is connected to a single device over *bluetooth classic* (not BLE), with RFCOMM/SPP. Every 60 seconds the application sends a message and gets a reply (simple polling). After a few days there is a command timeout and the BT driver restarts I've attached a firmware dump (obtained from /sys/class/bluetooth/hci0/devcoredump/data after crash happened), assuming it can be useful, there is no message in dmesg until the crash (I'm sorry it's truncated before the "Start FW dump" message so there is no timestamp for these, my understanding is that it was immediately afterwards) The FW reloading mechanism works, but this requires a reconnection so would be better addressed if possible. [ 0.000000] Linux version 6.12.105-0-at (builder@71056255c5a6) (aarch64-alpine-linux-musl-cc (Alpine 15.2.0) 15.2.0, GNU ld (GNU Binutils) 2.45.1) #1-Alpine SMP PREEMPT Mon Aug 24 07:48:35 UTC 2026 [...] [ 9.321032] wlan: version = SDIW612---18.99.8.p52-MM6X18540.p33-GPL-(FP92) [...] [ 10.349326] Bluetooth: hci0: FW already running. [ 38.303160] Bluetooth: MGMT ver 1.23 [170117.376944] Bluetooth: hci0: command tx timeout Bluetooth: hci0: ==== Start FW dump === Bluetooth: hci0: ==== FW dump complete === Bluetooth: hci0: Request Firmware: nxp/uartspi_n61x_v1.bin.se Bluetooth: hci0: FW Download Complete: 412940 bytes If there is any other information that would be useful for analysis please ask Thank you Re: IW612 bluetooth crash after a few days > 1.Is it possible to provide us the HCI logs as well as that will help to identify which command is getting timeout for which the firmware dump is getting generated. Could you clarify what you mean with this? Is there a command that can be run after the fact, or should we run hcidump or equivalent to dump all commands while the process is running? > 3.To get Wi-Fi driver loading parameters, you can provide us the: /lib/firmware/nxp/wifi_mod_para.conf We do not use this file so default parameters should be used here as well. We've reduced the log level from the default values so dmesg will not be of much help here either (I sent a link to dmesg in the previous reply) I'll check with our user if they use wifi at all during this time Re: IW612 bluetooth crash after a few days Hi, @martinetd  1.Is it possible to provide us the HCI logs as well as that will help to identify which command is getting timeout for which the firmware dump is getting generated. 2.Can you please provide the WLAN based use case as WLAN is running then check if WLAN is working fine during the firmware dump is getting generated? 3.To get Wi-Fi driver loading parameters, you can provide us the: /lib/firmware/nxp/wifi_mod_para.conf  or you can provide us a normal booting dmesg logs which including the whole process that WiFi/bluetooth loading. We can get the info from dmesg logs. 4.Currently, we do not have newer public github FW release than the one you are using: imx-firmware/FwImage_IW612_SD at lf-6.18.20_2.0.0 · nxp-imx/imx-firmware · GitHub So, I do not think this is an known issue. We prefer to have more info related to the use case and hci logs to track what happened or reproduce steps so that we can reproduce the issue locally. So if you have any further other info related to the issue, please share with us. Best regards, Christine. Re: IW612 bluetooth crash after a few days Hi @Christine_Li thank you for the quick reply > 1. If you are using btnxpuart driver, please help to provide me btnxpuart.c. We are using the btnxpuart provided in https://github.com/nxp-imx/linux-imx based on version lf-6.12.49-2.2.0 , you can find the exact file here https://github.com/atmark-techno/linux-6.12-at/blob/6.12.105-r0/drivers/bluetooth/btnxpuart.c > 2. Are you using Wi-Fi and Bluetooth/802.15.4 combo FW? Or you are using separate FW? We are using both: the wifi driver loads the combo FW at boot, and after crash the separate FW is reloaded (hence log naming the separate FW) When this crash happened the combo FW was loaded (first crash after boot) but my understanding is that it reproduces with both > 3. Can you please help to provide your Wi-Fi and Bluetooth driver load parameters? The only wifi parameter we explicitly set is drv_mode = 0x3 to disable the wifi direct interface we do not use; we do not set any bluetooth parameter. If you can tell me how to dump the exact settings I can ask our user to run commands to get the info for us. > 4.Can you please let me know your detailed reproduce steps? Since this is based on a user report I can't say much more than the description I gave (RFCOMM connection polled every 60s for a few days); I'm afraid it might depend on the actual sub device the chip is connected to. I'll try to find a device that can be pinged over RFCOMM and reproduce locally to provide you with a test script if that helps, but for now I couldn't find any release note with known bugs for the firmware/btnxpuart driver so I'd like to confirm if there is a known bug (and hopefully if you can get any information from the firmware dump) Thank you Re: IW612 bluetooth crash after a few days Hi, @martinetd  1.Are you using our nxp's btnxpuart driver for bluetooth? or you are using Linux Open Source Uart driver? If you are using btnxpuart driver, please help to provide me btnxpuart.c. 2.Are you using Wi-Fi and Bluetooth/802.15.4 combo FW? Or you are using separate FW? Because I see your log as below, so I just suspect you are using separate FW, need to double confirm with you. hci0: Request Firmware: nxp/uartspi_n61x_v1.bin.se 3.Can you please help to provide your Wi-Fi and Bluetooth driver load parameters? 4.Can you please let me know your detailed reproduce steps?  Best regards, Christine. Re: IW612 bluetooth crash after a few days > * BlueZ stack (currently confirming the exact version, sorry I forgot to ask) in case it matters, the BlueZ version is 5.82
記事全体を表示
Power ArchitectureのS32 Design Studio v2.1におけるPEmicro GDBローンチ失敗 こんにちは、 私がテストしている基板はMTRCKTSPS5744P(3相PMSMモーター制御開発キットとMPC5744P MCU)です。 何らかの理由で、ダウンロード処理がうまくいきません。 ダウンロードに失敗した後、デバッグボタンをクリックすると、このウィンドウが表示されます。 eunwoo_lee_0-1789496057004.png このエラーメッセージが表示されたウィンドウがポップアップします。 サービス開始順序の誤り PEmicro GDB起動失敗:GDBサーバーがターゲットプロセッサへの接続を確立できませんでした。接続と電源を確認してください。デバッグ構成の起動設定が正確であることを確認してください。 コンソールパネルにこのメッセージが表示されます。 127.0.0.1 から 127.0.0.1 を経由して接続します。ポート「53438」から7224への接続 PEエラー:警告。部品が稼働している間はレジスタが読み取れません。 PEエラー:警告。部品が稼働中はメモリを読み取れません。@0 (4バイト) PEエラー:警告。部品が稼働中はメモリを読み取れません。@0 (4バイト) PEエラー:警告。部品が稼働している間はレジスタが読み取れません。 PEエラー:警告。部品が稼働中はメモリを読み取れません。@0 (4バイト) PEエラー:警告。部品が稼働中はメモリを読み取れません。@0 (4バイト) PEエラー:警告。パートが実行中はバイナリを書けません。40001000 - 長さ: 0 - 値: バイナリデータ PEエラー:警告。パートが実行中はバイナリを書けません。40001000 - 長さ: 460 - 値: バイナリデータ PEエラー:警告。パートが実行中はバイナリを書けません。40001460 - 長さ: 460 - 値: バイナリデータ PEエラー:警告。パートが実行中はバイナリを書けません。400018c0 - 長さ: 460 - 値: バイナリデータ PEエラー:警告。パートが実行中はバイナリを書けません。40001d20 - 長さ:2e0 - 値:バイナリデータ PE-エラー:GDBクライアント処理:例外が発生しました:プログラム例外! 例外クラス: EIDCONNCLOSEDGRACEFULLY メッセージ:接続が正常に切断されました。 アドレス 0X0046EA89 127.0.0.1 経由で「127.0.0.1」から切断されました。ポート「53438」による7224からの切断 ターゲットとの接続が切断されました。 この問題に対する解決策をご存知ですか? ありがとうございます。 Re: PEmicro GDB Launch Failure in S32 Design Studio for Power Architecture v2.1 こんにちは、 この問題に対する解決策をご存知ですか? メッセージの通り、レジスタをその場で書き込む・読み取ることはできません。まずデバッガーでコードの実行を停止し、その後レジスタやメモリなどを修正できます。 MPC5744Pはユーザーコードを実行中で、P&Eプローブがデバイスを停止できないため、すべてのメモリ/レジスタアクセスが失敗し、ダウンロード操作が中止されます。 これはフラッシュプログラミングの問題というよりは、デバッガがダウンロード前にMPC5744Pを停止させることに失敗しているように見えます。 例えば、マイクロコントローラでSWT0を有効にしたSWはありますか? それとも、ソフトウェアが一切動作していない、まっさらなサンプルなのでしょうか? よろしくお願いいたします。 ピーター
記事全体を表示
NXP官方是否有用于配置S32K344芯片外部启动的代码例程? NXP官方是否有针对S32K344芯片配置外部启动的代码例程和教程?我们想将芯片配置为从SD卡启动。 Re: Does NXP official have a code routine for configuring external boot for S32K344 chip? 在非安全启动配置中,第一个引导加载程序是否从 ROM 运行(它是不可变的吗)? 能否将第一个引导加载程序配置为从外部源/闪存启动后续的引导加载程序/应用程序映像? Re: Does NXP official have a code routine for configuring external boot for S32K344 chip? 该设备不提供从外部存储器启动的选项。 该设备支持安全启动和非安全启动模式,但两种情况下都是内部闪存启动。
記事全体を表示
HB200x AUTOSAR R21-11 Version 0.8.0 not supported by S32K3_RTD_6_0_0_D2506_ASR_REL_4_7_REV_0000_2025 Hello NXP, I tried to integrate the HB200x AUTOSAR spec SDK into the S32 Design Studio but I am getting the following error message: Issue: Mc33hb is not found in the toolchain/IDE project. The project will not compile! Level: Error Type: Validation Tool: Toolchain/IDE project Origin: Peripherals Target: Toolchain/IDE project: M7_0 Resource: platform.driver.mc33hb Even the files CDD_Mb33Hb.c CDD_Mb33Hb.h etc., have not been added when the SDK was installed in the S32 Design Studio application (v3.6.4) Re: HB200x AUTOSAR R21-11 Version 0.8.0 not supported by S32K3_RTD_6_0_0_D2506_ASR_REL_4_7_REV_0000_ Hi,  seems you are using wrong RTD version. Based on HB200x AUTOSAR R21-11 0.8.0 release note this software can be used on top of SW32K3_RTD_4.4_R21-11_3.0.0_D2303_DS_updatesite.zip (which needs to be installed in S32 Design Studio IDE v3.5). PetrS_0-1789471295419.pngPetrS_0-1789471295419.png BR, Petr
記事全体を表示
ARINC615A JTAG アクセスパスワード保護によるデータ読み込み HSEファームウェアがインストールされていない場合、CUST_DB_PSWD_Aフィールドおよびデバイスライフサイクル構成を使ってS32K3のSWD/JTAGアクセスを制限できます 。このパスワード保護を有効にしても、プロセッサへのARINC 615Aソフトウェアデータロードがデバッグインターフェースではなくアプリケーションやブートローダーソフトウェアで処理する場合、何か影響はありますか? Re: ARINC615A Data loading with JTAG Access password protected CUST_DB_PSWD_AはSWD/JTAGのデバッグアクセスのみを制限します。ARINC 615Aの実装の詳細は詳しくありませんが、ソフトウェアの負荷が完全にアプリケーションやブートローダーによって処理されているなら、デバッグパスワード自体が影響を与えることはないと思います。 最終的には、これはアプリケーションごとに異なり、ARINC 615Aがあなたのシステムでどのように実装されているかによります。更新機構がデバッグインターフェースを使用しない場合、デバッグアクセス制限は一般的にソフトウェアの読み込みプロセスに依存しないはずです。追加の制限はライフサイクル構成やアプリケーションのセキュリティ設計によって異なります。
記事全体を表示
NXPの公式ウェブサイトには、S32K344チップの外部ブートを設定するためのコードルーチンはありますか? NXPの公式ウェブサイトには、S32K344チップの外部ブートを設定するためのコードルーチンとチュートリアルはありますか?チップをSDカードから起動するように設定したいのですが? Re: Does NXP official have a code routine for configuring external boot for S32K344 chip? セキュアブートではない構成の場合、最初のブートローダーはROMから実行されますか(変更不可能ですか)? この最初のブートローダーは、外部ソースやフラッシュからその後のブートローダーやアプリケーションイメージを起動するように設定できますか? Re: Does NXP official have a code routine for configuring external boot for S32K344 chip? このデバイスには、外部メモリからの起動オプションはありません。 デバイスはセキュアと非セキュアの起動モードの両方をサポートしていますが、いずれの場合も内部フラッシュブートです。
記事全体を表示
S32 Design Studio インストールの問題 S32 Design Studio(バージョン3.6.4)で問題が発生しています。インストール。インストール開始すると進行状況バーはすぐに終了しますが、インストールされたアプリケーションは見えませんでした。 この問題を解決する方法についてご指導ください。 システム仕様は、Windows 11、16GB RAM、1TB SSDです。このシステムは当社のITポリシーの対象です。 Re: S32 Design Studio Installation Issue 以下に、ご依頼いただいたログファイルを示します。 インストールを2回試みましたが、成功しませんでした。 Re: S32 Design Studio Installation Issue こんにちは@ashutoshsahu インストールログファイル(.log)を共有してもらえますか?それは以下の場所にあります: C:\NXP\S32DS.3.6.4\_S32S32プラットフォーム用Design Studio 3.6.4_installation\Logs BR、VaneB
記事全体を表示
MX95:生ビデオ書き込みスループットは最大約50MB/秒に制限されます こんにちは。生のカメラフレームをファイルに書き込む際に、スループット/フレームレートの問題が発生しています。フレームをストレージに書き込むと、実際のキャプチャレートが目標フレームレートを大幅に下回ります。書き込みを行わない純粋なキャプチャはフルフレームレートで動作するにもかかわらずです。私たちはその原因を理解したいのです。以下は、当社の環境設定です。 - ボード: i.MX95 19x19 LPDDR5 EVK - BSP:TechNexion Yocto 5.3(Whinlatter)、カーネル6.18.2 - カメラ:TechNexion TEVS-AR0234 (MIPI CSI-2) - キャプチャ装置はmedia-ctlで確認:tevs → csidev-4ad30000.csi → formatter@20 → クロスバー→ mxc_isi.0→ /dev/video0 ## テスト 1: キャプチャのみ、書き込みなし (ベースライン) センサーが30fpsにロックされている方法: V4L2-ctl -d /dev/v4l-subdev19 --set-subdev-fps pad=0,stream=0,fps=30 gst-launch-1.0-e libcamerasrc !video/x-raw、幅=1920、高さ=1080、フォーマット=YUY2、フレームレート=30/1 !fpsdisplaysink video-sink=fakesink text-overlay=false sync=false 結果:安定した29.98fps、フレーム落ちなし。 ## テスト2:生のフレームをファイルに書き込む gst-launch-1.0-e libcamerasrc !video/x-raw、幅=1920、高さ=1080、フォーマット=YUY2、フレームレート=30/1 !filesink location=/tmp/test.yuv 結果:約11.7fps(ファイルサイズ/キャプチャ時間で測定)、GStreamerログには繰り返し警告が表示されました。 警告 NxpNeoPipe neo_pipeline.cpp:3175画像0フレームが失われました!X を期待していたが Y を受け取った。 FPSがロックされていないと期待と受信の差は時間とともに広がりますが、センサーのFPSがターゲットに合わせるようにロックされると、1〜2フレームほど小さく保たれます。 `libcamerasrc`の代わりに`v4l2src device=/dev/video0`を使用して同じテストを繰り返しました。結果は同じ約11.7~11.8fpsでした。 同じテストを1280x720で繰り返したところ、約28.8fps(約53MB/s)となり、これは上記の1920x1080のテスト(約52MB/s)と同様のMB/sの上限値に相当します。 `/dev/video0` (mxc-isi) からキャプチャした生のフレームをストレージに書き込む際に、書き込み速度が約 50 MB/s に制限されるのは、現在の BSP/カーネル バージョンにおける想定される動作なのか、それとも設定項目を見落としている可能性があるのかを知りたいです。必要に応じて、完全なログ、『media-ctl』トポロジー出力、デバイスツリー情報の提供も喜んで承ります。 Yocto Project Re: MX95: raw video write throughput limited to ~50MB/s こんにちは、 @JosephAtNXPさん、迅速なご対応ありがとうございます。 根本原因が以下の要因にあるかどうか確認したい。さらに、この場合にReal-Time Yoctoを使うのは役立つでしょうか? キャプチャされたフレームは、連続メモリ割り当て器(CMA)によって割り当てられたDMAバッファに格納されます。ISPハードウェアからこのメモリへのDMA書き込みはボトルネックになったことはありません(ddを使ったローカルtmpfsの書き込み速度は最大819 MB/sに達し、ストレージメディアの制限は除外されます)。 ボトルネックは、CPUがこのバッファの内容を読み取るステップで発生します。これは、VPUハードウェアエンコーダがDMA経由で同じバッファを直接読み取ってもパフォーマンスに影響がないという事実によっても裏付けられています。これは、ボトルネックの原因がバス帯域幅やストレージデバイスの速度制限ではなく、メモリのキャッシュ属性構成、あるいは各バッファデキュー操作中のキャッシュコヒーレンシの維持コスト(例えば、キャッシュ無効化)にあることを強く示唆している。 Re: MX95: raw video write throughput limited to ~50MB/s こんにちは、 NXP Semiconductors製品にご関心いただきありがとうございます。 これはLinuxユーザーガイドで見られるように、予想される動作です。 さらに、フレームをファイルシステムに書き込むと、リアルタイムでは処理しきれないほどの膨大な量のデータが生成されます。その場合、アプリケーションがバッファをリサイクルする際に遅延が生じるため、周期的なフレームロスが発生することが予想されます。 回避策としては、キャプチャされたフレームを保存する前にハードウェアのビデオエンコーディングを使う方法があります。 よろしくお願いします。
記事全体を表示
RW612 / 村田製作所製 Type 2FR EVK – 起動後にSRAM常駐コードが破損する NXPチームの皆様、こんにちは。 私は 村田Type 2FR EVK(RW612 )をデバッグ中で、アプリケーションプログラムは外部QSPIフラッシュに正常に入力されるものの、正しく動作しません。 ハードウェア: 村田製作所製 2FR型 EVK (LBES0ZZ2FR) MCU:RW612 Cortex-M33 外部フラッシュメモリ:Winbond W25Q128、16MB デバッガ: SEGGER J-Link、S/N 69657567 100kHzでのSWD ボードはUSB-C経由で給電されます。 SWD: J11 ピン2 = SWDIO、ピン4 = SWCLK、ピン3 = GND J-LinkはRW612を正常に検出し、エラーなく外部フラッシュメモリへの書き込みを完了しました。 ソフトウェア: MCUXpresso IDE 25.6.136 RW612 SDK rdrow612bga_wifi_cli のサンプルから始めました。 W25Q128のFlexSPIフラッシュ構成を変更し、QSPIリンカーのサイズを8MBから16MBに変更しました。 ビルドはエラー/警告なしで完了しました。 問題: 起動後、CPUは最終的に以下の状態で停止します。   PC = 0x20005840 ip4_input() at lwip/src/core/ipv4/ip4.c:556   関数ip4_input()はSRAMの0x200056D4にありますが、その内容は破損しているようです。   0x200056D4: 0x4007EEBE 0xBC640C88 ...     しかし、QSPIフラッシュ内の対応するコードは有効であるように見える。 リンカーマップは.dataを示していますRAM常駐コードが含まれています。   LMA: 0x080F674C VMA: 0x20000000 Size: 0x1A0E4   そして、起動セクションの表には以下が指定されています。   0x080F674C → 0x20000000, length 0x1A0E4   ResetISR() は SystemInit() を呼び出し、続いて data_init() を呼び出し、この初期化を実行します。 SRAM自体がデバッガを通して読み書き可能であることも確認しました。 私の主な疑問は、 QSPIソースイメージは正常に見えるにもかかわらず、なぜRAM常駐コードが破損してしまうのかということです。 これは RW612の起動/RAM初期化、FlexSPIの設定、キャッシュ/MPU設定、起動設定、またはType2FR専用のメモリ構成に関連しているのでしょうか? また、 MCU-Link Proの代わりにSEGGER J-Link を使うと、このブート/デバッグフローに問題が起きると思いますか? .mapは提供できます。リンカースクリプト、startup_rw612.c、flash_config.c、必要に応じてデバッグログも出力します。 よろしくお願いします。 評価ボード Re: RW612 / Murata Type 2FR EVK – SRAM-resident code corrupted after boot こんにちは、ダニエルさん。 ご回答ありがとうございます。 以前はSDK 26.06を使っていましたが、プロジェクトはFRDM-RW612構成ではなくrdrw612bgaボードで設定されていました。 移行ガイドについては、はい、既に確認済みです。 [NXP FRDM-RW612モジュール移行ガイド]( https://github.com/NXP-APPCODEHUB/an-frdmrw612-module-migration-guide ) 村田製作所製Type 2FRの移行手順に従い、W25Q128(16MB)のフラッシュ構成と対応するリンカー構成を更新しました。 しかし、アプリケーションプログラムが正常に実行を始めるのに、最終的には「0x20005840」で「ip4_input()」で停止する問題に直面しています。また、SRAMから実行されるはずのコードは破損しているように見える一方、QSPIフラッシュ内の対応するコードは有効であるように見えることも判明しました。 ご提案に基づき、今後はFRDM-RW612構成の**26.06 SDKを使用し、そのベースラインからの移行アプローチを踏みます。結果をThreadに更新します。 ご指導いただき、改めて感謝申し上げます。 よろしくお願いいたします。 サクシー Re: RW612 / Murata Type 2FR EVK – SRAM-resident code corrupted after boot こんにちは、 どのSDKバージョンを使っているのか教えていただけますか? FRDM-RW612にはRDではなく26.06を使用することをお勧めします。 ところで、あなたはもうこれについて調べましたか? よろしくお願いいたします。 ダニエル。
記事全体を表示
DCMLCCレジスタを読み取ると、未定義値0x00000033が返されます。 こんにちは S32K314のDCMLCCレジスタを読み取ったところ、返された値は0x00000033、DCMRLC:0b011、DCMCLC:0b011でした。データシートにはこれらの値の定義が記載されていません。これらの値は何を意味するのでしょうか?DCMLCSの値を取得しようとしたところ、0x06186084が得られました。これは、私のチップがライフサイクルのどの段階にも達していないことを意味し、正常な値なのでしょうか? DCMCLC.jpegDCMCLC.jpeg DCMRLC.jpegDCMRLC.jpeg リカ Re: I get an undefine value 0x00000033 when I read the DCMLCC register はい、どうもありがとうございました。 Re: I get an undefine value 0x00000033 when I read the DCMLCC register こんにちは、リカさん。 ご迷惑をおかけして申し訳ございません。 この問題は文書管理部門に報告済みです。 0b011はCUST_DELを意味します よろしくお願いします、 ロビン
記事全体を表示
IMX6ULLにHABファームウェアを書き込む方法(USBについて) 私たちはIMX6ULLを使用しており、セキュアブート機能を実装したいと考えています。 現在のSDブートモードは実行され、開発ボードはSRKを書き、ファームウェアも署名済みです。次に、クローズ操作も実行しました(echo 0x02>HW_OCOTP_CFG5)。 書き込み後の通常の印刷情報は以下のとおりです。 セキュアブートが有効になっています HAB構成: 0xcc、HAB状態: 0x99 しかし、同じファームウェアをmfgtoolsツールに置きUSBで焼くと、基板が焼却システムに入らないことが判明しました。 ツールが動作を停止し、デバッグ用シリアルポートから出力情報が得られなくなります。 rxq_0-1789457007595.pngrxq_0-1789457007595.png 赤い枠で囲まれたファームウェア、%board_file%/u-boot.imx および firmware/zImage は署名済みのファームウェアです。 MfgTool.logには、ファームウェアがインポートされたことが記録されています。通常のプロセスでOSイメージにジャンプした後、インポートを開始したファームウェアが読み込まれるはずですが、実際にはデバッグシリアルポートに情報が出力されません。 rxq_1-1789457333755.pngrxq_1-1789457333755.png SDカードは正常に起動するのに、USBは起動しないのはなぜですか? USB焼却をサポートするためには何をすべきでしょうか?添付ファイルは、当社のSDによって開始されたセキュアブート製造プロセスです。
記事全体を表示