2413555_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2413555_en-US

2413555_en-US

HB200x AUTOSAR R21-11 Version 0.8.0 not supported by S32K3_RTD_6_0_0_D2506_ASR_REL_4_7_REV_0000_2025

Hello NXP,

I tried to integrate the HB200x AUTOSAR spec SDK into the S32 Design Studio but I am getting the following error message:

Issue: Mc33hb is not found in the toolchain/IDE project. The project will not compile!

Level: Error

Type: Validation

Tool: Toolchain/IDE project

Origin: Peripherals

Target: Toolchain/IDE project: M7_0

Resource: platform.driver.mc33hb

Even the files CDD_Mb33Hb.c CDD_Mb33Hb.h etc., have not been added when the SDK was installed in the S32 Design Studio application (v3.6.4)

Re: HB200x AUTOSAR R21-11 Version 0.8.0 not supported by S32K3_RTD_6_0_0_D2506_ASR_REL_4_7_REV_0000_

Hi, 

seems you are using wrong RTD version. Based on HB200x AUTOSAR R21-11 0.8.0 release note this software can be used on top of SW32K3_RTD_4.4_R21-11_3.0.0_D2303_DS_updatesite.zip (which needs to be installed in S32 Design Studio IDE v3.5).

PetrS_0-1789471295419.pngPetrS_0-1789471295419.png

BR, Petr

タグ(1)
評価なし
バージョン履歴
最終更新日:
1週間前
更新者: