UM11490 and Bluetooth Classic Dear NXP support, one of our customer is running the following commands from pag 149 of UM11490, but cannot see any waveform. Please kindly check and verify if any additional command / condition is missing. Thanks Best Regards Pier ------------------------------------ # RESET root@myboard:/home/BTtest# hcitool -i hci0 cmd 0x03 0x0003 < HCI Command: ogf 0x03, ocf 0x0003, plen 0 > HCI Event: 0x0e plen 4 01 03 0C 00 # ENABLE SCAN root@myboard:/home/BTtest# hcitool -i hci0 cmd 0x03 0x001a 0x3 < HCI Command: ogf 0x03, ocf 0x001a, plen 1 03 > HCI Event: 0x0e plen 4 01 1A 0C 00 # ENABLE EVENT FILTER root@myboard:/home/BTtest# hcitool -i hci0 cmd 0x03 0x0005 0x02 0x00 0x02 < HCI Command: ogf 0x03, ocf 0x0005, plen 3 02 00 02 > HCI Event: 0x0e plen 4 01 05 0C 00 # ENTER IN TEST MODE root@myboard:/home/BTtest# hcitool -i hci0 cmd 0x06 0x0003 < HCI Command: ogf 0x06, ocf 0x0003, plen 0 > HCI Event: 0x0e plen 4 01 03 18 00 # START THE TX TRANSMISSION root@myboard:/home/BTtest# hcitool -i hci0 cmd 0x3F 0x0019 0x80 0x80 0x80 0x80 0x01 0x00 0x01 0x01 0x0D 0x03 0x0F 0x00 0x00 0x00 0x00 0x00 0x00 0x04 < HCI Command: ogf 0x3f, ocf 0x0019, plen 18 80 80 80 80 01 00 01 01 0D 03 0F 00 00 00 00 00 00 04 > HCI Event: 0x0e plen 4 01 19 FC 00 # STOP THE TX TRANSMISSION root@myboard:/home/BTtest# hcitool -i hci0 cmd 0x3F 0x0019 0x80 0x80 0x80 0x80 0xF F 0x00 0x01 0x01 0x0D 0x03 0x0F 0x00 0x00 0x00 0x00 0x00 0x00 0x04 < HCI Command: ogf 0x3f, ocf 0x0019, plen 18 80 80 80 80 FF 00 01 01 0D 03 0F 00 00 00 00 00 00 04 > HCI Event: 0xff plen 6 19 01 39 00 00 00 -------------------- STOPPING THE SCAN FOR BLE AND CLASSIC BEFORE THE TX TRANSMISSION ---------------- # RESET root@myboard:/home/BTtest# hcitool -i hci0 cmd 0x03 0x0003 < HCI Command: ogf 0x03, ocf 0x0003, plen 0 > HCI Event: 0x0e plen 4 01 03 0C 00 # ENABLE SCAN root@myboard:/home/BTtest# hcitool -i hci0 cmd 0x03 0x001a 0x3 < HCI Command: ogf 0x03, ocf 0x001a, plen 1 03 > HCI Event: 0x0e plen 4 01 1A 0C 00 # ENABLE EVENT FILTER root@myboard:/home/BTtest# hcitool -i hci0 cmd 0x03 0x0005 0x02 0x00 0x02 < HCI Command: ogf 0x03, ocf 0x0005, plen 3 02 00 02 > HCI Event: 0x0e plen 4 01 05 0C 00 # ENTER IN TEST MODE root@myboard:/home/BTtest# hcitool -i hci0 cmd 0x06 0x0003 < HCI Command: ogf 0x06, ocf 0x0003, plen 0 > HCI Event: 0x0e plen 4 01 03 18 00 # DISABLE THE BLE SCAN root@myboard:/home/BTtest# hcitool -i hci0 cmd 0x03 0x001a 0x0 < HCI Command: ogf 0x03, ocf 0x001a, plen 1 00 > HCI Event: 0x0e plen 4 01 1A 0C 00 # DISABLE THE CLASSIC SCAN root@myboard:/home/BTtest# hcitool -i hci0 cmd 0x08 0x000C 0x00 0x00 < HCI Command: ogf 0x08, ocf 0x000c, plen 2 00 00 > HCI Event: 0x0e plen 4 01 0C 20 00 # START THE TX TRANSMISSION root@myboard:/home/BTtest# hcitool -i hci0 cmd 0x3F 0x0019 0x80 0x80 0x80 0x80 0x01 0x00 0x01 0x01 0x0D 0x03 0x0F 0x00 0x00 0x00 0x00 0x00 0x00 0x04 < HCI Command: ogf 0x3f, ocf 0x0019, plen 18 80 80 80 80 01 00 01 01 0D 03 0F 00 00 00 00 00 00 04 > HCI Event: 0x0e plen 4 01 19 FC 00 # STOP THE TX TRANSMISSION root@myboard:/home/BTtest# hcitool -i hci0 cmd 0x3F 0x0019 0x80 0x80 0x80 0x80 0xFF 0x00 0x01 0x01 0x0D 0x03 0x0F 0x00 0x00 0x00 0x00 0x00 0x00 0x04 < HCI Command: ogf 0x3f, ocf 0x0019, plen 18 80 80 80 80 FF 00 01 01 0D 03 0F 00 00 00 00 00 00 04 > HCI Event: 0xff plen 6 19 01 63 07 00 00 ** When disabling the scan before entering in the test mode, the stop for TX transmission give us: root@myboard:/home/BTtest# hcitool -i hci0 cmd 0x3F 0x0019 0x80 0x80 0x80 0x80 0xFF 0x00 0x01 0x01 0x0D 0x03 0x0F 0x00 0x00 0x00 0x00 0x00 0x00 0x04 < HCI Command: ogf 0x3f, ocf 0x0019, plen 18 80 80 80 80 FF 00 01 01 0D 03 0F 00 00 00 00 00 00 04 > HCI Event: 0xff plen 6 19 01 ED 04 00 00 For Wifi 5 GHz -------------------------------------------------------------------------------- Paramters: Continuous transmit, BW = 40 MHz, 802.11ac, No DFS, CH = 40, MCS0 (13.5), Power = 14 dBm root@myboard:/home/BTtest# cat /proc/mwlan/adapter0/config hardware_status=0 netlink_num=31 drv_mode=7 hssetpara=7,0xff,200,400 sdcmd52rw=0 0x0 0x00 rf_test_mode=1 tx_antenna=1 rx_antenna=1 band=1 bw=1 channel=44 radio_mode[0]=3 radio_mode[1]= total rx pkt count=0 rx multicast/broadcast pkt count=0 rx fcs error pkt count=0 tx_power=14 2 0 tx_continuous=0 tx_frame=1 4352 0xaaa 1024 1 20 4294967295 0 0 4294967295 0 0 0 -1 -1 -1 -1 -1 -1 -1 05:43:3f:c4:51:ff he_tb_tx=0 trigger_frame=0 otp_mac_add_rd_wr= 00:00:00:00:00:00 Re: UM11490 and Bluetooth Classic Hi @Christine_Li, sorry for missing the context: kernel version: lf-6.6.52-2.2.2 merged with 6.6.y community kernel FW version: IW612-18.99.3.p25.7, sepaated BT/WiFi FW, no combo product: IW612 UM11490 version: Rev. 1.8 — 2 June 2025 The following details will come ASAP dmesg logs or console logs when you load FW screenshot of the spectrum analyzer settings In the meanwhile, please let us know if you may need anything else. Thanks Best Regards Pier Re: UM11490 and Bluetooth Classic Hi, @pierluigi_p
Which Wi-Fi/Bluetooth product are you using?
And what is your Linux kernel version? WiFi/Bluetooth driver and FW version?
From the command logs, all HCI commands are completed successfully and the TX start command is accepted by the controller. In addition, the vendor-specific event returned by the TX stop command contains non-zero packet counters, which indicates that the controller believes packets have been transmitted during the test period.
Therefore, the issue does not appear to be caused by a missing HCI command in the test sequence.
I would recommend checking:
The spectrum analyzer center frequency and span settings. The Bluetooth channel configured by the TX test command. The RF antenna configuration on the board. Whether the Bluetooth firmware are loaded correctly.
Could you also share:
The chip being used (IW416/IW612/etc.)? The exact UM11490 version?
The dmesg logs or console logs when you load FW?
Are you loading a combo FW or BT only FW? A screenshot of the spectrum analyzer settings?
Best regards,
Christine. Re: UM11490 and Bluetooth Classic Just adding, it was attempted with different settings for HackRF (gain and graphic adjustments), and we can see the 2.4 GHz (wifi) waveforms. Furthermore, we tested using different firmwares, for different versions in the imx-firmware repository, which includes one firmware for RF-test (sduart_nw61x_rftm_v1.bin.se in https://github.com/nxp-imx/imx-firmware/blob/lf-6.1.1_1.0.0/nxp/FwImage_IW612_SD/IW612_SD_RFTest/sduart_nw61x_rftm_v1.bin.se) without success. Re: UM11490 and Bluetooth Classic Hello Pier and Christine I'm Helbert, the developer who started the thread in the Veriscite forum. Here are some attachments about the testing: Dmesg log (without the power configuration): Dmesg log (with the power configuration): Screenshot with the spectrum analyzer and the config file for 5 GHz (own implementation and NXP implementation) 5GHz-running-test.png after 5GHz-after-test.png Note: it was found that using -1 for power, we use the default value, however different values was experimented too. NXP script: NXP-5GHz-running-test.png Screenshot with the classic Bluetooth test: Bluetooth-2.4-Classic-RUNNING.png As you can see, there is no waveform generated Screenshot with the BLE test running: BLE-RUNNING-2.4-CH2.png Screenshot after the BLE testing (waveform interrupted): BLE-FINISHED.png We can see in the graphic below that the waveform was interrupted when finishing the test Modinfo log: Tested HCI cmds: Re: UM11490 and Bluetooth Classic Hi, @HelbertPaulino
Thanks for providing me the details.
Let me check your info and screenshot, then reply to you.
Please allow me some time.
Best regards,
Christine. Re: UM11490 and Bluetooth Classic Hi, @HelbertPaulino
Thanks for providing us the details.
Your screenshot only shows some Background noise, there is no any useful RF waveform information.
May I ask:
1.You are using our IW612-EVK? or any module? If module, would you mind let me know your module part number?
2.How is your HW connections with the test equipment?
3.Your question is for BT or Wi-Fi?
If for BT, I see your test commands, in our RF test guide, the stop command is:
hcitool -i hci0 cmd 0x3F 0x0019 0x80 0x80 0x80 0x80 0xFF
but you are sending:
root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x3F 0x0019 0x80 0x80 0x80 0x80 0xFF 0x00 0x01 0x01 0x0D 0x03 0x0F 0x00 0x00 0x00 0x00 0x00 0x00 0x04
Please follow exactly our guide command to execute.
Best regards,
Christine. Re: UM11490 and Bluetooth Classic Hello Christine, thanks for your checkings 1.You are using our IW612-EVK? or any module? If module, would you mind let me know your module part number? We have the module integrated into the SoM Variscite DART-IMX8M https://variscite.com/system-on-module-som/i-mx-8/i-mx-8m-plus/dart-mx8m-plus/ It has the part number: LBES5PL2EL.4 2.How is your HW connections with the test equipment We have wireless access to the equipment's radio through the HackRF One equipment, which can capture the signals using its antenna (but it can capture other signals too; that's the reason for why you are seeing some noise) 3 - Your question is for BT or Wi-Fi? It's for both. For classical Bluetooth, we weren't able to see the generated waveforms (only for Bluetooth Low Energy), and for Wifi, we couldn't capture signals in 5 GHz About the hci command, I saw both, and we have both recommended in the NXP/Murata documents In AN14114, we have the short command on page 47 In UM11490 we have the long command on page 150 For the classic Bluetooth, I think I found the solution. When checking the UM11490, the explanation for the command is: hcitool -i hci0 cmd The examples in the document set tx_test_interval as 0x0D, in this scenario, the interval seems to be a little longer and, hence, it's a little hard to see the generated waveform. It appears like noise. When setting this parameter to 0x01, I could see a consistent waveform. Furthermore, I decreased the frequency range because it's a low-BW waveform. So, I think this solves the Bluetooth issue. However, I'm still not able to see the 5 GHz waveform. Do you have any tips for it? Thanks very much for your assistance Re: UM11490 and Bluetooth Classic Hey Christhine, It was raised the possibility of having another Murata Module in my used SoM. I disassembled the mine and I detected that its part number is: LBEE5PL2DL Hence, I have to review if the commands for 2EL are applicable to this model too Re: UM11490 and Bluetooth Classic Hello Christine, Thanks very much for your support. Debugging here a little more, I found a potential trouble here. When changing the region using the files provided here: https://github.com/murata-wireless/nxp-linux-calibration/tree/imx-6-6-23/murata/files/2DL, I noticed a trouble with iw reg set Basically, following the idea posted here: https://murata.my.site.com/muratacommunity/s/question/0D5RC00001HGuiQ0AT/rf-test-mode-firmware-and-tools-for-murata-type-2dl-module-not-working I used the files directed for 2EL (and 2DL, they are the same), but when switching the regions, I could note that the iw reg get wasn't changing its location, by presenting the following message: HelbertPaulino_0-1784905230306.png Hence, when changing the regions to be used by the driver with the file *txpower*.bin, we weren't changing the system region. I saw that this has the potential to prevent the waveforms from being triggered, depending on the chosen region and settings applied to the radio. I removed the regulatory.db* files from Murata and used the original, and it seems to have better behavior. I was able to trigger some 5 GHz waveforms, and others I think are being masked by the noises May you confirm if the iw reg set / reg and the used regulatory files can affect the waveform generation? If yes, then I think we found the root cause of the problem. It's not Firmware / Script / Calibration files, but a region limitation. Do you think it makes sense or do you have another suspect for this? Thanks very much again Re: UM11490 and Bluetooth Classic Hi, @HelbertPaulino
Thanks for your info and glad to hear that Bluetooth is now working.
So now let's focus on the Wi-Fi 5G RF test mode issue.
LBEE5PL2DL module's Chipset is our NXP's WiFi/Bluetooth chipset: IW611.
The difference between IW611 and IW612 is: IW612 supports 802.15.4, but IW611 does not support.
But for WiFi and Bluetooth, IW611 and IW612 are same.
So it means, the commands for 2EL are applicable to this model(LBEE5PL2DL) too.
Then now please help to follow AN14114's section: 2 Wi-Fi RF test mode to set your board and start the WiFi 5G RF test.
Currently from your shared cat /proc/mwlan/adapter0/config results, I do not find any suspect points. The only thing is: please check your test equipment connections and also HW connections.
At the same time, let me check internally to see whether it is supported to test RF on these 2 modules. What I confirmed is: we can test on our IW611 or IW612 EVK board, but for these 2 modules, I need to check whether need to do any HW reworks to allow to test RF performance.
Once have any updates, will let you know.
Best regards,
Christine. Re: UM11490 and Bluetooth Classic Hi Christine, I didn't see this message and replied to the other. Yes, I tried different BW settings, but I'm trending to think the problem can be attributed to the region limitation and noise in some regions. Re: UM11490 and Bluetooth Classic Hi, @HelbertPaulino
Can you please have a try with changing 40MHz to 20 MHz bandwidth for initial capture?
echo "tx_frame=0" >> /proc/mwlan/adapter0/config
echo "bw=0" >> /proc/mwlan/adapter0/config
Your readback shows bw=1 , which AN14114 defines as 40 MHz ; bw=0 is 20 MHz .
For HackRF observation, 20 MHz is the better first test because 40 MHz Wi-Fi is harder to capture/recognize cleanly on a narrow or marginal SDR setup.
Please let me know whether it works fine for 20MHZ. Then we step by step to move to 40MHZ.
Best regards,
Christine. Re: UM11490 and Bluetooth Classic Hi, @HelbertPaulino
Can you please have a try with below command:
echo "tx_continuous=1 0 0xAAA 0 3 0x1100" >> /proc/mwlan/adapter0/config
instead of tx_frame command?
I found in your previous output of "cat /proc/mwlan/adapter0/config"
tx_frame=1 4352 0xaaa 1024 1 20 4294967295 0 0 4294967295 0 0 0 -1 -1 -1 -1 -1 -1 -1 05:43:3f:c4:51:ff
I worry it might not be recognized correctly.
Best regards,
Christine. Re: UM11490 and Bluetooth Classic Hey Christine I was verifying the command, and you are right, but I don't know why that parameters (SHORT_PREAMBLE and ADVANCED_CODING) was appearing as -1 (represented as 4294967295) Maybe in the first implementation for the code, they was wrongly set as -1. However, replying your request, now we can generate the waveform for 5 GHz (tx_frame). For tx_continuous I could see the waveforme, but in a lower amplitude (almost not possible to see) You can look the frame generation in the picture below: 5GHz-CH100-BW40-FRAME-0x1100-14.png When trying to trigger the continuous, I could see the waveform, but very smoothly 5GHz-CH100-BW40-CONTINUOUS-0x1100-14.png I used the configuration above. I think the problem of not being able to see the waveforms for channels is due to the noise we have in the equipment are bigger than the waveform generated. I requested the Hardware team to verify using a more powerful spectrum analyzer. I'm waiting for its response to close the question for the non-generated waveforms. But about the regions, do you think it can explain why some waveforms are not being generated? Re: UM11490 and Bluetooth Classic Hi, @HelbertPaulino
Yes, an incorrect Region/Regulatory Domain configuration can also explain why some 5 GHz Wi-Fi waveforms are not being generated, or why the device does not transmit at all on certain channels.
Does your Hardware team to verify using a more powerful spectrum analyzer?
Anything else I can do for you on this case?
Best regards,
Christine. Re: UM11490 and Bluetooth Classic Hello Christine, I think this confirmation and the tests that the guys did in another noiseless environment confirm that everything is now working properly. Thanks very much for your support. Nice to meet you Re: UM11490 and Bluetooth Classic Hi, @HelbertPaulino
Thanks for your reply and glad to hear that everything is now working properly.
Then would you please help to mark my answer as a solution for this thread so that we can close this case?
And also, please feel free to create new case to us if you have any other topic questions in the future.
We are always glad to support you!
Best regards,
Christine. Re: UM11490 and Bluetooth Classic Thanks very much again, Christine. I'll do that 🙂
記事全体を表示