FP92 p119.2 FW crash of 88W8997, 88W8987 when bring up WiFi if txpower.bin file included. HW: i.mx8mm or i.mx8mp, + AW-CM358 (88w8987) or Murata 1YM (88W8997) SW: SDK 6.6.3 WiFi: Tried NXP EVK board i.mx8mm PCIE8997--16.92.21.p119.2-MM6X16437.p3-GPL-(FP92) SD8987----16.92.21.p119.2-MM6X16437.p3-GPL-(FP92) Customer side: i.mx8mp kernel: 5.x SD8997 ---- 16.92.21.p119.2-16.92.21.p119.2-MM6X16437.P3-GPL Ref version: Tried i.mx8mm 6.1.22 SD8987----16.92.21.p76.5-MM5X16391.p3-GPL-(FP92) PCIE8997--16.92.21.p84.4-MM5X16391.p3-GPL-(FP92) No issue on this version. Steps: 1. Convert conf to txpower bin by (refer to UM11490) ./mlanutl mlan0 hostcmd txpwrlimit_cfg_8987.conf generate_raw txpower.bin or ./mlanutl mlan0 hostcmd txpwrlimit_cfg_8997.conf generate_raw txpower.bin OK: without this line: txpwrlimit_cfg=nxp/txpower.bin NOK(FW crash just after load txpower.bin): add this line txpwrlimit_cfg=nxp/txpower.bin in /lib/firmware/nxp/wifi_mod_para.conf and then bring up by modprobe moal mod_para=nxp/wifi_mod_para.conf FW crash after dmesg txpwrlimit_cfg=nxp/txpower.bin Logs share: NOK logs: 663_p1192_8987_fail.txt 663_p1192_8997_fail.txt OK logs: 663_p1192_8987_ok_noPwr.txt 663_p1192_8997_ok_noPwr.txt 6122_i.mx8mm_8987.txt 6122_p844_i.mx8mm_8997_noPwr_ok.txt 6122_p844_i.mx8mm_8997_withPwr_ok.txt Customer can share their logs if needed. Please help check if the procedure need to be changed after p119.2 Thanks. Re: FP92 p119.2 FW crash of 88W8997, 88W8987 when bring up WiFi if txpower.bin file included. Hi, @NancyHuang We have standalone release completed and available on the nxp.com with secure sign in. Can you please check if this link can be accessible to you for the Q2 release? Below link is for 88W8987: https://www.nxp.com/webapp/sps/download/license.jsp?colCode=SD.GEN.16.92.21.p119.3-MM6X16437.P21-GPL&appType=file1&DOWNLOAD_ID=null Below link is for 88W8997: Generic_SD-WLAN-UART-BT-8997-LNX_6_6_23-IMX8-16.92.21.p119.3-16.92.21.p119.3-MM6X16437.P21-GPL Generic_PCIE-WLAN-UART-BT-8997-LNX_6_6_23-IMX8-16.92.21.p119.3-16.92.21.p119.3-MM6X16437.P21-GPL If this is not accessible, then you may need to use Q2 (end of June) release available via i.MX BSP or Github release. Thanks, Christine. Re: FP92 p119.2 FW crash of 88W8997, 88W8987 when bring up WiFi if txpower.bin file included. Hi @Christine_Li Thanks for your reply. Could you tell us when the new firmware will be available? 6/28? Nancy Re: FP92 p119.2 FW crash of 88W8997, 88W8987 when bring up WiFi if txpower.bin file included. Hi, @yao_feng
I received our internal team feedback as below:
The reported issue is a regression issue and it is fixed already.
We have verified the changes on our local setup and it is working fine.
The release with the fixes will be available in Q2 (end of June).
Please help to update this info to our end customer and request them to verify on the Q2 release.
Thanks.
Best regards,
Christine. Re: FP92 p119.2 FW crash of 88W8997, 88W8987 when bring up WiFi if txpower.bin file included. Hi, @yao_feng
We are able to observe FW crash/Kernel panic as below on our local setup:
Message from syslogd@imx8mpevk at Wed Sep 20 11:32:59 2023 ...
kernel: Internal error: Oops: 0000000096000007 [#1] PREEMPT SMP
Message from syslogd@imx8mpevk at Wed Sep 20 11:32:59 2023 ...
kernel: Code: 91000f9c 1100077b 6b1b029f 54001a0b (38401743)
[ 244.448042] Timeout cmd id (244.444015) ??? [0xecf], act = 0x0
We are checking internally for further debugging the issue. We will update you soon.
Best regards,
Christine. Re: FP92 p119.2 FW crash of 88W8997, 88W8987 when bring up WiFi if txpower.bin file included. Hi, @yao_feng
Thanks for creating case to us.
Yes, I can also reproduced locally, and I am checking internally.
Once have any updates, I will let you know.
Best regards,
Christine. Re: FP92 p119.2 FW crash of 88W8997, 88W8987 when bring up WiFi if txpower.bin file included. Add logs. Customer board: i.mx8mp platform SW: BSP 5.15.129 WiFi version SD8997 ---- 16.92.21.p119.2-16.92.21.p119.2-MM6X16437.P3-GPL-(FP92) Module: Murata 1YM Attached logs. Logs.zip Re: FP92 p119.2 FW crash of 88W8997, 88W8987 when bring up WiFi if txpower.bin file included. Add more info. if set ps_mode=2 auto_ds=2 Got same result. Re: FP92 p119.2 FW crash of 88W8997, 88W8987 when bring up WiFi if txpower.bin file included. cont.
記事全体を表示