2035410_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2035410_en-US

2035410_en-US

CAN1 using in iMXRT1170 EVKB

Hello, 

I'm using the " iMXRT1176DVMAA" microcontroller - iMXRT1170 EVKB to implement the CAN Bus functionality.

I used CAN3 and it worked fine, there were two jumpers to remove  ( j102 & j103 )
and now I don't know if there are any jumpers or resistors to remove before using CAN1.

Any help ? 

Thank you.

Re: CAN1 using in iMXRT1170 EVKB

Hi @D_D97 ,

Thank you for your interest in the NXP MIMXRT product, I would  like to provide service for you.

I did a test, I connect MIMXRT1170-EVKB board CAN1(J83) and MIMXRT1050-EVKB board  CAN2(J11),  CAN communication works normally. So I think you can refer to what I do.

1.png2.png

For hardware modification, you need to mount   R2057 and R2058.

3.png

 

For software, you need set CAN1 pins.  You also need modify some code based on CAN1.

4.png

 

Wish it helps you.
If you still have question about it, please kindly let me know.

Wish you a nice day!

BR

MayLiu

Re: CAN1 using in iMXRT1170 EVKB

Hi @mayliu1 

I am using an  MIMXRT1170-EVKB board I have previously established CAN3 communication on the board using the Example codes available in the SDK.

Now I wanted to establish CAN1 communication on the same board and I came across your solution. Could you please share the photo for the hardware modification that you have mentioned as I am unable to locate the R2057 and R2058.. 

It would be great if you can share the example code as well. 

标记 (1)
无评分
版本历史
最后更新:
‎04-28-2026 03:12 AM
更新人: