MC9S12C64MFA Port T set up question MC9S12C64MFA, Code Warrior 5.9.0, coding in assembler. I am setting up Port T but I'm not sure I'm doing it right. Here is what I am trying to accomplish: PT0 is for PWM control of a solenoid valve. PT3 is a general purpose output. PT1,2 4,5,6,7 are all output compare channels. All are under port control with interrupt on compare match enabled. When I load the output compare value I will set the associated pin to the appropriate state. When the match occurs and the interrupt is triggered I will set the pin to the appropriate state in the ISR. Here is what I have so far: movb #$FF,DDRT ; All pins outputs movb #$01,MODRR ; PWM control on PT0, PT1,2,3 on Timer control movw #$0000,TCTL1 ; All pins under port control movb #$F6,TIOS ; Output Compare on PT1,2,4,5,6,7 movb #$01,PWME ; PWM control on PT0 Should this work? Regards, Robert Re: MC9S12C64MFA Port T set up question Game modes and events include team play, survival elimination, and seasonal tournaments planet clicker 3 online. Re: MC9S12C64MFA Port T set up question My goodness, I sure had that wrong! Thanks so much for the detailed explanation. As soon as I get my PCB finished I'll try that out. Regards, Robert Re: MC9S12C64MFA Port T set up question Hi,
I tried to do it without test. You can compare.
If the alternative function (another from GPIO) is enabled it takes precedence over all enable peripherals at pin with less priority. Priority starts from GPIO (the least) in the pin description table.
When you disconnect TIM from pin and you want to control them as output by SW in the interrupt(not by automatic OC function) then you have to set it as GPIO output mode.
// set ports PTT = ; // good to set initial value at the pins before // it is switched from input(default) to output DDRT = 0xFE; // pin 7,6,5,4, ,2,1 are driven by SW, pin 0 driven by PWM // pin 3 is also output in GPIO mode
//select pins connections MODRR = 0B00000001 // TIM,TIM,TIM,TIM, GPIO,TIM,TIM,PWM
// select TIM function TCTL1 = 0x00; // The TIM is disconnected from pins, value will be set manualy TIOS = 0xFE // TIM channels 7,6,5,4,3,2,1 in OC function
// Set PWM parameters, period, duty, polarity
....
// Set TIM parameters .. predcaler, period, OC value
....
// enable interrupt for TIM TIE = 0B11100110; // enable TIM interrupt for channel 7,6,5,4, 2,1
//enable interrupt globally asm CLI
// Run timer, set debug possibilities, set fast flag clear for TIM TSCR1 = 0xF0; // TEN-run timer; (TSWAI,TSFRZ)-good to set // to be able to debug; fast TIM flags clear,x,x,x,x
// Run PWM_0 PWME = 0x01; // run PWM0 at PT0
Best regards,
Ladislav
查看全文