Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
Please provide the AMMCLIB 1.1.44 S32DS plugin compatible with RTD 7.0.0 Hello, I encountered a version dependency issue when installing the AMMCLIB plugin in S32 Design Studio. I am collaborating with a colleague on the same project, and we are both using RTD version 7.0.0 and S32DS versions above 3.6. My colleague has installed AMMCLIB 1.1.44 and it is functioning normally; however, in my S32DS Extensions and Updates, I can only find AMMCLIB 1.1.46. When installing version 1.1.46, a prompt indicates that the following dependencies are missing: Missing required dependency: com.nxp.RTD.S32K3_S32M27X 7.0.1 could not be found. Missing requirement: com.nxp.AMMCLIB.S32K3xx.root.feature.feature.group 1.1.46.202609081018 requires com.nxp.RTD.S32K3_S32M27X.feature.feature.group [7.0.1,99.99.99) To maintain consistency in our team's development environment, we hope to continue using RTD 7.0.0 + AMMCLIB 1.1.44, integrating them through the RTD plugin method. Please assist in confirming: 1. Can you provide the download link, historical update site, or offline installation package for the S32DS plugin for AMMCLIB 1.1.44 for S32K3xx? 2. Which specific S32DS versions and updates are supported by this plugin? Is it compatible with RTD 7.0.0? 3. If the official download for the old version is no longer available, is there a supported method to obtain and install the plugin from a colleague's already installed 1.1.44 environment? What we need is the S32DS plugin/update site installation package, so as to use the S32 Configuration Tools to add the AMMCLIB component and generate code. The attachment is a screenshot of the error message indicating the installation failure. Thank you! Re: Please provide the AMMCLIB 1.1.44 S32DS plugin compatible with RTD 7.0.0 Hi @feixingren1  The AMMCLib package available through S32DS Extensions and Updates is RTD-dependent, as indicated by the package name. This means that it is designed to work with specific RTD versions and has software dependencies that must also be installed. In your case, the error message indicates that the package requires RTD 7.0.1, so the installation cannot be completed unless the required RTD version and its associated dependencies are present in your S32DS installation. Since you are specifically interested in AMMCLib v1.1.44, there is no need to install the version available through S32DS Extensions and Updates. Instead, you can download the standalone package for the desired version directly from Automotive Math and Motor Control Library Set for S32K3. Regarding integration, the User Manual for Automotive Math and Motor Control Library Set for NXP S32K3xx, MWCT2DxxS, and MWCT20xxS Devices includes a dedicated section that explains how to integrate the library into S32 Design Studio for S32 Platform as a standalone package. BR, VaneB
View full article
请提供 AMMCLIB 1.1.44S32DS插件与RTD 7.0.0兼容 您好,我在 S32 Design Studio 中安装 AMMCLIB 插件时遇到了版本依赖问题。 我正在与一位同事合作进行同一个项目,我们都在使用 RTD 版本 7.0.0 和 S32DS 版本 3.6 以上。我的同事安装了 AMMCLIB 1.1.44它运行正常;但是,在我的 S32DS 扩展和更新中,我只能找到 AMMCLIB 1.1.46。 安装 1.1.46 版本时,提示信息表明缺少以下依赖项: 缺少必需的依赖项: 找不到 com.nxp.RTD.S32K3_S32M27X 7.0.1。 缺少要求: com.nxp.AMMCLIB.S32K3xx.root.feature.feature.group 1.1.46.202609081018 需要 com.nxp.RTD.S32K3_S32M27X.feature.feature.group [7.0.1,99.99.99) 为了保持团队开发环境的一致性,我们希望继续使用 RTD 7.0.0 版本。+ AMMCLIB 1.1.44,通过RTD插件方法集成它们。 请协助确认: 1. 能否提供适用于 AMMCLIB 1.1.44 的 S32DS 插件的下载链接、历史更新站点或离线安装包?适用于 S32K3xx? 2. 此插件支持哪些具体的 S32DS 版本和更新?它与RTD 7.0.0兼容吗? 3.如果旧版本的官方下载已不再可用,是否有受支持的方法可以从同事已安装的 1.1.44 版本中获取并安装该插件?环境? 我们需要的是 S32DS 插件/更新站点软件包,以便使用 S32 配置工具添加 AMMCLIB 元器件并生成代码。 附件是显示安装失败的错误信息的屏幕截图。谢谢你! Re: Please provide the AMMCLIB 1.1.44 S32DS plugin compatible with RTD 7.0.0 你好@feixingren1 通过 S32DS 扩展和更新提供的 AMMCLib 软件包是 RTD 相关的,正如软件包名称所示。这意味着它设计用于特定的 RTD 版本,并且具有必须安装的软件依赖项。就您的情况而言,错误信息表明该软件包需要 RTD 7.0.1 版本。因此,除非您的 S32DS 安装中存在所需的 RTD 版本及其相关依赖项,否则无法完成安装。 既然您对 AMMCLib v1.1.44 特别感兴趣,无需安装通过 S32DS 扩展和更新提供的版本。或者,您可以直接从S32K3 汽车数学和电机控制库集下载所需版本的独立组网 (SA)软件包。 关于集成,NXP S32K3xx、MWCT2DxxS 和 MWCT20xxS 器件的汽车数学和电机控制库集用户手册包含一个专用的章节,解释了如何将该库作为独立软件包内置到 S32 平台的 S32 设计工作室中。 BR,VaneB
View full article
s32k396 基本セキュアブートに関する質問 32K396では、HSE FW 0.2.50.0 FULL_MEMが使用され、現在の有効期間はCUST_DELです。 テストプロセス:最初は、システムは正常に動作しました。次に、認証範囲内のアドレス 0x00453FF0 を 0xFF から 0xFE に変更し、AppBL ヘッダー、認証タグ、および IVT は変更しませんでした。IVT bootCfgWord を 0x00000009 に設定しました。電源をオフにしてから再度オンにした後、イメージをダウンロードせずに J-Link Attach 接続を使用し、空の SetupTarget を使用して接続中の RAM/ECC 初期化を無効にしました。この時点で、PC は 0x2040012E で停止しました。0x2040012C から 0x2040012E までの命令は WFI および WFI に戻る分岐であり、JTAG リカバリ待機ループと一致しています。現在、ユーザーのセキュアリカバリアプリケーションは構成されていません。 質問: BSB認証失敗後のこのバージョンの完全な処理プロセスと信頼できる基準を確認してください。JTAGリカバリ待機ループに入った後もGPR3ビット5が0のままなのはなぜですか?このビットは「SBAFブートアプリケーションカーネルがリカバリに入った」ことのみを示し、リカバリパスはHSE FWによってトリガーされることに関係していますか?また、どのステータスビットまたはエラーメッセージを使用して、失敗の原因がAppBL認証失敗であることを明確に確認する必要がありますか? Re: s32k396 Basic Secure Boot qeustion 詳細なテスト説明をありがとうございました。ここで重要なのは、ユーザーのSecure Recoveryアプリケーションが設定されていないということです。 あなたの設定でリカバリーフローがどのように機能するのか、詳しく教えていただけますか?特に: Secure Recoveryアプリケーションが設定されていない場合、AppBL認証失敗後にどのような復旧アクションが期待されますか? JTAGリカバリは明示的に設定され、有効化されていましたか? 観測されたWFIループ自体は予期せぬものとみなされるのか、それともGPR3[5]がクリアされたままであることだけが懸念事項なのか? J-Linkとの接続直後に読み取った、関連する復旧構成情報とHSE/SBAFステータス情報を提供してください。 ユーザーのSecure Recoveryアプリケーションが設定されていなければ、観察されるWFIループは予想されます。したがって、まずはAppBL認証失敗後の想定される回復フローとデバイスの動作を明確にしてください。 Re: s32k396 Basic Secure Boot qeustion gpr3のビット5が設定されていないことを確認しました。これはフラグビットであり、マニュアルにはリカバリモードでは1に設定されるべきと記載されています。なぜリカバリされなかったのでしょうか?詳細なテスト結果を添付します。
View full article
[S32K3] LVD割り込みについて こんにちは、 S32K3 MCUのLVD割り込み機能を使おうとしています。 MCUの設定でLVDIEEnable = trueに設定しています。 現在MCUには5Vが供給されていますが、Power_Ip_PMC_VoltageErrorIsr()は継続的にトリガーされています。 これは正常な動作なのか、それとも私が何か設定を間違えたのか教えていただきたいです。 Re: [S32K3] about LVD Interrupt こんにちは、 @danielmartynek 以下のピンに5Vの電圧が印加されています。 100ピンMCUの使用(FS32K312NHT0VPAST) VREFH: PIN 8 VDD_HV_A: ピン10 VDD_HV_A-2: ピン37 VDD_HV_A-3: ピン62 VDD_HV_A-4: ピン87 5Vが供給されているにもかかわらず、LVD5AFフラグレジスタが常にセットされたままになっている。 他に確認すべき箇所や記録簿はありますか? よろしくお願いいたします。 ショーン Re: [S32K3] about LVD Interrupt こんにちは、 @ssean さん。 LVD5AFをクリアした後も設定が維持される場合。 電圧は規定のしきい値よりも低くなければならない。 電圧を測定できますか? ありがとうございます ダニエル Re: [S32K3] about LVD Interrupt 部品番号を教えてもらえますか? あなたはどのRTD改訂版を使用していますか? ありがとうございました。 ダニエル Re: [S32K3] about LVD Interrupt こんにちは、 @danielmartynek さん。 現在、RTD 4.0.0を使用しています。HF04。 RTDコードにいくつかエラーがあることと、私の設定に問題があることを特定しました。 必要な調整を行った後、LVD電圧レベルで割り込みが正しくトリガーされることを確認しました。 再開まで今しばらくお待ちください。 よろしくお願いいたします。 ショーン・ソン
View full article
KEIL 与 LID2634 的兼容性 大家好, 我们正在采购LID2634板。 但是要刷写 NXP 固件,需要 KEIL MDK 5.36 许可证。(我是新手)。 经询问,KEIL 目前有 6 版本——但如果我想使用旧版本,我必须从他们那里购买专业许可证。 我的问题是: 1.是必须持有 KEIL 专业执照,还是必须持有 KEIL 5.36 证书?否则我应该选择基础版/社区版许可证吗? 2. 文件只提到了 KEIL 5.36 版本。购买前是否也应该确认一下编译器、调试器选项等兼容性问题? 3. 我看到大多数 CAS 示例都是用 Python 编写的——这是否意味着我只需要使用 KEIL 来烧录固件,而其余基于 Python 的逻辑都放在板载计算机中?如果我计划在NXP的MAC层之上进行开发。 4. 我还想知道是否有关于设置板、多标签和多锚点配置设置等的示例或 git 仓库可供参考,以便快速入门。 谢谢 Re: KEIL compatibility with LID2634 你好, 希望你一切都好。很抱歉给您带来不便,但由于该产品的信息受保密协议(NDA)约束,因此不对外公开。这不是分享该设备任何信息的安全渠道,出于同样的原因,我也没有相关数据。 因此,我建议您联系我们代理商网络|NXP中的一家代理商。或者,如果您有直接联系人曾帮助您了解该产品的信息或最初帮助您获得集成电路,请直接与他/她联系。 由此给您带来的不便,我深表歉意。 顺祝商祺! 里卡多
View full article
KW47:在调用 Gap_StartAdvertising 之前,是否必须等待 gAdvertisingStateChanged_c? 你好, 我正在 KW47 上实现广告控制。 要停止广告,我使用 Gap_StopAdvertising()。但是,有些情况下,在发出停止请求后,我希望在收到 gAdvertisingStateChanged_c 事件之前重新开始投放广告。 在这种情况下,当 Gap_StopAdvertising() 操作仍在进行时,调用 Gap_StartAdvertising() 是否安全? 具体来说,推荐使用以下哪种顺序? --- Gap_停止广告() ↓ 等待 gAdvertisingStateChanged_c ↓ Gap_StartAdvertising() ---- 或 --- Gap_停止广告() ↓ Gap_StartAdvertising() --- SDK 是否在内部处理状态转换,还是必须等待指示广告已停止的 gAdvertisingStateChanged_c 事件,然后才能调用 Gap_StartAdvertising()? 感谢您的支持。 顺祝商祺! 协议:蓝牙 Re: KW47: Is it necessary to wait for gAdvertisingStateChanged_c before calling Gap_StartAdvertising 你好@hyama , 能否提供更多关于您希望在收到 gAdvertisingStateChanged_c 事件之前重新启动广告的场景的背景信息? 建议的做法是等待 gAdvertisingStateChanged_c 事件,以验证广告状态转换是否已成功完成。Gap_StopAdvertising() 启动该过程,回调函数确认操作结果。例如,应用程序可能不会收到 gAdvertisingStateChanged_c 事件,而是收到 gAdvertisingCommandFailed_c 事件,这表明请求的操作无法完成。 BR 哈比卜 Re: KW47: Is it necessary to wait for gAdvertisingStateChanged_c before calling Gap_StartAdvertising 谢谢你的解释。 我们提出这个问题是因为我们预期 SDK 可能会在内部按顺序处理停止和启动请求,即使在收到 gAdvertisingStateChanged_c 事件之前调用了 Gap_StartAdvertising()。 由于等待 gAdvertisingStateChanged_c 事件是推荐的做法,我们将相应地修改我们的实现。 感谢您的支持。
View full article
s32k396 Basic Secure Boot qeustion On a 32K396, HSE FW 0.2.50.0 FULL_MEM is used, and the current lifetime is CUST_DEL. Testing Process: Initially, the system ran normally. Then, the address 0x00453FF0 within the authentication range was changed from 0xFF to 0xFE, while keeping the AppBL Header, authentication tag, and IVT unchanged. The IVT bootCfgWord was set to 0x00000009. After powering off and on again, a J-Link Attach connection was used, without downloading the image, and RAM/ECC initialization during connection was disabled using an empty SetupTarget. At this point, the PC stopped at 0x2040012E. The instructions from 0x2040012C to 0x2040012E are WFI and branches that jump back to WFI, consistent with the JTAG Recovery wait loop. Currently, no user Secure Recovery application is configured. Question: Please confirm the complete handling process and reliable criteria for this version after BSB authentication failure: Why is GPR3 bit5 still 0 even after entering the JTAG Recovery waiting loop? Is it related to the fact that this bit only indicates "SBAF boot application kernel into Recovery" and the current recovery path is triggered by HSE FW? And which status bit or error message should be used to clearly confirm that the failure is due to AppBL authentication failure? Re: s32k396 Basic Secure Boot qeustion Thank you for the detailed test description. The statement that no user Secure Recovery application is configured may be important here. Could you please clarify how the recovery flow is intended to work in your configuration? In particular: What recovery action is expected after the AppBL authentication failure if no Secure Recovery application is configured? Was JTAG Recovery explicitly configured and enabled? Is the observed WFI loop itself considered unexpected, or is the concern only that GPR3[5] remains cleared? Please provide the relevant recovery configuration and the HSE/SBAF status information read immediately after connecting with J-Link. The observed WFI loop may be expected if no user Secure Recovery application is configured. Therefore, please first clarify the intended recovery flow and the expected device behavior after the AppBL authentication failure. Re: s32k396 Basic Secure Boot qeustion We observed that bit 5 of gpr3 was not set. This is a flag bit, and the manual states that it should be set to 1 in recovery mode. Why didn't it recover? Detailed tests are attached.
View full article
S32R41: How to Enable and Verify Cortex-M7 Lockstep Functionality Hello NXP Team, I am working with the NXP S32R41 automotive radar SoC and using Lauterbach TRACE32 for debugging. I would like to understand how to enable and verify the hardware lockstep functionality of the Cortex-M7 cores on the S32R41. Could you please help clarify the following questions? How to enable Lockstep: Is the Cortex-M7 lockstep mode enabled by default on the S32R41, or does it need to be configured? If configuration is required, what are the exact steps to enable it? Is it controlled by hardware configuration, DCF records, startup software, or specific registers? Configuration registers: Which S32R41-specific registers and bit fields indicate whether Lockstep is enabled? Please provide the register names, addresses, bit positions, and expected values. How to verify Lockstep: How can I confirm that the Cortex-M7 cores are actually operating in hardware lockstep mode rather than independent mode? Is checking the configuration register sufficient, or are additional status registers required? Lockstep error detection: Which registers indicate the status of the lockstep comparator? How can I determine whether the comparator is functioning correctly and whether any lockstep mismatch has been detected? TRACE32 debugging: Is there a recommended TRACE32 command sequence or debugging procedure to inspect the lockstep configuration and status? Documentation: Could you point me to the relevant sections of the S32R41 Reference Manual, Safety Manual, or other official documentation describing the lockstep configuration and verification procedure? I want to ensure that the lockstep functionality is correctly enabled and that its operation can be verified using documented, S32R41-specific methods. Please note that I am specifically asking about the S32R41, not the S32K3 family, so I would appreciate register definitions and procedures applicable to the S32R41. Thank you for your support. Best regards Re: S32R41: How to Enable and Verify Cortex-M7 Lockstep Functionality Hello, On the S32R41, the Cortex‑M7 processors are implemented as hardware lockstep core pairs. Lockstep operation is part of the S32R41 hardware configuration and is not enabled by application software, startup code, or an S32K3-style UTEST_MISC[LOCKSTEP_EN] DCF record. The NXP S32R41 product information explicitly describes the Cortex‑M7 implementation as having a lockstep core configuration. 1. No software enable sequence is required 2. The configuration should not be verified using S32K3 registers 3. Debugger visibility provides a practical architectural indication TRACE32 connects to the logical Cortex‑M7 processor. It does not present the redundant checker core as an additional independently debuggable Cortex‑M7. Therefore, only the functional member of each lockstep pair is expected to appear as a debug target. 4. Lockstep mismatch reporting A mismatch detected by the Cortex‑M7 lockstep comparison logic is reported through the S32R41 safety fault-management path. The application must configure the corresponding FCCU fault and its required reaction in accordance with the S32R41 Safety Manual. 5. No special TRACE32 command is required to enable lockstep. 6. Please refer to the following S32R41-specific documents: S32R41 Reference Manual, particularly the Cortex‑M7, FCCU and reset/fault-management chapters; S32R41 Safety Manual, particularly the safety mechanisms covering Cortex‑M7 lockstep execution, lockstep comparison and FCCU fault handling; the device-specific FCCU fault mapping associated with the applicable S32R41 revision; the TRACE32 S32R41 startup scripts supplied with the supported S32R41 software/debug package. Best regards, Peter
View full article
Can_43_LLCE 1.0.9 (S32G):是否支持或计划支持构建后可加载配置? 你好, 我们正在跟进“CAN_LLCE 和 LLCE_Af 是否支持 Postbuild Loadable?”这个问题。(2025年4月)NXP 支持人员回答了 Can_43_LLCE 的“Postbuild 模型”。可加载的问题仍未解决。CAN_LLCE 和 LLCE_Af 是否支持 Postbuild Loadable? - NXP 社区 设置:S32G274A,S32G_LLCE_1_0_9(Can_43_LLCE 1.0.9,RTD AUTOSAR 4.4)。 目标:更新 CAN 配置,使其可在版本后加载,而无需重新刷写整个应用程序映像。 在 1.0.9 版本软件包中,我们看到: 构建后表是带有绝对指针的常量结构,会被编译到应用程序映像中。 我们没有找到任何可加载或可重定位的格式、S 记录输出或构建后数据的加载器。 问题: Can_43_LLCE 是否支持/计划支持版本后可加载配置?如果是,是哪个版本?何时发布的? 如果不行,那么在不完全重新刷写固件的情况下,更新 CAN 滤波器的官方方法是什么? 是否有关于使用 Can_43_LLCE 和 Llce_Af 进行构建后处理的应用笔记? 提前致谢, 艾曼 Re: Can_43_LLCE 1.0.9 (S32G): is post-build loadable configuration supported or planned? 你好, AymanYounis 感谢您与我们联系并提供信息。 我已经收到您的问题,我会帮您核实。 BR 乔伊 Re: Can_43_LLCE 1.0.9 (S32G): is post-build loadable configuration supported or planned? 你好, AymanYounis 感谢您与我们联系。 根据最新的 LLCE 手册,目前 CAN_LLCE 和 LLCE_Af 不支持 Postbuild Loadable。目前还没有添加此功能的明确计划。 根据内部建议,如果客户想要提出新的变更请求,则需要咨询市场部。需要提供更多业务信息。 我们目前没有相关文件可供参考,引用。给您带来的不便,敬请谅解。 BR 乔伊
View full article
S32R41:如何启用和验证 Cortex-M7 锁步功能 您好,NXP团队, 我正在使用 NXP S32R41 汽车雷达 SoC,并使用 Lauterbach TRACE32 进行调试。 我想了解如何在 S32R41 上启用和验证 Cortex-M7 内核的硬件锁步功能。 请问您能否帮忙解答以下问题? 如何启用锁步模式: S32R41 是否默认启用 Cortex-M7 锁步模式,还是需要手动配置?如果需要配置,具体步骤是什么?它是通过硬件配置、DCF 记录、启动软件还是特定寄存器来控制的? 配置寄存器:哪些S32R41特有的寄存器和位域指示是否启用了锁步功能?请提供寄存器名称、地址、位位置和预期值。 如何验证硬件锁步模式:如何确认 Cortex-M7 内核确实运行在硬件锁步模式而不是独立模式下?检查配置寄存器是否足够,还是需要额外的状态寄存器? 锁步错误检测:哪些寄存器指示锁步比较器的状态?如何确定比较器是否正常工作以及是否检测到任何锁步不匹配? TRACE32 调试:是否有推荐的 TRACE32 命令序列或调试程序来检查锁步配置和状态? 文档:能否指出 S32R41 参考手册、功能安全手册或其他官方文档中描述锁定步骤配置和验证程序的相关章节? 我希望确保锁定步进功能已正确启用,并且可以使用已记录的、S32R41 特定方法验证其运行情况。 请注意,我特指S32R41 ,而不是 S32K3 系列,因此我希望得到适用于 S32R41 的寄存器定义和程序。 感谢您的支持。 顺祝商祺! Re: S32R41: How to Enable and Verify Cortex-M7 Lockstep Functionality 你好, 在 S32R41 上,Cortex-M7 处理器以硬件锁步内核对的形式实现。锁步操作是 S32R41 硬件配置的一部分,并非通过应用程序软件、启动代码或 S32K3 风格的 UTEST_MISC[LOCKSTEP_EN] DCF 记录启用。NXP S32R41 产品信息明确描述了 Cortex-M7 实现采用锁步内核配置。 1.无需软件启用序列 2. 不应使用 S32K3 寄存器验证配置。 3. 调试器可见性提供了实际的架构指示 TRACE32 连接到逻辑 Cortex-M7 处理器。它没有将冗余的检查器核心作为额外的、可独立调试的 Cortex-M7 呈现出来。因此,只有每个锁步对的功能成员才会作为调试目标出现。 4. 锁步不匹配报告 Cortex-M7 锁步比较逻辑检测到的不匹配将通过 S32R41 功能安全故障管理路径报告。应用程序必须按照 S32R41 功能安全手册配置相应的 FCCU 故障及其所需的响应。 5. 无需特殊的 TRACE32 命令即可启用锁步。 6. 请参阅以下与 S32R41 相关的文档: S32R41 参考手册,特别是 Cortex-M7、FCCU 和复位/故障管理章节; S32R41 功能安全手册,特别是涵盖 Cortex-M7 锁步执行、锁步比较和 FCCU 故障处理的安全机制; 与适用的 S32R41 版本相关的设备特定 FCCU 故障映射; TRACE32 S32R41 启动脚本随受支持的 S32R41 软件/调试软件包一起提供。 顺祝商祺! Peter
View full article
Can_43_LLCE 1.0.9 (S32G): is post-build loadable configuration supported or planned? Hello, We are following up on "Do CAN_LLCE and LLCE_Af support Postbuild Loadable?" (April 2025). NXP support answered "Postbuild model" for Can_43_LLCE. The loadable question was left open. Do CAN_LLCE and LLCE_Af support Postbuild Loadable? - NXP Community Setup: S32G274A, S32G_LLCE_1_0_9 (Can_43_LLCE 1.0.9, RTD AUTOSAR 4.4). Goal: update CAN config as post-build loadable without reflashing the full application image. In the 1.0.9 package, we see: Post-build tables are const structures with absolute pointers, compiled into the application image. We found no loadable or relocatable format, S-record output, or loader for post-build data. Questions: Is post-build loadable configuration supported/planned for Can_43_LLCE? If yes, which version and when? If not, what is the supported way to update CAN filters without a full reflash? Is there an application note for post-build with Can_43_LLCE and Llce_Af? Thanks in advance, Ayman Re: Can_43_LLCE 1.0.9 (S32G): is post-build loadable configuration supported or planned? Hi,AymanYounis Thank you for contacting us and your information. I have received your question and will help you to check it. BR Joey Re: Can_43_LLCE 1.0.9 (S32G): is post-build loadable configuration supported or planned? Hi,AymanYounis Thank you for contacting us. According to the latest LLCE manual, currently CAN_LLCE and LLCE_Af do not support Postbuild Loadable. There are no definite plans to add this feature. According to internal suggestions, if a customer wants to propose a new change request, this requires consulting the marketing. More business information needs to be provided. We currently do not have relevant documents for reference. Apologize for the inconvenience caused. BR Joey
View full article
KW47: Gap_StartAdvertisingを呼び出す前に、gAdvertisingStateChanged_cを待つ必要がありますか? こんにちは、 KW47に広告制御機能を実装しています。 広告表示を停止するには、Gap_StopAdvertising() を使用します。しかし、停止リクエストを出した後にgAdvertisingStateChanged_cイベントを受け取る前に再び広告を始めたい場合もあります。 この状況において、Gap_StopAdvertising() 操作がまだ進行中である間に Gap_StartAdvertising() を呼び出すのは安全でしょうか? 具体的に、以下のどの手順が推奨されますか? --- Gap_StopAdvertising() ↓ gAdvertisingStateChanged_c を待機します ↓ Gap_StartAdvertising() ---- または --- Gap_StopAdvertising() ↓ Gap_StartAdvertising() --- SDKsは内部で状態遷移を処理しているのか、それとも広告が停止したことを示すgAdvertisingStateChanged_cイベント情報を待ってからGap_StartAdvertising()を呼び出す必要があるのか? 再開まで今しばらくお待ちください。 よろしくお願いいたします。 プロトコル:Bluetooth Re: KW47: Is it necessary to wait for gAdvertisingStateChanged_c before calling Gap_StartAdvertising こんにちは、 @hyama さん。 gAdvertisingStateChanged_cイベントを受け取る前に広告を再開したい場合の状況について、もう少し詳しく教えていただけますか? 推奨される方法は、広告状態の移行が成功裏に完了したことを確認するためにgAdvertisingStateChanged_cイベントを待つことです。Gap_StopAdvertising() は処理を開始し、コールバックは処理結果を確認します。例えば、gAdvertisingStateChanged_cイベントを受け取る代わりに、アプリケーションはリクエストされた操作が完了できないことを示すgAdvertisingCommandFailed_cイベントを受け取ることがあります。 BR ハビブ Re: KW47: Is it necessary to wait for gAdvertisingStateChanged_c before calling Gap_StartAdvertising ご説明いただきありがとうございます。 この質問をしたのは、たとえGap_StartAdvertising()がgAdvertisingStateChanged_cイベント情報を受け取る前に呼び出されていても、SDKsが内部で停止・開始リクエストを順番に処理する可能性があると予想していたからです。 gAdvertisingStateChanged_cイベントを待つことが推奨されているため、それに応じて実装を修正します。 再開まで今しばらくお待ちください。
View full article
Recommended BSP / Neutron SDK versioning strategy Hello, We are developing a PoC for an automotive application using the i.MX95 as our platform and would like to clarify the recommended Neutron SDK versioning strategy. We have read the "Neutron SDK Version Compatibility with Yocto BSP" table in NeutronSDKUserGuide.md and understand that the compiler and runtime must come from the same SDK. However, the guide does not say which version is recommended. Should we always use the latest Neutron SDK version (with the runtime upgraded) on our current BSP, or should we use the SDK version that is Default for that BSP? Environment - Board: IMX95LPD5EVK-19 - BSP: LF_6.18.20_2.0.0 - Neutron SDK: eiq-neutron-sdk-linux-3.2.3 - NeutronFirmware.elf, libNeutronDriver.so, and libneutron_delegate.so have been updated to the versions from Neutron SDK 3.2.3. Thank you! Re: Recommended BSP / Neutron SDK versioning strategy Hi, Thank you for your interest in NXP Semiconductor products, You can find what Neutron SDK version is included with every BSP at the end of Machine Learning User's Guide, e.g. Neutron SDK v3.2.1 is included in LF6.18.37_2.1.0 However, for development, customers are encouraged to use latest SDK revision, and documentation advises copying the binaries (used for conversion) to target: - Updating the Neutron Runtime - To update the neutron runtime on a target device, upload the files to the ir designated directories, as follows: | File | Target Directory | |------|------------------| | `NeutronFirmware.elf` | `/lib/firmware/` | | `libNeutronDriver.so` | `/lib/` | | `libneutron_delegate.so` | `/lib/` | Regards Re: Recommended BSP / Neutron SDK versioning strategy Hi Joseph, Thank you for your reply. We will use the latest SDK revision as recommended. Regards
View full article
Guidance Required for Enabling HSE/Crypto Support on S32K312 Non-AUTOSAR Project Hi Team, We are using S32 Design Studio 3.6.10 for the development of a Non-AUTOSAR application on the NXP S32K312 Mini Board. The project is currently based on FreeRTOS, using SW32K3_FreeRTOS_11.1.0_0.8.0_CD1_D2603_DesignStudio_updatesite.zip, which in turn uses SW32K3_S32M27x_RTD_R23-11_7.0.1_D2603_DesignStudio_updatesite.zip as the RTD version. We have successfully implemented the following UDS services: Service 0x10 – Diagnostic Session Control Service 0x22 – Read Data By Identifier Service 0x27 – Security Access Service 0x3E – Tester Present As part of the next development phase, we plan to implement UDS Service 0x29 (Authentication) and would like to leverage HSE/Crypto support for the implementation. To enable this, we installed: SW32K3_RTD_R23-11_7.0.1_P02_D2603_DesignStudio_updatesite.zip The installation completed successfully, and we can see Crypto-related folders (e.g., Crypto_43_HSE, CryIf, Csm, etc.) under the RTD installation directory. However, we are unable to find any HSE/Crypto components in: S32 Configuration Tools (.mex) Peripherals/Drivers view Sample Applications/Examples To verify the setup, we also created a new S32K312 sample project. However, the HSE/Crypto components are still not available for selection. Could you please help clarify the following: How can HSE/Crypto support be enabled for an S32K312 project in S32 Design Studio? Are any additional packages, plugins, SDKs, or HSE firmware required? Is there a specific RTD version or project configuration recommended for using HSE/Crypto together with FreeRTOS on the S32K312? Are the Crypto_43_HSE modules provided by the package intended only for AUTOSAR/EB Tresos-based projects, or can they also be used in Non-AUTOSAR S32 Design Studio projects? Are there any example projects or reference documents available for integrating HSE/Crypto in a Non-AUTOSAR S32K312 application? Any guidance or reference documentation related to HSE/Crypto integration would be greatly appreciated. Thanks & Regards, Pramod Jadhav Re: Guidance Required for Enabling HSE/Crypto Support on S32K312 Non-AUTOSAR Project Hi @pramodj2  In the thread S32DS 3.6.7 RTD 7.0.1 P02 HSE code generation error, I shared a step-by-step guide describing how I installed S32K3 Real-Time Drivers ASR R23-11 Version 7.0.1 P02. You may find it helpful to compare those steps with your current installation process. Also, when working with HSE, it is necessary to include the HSE Interface files in your project. These files can be obtained from the HSE Firmware package, specifically from the interface folder (C:\NXP\HSE_FW_S32K344_0_2_55_0\hse_full_mem\interface). Finally, although there are no RTD examples specifically developed for the S32K312, the examples available for other S32K3 devices can be used as a good reference, as the implementation is very similar across the family. You may also find the examples included in the HSE Demo App and the S32K3 MCUs for General Purpose HSE Demo Examples helpful. While these examples do not directly use the Crypto/Hse_Ip drivers, they demonstrate how to work with HSE services. BR, VaneB Re: Guidance Required for Enabling HSE/Crypto Support on S32K312 Non-AUTOSAR Project Hi @pramodj2  The HSE-B Reference Manual, training presentations, and application notes are under NDA and are therefore not publicly available. Access to these materials is provided only through Secure Files. If you do not currently have access to Secure Files, you can request it by following the procedure described in the NXP Secure Access Rights First-Time User Registration Guide. Additionally, the HSE Service API Reference Manual, which contains detailed information on how to install, configure, and use HSE, is included in the SE Interface files. It can be found, for example, at the following location: C:\NXP\HSE_FW_S32K344_0_2_55_0\docs If you plan to use the Hse_Ip/Crypto drivers, we also recommend referring to the Driver User Manual and Integration Manual. These documents provide detailed information about hardware and software requirements, supported configurations, usage guidelines, integration steps, and known limitations. These documents can be found, for example, at: C:\NXP\S32DS.3.6.5\S32DS\software\PlatformSDK_S32K3\RTD_CRYPTO\Crypto_43_HSE_TS_T40D34M70I1R0\doc Re: Guidance Required for Enabling HSE/Crypto Support on S32K312 Non-AUTOSAR Project Thank you for the quick support. I was able to successfully add the HSE driver by following the steps provided in the shared link. Could you please share any reference user manuals, application notes, or documentation that we can use to configure the HSE in the application and validate its functionality on the target board? Thank you for your assistance.
View full article
为在 S32K312 非 AUTOSAR 项目中启用 HSE/加密支持所需指南 大家好, 我们使用的是S32 设计工作室 3.6.10 版本。用于在NXP S32K312 Mini 板上开发非 AUTOSAR 应用程序。该项目目前基于FreeRTOS ,使用SW32K3_FreeRTOS_11.1.0_0.8.0_CD1_D2603_DesignStudio_updatesite.zip ,而SW32K3_S32M27x_RTD_R23-11_7.0.1_D2603_DesignStudio_updatesite.zip作为 RTD 版本。 我们已成功实施以下UDS服务: 服务 0x10 – 诊断会话控制 服务 0x22 – 通过标识符读取数据 服务 0x27 – 网络安全访问 服务 0x3E – 测试人员已就绪 作为下一开发阶段的一部分,我们计划实现UDS 服务 0x29(身份验证) ,并希望利用HSE/Crypto支持来实现该服务。 为了实现这一点,我们安装了: SW32K3_RTD_R23-11_7.0.1_P02_D2603_DesignStudio_updatesite.zip 安装已成功完成,我们可以在 RTD 安装目录下看到与加密相关的文件夹(例如Crypto_43_HSE 、 CryIf 、 Csm等)。但是,我们无法在以下位置找到任何HSE/Crypto 元器件: S32 配置工具(.mex) 外设/驱动程序视图 应用示例/范例 为了验证设置,我们还创建了一个新的 S32K312 示例项目。然而,HSE/Crypto 元器件目前仍无法选择。 请问您能否帮忙澄清以下问题: 如何在 S32 Design Studio 中为 S32K312 项目启用 HSE/加密支持? 是否需要其他软件包、插件、SDK 或 HSE 固件? 在 S32K312 上使用 HSE/Crypto 和 FreeRTOS 时,是否有推荐的特定 RTD 版本或项目配置? 该软件包提供的Crypto_43_HSE模块是否仅用于基于 AUTOSAR/EB Tresos 的项目,还是也可以用于非 AUTOSAR S32 Design Studio 项目? 是否有任何示例项目或参考文档可用于将 HSE/Crypto 集成到非 AUTOSAR S32K312 应用程序中? 任何与 HSE/Crypto 集成相关的指导或参考资料都将不胜感激。 谢谢,此致敬礼! 普拉莫德·贾达夫 Re: Guidance Required for Enabling HSE/Crypto Support on S32K312 Non-AUTOSAR Project 嗨@pramodj2 在S32DS 3.6.7 RTD 7.0.1 P02 HSE 代码生成错误主题中,我分享了一个分步指南,描述了我是如何安装 S32K3 实时驱动程序 ASR R23-11 版本 7.0.1 P02 的。您可以将这些步骤与您当前的安装过程进行比较,这可能会对您有所帮助。 另外,在使用 HSE 时,必须将 HSE 接口文件包含在您的项目中。这些文件可以从 HSE 固件代码包,软件包中获取,具体来说,可以从接口文件夹(C:\NXP\HSE_FW_S32K344_0_2_55_0\hse_full_mem\interface)中获取。 最后,虽然没有专门为 S32K312 开发的 RTD 示例,但其他 S32K3 设备的示例可以作为很好的参考,引用,因为该系列器件的实现方式非常相似。 您可能还会发现 HSE Demo App 中包含的示例和S32K3 MCU 通用 HSE Demo 示例很有帮助。虽然这些示例没有直接使用 Crypto/Hse_Ip 驱动程序,但它们演示了如何使用 HSE 服务。 BR,VaneB Re: Guidance Required for Enabling HSE/Crypto Support on S32K312 Non-AUTOSAR Project 嗨@pramodj2 HSE-B 参考手册、培训演示文稿和应用笔记均受保密协议约束,因此不对外公开。只有通过安全文件才能访问这些资料。 如果您目前没有访问安全文件的权限,您可以按照NXP 安全访问权限首次用户注册指南中描述的步骤提出申请。 此外,SE 接口文件中还包含 HSE 服务 API 参考手册,其中包含有关如何安装、配置和使用 HSE 的详细信息。例如,可以在以下地点找到它: C:\NXP\HSE_FW_S32K344_0_2_55_0\docs 如果您计划使用 Hse_Ip/Crypto 驱动程序,我们也建议您参考驱动程序用户手册和集成手册。这些文档提供了有关硬件和软件要求、支持的配置、使用指南、集成步骤和已知限制的详细信息。例如,您可以在以下位置找到这些文件: C:\NXP\S32DS.3.6.5\S32DS\software\PlatformSDK_S32K3\RTD_CRYPTO\Crypto_43_HSE_TS_T40D34M70I1R0\doc Re: Guidance Required for Enabling HSE/Crypto Support on S32K312 Non-AUTOSAR Project 感谢您的快速支持。我按照分享链接中提供的步骤,成功添加了 HSE 驱动程序。 能否提供一些参考用户手册、应用笔记或文档,以便我们在应用程序中配置 HSE 并验证其在目标板上的功能? 谢谢你的帮助。
View full article
PF09 文档 我正在寻找演示板 KITPF09FRDMEVB 的电路原理图。 我下载了 KITPF09FRDMEVB-DESIGN-FILES,但是 .DSN 文件已损坏。 请问您能否告诉我哪里可以找到电路图文件(PDF格式也行)? 先行致谢。 Re: PF09 documentation 谢谢! Re: PF09 documentation 你好, 请尝试使用 Allegro Capture CIS 打开 DSN 文件。我打开它没有任何问题。 如果您无法使用 捕获 CIS,请提交支持工单以获取进一步帮助。很遗憾,我无法通过这个渠道分享设计文件。 同时,请查阅附件中的PDF文件。
View full article
PF09 documentation Im looking for the electric schematics of the demo board KITPF09FRDMEVB. I downloaded KITPF09FRDMEVB-DESIGN-FILES but the .DSN file is corrupted. Please could tou tell me where can i find the electric schmatics files (also in PDF) Thanks in advance. Re: PF09 documentation THank you. Re: PF09 documentation Hello, Please try opening the DSN file using Allegro Capture CIS. I was able to open it without any issues. If you are unable to use Capture CIS, please open a support ticket for further assistance. Unfortunately, I cannot share the design files through this channel. In the meantime, please find the PDF file attached for your reference.
View full article
PF09のドキュメント デモボードKITPF09FRDMEVBの電気回路図を探しています。 KITPF09FRDMEVB-DESIGN-FILESをダウンロードしましたが、DSNファイルが破損しています。 エレクトリック・シュマティクスのファイル(PDFも含む)がどこで見つかるか教えていただけませんか? よろしくお願いいたします。 Re: PF09 documentation よろしくお願いします。 Re: PF09 documentation こんにちは、 Allegro Capture CISを使用してDSNファイルを開いてみてください。問題なく開けることができました。 Capture CISをご利用できない場合は、 サポートチケット を開設してさらなるサポートを依頼してください。残念ながら、このチャネルを通じてデザインファイルを共有することはできません。 参考資料として、添付のPDFファイルをご確認ください。
View full article
CLRD730と701の互換性 こんにちは、 私たちのお客様には多くのCLRD 701が導入されています。彼らはもっと買いたいと思っている。コードを変更せずに730でアプリケーションを動かす可能性はどんなものでしょうか? どうもありがとうございました。よろしくお願いいたします。 Re: CLRD730 compatibility with 701 こんにちは、@fox13 さん。 お元気でお過ごしでしょうか。 NXP製品を引き続きご利用いただきありがとうございます。 ご質問についてですが、CLRD730をアプリケーションに組み合わせることは可能なはずです。 Pegoda CLRD730デスクトップリーダーは、デフォルトのWindows CCIDドライバーで動作するよう設計されていることをご考慮ください。また 、 CLRD730データシート のセクション6.8「 PC/SCモード」 のご確認もお勧めします 統合に関する関連情報をカバーしています。 敬具 ジェイミー。
View full article
非AUTOSARプロジェクトでHSE/暗号資産サポートを有効にするためのガイダンスS32K312必要 チームの皆さん、こんにちは。 私たちはS32 Design Studio 3.6.10を使っていますNXP S32K312 Mini Board上で非AUTOSARアプリケーションの開発のために。このプロジェクトは現在、 FreeRTOSをベースとしており、 SW32K3_FreeRTOS_11.1.0_0.8.0_CD1_D2603_DesignStudio_updatesite.zipを使用しています。この FreeRTOS は、RTD バージョンとしてSW32K3_S32M27x_RTD_R23-11_7.0.1_D2603_DesignStudio_updatesite.zipを使用しています。 以下のUDSサービスを正常に実装しました。 サービス0x10 – 診断セッション制御 サービス0x22 – 識別子によるデータ読み取り サービス0x27 – セキュリティアクセス サービス0x3E – テスター存在 次の開発段階では、 UDSサービス0x29(認証) を実装する予定で、 HSE/暗号 サポートを活用して実装したいと考えています。 これを実現するために、以下をインストールしました。 SW32K3_RTD_R23-11_7.0.1_P02_D2603_DesignStudio_updatesite.zip インストールは無事完了し、RTDのインストールディレクトリの下にはCrypto関連のフォルダ(例: Crypto_43_HSE、 CryIf、 CSMなど)が確認できます。しかし、以下の場所にはHSE/Cryptoコンポーネントが見つかりません。 S32設定ツール(.mexファイル) ペリフェラル/ドライバビュー アプリケーション・例 設定を確認するため、S32K312用の新しいサンプルプロジェクトも作成しました。しかし、HSE/Cryptoコンポーネントはまだ選択できません。 以下の点を教えていただけますか? S32 Design StudioでS32K312プロジェクトに対してHSE/Cryptoのサポートを有効にするにはどうすればよいですか? 追加のパッケージ、プラグイン、SDKs、HSEファームウェアは必要ですか? S32K312上でFreeRTOSとHSE/Cryptoを併用する場合、推奨される特定のRTDバージョンやプロジェクト構成はありますか? パッケージに含まれる Crypto_43_HSE モジュールはAUTOSAR/EB Tresosベースのプロジェクト専用ですか?それともAUTOSAR以外のS32 Design Studioプロジェクトでも使用可能ですか? 非AUTOSAR S32K312アプリケーションでHSE/暗号資産を統合するための例となるプロジェクトや参考文献はありますか? HSE/暗号資産統合に関する指針や参考ドキュメントがあれば、ぜひ教えていただけると助かります。 よろしくお願いいたします。 プラモド・ジャダブ Re: Guidance Required for Enabling HSE/Crypto Support on S32K312 Non-AUTOSAR Project こんにちは、@pramodj2さん In the ThreadS32DS 3.6.7 RTD 7.0.1 P02 HSEコード生成エラー」では、S32K3 リアルタイム・ドライバ ASR R23-11 バージョン7.0.1 P02のインストール方法を説明するステップバイステップガイドを共有しました。これらの手順を現在のインストール手順と比較してみると、参考になるかもしれません。 また、HSEを扱う際には、プロジェクトにHSEインターフェースファイルを含める必要があります。これらのファイルはHSEファームウェアパッケージから入手可能で、特にインターフェースフォルダ(C:\NXP\HSE_FW_S32K344_0_2_55_0\hse_full_mem\interface)から入手可能です。 最後に、S32K312向けに特別に開発されたRTDの例はありませんが、他のS32K3デバイスの例はファミリ全体で非常に似た実装であるため、良い参考資料として利用できます。 HSEデモアプリに含まれているサンプルや、汎用HSEデモサンプル用のS32K3 MCUのサンプルも参考になるかもしれません。これらの例はCrypto/Hse_Ipドライバを直接使用していませんが、HSEサービスの扱い方を示しています。 BR、VaneB Re: Guidance Required for Enabling HSE/Crypto Support on S32K312 Non-AUTOSAR Project こんにちは、@pramodj2さん HSE-Bリファレンス・マニュアル、トレーニング発表、アプリケーションノートはNDAに属するため、公開されていません。これらの資料へのアクセスはSecure Filesを通じてのみ提供されます。 現在Secure Filesにアクセスできない場合は、 NXPのSecure アクセス Rights First Time ユーザー Registration Guideに記載された手順に従って申請できます。 さらに、HSEサービスのAPIリファレンス・マニュアルには、HSEのインストール、設定、使用方法に関する詳細な情報がSEインターフェースファイルに含まれています。例えば、以下の場所で見つけることができます。 C:\NXP\HSE_FW_S32K344_0_2_55_0\docs Hse_Ip/Cryptoドライバーを使用する予定がある場合は、ドライバーユーザーマニュアルおよび統合マニュアルも参照することをお勧めします。これらの文書は、ハードウェアおよびソフトウェアの要件、対応構成、使用ガイドライン、統合ステップ、既知の制限事項に関する詳細な情報を提供します。これらの文書は、例えば以下で見つけることができます: C:\NXP\S32DS.3.6.5\S32DS\software\PlatformSDK_S32K3\RTD_CRYPTO\Crypto_43_HSE_TS_T40D34M70I1R0\doc Re: Guidance Required for Enabling HSE/Crypto Support on S32K312 Non-AUTOSAR Project 迅速なサポートありがとうございます。共有リンクの手順に従ってHSEドライバを無事に追加できました。 HSEをアプリケーション内で設定し、ターゲットボード上でその機能を検証するための参考ユーザーマニュアル、アプリケーションノート、ドキュメントなどを教えていただけますか? ご協力ありがとうございました。
View full article