Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
Title: RW612 Flash Programming Verification Failed at 0x08400000 on Murata Type 2FR EVK Hello NXP Community, I am using the Murata Type 2FR (LBES0ZZ2FR-EVK) based on the NXP RW612 MCU and need help resolving a flash programming issue. Initially, I followed the Murata Type 2FR Wi-Fi CLI project and its documentation. I successfully built and flashed the Wi-Fi CLI application and connected the device to a Wi-Fi network. After that, I tried the Wi-Fi MQTT example, which also worked successfully on the same board. However, after some time, I suddenly became unable to program new firmware into the device. Problem description I have tried flashing different firmware binaries at their respective addresses: Application firmware: 0x08000000 Wi-Fi firmware: 0x08400000 Bluetooth firmware: 0x08540000 I also tried reflashing the previously working Wi-Fi CLI and Wi-Fi MQTT projects, but the problem persists. I can connect to the RW612 using SEGGER J-Link over SWD, and I can read the existing flash contents. However, programming fails during flash verification. The issue occurs with different firmware images and is not limited to one project or address. I came across the NXP Community article titled “How to solve flashing problems in FRDM-RW612 (flash lock)” and tried to follow the suggested recovery approach using MCUXpresso Secure Provisioning Tool. However, I have not been able to resolve the problem. I also tried the ROM ISP recovery approach using USB and UART, but neither method worked successfully. When using the USB approach, blhost -- list-memory reports: Specified USB HID device not found: 0x1FC9, 0x0020 The device is visible in Windows Device Manager as a USB serial port (COM16), but the provisioning tool does not detect the expected USB HID device. Current J-Link error I am using J-Link Commander V8.44 with the RW612 target selected. The debugger successfully connects to the Cortex-M33 over SWD, and the target voltage is approximately 3.3 V. When programming the Wi-Fi firmware binary rw61x_sb_wifi_a2.bin at 0x08400000, I receive the following error: J-Link>loadfile "...\\rw61x_sb_wifi_a2.bin" 0x8400000 Downloading file [...] J-Link: Flash download: Bank 0 @ 0x08000000: 1 range affected (589824 bytes) J-Link: Flash download: Total: 4.538s J-Link: Flash download: Program speed: 249 KB/s ****** Error: Verification failed @ address 0x08400000 Error while programming flash: Verify failed. Unable to perform operation! Command failed with exit code 1 The same general problem occurs when I try programming the application firmware and other previously working binaries. What I need help with Could this be caused by a flash write lock, security configuration, flash protection, or an incorrect flash programming algorithm? Is there a reliable procedure to recover or unlock the RW612 flash on the Murata Type 2FR EVK using MCUXpresso Secure Provisioning Tool? Can the FRDM-RW612 flash recovery procedure be safely applied to the Murata Type 2FR EVK? Are there any board-specific differences in entering ROM ISP mode? Since the debugger can connect and read flash contents, but programming fails verification, what should I check next? Is there a way to restore flash programming access without damaging the existing board configuration or permanently disabling debug access? I would appreciate a step-by-step recovery procedure, particularly for the MCUXpresso Secure Provisioning Tool and ROM ISP method. The board was previously working correctly with both the Wi-Fi CLI and Wi-Fi MQTT examples. The problem appeared later, without any intentional change to the hardware. Thank you for your help. Re: Title: RW612 Flash Programming Verification Failed at 0x08400000 on Murata Type 2FR EVK Hello @sakshee, hope you are doing well. I will address your questions below: > Could this be caused by a flash write lock, security configuration, flash protection, or an incorrect flash programming algorithm? The flash locking occurs when an application is written to the flash with an invalid flash configuration block (FCB), for example, when the application was built considering a different external flash device. In the case of the Murata Type 2FR it contains a different flash from the FRDM-RW612, hence, a different FCB is required for each board. Could you please confirm if an application build for the FRDM-RW612 was built and flashed to the 2FR EVK? > Is there a reliable procedure to recover or unlock the RW612 flash on the Murata Type 2FR EVK using MCUXpresso Secure Provisioning Tool? If the previous case happened and the flash was locked, the reliable way to unlock it is as stated in the mentioned post: How to solve flashing problems in FRDM-RW612 (flash lock), however, this guide focuses on unlocking the FRDM-RW612. In order to apply this guide to the Murata's flash, I'd recommend following the general steps below (referencing both the Secure Provisioning Tool and the post itself): Set the board to ISP mode. Open the workspace, and select the RD-RW612-BGA option, as well as the "rdrw612bga_gpio_led_output_extfls.s19" source executable image. Configure the UART interface. Once in the main workspace menu, make sure the flash configurations match with the EVK's flash configurations in the Boot Memory Configuration window (please see the image below) Follow the rest of the guide as-is. > Can the FRDM-RW612 flash recovery procedure be safely applied to the Murata Type 2FR EVK? Are there any board-specific differences in entering ROM ISP mode? No, both boards have different flash memories each, therefore you must consider the steps shared in the previous answer. Also, I'd recommend checking the migration guide for RW612 development boards as it provides specific considerations regarding this same topic and application customization. > Since the debugger can connect and read flash contents, but programming fails verification, what should I check next? Please first check the mentioned procedure and information and let me know your findings. > Is there a way to restore flash programming access without damaging the existing board configuration or permanently disabling debug access? The shared procedure should not generate any damage to your board configuration, nor the debug access ports. Please let me know if this helps.
View full article
推荐的 电路板支持包。/Neutron SDK 版本控制策略 你好, 我们正在使用 i.MX95 作为平台开发汽车应用的 PoC,并希望澄清推荐的 Neutron SDK 版本策略。 我们已经阅读了 NeutronSDKUserGuide.md 中的“Neutron SDK 版本与 Yocto 电路板支持包的兼容性”表格,并了解到编译器和运行时必须来自同一个 SDK。但是,该指南并未说明推荐哪个版本。 我们应该始终在当前的 电路板支持包。 上使用最新的 Neutron SDK 版本(运行时已升级),还是应该使用该 电路板支持包。 的默认 SDK 版本? 环境 - 板:IMX95LPD5EVK-19 - 电路板支持包:LF_6.18.20_2.0.0 - Neutron SDK:eiq-neutron-sdk-linux-3.2.3 - NeutronFirmware.elf、libNeutronDriver.so 和 libneutron_delegate.so 已更新至 Neutron SDK 3.2.3 的版本。 谢谢! Re: Recommended BSP / Neutron SDK versioning strategy 您好, 感谢您对恩智浦半导体产品的关注, 您可以在《机器学习用户指南》的末尾找到每个电路板支持包所包含的 Neutron SDK 版本,例如:Neutron SDK v3.2.1 包含在 LF6.18.37_2.1.0 中。 但是,对于开发工作,我们鼓励客户使用最新的 SDK 版本,并且文档建议将二进制文件(用于转换)复制到目标位置: - 更新 Neutron 运行时 - 要更新目标设备上的中子运行时间,请将文件上传到 其指定目录如下: 文件 | 目标目录 | |------|------------------| | `NeutronFirmware.elf`| `/lib/firmware/` | | `libNeutronDriver.so`| `/lib/` | | `libneutron_delegate.so` | `/lib/` | 此致 Re: Recommended BSP / Neutron SDK versioning strategy 嗨,约瑟夫, 感谢你的回复。我们将按照建议使用最新的SDK版本。 问候
View full article
标题:Murata Type 2FR EVK 上的 RW612 闪存编程验证失败,错误地址为 0x08400000 NXP社区的各位朋友,大家好! 我正在使用基于 NXP RW612 MCU 的 Murata Type 2FR (LBES0ZZ2FR-EVK) ,需要帮助解决闪存编程问题。 最初,我参考了 Murata Type 2FR Wi-Fi CLI 项目及其文档。我已成功构建并刷写了 Wi-Fi CLI 应用程序,并将设备连接到了 Wi-Fi 网络。之后,我尝试了 Wi-Fi MQTT 示例,该示例在同一块板上也成功运行。 然而,过了一段时间后,我突然无法将新的固件编程到设备中。 问题描述 我已尝试将不同的固件二进制文件刷入到各自的地址: 应用程序固件: 0x08000000 Wi-Fi固件版本: 0x08400000 蓝牙固件版本: 0x08540000 我还尝试重新刷写之前运行正常的 Wi-Fi CLI 和 Wi-Fi MQTT 项目,但问题仍然存在。 我可以通过 SEGGER J-Link 经由 SWD 连接到 RW612,并且可以读取现有的闪存内容。然而,在闪存验证过程中编程失败。该问题在不同的固件镜像中都会出现,并且不局限于某个项目或地址。 我偶然看到NXP社区一篇题为“如何解决FRDM-RW612的烧录问题(闪存锁定)”的文章,并尝试使用MCUXpresso安全配置工具按照建议的方法进行恢复。然而,我仍然无法解决问题。 我还尝试了使用 USB 和 UART 进行 ROM ISP 恢复的方法,但两种方法都失败了。使用 USB 方法时, blhost -- list-memory命令报告: 未找到指定的 USB HID 设备:0x1FC9、0x0020 该设备在 Windows 设备管理器中显示为 USB 串行端口 (COM16),但配置工具无法检测到预期的 USB HID 设备。 当前 J-Link 错误 我正在使用 J-Link Commander V8.44,并选择了 RW612 目标。调试器通过 SWD 成功连接到 Cortex-M33,目标电压约为 3.3 V。 当对地址为0x08400000 的Wi-Fi 固件二进制文件rw61x_sb_wifi_a2.bin进行编程时,出现以下错误: J-Link>loadfile "...\\rw61x_sb_wifi_a2.bin" 0x8400000 Downloading file [...] J-Link: Flash download: Bank 0 @ 0x08000000: 1 range affected (589824 bytes) J-Link: Flash download: Total: 4.538s J-Link: Flash download: Program speed: 249 KB/s ****** Error: Verification failed @ address 0x08400000 Error while programming flash: Verify failed. Unable to perform operation! Command failed with exit code 1 当我尝试对应用程序固件和其他以前可以正常运行的二进制文件进行编程时,都会出现同样的问题。 我需要哪些方面的帮助? 这可能是由于闪存写入锁定、网络安全配置、闪存保护或错误的闪存编程算法造成的吗? 使用 MCUXpresso Secure Provisioning Tool 是否有可靠的方法来恢复或解锁 Murata Type 2FR EVK 上的 RW612 闪存? FRDM-RW612 的闪存恢复程序可以安全地应用于 Murata Type 2FR EVK 吗?进入 ROM ISP 模式时,不同板之间是否存在板级差异? 既然调试器可以连接并读取闪存内容,但编程验证失败,接下来我应该检查什么? 有没有办法在不损坏现有板配置或永久禁用调试访问的情况下恢复闪存编程访问权限? 我希望能够获得详细的恢复步骤说明,特别是针对 MCUXpresso 安全配置工具和 ROM ISP 方法的说明。 该板之前使用 Wi-Fi CLI 和 Wi-Fi MQTT 示例都能正常工作。问题出现于之后,并非人为对硬件进行任何改动。 感谢您的帮助。 Re: Title: RW612 Flash Programming Verification Failed at 0x08400000 on Murata Type 2FR EVK 你好@sakshee ,希望你一切都好。 下面我将回答您的问题: 这可能是由于闪存写入锁定、网络安全配置、闪存保护或错误的闪存编程算法引起的吗? 当应用程序使用无效的闪存配置块 (FCB) 写入闪存时,就会发生闪存锁定,例如,当应用程序在构建时考虑了不同的外部闪存设备。以 Murata Type 2FR 为例,它包含与 FRDM-RW612 不同的闪存,因此每块板都需要不同的 FCB。请问是否已构建 FRDM-RW612 的应用程序版本并将其刷写到 2FR EVK 中? > 是否有可靠的方法可以使用 MCUXpresso Secure Provisioning Tool 恢复或解锁 Murata Type 2FR EVK 上的 RW612 闪存? 如果发生了上述情况并且闪存被锁定,则可靠的解锁方法如上述帖子中所述:如何解决 FRDM-RW612 的刷机问题(闪存锁定) ,但是,本指南重点介绍如何解锁 FRDM-RW612。为了将本指南应用于 Murata 的闪存,我建议按照以下一般步骤操作(参考安全配置工具和本文本身): 将板设置为ISP模式。 打开工作区,选择 RD-RW612-BGA 选项,以及“rdrw612bga_gpio_led_output_extfls.s19”;源可执行映像。 配置UART接口。 进入主工作区菜单后,请确保闪存配置与 EVK 的启动内存配置窗口中的闪存配置相匹配(请参见下图)。 请按指南其余部分的步骤操作。 > FRDM-RW612 的闪存恢复程序可以安全地应用于 Murata Type 2FR EVK 吗?进入 ROM ISP 模式时,不同板之间是否存在差异? 不,两块板的闪存各不相同,因此您必须考虑上一个答案中提到的步骤。另外,我建议您查看RW612 开发板的迁移指南,因为它提供了有关此主题和应用程序定制的具体注意事项。 既然调试器可以连接并读取闪存内容,但编程验证失败,接下来我应该检查什么? 请先核对上述步骤和信息,并将您的核对结果告知我。 > 是否有办法在不损坏现有板配置或永久禁用调试访问的情况下恢复闪存编程访问权限? 共享程序不应对您的电路板配置或调试访问端口造成任何损坏。 请告诉我这是否有帮助。
View full article
タイトル: RW612 フラッシュプログラミング検証が、Murata Type 2FR EVK の 0x08400000 で失敗しました こんにちは、NXPコミュニティの皆さん、 私はNXP RW612 MCUをベースにしたMurata Type 2FR(LBES0ZZ2FR-EVK)を使っており、フラッシュプログラミングの問題を解決する助けが必要です。 最初は村田Type 2FR Wi-Fi CLIプロジェクトとそのドキュメントをフォローしていました。Wi-Fi CLIアプリケーションを無事に構築・フラッシュし、デバイスをWi-Fiネットワークに接続しました。その後、Wi-Fi MQTTのサンプルを試してみたところ、同じボード上で正常に動作しました。 しかし、しばらくすると、突然、デバイスに新しいファームウェアを書き込むことができなくなってしまった。 問題の説明 それぞれのファームウェアバイナリを、対応するアドレスに書き込んでみました。 アプリケーションファームウェア:0x08000000 Wi-Fiファームウェア: 0x08400000 Bluetoothファームウェア: 0x08540000 以前正常に動作していたWi-Fi CLIとWi-Fi MQTTプロジェクトを再フラッシュしてみましたが、問題は解決しませんでした。 SEGGER J-Linkを使ってSWD経由でRW612に接続でき、既存のフラッシュの内容も読み取れます。しかし、フラッシュ検証中にプログラミングが失敗する。この問題は様々なファームウェアイメージで発生し、特定のプロジェクトやアドレスに限定されるものではありません。 NXPコミュニティの「FRDM-RW612(フラッシュロック)のフラッシュ問題の解決方法」という記事を見つけ、MCUXpresso Secure Provisioning Toolを使って提案された回復方法を試しました。しかし、問題を解決できていません。 USBとUARTを使ったROM ISP復旧方法も試しましたが、どちらもうまくいきませんでした。USB方法を使うと、 blhost -- list-memory の報告: 指定されたUSB HIDデバイスが見つかりません: 0x1FC9、0x0020 デバイスはWindowsデバイスマネージャーでUSBシリアルポート(COM16)として表示されますが、プロビジョニングツールは期待されるUSB HIDデバイスを検出しません。 現在のJ-Linkエラー 私はRW612ターゲットを選択したJ-Link Commander V8.44を使用しています。デバッガはSWD経由でCortex-M33に接続し、目標電圧は約3.3Vです。 Wi-Fiファームウェアバイナリrw61x_sb_wifi_a2.binをアドレス0x08400000に書き込む際に、以下のエラーが発生します。 J-Link>loadfile "...\\rw61x_sb_wifi_a2.bin" 0x8400000 Downloading file [...] J-Link: Flash download: Bank 0 @ 0x08000000: 1 range affected (589824 bytes) J-Link: Flash download: Total: 4.538s J-Link: Flash download: Program speed: 249 KB/s ****** Error: Verification failed @ address 0x08400000 Error while programming flash: Verify failed. Unable to perform operation! Command failed with exit code 1 同じような一般的な問題は、アプリケーションのファームウェアや以前は動作していたバイナリをプログラムしようとすると発生します。 私が助けを必要としているのは これはフラッシュ書き込みロック、セキュリティ設定、フラッシュ保護、あるいは誤ったフラッシュプログラミングアルゴリズムが原因かもしれません。 MCUXpresso Secure Provisioning Toolを使用して、Murata Type 2FR EVKのRW612フラッシュを復元またはロック解除するための信頼できる手順はありますか? FRDM-RW612フラッシュリカバリー手順は村田タイプ2FR EVKに安全に適用できますか?ROM ISPモードに入る際、基板固有の違いはありますか? デバッガは接続してフラッシュの内容を読み取れるのに、プログラムが検証に失敗するので、次に何を確認すればいいのでしょうか? 既存のボード構成を壊さず、デバッグアクセスを永久に無効化せずにフラッシュプログラミングアクセスを復元する方法はありますか? 特にMCUXpressoセキュアプロビジョニングツールとROM ISP方法について、段階的な復旧手順を教えていただけるとありがたいです。 以前は、このボードはWi-Fi CLIとWi-Fi MQTTの両方のサンプルで正常に動作していました。問題は後になって発生したが、ハードウェアに意図的な変更は一切加えていない。 ご協力ありがとうございます。 Re: Title: RW612 Flash Programming Verification Failed at 0x08400000 on Murata Type 2FR EVK こんにちは、 @sakshee さん。お元気でお過ごしでしょうか。 ご質問にお答えします。 > これはフラッシュ書き込みロック、セキュリティ設定、フラッシュ保護、または誤ったフラッシュプログラミングアルゴリズムによって引き起こされる可能性はありますか? フラッシュロックは、アプリケーションが無効なフラッシュ構成ブロック(FCB)でフラッシュに書き込みられた場合、例えば異なる外部フラッシュデバイスを想定してアプリケーションが構築された場合に発生します。村田タイプ2FRの場合はFRDM-RW612とは異なるフラッシュを搭載しているため、各基板ごとに異なるFCBが必要です。FRDM-RW612のアプリケーションビルドが2FR EVKにビルドされ、フラッシュされたかどうか確認していただけますか? MCUXpresso Secure Provisioning Toolを使用して、Murata Type 2FR EVKのRW612フラッシュを復元またはロック解除するための信頼できる手順はありますか? 前述のケースでフラッシュがロックされている場合、信頼できる解除方法は前述の投稿「 FRDM-RW612(フラッシュロック)でのフラッシュ問題の解決方法」ですが、このガイドではFRDM-RW612の解除に焦点を当てています。このガイドを村田製作所製フラッシュメモリに適用するには、以下の一般的な手順に従うことをお勧めします(セキュアプロビジョニングツールとこの記事の両方を参照してください)。 ボードをISPモードに設定してください。 ワークスペースを開き、RD-RW612-BGAオプションと「rdrw612bga_gpio_led_output_extfls.s19」を選択します。ソース実行可能イメージ。 UARTインターフェースの設定をしてください。 メインワークスペースメニューに入ったら、ブートメモリ構成ウィンドウで、フラッシュ構成がEVKのフラッシュ構成と一致していることを確認してください(下の画像を参照)。 残りの手順はガイドの指示通りに行ってください。 >FRDM-RW612フラッシュリカバリー手順は村田タイプ2FR EVKに安全に適用できますか?ROM ISPモードに入る際に基板固有の違いはありますか? いいえ、両方のボードはそれぞれ異なるフラッシュメモリーを持っているので、前の回答で説明した手順を考慮する必要があります。また、 RW612開発ボードの移行ガイド も確認することをお勧めします。同じトピックやアプリケーションのカスタマイズに関する具体的な注意点が記載されています。 > デバッガは接続してフラッシュの内容を読み取れるのに、プログラミングが検証に失敗するので、次に何を確認すればいいでしょうか? まず、記載されている手順と情報をご確認いただき、その結果をお知らせください。 > 既存の基板構成を損傷したり、デバッグアクセスを永久に無効にしたりせずに、フラッシュプログラミングへのアクセスを復元する方法はありますか? 共有手順はボード構成やデバッグアクセスポートにダメージを与えることはありません。 これが役に立つかどうか教えてください。
View full article
CLRD730 compatibility with 701 Hello, We have a customer with many CLRD 701 deployed. They would like to buy more. What is the chance to have their application working with the 730 without modifying the code ?  Thanks a lot and best regards. Re: CLRD730 compatibility with 701 Hello @fox13 , Hope you are doing great. Thank you for continuing to choose NXP products. Regarding your question, it should be possible to use the CLRD730 with your application. Please consider that the Pegoda CLRD730 desktop reader is designed to work with the default Windows CCID driver.  We also encourage you to review Section 6.8 "PC/SC mode" of the CLRD730 datasheet, which covers relevant information for your integration. Best Regards, Jaime.
View full article
推奨されるBSP / Neutron SDKのバージョン管理戦略 こんにちは、 私たちはi.MX95をプラットフォームとして用いる自動車アプリケーション向けのPoCを開発しており、推奨されるNeutron SDKのバージョン管理戦略について明確にしたいと思います。 NeutronSDKUserGuide.md 年の「Neutron SDK Version Compatibility with Yocto BSP」の表を読み、コンパイラとランタイムは同じSDKから来なければならないと理解しています。しかし、ガイドにはどのバージョンが推奨されているかは明記されていない。 現在のBSPでは常に最新のNeutron SDKバージョン(ランタイムがアップグレードされたもの)を使うべきでしょうか、それともそのBSPのデフォルトバージョンを使うべきでしょうか? 環境 - ボード:IMX95LPD5EVK-19 - BSP:LF_6.18.20_2.0.0 - Neutron SDK: eiq-neutron-sdk-linux-3.2.3 - NeutronFirmware.elf、libNeutronDriver.so、libneutron_delegate.soはNeutron SDK 3.2.3のバージョンに更新されています。 ご回答をお待ちしています。 Re: Recommended BSP / Neutron SDK versioning strategy こんにちは、 NXP Semiconductors製品にご関心いただきありがとうございます。 機械 学習ユーザーガイドの最後に、すべてのBSPに含まれるNeutron SDKバージョンを確認できます。Neutron SDK v3.2.1はLF6.18.37_2.1.0に含まれています。 しかし、開発に関しては、お客様に最新のSDKリビジョンを使用することが推奨されており、ドキュメントには変換に使われるバイナリをコピーして以下を対象にすることが推奨されています: - Neutron ランタイムの更新 - ターゲットデバイスでNeutronランタイムを更新するには、ファイルを IRは以下の通りにディレクトリを指定しています: | ファイル | 対象ディレクトリ | |------|------------------| | `NeutronFirmware.elf`|'/lib/firmware/' | |「libNeutronDriver.so」|'/lib/' | |『libneutron_delegate.so』 |『/lib/』 | よろしくお願いします。 Re: Recommended BSP / Neutron SDK versioning strategy こんにちは、ジョセフさん。 お返事ありがとうございます。推奨される最新のSDKリビジョンを使用します。 よろしくお願いいたします
View full article
CLRD730 与 701 的兼容性 你好, 我们有一位客户部署了许多 CLRD 701。他们还想买更多。不修改代码,他们的应用程序与730兼容的可能性有多大? 非常感谢,并致以最诚挚的问候。 Re: CLRD730 compatibility with 701 你好@fox13 , 希望你一切都好。 感谢您一直以来选择恩智浦产品。 关于您的问题,CLRD730 应该可以与您的应用程序一起使用。 请注意,Pegoda CLRD730 桌面读卡器设计用于默认的 Windows CCID 驱动程序。我们还建议您查阅 CLRD730 数据手册 的 6.8 节“ PC/SC 模式” ,其中包含与您的集成相关的必要信息。 此致, 杰米。
View full article
Example S32K311 SPI LinTrcv_fs23 MCAL S32DS3.6.11 RTD7.0.1 ***************************************************************************** *Detailed Description: *This is a basic communication example for LIN transceiver module of FS23 SBC with SPI interface. *The FS23 SBC on the S32K31XEVB-Q100 board integrated a LIN transceiver. To test LIN communication, another board or a LIN analyzer must be used. *In this example, the S32K311 configures and controls the FS23 via LPSPI0. *The FS23 LinTrcv driver is initialized by calling LinTrcv_43_fs23_Init(), while LinTrcv_43_fs23_SetOpMode() is used to change the operating mode of the integrated LIN transceiver. *After initialization is complete, the S32K3 transmits a LIN frame with ID 0x1A. *At this stage, the LIN frame should be received by the LIN analyzer connected to the J9 LIN bus interface on the S32K31XEVB-Q100 board. *LED Indications: Blue LED ON: LIN frame transmission in progress Blue LED OFF: LIN frame transmission completed Red LED flashes: LIN frame transmission timed out *---------------------------------------------------------------------------- *Test HW: * S32K31XEVB-Q100 Board SCH-55131 REV A1 P32K311HVS 0P98C * PCAN-USB Pro * PCAN-USB Pro | S32K31XEVB-Q100 ------------------------|-------------------- LIN LIN2.4 | J9.1 VBAT LIN2.9 | J9.2 GND LIN2.5 | J9.4 - S32K31XEVB-Q100 Jumper Configuration: J25 1-2 https://www.nxp.com/document/guide/getting-started-with-the-s32k31xevb-q100-evaluation-board-for-general-purpose:GS-S32K31XEVB-Q100?section=plug-it-in_plug-it-in-1 Test SW: *PLIN-View Pro *SDK: * S32K3_S32M27x Real-Time Drivers ASR R23-11 Version 7.0.1 (SW32K3_S32M27x_RTD_R23-11_7.0.1_D2603_DesignStudio_updatesite.zip) * 2.0.0 SBC FS23 R23-11 2.0.0 (SBC_FS23_R23-11_2.0.0_D2604_DesignStudio_updatesite.zip) *Debugger: S32DS 3.6.11, OpenSDA/ PEmicro Multilink Universal FX *Target: internal_FLASH *Reference Documentation: * AN14041 FS23 quick start guide (Rev. 2.0 23 January 2025) * AN14129 FS23 implementation and behaviors (Rev. 2.0 13 December 2024) * FS23, Safety System Basis Chip (SBC) with Power Management, CAN FD and LIN Transceivers Data Sheet (Rev. 8.0 30 June 2025) * RTD_SBC_FS23_UM.pdf C:\NXP\S32DS.3.6.11_S32K3_RTD701\S32DS\software\common\SBC_FS23\Sbc_fs23_TS_T40DXXM20I0R0\doc * RTD_LINTRCV_43_FS23_UM.pdf C:\NXP\S32DS.3.6.11_S32K3_RTD701\S32DS\software\common\SBC_FS23\LinTrcv_43_fs23_TS_T40DXXM20I0R0\doc * AUTOSAR_CP_SWS_LINDriver.pdf https://www.autosar.org/fileadmin/standards/R23-11/CP/AUTOSAR_CP_SWS_LINDriver.pdf * This example is migrated from LinTrcv_fs23_Example_S32K312. The method of migrating refers to the video "2.S32DS CT MCAL demo porting K344 to K312 based on RTD500": https://community.nxp.com/t5/S32K-Knowledge-Base/S32K3-Tools-Part-How-to-port-RTD-s-existing-MCAL-demo-to-other/ta-p/1966315 ***************************************************************************** * Revision History: * Ver Date Author Description of Changes * 0.0 10-14-2026 Robin Shen Initial version *****************************************************************************
View full article
在 EB Tresos 30.0 中无法选择 mcal 端口模块的 PortPinMode。 我发现 EB tresos 30.0 与 29.0 非常不同。29.0 版本一切顺利,但 30.0 版本出现了很多问题。 至于端口模块的配置项“PortPin Mode”,除了 GPIO 之外,我没有看到任何其他选项。 例如这个 UART TX 引脚,我无法将其修改为 UART TX 选项。 这是什么原因呢?如何解决这个问题? Re: PortPinMode of mcal port module could not be select in EB tresos 30.0 请问有人能给些建议吗? Re: PortPinMode of mcal port module could not be select in EB tresos 30.0 您好,请问您能否提供一下您使用的芯片和RTD版本? 此外,您是否尝试过使用旧版编辑器? 1. 关闭EB。 2.编辑C:\EB\tresos_32_1_4\configuration中的defaultPreferences.properties setLegacyEditorAsDefault: true 3. 保存,重新打开 EB 和模块,然后测试您的配置。 Re: PortPinMode of mcal port module could not be select in EB tresos 30.0 这可能与 EB tresos 30.0 中的新编辑器和 MCU/Port 插件之间的兼容性问题有关。总之,我很高兴听到切换到旧版编辑器解决了这个问题。 Re: PortPinMode of mcal port module could not be select in EB tresos 30.0 您好,谢谢您的回复。切换到旧版编辑器后,看起来就正常了。 这是什么原因呢?为什么使用最新版本 30.0 的编辑器会出现这个问题?
View full article
PN7160 Burning Hello, I am currently using a PN7160 kit ending with EVK, and we used the hat that connects to the pi, making sure it was seated correctly (as far as we know) and it worked perfectly yesterday making sure it was communicating over I2C, but today when we came back to the lab and plugged it in (unchanged from last night) some smoke started coming out of the IC on the PN7160, so we unplugged it The Pi boots up normally without the pn7160 on so I’m not sure what happened between yesterday and today but it was locked away and I am the only one with a key. We’re doing a sponsored project with Toyota, and he advised us to talk to the support team, so we were just seeing if y’all had any advice or idea what happened Re: PN7160 Burning We don't meet this issue before. I would suggest you to try another PN7160 EVK board.
View full article
S32 Design Studio for Power Architecture 2017.R1 在许可证过期后显示“缺少许可证” 您好,NXP支持团队, 我正在 Windows 系统上使用S32 Design Studio for Power Architecture 2017.R1 版本。现在 IDE 显示“缺少许可证” ,而且许可证似乎已经过期。 Re: S32 Design Studio for Power Architecture 2017.R1 shows “License missing” after license expired 你好, 您的S32DS许可证已延期。请使用您之前的激活码重新激活S32DS。
View full article
S32 Design Studio for Power Architecture 2017.R1 はライセンス満了後に「ライセンス不足」と表示します こんにちは、NXPサポートチームの皆さん、 私はWindowsの S32 Design Studio for Power Architecture 2017.R1 を使っています 。IDEでは「 ライセンス不足」 と表示 され、ライセンスは期限切れのようです。 Re: S32 Design Studio for Power Architecture 2017.R1 shows “License missing” after license expired こんにちは、 お客様のS32DSライセンスが延長されました。以前のコードを使用して、S32DSを再度有効化してください。
View full article
S32 Design Studio for ARM v2018 R1 はライセンスが期限切れとなり、インストールできなくなりました。 以前はS32K144を使用しており、S32 Design Studio for ARM v2018 R1をインストールしていました。しばらく使用した後、期限切れと表示されました。現在はfs65を使用しており、いくつかのサンプルコードを学習する必要があります。サンプルコードは、S32 Design Studio for ARM v2018 R1開発環境に基づいています。インストール中にアクティベーションコードを正常に検証できず、オフラインインストールも機能しませんでした。しかし、ビュー数に拡張機能が見つかりませんでした。 認証コードを入力させていただくか、期限切れのアカウントを復元していただけますでしょうか?よろしくお願いいたします。 以前はS32 Design Studio for ARM v2018 R1でS32K144を使用していましたが、しばらく使用した後、有効期限切れの通知を受け取りました。現在FS65を使用しており、S32 Design Studio for ARM v2018 R1開発環境に基づいたサンプルコードを研究する必要があります。しかし、オンラインでもオフラインでもアクティベーションコードを正常に認証できず、ライセンスを延長するオプションも見つかりません。 アクティベーションコードの認証、または有効期限切れの問題を解決するお手伝いをしていただけませんか?ありがとう! Re: S32 Design Studio for ARM v2018 R1过期后,无法再安装 こんにちは、 お客様のS32DSライセンスが延長されました。以前のコードを使用して、S32DSを再度有効化してください。 Re: S32 Design Studio for ARM v2018 R1过期后,无法再安装 インストールは無事完了しました。ご協力ありがとうございました!
View full article
S32 Design Studio for ARM v2018 R1过期后,无法再安装 之前使用S32K144,安装S32 Design Studio for ARM v2018 R1后,之后使用一段时间就提示过期了,现在在使用fs65,发现需要学习一下实例代码,实例代码基于S32 Design Studio for ARM v2018 R1开发环境,安装的时候,激活码无法验证成功,离线也不行,但是我在view count找不到延期。 能否让我可以验证码能通过或者解除我的过期,谢谢! I previously used the S32K144 with S32 Design Studio for ARM v2018 R1, but after using it for a while, I received an expiration notice. I am now working with the FS65 and need to study the example code, which is based on the S32 Design Studio for ARM v2018 R1 development environment. However, I am unable to successfully validate the activation code—neither online nor offline—and I cannot find an option to extend the license. Could you please help me get the activation code validated or resolve the expiration issue? Thank you! Re: S32 Design Studio for ARM v2018 R1过期后,无法再安装 你好, 您的S32DS许可证已延期。请使用您之前的激活码重新激活S32DS。 Re: S32 Design Studio for ARM v2018 R1过期后,无法再安装 现在可以安装成功了,非常感谢支持!
View full article
S32 Design Studio for ARM v2018 R1 has expired and can no longer be installed. Previously, I used S32K144 and installed S32 Design Studio for ARM v2018 R1. After using it for a while, it showed as expired. Now I'm using fs65 and I need to study some example code. The example code is based on the S32 Design Studio for ARM v2018 R1 development environment. During installation, the activation code could not be verified successfully, and offline installation didn't work either. However, I couldn't find the extension in the view count. Could you please allow me to pass the verification code or undo my expired account? Thank you! I previously used the S32K144 with S32 Design Studio for ARM v2018 R1, but after using it for a while, I received an expiration notice.I am now working with the FS65 and need to study the example code, which is based on the S32 Design Studio for ARM v2018 R1 development environment.However, I am unable to successfully validate the activation code—neither online nor offline—and I cannot find an option to extend the license. Could you please help me get the activation code validated or resolve the expiration issue?Thank you! Re: S32 Design Studio for ARM v2018 R1过期后,无法再安装 Hi,  your S32DS license has been extended. Please activate S32DS again with your old code.  Re: S32 Design Studio for ARM v2018 R1过期后,无法再安装 The installation was successful. Thank you so much for your support!
View full article
S32 Design Studio for Power Architecture 2017.R1 shows “License missing” after license expired Hi NXP Support team, I am using S32 Design Studio for Power Architecture 2017.R1 on Windows. The IDE now shows “License missing”, and it seems the license has expired. Re: S32 Design Studio for Power Architecture 2017.R1 shows “License missing” after license expired Hi,  your S32DS license has been extended. Please activate S32DS again with your old code. 
View full article
PN7160 燃焼 こんにちは。私は現在、EVKで終わったPN7160キットを使っています。パイに接続する帽子を使い、正しく接続されているか確認しました(私たちの知る限り)。昨日はI2Cで通信しているのを確認し、問題なく動作していましたが、今日ラボに戻って昨夜と同じように接続したところ、PN7160のICから煙が出始めたSO、プラグを抜きました pn7160をつけていないとPiは正常に起動するので、昨日から今日の間に何があったのかはわかりませんが、鍵はロックされていて、私だけが鍵を持っています。 私たちはトヨタとスポンサー付きプロジェクトを行っていて、サポートチームに相談するよう勧められたので、皆さんに何かアイデアや何が起きたのか分かるか聞きたかっただけです Re: PN7160 Burning 私たちはこれまでこの問題に遭遇したことがありません。別のPN7160 EVKボードを試してみることをお勧めします。
View full article
PN7160燃烧 您好,我目前使用的是型号以 EVK 结尾的 PN7160 开发板,我们使用了连接到树莓派的扩展板,并确保其正确连接(据我们所知)。昨天一切正常,I2C 通信也正常。但今天我们回到实验室并再次连接(与昨晚的连接方式相同)后,PN7160 芯片上的集成电路开始冒烟,所以我们立即拔掉了电源。 即使没有 pn7160,Pi 也能正常启动,所以我不太清楚昨天到今天之间发生了什么,但它被锁起来了,只有我有钥匙。 我们正在和丰田合作做一个赞助项目,他建议我们联系他们的支持团队,所以我们想看看大家有没有什么建议或者知道发生了什么。 Re: PN7160 Burning 我们之前从未遇到过这个问题。我建议您尝试使用另一块PN7160 EVK板。
View full article
MCALポートモジュールのPortPinModeはEB tresos 30.0で選択できませんでした EB tresos 30.0は29.0とは全く違うと感じます。バージョン29.0ではすべて順調だったが、バージョン30.0では多くの問題が発生した。 ポートモジュールの「PortPin Mode」設定項目については、GPIO以外の選択肢が見当たりませんでした。 例えばUART TXピンの場合、UART TXオプションに変更できませんでした。 その理由は?どうすれば解決できますか? Re: PortPinMode of mcal port module could not be select in EB tresos 30.0 どなたかアドバイスをいただけませんか? Re: PortPinMode of mcal port module could not be select in EB tresos 30.0 こんにちは、使っているChipとRTDのバージョンを教えてもらえますか? それに、従来の編集ソフトで試してみましたか? 1. EBをシャットダウンする。 2. C:\EB\tresos_32_1_4\configuration のdefaultPreferences.properties を編集します。 setLegacyEditorAsDefault: true 3. 保存してEBとモジュールを再度開き、設定を試してください。 Re: PortPinMode of mcal port module could not be select in EB tresos 30.0 こんにちは、ご返信ありがとうございます。レガシーエディターに切り替えると正常に見えます。 その理由は?最新バージョンのエディタ(バージョン30.0)を使用すると、なぜそのような問題が発生するのでしょうか? Re: PortPinMode of mcal port module could not be select in EB tresos 30.0 これはEB Tresos 30.0の新しいエディタとMCU/Portプラグインとの互換性の問題に関連している可能性があります。いずれにせよ、レガシーエディタに切り替えたことで問題が解決したと聞いて安心しました。
View full article
PortPinMode of mcal port module could not be select in EB tresos 30.0 I find EB tresos 30.0 is very different from 29.0. Everything go smoothly in 29.0, but has many problem on 30.0. As for the configuration item "PortPin Mode" of port module, I could not see any option except GPIO. Such as this one for UART TX pin, I could not modify it to UART TX option. What's the reason for this? How to solve it? Re: PortPinMode of mcal port module could not be select in EB tresos 30.0 Could any one give some advice? Re: PortPinMode of mcal port module could not be select in EB tresos 30.0 Hi, Can you pls provide the Chip and RTD version you are using? Besides, have you tried in legacy editor?: 1. Shutdown EB。 2. Edit defaultPreferences.properties in C:\EB\tresos_32_1_4\configuration setLegacyEditorAsDefault: true 3. save, reopen EB and Module and try your configuration Re: PortPinMode of mcal port module could not be select in EB tresos 30.0 It may be related to a compatibility issue between the new editor in EB tresos 30.0 and the MCU/Port plugin. In any case, I’m glad to hear that switching to the legacy editor resolved the issue. Re: PortPinMode of mcal port module could not be select in EB tresos 30.0 Hi, thanks for your reply. It looks normal after I switch to legacy editor. What's the reason for this? Why it has that problem when using latest editor of version 30.0?
View full article