Hello,
We are following up on "Do CAN_LLCE and LLCE_Af support Postbuild Loadable?" (April 2025). NXP support answered "Postbuild model" for Can_43_LLCE. The loadable question was left open. Do CAN_LLCE and LLCE_Af support Postbuild Loadable? - NXP Community
Setup: S32G274A, S32G_LLCE_1_0_9 (Can_43_LLCE 1.0.9, RTD AUTOSAR 4.4).
Goal: update CAN config as post-build loadable without reflashing the full application image.
In the 1.0.9 package, we see:
Questions:
Thanks in advance,
Ayman
Hi,AymanYounis
Thank you for contacting us and your information.
I have received your question and will help you to check it.
BR
Joey