Multi Source Translation Content

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Multi Source Translation Content

讨论

排序依据:
TED-Kit 2 (OM6716) GUI 软件下载说明申请 尊敬的恩智浦技术支持团队: 我是jwHyun, 请问能否提供下载图形用户界面软件包的说明,以便我们将其提供给我们的客户? 请您在方便的时候尽快指导我们完成注册/下载流程。 感谢您提前给予的支持。 Re: Request for TED-Kit 2 (OM6716) GUI Software Download Instructions 我在另一个案件中回复过你。谢谢。
查看全文
TEA1716 сalculation file Hello, I am looking for an Excel calculation file for the TEA1716 IC, similar to those provided in the development tools for other chips in the TEA series. I am using the TEA1716DB1255 development board and following the relevant documentation, but I would also like to access the calculation file if one exists. Thank you for your reply, and have a great day! Power solution Re: TEA1716 сalculation file Hello, An Excel-based calculation sheet for the TEA1716 exists ("Calculation sheet TEA1716 draft V1_4") and serves as the replacement for the original online design tool, which is no longer operational. Please find it attached. For reference alongside the calculation sheet, the key documents for your TEA1716DB1255 work are: AN11179 — detailed design guidance including worked calculation examples UM10557 — TEA1716DB1255 demo board documentation BRs, Tomas
查看全文
TED-Kit 2(OM6716)GUIソフトウェアダウンロード手順の要請 親愛なるNXPサポートチームへ、 私はjwヒョンです。 お客様にお渡しできるように、GUIソフトウェアパッケージのダウンロード方法について教えていただけますか? お手数ですが、登録/ダウンロードの手順について、できるだけ早くご教示いただければ幸いです。 サポートにあらかじめ感謝いたします。 Re: Request for TED-Kit 2 (OM6716) GUI Software Download Instructions 別のCASEであなたに返答した。ありがとう。
查看全文
On-chip secure NVM (S32K314) The Secure NVM mapping(FULL_MEM) described in HSE FW install for S32K3xx.pdf is as follows: HSE data flash is 160KB,APP data flash is 88KB,total : 160KB+88KB=248KB luojing_0-1789619650388.png luojing_1-1789619740147.png However, the dflash allocation described in S32K3XXRM.pdf is as follows: The total size of dflash is 128KB luojing_2-1789619854070.png Why are the Dflash sizes mentioned in the two documents different? Note: I am using the HSE firmware version HSE_FW_S32K344_0_2_55_0_S2502.exe luojing_3-1789620886731.png Re: sRe: On-chip secure NVM (S32K314) All these information you will find in HSE-B Firmware Reference Manual. It is a secure file, so following procedure is needed to follow unless you have already done it before: https://www.nxp.com/docs/en/user-guide/nxp-secure-access-rights-registration.pdf For better understanding you may also see following link: https://www.nxp.com/support/support/secure-access-rights:SEC-ACCESS Re: sRe: On-chip secure NVM (S32K314) The HSE FW install for S32K3xx.pdf only specifies the range of HSE Pflash and dflash, without specifying the RAM range. What is the RAM range used by HSE? What are the starting address and size? Is there a specific document describing it? Re: sRe: On-chip secure NVM (S32K314) Secure data flash starts at 0x10016000 (for FULL_MEM) having 168KB. It is the same on all derivatives. The appnote is not up to date. Re: sRe: On-chip secure NVM (S32K314) luojing_0-1789654909700.png Is it incorrect for HSE (FULL UMEM) Dflash size to be 160KB? Should it be 128KB-88KB=40KB? sRe: On-chip secure NVM (S32K314) It is described here: davidtosenovjan_0-1789654479428.png
查看全文
片上安全型非易失性存储器(S32K314) HSE FW install for S32K3xx.pdf 中描述的 Secure NVM 映射(FULL_MEM)如下: HSE 数据闪存为 160KB,APP 数据闪存为 88KB,总计:160KB+88KB=248KB 罗静_0-1789619650388.png 罗静_1-1789619740147.png 然而,S32K3XXRM.pdf 中描述的 dflash 分配如下: dflash的总大小为128KB 罗晶_2-1789619854070.png 为什么两份文件中提到的Dflash容量大小不同? 注意:我使用的是 HSE 固件版本 HSE_FW_S32K344_0_2_55_0_S2502.exe 罗静_3-1789620886731.png Re: sRe: On-chip secure NVM (S32K314) 所有这些信息都可以在 HSE-B 固件参考手册中找到。 这是一个安全文件,因此除非您之前已经操作过,否则需要按照以下步骤操作: https://www.nxp.com/docs/en/user-guide/nxp-secure-access-rights-registration.pdf 为了更好地理解,您还可以参考以下链接: https://www.nxp.com/support/support/secure-access-rights:SEC-ACCESS Re: sRe: On-chip secure NVM (S32K314) S32K3xx 的 HSE FW 安装说明.pdf 仅指定了 HSE Pflash 和 dflash 的范围,而没有指定 RAM 的范围。HSE使用的内存范围是多少? 起始地址和大小是多少? 是否有相关文件进行描述? Re: sRe: On-chip secure NVM (S32K314) 安全数据闪存从 0x10016000 开始(对于 FULL_MEM),大小为 168KB。所有衍生品都一样。 该应用说明已过时。 Re: sRe: On-chip secure NVM (S32K314) 罗晶_0-1789654909700.png HSE(完整 UMEM)Dflash 大小为 160KB 是否不正确?应该是 128KB-88KB=40KB 吗? sRe: On-chip secure NVM (S32K314) 具体描述如下: davidtosenovjan_0-1789654479428.png
查看全文
Regarding AFM907N PA Can you share tuned layout for 915MHz frequency range if available Re: Regarding AFM907N PA Hello lavanyaemsec Good day! We regret to inform you that we do not have a reference layout for 915 MHz; the closest one would be the... AFM907N 760-870 MHz Reference Circuit Design Files Which can be found on the official AFM907N page in the design resources section. We apologize for any inconvenience this may cause. Have a great day and best of luck.
查看全文
TEA1716計算ファイル こんにちは、TEA1716 IC用のExcel計算ファイルを探しています。これはTEAシリーズの他のチップの開発ツールに付属しているものに似ています。 TEA1716DB1255の開発ボードを使い、関連するドキュメントに従っていますが、もし存在すれば計算ファイルにもアクセスしたいです。 ご返信ありがとうございます。良い一日をお過ごしください! 電源ソリューション Re: TEA1716 сalculation file こんにちは、 TEA1716用のExcelベースの計算シート(「計算シートTEA1716ドラフトV1_4」)が存在し、元のオンライン設計ツールの代替として機能しています。元のオンライン設計ツールは現在は運用されていません。添付ファイルをご確認ください。 計算シートと並べて参照するために、TEA1716DB1255作業の主要な文書は以下の通りです: AN11179 — 計算例を含む詳細な設計ガイダンス UM10557 — TEA1716DB1255デモボードのドキュメント BRs、トーマス
查看全文
NFC Hi NXP team, Hello, I would like to ask, can the PCA943X connected to a coil directly obtain energy from the phone's NFC, or is another chip needed? Thank you! Re: NFC Hello ZHELI1,  You have to tuned the NFC antenna  using CP and CS to approx 13.56 MHz. For that, the Vector Network analyzer has to be used.  Cp defines the resonance frequency and Cs the system Q factor. The 0-resistors are just for disconecting the rectifier. This might be good for the development phase.  BR Tomas  Re: NFC Hello Tomas, Yes, I am using a mobile phone for reading. Hello, I would like to ask, in this diagram, is Cp used for resonance? Then what is Cs used for (energy storage?)? And is this 0-ohm resistor used for a jumper? I tested this device yesterday. After the antenna and capacitor resonated and matched, I aligned the mobile phone NFC with the coil, and then connected the output to a small LED light. This small light intermittently lights up, and the brightness is not high, not even as high as the energy provided by the NFC chip (10mW). Thank you Re: NFC Hello sir, Unfortunately, the use of PCA943x requires rectifier diodes as shared by Tomas (06-25-24). Additionally for the communication, the matching circuit needs the NTAG or a CRN120. Please request access to AN12641 for further hardware guidelines. Unfortunately, these are restricted to secure files, to get access to them, please follow this guide: https://www.nxp.com/docs/en/user-guide/nxp-secure-files-user-guide.pdf I hope this information may have been useful. Re: NFC Hello Fabian, I have already purchased the PCA943x through official channels, but I don't know which two pins connect to the coil and which two pins connect to the output. Is the usage similar to the NTG5 and NTH2111? Thank you Re: NFC Hello sir, Unfortunately, we don't have any other device that is able to deliver this amount of power besides the PCA943x. Regarding the I2C interface, please keep in mind that this is a slave device. On the other hand, CRN120 is also a T2T that can be read by the Smartphone. My apologies sir but, I believe there isn't a single solution device that will fill your needs. Re: NFC Hello ZHELI1 , I was just referring to your last post :  "Hello Tomas, I haven't heard from you for a long time. I hope you are well.I am not using NFC for communication, only for power supply, to power a rotating platform that requires 3V and 25mA of current. Thank you" For that scenario, you should be OK with the energy harvester I provided last time.  About NFC chips supporting build-in energy harvesting. We offer NTAG I2C (energy harvesting up to 10mW) and NTAG5 (energy harvesting up to 30mW).  But if your design requires NFC communication, you can extend the energy-harvesting circuit with the NTAG I2C as shown below:  Tomas_Parizek_0-1719379302870.png BTW. what should be your reader? Do you plan to use a mobile phone?  BR Tomas  Re: NFC Hello Fabian Thank you very much for your response. Here is my requirement: I need an NFC chip that can be connected to a coil I made to form a resonant circuit and use a mobile phone for both power transmission and data communication. It should be capable of outputting a current and voltage sufficient to drive a rotating disc (requires 3V voltage and 25mA current). It needs to support a sensor system (including an MCU and an accelerometer) to collect the acceleration information of the rotating disc. The collected acceleration data should be transmitted directly to a mobile phone via an I2C interface, meaning the NFC chip should support wireless reading. Therefore, I need an NFC chip with high power output. but other products currently have a maximum output of only 30mW(NTAG5 AND NT3H2111). Thank you! Re: NFC Hello sir, This is Fabian from customer support. Could you please help us by explaining a little more your application since we are a little confused about it?  From what we understand you are looking for a power harvesting application that is able to output around 80mW. Is it possible to decrease this output? Now regarding the data transfer you mentioned, over which interface are you looking to transfer data, a wired or through RF? Thank you very much for the clarification, please remember that the more information we have, the better our recommendation will be. Re: NFC Hello Tomas, This means I don't need to purchase any NFC chips, right? If I still need a little bit of data transfer, does it mean there are no suitable NFC chips available at the moment? Thank you Re: NFC Hello ZHELI1,  For your application, You can consider the following structure (see the attachment).  For the rectifier diodes, I would recommend PMEG3005AEA.  BR Tomas  Re: NFC Hello Tomas, I haven't heard from you for a long time. I hope you are well.I am not using NFC for communication, only for power supply, to power a rotating platform that requires 3V and 25mA of current. Thank you Re: NFC Hello ZHELI1 , NTAG5 can provide up to 30mW.  But do you need any NFC communication or only pure energy harvesting?  BR Tomas  Re: NFC Hello Tomas, Previously, I used the NT3H2111, which could provide around 10mW. However, for my scenario, I need about 80mW. Can the NTAG5 provide such a high power output? Thank you Re: NFC Hello ZHELI1,  Good question!  The PCA943X is mainly used in ecosystems including an MCU + NFC Tag. For your application, the NTAG5 (Link or Switch) might be used. The NTAG5 has a very nice capability of energy harvesting.  What is your power requirement?  BR Tomas  Re: NFC Hi Tomas, And the capacitors that are added to the NTAG (CS'...). What are them for? Which values should they have? Thanks.
查看全文
TEA1716 计算文件 您好,我正在寻找TEA1716 IC的Excel计算文件,类似于TEA系列其他芯片开发工具中提供的计算文件。我使用的是TEA1716DB1255开发板,并按照相关文档进行操作,但我也想获取该计算文件(如果存在的话)。谢谢您的回复,祝您一切顺利! 电源解决方案 Re: TEA1716 сalculation file 你好, TEA1716 有一个基于 Excel 的计算表(“TEA1716 计算表草案 V1_4”),它取代了不再运行的原始在线设计工具。请查收附件。 除计算表外,您完成 TEA1716DB1255 工作所需的关键文件如下: AN11179 — 详细设计指南,包括计算示例 UM10557 — TEA1716DB1255 演示板文档 BRs,托马斯
查看全文
NFC こんにちは、NXPチームの皆様、 こんにちは、お聞きしたいのですが、コイルに接続されたPCA943Xは、電話のNFCから直接エネルギーを取得できますか、それとも別のチップが必要ですか? ご回答をよろしくお願い申し上げます。 Re: NFC Hello ZHELI1,  CPとCSを使用してNFCアンテナを約13.56MHzに調整する必要があります。そのためには、ベクトルネットワークアナライザを使用する必要があります。 Cpは共振周波数を定義し、CsはシステムのQ係数を定義します。0抵抗器は、整流器を切り離すためだけのものです。これは開発フェーズに適しているかもしれません。 BR Tomas  Re: NFC こんにちはトーマス、 はい、携帯電話を使って読んでいます。こんにちは、この図でCpは共振に使用されていますか?では、セシウムは何に使われているのでしょうか(エネルギー貯蔵)?また、この0Ω抵抗はジャンパに使われるのでしょうか?昨日、このデバイスをテストしました。アンテナとコンデンサが共振して一致した後、携帯電話のNFCをコイルに合わせ、出力を小さなLEDライトに接続しました。この小さなライトは断続的に点灯し、明るさは高くなく、NFCチップによって提供されるエネルギー(10mW)ほど高くはありません。 ありがとうございます Re: NFC こんにちは、サー。 残念ながら、PCA943xの使用には、Tomas(06-25-24)が共有している整流ダイオードが必要です。 さらに、通信のために、マッチング回路にはNTAGまたはCRN120が必要です。ハードウェアに関する詳細なガイドラインについては、AN12641へのアクセスをリクエストしてください。 残念ながら、これらは安全なファイルに制限されているため、それらにアクセスするには、次のガイドに従ってください https://www.nxp.com/docs/en/user-guide/nxp-secure-files-user-guide.pdf この情報がお役に立てたでしょうか。 Re: NFC こんにちはファビアン、 私はすでに公式チャネルを通じて PCA943x を購入しましたが、どの 2 つのピンがコイルに接続され、どの 2 つのピンが出力に接続されているのかわかりません。NTG5やNTG NTH2111と使い方は似ていますか? ありがとうございます Re: NFC こんにちは、サー。 残念ながら、PCA943x以外にこの量の電力を供給できるデバイスは他にありません。I2Cインターフェースについては、スレーブデバイスであることに留意してください。一方、CRN120もスマートフォンで読み込めるT2Tです。 申し訳ありませんが、あなたのニーズを満たす単一のソリューションデバイスはないと思います。 Re: NFC Hello ZHELI1 , 私はちょうどあなたの最後の投稿を参照していました: 「こんにちは、トーマス。」 長い間、あなたから連絡が来ていません。お元気でいらっしゃいますように。私は通信にNFCを使用せず、3Vと25mAの電流を必要とする回転プラットフォームに電力を供給するための電源のみに使用しています。 ありがとうございました" そのシナリオでは、前回提供したエナジーハーベスターで問題ないはずです。 ビルトインエナジーハーベスティングをサポートするNFCチップについて。NTAG I2C(最大10mWの環境発電)とNTAG5(最大30mWの環境発電)を提供しています。 ただし、設計でNFC通信が必要な場合は、次に示すように、NTAG I2Cを使用してエナジーハーベスティング回路を拡張できます。 Tomas_Parizek_0-1719379302870.png ところで。あなたの読者は何であるべきですか?携帯電話を使う予定はありますか? BR Tomas  Re: NFC こんにちはファビアン ご回答いただき、誠にありがとうございました。これが私の要件です:共振回路を形成し、電力伝送とデータ通信の両方に携帯電話を使用するために作成したコイルに接続できるNFCチップが必要です。 回転ディスクを駆動するのに十分な電流と電圧を出力できる必要があります(3V電圧と25mAの電流が必要です)。 回転ディスクの加速度情報を収集するためのセンサーシステム(MCUと加速度計を含む)をサポートする必要があります。収集された加速度データは、I2Cインターフェースを介して携帯電話に直接送信する必要があるため、NFCチップはワイヤレス読み取りをサポートする必要があります。 したがって、高出力のNFCチップが必要です。しかし、他の製品は現在、最大出力が30mW(NTAG5およびNT3H2111)しかありません。 ありがとうございます! Re: NFC こんにちは、サー。 カスタマーサポートのファビアンです。 私たちはそれについて少し混乱しているので、あなたのアプリケーションをもう少し説明して助けていただけますか? 私たちが理解しているところによると、あなたは約80mWを出力できるパワーハーベスティングアプリケーションを探しています。この出力を減らすことは可能ですか? さて、あなたが言及したデータ転送に関して、有線またはRFを介して、どのインターフェースでデータを転送しようとしていますか? 説明していただきありがとうございます、情報が多ければ多いほど、推奨事項が改善することを忘れないでください。 Re: NFC こんにちはトーマス、 これは、NFCチップを購入する必要がないことを意味しますよね?それでも少しデータ転送が必要な場合、現時点では適切なNFCチップがないということですか? ありがとうございます Re: NFC Hello ZHELI1,  アプリケーションでは、次の構造を検討できます (添付ファイルを参照)。 整流ダイオードには、PMEG3005AEAをお勧めします。 BR Tomas  Re: NFC こんにちはトーマス、 長い間、あなたから連絡が来ていません。お元気でいらっしゃいますように。私は通信にNFCを使用せず、3Vと25mAの電流を必要とする回転プラットフォームに電力を供給するための電源のみに使用しています。 ありがとうございます Re: NFC Hello ZHELI1 , NTAG5 は最大 30mW を提供できます。しかし、NFC通信が必要ですか、それとも純粋なエネルギーハーベスティングのみが必要ですか? BR Tomas  Re: NFC こんにちはトーマス、 以前は、約10mWを提供できるNT3H2111を使用していました。ただし、私のシナリオでは、約80mWが必要です。NTAG5はこれほどの高出力を提供できますか? ありがとうございます Re: NFC Hello ZHELI1,  いい質問! このPCA943Xは、主にMCU+NFCタグなどのエコシステムで使用されます。アプリケーションによっては、NTAG5(リンクまたはスイッチ)を使用できます。NTAG5は、エネルギーハーベスティングの非常に優れた機能を備えています。 必要な電力はどれくらいですか? BR Tomas  Re: NFC こんにちは、トマスさん。 そしてNTAGに追加されるコンデンサ(CSなど)も含まれます。それらは何のためにあるのですか?彼らはどのような価値観を持つべきでしょうか? ありがとう。
查看全文
NFC 您好,NXP团队: 你好,请问一下PCA943X接上线圈可以直接从手机NFC获取能量吗,还是需要另外加一个芯片? 非常感谢! Re: NFC Hello ZHELI1,  您必须使用 CP 和 CS 将 NFC 天线调整至约 13.56 MHz。为此,必须使用矢量网络分析仪。 Cp 定义谐振频率,Cs 定义系统 Q 因子。0 电阻仅用于断开整流器。这可能对开发阶段有好处。 BR Tomas  Re: NFC 你好,Tomas, 是的,我正在用手机阅读。你好,请问一下,这个图中,Cp是用来共振的吗?那么 Cs 是用来做什么的(储能?)?这个 0 欧姆电阻器是用于跳线的吗?我昨天测试了这个设备。待天线和电容谐振匹配后,我将手机NFC与线圈对齐,然后将输出连接到一个小的LED灯。这盏小灯断断续续地亮着,而且亮度不高,甚至不如NFC芯片提供的能量(10mW)。 谢谢 Re: NFC 你好先生, 不幸的是,PCA943x 的使用需要整流二极管,正如 Tomas (06-25-24) 所分享的那样。 此外,对于通信,匹配电路需要 NTAG 或 CRN120。请请求访问 AN12641 以获取更多硬件指南。 不幸的是,这些仅限于安全文件,要访问它们,请遵循以下指南: https://www.nxp.com/docs/en/user-guide/nxp-secure-files-user-guide.pdf 我希望这些信息对您有所帮助。 Re: NFC 你好,Fabian, 我已经通过官方渠道购买了PCA943x,但是不知道哪两个引脚接线圈,哪两个引脚接输出。用法和NTG5、NTH2111类似吗? 谢谢 Re: NFC 你好先生, 不幸的是,除了 PCA943x 之外,我们没有任何其他设备能够提供这种功率。关于 I2C 接口,请记住这是一个从设备。另一方面,CRN120 也是一款可以通过智能手机读取的 T2T。 先生,很抱歉,但我相信没有一种解决方案设备可以满足您的需求。 Re: NFC Hello ZHELI1 , 我刚才提到了你的上一篇文章: “你好,托马斯, 好久没收到你的消息了。希望你一切都好。我使用NFC不是为了通讯,只是为了给一个需要3V电压和25mA电流的旋转平台供电。 谢谢” 对于这种情况,您应该可以使用我上次提供的能量收集器。 关于支持内置能量收集的 NFC 芯片。我们提供 NTAG I2C(能量收集高达 10mW)和 NTAG5(能量收集高达 30mW)。 但是如果您的设计需要 NFC 通信,您可以使用 NTAG I2C 扩展能量收集电路,如下所示: Tomas_Parizek_0-1719379302870.png 顺便问一下,你的读者应该是谁?您打算使用手机吗? BR Tomas  Re: NFC 你好,法比安 非常感谢您的回复。我的要求是这样的:我需要一个NFC芯片,它可以连接到我制作的线圈上,形成谐振电路,并使用手机进行电力传输和数据通信。 它应该能够输出足够的电流和电压来驱动旋转的圆盘(需要 3V 电压和 25mA 电流)。 需要支持传感器系统(包括MCU和加速度计)来采集旋转圆盘的加速度信息。收集到的加速度数据应该通过I2C接口直接传输到手机,这意味着NFC芯片应该支持无线读取。 因此我需要一个具有高功率输出的NFC芯片。但其他产品目前最大输出仅为30mW(NTAG5和NT3H2111)。 谢谢你! Re: NFC 你好先生, 我是客户支持部门的 Fabian。 由于我们对此有点困惑,您能否帮助我们进一步解释一下您的应用程序? 据我们了解,您正在寻找能够输出约 80mW 的能量收集应用。有可能减少这个产量吗? 现在关于您提到的数据传输,您希望通过哪个接口传输数据,有线还是通过射频? 非常感谢您的澄清,请记住,我们掌握的信息越多,我们的建议就越好。 Re: NFC 你好,Tomas, 这意味着我不需要购买任何 NFC 芯片,对吗?如果我仍然需要一点数据传输,是否意味着目前没有合适的 NFC 芯片可用? 谢谢 Re: NFC Hello ZHELI1,  对于您的应用程序,您可以考虑以下结构(参见附件)。 对于整流二极管,我推荐PMEG3005AEA 。 BR Tomas  Re: NFC 你好,托马斯, 我很久没有收到你的消息了。我希望你一切都好。我没有使用 NFC 进行通信,仅用于供电,为需要 3V 和 25mA 电流的旋转平台供电。 谢谢 Re: NFC Hello ZHELI1 , NTAG5 可提供高达 30mW 的功率。但是您是否需要任何 NFC 通信或仅需要纯能量收集? BR Tomas  Re: NFC 你好,托马斯, 之前我用的是NT3H2111,可以提供大约10mW。然而,就我的情况而言,我需要大约 80mW。NTAG5 能提供如此高的功率输出吗? 谢谢 Re: NFC Hello ZHELI1,  好问题! PCA943X 主要用于包含 MCU + NFC 标签的生态系统。对于您的应用,可以使用 NTAG5(链路或开关)。NTAG5 具有非常出色的能量收集能力。 您的电力需求是多少? BR Tomas  Re: NFC 嗨,托马斯, 以及添加到 NTAG (CS'...) 的电容。它们是做什么用的?他们应该具备哪些价值观? 谢谢。
查看全文
オンチップセキュアNVM(S32K314) HSE FW install for S32K3xx.pdfに記載されているセキュアNVMマッピング(FULL_MEM)は以下のとおりです。 HSEデータフラッシュは160KB、APPデータフラッシュは88KB、合計:160KB+88KB=248KB 羅京_0-1789619650388.png luojing_1-1789619740147.png ただし、S32K3XXRM.pdfに記載されているdflashの割り当ては以下のとおりです。 dflashの合計サイズは128KBです。 luojing_2-1789619854070.png なぜ2つの文書に記載されているDflashのサイズが異なるのですか? 注:私はHSEファームウェアバージョンHSE_FW_S32K344_0_2_55_0_S2502.exeを使用しています。 luojing_3-1789620886731.png Re: sRe: On-chip secure NVM (S32K314) これらの情報はすべてHSE-Bファームウェアリファレンスマニュアルに記載されています。 これは安全なファイルなので、すでに行ったことがない限り、以下の手順に従う必要があります。 https://www.nxp.com/docs/en/user-guide/nxp-secure-access-rights-registration.pdf より理解を深めるために、以下のリンクもご参照ください。 https://www.nxp.com/support/support/secure-access-rights:SEC-ACCESS Re: sRe: On-chip secure NVM (S32K314) S32K3xx 用の HSE FW インストールに関する PDF ファイルでは、HSE Pflash と dflash の範囲のみが指定されており、RAM の範囲は指定されていません。HSEが使用するRAMの範囲は? 開始地点の住所とサイズを教えてください。 それについて説明した特定の文書はありますか? Re: sRe: On-chip secure NVM (S32K314) セキュアデータフラッシュは、0x10016000 (FULL_MEMの場合) から始まり、168KB の容量を持ちます。これは全てのデリバティブ商品に共通する。 アプリケーションノートは最新ではありません。 Re: sRe: On-chip secure NVM (S32K314) 羅京_0-1789654909700.png HSE(FULL UMEM)のDflashサイズが160KBというのは間違いでしょうか?128KB-88KB=40KBになるべきでしょうか? sRe: On-chip secure NVM (S32K314) 以下に説明します。 davidtosenovjan_0-1789654479428.png
查看全文
S32DS v3.5 license expired, entitlement valid, no EXTEND button and Return not allowed Hello NXP support, My NXP account holds valid entitlement for S32DS v3.5, but the generated license expired. Fulfillment ID: 113445398 IDE: S32 Design Studio for S32 Platform v3.5 License Expiry: Aug 8, 2026 Entitlement Expiry: Sep 16, 2030 Machine ID: A5883F5CCBF60C6BECC55C5A0CC9D1C68DA192AD Current situation: 1. The license management page has no EXTEND button. 2. Return license is disabled, cannot release this fulfillment. 3. The entitlement is still valid until Sep 16, 2030. Could you help refresh this fulfillment license to entitlement expiry date Sep 16,2030? I have attached the screenshot of license list for your reference. Thanks. LicenseNotAllow.png Re: S32DS v3.5 license expired, entitlement valid, no EXTEND button and Return not allowed Thank you very much for your help. I have reactivated S32DS successfully. Re: S32DS v3.5 license expired, entitlement valid, no EXTEND button and Return not allowed Hi,  I returned old licenses, you should be able activate S32DS again with your old code. 
查看全文
关于 AFM907N PA 如果有的话,能否分享一下针对 915MHz 频率范围的调谐布局? Re: Regarding AFM907N PA 你好 lavanyaemsec 再会! 很遗憾地通知您,我们没有 915 MHz 的参考布局图;最接近的应该是…… AFM907N 760-870 MHz 参考电路设计文件 可以在AFM907N官方页面的设计资源部分找到。 对于可能由此导致的不便,我们深感抱歉。 祝你今天过得愉快,一切顺利。
查看全文
S32DS v3.5 许可证已过期,授权仍然有效,没有“延长”按钮,且不允许退货。 Hello NXP support, My NXP account holds valid entitlement for S32DS v3.5, but the generated license expired. Fulfillment ID: 113445398 IDE: S32 Design Studio for S32 Platform v3.5 License Expiry: Aug 8, 2026 Entitlement Expiry: Sep 16, 2030 Machine ID: A5883F5CCBF60C6BECC55C5A0CC9D1C68DA192AD Current situation: 1. The license management page has no EXTEND button. 2. Return license is disabled, cannot release this fulfillment. 3. The entitlement is still valid until Sep 16, 2030. Could you help refresh this fulfillment license to entitlement expiry date Sep 16,2030? I have attached the screenshot of license list for your reference. Thanks. LicenseNotAllow.png Re: S32DS v3.5 license expired, entitlement valid, no EXTEND button and Return not allowed 非常感谢您的帮助。我已经成功重新激活了S32DS。 Re: S32DS v3.5 license expired, entitlement valid, no EXTEND button and Return not allowed 你好, 我已经退回了旧的许可证,您应该可以使用之前的激活码再次激活S32DS。
查看全文
Request for TED-Kit 2 (OM6716) GUI Software Download Instructions Dear NXP Support Team, i am jwHyun, Could you please provide instructions on how to download the GUI software package, so that we can pass this along to our customer? We would appreciate your guidance on the registration/download process at your earliest convenience. Thank you in advance for your support. Re: Request for TED-Kit 2 (OM6716) GUI Software Download Instructions Replied you in another case. Thanks.
查看全文
MCXN947 HPDAC backport I am backporting the Zephyr nxp_hpdac driver to Zephyr 4.3 for an MCXN947-based board. The upstream driver does not use a device init callback. However, on Zephyr 4.3 the HPDAC does not work correctly unless I explicitly initialize the DAC2 clock, SPC analog modules and reset before using the peripheral. I added an nxp_hpdac_init() function which performs the following steps: CLOCK_SetClkDiv(kCLOCK_DivDac2Clk, 1U) CLOCK_AttachClk(kFRO_HF_to_DAC2) CLOCK_EnableClock(kCLOCK_Dac2) SPC_EnableActiveModeAnalogModules(SPC0, kSPC_controlDac2) SPC_EnableLowPowerModeAnalogModules(SPC0, kSPC_controlDac2) RESET_PeripheralReset(kDAC2_RST_SHIFT_RSTn) DAC14_DoSoftwareReset() DAC14_DoFIFOReset() SPC_EnableActiveModeAnalogModules(SPC0, kSPC_controlVref) These initialization steps were based on the MCXN947 reference manual and implemented using the corresponding MCUX SDK APIs. The init function is registered as the device init callback through DEVICE_DT_INST_DEFINE(). With these changes, the HPDAC works correctly. I also checked the Zephyr MCUX SYSCON clock-control driver and the mcux_lpc_syscon_clock.h bindings, but I could not find an HPDAC/DAC2 clock identifier or clock-control implementation for this peripheral, so I am currently using the MCUX SDK clock, SPC and reset APIs directly. My questions are: 1. Is this the correct approach when backporting the MCXN947 HPDAC driver? 2. In newer Zephyr versions, are these resources initialized somewhere else, or does the upstream nxp_hpdac driver assume that they have already been configured? 3. Is the HPDAC device init callback the correct place for this MCXN947-specific initialization, or should these steps be handled elsewhere in Zephyr? I have attached the complete backported driver for reference. Analog(ADC|CMP|DAC|OpAmps) Clock|Timers MCXN 回复: MCXN947 HPDAC backport Hi  @wesOS  1. Is this the correct approach when backporting the MCXN947 HPDAC driver? Yes, this is a reasonable and practical approach for the backport. If the required DAC2 clock, SPC analog modules, VREF, and reset resources are not initialized elsewhere in the Zephyr 4.3 environment, performing the initialization in the driver is necessary to ensure correct HPDAC operation. 2. In newer Zephyr versions, are these resources initialized somewhere else, or does the upstream nxp_hpdac driver assume that they have already been configured? HPDAC support has already been added upstream: https://github.com/zephyrproject-rtos/zephyr/pull/104642 However, I performed a quick verification using the current upstream implementation and observed that the DAC2 clock does not appear to be configured. For example, CLOCK_GetDacClkFreq(2) reports 0 Hz in my test environment, while the equivalent MCUX SDK example reports 48 MHz after the DAC clock is configured. Based on this observation, it appears that the current driver may be assuming that certain device resources have already been configured. Could you please double-check the clock configuration path on your side as well? I will also report this to our Zephyr team for further investigation and work with them to address the issue if a missing clock initialization bug is confirmed. 3. Is the HPDAC device init callback the correct place for this MCXN947-specific initialization, or should these steps be handled elsewhere in Zephyr? For a backport, placing this logic in the HPDAC device initialization callback is a practical and acceptable solution. That said, the MCXN947-specific DAC2 clock, SPC, VREF, and reset configuration should ideally be clearly isolated as SoC-specific functionality rather than embedded as generic HPDAC behavior. In the longer term, these resources would preferably be managed through Zephyr infrastructure such as clock, reset, or power-management frameworks where applicable. BR Harry 回复: MCXN947 HPDAC backport Thanks, I double-checked the DAC2 clock path on my MCXN947 setup. Before the HPDAC driver configures the clock: dac_nxp_hpdac: DAC2 clock before config: 0 Hz After: CLOCK_SetClkDiv(kCLOCK_DivDac2Clk, 1U); CLOCK_AttachClk(kFRO_HF_to_DAC2); CLOCK_EnableClock(kCLOCK_Dac2); I get: dac_nxp_hpdac: DAC2 clock after config: 48000000 Hz So I am seeing the same behavior on my side: the DAC2 clock is not configured before the HPDAC driver initialization. Your explanation about keeping the MCXN947-specific resource handling isolated also makes sense. What I am mainly trying to understand now is how you expect that initialization to be divided in the eventual upstream solution. For example, do you expect the DAC2 clock configuration, SPC/VREF setup and reset handling to each move into their corresponding Zephyr/SoC infrastructure, with `dac_nxp_hpdac.c` only keeping the generic HPDAC initialization? I am mainly asking so I can understand the intended ownership of each initialization step and keep the backport reasonably aligned with that direction. Thank you. BR  Ouassim 回复: MCXN947 HPDAC backport Hi @wesOS  Thanks for confirming your results. The fact that both of us observe DAC2 clock before config: 0 Hz and 48000000 Hz after the clock configuration strongly suggests that the DAC2 clock is not initialized before the HPDAC driver runs. I have already reported the bug fix to our internal Zephyr team. After looking further into the FRDM-MCXN947 implementation, I found that the existing DAC clock initialization is currently handled at the board level rather than in the DAC drivers themselves. zephyr/boards/nxp/frdm_mcxn947/board.c the function: void board_early_init_hook(void) performs the clock and SPC initialization for both DAC0 and DAC1: #if DT_NODE_HAS_STATUS_OKAY(DT_NODELABEL(dac0)) SPC_EnableActiveModeAnalogModules(SPC0, kSPC_controlDac0); CLOCK_SetClkDiv(kCLOCK_DivDac0Clk, 1u); CLOCK_AttachClk(kFRO_HF_to_DAC0); CLOCK_EnableClock(kCLOCK_Dac0); #endif #if DT_NODE_HAS_STATUS_OKAY(DT_NODELABEL(dac1)) SPC_EnableActiveModeAnalogModules(SPC0, kSPC_controlDac1); CLOCK_SetClkDiv(kCLOCK_DivDac1Clk, 1u); CLOCK_AttachClk(kFRO_HF_to_DAC1); CLOCK_EnableClock(kCLOCK_Dac1); #endif Based on the current implementation, my expectation would be to keep the solution consistent with the existing board design. In other words, the DAC2 clock initialization could be added to board_early_init_hook() alongside the existing DAC0/DAC1 initialization rather than placing board-specific clock setup into the generic HPDAC driver. BR Harry
查看全文
KW47B42ZB7 熔丝写入问题 Lu888_0-1788925610415.pngLu888_0-1788925610415.pngLu888_0-1788925610415.png 如图所示,我无法写入熔丝 0xa,但已成功写入熔丝 0x1f。我不知道为什么 Re: KW47B42ZB7 Fuse write issue 嗨@Christine_Li , 这是否意味着不能使用 blhost 的 熔丝-program 命令来对 kw47 的生命周期进行编程? Re: KW47B42ZB7 Fuse write issue 你好, @Lu888 感谢您向我们提交案件。 根据你提供的信息,我认为你可以执行 fuse-read 命令,这意味着你不在“OEM 打开后”状态下。 但根据: KW47SRM.pdf 原因如下: 下表中的 RO 表示用户不能使用 MGMT_FUSE_PROGRAM 来写入生命周期熔丝,而是可以使用 MGMT_ADVANCE_LIFECYCLE 或 MGMT_SET_RETURN_FA_MODE。 Christine_Li_0-1788944686191.pngChristine_Li_0-1788944686191.pngChristine_Li_0-1788944686191.png 如果要更改生命周期,可以使用以下命令: SB3 文件中的 MGMT_ADVANCE_LIFECYCLE。 Christine_Li_1-1788944712390.pngChristine_Li_1-1788944712390.pngChristine_Li_1-1788944712390.png 顺祝商祺! Christine。 Re: KW47B42ZB7 Fuse write issue 你好, @Lu888 请问您能否帮忙查看一下您主板目前的生命周期? 您可以在已经执行过先前命令的板上使用以下命令: Christine_Li_0-1789109774271.pngChristine_Li_0-1789109774271.png blhost -p com4 熔丝-read 0xa 4 我想知道你的主板是否已经更换为 OEM-Closed 版本。 因为我发现根据这篇AN: KW47 生命周期管理 你使用的命令是正确的,可以用来改变生命周期。这与我之前的评论相矛盾。 顺祝商祺! Christine。 Re: KW47B42ZB7 Fuse write issue 你好, @Lu888 你有没有机会看我之前的评论? 关于这个案子,我还能为您做些什么吗? 如果您在这个帖子里还有任何我可以帮忙的地方,请随时告诉我。 顺祝商祺! Christine。
查看全文
KW47B42ZB7 Fuse write issue Lu888_0-1788925610415.pngLu888_0-1788925610415.pngLu888_0-1788925610415.png As shown, I cannot write to fuse 0xa, but I have successfully written to fuse 0x1f. I don't know why Re: KW47B42ZB7 Fuse write issue Hi @Christine_Li , Does it mean that the fuse-program command of blhost cannot be used to program the lifecycle in kw47? Re: KW47B42ZB7 Fuse write issue Hi, @Lu888  Thanks for creating case to us. From your provided info, I think you can execute fuse-read command means you are not in "After OEM Open" state. But according to: KW47SRM.pdf The reason is: The RO in the following table indicates that user cannot use MGMT_FUSE_PROGRAM to write the lifecycle fuses, instead, he can use MGMT_ADVANCE_LIFECYCLE or MGMT_SET_RETURN_FA_MODE. Christine_Li_0-1788944686191.pngChristine_Li_0-1788944686191.pngChristine_Li_0-1788944686191.png If you want to change lifecycle, you can use this command: MGMT_ADVANCE_LIFECYCLE in SB3 file. Christine_Li_1-1788944712390.pngChristine_Li_1-1788944712390.pngChristine_Li_1-1788944712390.png Best regards, Christine. Re: KW47B42ZB7 Fuse write issue Hi, @Lu888  Can you please help to check what is your board's lifecycle currently? You can use below command on your board which already been executed previous commands: Christine_Li_0-1789109774271.pngChristine_Li_0-1789109774271.png blhost -p com4 fuse-read 0xa 4 I want to know whether your board already been changed into OEM-Closed. Because I found  that according to this AN: KW47 Managing Lifecycles you are using correct commands to change lifecycle. Which is conflict with my previous comment. Best regards, Christine. Re: KW47B42ZB7 Fuse write issue Hi, @Lu888  Did you get any chance to read my previous comment? Anything else I can do for you on this case? Please do not hesitate to let me know if still have any thing I can do for you on this thread. Best regards, Christine.
查看全文
refence configuration path In Simulink, when configuring the hardware, I am trying to change the directory for the reference configuration to a relative path. Simulink -> HW-Settings -> Hardware Implementation -> Target hardware resources -> Referenced Configuration Reference Configuration Path = '.\generated\referenced_config' Unfortunately, it is not possible to enter a relative path here. Nor have I so far been able to set the path via a MATLAB script. Although the script appears to set the path in CoderTargetData, it is not actually applied. Either the old path remains active, or an empty path is applied. Is there a way to set a relative path for the reference configuration? Re: refence configuration path Hi, @AlexG124, Thanks for the details. Could you please help us and let us know what are the MBDT toolbox version, as well as the MATLAB version that you are currently using? In case you are using S32K3 toolbox, there is a model example showcasing the referenced configuration workflow, under model_ref/s32k3xx_refconfig_s32ct folder. Here you will find a MATLAB script called s32k3xx_refconfig_update_paths_callback.m that could help in achieving your goal. It will be also helpful if you could let us know more details on your referenced configuration way of working, usage and application flow. Best regards, Dragos
查看全文