Multi Source Translation Content

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Multi Source Translation Content

讨论

排序依据:
S32 デザインスタジオのライセンスが切れました こんにちは、 私のS32デザインスタジオライセンスはもうすぐ期限切れになります。 免許の更新は可能ですか? ライセンスコードは085B-C474-AA78-FC99です。 ご回答をお待ちしています。 Re: s32 design studio license expired こんにちは、 お客様のS32DSライセンスが延長されました。 Re: s32 design studio license expired こんにちは、 今あなたのアカウントを確認したところ、ライセンスは2030年まで有効です。ライセンスが本当に期限切れでないまで待つか、既存のライセンスを返却して古いコードで再度有効化することもできます。 Re: s32 design studio license expired こんにちは、 ssong_0-1789444671642.png まだ延長されていないようです。もう一度確認してもらえますか?ありがとう。
查看全文
S32 设计工作室平台 + SW32G2 + RTD 版本选择 我参考了《S32G-VNP-RDB2 软件启用指南》,建议的软件版本为 SW32G2_S32DS_3.4.0_D2012.zip + S32DS.3.4_b201217_win32.x86_64.exe + 实时驱动程序 S32_RTD_4.4_1.0.0_HF01_D2102_DS_Updatesite.zip。 但我实际下载的是 S32DS.3.4_b201217_win32.x86_64.exe +SW32G2_S32DS_3.4.1_D2104.zip +SW32G_RTD_4.4_3.0.2_HF01_DS_updatesite_D2204.zip。 当我尝试添加新的 RGB LED 灯并打开外设工具时,它会显示“外设:[SDK] 更新代码失败 - 代码生成失败”。我不确定不同的软件版本组合是否会导致这些错误。 Re: S32 Design Studio Platform + SW32G2 + RTD version selection 你好, guang1994 我会内部回复你。 BR 乔伊
查看全文
S32K358 about Cache operation 我在S32DS 中编写S32K358 的程序,建立OTA 升级程序需要操作内部FLASH,当调用上述函数时,我能够编译通过,但是CTRL+鼠标左键却无法找到上述函数,这是正常现象吗?  屏幕截图 2026-09-15 141928.png 屏幕截图 2026-09-15 141953.png Re: S32K358 about Cache operation 嗨@sunshine88 , 您能尝试重建索引吗? danielmartynek_0-1789469464382.png 谢谢! BR,丹尼尔
查看全文
imx95 AHAB SGKサポート こんにちは、 私はi.MX95でAHABのセキュアブートサポートに取り組んでおり、サポートされている署名キーの階層を確認したいと思っています。 i.MX9の一部のバリアント、例えばi.MX93は現在、AHABコンテナ署名のためのサブリグネーミングキー(SGK)をサポートしておらず、SRKベースの署名のみがサポートされていると理解しています。ここで説明しています: https://community.nxp.com/t5/i-MX-Processors/imx93-AHAB-SGK-support/td-p/2181212 i.MX95が、SRK証明書にCAフラグを付けた下位キー(SGK)を使ってAHABブートコンテナに署名できるのか、それとも現在リリースされたELEファームウェアが直接SRKベースの署名のみをサポートしているのか、確認していただけますか? SGKがサポートされている場合、サポートはi.MX95シリコンリビジョン、ELEファームウェアバージョン、AHABコンテナフォーマット、またはBSPリリースによって異なるのかも教えていただけますか? Re: imx95 AHAB SGK support どなたか助けていただけますか? Re: imx95 AHAB SGK support こんにちは、 返信が遅れて申し訳ございません。もしまだお役に立つようでしたら、チームに確認したところ、AおよびBのどちらのシリコンリビジョンでもサポートされていないことが分かりました。 よろしくお願いいたします。 アルド。 Re: imx95 AHAB SGK support ご説明ありがとうございます、@AldoG さん。
查看全文
imx95 AHAB SGK support Hello, I am working on AHAB secure boot support on i.MX95 and would like to confirm the supported signing-key hierarchy. I understand that some i.MX9 variants, such as i.MX93, currently do not support subordinate signing keys (SGK) for AHAB container signing, and only SRK-based signing is supported, as discussed here: https://community.nxp.com/t5/i-MX-Processors/imx93-AHAB-SGK-support/td-p/2181212 Could you please confirm whether i.MX95 supports signing AHAB boot containers using subordinate keys (SGK), with the SRK certificate carrying the CA flag, or whether the current released ELE firmware supports only direct SRK-based signing? If SGK is supported, could you also clarify whether support depends on the i.MX95 silicon revision, ELE firmware version, AHAB container format, or BSP release? Re: imx95 AHAB SGK support Can anyone help me here? Re: imx95 AHAB SGK support Thanks for the clarification @AldoG. Re: imx95 AHAB SGK support Hello, Please do accept my apologize for the lack of response, if it is still useful, after confirmation with team, it is not supported on either A or B silicon revisions. Best regards/Saludos, Aldo.
查看全文
問題: IMX_SEC_ENCLAVE の依存関係と解放後使用を修正する Hello これは、GitHub のこのプルリクエストのフォローアップです。 提供されたパッチは最終的に適用されなかったようで、lf-6.18.y には含まれていません。 Kconfigコミットは、NVMEM_IMX_OCOTP_SCUがmである場合にエンクレイブドライバがyになれないようにするためで、プローブのディフェースを回避するために必要です。 そうしないと、こうなります。 root@colibri-imx8x-14985125:~# dmesg -l err [ 1.708145] rtc-ds1307 1-0068: hctosys: unable to read the hardware clock [ 2.072996] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 2.078636] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 2.084513] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 2.111555] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 2.117209] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 2.123110] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 2.141671] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 2.147303] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 2.153200] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 2.171418] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 2.177065] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 2.182929] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 5.744448] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 5.750217] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 5.756186] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 5.877660] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 5.888247] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 5.894232] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 10.324138] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 10.349783] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 10.374692] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 11.731697] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 11.738134] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 11.747692] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 12.284910] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 12.295720] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 12.307723] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 12.410541] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 12.426771] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 12.443446] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 12.644550] debugfs: '5f1a0000.phy' already exists in 'regmap' [ 12.655906] debugfs: '5f1a0000.phy' already exists in 'regmap' [ 12.670039] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 12.688813] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 12.696063] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 12.765923] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 12.775810] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 12.786887] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 12.839515] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 12.847285] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 12.853801] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 12.936721] nvmem imx-scu-ocotp0: cell mac raw len 6 unaligned to nvmem word size 4 [ 12.951328] nvmem imx-scu-ocotp0: cell mac raw len 6 unaligned to nvmem word size 4 [ 13.708903] genpd_provider mu_a1: failed to power off resource 214 ret -22 [ 16.701904] Bluetooth: hci0: unexpected event for opcode 0x0000 root@colibri-imx8x-14985125:~# 2回目のコミットではドライバにリファクタリングが行われており、NXPが対応しているかはわかりません コミット9703dfecc735(「LF-15802: ドライバ: ファームウェア: imx: SEドライバーの削除を修正」) SEチームに確認してもらえますか? よろしくお願いいたします フランツ Re: ISSUE: fix dependency for IMX_SEC_ENCLAVE and use-after-free こんにちは、 まだ解決していないようですので、社内のソフトウェアチームに確認して確認します。 よろしくお願いいたします。 アルド。
查看全文
S32 Design Studio for ARM 2.2 cannot be activated. Install S32 Design Studio for ARM 2.2: 1. Selecting "online" during activation results in the error shown in Figure 1. Using https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/Troubleshooting-Activation-fails-with-error-message-FNP-ERROR-0/ta-p/1123259 results in the error shown in Figure 2. However, my computer's FlexNet service... Licensing Service in startup state 2. After following the official website's steps exactly when using offline activation, I encountered the error shown in Figure 3. How can I correctly activate and install this version of the software? Re: 安装S32 Design Studio for ARM 2.2无法激活 I followed the steps exactly, but it still doesn't work. Re: 安装S32 Design Studio for ARM 2.2无法激活 Hi @aether  The FNP Error 20 is usually related to components not being installed correctly or not being accessible to the current user. Could you please try the following: Fully uninstall S32DS for ARM v2.2 and remove any remaining files in C:\NXP\S32DS_ARM_v2.2. Back up and clear the contents of the hidden folder C:\ProgramData\FLEXnet\. Re-download and install the base S32DS for ARM v2.2 package (without Update 2). Run the installer with Administrator privileges and ensure that antivirus or security software is not blocking. BR, VaneB Re: 安装S32 Design Studio for ARM 2.2无法激活 Hi @aether  Could you please share the installation log file (.log)? It should be located under: C:\NXP\S32DS_ARM_v2.2\_S32 Design Studio for ARM Version 2.2_installation\Logs
查看全文
S32 Design Studio Platform + SW32G2 + RTD version selection I refer to the S32G-VNP-RDB2 SOFTWARE ENABLEMENT GUIDE, the suggested software version was SW32G2_S32DS_3.4.0_D2012.zip + S32DS.3.4_b201217_win32.x86_64.exe + Real Time Drivers S32_RTD_4.4_1.0.0_HF01_D2102_DS_Updatesite.zip.  But I actually download S32DS.3.4_b201217_win32.x86_64.exe +SW32G2_S32DS_3.4.1_D2104.zip +SW32G_RTD_4.4_3.0.2_HF01_DS_updatesite_D2204.zip.  When I want to new the Light Up RGB LED and open peripherals tool, It will show "Peripherals: [SDK] Failed to update code - Code generation failed“. I'm not sure if the different software version combination causing these error. Re: S32 Design Studio Platform + SW32G2 + RTD version selection Hi, guang1994 I will reply to you internally. BR Joey
查看全文
ISSUE: fix dependency for IMX_SEC_ENCLAVE and use-after-free Hello This is a follow up from this PR on github. It seems that the patches provided were at the end not applied as it's not present in lf-6.18.y. The Kconfig commit is needed to make sure that the Enclave driver cannot be y when NVMEM_IMX_OCOTP_SCU is m, thus avoiding probe defers. Otherwise you get this: root@colibri-imx8x-14985125:~# dmesg -l err [ 1.708145] rtc-ds1307 1-0068: hctosys: unable to read the hardware clock [ 2.072996] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 2.078636] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 2.084513] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 2.111555] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 2.117209] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 2.123110] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 2.141671] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 2.147303] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 2.153200] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 2.171418] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 2.177065] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 2.182929] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 5.744448] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 5.750217] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 5.756186] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 5.877660] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 5.888247] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 5.894232] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 10.324138] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 10.349783] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 10.374692] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 11.731697] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 11.738134] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 11.747692] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 12.284910] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 12.295720] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 12.307723] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 12.410541] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 12.426771] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 12.443446] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 12.644550] debugfs: '5f1a0000.phy' already exists in 'regmap' [ 12.655906] debugfs: '5f1a0000.phy' already exists in 'regmap' [ 12.670039] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 12.688813] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 12.696063] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 12.765923] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 12.775810] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 12.786887] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 12.839515] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 12.847285] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 12.853801] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 12.936721] nvmem imx-scu-ocotp0: cell mac raw len 6 unaligned to nvmem word size 4 [ 12.951328] nvmem imx-scu-ocotp0: cell mac raw len 6 unaligned to nvmem word size 4 [ 13.708903] genpd_provider mu_a1: failed to power off resource 214 ret -22 [ 16.701904] Bluetooth: hci0: unexpected event for opcode 0x0000 root@colibri-imx8x-14985125:~# On the second commit submitted, there has been some refactoring in the driver and I'm not sure if this has been addressed by NXP with commit 9703dfecc735 ("LF-15802: drivers: firmware: imx: Fix the SE driver remove") Could  maybe the SE team confirm? kinds regards Franz Re: ISSUE: fix dependency for IMX_SEC_ENCLAVE and use-after-free Hello, I see that this has not been solved yet, will check with internal software team and confirm about this. Best regards/Saludos, Aldo.
查看全文
imx95 AHAB SGK 支持 你好, 我正在研究 i.MX95 上的 AHAB 安全启动支持,并想确认支持的签名密钥层次结构。 我了解到,某些 i.MX9 变体(例如 i.MX93)目前不支持 AHAB 容器签名的从属签名密钥 (SGK),而仅支持基于 SRK 的签名,如这里所讨论的: https://community.nxp.com/t5/i-MX-Processors/imx93-AHAB-SGK-support/td-p/2181212 请问 i.MX95 是否支持使用带有 CA 标志的 SRK 证书对 AHAB 启动容器进行从属密钥 (SGK) 签名,还是当前发布的 ELE 固件仅支持直接基于 SRK 的签名? 如果支持 SGK,能否也说明一下,支持是否取决于 i.MX95 芯片版本、ELE 固件版本、AHAB 容器格式或 BSP 版本? Re: imx95 AHAB SGK support 请问有人能帮帮我吗? Re: imx95 AHAB SGK support 你好, 对于未能及时回复您,我深表歉意。如果该功能仍然有用,经与团队确认,A 或 B 芯片版本均不支持该功能。 此致敬礼/Saludos, 阿尔多。 Re: imx95 AHAB SGK support 感谢@AldoG的澄清。
查看全文
S32 Design Studio プラットフォーム + SW32G2 + RTD バージョン選択 私はS32G-VNP-RDB2 ソフトウェア イネーブルメント ガイドを参照しており、推奨されているソフトウェアバージョンはSW32G2_S32DS_3.4.0_D2012.zip+R S32DS.3.4_b201217_win32.x86_64.exe+リアルタイム・ドライバ S32_RTD_4.4_1.0.0_HF01_D2102_DS_Updatesite.zipでした。 しかし、実際にダウンロードしたのは S32DS.3.4_b201217_win32.x86_64.exe +SW32G2_S32DS_3.4.1_D2104.zip +SW32G_RTD_4.4_3.0.2_HF01_DS_updatesite_D2204.zip です。 RGBLEDを点灯してペリフェラルを起動しようとすると、「ペリフェラル:[SDK] コード更新に失敗 - コード生成に失敗」と表示されます。ソフトウェアのバージョンが違うからこそエラーが原因なのかは分かりません。 Re: S32 Design Studio Platform + SW32G2 + RTD version selection こんにちは、 guang1994 社内で返信させていただきます。 BR ジョーイ
查看全文
问题:修复 IMX_SEC_ENCLAVE 和释放后使用依赖项。 Hello 这是对 GitHub 上这个 PR的后续跟进。 提供的补丁似乎最终没有应用,因为 lf-6.18.y 中没有这些补丁。 需要 Kconfig 提交来确保当 NVMEM_IMX_OCOTP_SCU 为 m 时 Enclave 驱动程序不能为 y,从而避免探测延迟。 否则你会看到这样的结果: root@colibri-imx8x-14985125:~# dmesg -l err [ 1.708145] rtc-ds1307 1-0068: hctosys: unable to read the hardware clock [ 2.072996] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 2.078636] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 2.084513] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 2.111555] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 2.117209] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 2.123110] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 2.141671] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 2.147303] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 2.153200] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 2.171418] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 2.177065] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 2.182929] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 5.744448] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 5.750217] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 5.756186] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 5.877660] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 5.888247] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 5.894232] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 10.324138] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 10.349783] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 10.374692] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 11.731697] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 11.738134] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 11.747692] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 12.284910] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 12.295720] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 12.307723] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 12.410541] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 12.426771] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 12.443446] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 12.644550] debugfs: '5f1a0000.phy' already exists in 'regmap' [ 12.655906] debugfs: '5f1a0000.phy' already exists in 'regmap' [ 12.670039] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 12.688813] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 12.696063] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 12.765923] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 12.775810] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 12.786887] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 12.839515] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 12.847285] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 12.853801] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 12.936721] nvmem imx-scu-ocotp0: cell mac raw len 6 unaligned to nvmem word size 4 [ 12.951328] nvmem imx-scu-ocotp0: cell mac raw len 6 unaligned to nvmem word size 4 [ 13.708903] genpd_provider mu_a1: failed to power off resource 214 ret -22 [ 16.701904] Bluetooth: hci0: unexpected event for opcode 0x0000 root@colibri-imx8x-14985125:~# 在提交的第二个版本中,驱动程序进行了一些重构,我不确定NXP是否已经解决了这个问题。 提交 9703dfecc735(“LF-15802:驱动程序:固件:imx:修复 SE 驱动程序移除”) SE团队能否确认一下? 此致敬礼 弗朗茨 Re: ISSUE: fix dependency for IMX_SEC_ENCLAVE and use-after-free 你好, 我看到这个问题还没有解决,我会和内部软件团队确认一下。 此致敬礼/Saludos, 阿尔多。
查看全文
S32K358 about Cache operation I am writing an S32K358 program in S32DS. To create an OTA upgrade program, I need to manipulate the internal FLASH. When I call the above function, I can compile it successfully, but I cannot find the above function by pressing CTRL+left mouse button. Is this normal? Screenshot 2026-09-15 141928.png Screenshot 2026-09-15 141953.png Re: S32K358 about Cache operation Hi @sunshine88, Can you try rebuilding the index? danielmartynek_0-1789469464382.png Thank you, BR, Daniel
查看全文
S32K358 キャッシュ操作について S32DSでS32K358プログラムを作成しています。OTAアップグレードプログラムを作成するために、内部FLASHを操作する必要があります。上記の関数を呼び出すとコンパイルは正常に完了しますが、Ctrlキーを押しながらマウスの左ボタンを押しても上記の関数が見つかりません。これは正常な動作でしょうか? スクリーンショット 2026-09-15 141928.png スクリーンショット 2026-09-15 141953.png Re: S32K358 about Cache operation こんにちは@sunshine88 さん インデックスを再構築してみることはできますか? danielmartynek_0-1789469464382.png ありがとうございました。 BR、ダニエル
查看全文
S32K312用RTDの取り付け 私はS32K312のために、S32 Design Studio v 3.6.6 で以下の開発環境を設定しようとしています。 1. SW32K3_S32M27x_RTD_R23-11_7.0.1_D2603_DesignStudio_updatesite.zip をダウンロードしました。 2. S32 Design Studio 3.6.6で「S32拡張とアップデート」を開いたWindows 11で動作し、S32K3のリアルタイム・ドライバをインストールしました(示す通り): durga_choudhury_0-1788877584959.pngdurga_choudhury_0-1788877584959.pngdurga_choudhury_0-1788877584959.pngdurga_choudhury_0-1788877584959.pngdurga_choudhury_0-1788877584959.pngdurga_choudhury_0-1788877584959.pngdurga_choudhury_0-1788877584959.pngdurga_choudhury_0-1788877584959.pngdurga_choudhury_0-1788877584959.png 3. IDEを再起動するよう促されたら(PCの再起動も試しました) これではK3ファミリのサポートが見当たりません。「新規プロジェクト」ダイアログには、このオプションは表示されません。 durga_choudhury_1-1788877756997.pngdurga_choudhury_1-1788877756997.pngdurga_choudhury_1-1788877756997.pngdurga_choudhury_1-1788877756997.pngdurga_choudhury_1-1788877756997.pngdurga_choudhury_1-1788877756997.pngdurga_choudhury_1-1788877756997.pngdurga_choudhury_1-1788877756997.pngdurga_choudhury_1-1788877756997.png 下記のように「S32K3XX」ドライバーをインストールしようとすると: durga_choudhury_2-1788877862245.pngdurga_choudhury_2-1788877862245.pngdurga_choudhury_2-1788877862245.pngdurga_choudhury_2-1788877862245.pngdurga_choudhury_2-1788877862245.pngdurga_choudhury_2-1788877862245.pngdurga_choudhury_2-1788877862245.pngdurga_choudhury_2-1788877862245.pngdurga_choudhury_2-1788877862245.png 以下のようなエラーが表示されます。 durga_choudhury_3-1788877910412.pngdurga_choudhury_3-1788877910412.pngdurga_choudhury_3-1788877910412.pngdurga_choudhury_3-1788877910412.pngdurga_choudhury_3-1788877910412.pngdurga_choudhury_3-1788877910412.pngdurga_choudhury_3-1788877910412.pngdurga_choudhury_3-1788877910412.pngdurga_choudhury_3-1788877910412.png この一連のプロセスをS32DS v.6.2で繰り返すと少し改善されました。「新しいプロジェクト」ダイアログにK312のオプションが表示されていますが、SDKは表示されていません。 durga_choudhury_4-1788878190320.pngdurga_choudhury_4-1788878190320.pngdurga_choudhury_4-1788878190320.pngdurga_choudhury_4-1788878190320.pngdurga_choudhury_4-1788878190320.pngdurga_choudhury_4-1788878190320.pngdurga_choudhury_4-1788878190320.pngdurga_choudhury_4-1788878190320.pngdurga_choudhury_4-1788878190320.png 私は何が間違っているのでしょうか? Re: Installing RTD for S32K312 こんにちは、 @VaneBさん 残念ながら、S32DS 3.6.6 には同等の機能がありません。また、RTDのバージョンを7.0.1から6.0.0にダウングレードしてみました。 3.6.6で動作する特定のバージョンはありますか? Re: Installing RTD for S32K312 こんにちは、 @durga_choudhuryさん このスクリーンショットは私のS32DS 3.6.10のものです。インストール;しかし、あなたのIDEでも同様のセットアップが見られるはずです。 VaneB_0-1788893776567.pngVaneB_0-1788893776567.pngVaneB_0-1788893776567.pngVaneB_0-1788893776567.pngVaneB_0-1788893776567.pngVaneB_0-1788893776567.pngVaneB_0-1788893776567.pngVaneB_0-1788893776567.pngVaneB_0-1788893776567.png また、あなたが共有してくれたスクリーンショットを見る限り、RTD 7.0.1をインストールできているのがわかります。RTD 7.0.1はS32K3開発パッケージに依存しているため、すでにそのパッケージがインストールされている可能性が高いです。 Re: Installing RTD for S32K312 こんにちは、 @VaneBさん あなたのコメントについて、もう少し詳しく説明してください。 S32K1xx用の「開発パッケージ」がインストールされているのを確認しました(これも私が使っているMCUファミリです): durga_choudhury_0-1788891225434.pngdurga_choudhury_0-1788891225434.pngdurga_choudhury_0-1788891225434.pngdurga_choudhury_0-1788891225434.pngdurga_choudhury_0-1788891225434.pngdurga_choudhury_0-1788891225434.pngdurga_choudhury_0-1788891225434.pngdurga_choudhury_0-1788891225434.pngdurga_choudhury_0-1788891225434.png しかし、K3には同様のものは見当たらない。 では、どうやってインストールすればいいのでしょうか?繰り返しますが、これまでに私がやったことは以下の通りです: 1. SW32K3_S32M27x_RTD_R23-11_7.0.1_D2603_DesignStudio_updatesite.zip をダウンロードしました 2. S32 DS v 3.6.6にアップデートサイトとして追加しました。 3. 以下のものをインストールしました。 durga_choudhury_1-1788891394005.pngdurga_choudhury_1-1788891394005.pngdurga_choudhury_1-1788891394005.pngdurga_choudhury_1-1788891394005.pngdurga_choudhury_1-1788891394005.pngdurga_choudhury_1-1788891394005.pngdurga_choudhury_1-1788891394005.pngdurga_choudhury_1-1788891394005.pngdurga_choudhury_1-1788891394005.png Re: Installing RTD for S32K312 こんにちは、 @durga_choudhuryさん S32DS 3.6.6からインストール時には、S32K3開発パッケージがインストールされていないようです。 S32DS 3.6.2に関して、RTD 7.0.1はS32DS 3.6.4を使用して開発および検証されたことにご注意ください。したがって、S32DS 3.6.4 の使用をお勧めします。または、互換性を確保し、潜在的な問題を回避するために、より新しいリリースを使用してください。 他に確認すべき点として、ツールチェーンが挙げられます。プロジェクトを作成する際は、NXP GCC 10.2.0がインストールされ、プロジェクトツールチェーンとして選択されていることを確認してください。 BR、VaneB Re: Installing RTD for S32K312 こんにちは、 @durga_choudhuryさん 私の環境では、RTD 7.0.0を使用しています。S32DS 3.6.6と共にインストールされました。しかし、前述のとおり、これらのバージョン間でセットアップ方法が非常に似ているため、RTD 7.0.1は問題なく動作するはずです。 設置の詳細を教えていただけますか? Re: Installing RTD for S32K312 こんにちは、 @VaneBさん サポートありがとうございます。URLをもう一度確認してもらえますか?この方法でアップデートしようとすると、S32 DS から次のようなエラーが発生します。 durga_choudhury_0-1789063889394.pngdurga_choudhury_0-1789063889394.pngdurga_choudhury_0-1789063889394.pngdurga_choudhury_0-1789063889394.pngdurga_choudhury_0-1789063889394.pngdurga_choudhury_0-1789063889394.pngdurga_choudhury_0-1789063889394.png 例えば、RESTタイプのアプリケーションでアクセスしようとすると、wgetを実行すると、HTTPエラー404(見つかりません)が発生します。 それはNXP内部の問題かもしれません(つまり、(公開サーバーではない)? Re: Installing RTD for S32K312 こんにちは、 @durga_choudhuryさん 以下の方法を試していただけますか?S32DSでは「新しいソフトウェアをインストールする→ヘルプ」へ行きます...これによりインストールウィンドウが開きます。「作業対象:」フィールドに、次の更新サイトを入力します。 https://www.nxp.com/lgfiles/updates/Eclipse/S32DS_3.6 利用可能なアップデートの一覧が、以下に示すような形で表示されます。リストにS32 Design Studio S32K3xx開発パッケージが見つかるか確認し、インストールを試してみてください。 VaneB_0-1789057150680.pngVaneB_0-1789057150680.pngVaneB_0-1789057150680.pngVaneB_0-1789057150680.pngVaneB_0-1789057150680.pngVaneB_0-1789057150680.png パッケージが表示されなかったりインストールが失敗した場合は、最新のS32DSバージョンへのアップデートをおすすめします。現在のインストール環境に一部のコンポーネントが不足しているか、インストール/アップデート中に何らかの破損が発生した可能性があります。 Re: Installing RTD for S32K312 こんにちは、 @VaneBさん 以下に、私が試した2つのファイルを示します(どちらも同じ問題が発生しました)。 durga_choudhury_0-1789048352154.pngdurga_choudhury_0-1789048352154.pngdurga_choudhury_0-1789048352154.pngdurga_choudhury_0-1789048352154.pngdurga_choudhury_0-1789048352154.png S32DSに関する情報は以下のとおりです。 durga_choudhury_1-1789048467186.pngdurga_choudhury_1-1789048467186.pngdurga_choudhury_1-1789048467186.pngdurga_choudhury_1-1789048467186.pngdurga_choudhury_1-1789048467186.png 以下に、インストール手順の詳細を、1枚のスクリーンショットに収まる範囲で示します。他に何か情報が必要ですか? durga_choudhury_2-1789048687291.pngdurga_choudhury_2-1789048687291.pngdurga_choudhury_2-1789048687291.pngdurga_choudhury_2-1789048687291.pngdurga_choudhury_2-1789048687291.png Re: Installing RTD for S32K312 こんにちは、 @VaneBさん 残念ながら、私の環境では動作しません。 durga_choudhury_0-1789083559046.pngdurga_choudhury_0-1789083559046.pngdurga_choudhury_0-1789083559046.pngdurga_choudhury_0-1789083559046.png Re: Installing RTD for S32K312 こんにちは、 @durga_choudhuryさん 提供されたリンクは通常のウェブアドレスではないことにご注意ください。これはS32DSが利用可能なソフトウェアパッケージやアップデートにアクセスするためのアップデートサイトに対応しています。 更新サイトの完全なリストを表示するには、S32DS拡張機能と更新ウィンドウを開き、「サイトの管理」を選択します。そこにはIDEが認識するすべての更新サイトが見つかります。 Re: Installing RTD for S32K312 こんにちは、 @durga_choudhuryさん 別のマシンでテストしていただけますか? また、アップデートサイトへのアクセスを妨げるファイアウォールやプロキシ、セキュリティポリシーがないかITチームに確認する価値があります。 Re: Installing RTD for S32K312 これは確かに、当社のプロキシサーバーに何らかの問題があるようです。企業ネットワーク外のコンピュータで動作します。 サポートありがとうございます。
查看全文
KW45:编程/调试期间间歇性线路确认故障和闪存擦除失败 大家好, 我目前正在使用基于 KW45 的定制板,在固件编程和调试过程中遇到了间歇性问题。 我分别使用 SEGGER J-Link 和 NXP MCU-Link 调试探针测试了该电路板,两种探针都出现了该问题。 定制板的启动配置与 KW45 EVK 相同,JTAG/SWD 连接也已检查,看起来是正确的。 然而,我发现出现了以下情况: 当我尝试转储或编程一个已知可以正常运行的应用程序时: 有时应用程序编程成功,但在编程或启动调试会话后,设备最终会跳转到故障地址。 调试器随后在该位置停止。 在某些编程或转储尝试过程中,我收到 Wire ACK 故障。 MCUXpresso 在其他时候报道: 执行 MI 命令时出错 我还尝试使用 MCUXpresso 擦除闪存,但闪存擦除操作本身并未成功完成。 已执行的检查 已检查 JTAG/SWD 连接,连接似乎正常。 我们使用 SEGGER J-Link 和 NXP MCU-Link 调试探针测试了该问题。 已将启动配置与 KW45 EVK 进行了比较。 我使用一个已知可以正常运行的应用程序进行测试。 该问题是间歇性的:有时编程成功,但有时会出现 Wire ACK 故障或 MI 命令错误。 也尝试过闪存擦除,但未能成功完成。 我的问题 什么原因会导致 KW45 在转储或编程代码时间歇性地报告 Wire ACK 故障? 执行 MI 命令时出错? 编程后跳转到或停止在意外或无效的内存地址? 即使尝试完全擦除闪存也失败了吗? 由于该问题包括间歇性 Wire ACK 故障和闪存擦除期间的故障,我怀疑这可能与调试接口、SWD/JTAG 信号完整性、电源稳定性、RESET 序列、闪存控制器状态、设备安全/配置、启动配置或其他硬件级问题有关,而不是应用程序本身的问题。 请问您能否提供以下方面的推荐操作流程: 恢复或擦除 KW45 设备。 确认调试接口功能正常。 检查设备是否已锁定或处于阻止正常编程的状态。 确定 Wire ACK 故障是由目标硬件、调试探针、电源/复位行为还是 SWD/JTAG 信号完整性引起的。 如有需要,我可以提供以下信息: MCUXpresso IDE 版本:25.6.1 测试的调试探针:SEGGER J-Link 和 NXP MCU-Link 完整的错误日志,包括 Wire ACK 故障详情。 调试控制台输出 JTAG/SWD 和启动连接示意图 SWD/JTAG时钟频率 电源和 RESET 配置 来自故障状态的内存/寄存器信息 非常感谢您能提供任何故障排除步骤方面的指导。 先行致谢。 Re: KW45: Intermittent Wire ACK Fault During Programming/Debugging and Flash Erase Failure 你好,希望你一切都好。   首先,请您确认一下您定制主板的一些硬件细节: BOOT_CFG (PTA4) 网络是否有下拉电阻连接到 GND?VDD_SYS 和 VDD_CORE 去耦电容是否已安装?因为这些是提供反馈通路并维持内部稳压器输出电压稳定性所必需的。   要尝试恢复设备,请尝试以下步骤: 您能否通过 ISP 模式访问您的设备?为此,在 RESET 期间将 BOOT_CONFIG (PTA4) 拉高,以强制设备进入 ISP 模式(在 KW47-EVK 上,这是 SW4)。 进入ISP模式后,打开命令提示符并运行以下命令: # Confirms ROM bootloader communication is working, a successful response confirms the device is reachable via ISP blhost.exe -p COMX get-property 1 # Reveals whether the device is in OEM_OPEN or a secured lifecycle state blhost.exe -p COMX get-property 07 # Perform a mass erase of the CM33 and NBU Program Flash blhost.exe -p COMX flash-erase-all blhost.exe -p COMX flash-erase-all 2 之后,您可以尝试运行 hello_world 或 BLE 示例,以确保电路板正常工作。 另外,请确认一下,您之前运行的是哪个应用程序?你有没有用低功耗的例子进行测试?设备也可能进入了低功耗状态,在低功耗运行期间禁用了SWD调试接口,这将导致LinkServer或J-Link无法正常连接。 此致, 索菲亚。 Re: KW45: Intermittent Wire ACK Fault During Programming/Debugging and Flash Erase Failure 您好,女士。 感谢您的详细回复。 关于硬件细节: BOOT_CFG (PTA4) 下拉:是的,我们定制的板上的 BOOT_CFG (PTA4) 网络有一个下拉电阻连接到 GND。 VDD_SYS 和 VDD_CORE 去耦电容:是的,所需的去耦电容已安装在板上。我已附上相关的原理图部分/图像,显示了VDD_SYS 和 VDD_CORE 的连接以及去耦电容。 同时,我将按照您建议的步骤,通过ISP 模式访问设备,并尝试使用 blhost 命令检查设备状态并执行批量擦除。 关于之前运行的应用程序: 该应用程序基于FreeRTOS ,并集成了以下外设/模块: FreeRTOS LPSPI0 带 DMA 通用IO LPSPI1 带 FIFO WDOG 关于低功耗问题,我在应用中并没有特意使用任何具体的低功耗示例。 我将执行 ISP 恢复程序,并告知您结果,特别是以下方面: 获取属性 1 获取属性 07 全部擦除 全部擦除 2 如果您建议在进行这些测试时进行任何其他硬件检查或测量,请告诉我。 普拉山斯1_0-1789454497591.png Prashanth1_1-1789454501864.png 再次感谢您的支持。 此致, 普拉桑特
查看全文
Does NXP official have a code routine for configuring external boot for S32K344 chip? Does NXP official have a code routine and tutorial for configuring external boot for S32K344 chip? We would like to configure the chip to boot from the SD card? Re: Does NXP official have a code routine for configuring external boot for S32K344 chip? In a nonsecure boot configuration - does the first bootloader run from ROM (is it immutable)? Can this first bootloader be configured to boot the subsequent bootloaders/application images from an external source/flash? Re: Does NXP official have a code routine for configuring external boot for S32K344 chip? This device does not offer an option to boot from external memory. Device supports secure and nonsecure boot modes but in both cases it is internal flash boot.
查看全文
GUI Guider 1.10.1 では、背景の不透明度が 0 の場合、背景スタイルのプロパティが省略されます。 環境 GUI Guider: 1.10.1 LVGL: 8.3 ウィジェット: ボタン スタイルパーツ: LV_PART_MAIN スタイル状態: LV_STATE_DEFAULT 問題の説明 GUI Guider 1.10.1 で再現可能なコード生成の問題を発見しました。 ボタンに背景色が設定されているにもかかわらず、背景の不透明度が0に設定されている場合、GUI Guiderは対応する背景色プロパティを生成しません。 実行時に背景の透明度を動的に変更すると、予期しない動作が発生します。 再生 ボタンを作成して設定します。 背景色:#F08300 背景の不透明度: 0 次に、LVGL 8.3コードを生成します。 GUI Guider が生成するもの: lv_obj_set_style_bg_opa(ui->screen_password_btn_15, 0、 LV_PART_MAIN | LV_STATE_DEFAULT); しかし、設定した背景色は生成されません。 lv_obj_set_style_bg_color(ui->screen_password_btn_15, lv_color_hex(0xF08300) LV_PART_MAIN | LV_STATE_DEFAULT); テスト:背景の不透明度のみを0から1に変更する 背景色の#F08300はそのままに、背景の不透明度だけを0から1に変更しました。 コードを再生成した後、GUI Guiderは以下を生成します。 lv_obj_set_style_bg_opa(ui->screen_password_btn_15, 1、 LV_PART_MAIN | LV_STATE_DEFAULT); lv_obj_set_style_bg_color(ui->screen_password_btn_15, lv_color_hex(0xF08300) LV_PART_MAIN | LV_STATE_DEFAULT); lv_obj_set_style_bg_grad_dir(ui->screen_password_btn_15, LV_GRAD_DIR_NONE、 LV_PART_MAIN | LV_STATE_DEFAULT); したがって、生成されるコードは、背景の不透明度が正確に0であるかどうかによって異なります。 背景の不透明度 = 0: bg_opaが生成されます bg_color は生成されません 背景の不透明度 = 1: bg_opaが生成されます bg_color が生成されます その他の背景プロパティも生成されます 実行時への影響 私のアプリケーションは背景の不透明度を使って現在選択されているパスワード番号を示します。 背景色はGUI Guiderで #F08300 として設定され、アプリケーションは背景の不透明度のみを動的に変更します。 例: lv_obj_set_style_bg_opa(btn, LV_OPA_COVER、 LV_PART_MAIN | LV_STATE_DEFAULT); 初期の背景不透明度が0のボタンの場合、生成されるコードには設定された背景色が含まれません。 アプリケーションが不透明度を0からLV_OPA_COVERに変更すると、ボタンはGUI Guiderで設定された #F08300 色の代わりにLVGLテーマまたはデフォルトの背景色を表示します。 その動作は以下のとおりです。 GUI Guiderの設定: 背景色 = #F08300 背景の不透明度 = 0 生成されたコード: bg_opa = 0 bg_color は生成されません ランタイム: bg_opa が LV_OPA_COVER に変更されました 結果: #F08300の代わりに、デフォルトまたはテーマの背景色が表示されます。 応急措置 アプリケーションコード内で背景色を明示的に設定すると、以下の問題が解決します。 lv_obj_set_style_bg_color(btn, lv_color_hex(0xF08300) LV_PART_MAIN | LV_STATE_DEFAULT); lv_obj_set_style_bg_opa(btn, LV_OPA_COVER、 LV_PART_MAIN | LV_STATE_DEFAULT); 別の回避策としては、GUI Guiderで背景の不透明度を1に設定する方法があります。これにより、GUI Guiderは設定された背景色を生成するようになります。 しかし、これは初期のUI状態を変更してしまうため、理想的とは言えません。 期待される動作 背景色と背景の不透明度は、それぞれ独立したLVGLスタイルプロパティです。 ユーザーが明示的に以下を設定する場合: 背景色 = #F08300 背景の不透明度 = 0 GUI Guiderは、生成されたコードにおいて両方のプロパティを保持するはずです。 lv_obj_set_style_bg_opa(btn, 0、 LV_PART_MAIN | LV_STATE_DEFAULT); lv_obj_set_style_bg_color(btn, lv_color_hex(0xF08300)、 LV_PART_MAIN |LV_STATE_DEFAULT); bg_color bg_opa が0のときは目に見える影響はありませんが、アプリケーションが実行時に動的にbg_opaが変化すると重要になります。 現在のコード生成動作では、GUI Guiderで設定された背景色情報が失われます。 実際の行動 GUI Guider 1.10.1 では、背景の不透明度が 0 の場合、背景スタイルのプロパティが省略されるようです。 不透明度を0から1に変更するだけで、背景色やその他の背景プロパティが再生成されます。 再現手順 GUI Guider 1.10.1 でボタンを作成する。 背景色を#F08300に設定してください。 背景の不透明度を0に設定してください。 LVGL 8.3コードを生成します。 値0のlv_obj_set_style_bg_opaが生成されていることを確認してください。 #F08300 を指定した lv_obj_set_style_bg_color は生成されないことに注意してください。 背景の不透明度のみを0から1に変更してください。 コードを再度生成してください。 #F08300 を指定した lv_obj_set_style_bg_color が生成されていることを確認してください。 実行時に、元のボタンの不透明度をLV_OPA_COVERに変更します。 設定された背景色は、アプリケーションが明示的に設定しない限り表示bg_colorないことに注意してください。 質問 これはGUI Guider 1.10.1における意図的なコードサイズ最適化なのでしょうか、それともコード生成の問題なのでしょうか? もしこの最適化が意図的であれば、GUI Guiderはバックグラウンド不透明度が0のときにバックグラウンドプロパティを保持するオプションを提供してくれますか? ランタイムアプリケーションはLVGLスタイルのプロパティを動的に変更することが多いため、初期の不透明性だけでbg_colorを省略すると、UI設定とは異なる実行時の挙動が生じる可能性があります。 Re: GUI Guider 1.10.1 omits background style properties when Background Opacity is 0 こんにちは、 @zzjgood さん、 投稿ありがとうございます。 あなたが説明した行動を再現できます。これはコード生成の問題だと思います。ユーザーが背景色を明示的に設定する場合、GUI Guiderは初期の背景不透明度が0でも対応するbg_colorコードを保持するか、透明オブジェクトの背景スタイルプロパティを保持するオプションを提供するべきです。この件はGUI-Guiderチームに報告し、修正を依頼します。さらに、当社の内部エスカレーションプロセスに基づき、以下の情報を提供していただけるとありがたいです。 - どのNXP製品を使っていますか? - 最終的なアプリケーションは? 現在の実用的な回避策は、アプリケーションコード内で背景色と不透明度の両方を明示的に設定することです。 コピー lv_obj_set_style_bg_color(btn, lv_color_hex(0xF08300), LV_PART_MAIN | LV_STATE_DEFAULT); lv_obj_set_style_bg_opa(btn, LV_OPA_COVER, LV_PART_MAIN | LV_STATE_DEFAULT); お役に立てば幸いです。 BR セレステ Re: GUI Guider 1.10.1 omits background style properties when Background Opacity is 0 はい、ご返信ありがとうございます。 Re: GUI Guider 1.10.1 omits background style properties when Background Opacity is 0 こんにちは、 @zzjgood さん、 お元気でお過ごしでしょうか。 この件に関して最新情報が入りました。バージョン1.10.1では、不透明度が0に設定されている場合に背景スタイルのコード生成をスキップする動作は、不要な生成コードを削減するために意図的に設計されたものです。同じ論理は境界線のスタイルにも当てはまります。 お客様のユースケースでは、残りのスタイルコードを生成することが依然として有益であることは理解しています。しかし、v1.xブランチは既に更新されていません。対照的に、v2.xは値に関係なくユーザー設定のスタイルプロパティをすべて生成し、あなたのシナリオを完全にサポートします。 したがって、Gui-guider v2.xへの移行をお勧めします。 現代的な組み込みGUIファストを作成 | NXP Semiconductors よろしくお願いいたします。 セレステ
查看全文
安装S32 Design Studio for ARM 2.2无法激活 安装S32 Design Studio for ARM 2.2: 1.在激活时选择online则报图一错误,使用https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/Troubleshooting-Activation-fails-with-error-message-FNP-ERROR-0/ta-p/1123259后报图二错误,但是我的电脑服务中FlexNet Licensing Service时启动状态 2.使用offline激活,完全参照官网步骤后,报图三错误,我该如何正确激活并安装此版本软件? Re: 安装S32 Design Studio for ARM 2.2无法激活 我已经完全按照步骤做了,依旧不行 Re: 安装S32 Design Studio for ARM 2.2无法激活 嗨@aether FNP 错误 20 通常与组件未正确安装或当前用户无法访问有关。请尝试以下步骤: 完全卸载 S32DS for ARM v2.2,并删除 C:\NXP\S32DS_ARM_v2.2 中所有剩余的文件。 备份并清除隐藏文件夹 C:\ProgramData\FLEXnet\ 的内容。 重新下载并安装适用于 ARM 的基本 S32DS v2.2 软件包(不包含 Update 2)。 以管理员权限运行安装程序,并确保防病毒软件或安全软件没有阻止安装程序运行。 BR,VaneB Re: 安装S32 Design Studio for ARM 2.2无法激活 嗨@aether 能否请您提供一下安装日志文件(.log)?它应该位于: C:\NXP\S32DS_ARM_v2.2\_S32 Design Studio for ARM Version 2.2_installation\Logs
查看全文
ARINC615A 数据加载,使用 JTAG 访问密码保护 当未安装 HSE 固件时,可以使用CUST_DB_PSWD_A字段和设备生命周期配置来限制 S32K3 上的 SWD/JTAG 访问。假设更新是由应用程序或引导加载程序软件处理,而不是通过调试接口处理,启用此密码保护是否会对向处理器执行 ARINC 615A 软件数据加载产生任何影响? Re: ARINC615A Data loading with JTAG Access password protected CUST_DB_PSWD_A 仅限制 SWD/JTAG 调试访问。我不熟悉您的 ARINC 615A 实现的细节,但如果软件加载完全由您的应用程序或引导加载程序处理,我认为调试密码本身不会产生任何影响。 最终,这是特定应用,取决于 ARINC 615A 在您的系统中是如何实现的。如果更新机制不使用调试接口,则调试访问限制通常应独立于软件加载过程。任何其他限制都将取决于您的生命周期配置和应用程序网络安全设计。
查看全文