Hello
这是对 GitHub 上这个 PR的后续跟进。
提供的补丁似乎最终没有应用,因为 lf-6.18.y 中没有这些补丁。
需要 Kconfig 提交来确保当 NVMEM_IMX_OCOTP_SCU 为 m 时 Enclave 驱动程序不能为 y,从而避免探测延迟。
否则你会看到这样的结果:
root@colibri-imx8x-14985125:~# dmesg -l err [ 1.708145] rtc-ds1307 1-0068: hctosys: unable to read the hardware clock [ 2.072996] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 2.078636] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 2.084513] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 2.111555] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 2.117209] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 2.123110] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 2.141671] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 2.147303] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 2.153200] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 2.171418] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 2.177065] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 2.182929] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 5.744448] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 5.750217] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 5.756186] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 5.877660] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 5.888247] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 5.894232] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 10.324138] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 10.349783] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 10.374692] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 11.731697] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 11.738134] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 11.747692] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 12.284910] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 12.295720] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 12.307723] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 12.410541] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 12.426771] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 12.443446] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 12.644550] debugfs: '5f1a0000.phy' already exists in 'regmap' [ 12.655906] debugfs: '5f1a0000.phy' already exists in 'regmap' [ 12.670039] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 12.688813] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 12.696063] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 12.765923] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 12.775810] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 12.786887] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 12.839515] fsl-se secure-envlave-1: Fail to read FIPS fuse [ 12.847285] fsl-se secure-envlave-1: Failed to fetch SoC Info. [ 12.853801] fsl-se secure-envlave-1: failed[-EPROBE_DEFER] to fetch SoC Info [ 12.936721] nvmem imx-scu-ocotp0: cell mac raw len 6 unaligned to nvmem word size 4 [ 12.951328] nvmem imx-scu-ocotp0: cell mac raw len 6 unaligned to nvmem word size 4 [ 13.708903] genpd_provider mu_a1: failed to power off resource 214 ret -22 [ 16.701904] Bluetooth: hci0: unexpected event for opcode 0x0000 root@colibri-imx8x-14985125:~#
在提交的第二个版本中,驱动程序进行了一些重构,我不确定NXP是否已经解决了这个问题。
提交 9703dfecc735(“LF-15802:驱动程序:固件:imx:修复 SE 驱动程序移除”)
SE团队能否确认一下?
此致敬礼
弗朗茨
你好,
我看到这个问题还没有解决,我会和内部软件团队确认一下。
此致敬礼/Saludos,
阿尔多。