Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
i.MX 8ULP uSDHC - HS400 Enhanced Strobe: validation and CMD response sampling Hi, We use the on-board eMMC (JEDEC 5.1) on i.MX 8ULP (uSDHC0) in HS400 Enhanced Strobe (200 MHz, 8-bit, 1.8 V). Our U-Boot eMMC host and card-switching code is identical to NXP lf-6.1.55-2.2.1, and the EVK device tree also enables mmc-hs400-enhanced-strobe. During evaluation we have occasionally seen a data CRC error or no response to CMD12/CMD13 during eMMC reads in U-Boot. In our tests, only a host reset or a card re-initialization recovered it. 1. Is HS400 Enhanced Strobe validated and recommended on i.MX 8ULP? The datasheet (IMX8ULPIEC Rev.1) does not mention it. If it is not, is standard HS400 the recommended configuration? Also, which AC timing applies to the CMD response at the SoC pins in HS400 / Enhanced Strobe? 2. In Enhanced Strobe, where no tuning is performed, what samples the CMD response: the data strobe or the internal sampling clock? The reference manual's "Switch to HS400 mode" requires HS200 tuning "to synchronize the command response on the CMD line to CLK" and writes the result back with MIX_CTRL[SMP_CLK_SEL] = 1 (steps 6, 10-12). "Switch to HS400 enhanced mode" has no such step. The i.MX 93 reference manual (38.3.10.5) has the same flow and no description either. Thank you in advance. Best regards, mio i.MX8ULP Re: i.MX 8ULP uSDHC - HS400 Enhanced Strobe: validation and CMD response sampling Hi @mio  Sorry to reply late: 1. i.MX 8ULP supports HS400ES mode.  https://github.com/nxp-imx/linux-imx/blob/lf-6.1.55-2.2.2/drivers/mmc/host/sdhci-esdhc-imx.c#L334 CMD input/output follows the SDR104 CMD input/output timing specification, specifically parameters SD5, SD6 and SD7 in RM Table 35. 2. In Enhanced Strobe mode DATA OUT, CRC Response and CMD Response are all synched to STROBE clocks. The timing relation between CMD Response output signals and STROBE clocks is the same as defined for DATA Out to STROBE clocks B.R Re: i.MX 8ULP uSDHC - HS400 Enhanced Strobe: validation and CMD response sampling Hello, Thank you for the answer. Just to confirm that I understand correctly: 1. On i.MX 8ULP in HS400 Enhanced Strobe mode, the uSDHC samples the CMD response with its internal sampling clock (CLK-based, not the data strobe), and the CMD input/output timing requirement is SD5/SD6/SD7 in Table 35 of the data sheet (referenced to CLK), the same as in HS400. 2. Since no tuning is performed in Enhanced Strobe, the fixed sampling clock is used for CMD (we read SMP_CLK_SEL = 0 in this mode), and the strobe (STROBE_DLL) is used only for capturing the data on DAT[7:0]. Is this correct? Thank you very much for your help. Best regards, Mio
View full article
S32K376NHT1MJBST: applicable power estimator and per-supply current data Hello, Could you please identify the applicable power-estimation tool and supply-current data for S32K376NHT1MJBST? Does S32K-PET support this exact derivative? Which tool and device-dataset revisions should be used? If it is not supported, what is the recommended current NXP method? For externally supplied V15 with the external NMOS V11 regulator arrangement, how should reported demand be attributed to V15, V11, VDD_HV_A/B and other analog/bias supplies? Please identify what is included or excluded, especially regulator losses, shared core/lockstep demand, I/O loading and peripheral currents, so these are not counted twice. Which applicable public documents, data or characterization method cover worst-case supply current versus voltage/temperature, and peaks during reset, startup, wake and clock/mode changes? Please distinguish typical/average estimates from guaranteed limits and identify their conditions. The public PET page and setup guide have been reviewed. Their family-level support listing and initial average-power scope do not identify the exact derivative or all physical-supply contributions. We are seeking the applicable sources and method, not an application-specific current result without a defined operating profile. Please point to the appropriate public material or support route if these details are not public. Thank you. Re: S32K376NHT1MJBST: applicable power estimator and per-supply current data Hello @JonasGranlund, 1. As of now, the S32K PET tool does not support S32K39/37/36 devices. The recommended method is to refer to S32K396's Data Sheet (Rev. 5) for supply current data, specifically: 6.7 Supply currents (Standby and RUN mode tables) 6.9 Cyclic wake-up average current calculation 2. The datasheet supply current tables report current at the following rails independently: VDD_HV_A is catalogued as the main I/O and analog supply, and it covers both I/O pads in the VDD_HV_A bank and all analog blocks.  VDD_HV_B is the secondary I/O supply and covers I/O pads in the VDD_HV_B bank only. You can refer to "S32K39_and_S32K37_IOMUX.xlsx" attachment inside the Reference Manual in order to identify which pin belongs to which power domain. V11 is generated by V15 using external NMOS. The external V1.5 power supply should be turned off before entering LPM mode. IO load current is not included in measurements. The actual current requirements for IOs will depend on the I/O configuration in the application. Refer to the DC characteristics tables in the S32K39 Data sheet. Lockstep/dual-core demand is included in the core supply figures in the data sheet; the power consumption is specified to be the same because there are no separate specifications depending on the load of the cores. 3. Data Sheet values include ambient temperature, typical and maximum values.  As far as I know, there are no specific S32K39 documents detailing worst-case scenario currents, peaks during reset, etc. However, S32K3 Low Power Management AN and demos document provide power mode transitions, clock operation in low-power modes, hardware considerations and quiescent current. It is focused on a more family-level, referencing S32K3xx in general, rather than S32K39-37-36 specifics. I've also sent you a private message in community sharing S32K3 Low Power Lab presentation, which explains S32K3 low power behavior and considerations. Best regards, Julián
View full article
S32K376NHT1MJBST:适用的功率估算器和单电源电流数据 你好, 请问您能否提供适用于 S32K376NHT1MJBST 的功率估算工具和供电电流数据? S32K-PET 是否支持这种特定衍生物?应该使用哪些工具和设备数据集版本?如果不支持,NXP 目前推荐的方法是什么? 对于采用外部 NMOS V11 稳压器配置的外部供电 V15,应如何将报告的需求分配给 V15、V11、VDD_HV_A/B 和其他模拟/偏置电源?请明确哪些项目包含在内,哪些项目不包含在内,特别是调节器损耗、共享核心/锁定步进需求、I/O 负载和外围电流,以免重复计算。 哪些适用的公共文件、数据或表征方法涵盖了最坏情况下的供电电流与电压/温度的关系,以及RESET、启动、唤醒和时钟/模式变化期间的峰值?请区分典型/平均估价和保证限额,并说明其适用条件。 已审核公开的PET页面和设置指南。他们的家族级支持清单和初始平均功率范围并未明确指出具体的衍生品或所有实物供应贡献。我们寻求的是适用的资源和方法,而不是没有明确操作规范的特定应用的当前结果。 如果这些信息不公开,请指出相应的公开资料或支持途径。 谢谢! Re: S32K376NHT1MJBST: applicable power estimator and per-supply current data 你好@JonasGranlund , 1.目前,S32K PET 工具不支持 S32K39/37/36 设备。推荐的方法是参考 S32K396 的数据手册(修订版)。5)关于供应电流数据,具体而言: 6.7 电源电流(待机和运行模式表) 6.9 循环唤醒平均电流计算 2. 数据手册中的电流表分别报告以下各轨的电流: VDD_HV_A被列为主 I/O 和模拟电源,它覆盖 VDD_HV_A 组中的两个 I/O 焊盘和所有模拟模块。 VDD_HV_B是辅助 I/O 电源,仅覆盖 VDD_HV_B 组中的 I/O 焊盘。您可以参考参考手册中的“S32K39_and_S32K37_IOMUX.xlsx”附件,以确定哪个引脚属于哪个电源域。 V11由 V15 利用外部 NMOS 产生。进入LPM模式前,应关闭外部V1.5电源。 测量中不包括 I/O 负载电流。实际的 I/O 电流需求将取决于应用程序中的 I/O 配置。请参阅 S32K39 数据表中的直流特性表。 数据表中核心供电量中包含了锁步/双核需求;由于没有根据核心负载单独制定的规格,因此功耗规定为相同。 3. 数据表中的数值包括环境温度、典型值和最大值。 据我所知,没有专门针对 S32K39 的文件详细说明最坏情况下的电流、RESET 期间的峰值等。然而, S32K3 低功耗电源管理单元 AN 和演示文档提供了电源模式转换、低功耗电源模式下的时钟操作、硬件注意事项和静态电流。它更侧重于家族层面,一般参考 S32K3xx,而不是 S32K39-37-36 的具体细节。 我还通过社区分享 S32K3 低功耗实验室演示文稿向您发送了一条私信,其中解释了 S32K3 的低功耗特性和注意事项。 此致, 朱利安
View full article
SodaPeakは買う価値があるのか?2026年に向けた正直なレビュー ソーダピーク: 従来のサプリメントがカプセルを飲み込んだり粉末を用意したりするのに対し、SodaPeakは忙しいライフスタイルに合うシンプルなアプローチを提供します。この製品は、男性の健康において重要な3つの分野、すなわち日常のエネルギー、身体的持久力、そして全体的な活力に焦点を当てています。 公式サイト: https://finance.yahoo.com/healthcare/articles/sodapeak-launch-2026-advanced-soda-174000686.html
View full article
S32K376NHT1MJBST:適用可能な電力推定器および電源ごとの電流データ こんにちは、 S32K376NHT1MJBSTに適用される電力推定ツールと供給電流データを教えていただけますか? S32K-PETはこの派生モデルをサポートしていますか?どのツールとデバイスデータセットの改訂版を使用すべきですか?もしサポートされていない場合、現在の推奨されているNXP方法は何ですか? 外部供給のV15に外部NMOSのV11レギュレータ配置がある場合、報告された需要はV15、V11、VDD_HV_A/Bおよびその他のアナログ/バイアス供給にどのように帰属すべきでしょうか?特にレギュレーター損失、共有コア/ロックステップ需要、I/O負荷、ペリフェラル電流などを含め、何が含まれているか、何が除外されているかを特定してください。これらが二重にカウントされないようにするためです。 どの適用可能な公文書、データ、特性評価方法が、最悪のケースの電源電流と電圧/温度、リセット、起動、ウェイク、クロック/モード変更時のピークをカバーしていますか?標準値/平均値と保証限度額を区別し、それぞれの条件を明記してください。 公開されているPETページとセットアップガイドを確認しました。ファミリレベルの支援リストと初期の平均出力範囲では、正確な微分やすべての物理的供給貢献は特定されていません。私たちは、定義された運用プロファイルのない応用特有の現行結果ではなく、適用される情報源と方法を求めています。 これらの詳細が公開されていない場合は、適切な公開資料やサポートルートをご紹介ください。 よろしくお願いします。 Re: S32K376NHT1MJBST: applicable power estimator and per-supply current data こんにちは、@JonasGranlund さん。 1.現時点で、S32K PETツールはS32K39/37/36デバイスをサポートしていません。推奨される方法は、S32K396のデータシート(Rev.5) 供給電流データについては、具体的には: 6.7 供給電流(スタンバイモードおよび動作モードの表) 6.9 周期的なウェイクアップ平均電流の計算 2. データシートの供給電流表には、以下のレールにおける電流が個別に記載されています。 VDD_HV_A メインのI/Oおよびアナログ電源としてカタログ化されており、VDD_HV_AバンクのI/Oパッドとすべてのアナログブロックをカバーしています。 VDD_HV_Bは二次I/O電源であり、VDD_HV_Bバンク内のI/Oパッドのみを対象としています。どのピンがどのパワードメインに属しているかを特定するために、リファレンスマニュアル内の「S32K39_and_S32K37_IOMUX.xlsx」アタッチメントを参照できます。 V11は、外部NMOSを用いてV15によって生成される。LPMモードに入る前に、外部V1.5電源をオフにしてください。 IO負荷電流は測定値に含まれていません。IOの現在の要件は、アプリケーションのI/O構成によって異なります。S32K39データシートのDC特性表を参照してください。 データシートのコア供給量には、ロックステップ/デュアルコア動作時の需要が含まれています。コアの負荷に応じて個別の仕様が定められていないため、消費電力は同じ値として規定されています。 3.データシートの値には、周囲温度、標準値、最大値が含まれます。 私の知る限り、最悪のシナリオの電流やリセット時のピークなどを詳述したS32K39の文書は存在しません。しかし、S32K3の低電力パワーマネージメントANおよびデモでは、電源モードの遷移、低消費電力モードのクロック動作、ハードウェアの考慮事項、静止電流が記載されています。よりファミリレベルに焦点を当てており、S32K39-37-36の詳細ではなく、S32K3xx全体を指しています。 S32K3の低消費電力動作と留意事項について説明したS32K3低消費電力ラボのプレゼンテーションを、コミュニティ共有のプライベートメッセージでお送りしました。 よろしくお願いします、 ジュリアン
View full article
88W8987 使用 FreeRTOS 时,AP 模式下 WPA2 认证间歇性失败 您好, 我们使用基于 88W8987 的 Murata LBEE5QD1ZM 模块,通过 SDIO 连接到运行 FreeRTOS 和 NXP Wi-Fi 驱动程序的 i.MX RT1176。 某些设备,特别是 Multilaser M10 安卓平板电脑,经常无法使用 PSK/CCMP 连接到我们的 WPA2-Personal AP。有时,同一台平板电脑在多次尝试后才能成功连接。其他设备,例如三星 S9 FE,连接正常。 虽然安卓系统显示“正在获取 IP 地址”,但日志显示 WPA2 四次握手过程中出现故障: - AP 报告了站点关联,但没有 RSN_CONNECTED 事件。 - Android 日志显示接收到 EAPOL 消息 3 并发送消息 4,随后 AP 再次转发消息 3。 - 关联后约 18 秒,AP 报告取消认证,原因为 1。 - 当出现 RSN_CONNECTED 时,DHCP 正常完成。 受影响的平板电脑可以正常工作,开放式和 WEP 连接均可正常使用。固件版本 16.91.21.p82 和 16.92.21.p156.4 仍然存在此问题。 一个重要的对比是另一款在 Linux 下使用相同模块模型的产品:M10 使用 WPA2-PSK/CCMP 成功连接,验证芯片通过 hostapd 在主机上运行。在我们的 FreeRTOS 实现中,握手由 88W8987 固件管理。 这些观察结果表明固件管理的验证芯片存在互操作性问题。但是,如果没有空中捕获,我们无法确认消息 4 是否到达模块,也无法确认为什么它不被接受。 这是已知问题吗?是否有固件修复程序或诊断选项来跟踪验证芯片状态并确定握手无法完成的原因? 此致, JV Melo。 Re: 88W8987 Intermittent WPA2 Authentication Failure in AP Mode with FreeRTOS 你好@joseviniciusmelo 能否帮忙分享一下iMX1176的SDK版本? 顺祝商祺! 肖恩 Re: 88W8987 Intermittent WPA2 Authentication Failure in AP Mode with FreeRTOS 嗨,肖恩, 我测试了以下88W8987固件版本和SDK: 16.91.21.p82,MCUXpresso SDK 2.13.1; 16.92.21.p156.4,带 MCUXpresso SDK 26.09.00; 在我们的 FreeRTOS 平台上,两个版本都出现了同样的间歇性 WPA2 身份验证失败问题。 同一台平板电脑可以成功连接到另一台在 Linux 系统下使用相同模块型号的产品,其中 hostapd 在主机上处理 WPA2 握手。由于模块固件在我们的 FreeRTOS 平台上处理握手,我们怀疑与固件的 WPA2 验证芯片存在互操作性问题。 此致, JV Melo。
View full article
88W8987 Intermittent WPA2 Authentication Failure in AP Mode with FreeRTOS Hi, We are using the Murata LBEE5QD1ZM module, based on the 88W8987, connected through SDIO to an i.MX RT1176 running FreeRTOS and the NXP Wi-Fi driver. Some devices, especially a Multilaser M10 Android tablet, frequently fail to connect to our WPA2-Personal AP using PSK/CCMP. Occasionally, the same tablet connects successfully after several attempts. Other devices, such as a Samsung S9 FE, connect normally. Although Android displays “Obtaining IP address,” the logs indicate a failure during the WPA2 four-way handshake: - The AP reports station association, but no RSN_CONNECTED event. - Android logs indicate reception of EAPOL message 3 and transmission of message 4, followed by further retransmissions of message 3 from the AP. - Approximately 18 seconds after association, the AP reports deauthentication with reason 1. - When RSN_CONNECTED does occur, DHCP completes normally. Open and WEP connections work with the affected tablet. The problem persists with firmware versions 16.91.21.p82 and 16.92.21.p156.4. An important comparison is another product using the same module model under Linux: the M10 connects successfully using WPA2-PSK/CCMP, with the authenticator running on the host through hostapd. In our FreeRTOS implementation, the handshake is managed by the 88W8987 firmware. These observations suggest an interoperability issue in the firmware-managed authenticator. However, without an over-the-air capture, we cannot confirm whether message 4 reaches the module or why it is not accepted. Is this a known issue? Is there a firmware fix or diagnostic option to trace the authenticator state and determine why the handshake does not complete? Best regards, J. V. Melo. Re: 88W8987 Intermittent WPA2 Authentication Failure in AP Mode with FreeRTOS Hello @joseviniciusmelo  Could you help share sdk version of iMX1176? Best Regards Shaun Re: 88W8987 Intermittent WPA2 Authentication Failure in AP Mode with FreeRTOS Hi Shaun, I tested the following 88W8987 firmware versions and SDKs: 16.91.21.p82 with MCUXpresso SDK 2.13.1; 16.92.21.p156.4 with MCUXpresso SDK 26.09.00; The same intermittent WPA2 authentication failure occurred with both versions on our FreeRTOS platform. The same tablet connects successfully to another product that uses the same module model under Linux, where hostapd handles the WPA2 handshake on the host. Since the module firmware handles the handshake on our FreeRTOS platform, we suspect an interoperability issue with the firmware’s WPA2 authenticator. Best regards, J. V. Melo.
View full article
Is SodaPeak Worth Buying? An Honest Review for 2026 SodaPeak:- Unlike traditional supplements that require swallowing capsules or preparing powders, SodaPeak offers a simple approach that can fit into a busy lifestyleThe product focuses on three important areas of men's wellness: everyday energy, physical endurance, and general vitality. Official Website:- https://finance.yahoo.com/healthcare/articles/sodapeak-launch-2026-advanced-soda-174000686.html
View full article
Does i.MX 95 support simultaneous 4K60 decode/encode? Hi, Does i.MX 95 support simultaneous 4K60 decode/encode? If not, does NXP have other processor that can support it? Thanks, Fan Evaluation Board Re: Does i.MX 95 support simultaneous 4K60 decode/encode? Hi @fan99  Simultaneous 4K60 decoding and 4K60 encoding is not supported. The iMX95 VPU supports up to 4K60 shared between encode and decoder.  Best Regards, Zhiming
View full article
MPC8308CVMAFD 与 MPC8308CVMAFDA 您好, 我们希望就以下零件编号寻求您的技术意见: MPC8308CVMAFD MPC8308CVMAFDA 请问这两个零件编号之间有什么区别吗? 根据产品规格书,附加字母“A”表示版本号。然而,我们未能找到任何进一步的信息来解释具体的版本号及其对设备的影响。 请您确认这两个零件编号在电气性能和功能上是否相同,是否可以互换。 非常感谢您的帮助。 Re: MPC8308CVMAFD Vs MPC8308CVMAFDA ### 1. 两个零件编号的区别 **MPC8308CVMAFD** 和 **MPC8308CVMAFDA** 之间的唯一区别在于 **内部硅步进/版本**: * **`MPC8308CVMAFD`**:代表**硅版本 1.0**。 * **系统版本寄存器 (SVR):** `0x8101_0110` * **`MPC8308CVMAFDA`**:代表**硅修订版 1.1**(末尾字母**“A”**表示飞思卡尔/恩智浦部件编号方案中的修订版 1.1)。 * **系统版本寄存器 (SVR):** `0x8101_0111` 两台设备的标称参数完全相同: * **封装:** 473引脚MAPBGA(19毫米×19毫米,0.8毫米引脚间距) * **温度等级:**扩展/工业级(`C` = -40°C 至 105°C $T_j$) * **核心频率:** 333 MHz (`AF`) * **DDR 数据速率:** 266–333 MHz (`D`) * **无铅/符合RoHS标准:**无铅MAPBGA(`VM`) --- ### 2. 硬件等效性(外形、尺寸、功能) * **电气和机械方面:** **引脚完全匹配,即插即用。** * 无需对PCB布局、原理图、布线、电源或去耦进行任何更改。 * 焊球分配、电压轨($V_{DD} = 1.0\text{V}$、$G_{VDD} = 1.8\text{V}$、$N_{VDD} = 3.3\text{V}$)、I/O 驱动强度和 AC/DC 时序规格相同。 --- ### 3. 硅芯片差异及软件影响 Silicon Revision 1.1 (`MPC8308CVMAFDA`) 版本,其中包含了对 Revision 1.0 的一些内部错误/勘误的修复。 对于 99% 的应用,**Rev 1.1 完全向下兼容 Rev 1.0**。但是,请记住以下两点软件方面的注意事项: 1. 系统版本寄存器 (SVR) 检查: * 如果您的引导加载程序(U-Boot)、内核或专有固件明确读取并匹配精确的 32 位 SVR 值: * Rev 1.0 返回 `0x8101_0110` * 版本 1.1 返回 `0x8101_0111` * 确保代码中的任何硬件版本检查屏蔽或接受低 4 位(例如,与 `0x8101_011x` 匹配或检查 $\ge \text{Rev } 1.0$),以免启动序列停止。 2. **硅谷勘误解决方法:** * Rev 1.0 中存在的几个已知错误在 Rev 1.1 中得到解决或改进(记录在 *MPC8308 芯片错误* 文档 `MPC8308CE` 中)。 * 固件中针对 Rev 1.0 实现的软件变通方案在 Rev 1.1 上将继续安全运行。 --- ### 总结建议 **MPC8308CVMAFDA 是 MPC8308CVMAFD 的直接推荐替代品。**它们在外形、尺寸和功能上都是即插即用的替代品。只要你的固件没有对 SVR 寄存器进行硬编码的精确匹配检查,你就可以安全地替换 `MPC8308CVMAFDA`,而无需重新设计板。
View full article
P3B1602 I2C/I3C PCIe CEM仕様準拠 フォーラムの皆様へ PCIe CEM仕様リビジョン6.0.1では、SMBus(I2C)を3.3V、I3Cを1.8Vと定義しています。 P3B1602はI2Cモードで3.3V(内部抵抗で3.3V)で、I3Cモードで1.8Vをサポートしていますか? 両方のモードに対応するには、P3B1602の電源電圧を変更する必要があるということですよね? ありがとう。 敬具 モーリッツ Re: P3B1602 I2C/I3C PCIe CEM Spec Compliant こんにちは、郭さん  ご説明いただきありがとうございます。 同じSCLとSDAネットで2つのP3B1602を並列に使うことはできますか?ただし、1.8Vと3.3VのVCCB電源を使うことは可能でしょうか。 OEピンでアクティブにするために必要なものだけを抜き取ればいいのでしょうか? 敬具 モーリッツ Re: P3B1602 I2C/I3C PCIe CEM Spec Compliant こんにちは、モーリッツさん P3B1602両方の電圧レベルをサポートしていますが、同じBサイドバスが3.3 V SMBus/I²Cと1.8V I3Cの間をスイッチする必要がある場合は、対応するVCCBをスイッチし、すべての外部プルアップ抵抗器およびコネクテッド機器のレベル要件を検証する必要があります。 よろしくお願いします! BR Re: P3B1602 I2C/I3C PCIe CEM Spec Compliant こんにちは、モリッツさん よりよく理解するために接続図を教えていただけますか?BR Re: P3B1602 I2C/I3C PCIe CEM Spec Compliant こんにちは、モリッツさん よりよく理解するために接続図を教えていただけますか?BR Re: P3B1602 I2C/I3C PCIe CEM Spec Compliant こんにちは、郭さん  私の計画はこうです。 敬具 モーリッツ Re: P3B1602 I2C/I3C PCIe CEM Spec Compliant こんにちは、モーリッツさん 1.8Vまたは3.3VのチャネルはOEを通じて選択可能です。しかし、OEは単なるソフトウェア信号選択ではありません。相互排他性、デフォルトオフ状態、スイッチングデッドゾーンを確保しなければなりません。 Re: P3B1602 I2C/I3C PCIe CEM Spec Compliant こんにちは、郭さん。 FPGAで対応できると思います。 要約すると、相互排他性が確保され、有効化の間に遅延が設けられていれば、問題はないということですね? 分かりやすくするために、プルダウン抵抗は省略しました。 敬具 モーリッツ Re: P3B1602 I2C/I3C PCIe CEM Spec Compliant こんにちは、モーリッツさん これらのB側ピンに外部プルアップ抵抗がない場合は、問題ないはずです。
View full article
i.MX 95は同時4K60のデコード/エンコードをサポートしていますか? こんにちは、 i.MX 95は同時4K60のデコード/エンコードをサポートしていますか?もしなければ、NXPにはサポートできる他のプロセッサはありますか? ありがとうございます ファン 評価ボード Re: Does i.MX 95 support simultaneous 4K60 decode/encode? こんにちは、 @fan99さん 4K60のデコードとエンコードの同時実行はサポートされていません。iMX95 VPUはサポート エンコード側とデコーダー側で最大4K60fpsを共有可能。 よろしくお願いします、 志明
View full article
CMake 版本长路径问题 错误:MCUXpresso VS Code 扩展程序由于compile_commands.json 文件中缺少output字段,无法构建有效的 CMake 项目。 产品: MCUXpresso for VS Code 元器件: MCUXpresso 扩展 — 版本项目/Windows 长路径验证 主机操作系统: Windows 11 目标MCU: NXP i.MX RT1186(Cortex-M33) 构建系统: CMake + Ninja 扩展版本: 26.9.44 严重性:版本操作已阻止;有变通方案 问题描述 MCUXpresso VS Code 扩展程序无法对一个原本有效的 CMake 项目进行版本“版本项目”命令时。 显示以下错误信息: The "path" argument must be of type string. Received undefined 错误发生在 MCUXpresso 扩展的 JavaScript 代码中,而不是 CMake 配置或版本过程中。 同一个项目使用这两种方法都能成功构建: 标准的 VS Code CMake 工具构建任务。 命令行版本: cmake --build .\dbe_flexspi_nor_debug --parallel 禁用 MCUXpresso 扩展的 Windows 长路径警告可以彻底解决此问题。 重现步骤 在 Windows 11 上的 VS Code 中打开一个 MCUXpresso SDK v2 独立项目。 使用包含自定义配置和版本预设的有效CMakePresets.json文件。 使用 CMake 成功配置项目。 确保生成的编译数据库( compile_commands.json )包含没有output属性的条目。 从 MCUXpresso 扩展 GUI调用版本项目。 实际结果:版本操作失败,并显示以下错误信息: The "path" argument must be of type string. Received undefined 预期结果: MCUXpresso 应接受没有输出属性的有效编译数据库条目,并成功执行构建任务。 根本原因分析 使用 Chrome DevTools 对扩展程序捆绑的extension.js进行调查后发现,故障发生在 Windows 长路径验证期间,也就是在执行实际版本任务之前。 相关代码遍历编译数据库条目: for (const entry of result.getDomainEntries()) { if (!entry.error) { if (entry.jsonData.some(item => checkPath(item))) return true; } } 路径检查函数(在压缩包中名为_S )包含等价于以下逻辑: function checkPath(entry) { const outputPath = path.isAbsolute(entry.output) ? entry.output : path.join(entry.directory, entry.output); return isLongPath(entry.file) || isLongPath(outputPath); } 在 JSON 编译数据库格式中,输出属性是可选的。一个有效的条目只能包含目录、命令和文件。 但是,该扩展程序直接将entry.output传递给path.isAbsolute(),而没有验证该属性是否存在。 对于没有输出的条目,这实际上就变成了: path.isAbsolute(undefined); Node.js 抛出TypeError,该错误会传播到 MCUXpresso 版本操作中,并阻止版本任务运行。 这似乎是该扩展程序的长路径验证逻辑中的一个错误。 已确认的解决方法 将以下设置添加到工作区的.vscode/settings.json文件中: { "mcuxpresso.long.path.warn": false } 结果: MCUXpresso GUI 版本命令成功完成。 这证实了故障与扩展程序的长路径验证有关。禁用此警告不需要对 CMake 配置或构建工具链进行任何更改。 建议的修复方案 该扩展程序应处理没有输出属性的编译数据库条目。 可能的方法包括: 在调用path.isAbsolute()或path.join()之前,检查entry.output是否为非空字符串。 如果缺少输出,则跳过该条目的输出路径验证,同时继续验证源文件路径。 或者,尽可能根据可用的编译元数据确定输出路径。 有效的编译数据库中缺少可选字段绝不应导致“版本项目”命令失败。 更多信息 使用自定义 CMake 预设和成功配置的 MCUXpresso SDK 项目重现了该问题。在整个调查过程中,版本通过 CMake 工具和命令行完成。 解决方法已验证:将mcuxpresso.long.path.warn设置为false可恢复通过 MCUXpresso GUI 成功构建。 报告的根本原因基于对扩展程序捆绑的 JavaScript 的静态检查和调试器观察结果。未独立捕获到触发信号异常的具体编译数据库记录。 请考虑在 MCUXpresso for VS Code 扩展的未来版本中修复此问题。 Re: Cmake Build Long Paths Issue 嗨@alexander_safonov , 感谢您的耐心等待并报告此问题。 我已经与内部团队确认,他们已经意识到这个问题,并计划在未来的更新中解决。 再次感谢您宝贵的反馈和理解。   祝你今天过得愉快。   顺祝商祺! 刘梅
View full article
MPC8308CVMAFD Vs MPC8308CVMAFDA Hi, We would like to seek your technical expertise regarding the following part numbers: MPC8308CVMAFD MPC8308CVMAFDA Could you please clarify whether there are any differences between these two part numbers? According to the datasheet, the additional letter “A” indicates a revision level. However, we could not find any further information explaining the specific revision or its impact on the device. We would appreciate your confirmation on whether these two part numbers are electrically and functionally equivalent and interchangeable. Thank you very much for your assistance. Re: MPC8308CVMAFD Vs MPC8308CVMAFDA ### 1. Difference Between the Two Part Numbers The only difference between **MPC8308CVMAFD** and **MPC8308CVMAFDA** is the **internal silicon stepping / revision**: * **`MPC8308CVMAFD`**: Represents **Silicon Revision 1.0**. * **System Version Register (SVR):** `0x8101_0110` * **`MPC8308CVMAFDA`**: Represents **Silicon Revision 1.1** (the trailing letter **“A”** designates Rev 1.1 in Freescale/NXP’s part numbering scheme). * **System Version Register (SVR):** `0x8101_0111` Both devices share identical nominal parameters: * **Package:** 473-pin MAPBGA (19 mm × 19 mm, 0.8 mm pitch) * **Temperature Grade:** Extended / Industrial (`C` = -40°C to 105°C $T_j$) * **Core Frequency:** 333 MHz (`AF`) * **DDR Data Rate:** 266–333 MHz (`D`) * **Lead-free / RoHS:** Pb-free MAPBGA (`VM`) --- ### 2. Hardware Equivalence (Form, Fit, Function) * **Electrically & Mechanically:** **100% Pin-to-Pin and Drop-in Equivalent.** * No PCB layout, schematic, routing, power supply, or decoupling changes are required. * Ball assignments, voltage rails ($V_{DD} = 1.0\text{V}$, $G_{VDD} = 1.8\text{V}$, $N_{VDD} = 3.3\text{V}$), I/O drive strengths, and AC/DC timing specifications are identical. --- ### 3. Silicon Differences & Software Impact Silicon Revision 1.1 (`MPC8308CVMAFDA`) was released to incorporate minor internal bug/errata fixes over Revision 1.0. For 99% of applications, **Rev 1.1 is fully backward-compatible with Rev 1.0**. However, keep the following two software considerations in mind: 1. **System Version Register (SVR) Checks:** * If your bootloader (U-Boot), kernel, or proprietary firmware explicitly reads and matches the exact 32-bit SVR value: * Rev 1.0 returns `0x8101_0110` * Rev 1.1 returns `0x8101_0111` * Ensure any hardware revision checks in your code mask out or accept the lower 4 bits (e.g., matching against `0x8101_011x` or checking $\ge \text{Rev } 1.0$) so the boot sequence does not halt. 2. **Silicon Errata Workarounds:** * Several known errata present in Rev 1.0 were resolved or improved in Rev 1.1 (documented in the *MPC8308 Chip Errata*, document `MPC8308CE`). * Software workarounds implemented in firmware for Rev 1.0 will continue to operate harmlessly on Rev 1.1. --- ### Summary Recommendation **MPC8308CVMAFDA is the direct, recommended replacement for MPC8308CVMAFD.** They are form, fit, and functional drop-in replacements. You can safely substitute `MPC8308CVMAFDA` without board redesign, provided your firmware does not hardcode an exact match check on the SVR register.
View full article
Cmake Build Long Paths Issue Bug: MCUXpresso VS Code extension fails to build a valid CMake project due to missing output field in compile_commands.json Product: MCUXpresso for VS Code Component: MCUXpresso extension — Build Project / Windows long-path validation Host OS: Windows 11 Target MCU: NXP i.MX RT1186 (Cortex-M33) Build system: CMake + Ninja Extension version: 26.9.44 Severity: Build operation blocked; workaround available Problem description The MCUXpresso VS Code extension fails to build an otherwise valid CMake project when using the extension's Build Project command. The following error is displayed: The "path" argument must be of type string. Received undefined The error occurs inside the MCUXpresso extension's JavaScript code, rather than in the CMake configuration or build process. The same project builds successfully using both: The standard VS Code CMake Tools build task. The command-line build: cmake --build .\dbe_flexspi_nor_debug --parallel Disabling the MCUXpresso extension's Windows long-path warning completely resolves the issue. Steps to reproduce Open an MCUXpresso SDK v2 freestanding project in VS Code on Windows 11. Use a valid CMakePresets.json containing custom configure and build presets. Configure the project successfully using CMake. Ensure that the generated compilation database (compile_commands.json) contains entries without an output property. Invoke Build Project from the MCUXpresso extension GUI. Actual result: The build operation fails with: The "path" argument must be of type string. Received undefined Expected result: MCUXpresso should accept valid compilation database entries without an output property and execute the build task successfully. Root cause analysis Investigation of the extension's bundled extension.js using Chrome DevTools revealed that the failure occurs during Windows long-path validation, before execution of the actual build task. The relevant code iterates over compilation database entries: for (const entry of result.getDomainEntries()) { if (!entry.error) { if (entry.jsonData.some(item => checkPath(item))) return true; } } The path-checking function (named _S in the minified bundle) contains logic equivalent to: function checkPath(entry) { const outputPath = path.isAbsolute(entry.output) ? entry.output : path.join(entry.directory, entry.output); return isLongPath(entry.file) || isLongPath(outputPath); } The output property is optional in the JSON Compilation Database format. A valid entry may contain only directory, command, and file. However, the extension passes entry.output directly to path.isAbsolute() without verifying that the property exists. For entries without output, this effectively becomes: path.isAbsolute(undefined); Node.js throws a TypeError, which propagates through the MCUXpresso build operation and prevents the build task from running. This appears to be a bug in the extension's long-path validation logic. Confirmed workaround Add the following setting to the workspace's .vscode/settings.json: { "mcuxpresso.long.path.warn": false } Result: The MCUXpresso GUI Build command completes successfully. This confirms that the failure is associated with the extension's long-path validation. Disabling the warning does not require any changes to the CMake configuration or build toolchain. Suggested fix The extension should handle compilation database entries without an output property. Possible approaches include: Check whether entry.output is a non-empty string before calling path.isAbsolute() or path.join(). If output is missing, skip output-path validation for that entry while continuing to validate the source file path. Alternatively, determine the output path from available compilation metadata when possible. Missing optional fields in a valid compilation database should never cause the Build Project command to fail. Additional information The issue was reproduced with custom CMake presets and a successfully configured MCUXpresso SDK project. The build worked through CMake Tools and the command line throughout the investigation. The workaround was verified: setting mcuxpresso.long.path.warn to false restored successful builds through the MCUXpresso GUI. The reported root cause is based on static inspection of the extension's bundled JavaScript and debugger observations. The specific compilation database record triggering the exception was not independently captured. Please consider fixing this in a future release of the MCUXpresso for VS Code extension. Re: Cmake Build Long Paths Issue Hi @alexander_safonov , Thank you for your patience and for reporting this issue. I have confirmed with our internal team that the issue has been acknowledged and is planned to be addressed in a future update.  Thank you again for your valuable feedback and understanding.   Wish you a nice day.   Best Regards May Liu
View full article
P3B1602 I2C/I3C PCIe CEM 规范符合 尊敬的论坛成员: PCIe CEM 规范 6.0.1 版定义了 SMBus (I2C) 为 3.3V 和 I3C 为 1.8V。 P3B1602在I2C模式下是否支持3.3V(内部电阻接至3.3V),在I3C模式下是否支持1.8V? 我想,为了同时满足这两种模式,P3B1602 的供电电压需要改变,对吗? 谢谢。 此致敬礼 莫里茨 Re: P3B1602 I2C/I3C PCIe CEM Spec Compliant 郭老师您好,  谢谢你的解释。 我可以将两个 P3B1602 并联使用在同一条 SCL 和 SDA 线上,但分别采用 1.8V 和 3.3V 的 VCCB 供电吗? 只需要拔掉我需要激活的那个引脚,用原厂引脚连接即可? 亲切的问候 莫里茨 Re: P3B1602 I2C/I3C PCIe CEM Spec Compliant 嗨,莫里茨 P3B1602 支持两种电压等级,但如果同一 B 侧总线需要在 3.3 V SMBus/I²C 和 1.8 V I3C 之间切换,则必须切换相应的 VCCB,并且必须验证所有外部上拉电阻和连接设备的电平要求。 谢谢您! BR Re: P3B1602 I2C/I3C PCIe CEM Spec Compliant 嗨,莫里茨 请您提供一下连接图,以便我更好地理解!BR Re: P3B1602 I2C/I3C PCIe CEM Spec Compliant 嗨,莫里茨 可通过 OE 选择 1.8 V 或 3.3 V 通道。然而,OE 不仅仅是一个简单的软件信号选择;它必须确保互斥性、默认关闭状态和切换死区。 Re: P3B1602 I2C/I3C PCIe CEM Spec Compliant 嗨,莫里茨 请您提供一下连接图,以便我更好地理解!BR Re: P3B1602 I2C/I3C PCIe CEM Spec Compliant 郭老师您好, 我认为这可以在FPGA中处理。 总之,如果能保证互斥性,并在启用操作之间设置延迟,您认为就没有问题了吧? 为了清晰起见,我省略了下拉电阻。 亲切的问候 莫里茨 Re: P3B1602 I2C/I3C PCIe CEM Spec Compliant 郭老师您好,  我的计划大致如下。 亲切的问候 莫里茨 Re: P3B1602 I2C/I3C PCIe CEM Spec Compliant 嗨,莫里茨 如果这些 B 侧引脚没有外部上拉电阻,应该就没问题。
View full article
P3B1602 I2C/I3C PCIe CEM Spec Compliant Dear Forum, PCIe CEM Spec Revision 6.0.1 defines SMBus (I2C) with 3.3V and I3C with 1.8V Does the P3B1602 support 3.3V in I2C mode (internal resistors to 3.3V) and 1.8V in I3C Mode?   I suppose to comply to both modes the supply voltage of P3B1602 needs to be changed, right?  Thank you.  Kind regards Moritz Re: P3B1602 I2C/I3C PCIe CEM Spec Compliant Hi Guo,  thank you for the clarification. Can I use 2 P3B1602 in parallel on the same SCL and SDA nets but with 1.8V and 3.3V VCCB Supply.  Just pulling only the one I need active with the OE pin? Kind regards Moritz Re: P3B1602 I2C/I3C PCIe CEM Spec Compliant HI Moritz P3B1602 supports both voltage levels, but if the same B-side bus needs to switch between 3.3 V SMBus/I²C and 1.8 V I3C, the corresponding VCCB must be switched, and all external pull-up resistors and connected devices' level requirements must be verified. Thanks! BR Re: P3B1602 I2C/I3C PCIe CEM Spec Compliant Hi Guo,  my plan looks like this.  Kind regards Moritz Re: P3B1602 I2C/I3C PCIe CEM Spec Compliant Hi Moritz Could you please give your connection diagram for better understand! BR Re: P3B1602 I2C/I3C PCIe CEM Spec Compliant Hi Guo, I think this can be handled in the FPGA. In summay, if the mutual exclusivity is ensured and a delay between enables is implemented, you see no issue correct? I've omitted the pull down resistors for clarity. Kind regards Moritz Re: P3B1602 I2C/I3C PCIe CEM Spec Compliant HI Moritz The 1.8 V or 3.3 V channels can be selected through OE. However, OE is not just a simple software signal selection; it must ensure mutual exclusivity, default off state, and switching dead zone. Re: P3B1602 I2C/I3C PCIe CEM Spec Compliant Hi Moritz Could you please give your connection diagram for better understand! BR Re: P3B1602 I2C/I3C PCIe CEM Spec Compliant Hi Moritz If there is no external pull up for these B side pins, it should be no problem.
View full article
i.MX 8MPlus (m865S) DDR 寄存器编程辅助工具 (RPA)   这是针对与 i.MX 8M Plus DDR 初始化相关寄存器的详细编程辅助资料。 LPDDR4 DDR4  如需更多详细信息,请参阅 mScale DDR 工具主页面: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/1104467 请注意,此页面仅用于存储 RPA 电子表格。如有疑问,请创建新的社区主题。 i.MX 8M | i.MX 8M Mini | i.MX 8M Nano
View full article
i.MX 8MPlus (m865S) DDR Register Programming Aids (RPA)   This is a detailed programming aid for the registers associated with i.MX 8M Plus DDR initialization. LPDDR4 DDR4  For more details, refer to the main mScale DDR tools page: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/1104467 Please note that this page is only intended to store the RPA spreadsheets. For questions, please create a new community thread. i.MX 8M | i.MX 8M Mini | i.MX 8M Nano
View full article
i.MX 8MPlus (m865S) DDR レジスタプログラミング支援 (RPA)   これは、i.MX 8M Plus DDR 初期化に関連するレジスタの詳細なプログラミング支援です。 LPDDR4 DDR4 詳細については、mScale DDR ツールのメインページをご参照ください。 https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/1104467 このページは、RPAスプレッドシートの保存のみを目的としていることに注意してください。ご不明な点がございましたら、新しいコミュニティスレッドを作成してください。 i.MX 8M | i.MX 8M Mini | i.MX 8M Nano
View full article