Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
i.MX RT1180 EtherCAT Interface Design Explained 1. Overview This article describes the signal functions and connection recommendations for the i.MX RT1180 EtherCAT interface, covering PHY selection, clock and reset signals, MII/RMII interfaces, synchronization and latch signals, and status indication signals. It serves as a reference for EtherCAT hardware design. 2. PHY Selection The i.MX RT1180 EtherCAT controller uses Beckhoff IP. PHY selection must comply with the requirements in Beckhoff's PHY Selection Guide, available at the following link: https://download.beckhoff.com/download/document/io/ethercat-development-products/an_phy_selection_guidev3.2.pdf The i.MX RT1180 EtherCAT controller supports MII/RMII interfaces. Therefore, select a PHY that supports the corresponding interface; do not use a PHY that supports only RGMII. 3. EtherCAT Interface Signals and Connection Recommendations ECAT Signal Description and Recommendations CLKOUT25M Configuring the pin for the CLKOUT25M function enables a 25 MHz clock output. This clock shares the same source as ECAT_CLK_ROOT and requires no additional register configuration for clock division. It is strongly recommended to connect this signal to the XTAL inputs of both PHYs for better clock synchronization. If this signal is not used, an external 25 MHz clock source must be provided for the PHYs. RESET_OUT This signal must be connected to the reset inputs of both PHYs. If PHY reset is controlled only through a GPIO, the PHYs cannot be reset through the EtherCAT protocol. RESET_OUT is active high. If the PHY reset input is active low, additional inverting logic is required. SCL, SDA Connect to an external EEPROM. MDC,MDIO PHY management interface used to access the registers of a PHY based on its address. In i.MX RT1180 EtherCAT applications, the hardware addresses of the two PHYs must be consecutive. (MII/RMII Interface) MII (Recommended) RMII PT0_RX_CLK/PT1_RX_CLK Connect to the RX_CLK pin of PHY0/PHY1 Refer to the selected PHY's datasheet: if REF_CLK is provided through its RX_CLK pin, connect to that pin and leave TX_CLK unconnected. PT0_RX_DV/PT1_RX_DV Connect to the RX_DV pin of PHY0/PHY1 PT0_RX_ER/PT1_RX_ER Connect to the RX_ER pin of PHY0/PHY1 PT0_RXD_0/PT1_RXD_0 Connect to the RXD_0 pin of PHY0/PHY1 PT0_RXD_1/PT1_RXD_1 Connect to the RXD_1 pin of PHY0/PHY1 PT0_RXD_2/PT1_RXD_2 Connect to the RXD_2 pin of PHY0/PHY1 Leave unconnected PT0_RXD_3/PT1_RXD_3 Connect to the RXD_3 pin of PHY0/PHY1 Leave unconnected PT0_TX_CLK/PT1_TX_CLK Connect to the TX_CLK pin of PHY0/PHY1 Refer to the selected PHY's datasheet: if REF_CLK is provided through its TX_CLK pin, connect to that pin and leave RX_CLK unconnected. PT0_TX_EN/PT1_TX_EN Connect to the TX_EN pin of PHY0/PHY1 PT0_TXD_0/PT1_TXD_0 Connect to the TXD_0 pin of PHY0/PHY1 PT0_TXD_1/PT1_TXD_1 Connect to the TXD_1 pin of PHY0/PHY1 PT0_TXD_2/PT1_TXD_2 Connect to the TXD_2 pin of PHY0/PHY1 Leave unconnected PT0_TXD_3/PT1_TXD_3 Connect to the TXD_3 pin of PHY0/PHY1 Leave unconnected LINK_MII_0/LINK_MII_1 Connect to the Link Status outputs of PHY0/PHY1, respectively. Refer to the selected PHY's datasheet for the specific pins. These signals must be connected; otherwise, EtherCAT will not function properly. SYNC_OUT_0/SYNC_OUT_1 Two hardware synchronization output signals generated by the EtherCAT Distributed Clocks, corresponding to SYNC0 and SYNC1, respectively. Whether to route these signals out depends on the application requirements. LATCH_IN_0/LATCH_IN_1 External event input signals used to latch the current Distributed Clock System Time when an event occurs. These signals may be left unconnected if not used. LED_ERR,LED_RUN,LED_STATE_RUN EtherCAT status indication LED signals. LINK_ACT_0/LINK_ACT_1 Indicate the link and activity status of the EtherCAT slave. Connect to the Link/Activity LEDs for Port 0/Port 1, respectively. It is important to distinguish between the following two types of signals: LINK_MII_0/LINK_MII_1: Link Status signals from the PHYs that reflect the link status. These are input signals to the EtherCAT controller. LINK_ACT_0/LINK_ACT_1: Link and activity status signals output by the EtherCAT controller to drive the Link/Activity LEDs. The link and activity status LEDs can be controlled by either the ESC or the PHY, at the designer's discretion.
View full article
FRDM-MCXE32B: Hands-On Prerequisites Introduction This document guides you through installing the tools and materials required for the FRDM-MCXE32B hands-on labs. Required Materials The hardware and software requirements may vary by exercise, but the following items are required for most hands-on labs. Hardware Requirements FRDM-MCXE32B board                  Personal computer USB Type-C cable Software Requirements MCUXpresso Installer (Recommended) IDE: Visual Studio Code (latest version) SDK: v26.09.00 or later MCUXpresso extension for VS Code (latest version) LinkFlash tool (included with the LinkServer installation) Windows operating system (these hands-on labs were developed and tested on Windows 11) Hands-On Prerequisites Guide. Hands-On Training
View full article
S32 设计工作室许可证已过期 尊敬的恩智浦: S32 Design Studio 3.5 许可证即将到期。 请问您能否帮忙延长许可证期限? 谢谢。 激活ID:29E6-6248-FCB2-DBB6 Re: S32 Design Studio License Expired 你好, 您的S32DS许可证已延期。请使用您之前的激活码重新激活S32DS。
View full article
更新和构建 S32K344 应用程序代码中心示例时出错 我正在尝试按照这个演示教程操作 FRDM S32K344 板: https://mcuxpresso.nxp.com/appcodehub?search=dm-adc-profiling-freemaster-s32k344 我已经安装了正确的软件依赖项,但是当我尝试点击“更新代码并版本项目”时,出现以下错误。我已经尝试重启我的电脑和S32DS,重新创建一个新的工作区,并检查了其他扩展程序,但都无法解决这个错误。非常感谢您的支持! Re: Errors Updating & Building S32K344 App Code Hub Example 您好, 示例说明指出,此示例是使用 FRDM Automotive Bundle for S32K3 + S32M27 开发的。 以下列出的驱动程序并非全部都在本示例中使用。但是,至少以下两个软件包必须正确安装在 S32DS 3.6.8 中。加载演示之前: S32K3 实时驱动程序 AUTOSAR 4.9,版本 7.0.1 S32K3 FreeMASTER 驱动程序 请确保这些软件包已正确安装在您的 S32DS 3.6.x 版本中。环境。 驱动程序安装成功后,即可从 ACH 正常加载给定的示例,并执行 UpdateCode 和版本命令。 BR,彼得   Re: Errors Updating & Building S32K344 App Code Hub Example 更正我之前的回复。为了使 S32K344 演示环境正常运行,需要进行以下设置更改: 下载所需的软件包和 Design Studio 更新站点 ZIP 文件。 在 S32DS 3.6.x 中,打开扩展和更新 → 添加更新站点。 添加每个 ZIP 文件,关闭“添加更新站点”对话框,选择可用元器件,然后单击“安装” 。 安装完成后重启S32DS。 在安装任何 RTD 相关软件包之前,请先安装完整的 S32K3/S32M27x RTD 7.0.1 基本软件包。 创建项目时请使用 GCC 10.2 工具链。 工作包内含: S32K3xx 开发包 S32K3 FreeMASTER 串行通信驱动程序 S32K3 RTD AUTOSAR R23-11 版本 7.0.1 S32K3_S32M27x RTD AUTOSAR R23-11 版本 7.0.1 S32K3XX RTD AUTOSAR R23-11 版本 7.0.1 AMMCLIB 适用于 S32K3xx/S32M27x,RTD 相关 适用于 S32K3xx 的 FreeRTOS 重要提示: QLP06/P02 是一个附加软件包,而不是完整的 RTD。请勿单独安装 QLP06/P02。首先安装基本 RTD 软件包,然后仅在需要时才安装 QLP06/P02。单独安装会产生以下结果: 缺少必需依赖项:com.nxp.RTD.S32K3_S32M27X 0.0.0 对于这个特定的 S32K344 演示,所需的最低软件包是基本的 S32K3 RTD 7.0.1 软件包和 S32K3 FreeMASTER 驱动程序。其他软件包是更大软件包的一部分,或者可能是项目依赖项所必需的。本 S32K344 演示不需要 K39xx RTD 软件包。 Re: Errors Updating & Building S32K344 App Code Hub Example 你好,彼得。 非常感谢您的回复。我按照您的指示操作,但在 K39xx R23-11 RTD 软件包上收到以下错误: 演示真的需要这个吗?因为软件包里只提到了 S32K3 9 x,而没有提到 S3K3 4 x。 最好的, Andrew Re: Errors Updating & Building S32K344 App Code Hub Example 您好, 我理解您对RTD包装编号和描述的疑虑。 您也说得对,7.0.1.QLP5/6/P02 是包含加密驱动程序的附加软件包。这些软件包必须安装在基础 S32K3 RTD 7.0.1 软件包之上。 但是,ACH 演示会引导您使用汽车软件包管理器和FRDM 汽车 S32K3 + S32M27 板安装包。如果您选择实时驱动程序 7.0.1 ,你可以看到它所代表的确切文件。 如果允许软件包管理器生成捆绑安装程序,它将选择正确的软件包进行安装。没错,并非所有这些软件包对于这个特定示例都是必需的;如前所述,只需要 RTD 和 FreeMASTER 驱动程序。 如果在软件库中找到了所需的文件,请在软件包管理器中搜索显示的确切名称,以识别正确的软件包。 关于 S32K3 RTD 7.0.1 软件包的安装,它包含四个驱动程序。本 S32K344 ADC 示例不需要 S32K39x 和 S32M27x 驱动程序。但是,强烈建议安装所有四个驱动程序,主要是因为未来的更新可能取决于基础软件包。 BR,彼得  
View full article
漏洞:dw-mipi-dsi:在非突发DSI桥接器上720p60分辨率输出异常 你好, 我们发现 NXP 下游内核 (lf-6.18.y) 存在问题,我们认为问题是由以下原因造成的: ▎ LF-14666-2:drm/bridge:synopsys:dw-mipi-dsi:实现 720p60 的修复 在 i.MX95 上使用 TI SN65DSI86(DSI 转 DisplayPort)时,720p60 会出现图像闪烁。 在非突发模式下,DSI_VID_HLINE_TIME 为 htotal * bpp / (lanes * 😎 通道字节时钟周期,如果不是整数则向上取整。对于 4 通道 RGB888 的 720p60,数值为 1237.5,四舍五入为 1238。这样一来,DSI 线就比 DPI 线长,误差会在帧内累积。只有在 HFP 期间返回 LP 才会将每行的行计时器与 DPI 重新同步。 Mainline 始终在 HFP 中启用 LP。LF-14666-2 将其设为可选的,仅当 DSI 设备设置 MIPI_DSI_MODE_VIDEO_NO_HFP 时才可设置。这对于 LT8912B 来说是有效的,因为 LF-14666-1 向该驱动程序添加了标志。但是舍入操作来自主机控制器,而不是设备,因此,只要线路时间为小数,所有其他未设置标志的桥接器或面板(例如 SN65DSI86)现在都会中断。 我已在邮件中附上一个补丁,可以解决我们遇到的问题,如果有人能帮忙看一下,我将不胜感激。 谢谢, 安托万·古比 Linux
View full article
BUG: dw-mipi-dsi: 720p60 broken on non-burst DSI bridges Hello, We have an issue with the NXP downstream kernel (lf-6.18.y) that we think is caused by: ▎ LF-14666-2: drm/bridge: synopsys: dw-mipi-dsi: Implement fixup for 720p60 On i.MX95 with a TI SN65DSI86 (DSI to DisplayPort), 720p60 gives a flickering image. In non-burst mode, DSI_VID_HLINE_TIME is htotal * bpp / (lanes * 😎 lane byte clock cycles, rounded up when that isn't an integer. For 720p60 on 4 lanes with RGB888 that's 1237.5, rounded to 1238. The DSI line is then longer than the DPI line, and the error builds up over the frame. Only returning to LP during HFP resyncs the line timer to DPI on every line. Mainline always enables LP in HFP. LF-14666-2 made it optional, only when the DSI device sets MIPI_DSI_MODE_VIDEO_NO_HFP. That works for LT8912B, because LF-14666-1 adds the flag to that driver. But the rounding comes from the host controller, not from the device, so every other bridge or panel that doesn't set the flag (SN65DSI86 for example) is now broken whenever the line time is fractional. I attached to this message a patch the corrects the issue for us, I would appreciate if anyone can take a look at this. Thanks, Antoine Gouby Linux
View full article
imx93:SRK撤销 你好, 我正在尝试对我的已关闭的imx93板执行密钥撤销操作。 我的脑脊液文件内容如下: [标题] 目标 = AHAB 版本 = 1.0 [安装SRK] 文件 = "../cst-3.4.0/crts/SRKtable.bin" 来源 = "../cst-3.4.0/crts/SRK2_sha384_secp384r1_v3_usr_crt.pem" 来源索引 = 1 源集 = OEM 撤销次数 = 0x1 [验证数据] 文件 = "spl.bin" 偏移量 = 0x400 0x490 其思路是使用 SRK2 进行签名,并撤销 SRK1(0x1 位掩码)。从该镜像启动可以正常工作,但我仍然可以从使用 SRK1 签名的镜像启动。 撤销 SRK1 还需要做其他什么吗? 谢谢! 马蒂厄 Re: imx93: SRK revocation 您好,我也在研究 i.MX93 上的 SRK 撤销,谢谢您的提示。ahab_commit 0x10 的确是使撤销生效的原因,但我对其输出以及如何在现场设备上使用它有一个疑问。 在一台封闭的 i.MX93 上,我启动了第一个镜像,该镜像包含一个容器,该容器使用 SRK 表的第一个密钥 (SRK0) 和第四个密钥(掩码 0x8,SRK3)的撤销位进行签名,但撤销尚未应用,然后从 u-boot 控制台运行了 ahab_commit 0x10: - 第一次提交回答“Ahab 提交成功”。信息类型为 0x10”,然后第 4 个密钥似乎被撤销了:用该密钥签名的镜像(在提交之前启动)之后被拒绝; - 之后,连续三次运行完全相同的命令(相同的参数,相同的 u-boot),总是回答“Ahab commit 成功”。信息类型为 0x0,ahab_status 中没有事件。 “信息类型”值是什么意思?这是实际已执行操作的掩码吗?所以 0x0 表示没有什么需要执行的?据我所知,没有其他方法可以知道撤销是否仍在进行中(撤销前后可读的熔丝组和 ele_info 完全相同)。 这对于现场设备来说很重要,因为没有人可以在 u-boot 控制台中输入命令:提交必须由 u-boot 自动运行(启动命令)。该命令应该只运行一次(需要添加一个标志来跟踪它),还是可以每次启动时都将其保留在启动命令中?我更倾向于第二种方案,这样即使跳过了某些更新版本,任何新版本都可以包含撤销信息。 谢谢您! Re: imx93: SRK revocation 成功了,谢谢。不过,我必须添加对 ahab_commit 主线版本的支持: https://lists.denx.de/pipermail/u-boot/2024-March/548873.html Re: imx93: SRK revocation 检查是否缺少步骤 ahab_commit 0x10 此致 哈维
View full article
imx93: SRK revocation Hello, I am trying to perform key revocation on my closed imx93 board. My CSF file looks like: [Header] Target = AHAB Version = 1.0 [Install SRK] File = "../cst-3.4.0/crts/SRKtable.bin" Source = "../cst-3.4.0/crts/SRK2_sha384_secp384r1_v3_usr_crt.pem" Source index = 1 Source set = OEM Revocations = 0x1 [Authenticate Data] File = "spl.bin" Offsets = 0x400 0x490 The idea is to sign with SRK2 and revoke SRK1 (0x1 bitmask). Booting from that image works fine, but I can still also boot from an image signed with SRK1. Is there anything else that needs to be done in order to revoke SRK1? Thanks, Mathieu Re: imx93: SRK revocation Hello, I am working on SRK revocation on i.MX93 too, and thanks for the hint. ahab_commit 0x10 is indeed what makes the revocation effective, but I have a question about its output and about how to use it on devices in the field. On a closed i.MX93, I booted the first image carrying a container signed with the first key of the SRK table (SRK0) and with the revoke bit of the 4th key (mask 0x8, SRK3), with the revocation not yet applied, and ran ahab_commit 0x10 from the u-boot console: - this first commit answered "Ahab commit succeeded. Information type is 0x10", and the 4th key then seems to be revoked: an image signed with it, which booted before the commit, is refused afterwards; - after that, running exactly the same command again (same argument, same u-boot), three times in a row, always answers "Ahab commit succeeded. Information type is 0x0", with no events in ahab_status. What does the "Information type" value mean? Is it the mask of what has actually been committed, so 0x0 means nothing was left to commit? As far as I can see there is no other way to know whether a revocation is still pending (the readable fuse banks and ele_info are identical before and after). This matters for devices in the field, where nobody can type the command in the u-boot console: the commit has to be run automatically by u-boot (boot command). Should it be run only once, which would need a flag to track it, or is it fine to leave it in the boot command at every boot? I would prefer the second option, so that any new build can carry the revocation even if some update version was skipped. Thanks! Re: imx93: SRK revocation That worked thanks. I had to add support for ahab_commit mainline though: https://lists.denx.de/pipermail/u-boot/2024-March/548873.html Re: imx93: SRK revocation check if missing the step ahab_commit 0x10 Regards Harvey
View full article
バグ:dw-mipi-dsi:非バーストDSIブリッジで720p60が壊れています こんにちは、 NXPのダウンストリームカーネル(lf-6.18.y)に問題が発生しており、その原因は以下の通りだと考えています。 ▎ LF-14666-2: drm/bridge: synopsys: dw-mipi-dsi: 720p60 の修正を実装 TI SN65DSI86(DSI-DisplayPort変換アダプタ)を搭載したi.MX95では、720p60で画像がちらつく。 非バーストモードでは、DSI_VID_HLINE_TIME は htotal * bpp / (lanes * 😎 レーンバイトクロックサイクル。整数でない場合は切り上げ。720p60で4レーン、RGB888の場合、1237.5となり、四捨五入すると1238になります。DSIラインはDPIラインよりも長くなり、フレーム全体にわたって誤差が蓄積されていく。HFP中にLPに戻った場合のみ、すべてのラインでラインタイマーがDPIに再同期されます。 メインラインでは常にHFPでLPが有効になります。LF-14666-2では、DSIデバイスがMIPI_DSI_MODE_VIDEO_NO_HFPを設定した場合のみ、これをオプションにしました。これはLT8912Bに合っています。なぜならLF-14666-1はそのドライバにフラグを追加するからです。しかし、丸めはデバイスではなくホストコントローラから来ているため、フラグを設定しない他のブリッジやパネル(例えばSN65DSI86)は、ライン時間が分数になると壊れてしまいます。 このメッセージに問題を修正するパッチを添付しました。どなたか見ていただけるとありがたいです。 ありがとう、 アントワーヌ・グビー Linux
View full article
imx93: SRKの取り消し こんにちは、 私は、閉鎖済みのimx93ボード上で鍵の失効処理を実行しようとしています。 私のCSFファイルは次のようになっています。 [ヘッダ] ターゲット=アハブ バージョン = 1.0 [SRKをインストール] ファイル = "../cst-3.4.0/crts/SRKtable.bin" ソース = "../cst-3.4.0/crts/SRK2_sha384_secp384r1_v3_usr_crt.pem" ソースインデックス = 1 ソースセット = OEM 取り消し = 0x1 [データの認証] ファイル = "spl.bin" オフセット = 0x400 0x490 このアイデアはSRK2に署名し、SRK1(0x1ビットマスク)を取り消すことです。そのイメージから起動しても問題ありませんが、SRK1で署名されたイメージからも起動できます。 SRK1の資格を取り消すために、他に何か必要な手続きはありますか? ありがとうございます マチュー Re: imx93: SRK revocation こんにちは。私もi.MX93でSRKの失効処理に取り組んでおり、ヒントをありがとうございます。ahab_commit 0x10 は確かに失効を有効にするものですが、その出力と、現場のデバイスでどのように使用するかについて質問があります。 閉じた状態の i.MX93 上で、SRK テーブルの最初のキー (SRK0) と 4 番目のキーの失効ビット (マスク 0x8、SRK3) で署名されたコンテナを含む最初のイメージを起動し、失効処理はまだ適用されていません。そして、u-boot コンソールから ahab_commit 0x10 を実行しました。 - この最初のコミットは「Ahab コミットが成功しました」と回答しました。情報タイプは「0x10」であり、4番目のキーが失効したようです。コミット前に起動した、そのキーで署名されたイメージは、その後拒否されます。 その後、まったく同じコマンド(同じ引数、同じ u-boot)を 3 回連続で実行すると、常に「Ahab コミットが成功しました」という応答が返されます。情報タイプは0x0」であり、ahab_statusにイベント情報はありません。 「情報タイプ」の値は何を意味しますか?それは実際に犯されたことの仮面で、犯すことが何も残っていない0x0なのでしょうか?私の知る限り、取り消しがまだ保留中かどうかを知る他の方法はない(ヒューズバンクとele_infoは前後で同一です)。 これは現場のデバイスで重要で、u-bootコンソールでコマンドを入力できないため、コミットはu-boot(起動コマンド)によって自動的に実行されなければなりません。一度だけ実行するようにすれば、それを追跡するためのフラグが必要になりますが、それとも毎回起動時のブートコマンドに含めておいても問題ありませんか?私は後者の方が好みです。そうすれば、新しいビルドはアップデートバージョンがスキップされていても取り消しを継続できるからです。 よろしくお願いします! Re: imx93: SRK revocation うまくいきました、ありがとうございます。ただ、メインラインのサポートahab_commit追加しなければなりませんでした: https://lists.denx.de/pipermail/u-boot/2024-March/548873.html Re: imx93: SRK revocation ahab_commit 0x10 のステップが欠落していないか確認します よろしくお願いします。 Harvey
View full article
S32G399A octal DTR reads fail with Macronix MX66UM2G45G QSPI flash Hi Community, We have a custom board based on the S32G399A-RDB3 reference design. The main change to the boot flash is that we replaced the MX25UW51245G (64 MB) with a Macronix MX66UM2G45G (256 MB, 1.8 V octal, JEDEC ID C2 80 3C). Everything works in 1-1-1 SPI. We cannot get 8D-8D-8D (octal DTR) reads to return correct data, and we would like help from NXP. We also could not find this part in any S32 BSP release up to bsp48.0, although AMD's U-Boot has supported it since 2024.1. Software TF-A bsp43.0-2.10.7, U-Boot bsp43.0-2022.04, Linux bsp43.0 (6.6.52) BootROM QSPI parameters: mx66_sim133sdr.bin (512 bytes, "OPI SDR 133 MHz"), taken unchanged from S32 Design Studio 3.6.1, Platform SDK S32XX 4.0.0, processors/S32G399A/.../quadspi/default_boot_images/. We did not generate it with U-Boot's s32cc_qspiparams tool. U-Boot changes: the flash ID entry for 0xC2803C, plus the octal-SDR soft reset. The BootROM leaves the flash in OPI SDR, and without the reset RDID returns 00 00 00. What works: - Boot from QSPI at 1-1-1, 133 MHz (~16 MB/s), in BootROM, TF-A, U-Boot and Linux. - Linux reads and writes, after we forced the IP-command path. With the flash in 1-bit mode, the AHB direct-map read path in spi-fsl-qspi.c causes a synchronous external abort or a hang. What we did to enable octal DTR in U-Boot 1. Set spi-tx-bus-width / spi-rx-bus-width to 8. The flash then negotiates and enables 8D-8D-8D: opcode 0xEE, octal_dtr_enable() returns 0, and probe reports 256 MiB. 2. Found a dummy-cycle mismatch. SFDP gave 14 dummy cycles, but the flash defaults to 20 (CR2 at 0x300). We now program CR2[0x300] = 0 (20 cycles) and set read_dummy = 20. Before this fix, reads returned random data that changed on every read of the same address: *** Warning - bad CRC, using default environment Too large ELF file, size: 3568570404 <- PFE firmware header, read 1 Too large ELF file, size: 1226703397 <- same header, read 2 Bad Linux ARM64 Image magic! 3. Read the ID back in DTR mode: 3c 3c 3c 3c c2 c2. Both correct values come back, so we believe the flash really is in octal DTR. The problem Expected first bytes at the kernel offset: 1f 20 03 d5 19 80 31 14. The controller registers (read individually) are: MCR 030f00cc SMPR 33000000 DLLCRA c280000d DLCR 40ff40ff DLLSR 8000c078 (both DLLs locked) FR 09000001 (no DLPFF flag) - MCR DQS source = external (driver default for DDR): we get only 2 DTR clocks of data, then zeros: 1f 20 1f d5 00 00 00 00. The result is deterministic, and the controller reports a successful transfer. - MCR DQS source = internal (MCR[25:24] = 1): all the data arrives, but one DDR edge lags the other by exactly one clock: expected: 1f 20 | 03 d5 | 19 80 | 31 14 read: 1f 20 | 1f d5 | 03 80 | 19 14 | 31 .. The second byte of every pair is correct. The first byte of every pair is the correct sequence, delayed by one clock. DQS source sweep (MCR[25:24], BSWAP on/off), first 12 bytes read: bswap src MCR data result on 2 020f00cc 19 80 19 19 14 14 31 14 00 00 00 00 bad on 3 030f00cc 1f 20 1f d5 00 00 00 00 00 00 00 00 bad off 0 000f00cc 31 0c 00 1d 55 02 19 18 31 20 00 00 bad off 1 010f00cc 1f 20 1f d5 03 80 19 14 31 00 00 00 bad off 2 020f00cc 80 19 19 19 14 14 14 31 00 00 00 00 bad off 3 030f00cc 20 1f d5 1f 00 00 00 00 00 00 00 00 bad What we swept, with a full disable -> configure -> enable -> DLL-lock cycle each time (none fixed it): - SMPR DLLFSMPFA/FB_NTH 0-7, with DLP on and off - MCR END_CFG 0-3, with SFACR BSWAP on and off: this only reorders the same wrong bytes - MCR DQS source 0-3 - SMPR DDRSMP 0-7, with FSPHS on and off: no effect at all on the data Code changes (test builds only, on top of the bsp43.0 sources) TF-A fdts/s32cc-nxp-flash-macronix.dtsi (the DTB that U-Boot uses): mx66um2g45g@0 { compatible = "jedec,spi-nor"; spi-tx-bus-width = <8>; /* was 1 */ spi-rx-bus-width = <8>; /* was 1 */ }; U-Boot drivers/mtd/spi/spi-nor-core.c, spi_nor_macronix_octal_dtr_enable(), before CR2[0x0] is switched to DTR OPI: u8 dc = 0x00; /* CR2[0x300] = 0 -> 20 dummy */ write_enable(nor); op = (struct spi_mem_op) SPI_MEM_OP(SPI_MEM_OP_CMD(SPINOR_OP_WRCR2, 1), SPI_MEM_OP_ADDR(4, 0x300, 1), SPI_MEM_OP_NO_DUMMY, SPI_MEM_OP_DATA_OUT(1, &dc, 1)); spi_mem_exec_op(nor->spi, &op); spi_nor_wait_till_ready(nor); nor->read_dummy = 20; /* SFDP gave 14 */ U-Boot drivers/spi/fsl_qspi.c, enable_octal_ddr(), DQS source test (internal DQS instead of the octal_ddr_conf default DQS_EXTERNAL): mcr |= octal_ddr_conf.mcr; mcr &= ~QUADSPI_MCR_DQS_EXTERNAL; /* clear MCR[25:24] */ mcr |= QUADSPI_MCR_DQS_INT_PAD; /* MCR[25:24] = 1 */ qspi_writel(q, mcr, base + QUADSPI_MCR); The register sweeps used a test U-Boot command that repeats the full enable_octal_ddr() sequence (MDIS=1, program MCR/SMPR/DLCR/SFACR, MDIS=0, wait for DLL lock) for each setting, then reads 512 bytes 3 times. Board side: DQS is pinmuxed (pads 85-93, IMCR 540-548). Questions 1. Is external DQS required for 8D-8D-8D at 133 MHz on the S32G3 QuadSPI? Is "2 clocks then zeros" a known symptom of a missing or bad DQS return? 2. Is internal DQS (loopback) supported in DDR mode? If so, which register settings fix the one-clock skew between edges? DLLCRA slave-delay settings, perhaps? 3. Do you have validated QuadSPI settings (MCR/SMPR/DLLCRA/FLSHCR), or a BootROM parameter set, for the MX66UM2G45G or another 1.8 V Macronix octal part on S32G3? The same S32DS folder also has mx66_sim133ddr.bin. Has that octal DTR boot image been validated on S32G3, and on which board? 4. Is the AHB read path in the Linux spi-fsl-qspi driver validated only for octal DTR? Is it expected to fault when the flash runs in 1-1-1? 5. Is NXP planning to add the MX66UM2G45G (JEDEC ID C2 80 3C) to the S32 BSP? We checked the U-Boot, Linux and TF-A releases up to bsp48.0 and found no entry for it. AMD's U-Boot fork (u-boot-xlnx) has supported this part with octal-DTR read and program since its 2024.1 release, and mainline U-Boot supports its 1 Gbit sibling, the MX66UM1G45G (C2 80 3B). If support is planned, which BSP release is it targeted for? Would it include validated QuadSPI and BootROM parameters for octal DTR? We can share full logs and the register sweep tables. Thank you. Re: S32G399A octal DTR reads fail with Macronix MX66UM2G45G QSPI flash Hi Dheeraj, Thank you for the detailed information. Since this issue involves a custom board and the MX66UM2G45G, which is different from the flash used on the S32G3 RDB3, we cannot reproduce or validate the behavior on an equivalent setup. Nevertheless, I will do my best to assist and coordinate further investigation as needed. You mentioned that 8D-8D-8D Octal DTR cannot be used, but the Software section lists mx66_sim133sdr.bin. Since this indicates an SDR image, please clarify whether mx66_sim133sdr.bin or mx66_sim133ddr.bin is being used, and whether both the flash and QuadSPI controller are configured for Octal DTR before the read. The read-ID result 3c 3c 3c 3c c2 c2 shows that communication is occurring, but it does not fully confirm correct 8D-8D-8D operation. If possible, please provide oscilloscope captures of SCLK, DQS, and SIO[0:7] during the read-ID and failing read operations. As a diagnostic, please repeat the same read at a lower Clock frequency, such as approximately 104 MHz, 84 MHz, and 66 MHz, while keeping the Octal DTR and DQS configuration consistent.The controller clock, flash dummy-cycle setting, LUT sequence, and other timing parameters must remain consistent with the selected frequency. Any change in the data or error pattern could indicate a timing or signal-integrity issue. For reference, please review: S32 Flash Tool User Guide, UG10237, Section 4. S32 Flash Tool for S32 Platform AN13563, S32G QuadSPI Deep Dive, Section 4 and 5. HOWTO: Use FlashSDK to add support for QuadSPI flash memory devices The questions raised require additional investigation and may involve other NXP teams. I will provide further information as it becomes available. Best regards, Aldo Re: S32G399A octal DTR reads fail with Macronix MX66UM2G45G QSPI flash Hi Aldo, Thank you for the suggestions. Here is what we found. 1. Bin file We use mx66_sim133sdr.bin. It is only used by the BootROM to load BL2 in octal SDR at 133 MHz, which works. Octal DTR is enabled later in U-Boot, and both the flash and the controller are in 8D-8D-8D for the failing reads. We have not tried mx66_sim133ddr.bin yet. Its controller settings (MCR 0x030F00CC, DLLCR 0x8280000C, SMPR 0x44000000, external DQS) are the same ones we tested in U-Boot below, so we expect the same failure. 2. Controller settings We used the S32G3 data sheet Table 54 "DDR-133MHz" column: MCR 0x030F00CC, SMPR 0x44000000, DLLCRA 0x8280000D, FLSHCR 0x00010303, SFACR BSWAP. The DLL locks (DLLSR 0x8000C014). 3. Failure pattern with external DQS Command, address and dummy cycles are correct and the first 16-bit word is read correctly. After that, data is captured only on some DQS edges. Words are repeated and others are skipped. Example (16 bytes): Expected:   54 71 00 90 94 a2 2e 91 f5 5b 02 a9 13 41 38 d5 Read:          54 71 54 54 00 90 00 00 94 a2 38 d5 38 38 95 06 4. Settings sweep with external DQS No setting works: NTH 0-7, DLL auto/manual/bypass, slave delay offset 0-7 and coarse 0-15, TDH 0-2, DDRSMP 0-7. The QSPI pad configuration is correct (MSCR = 0x00282001 for all QSPI pads including DQS PF_13). 5. Frequency sweep We tested 133, 100, 80 and 66.7 MHz (the closest rates to 104/84/66 MHz we can generate). External DQS fails at every frequency with the same pattern. 6. Internal DQS With internal DQS (MCR 0x010F00CC) and the DLL in manual mode, octal DTR reads are correct (verified with 16 MB CRC checks). The working slave delay offsets widen as the clock drops: 133 MHz: 7, 100 MHz: 4-7, 80 MHz: 2-7, 66.7 MHz: 1-7. Octal SDR (8S-8S-8S) at 133 MHz also works reliably. Since the external DQS path fails at every frequency and setting, we suspect a problem on the DQS signal on our board. Note that DQS is shared with a second flash device on the same bus which is not enabled. We will capture SCLK, DQS and SIO with the oscilloscope and share the images. Is there anything else on the controller side we should check for external DQS? -Dheeraj Re: S32G399A octal DTR reads fail with Macronix MX66UM2G45G QSPI flash Hi Aldo, Thank you for the response. To clarify, we are using mx66_sim133sdr.bin. It is used only by the BootROM, so it does not affect the octal DTR problem. Octal DTR is enabled later, at U-Boot stage, when the SPI-NOR framework switches the flash to DTR and enable_octal_ddr() configures the QuadSPI controller. Both the flash and the controller are in 8D-8D-8D before the failing reads. We will still try mx66_sim133ddr.bin and share the result. Also, as suggested, we will also repeat the reads at lower clock frequencies, keeping the other properties consistent, and report any change in the data or error pattern. We will also capture oscilloscope images of SCLK, DQS and SIO[0:7] during the read-ID and failing read operations, and get back to you with them soon. Regards, Dheeraj Re: S32G399A octal DTR reads fail with Macronix MX66UM2G45G QSPI flash Hi Dheeraj, Thank you for the additional test results.  Our initial responses to your first questions are provided below. Based on the information currently available, please consider the following: 1. As you know, the validated S32G3 controller configuration for 133 MHz DDR is documented in Table 54 of the S32G3 Data Sheet, under the “DDR-133MHz” column. This configuration uses external DQS. The “two clocks then zeros” behavior is compatible with a problem in the DQS path, but we cannot confirm it as a definitive symptom without reviewing the waveforms. Since external DQS fails with the same pattern from 133 MHz down to 66.7 MHz, while internal DQS works with manual delay settings, a board-level DQS signal or timing issue remains a reasonable possibility. 2. DLLCRA is used to generate the quantized delay. However, we do not currently have a validated DLLCRA value that can be recommended to correct the one-clock skew on your custom board. Internal DQS may be useful as a diagnostic, but external DQS remains the recommended configuration for DDR-133 operation. 3. Please use the recommended DDR-133 settings in the S32G3 Data Sheet as the controller reference. The mx66_sim133ddr.bin image is expected to have been verified by the software team, but the validation board and detailed test conditions are not currently available. You may open the image with the QuadSPI Configuration Tool in S32DS to inspect the configuration.  4. The BSP implementation needs to be checked. In addition, the AHB read sequence must match the protocol currently used by the flash. If the flash is in 1-1-1 mode while the AHB path is configured for an octal DTR sequence, a fault or hang can occur. For 1-1-1 operation, the AHB LUT and flash state must be configured consistently.  5. The current BSP device-tree configuration is intended for the MX25UW51245G used on the RDB3. When a different flash device is selected, the user is expected to update the device-tree and flash configuration as needed. At this time, I cannot confirm a planned BSP release that will add the MX66UM2G45G or provide board-specific validated Octal DTR parameters. I have already requested oscilloscope captures of SCLK, DQS, and SIO[0:7] during the read-ID and failing read operations. Please share those captures when available. They will be important for determining whether the external DQS signal is reaching and being sampled correctly. If the captures show that additional measurements are needed, I will let you know. The relevant references are the S32G3 Data Sheet and the QuadSPI Configuration Tool in S32DS. AN13563 may help explain the reconfiguration-image structure and generation flow, but its examples should not be treated as a direct validation for this S32G399A and MX66UM2G45G combination. Best regards,  Aldo.
View full article
Errors Updating & Building S32K344 App Code Hub Example I am trying to follow this demo for the FRDM S32K344 board: https://mcuxpresso.nxp.com/appcodehub?search=dm-adc-profiling-freemaster-s32k344  I installed the correct SW dependencies but once I try to click "Update Code and Build Project" I get the following errors. I've tried restarting my PC and S32DS, recreate a new workspace, and check other extensions and nothing has gotten rid of this bug. Thank you kindly in advance for your support! Re: Errors Updating & Building S32K344 App Code Hub Example Hi, the example description states this example was developed using the FRDM Automotive Bundle for S32K3 + S32M27.  Not all the drivers listed below are used in this example. However, at least the following two packages must be properly installed in S32DS 3.6.8 before loading the demo: S32K3 Real-Time Drivers AUTOSAR 4.9, Version 7.0.1 S32K3 FreeMASTER Driver Please make sure that these packages are correctly installed in your S32DS 3.6.x environment. After succesfull drivers installation, the given example can be normally loaded from ACH and execute UpdateCode and Build. BR, Petr   Re: Errors Updating & Building S32K344 App Code Hub Example Correction to my previous reply. The following setup changes were needed to get the S32K344 demo environment working: Download the required software packages and Design Studio update-site ZIP files. In S32DS 3.6.x, open Extensions and Updates → Add Update Sites. Add each ZIP file, close the Add Update Sites dialog, select the available components, and click Install. Restart S32DS after installation. Install the complete base S32K3/S32M27x RTD 7.0.1 package before installing any RTD-dependent package. Use the GCC 10.2 toolchain when creating the project. The working package set included: S32K3xx Development Package S32K3 FreeMASTER Serial Communication Driver S32K3 RTD AUTOSAR R23-11 Version 7.0.1 S32K3_S32M27x RTD AUTOSAR R23-11 Version 7.0.1 S32K3XX RTD AUTOSAR R23-11 Version 7.0.1 AMMCLIB for S32K3xx/S32M27x, RTD dependent FreeRTOS for S32K3xx Important: QLP06/P02 is an add-on package, not the complete RTD. Do not install QLP06/P02 by itself. Install the base RTD package first, then install QLP06/P02 only if it is required. Installing it alone produces: Missing required dependency: com.nxp.RTD.S32K3_S32M27X 0.0.0 For this specific S32K344 demo, the minimum required packages are the base S32K3 RTD 7.0.1 package and the S32K3 FreeMASTER Driver. The other packages are part of the broader bundle or may be needed by project dependencies. The K39xx RTD package is not required for this S32K344 demo. Re: Errors Updating & Building S32K344 App Code Hub Example Hi Petr. Thank you kindly for the reply. I followed your instructions and received the following error on the K39xx R23-11 RTD package: Do I really need this for the demo since the package only mentions S32K39x and not S3K34x? Best, Andrew Re: Errors Updating & Building S32K344 App Code Hub Example Hi, I understand your doubts about the RTD package numbering and descriptions. You are also correct that 7.0.1.QLP5/6/P02 are add-on packages containing Crypto drivers. These packages must be installed on top of the base S32K3 RTD 7.0.1 package. However, the ACH demo directs you to the Automotive Software Package Manager and the FRDM Automotive S32K3 + S32M27 Board Installation Package. If you select Real-Time Drivers 7.0.1, you can see the exact file it represents. If you allow the Package Manager to generate a bundle installer, it will select the correct packages for installation. It is correct that not all of these packages are necessary for this particular example; as mentioned, only the RTD and FreeMASTER driver are required. If you locate the necessary files in your software library, search for the exact names displayed in the Package Manager to identify the correct packages. Regarding the S32K3 RTD 7.0.1 package installation, it contains four drivers. The S32K39x and S32M27x drivers are not required for this S32K344 ADC example. However, it is highly advisable to install all four drivers, mainly because future updates may depend on the base package. BR, Petr  
View full article
S32 Design Studioのライセンスが切れました 親愛なるNXPへ: S32 Design Studio 3.5のライセンスがまもなく期限切れになります。      ライセンス延長を手伝ってもらえますか?      ありがとう。 アクティベーションID: 29E6-6248-FCB2-DBB6 Re: S32 Design Studio License Expired こんにちは、 お客様のS32DSライセンスが延長されました。以前のコードを使用して、S32DSを再度有効化してください。
View full article
S32G399Aの8進数DTR読み取りがMacronix MX66UM2G45G QSPIフラッシュで失敗する こんにちは、コミュニティの皆さん。 私たちはS32G399A-RDB3リファレンスデザインを基にしたカスタムボードを持っています。主な ブートフラッシュの変更点は、MX25UW51245G (64 MB) を Macronix MX66UM2G45G (256 MB、1.8 V 8進数、JEDEC ID C2 80 3C)。すべて 1-1-1 SPIで動作します。8D-8D-8D(八進DTR)読み取りを正しく返すことはできません そしてNXPに助けを求めています。また、この部分はどの中にも見つかりませんでした S32 BSPはbsp48.0までリリースされています。AMDのU-Bootは、 2024.1. ソフトウェア TF-A bsp43.0-2.10.7、U-Boot bsp43.0-2022.04、Linux bsp43.0(6.6.52) BootROM QSPIパラメータ:mx66_sim133sdr.bin(512バイト、「OPI SDR 133 MHz」)、 S32 Design Studio 3.6.1から変更せずに採用されました。プラットフォーム SDK S32XX 4.0.0, プロセッサー/S32G399A/.../quadspi/default_boot_images/。私たちは生成しませんでした U-Bootのs32cc_qspiparamsツールを使用してください。 U-Bootの変更点:0xC2803CのフラッシュIDエントリ、および8進数SDRソフト リセット。BootROMはフラッシュをOPI SDRのままにし、リセットRDIDなしで 00 00 00 を返します。 効果的な点: - QSPIから1-1-1、133 MHz(~16 MB/s)、BootROM、TF-A、u-Bootで起動 Linux。 - LinuxはIPコマンドパスを強制した後に読み書きを行います。フラッシュと共に 1ビットモードでは、spi-fsl-qspi.cのAHBダイレクトマップ読み取りパス原因となる 同期的な外部アボートまたはハング。 U-Bootで8進数DTRを有効にするために行ったこと 1. spi-tx-bus-width / spi-rx-bus-width を 8 に設定します。するとフラッシュがネゴシエートし、 8D-8D-8D を有効にする: オペコード 0xEE、octal_dtr_enable() は 0 を返し、プローブ 256 MiB と報告されています。 2. ダミーサイクルの不一致が見つかりました。SFDPは14回のダミーサイクルを実行したが、フラッシュ デフォルト値は20(CR2、アドレスは0x300)です。ここで、CR2[0x300] = 0 (20サイクル) とプログラムします。 そして、read_dummy = 20 に設定します。この修正前は、読み取りによってランダムなデータが返されていました。 同じアドレスを読み取るたびに変更されます。 *** Warning - bad CRC, using default environment Too large ELF file, size: 3568570404 <- PFE firmware header, read 1 Too large ELF file, size: 1226703397 <- same header, read 2 Bad Linux ARM64 Image magic! 3. DTRモードでIDを読み戻します: 3c 3c 3c 3c c2 c2。両方の正しい値が揃っています 戻ってきて、私たちはフラッシュが本当に八進DTRにあると考えています。 問題 カーネルオフセットでの最初のバイトの期待値: 1f 20 03 d5 19 80 31 14。その コントローラレジスタ(個別に読み取る)は以下の通りです: MCR 030f00cc SMPR 33000000 DLLCRA c280000d DLCR 40ff40ff DLLSR 8000c078 (both DLLs locked) FR 09000001 (no DLPFF flag) - MCR DQS source = 外部(DDRのドライバーデフォルト):DTRクロックは2つだけです データの後、ゼロ:1f 20 1f d5 00 00 00 00 00。結果はデターミニスティックである。 そして管制官が転送成功を報告します。 - MCR DQS ソース = 内部 (MCR[25:24] = 1): すべてのデータが到着しますが、1 つ DDRエッジは、もう一方のエッジに対してちょうど1クロック遅れている。 expected: 1f 20 | 03 d5 | 19 80 | 31 14 read: 1f 20 | 1f d5 | 03 80 | 19 14 | 31 .. 各ペアの2バイト目は正しい。各ペアの最初のバイトは 正しいシーケンスが、1クロック分遅れて表示される。 DQSソーススイープ(MCR[25:24]、BSWAPオン/オフ)、最初の12バイトを読み取ります。 bswap src MCR data result on 2 020f00cc 19 80 19 19 14 14 31 14 00 00 00 00 bad on 3 030f00cc 1f 20 1f d5 00 00 00 00 00 00 00 00 bad off 0 000f00cc 31 0c 00 1d 55 02 19 18 31 20 00 00 bad off 1 010f00cc 1f 20 1f d5 03 80 19 14 31 00 00 00 bad off 2 020f00cc 80 19 19 19 14 14 14 31 00 00 00 00 bad off 3 030f00cc 20 1f d5 1f 00 00 00 00 00 00 00 00 bad 完全な無効化→設定→有効化→DLLロックサイクルで掃討した 毎回(どれも解決しなかった): - SMPR DLLFSMPFA/FB_NTH 0-7、DLPオン/オフ - MCR END_CFG 0-3、SFACR BSWAP のオン/オフ: これは同じものを並べ替えるだけです 間違ったバイト - MCR DQSソース0-3 - SMPR DDRSMP 0-7、FSPHSのオン/オフ:データに全く影響なし コードの変更(テストビルドのみ、bsp43.0 をベースに)情報源) TF-A fdts/s32cc-nxp-flash-macronix.dtsi(U-Bootが使用するDTB): mx66um2g45g@0 { compatible = "jedec,spi-nor"; spi-tx-bus-width = <8>; /* was 1 */ spi-rx-bus-width = <8>; /* was 1 */ }; U-Boot ドライバ/mtd/spi/spi-nor-core.c, spi_nor_macronix_octal_dtr_enable(), CR2[0x0]がDTR OPIにスイッチ前に: u8 dc = 0x00; /* CR2[0x300] = 0 -> 20 dummy */ write_enable(nor); op = (struct spi_mem_op) SPI_MEM_OP(SPI_MEM_OP_CMD(SPINOR_OP_WRCR2, 1), SPI_MEM_OP_ADDR(4, 0x300, 1), SPI_MEM_OP_NO_DUMMY, SPI_MEM_OP_DATA_OUT(1, &dc, 1)); spi_mem_exec_op(nor->spi, &op); spi_nor_wait_till_ready(nor); nor->read_dummy = 20; /* SFDP gave 14 */ U-Bootドライバ/spi/fsl_qspi.c、enable_octal_ddr()、DQSソーステスト (octal_ddr_confのデフォルトDQS_EXTERNALではなく内部DQS): mcr |= octal_ddr_conf.mcr; mcr &= ~QUADSPI_MCR_DQS_EXTERNAL; /* clear MCR[25:24] */ mcr |= QUADSPI_MCR_DQS_INT_PAD; /* MCR[25:24] = 1 */ qspi_writel(q, mcr, base + QUADSPI_MCR); レジスタスイープでは、完全なU-Bootコマンドを繰り返すテストU-Bootコマンドが使用されました。 enable_octal_ddr() シーケンス (MDIS=1、プログラム MCR/SMPR/DLCR/SFACR、MDIS=0、 各設定に対してDLLロックを待機し、その後512バイトを3回読み取ります。 基板側: DQSはピン多重化されています(パッド85~93、IMCR 540~548)。 質問 1.S32G3 QuadSPIで133MHzの8D-8D-8D動作を実現するには、外部DQSが必要ですか?は 「時計が2つ表示されてからゼロが表示される」というのは、DQSの返却が欠落しているか、不良であることを示す既知の症状ですか? 2. DDRモードでは内部DQS(ループバック)はサポートされていますか?もしそうなら、どのレジスターか 設定でエッジ間の1クロックのクロックスキューを修正できますか?DLLCRAスレーブ遅延設定、 多分? 3. QuadSPI 設定 (MCR/SMPR/DLLCRA/FLSHCR) の検証済み、または BootROMパラメータセット(MX66UM2G45Gまたはその他の1.8V Macronix 8進数用) S32G3の部品ですか?同じS32DSフォルダには、mx66_sim133ddr.binも含まれています。それはある 8進数DTRブートイメージはS32G3で検証済みで、どのボードで確認されていますか? 4. Linuxのspi-fsl-qspiドライバにおけるAHB読み取りパスは、 八進DTR?フラッシュが1-1-1で動作すると故障するのが普通でしょうか? 5. NXPはS32 BSPにMX66UM2G45G(JEDEC ID C2 80 3C)を追加する計画ですか? U-Boot、Linux、TF-Aのbsp48.0までのリリースを調べましたが、見つかりませんでした その入り口。AMDのU-Bootフォーク(u-boot-xlnx)はこの部分をサポートしています。 2024.1リリース以降のoctal-DTR読み取りおよびプログラム、そしてメインラインのU-Boot 1 Gbitの兄弟機であるMX66UM1G45G(C2 80 3B)をサポートしています。もしサポートが 計画中ですが、どのBSPリリースをターゲットにしていますか?検証済みのものも含まれますか 8進数DTR用のQuadSPIおよびBootROMパラメータは? ログ全体とレジスタスイープテーブルを共有できます。ありがとう。 Re: S32G399A octal DTR reads fail with Macronix MX66UM2G45G QSPI flash こんにちは、アルドさん。 ご回答ありがとうございます。 念のため申し上げますが、弊社ではmx66_sim133sdr.binを使用しています。これはBootROMでのみ使用されるため、オクタルDTRの問題には影響しません。 オクタルDTRは、後にU-Boot段階でSPI-NORフレームワークがフラッシュをDTRにスイッチし、 enable_octal_ddr() がQuadSPIコントローラを設定することで有効になります。フラッシュもコントローラも読み込みが失敗する前に8D-8D-8Dになっています。引き続きmx66_sim133ddr.binを試してみて、結果を共有します。 また、ご提案いただいたように、他の特性を一定に保ちながら、より低いクロック周波数で読み取りを繰り返し、データやエラーパターンに変化があった場合は報告します。 また、読み取りID処理中および読み取り失敗時のSCLK、DQS、SIO[0:7]のオシロスコープ画像も取得し、近日中にお送りいたします。 よろしくお願いいたします。 ディラージ Re: S32G399A octal DTR reads fail with Macronix MX66UM2G45G QSPI flash こんにちは、アルドさん。 ご提案ありがとうございます。私たちが発見したことは以下のとおりです。 1. バイナリファイル 私たちはmx66_sim133sdr.binを使用します。これは、BootROMがBL2を133MHzの8進数SDRでロードするためにのみ使用され、正常に動作します。U-Bootでは後で8進DTRが有効になり、読み込み失敗時はフラッシュとコントローラの両方が8D-8D-8Dになっています。mx66_sim133ddr.binはまだ試していません。コントローラ設定(MCR 0x030F00CC、DLLCR 0x8280000C、SMPR 0x44000000、外部DQS)は、下のU-Bootでテストしたものと同じなので、同じ故障が起こると予想しています。 2. コントローラ設定 S32G3のデータシート表54「DDR-133MHz」欄を使用しました:MCR 0x030F00CC、SMPR 0x44000000、DLLCRA 0x8280000D、FLSHCR 0x00010303、SFACR BSWAP。DLLがロックされています(DLLSR 0x8000C014)。 3. 外部DQSにおける障害パターン コマンド、アドレス、ダミーサイクルは正しく、最初の16ビットワードも正しく読み取られています。その後は、一部のDQSエッジでのみデータが取得されます。単語が繰り返されたり、省略されたりする。 例(16バイト): 予想される値: 54 71 00 90 94 a2 2e 91 f5 5b 02 a9 13 41 38 d5 読み上げ: 54 71 54 54 00 90 00 00 94 a2 38 d5 38 38 95 06 4. 外部DQSによる設定スイープ どの設定も動作しません:NTH 0-7、DLL車載/マニュアル/バイパス、スレーブディレイオフセット0-7、粗い0-15、TDH 0-2、DDRSMP 0-7。QSPIパッド構成は正しいです(DQS PF_13を含むすべてのQSPIパッドのMSCRは0x00282001です)。 5. 周波数スイープ 133、100、80、66.7 MHz(104/84/66 MHzに最も近い周波数)をテストしました。外部DQSは、あらゆる周波数において同じパターンで故障する。 6. 内部DQS 内部DQS(MCR 0x010F00CC)とDLLがマニュアルモードの場合、8進数DTRの読み取りは正しい(16MBのCRCチェックで検証済み)。クロック周波数が低下するにつれて、動作スレーブの遅延オフセットは広がります。133 MHz: 7、100 MHz: 4-7、80 MHz: 2-7、66.7 MHz: 1-7。 133MHz帯の8S-8S-8SオクタールSDRも安定して動作します。 外部DQS経路がすべての周波数と設定で失敗するため、基板上のDQS信号に問題があると疑っています。DQSは、同じバス上の別のフラッシュデバイスと共有されていますが、そのフラッシュデバイスは有効になっていません。オシロスコープを使用してSCLK、DQS、SIOの波形をキャプチャし、その画像を共有します。 コントローラ側で外部DQSを確認するべき他に何かありますか? -ディラージ Re: S32G399A octal DTR reads fail with Macronix MX66UM2G45G QSPI flash こんにちは、ディーラージさん。 詳細な情報を提供していただきありがとうございます。 この問題はカスタムボードとMX66UM2G45Gに関わっており、S32G3 RDB3で使われているフラッシュとは異なり、同等のセットアップで同じ動作を再現または検証することはできません。とはいえ、必要に応じて、さらなる調査を支援し、調整するために最善を尽くします。 8D-8D-8DのオクタルDTRは使えないとおっしゃっていましたが、ソフトウェアのセクションにはmx66_sim133sdr.binが記載mx66_sim133sdr.binされています。これはSDRイメージを示しているため、mx66_sim133sdr.binかmx66_sim133ddr.binが使われているのか、また読み込み前にフラッシュとQuadSPIコントローラの両方がオクタルDTRに設定されているかを明確にしてください。 read-IDの結果3c 3c 3c 3c c2 c2は通信が行われていることを示していますが、8D-8D-8Dの動作が正しいことを完全に確認するものではありません。可能であれば、read-ID実行時および読み取り失敗時のSCLK、DQS、SIO[0:7]のオシロスコープ波形を提供してください。 診断として、同じ読み出しを約104MHz、84MHz、66MHzなど 低いクロック周波数で繰り返し、オク進DTRとDQSの設定は一定に保ってください。コントローラクロック、フラッシュダミーサイクル設定、LUTシーケンス、その他のタイミングパラメータは選択した周波数と一貫していなければなりません。 データやエラーパターンの変化は、タイミングや信号の整合性の問題を示す可能性があります。 参考までに、以下をご確認ください。 S32 Flash Tool ユーザーガイド、UG10237、セクション4。 S32プラットフォーム向けS32フラッシュツール AN13563、S32G QuadSPIの詳細解説、セクション4および5。 HOWTO:FlashSDKを使ってQuadSPIフラッシュメモリデバイスのサポートを追加してください 提起された疑問点については、さらなる調査が必要であり、NXPの他のチームが関与する可能性もあります。新たな情報が入り次第、お知らせいたします。 よろしくお願いします、 アルド Re: S32G399A octal DTR reads fail with Macronix MX66UM2G45G QSPI flash こんにちは、ディーラージさん。 追加の検査結果をありがとうございます。 お客様からいただいた最初のご質問に対する回答は以下のとおりです。 現在入手可能な情報に基づき、以下の点をご検討ください。 1.ご存知の通り、133 MHz DDR用の検証済みS32G3コントローラ構成は、S32G3データシートの表54の「DDR-133MHz」欄に記載されています。この構成では外部DQSを使用します。「2つのクロックが経てゼロになる」挙動はDQS経路の問題と両立しますが、波形を確認しなければ決定的な症状として確認できません。外部DQSが133MHzから66.7MHzまで同じパターンで失敗する一方、内部DQSは手動遅延設定で動作するため、基板レベルのDQS信号またはタイミングの問題である可能性が十分に考えられます。 2.量子化遅延を生成するためにDLLCRAが使用されます。しかし、現時点ではカスタムボードの1クロックのクロックスキューを修正するための有効なDLLCRA値を持っていません。内部DQSは診断ツールとして役立つ場合があるが、DDR-133の動作には外部DQSが推奨される構成である。 3. コントローラの参考として、S32G3データシートに記載されている推奨されるDDR-133設定をご利用ください。mx66_sim133ddr.bin画像はソフトウェアチームによって検証された見込みですが、検証ボードや詳細なテスト条件は現時点では入手できません。S32DSのQuadSPI構成ツールでイメージを開き、構成を確認できます。 4. BSPの実装を確認する必要があります。さらに、AHBの読み取りシーケンスは、フラッシュメモリで現在使用されているプロトコルと一致している必要があります。フラッシュが1-1-1モードで、AHB経路がオクタルDTRシーケンスに設定されている場合、故障やハングが発生することがあります。1-1-1動作の場合、AHB LUTとフラッシュの状態は一貫して設定する必要があります。 5.現在のBSPデバイスツリー構成は、RDB3で使用されるMX25UW51245Gを対象としています。異なるフラッシュデバイスを選択すると、ユーザーは必要に応じてデバイスツリーやフラッシュの設定を更新することが期待されます。現時点では、 MX66UM2G45Gを追加したり、基板固有の検証済みOctal DTRパラメータを提供する予定のBSPリリースを確認できていません。 私は既に、読み取りID処理中および読み取り失敗時のSCLK、DQS、およびSIO[0:7]のオシロスコープ波形を要求しました。入手可能な場合は、それらの画像を共有してください。これらは、外部DQS信号が正しく到達し、正しくサンプリングされているかどうかを判断する上で重要となる。計測結果から追加の測定が必要と判断された場合は、ご連絡いたします。 関連する資料としては、S32G3データシートとS32DSに含まれるQuadSPI構成ツールが挙げられます。AN13563は再構成イメージの構造と生成フローを説明するのに役立つかもしれませんが、その例はS32G399AとMX66UM2G45Gの組み合わせに対する直接的な検証として扱うべきではありません。 よろしくお願いします、 アルド。
View full article
S32 Design Studio License Expired Dear NXP:      The S32 Design Studio 3.5 license is about to expire.      Could you please help extend the license?      Thank you.      ActivationId: 29E6-6248-FCB2-DBB6 Re: S32 Design Studio License Expired Hi,  your S32DS license has been extended. Please activate S32DS again with your old code. 
View full article
使用 Macronix MX66UM2G45G QSPI 闪存时,S32G399A 八进制 DTR 读取失败 大家好, 我们有一款基于 S32G399A-RDB3 参考设计的定制板。主要 启动闪存的更改在于,我们将 MX25UW51245G (64 MB) 替换为…… Macronix MX66UM2G45G(256 MB,1.8 V 八脚,JEDEC ID C2 80 3C)。一切 适用于 1-1-1 SPI 模式。我们无法获取正确的 8D-8D-8D(八进制 DTR)读取结果。 我们需要数据,并希望得到 NXP 的帮助。我们也找不到这部分内容。 S32 电路板支持包。版本最高可达 bsp48.0,尽管 AMD 的 U-Boot 自那时起就支持它了。 2024.1. 软件 TF-A bsp43.0-2.10.7,U-Boot bsp43.0-2022.04,Linux bsp43.0(6.6.52) BootROM QSPI 参数:mx66_sim133sdr.bin(512 字节,“OPI SDR 133 MHz”), 直接取自 S32 Design Studio 3.6.1,未做任何修改。平台 SDK S32XX 4.0.0 processors/S32G399A/.../quadspi/default_boot_images/。我们没有生成 使用 U-Boot 的 s32cc_qspiparams 工具。 U-Boot 更改:闪存 ID 条目为 0xC2803C,以及八进制 SDR 软启动 重置。BootROM 将闪存设置为 OPI SDR 模式,并且不包含 RESET RDID。 返回 00 00 00。 有效的方法: - 从 QSPI 以 1-1-1 模式、133 MHz(~16 MB/s)启动,在 启动ROM、TF-A、U-启动 中均可实现。 Linux。 - 在我们强制执行 IP 命令路径后,Linux 可以进行读写操作。闪光灯 在 1 位模式下,spi-fsl-qspi.c 中的 AHB 直接映射读取路径导致 同步外部中止或挂起。 我们在 U-Boot 中启用八进制 DTR 的方法 1. 将 spi-tx-总线-width / spi-rx-总线-width 设置为 8。然后闪存会进行协商并 启用 8D-8D-8D:操作码 0xEE,octal_dtr_enable() 返回 0,并进行探测 报告显示 256 MiB。 2. 发现虚拟周期不匹配。SFDP 提供了 14 个虚拟循环,但闪光灯 默认值为 20(CR2 位于 0x300)。我们现在将 CR2[0x300] 编程为 0(20 个周期) 并设置 read_dummy = 20。在此修复之前,读取操作返回的是随机数据。 每次读取同一地址时都会发生变化: *** Warning - bad CRC, using default environment Too large ELF file, size: 3568570404 <- PFE firmware header, read 1 Too large ELF file, size: 1226703397 <- same header, read 2 Bad Linux ARM64 Image magic! 3. 在 DTR 模式下读取 ID:3c 3c 3c 3c c2 c2。两个正确值都来自 由此可见,我们认为闪光灯确实是八进制 DTR。 问题 内核偏移处的预期首字节:1f 20 03 d5 19 80 31 14。这 控制器寄存器(单独读取)包括: MCR 030f00cc SMPR 33000000 DLLCRA c280000d DLCR 40ff40ff DLLSR 8000c078 (both DLLs locked) FR 09000001 (no DLPFF flag) - MCR DQS 源 = 外部(DDR 驱动程序默认值):我们只能获得 2 个 DTR 时钟 数据,然后是零:1f 20 1f d5 00 00 00 00。结果是确定性的。 控制器报告转账成功。 - MCR DQS 源 = 内部 (MCR[25:24] = 1): 所有数据都已到达,但有一个 DDR 时钟周期比其他时钟周期慢一个时钟周期: expected: 1f 20 | 03 d5 | 19 80 | 31 14 read: 1f 20 | 1f d5 | 03 80 | 19 14 | 31 .. 每对数据中的第二个字节都是正确的。每对数据的第一个字节是 正确的序列,延迟一个时钟周期。 DQS 源扫描(MCR[25:24],BSWAP 开/关),读取前 12 个字节: bswap src MCR data result on 2 020f00cc 19 80 19 19 14 14 31 14 00 00 00 00 bad on 3 030f00cc 1f 20 1f d5 00 00 00 00 00 00 00 00 bad off 0 000f00cc 31 0c 00 1d 55 02 19 18 31 20 00 00 bad off 1 010f00cc 1f 20 1f d5 03 80 19 14 31 00 00 00 bad off 2 020f00cc 80 19 19 19 14 14 14 31 00 00 00 00 bad off 3 030f00cc 20 1f d5 1f 00 00 00 00 00 00 00 00 bad 我们通过完整的禁用 -> 配置 -> 启用 -> DLL 锁定循环彻底清除了所有问题。 每次都这样(但都没能解决问题): - SMPR DLLFSMPFA/FB_NTH 0-7,DLP 开启和关闭 - MCR END_CFG 0-3,SFACR BSWAP 开启和关闭:这只会重新排序相同的 错误字节 - MCR DQS 源 0-3 - SMPR DDRSMP 0-7,无论 FSPHS 开启还是关闭:对数据完全没有影响 代码更改(仅限测试版本,基于 bsp43.0)(来源) TF-A fdts/s32cc-nxp-flash-macronix.dtsi(U-Boot 使用的 DTB): mx66um2g45g@0 { compatible = "jedec,spi-nor"; spi-tx-bus-width = <8>; /* was 1 */ spi-rx-bus-width = <8>; /* was 1 */ }; U-Boot drivers/mtd/spi/spi-nor-core.c,spi_nor_macronix_octal_dtr_enable(), 在 CR2[0x0] 切换到 DTR OPI 之前: u8 dc = 0x00; /* CR2[0x300] = 0 -> 20 dummy */ write_enable(nor); op = (struct spi_mem_op) SPI_MEM_OP(SPI_MEM_OP_CMD(SPINOR_OP_WRCR2, 1), SPI_MEM_OP_ADDR(4, 0x300, 1), SPI_MEM_OP_NO_DUMMY, SPI_MEM_OP_DATA_OUT(1, &dc, 1)); spi_mem_exec_op(nor->spi, &op); spi_nor_wait_till_ready(nor); nor->read_dummy = 20; /* SFDP gave 14 */ U-Boot drivers/spi/fsl_qspi.c,enable_octal_ddr(),DQS 源测试 (内部 DQS 而不是 octal_ddr_conf 默认的 DQS_EXTERNAL): mcr |= octal_ddr_conf.mcr; mcr &= ~QUADSPI_MCR_DQS_EXTERNAL; /* clear MCR[25:24] */ mcr |= QUADSPI_MCR_DQS_INT_PAD; /* MCR[25:24] = 1 */ qspi_writel(q, mcr, base + QUADSPI_MCR); 寄存器扫描使用了一条测试用的 U-Boot 命令,该命令重复执行完整的操作。 enable_octal_ddr() 序列(MDIS=1,程序 MCR/SMPR/DLCR/SFACR,MDIS=0, 等待 DLL 锁定)对于每个设置,然后读取 512 字节 3 次。 板面: DQS 采用引脚复用(焊盘 85-93,IMCR 540-548)。 问题 1.在 S32G3 QuadSPI 上,133 MHz 频率下,8D-8D-8D 是否需要外部 DQS?是 “2 个时钟然后是 0”是 DQS 返回缺失或错误的一个已知症状吗? 2. DDR 模式下是否支持内部 DQS(环回)?如果是这样,是哪个注册表 设置可以修复边缘之间的一个时钟刻度偏差吗?DLLCRA 从属延迟设置, 也许? 3. 您是否已验证 QuadSPI 设置(MCR/SMPR/DLLCRA/FLSHCR)? 适用于 MX66UM2G45G 或其他 1.8V Macronix 八进制微控制器的 BootROM 参数集 S32G3 的部件是什么?S32DS 文件夹中还包含 mx66_sim133ddr.bin。有那个吗? 八进制 DTR 启动映像已在 S32G3 上验证过,是在哪款板上验证过的? 4. Linux spi-fsl-qspi 驱动程序中的 AHB 读取路径是否仅针对以下情况进行验证 八进制DTR?当闪存以 1-1-1 模式运行时,是否预期会出现故障? 5. NXP 是否计划将 MX66UM2G45G(JEDEC ID C2 80 3C)添加到 S32 电路板支持包。中? 我们检查了 U-Boot、Linux 和 TF-A 的版本,最高到 bsp48.0,没有发现任何问题。 它的条目。AMD 的 U-Boot 分支(u-boot-xlnx)已支持此部分。 自 2024.1 版本发布以来,八进制 DTR 的读取和编程以及主线 U-Boot 均已支持。 支持其 1 Gbit 同系列产品 MX66UM1G45G (C2 80 3B)。如果支持是 计划中,目标 电路板支持包。版本是什么?它会包含已验证的内容吗? QuadSPI 和 BootROM 的八进制 DTR 参数是什么? 我们可以共享完整的日志和寄存器扫描表。谢谢。 Re: S32G399A octal DTR reads fail with Macronix MX66UM2G45G QSPI flash 嗨,阿尔多, 谢谢你的建议。以下是我们发现的情况。 1. 二进制文件 我们使用 mx66_sim133sdr.bin。它仅供 BootROM 使用,以 133 MHz 的八进制 SDR 格式加载 BL2,并且有效。八进制 DTR 在 U-Boot 中稍后启用,闪存和控制器在读取失败时都处于 8D-8D-8D 模式。我们还没有尝试过 mx66_sim133ddr.bin。其控制器设置(MCR 0x030F00CC、DLLCR 0x8280000C、SMPR 0x44000000、外部 DQS)与我们在下面的 U-Boot 中测试的设置相同,因此我们预计会出现相同的故障。 2. 控制器设置 我们使用了 S32G3 数据表第 54 表“DDR-133MHz”列:MCR 0x030F00CC、SMPR 0x44000000、DLLCRA 0x8280000D、FLSHCR 0x00010303、SFACR BSWAP。DLL 锁(DLLSR 0x8000C014)。 3. 外部DQS的故障模式 命令、地址和虚拟周期均正确,并且第一个 16 位字已正确读取。之后,仅在某些 DQS 边上捕获数据。有些词语重复出现,有些词语则被跳过。 示例(16 字节): 预期:54 71 00 90 94 a2 2e 91 f5 5b 02 a9 13 41 38 d5 读取:54 71 54 54 00 90 00 00 94 a2 38 d5 38 38 95 06 4. 使用外部 DQS 进行设置扫描 任何设置均无效:NTH 0-7,DLL 自动/手动/旁路,从属延迟偏移 0-7 和粗略 0-15,TDH 0-2,DDRSMP 0-7。QSPI 焊盘配置正确(所有 QSPI 焊盘,包括 DQS PF_13,MSCR = 0x00282001)。 5. 频率扫描 我们测试了 133、100、80 和 66.7 MHz(这是我们能生成的最接近 104/84/66 MHz 的速率)。外部DQS在每个频率上都以相同的模式失效。 6. 内部 DQS 使用内部 DQS(MCR 0x010F00CC)和手动模式下的 DLL,八进制 DTR 读取是正确的(已通过 16 MB CRC 检查验证)。随着时钟频率下降,工作从机延迟偏移量增大:133 MHz:7,100 MHz:4-7,80 MHz:2-7,66.7 MHz:1-7。 八路 SDR (8S-8S-8S) 在 133 MHz 频率下也能可靠工作。 由于外部 DQS 路径在每个频率和设置下都失效,我们怀疑是板上的 DQS 信号出了问题。请注意,DQS 与同一总线上的第二个闪存设备共享,但该设备未启用。我们将使用示波器捕获 SCLK、DQS 和 SIO 信号,并分享图像。 对于外部DQS,控制器方面还有其他需要检查的地方吗? -迪拉杰 Re: S32G399A octal DTR reads fail with Macronix MX66UM2G45G QSPI flash 嗨,阿尔多, 谢谢你的回复。 澄清一下,我们使用的是mx66_sim133sdr.bin 。它仅供 BootROM 使用,因此不会影响八进制 DTR 问题。 八进制 DTR 稍后在 U-启动 阶段启用,此时 SPI-或非 框架将闪存切换到 DTR,并且enable_octal_ddr()配置 QuadSPI 控制器。在读取失败之前,闪存和控制器都处于 8D-8D-8D 状态。我们仍将尝试使用mx66_sim133ddr.bin ,并分享结果。 此外,正如建议的那样,我们还将以较低的时钟频率重复读取,保持其他属性一致,并报告数据或错误模式的任何变化。 我们还将在读取 ID 和读取失败操作期间捕获 SCLK、DQS 和 SIO[0:7] 的示波器图像,并尽快将它们反馈给您。 问候, 迪拉杰 Re: S32G399A octal DTR reads fail with Macronix MX66UM2G45G QSPI flash 嗨,迪拉杰, 感谢您提供如此详细的信息。 由于此问题涉及定制板和 MX66UM2G45G,而 MX66UM2G45G 与 S32G3 RDB3 上使用的闪存不同,因此我们无法在等效设置上重现或验证此行为。不过,我将尽我所能协助并协调后续调查工作。 您提到无法使用 8D-8D-8D 八进制 DTR,但软件部分列出了mx66_sim133sdr.bin 。由于这表明这是一个 SDR 镜像,请说明使用的是mx66_sim133sdr.bin还是mx66_sim133ddr.bin ,以及在读取之前是否已将闪存和 QuadSPI 控制器配置为八进制 DTR。 读取 ID 结果3c 3c 3c 3c c2 c2表明通信正在进行,但并不能完全确认 8D-8D-8D 操作正确。如果可以,请提供读取 ID 和读取失败操作期间示波器捕获的SCLK、DQS 和 SIO[0:7]。 作为诊断步骤,请在较低的时钟频率下(例如约 104 MHz、84 MHz 和 66 MHz)重复相同的读取操作,同时保持八进制 DTR 和 DQS 配置一致。控制器时钟、闪存虚拟周期设置、LUT 序列和其他时序参数必须与所选频率保持一致。 数据或错误模式的任何变化都可能表明存在时序或信号完整性问题。 请参考以下内容: S32 刷机工具用户指南,UG10237 ,第 4 节。 面向S32平台的S32 Flash Tool AN13563,S32G QuadSPI 深度解析,第 4 节和第 5 节。 操作指南:使用 FlashSDK 添加对 QuadSPI 闪存设备的支持 提出的问题需要进一步调查,可能还会牵涉到恩智浦的其他团队。如有更多信息,我将及时提供。 此致, 阿尔多 Re: S32G399A octal DTR reads fail with Macronix MX66UM2G45G QSPI flash 你好,迪拉杰, 感谢您提供的补充检测结果。 以下是我们对您第一个问题的初步答复。 根据目前掌握的信息,请考虑以下几点: 1.如您所知,经验证的 133 MHz DDR 的 S32G3 控制器配置记录在 S32G3 数据手册的表 54 中,“DDR-133MHz”列下。此配置使用外部 DQS。“两个时钟信号然后变为零”的行为与 DQS 路径中的问题相符,但如果不查看波形,我们无法确认这是否是确切的症状。由于外部 DQS 从 133 MHz 到 66.7 MHz 都出现相同的故障模式,而内部 DQS 在手动延迟设置下可以正常工作,因此板级 DQS 信号或时序问题仍然是一个合理的可能性。 2. DLLCRA 用于生成量化延迟。但是,我们目前还没有经过验证的 DLLCRA 值可以推荐用于纠正您定制板上的一个时钟周期偏差。内部 DQS 可能有助于诊断,但外部 DQS 仍然是 DDR-133 操作的推荐配置。 3.请使用 S32G3 数据手册中推荐的 DDR-133 设置作为控制器参考。mx66_sim133ddr.bin 镜像应该已经过软件团队的验证,但验证板和详细的测试条件目前尚不可用。您可以使用S32DS中的QuadSPI配置工具打开镜像文件来检查配置信息。 4.需要检查 电路板支持包。 实现情况。此外,AHB 读取序列必须与闪存当前使用的协议相匹配。如果闪存处于 1-1-1 模式,而 AHB 路径配置为八进制 DTR 序列,则可能会发生故障或挂起。对于 1-1-1 操作,AHB LUT 和闪存状态必须配置一致。 5.当前的电路板支持包。设备树配置适用于 RDB3 上使用的 MX25UW51245G。当选择不同的闪存设备时,用户需要根据需要更新设备树和闪存配置。目前,我无法确认计划中的电路板支持包。版本是否会添加 MX66UM2G45G,也无法提供针对特定电路板的已验证八路 DTR 参数。 我已经要求在读取 ID 和读取失败操作期间捕获 SCLK、DQS 和 SIO[0:7] 的示波器波形。请在获得捕获后分享出来。它们对于确定外部 DQS 信号是否到达并被正确采样至关重要。如果捕获的数据表明需要进行其他测量,我会通知您。 相关参考资料为 S32G3 数据手册和 S32DS 中的 QuadSPI 配置工具。AN13563 可能有助于解释重配置映像结构和生成流程,但其示例不应被视为对 S32G399A 和 MX66UM2G45G 组合的直接验证。 此致, 阿尔多。
View full article
エラーの更新とアプリコードハブS32K344ビルディング例 FRDM S32K344ボード用のこちらのデモを参考にしています: https://mcuxpresso.nxp.com/appcodehub? search=dm-adc-profiling-freemaster-s32k344 正しいソフトウェア依存関係をインストールしましたが、「コードの更新とプロジェクトのビルド」をクリックしようとすると、次のエラーが発生します。PCとS32DSを再起動したり、新しいワークスペースを作成したり、他の拡張機能を確認したりしてみましたが、このバグは解消されませんでした。サポートに心より感謝いたします! Re: Errors Updating & Building S32K344 App Code Hub Example こんにちは、 例の説明はTと述べています。彼の例はFRDMオートモーティブバンドルを用いてS32K3 + S32M27を用いて開発されました。 以下に挙げるすべてのドライバがこの例で使われているわけではありません。ただし、少なくとも以下の2つのパッケージはS32DS 3.6.8に正しくインストールされている必要がありますデモを読み込む前に: S32K3 リアルタイム・ドライバ AUTOSAR 4.9、バージョン7.0.1 S32K3 FreeMASTERドライバ これらのパッケージがS32DS 3.6.xに正しくインストールされているか必ず確認してください環境。 成功したドライバーインストール後、通常はACHからこの例を読み込み、UpdateCodeとBuildを実行します。 BR、ペトル   Re: Errors Updating & Building S32K344 App Code Hub Example こんにちは、ペトルさん。 ご返信いただき、誠にありがとうございます。あなたの指示に従いましたが、K39xx R23-11 RTDパッケージで以下のエラーが発生しました: パッケージにはS32K39xしか記載されておらず、S3K34xは記載されていないので、デモで本当にこれが必要ですか? 最高、 Andrew Re: Errors Updating & Building S32K344 App Code Hub Example 前回の返信を訂正します。S32K344デモ環境を動作させるには、以下の設定変更が必要でした。 必要なソフトウェアパッケージとDesign Studioの更新サイトZIPファイルをダウンロードしてください。 S32DS 3.6.xでは、拡張機能と更新を開く → 更新サイトの追加。 各ZIPファイルを追加し、[更新サイトの追加]ダイアログを閉じ、利用可能なコンポーネントを選択して、 [インストール]をクリックします。 インストール後、S32DSを再起動してください。 RTD依存パッケージをインストールする前に、必ずS32K3/S32M27x RTD 7.0.1の基本パッケージ全体をインストールしてください。 プロジェクトを作成する際は、GCC 10.2ツールチェーンを使用してください。 作業パッケージセットには以下が含まれていました: S32K3xx開発パッケージ S32K3 FreeMASTER シリアル通信ドライバ S32K3 RTD AUTOSAR R23-11 バージョン 7.0.1 S32K3_S32M27x RTD AUTOSAR R23-11 バージョン 7.0.1 S32K3XX RTD AUTOSAR R23-11 バージョン 7.0.1 AMMCLIB(S32K3xx/S32M27x用、RTD依存) S32K3xx向けFreeRTOS 重要: QLP06/P02はアドオンパッケージであり、完全なRTDではありません。QLP06/P02を単独でインストールしないでください。まず基本のRTDパッケージをインストールし、必要な場合にのみQLP06/P02をインストールしてください。単独でインストールすると、以下の結果になります。 必要な依存関係が不足しています: com.nxp.RTD.S32K3_S32M27X 0.0.0 この特定のS32K344デモでは、最低限必要なパッケージはベースのS32K3 RTD 7.0.1パッケージとS32K3 FreeMASTERドライバです。他のパッケージはより広いバンドルの一部であったり、プロジェクト依存関係によって必要になる場合があります。このS32K344デモにはK39xx RTDパッケージは必須ではありません。 Re: Errors Updating & Building S32K344 App Code Hub Example こんにちは、 RTDのパッケージ番号や説明についてのご不安は理解しています。 また、7.0.1.QLP5/6/P02はCryptoドライバを含むアドオンパッケージであることも正しいです。これらのパッケージは、ベースのS32K3 RTD 7.0.1パッケージの上にインストールする必要があります。 ただし、ACHのデモではオートモーティブ ソフトウェア パッケージ マネージャと FRDM Automotive S32K3 + S32M27ボードインストールパッケージへ案内されます。リアルタイム・ドライバ 7.0.1を選択すると、そのファイルが正確に表示されているのが見えます。 パッケージマネージャーでバンドルインストーラーを生成させれば、正しいパッケージを選択してインストールします。この特定の例では、これらのパッケージすべてが必須というわけではありません。前述の通り、必要なのはRTDとFreeMASTERドライバのみです。 ソフトウェアライブラリで必要なファイルを見つけたら、パッケージマネージャーで正確な名前を検索して正しいパッケージを特定してください。 S32K3 RTD 7.0.1パッケージのインストールに関しては、4つのドライバが含まれています。この S32K344 ADC 例では S32K39x および S32M27x ドライバは必須ではありません。しかし、今後のアップデートはベースパッケージによって異なる可能性があるため、4つのドライバすべてをインストールすることが強く推奨されます。 BR、ペトル  
View full article
Hands-On: Real-Time Control, Sensing, and Visualization with FRDM-A-S32K344 Attached is hands-on presentation Real-Time Control, Sensing, and Visualization with FRDM-A-S32K344 used during Electronica 2026 edge lab LIVE! event The presentation is designed for ​FRDM-A-S32K344 board, but might be reused also for different MCUs/boards with consideration board and pins specification. Brief Content: FRDM-A-S32K344 Board Overview​ Hands-On Application Code Hub (ACH) project Add Timer, GPIO and ADC pins Clock Configuration tips Push buttons Periodic Interrupt FreeMASTER Data Recording FreeMASTER Recorder Tips and Tricks​ As Initial example code we used Real-Time ADC Monitoring and LED Dimming Using FreeMASTER example from Application Code Hub. The content is Public: Free to use, modify, extend and share. We would be happy if you share with us significant improvements, modifications or porting to other boards/derivatives.   S32K3 , #FRDM-A-S32K344, S32DS-S32PLATFORM , FREEMASTER 
View full article
S32プラットフォーム用S32デザインスタジオ3.5ライセンス 私はノートパソコンとデスクトップパソコンをそれぞれ1台ずつ持っています。ノートパソコンでS32 Design Studioをアンインストールして再インストールするには、S32 Platform 3.5用のライセンスが2つ必要です。
View full article
s32k2018.R1 は延期できません。 このアクティベーションコードの有効期限を次回の期間まで延長していただけますでしょうか?よろしくお願いいたします。 アクティベーションコード D870-0066-E5E6-ACC7 Re: s32k2018.R1没办法延期 こんにちは、 お客様のS322DSライセンスが延長されました。以前のコードを使用して、S32DSを再度有効化してください。
View full article