LPCマイクロコントローラ・ナレッジ・ベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC Microcontrollers Knowledge Base

ディスカッション

ソート順:
    Writing this post just want to remind the customer of RAM allocation when use the on-chip CAN drivers in LPC11C24. Otherwise, when meet the abnormal issues, it is difficult to locate the root reason and it also causes a waste of time.      Now, take a real customer question as an example, to highlight the RAM allocation importance when using the on-chip CAN API in LPC11C24. Problem description     Customer used the LPC11C24 on-chip CAN API to realize the CAN frames sending and receiving, the CAN code was from the official lpcopen, and it worked OK when he just used the CAN code. But when customer added the UART code, they found the code always enter hardfault after a short time running. They test the UART code which without the CAN code directly, the UART code worked perfectly. It means, independent UART code and independent CAN code are all working normally, but when combine the UART and on-chip CAN code together, the code will enter hardfault. Problem analysis From the Cortex M0 devices generic user guide, we can get the information about the hard fault:     Faults are a subset of exceptions, see Exception model. All faults result in the HardFault exception being taken or cause lockup if they occur in the NMI or HardFault handler. The faults are:      execution of an SVC instruction at a priority equal or higher than SVCall      execution of a BKPT instruction without a debugger attached      a system-generated bus error on a load or store      execution of an instruction from an XN memory address      execution of an instruction from a location for which the system generates a bus fault      a system-generated bus error on a vector fetch      execution of an Undefined instruction      execution of an instruction when not in Thumb-State as a result of the T-bit being previously cleared to 0      an attempted load or store to an unaligned address Now we debug the problem project to check, which detail code line caused this hardfault problem. When the code enters the hardfault handler, check the MSP address in the flash, then find the LR register, which will link to the code before entering in the hardfault handler, the following are the according debug result:   The LR register is 0X1FFF2C1F, it means before enter in hardfault handler, the code runs to this address code. Now, check the 0X1FFF2C1F in the memory map.    We can find the address is in the ROM area, because we just use the ROM CAN driver, UART is just the pure register control code, then we can get the problem still relate to the on-chip CAN driver, not the UART code. But we can’t see or debug the detail ROM CAN driver directly, we still can’t find the root problem.    Even we know the problem is not caused by the UART, but another important clue which relates to the UART function also influence the test result after I do a lot of testing. In the customer code, he defines the UART user transmit and receive buffer like this: #define UART_SRB_SIZE 128    // Send #define UART_RRB_SIZE 32    // Receive /* Transmit and receive buffers */ static uint8_t rxbuff[UART_RRB_SIZE], txbuff[UART_SRB_SIZE];   On one occasion, I tried changing #define UART_SRB_SIZE 128 To  #define UART_SRB_SIZE 32 Just minimize the txbuff size, I found the code won’t enter in the hardfault handler any more. It seems very strange and contradiction with the hardfault handler enter point which is test before.    I also check the generated code size, the used RAM and flash size is:   text       data        bss        dec        hex    filename    7672          0        244       7916       1eec    pscan.axf LPC11C24 RAM is 8K, here just 244 Bytes, the stack also use the whole RAM, so the 8K RAM size should be enough to use.   In this situation, I check the project’s .map file about the txbuff with 128 and 32 respectively.    1)txbuff with 128Bytes Rxbuff and txbuff occupy the RAM address from 0X10000048 to 0X100000E8.     2)txbuff with 32Bytes Rxbuff and txbuff occupy the RAM address from 0X10000048 to 0X10000088. We can find the txbuff start address is the same, just the end address has difference.    With these information, we checked the LPC11C24 user manual chapter C_CAN on-chip drivers again, we found a significant description:      0X10000050 to 0X100000B8 is used by the on-chip CAN API RAM, and from the issue project, memory map file, we can find rxbuff and txbuff RAM address is 0X10000048 to 0X100000E8, it already occupies the whole CAN API RAM, this is the key point. Minimize the txbuff, then rxbuff and txbuff occupy the RAM address from 0X10000048 to 0X10000088, this address doesn’t occupy the whole on chip CAN API RAM, in this situation, the problem doesn’t happen, I think the used CAN API may in the RAM address 0X10000089-0X100000B8.    Anyway, just minimize the buffer size can’t solve the problem from the root side. We must follow the user manual to keep the RAM address from 0x10000050 to 0x100000b8 won’t be used by any other application code.   Problem solutions      From the above chapter, we can find the root problem is the application code occupies the on-chip CAN RAM, to solve the problem, we need to modify the linker file, to prevent the usage of on-chip CAN RAM range.      Because the customer is using the LPCXPresso IDE, then we take this IDE as an example, to protect the RAM address 0x10000050 to 0x100000b8. From the above, we can get that the LPCX11C24 have 8Kbytes RAM, normally, customer will define it just in one, now we divide the RAM to two pieces. 1) RAM2: Location 0X10000000, size 0X100 2) RAM: Location 0X10000100, size 0X1F00 In the LPCXpresso, Project Properties -> C/C++ Build -> MCU settings, then modify it like this:     Then generate the code, and check the map file again.   RAM address from 0x10000000 to 0X10000FF is not used by any other application code. All the application code RAM is using from address 0x10000100. After long time testing, we find the hardfault problem never happens, on customer side, it also works OK. In conclusion, when customer want to use the on-chip CAN API, they need to protect the RAM address from 0x10000050 to 0x100000b8 in the linker file.    
記事全体を表示
The following document contains a list of documents, questions and discussions that are relevant in the community based on the amount of views they are receiving each month. If you are having a problem, doubt or getting started in LPC or MCUXpresso you should check the following links to see if your doubt have been already solved in the following documents and discussions. MCUXpresso MCUXpresso Supported Devices Table  FAQ: MCUXpresso Software and Tools  How to create a new LPC project using LPCOpen and MCUXpresso IDE  Introducing MCUXpresso SDK v.2 for LPC54xxx Series  Generating a downloadable MCUXpresso SDK v.2 package  Using the MCUXpresso Pins Tool   MCUXpresso Config Tools is now available!   LPC55xx Multicore Applications with MCUXpresso IDE  LPC information LPC5460x MCU Family Overview  USB with NXP Microcontrollers LWIP memory requirements  LPC800 Four-Part Webinar Series!  The LPC804 Programmable Logic Unit (PLU)   LPC84x Technical Training - Now Available Guides and Examples Flashing and Installing the new firmware and drivers for LPC11U35 debug probes  Enabling debug output  USB FLASH download, programming, and security tool (DFUSec)  DMA Ping-Pong application  Getting start with LPCXpresso54608 & emWin Graphics;  Capacitive Touch example using the LPC845 Breakout Board  OLED Display Application Example using LPC845 Breakout Board and SPI  Mixed-Signal Logic Analyzer & Oscilloscope (Lab Tool) Solution  LPC FAQ How to calculate the value of crystal load capacitors? Can I send a message with X/Y/Z bits in the ID?  What is the difference between error active and error passive? What is the sample point for?  How can I verify the configured CAN bitrate, using an oscilloscope? 
記事全体を表示
MCUXpresso Config Tools is now available! You can access it on the following link: Welcome to MCUXpresso | MCUXpresso Config Tools  Overview. MCUXpresso Config Tools provides a set of system configuration tools that help users of all levels with a Kinetis or LPC-based MCU solution. Let it be your guide from first evaluation to production development. High Quality, Comprehensive Enablement - Production-grade, rigorously tested software and tools. - Easy-to-use SDK, IDE and configuration tools. Compatibility Across MCUs - Supports Kinetis, LPC Cortex-M. - Easy migration and scalability between MCUs. Note: i.MX Cortex-M device support coming in 2017 Interoperability Across Tools - Common experience and broader support through fewer, more cohesive software and tools. - Seamless development using SDK, IDE and Config tools together. - SDK and configuration tools also support the large ecosystem of NXP’s partner IDEs. Features. Architecture - CMSIS-CORE compatible - Single driver for each peripheral - Transactional APIs w/ optional DMA support for communication peripherals Integrated RTOS - FreeRTOS, µC/OS-II & -III - RTOS-native driver wrappers Integrated Stacks and Middleware - USB Host, Device and OTG - lwIP, FatFS - Crypto acceleration plus wolfSSL & mbedTLS - SD and eMMC card support Reference Software - Peripheral driver usage examples - Application demos - FreeRTOS usage demos License - BSD 3-clause for startup, drivers, USB stack Toolchains - IAR®, ARM® Keil®, GCC w/ Cmake - + MCUXpresso IDE Quality - Production-grade software - MISRA 2004 compliance - Checked with Coverity® static analysis tools Configuration and development tools.   SDK Builder packages custom SDKs based on user selections of MCU, evaluation board, and optional software components. Pins, Clocks, and Peripheral(1) tools generate initialization C code for custom board support. Project Generator(1) creates new SDK projects  or clones existing ones. Power Estimation tool provides energy and battery-life estimates based on a user’s application model Power Analyzer(1) measures and displays energy consumption data. (1)Coming 2017 Related links: Introducing MCUXpresso SDK v.2 for LPC54xxx Series  Generating a downloadable MCUXpresso SDK v.2 package  How to start with SDK v.2.0 for LPC5411x using LPCXpresso IDE  https://community.nxp.com/docs/DOC-333369   
記事全体を表示
Description The Telephone Answering Machine Design Example is a sophisticated telephone answering machine that provides everything commercial devices offer and more. Noteworthy features include improved voice quality and increased storage capacity over commercial machines. Additionally, Internet connectivity enables convenient messaging in the form of SMS messages or e-mails from anywhere in the world. Virtual answering machines can be set up for four different users. A user-friendly interface makes learning how to use this device and taking advantage of its many special features easy for anyone, regardless of their electronics savvy. The highly efficient system is designed around an LPC2138 microcontroller, which features an ARM7 RISC processor. Built with a small handful of components, the Telephone Answering Machine Design Example is cost-effective. The thoughtful inclusion of an external flash memory card and well-chosen algorithms for nearly unlimited storage capacity of crystal-clear messages contribute to the success of the design. Block Diagram Documentation Telephone Answering Machine Products Below are recommended microcontrollers for use in implementing a telephone answering machine. Comparison Table Product Pins On-Chip Flash On-Chip RAM Comments LPC2138 64 512KB 32KB Base microcontroller used in the design example. LPC2136 64 256KB 32KB A lower-cost microcontroller with the same amount of on-chip RAM but with only half the on-chip flash memory. LPC2146 64 256KB 32KB + 8KB An upgraded microcontroller with a USB interface. USB could be used instead of Ethernet to connect to a PC if Internet functionality is not desired. More Information Images Working Prototype Circuit Blocks Answer Flow Telephone Answering Machine Schematics Example Code Bill of Materials Disclaimer This design example shows possible hardware and software techniques used to implement the design. It is imperative that the viewer use sound engineering judgment in determining the fitness of this design example for any particular application. This design example may include information from 3rd parties and/or information which may require further licensing or otherwise. Additional hardware or software design may be required. NXP Semiconductors does not support or warrant this information for any purpose other than an informational design example. documentation.pdf 927.44 KB schematics.pdf 92.13 KB example.code_.zip 646.98 KB bom.txt 1.39 KB
記事全体を表示
This content was originally contributed to lpcware.com by Dirceu Rodrigues Introduction My work evaluating the SCT peripheral with the Hitex LPC4350 board (ARM Cortex-M4/M0) included the generation of non standard PWM signals for use in Power Electronics. At the end, some results would be compared with solutions based on LPC1114 (Cortex-M0), for example.  The first idea was to apply a concept that I had used when developing universal controllers for laser printer fuser, at 2001. This is a gate drive for MOSFET / IGBT isolated by pulse transformers. Two pulses Gate Drive – LPC1114 solution The circuit is implemented with pulse transformers (20 kHz PWM frequency) using the gate-source capacitance as memory. A Schottky diode avoids the stored charge to leak through windings. Thus, it's possible to achieve duty-cycles near to 0 and 100 %, simply applying 1 µs pulses shifted in time - one for charge, other for discharge. A very simplified schematic is shown in Figure 1.       Figure 1. Simplified circuit. My solution for the LPC1114 - Cortex-M0, uses two timers in a different scheme: Phase-out or lead/lag the counter values. With CT32B0 and CT32B1 32 bit timers, the behavior, including the pulsed outputs, is better understood looking on Figures 2 and 3 for duty-cycles of 75% and 25%. As opposed to common solutions, for each timer, the MR0 and MR1 matching registers values are constant. The difference between them is equivalent to pulse width (1 µs). The MR0 value also defines the period. The duty-cycle it’s determined through the expression:   DC = TC1 / MR0                                   (1) Where, TC1 is the CT32B1 timer value when this one, for the CT32B0, is zero.      In order to change the duty-cycle, the code in foreground task establishes a new TC1 and enables the CT32B0 overflow interrupt, where  this value is effectively loaded on CT32B1 timer in a safe point (to avoid jitter and other dangerous edges on outputs). Also, the CT32B0 ISR disables itself at the end, ensuring low interrupt overhead. For safety, the first applied pulse is a “discharge pulse”. This solution was proven driving a 930 W (120V/8.7 A) single-phase induction motor and it can be seen in reference [1], using a synchronous AC version of circuit shown in Figure 1 (no diode, four mosfets).      Figure 2. LPC1114 Two Pulses Gate Drive solution - DC 75%.  Figure 3. LPC1114 Two Pulses Gate Drive solution - DC 25%.      Two pulses Gate Drive – LPC4350 SCT solution The equivalent SCT implementation for the Two Pulses Gate Driver has the advantage of saving one timer. The pulse generation can be accomplished through a Mealy finite state machine plus the companion SCT counter. The LPC4350 generates 1 µs pulses with repetition rate of 20 kHz on CTOUT_4 and CTOUT_5 outputs. Two pushbuttons allow that a falling edge on CTIN_2 input, start the timer and a low value on CTIN_6, stop it. The counter operates as a unified 32 bit timer (UNIFY = 1) counting up and down (BIDIR = 1). ADC0 input is used to read the voltage on R26 potentiometer. So, the firmware can convert it in PWM change. As for LPC1114, the LPC4350 core and SCT runs in 48 MHz. Register MATCH 0 defines half-period. The difference between MATCH 2 and MATCH 1 registers is equivalent to pulse width (1 µs). In other words: PULSE_WIDTH = MATCH 2 - MATCH 1                       (2) Despite this difference be constant, now the MATCH 2 and MATCH 1 contents must change at the same time. Figures 4 and 5 show the waveforms for duty-cycles 15 % and 85 %. For example, the duty-cycle can be determined through the expression: DC = 1 – (MATCH 1 + 0.5*PULSE_WIDTH )/ MATCH 0        (3) Figure 4. SCT Two Pulses Gate Drive solution - DC 15%. Note: In companion source code, the PULSE_WIDTH is referred as PULSE_LENGTH. Figure 5. SCT Two Pulses Gate Drive solution – DC 85%. In order to achieve this behavior, one simple Finite State Machine with two states has been defined (Table 1): STATE Meaning 0 CTOUT_4 pulse generation 1 CTOUT_5 pulse generation Table 1. Definition of states. Figure 6 illustrates the relationship between the counter, states and interrupts. The PWM updating scheme takes advantage of following SCT property (as stated on User Manual): “A MATCH register is loaded from the corresponding MATCHREL register when BIDIR is 1 and the counter reaches 0”. In this application, the ADC0 interrupts MCU in a 24 Hz rate, triggered by TIMER0 MR0 (EM0 rising edge). The code on this ISR determines the new MATCH 1, saves it on global variable match1 and enables the SCT interrupt associated with event “counter reach limit” - in fact, event for MATCH 0. Here note, as stated in expression (3), that DC depends only on MATCH1, since MATCH 0 is constant. The ISR code for MATCH 0 event, updates MATCHREL 1 and MATCHREL 2 registers based on variable match1. Also disables the associated interrupt for low overhead. When counter reaches 0, the MATCH 1, 2 registers will be reloaded from the MATCHREL 1, 2 values automatically. This procedure should avoid jitter and other dangerous edges on outputs. Note that MATCH registers are never handled by software when counter is running. The new desired values are indirectly loaded on MATCHREL registers. The first values for MATCH registers are intentionally unreachable (> MATCH 0). This ensures that only ADC readings brought useful values to them. The on board potentiometer generates a voltage from 0 V to 3.3 V, which translates to 0 – 1023 range by the 10 bit AD converter. The MIN_MATCH1 and MAX_MATCH1 predefined values equates to 36 and 1116 (equivalent to duty-cycle 5 % and 95 % DC). Therefore, the software relates ADC0 voltage to with match1 variable approximately through the expression: match1 = [(MAX_MATCH1 - MIN_MATCH1)*ADC0] / 1024 +            (4)                                                  MIN_MATCH1 Note: In the companion source code, the division by 1024 is performed with a 10 bit right shift.           Figure 6. PWM updating scheme - DC 50%. Table 2 lists the eight states comprising the state machine for the current application. The companion state transition diagram is showed on Figure 7. Here, note other SCT important property, as stated on User’s Manual: “If more than one event associated with the same counter occurs in a given clock cycle, only the state change specified for the highest-numbered event among them takes place”. This applies to events 6 and 7. In normal operation, the event 6 happens periodically in State 1; but when a pushbutton press causes a low level on CTIN_6, the event 7 is fired on State 1 and counter is stopped. The state is driven to 0, with the outputs cleared (until one falling edge on CTIN_2 initiates the counting). EVENT ID Happens in state Conditions Actions 0 0 Falling edge on CTIN_2 Start counter 1 0 Counter reach MATCH 1 when counting up Set CTOUT_4 (pulse rise) 2 0 Counter reach MATCH 2 when counting up Clear CTOUT_4 (pulse fall) 3 0 Counter reach MATCH 0 Limit counter (defines the half period) Int. to update MATCHREL 1/ 2 Change to STATE 1 4 1 Counter reach MATCH 2 when counting down Set CTOUT_5 (pulse rise) 5 1 Counter reach MATCH 1 when counting down Clear CTOUT_5 (pulse fall) 6 1 Counter reach MATCH 3 (0) MATCH 1/ 2 automatic reloading Change to STATE 0 7 1 Counter reach MATCH 3 (0) AND Low value on CTIN_6 Stop counter MATCH 1/ 2 automatic reloading Change to STATE 0 Table 2. Definition of states. Figure 7. State transition diagram. Conclusion The PWM generation carried out by two short pulses shifted in time is a good alternative when isolation and duty-cycles far from 50% are required - specially driving gate charge devices like Mosfet/IGBT. The main advantage over opto-isolated implementations is not necessary create an auxiliary power supply.  Regarding to the architecture, the designer can use microcontrollers equipped with UP/DOWN timers (bidirectional), but is required some external glue logic in order to generate those short pulses. In comparison with the LPC1114 presented solution, the SCT version consumes just one timer/counter. As shown, the SCT peripheral is very independent, resulting in low (or no) MCU intervention after an initial configuration. This simple application used only two inputs, two outputs, two states and eight events. For more complex designs, the SCT provides up to 8 inputs, 16 outputs, 16 events and 32 states. I’ve future plans to make other power electronics applications based on SCT, including a small dot matrix printer controller. Code Red company   provides a tool to draw state diagrams and automatically generate code for the SCT engine, called Red State [2] (not used in this application). Finally, I would like to thank David Donley from NXP, who assisted me by answering my technical enquiries about the State Configurable Timer and suggesting improvements on code. References     [1]    http://www.youtube.com/DirceuRodriguesJr     [2]    http://www.code-red-tech.com/lpcxpresso
記事全体を表示
The minimum saturation current spec of Inductor is 300mA in the LPC55xx internal DC/DC converter, why is it 300mA, what is the actual current flowing through the inductor? 1)This is internal DC/DC converter block diagram for LPC55xx, on the LX pin, the 4.7uH inductor and 22uF capacitor are required, the FB pin is the detected pin to sense the output voltage, the DC/DC converter provide about 1.1V power for the VDD_PMU power supply pin. Let's discuss the current flowing through the inductor L1 via LX pin   2)compute the actual current flowing the inductor The above circuit is the illustrating block diagram, the control regulation uses PWM signal to control the MOSFET, but the high time of the PWM signal is constant for each PWM cycle, in other words, the on-time of the MOSFET is constant, for the LPC55S69 internal DC/DC converter, the on-time Δt is 0.52us, which means that the interval of MOSFET turning-on time is 0.52us. Assume that the VDC_IN is 3.3V, the output voltage of the DC/DC converter is 1.1V, the constant high time of the PWM signal is 0.52uS. when the MOSFET is on, the capacitor will be charged.   The above figure is the waveform tested on the LX pin of LPC55S68 on the LPC55S69-EVK board, you can measure via scope that the high time of the yellow PWM signal is 0.52uS, during which the MOSFET turns on, the capacitor is charged. The inductor works in DCM mode(discontinuous current mode)   The incremental current flowing the inductor during the MOSFET turns on: ΔI= (VDC_IN-VDC_OUT)* Δt/L=(3.3V-1.1V)*0.52*10**(-6)/4.7*10**(-6)=243mA.   3)The actual flowing current through the inductor is about 250mA for each PWM cycle, so when you select the inductor, the saturation current spec must be greater than actual current, the minimum required saturation current spec for the 4.7uH inductor is 300mA, when you select inductor for the DC/DC converter, you should select the inductor with 300mA or above saturation current .
記事全体を表示
Recently, customers reported that the number of PWM generated by SCTimer module was inconsistent between LPC55s06 user manual and data sheet. There are many kinds of PWM generation formats, so the maximum number of PWM generated by SCTimer is also different. I think the user manual and data sheet are not very clear, so this paper makes a specific analysis. It mainly depends on SCTimer resources, such as the number of events and output channels. For all LPC series, the mechanism of SCTimer generating PWM is the same. Therefore, this paper takes LPC55s6 as an example. LPC55s06 user manual: The SCTimer/PWM supports: – Eight inputs. – Ten outputs. – Sixteen match/capture registers. – Sixteen events. – Thirty two states. According to the different control modes of generating PWM wave, this paper is divided into single-edge PWM control, dual-edge PWM control and center-aligned PWM control. 1. Single-edge PWM control The figure below shows two single-edge control PWM waves with different duty cycles and the same PWM cycle length.   It can be seen from the above figure that the two PWM waves require three events: when the counter reaches 41, 65 and 100 respectively. Because of the same PWM cycle length, all PWM outputs need only one period event. Summary: The cycle length of all PWM waves are the same, so only one period event is required. The duty cycles of each PWM are different, and each PWM requires an event. The SCTimer of LPC55s06 has 16 events, one is used as PWM period event, and there are 15 left. Theoretically, 15 channels of PWM can be generated. However, LPC55s06 has only 10 outputs, so it can generate up to 10 single-edge control PWM waves. 2. Dual-edge PWM control The figure below shows three Dual-edge control PWM waves with different duty cycles and the same PWM cycle length.   It can be seen from the above figure that the three PWM waves require seven events: when the counter reaches 1, 27, 41, 53, 65, 78, 100.  Summary: PWM cycle length control needs one event, and each PWM duty cycle needs two events to trigger. The SCTimer of LPC55s06 has 16 events, one as PWM frequency event, and the remaining 15, so it can generate up to 7 dual-edge control PWM waves. 3. Center-aligned PWM control Center-aligned PWM control is a special case of dual-edge PWM control. The figure below shows two center-aligned PWM waves with different duty cycles and the same PWM duty length.   It can be seen from the above figure that the two center-aligned PWM waves need three events in total, which are the PWM cycle length and the duty cycle trigger of the two PWM waves. Because the left and right are symmetrical, only one event is needed to control the duty cycle of one PWM. Summary: All PWM have the same cycle length, so an event is required. The duty cycle of each PWM circuit is different, but the left and right are symmetrical, and an event trigger is required for each circuit. The SCTimer of LPC55s06 has 16 events, one is used as PWM cycle length, and there are 15 left. Theoretically, 15 channels of PWM can be generated, but LPC55s06 has only 10 outputs, so it can generate up to 10 channels of unilateral control PWM wave. Summary:   Maximum number of PWM generated by LPC55s6 SCTimer: Single-edge PWM control: 10 Dual-edge PWM control: 7 Center-aligned control: 10   The number of SCTimer events and output channels is different with different chips, but the analysis method is the same. Customers can analyze whether the SCTimer in a certain chip meets the requirements.
記事全体を表示
Symptoms Many LPC55 users experienced connection failure when using ISP USB0 for firmware update. In practice, we don’t suggest user updating firmware via ISP USB0 for LPC55(S)6x/ 2x,LPC55(S)1x/0x parts. Diagnosis LPC55 USB0 is Full Speed USB port. The default setting of CMPA turns off the USB0 port. Some users may reconfigure CMPA to enable ISP USB0 in order to use ISP USB0 BOOT, but this is not recommended in practice. LPC55 ISP USB0 uses internal FRO as clock source. According to LPC55 data sheet, the FRO accuracy is only +-2%, while the FS USB data rate tolerance specification is +-2500ppm(+-0.25%). Obviously, the LPC55 FRO spec can’t meet the USB0 clock accuracy requirement. See below extraction from NXP manuals. Fig 1. The accuracy of FRO ( Extracted from LPC55S69 Datasheet )   Fig 2. The accuracy requirement of USB FS( Extracted from TN00063 )  Some users may wonder why USB0 can use internal FRO as clock source in the user application?  Whenever internal clock source FRO is used as USB0 clock source, we must calibrate FRO in source code for communication. That’s to say, trim FRO to an accurate frequency. We can see FRO trim in many MCUXPressoSDK USB demos. When using FRO as the USB0 clock source, in order to ensure the USB0 clock accuracy, we must use the USB0 SOF frame synchronization to calibrate the FRO in order to ensure the accuracy of FS USB clock source (reference design of TN00063, TN00063-LPC5500 Crystal-less USB Solution). Unfortunately, the BOOT ROM of LPC55 does not support USB SOF calibrating FRO. As a result, even if we enable ISP USB0, the FRO clock drift can still cause USB0 communication failure under non-room temperature conditions. Solution Since ISP USB0 is not recommended for firmware update, the user manual no longer announces the enablement bit of ISP USB0 in CMPA. If you need to use USB0 for firmware update, we recommend using ISP USB1 (High Speed USB), because USB1 uses accurate external clock source which can ensure the ISP USB1 working stable. In addition, the communication protocol of ISPUSB complies with BLHOST specification. For details, see:  blhost User's Guide - NXP  
記事全体を表示
This article mainly introduces how to config CTIMER match 3 trigger ADC in LPC804, includes how to config related registers, and the code under SDK. Other LPC serials, also can refer to this DOC. 1.How To Configure ADC Part. 2.How to Configure CTIMER Part 3.Project Basic Information 4.Reference   Project is attached, it base on MCUXpresso IDE v11.1.1,  LPCXpresso804 board.  
記事全体を表示
This content was originally contributed to lpcware.com by Steve Sabram This example project implements acoustic range, finite infinite response (FIR) filters using the LPC4350 demo board and the ARM CMSIS DSP library. A sound resource of a science fiction “zap gun” plays out the headphone jack of the demo board. This sound sample is great for demonstration since it has many low-, mid-, and high-frequency components along the acoustical band. You play the sound resource by touching the capacitive touch buttons on the demo board as explained by the menu shown on the demo board’s LCD. It is best to listen to the sound with a headphone or ear buds. Each of the four buttons plays the same sound resource differently: 1)  Raw – The unprocessed sound plays according to its format (sample rate of 44.1 kHz, 16-bit sample and mono sound). 2)  Low Pass – filtered through a low pass, Butterworth filter with a cutoff of 5 kHz, similar to the bandwidth of a common analog telephone. When played, notice that high pitch components are removed similar       to the sound heard over a telephone. 3)  High Pass – filtered through a high pass, Butterworth filter with a low frequency cutoff of 8 kHz. Notice that the sound is lower in volume since only the upper harmonic components are played. 4)  Backward Mask – The sound resource sample plays in reverse order. The “Zap!” is now a “Zoup!” The digital filters were designed with a favorite public domain tool, WinFilter (http://www.winfilter.20m.com/)       accompanying this example. With exposure of this free DSP design tool via NXP, I hope its author expands its features.
記事全体を表示
In this document, I will explain how to create a project to use the SPIFI library version 1.03 with the LPC4370. For this we will need the following tools: MCUXpresso IDE 10.2. Link LPC-LINK2 to use it as an evaluation board for the LPC4370. Link External debugger. In my case, I used another LPC-LINK2 board. LPCOpen v2_12 for the LPC4370, this version comes with the installation of MCUXpresso IDE. SPIFI library v1.3. Link Code Example lpcopen_2_12_lpcxpresso_ngx_xplorer_1830_SPIFI_v1.0. Link First, download and install all the tools needed. In your workspace of MCUXpresso we will import (1) three projects of the LPCOpen v2_12 for the LPC4370: periph_blinky, lpc_board_nxp_lpclink2_4370 and lpc_chip_43xx.  The LPCOpen zip file is in the next path of your PC: C:\nxp\MCUXpressoIDE_10.2.1_795\ide\Examples\LPCOpen (2) Extract the files of the zip named lpclibspifi_lpcxpresso_1.03_68 that we downloaded before. The folder that we need is spifilib_m4f. Drag and drop this folder into the Project Explorer on your workspace of the LPC4370, after choosing copy and you should see the spifilib_m4f in your Project Explorer. Once you imported correctly the SPIFI library, select the library (1) on the project explorer window and build it (2). Once you do this you should see that a new folder called Debug appear (3). Now we need to edit the properties of the periph_blinky example to add the library spifilib_m4f to the project. To do this, right click on the project and click properties. Once in the properties window click on C/C++ Build (1) > Settings (2) > Includes (under the section MCU C Compiler) (3). In the includes window click Add… (1) > Workspace (2) > spifilib_m4f (3) > inc (4) > click OK (5) on the window Folder Selection > click OK (6) on the window Add directory path. You should see the following on the include paths. Now, go to the libraries (1) option under the section MCU Linker, on the section Libraries (-I) click Add… (2) finally write the name of the library (spifilib_m4f) (3) and click OK (4). Under the section Library search path (-L) click Add… (1) > Workspace (2) > spifilib_m4f (3) > Debug (4) > OK (5). If you see the same as shown in the below image you are good to go so click Apply and close. To check if you did the below steps correct let’s do the following. On the project periph_blinky in the file systick.c include the file spifilib_api.h and compile the project. If the project compiles without problems it means that you imported correctly the spifi library. If you found problems please stop and repeat all the steps mentioned before. Now that we added successfully the library we can start to migrate the example for the LPC1830 that we download before. First, unzip the file lpcopen_2_12_lpcxpresso_ngx_xplorer_1830_SPIFI_v1.0. Once you unzipped the file go to the following path: spifilib_blinky > example > src. Open the file named Blinky.c and copy all the content of the file. Now go to the file systick.c on your workspace of MCUXpresso within the project periph_blinky, delete all the content of this file and paste what you copied before. Do not compile at this point or you will receive multiple errors! Go back to the path spifilib_blinky > example > src on your PC. Drag and drop the file called spifi_setup.c into the folder src of your project periph_blinky on your Workspace. Open the file that we just copy into our workspace and go to line 46 of the code. Here we are creating a buffer of 64KB that we will use later to write in the SPIFI. The __BSS(RAM3) is to save this buffer in the RAM block three of memory. The problem here is that the block of RAM3 in the LPC4370 is not big enough to store the buffer of 64KB (see below image), so let’s change this for either RAM or RAM2 that are big enough to store the buffer. Now that we added the spifi_setup file let’s go back to the systick.c file and add the external declaration for the function spifiSetUp. At this point, if we compile the project we shouldn’t see any problems, only some warnings because of the functions and variables that we are not using. We are almost done, we are missing the most important thing. With this demo you will be writing, deleting and reading the SPIFI memory, this means that you cannot be executing form the SPIFI flash memory. You need to move to the RAM memory all the functions that are going to make this. This is the reason why in the file systick.c we don’t have any function that interacts directly with the SPIFI, this will make much easier the work of moving all the functions that interact with the SPIFI memory to RAM. The function spifiSetUp is the one that will make all the tests on the SPIFI and it is in the spifi_setup file, so we will need to move this entire file to RAM along with the SPIFI library. We will use three different scripts to move the library and the file spifi_setup to RAM. You can learn more about this in the following community post: https://community.nxp.com/thread/389110. First, right click on the folder of the project > new > folder, the name of the folder must be linkscripts. According to the sections Relocating particular objects into RAM and Relocating particular libraries into RAM of the community post mentioned before we need to create three files in this new folder: main_text.ldt, main_rodata.ldt and main_data.ldt. To do this, right click on the folder linkscripts > new > file. Here is the content that you should have on the three files that we just created. Do not include on the files the text that is in bold, that's just for reference! File main_data.ldt *libspifilib_m4f.a:(.text*) *libspifilib_m4f.a:(.rodata .rodata.* .constdata .constdata.*) *spifi_setup.o(.text*) *spifi_setup.o(.rodata .rodata.* .constdata .constdata.*) . = ALIGN(${text_align}); *(.data*) File main_rodata.ldt *(EXCLUDE_FILE(*libspifilib_m4f.a: *spifi_setup.o) .rodata) *(EXCLUDE_FILE(*libspifilib_m4f.a: *spifi_setup.o) .rodata.*) *(EXCLUDE_FILE(*libspifilib_m4f.a: *spifi_setup.o) .constdata) *(EXCLUDE_FILE(*libspifilib_m4f.a: *spifi_setup.o) .constdata.*) . = ALIGN(${text_align}); File main_text.ldt *(EXCLUDE_FILE(*libspifilib_m4f.a: *spifi_setup.o) .text*) After finishing with the three files you are done with the demo! It’s important to mention that if you want to go inside the function spifiSetUp while debugging you need to set a breakpoint inside the function. While debugging we can see that before calling the function spifiSetUp we are running from the SPIFI flash memory and once we enter to the function we are running from RAM memory. Once we run the demo successfully we should see the following in a terminal and the LED1 will be blinking. Hope this guide is helpful! Best Regards, Victor.
記事全体を表示
Link to board: http://www.lpcware.com/content/devboard/android-open-accessory-aoa-kit Android Demos There are three demos available for download on the Embedded Artists website http://embeddedartists.com/products/app/aoa_kit.php The code bundle contains the following: Demo 1: Android Open Accessory demo which lets you control and monitor the AOA Board (LPC1769 side) from an Android device. Demo 2: Android Open Accessory demo which lets an Android device detect CAN nodes (such as the LPC11C24 side of the AOA board) in a CAN network. The CAN nodes can be controlled and monitored from the Android device. Demo 3: Android Open Accessory demo which lets an Android device detect Xbee nodes in an Xbee network. The Xbee nodes can be controlled and monitored from the Android device. FreeRTOS has been ported to the board and a demo is available that show how to use it. lwIP v1.4.0 has been ported to the board. The httpserver_raw (webserver) application from the lwIP contrib package is available with a small modification to use the on-board SD-card interface instead of the ROM based file system. FatFs file system module has been ported to the board. The lwIP demo (based on httpserver_raw) is using this module to access files on an SD card. nxpUSBlib is available and used in the AOA demos. How to setup the projects in LPC Xpresso Make sure that the latest version of the LPCXpresso IDE is installed. Download the package of sample application projects into the Eclipse workspace. The package can be downloaded (as a zip-file) from Embedded Artists’ support page after registering the product. The zip-file contains all project files and is a simple way to distribute complete Eclipse projects. Start the LPCXpresso IDE and select a new (and empty) workspace directory. Select the Import and Export tab in the Quickstart Panel and then Import archived projects (zip), see Figure 1 below. Browse and select the downloaded zip file containing the archived sample applications. Select all sub-projects to be imported, see Figure 2 below. By default the NXP USB library has been configured for USB device only. This needs to be changed to USB host. Right click on the nxpUSBlib project and select Build Configuration, then Set Active. In the list select LPC17xx_Host. See Figure 3. The projects are now imported. Click (to select) the project to work with. Click Build in the Quickstart Panel (under Start Here). See Figure 4 There is also a video on how to setup Demo 1 and get it running by connecting your android device. (Getting started video provided by Embedded Artists) http://www.youtube.com/watch?v=l3f2ss1IdV0&feature=player_embedded
記事全体を表示
In newer version of LPC Boot ROM , checksum is added in location 7 ( offset 0x0000001C in vector table ) of Boot ROM. For some LPC device, for example LPC8N04, older Boot ROM version 0.12 (equipped in Rev B board) doesn’t contain checksum but newer version 0.14( equipped in Rev C board ) adds it. Boot ROM checksum is a criteria for valid user code. Bootloader can jump to user code only when detects checksum value correct. Otherwise, it stays at boot code.   Scenario: User may have this annoying problem: the program runs well if download code to LPC flash with debugger. However power off and on again, the code won’t run any more. If you also experience same in field, you may consider the possibility of Boot ROM checksum failed. This document tells how overcome this problem. 1. calculate checksum value by hand 2. calculate checksum value with Keil elfdwt.exe For detail, see attached article.
記事全体を表示
How to start with SDK v.2.0 for LPC5411x using LPCXpresso IDE This document gives an overview of SDK v.2.0 for LPC5411x and also describes the steps required to build, run, and debug an example application provided in the SDK using LPCXpresso IDE. The steps described in the document are for the LPCXpresso54114 board (OM13089).   SDK for LPC5411x Derivatives Overview   The Software Development Kit (SDK) provides comprehensive software support for Microcontrollers. The SDK includes a flexible set of peripheral drivers designed to speed up and simplify development of embedded applications. Along with the peripheral drivers, the SDK provides an extensive and rich set of example applications covering everything from basic peripheral use case examples to full demo applications. The SDK also contains RTOS kernels and various other middleware to support rapid development on devices. SDK board support provides example applications for development and evaluation boards. Board support packages are found inside of the top level boards folder, and each supported board has its own folder (a SDK package can support multiple boards). Within each <board_name> folder there are various sub-folders to classify the type of examples they contain. These include (but are not limited to): demo_apps: Full-featured applications intended to highlight key functionality and use cases of the target MCU. These applications typically use multiple MCU peripherals and may leverage stacks and middleware. driver_examples: Simple applications intended to concisely illustrate how to use the SDK’s peripheral drivers for a single use case. These applications typically only use a single peripheral, but there are cases where multiple are used (for example, ADC conversion using DMA). rtos_examples: Basic FreeRTOS examples showcasing the use of various RTOS objects (semaphores, queues, and so on) and interfacing with the SDK’s RTOS drivers multicore_examples: Applications for both cores showing the usage of multicore software components and the interaction between cores.   Build, run and debug a SDK example   This section describes the steps required to configure LPCXpresso IDE to build, run, and debug an example application. The hello_world demo application targeted for the LPCXpresso54114 is used as an example, though these steps can be applied to any example application in the SDK.   1. Download and install the latest LPCXpresso version from the next link: http://www.nxp.com/products/software-and-tools/software-development-tools/software-tools/lpc-microcontroller-utilities/lpcxpresso-ide-v8.2.2:LPCXPRESSO 2. Follow the steps describe here to download the Software Development Kit (SDK) v2.0 for LPCXpresso54114: Generating a downloadable MCUXpresso SDK v.2 package  3. Select "File -> Import" from the LPCXpresso IDE menu. In the window that appears, expand the "General" folder and select "Existing Projects into Workspace". Then, click the "Next" button.       4. Click the "Browse" button next to the "Import from file:" option, and point to the example application project, which can be found using this path: <install_dir>/boards/<board_name>/<example_type>/<application_name>/lpcx/cm4 For this example, the specific location is: <install_dir_SDK_2.0_LPCXpresso54114>\boards\lpcxpresso54114\demo_apps\hello_world\lpcx\cm4 Then Click the "Finish" button. 5. There are two project configurations (build targets) supported for each SDK project: Debug – Compiler optimization is set to low, and debug information is generated for the executable. This target should be selected for development and debug. Release – Compiler optimization is set to high, and debug information is not generated. This target should be selected for final application deployment. So it is necessary to choose the appropriate build target. For this example, select the "Debug" target.   6. Build the project using the hammer icon. 7. Connect the development platform to your PC via USB cable between the Link2 USB connector (named Link for some boards) and the PC USB connector. If connecting for the first time, allow some seconds for the devices to enumerate.   8. In the Windows operating system environment, open the terminal application on the PC and connect to the debug serial port number. For this example it is used Tera Term.   Configure the terminal with these settings: 115200 No parity 8 data bits 1 stop bit    9. In LPCXpresso IDE, click on “Debug Configurations”. In the Debug Configurations dialog box, select the debug configuration that corresponds to the hardware platform you’re using. In this example, select is the CMSIS-DAP option under C/C++ (NXP Semiconductors) MCU Application. 10. After selecting the debugger interface, click the "Debug" button to launch the debugger. 11. Additional dialog windows may appear to select LPC-INK2 CMSIS-DAP emulator and core in case of multicore derivatives. Select it and click the "OK" button. Then select the Cortex-M4. The application is downloaded to the target and automatically run to main():    12. Start the application by clicking the "Resume" button. The hello_world application is now running and a banner is displayed on the terminal. Enjoy!!   Related links: Introducing MCUXpresso SDK v.2 for LPC54xxx Series  Generating a downloadable MCUXpresso SDK v.2 package  MCUXpresso Config Tools is now available!  
記事全体を表示
This document explains how to start with LPCXpresso845-MAX Evaluation Board building, running and debugging example codes. Introduction   Based on the ARM Cortex-M0+ core, LPC84x is a low-cost, 32-bit MCU family operating at frequencies of up to 30 MHz. The LPC84x MCU family supports up to 64 KB of flash memory and 16 KB of SRAM. There is no LPCOpen nor SDK for LPC84x, however there is an example code bundles (register level) available for this family. The example code bundles offer a fastest, and simplest way for user to learn how to program each peripheral before progressing to more advance features of the peripheral. New users of LPC84x can step through the Example Code like a tutorial. Each project contains concise and accurate explanations in Readme files and comments in source files help the user to start/debug quickly. LPC845 Example Code Bundle is available for KEIL, MCUXpresso and IAR IDEs and you can download it from next link:   http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/lpc-cortex-m-mcus/lpc800-series-cortex-m0-plus-mcus/low-cost-microcontrollers-mcus-based-on-arm-cortex-m0-plus-cores:LPC84X?tab=Design_Tools_Tab Build, run and debug an example   This section describes the steps required to build, run, and debug an example application. 1. Download the LPC845 Example Code Bundle MCUXpresso from the next link:  http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/lpc-cortex-m-mcus/lpc800-series-cortex-m0-plus-mcus/low-cost-microcontrollers-mcus-based-on-arm-cortex-m0-plus-cores:LPC84X?tab=Design_Tools_Tab 2. Open MCUXpresso IDE. 3. Select "Import project(s) …" from the Quickstart Panel. 4. Click the "Browse" button and point to the LPC845-Example-Code-Bundle-MCUXpresso.zip, which should be downloaded previously, and then click “Next” button. 5. By default all the projects are selected, however you can select only the desired example project. In order to build the example project, it is necessary to add in the workspace the following projects: common peripherals_lib utilities_lib For this document, we are using the Multi_Timer_Blinky example project. 6. Build the project using the hammer icon on Quickstar Panel.  7. Connect the development platform to your PC via USB cable. If connecting for the first time, allow some seconds for the devices to enumerate.   8. This example runs from Flash. To run this code you have two options: a) Download and Debug.    b) Load to flash using the “run” IDE icon and press the reset button on the board. Note: It may be necessary to power-cycle the board in order to regain control of the reset button after programming. At this moment, you can be able to run or debug the example project. I hope this helps!!!
記事全体を表示
LPC: Regarding to Internal Clock Calibration In MCU development, using the internal crystal oscillator as a clock source instead of the external crystal oscillator can save costs. But the clock frequency generated by the internal crystal oscillator is affected by temperature and MCU frequency more than external crystal oscillator. Many customers have questions about the internal clock accuracy, whether the internal clock can be used for USB transmission, and how to calibrate the internal clock. This article mainly explains this. 1. Calibrate internal clock by FREQTRIM Normally, we can only calibrate the internal clock by adjusting the FREQTRIM value. The internal clock frequency is affected by temperature, MCU frequency and other factors. The FRO control register can calibrate the internal clock, as follows:   The FREQTRIM register value ranges from 0 to 255, and each adjustment step is about 0.1% of the internal clock frequency. There is no precise formula to express the relationship between the FREQTRIM value and the FRO frequency. The ideal FREQTRIM value can only be determined by adjusting FREQTRIM in code and observing FRO output waveform with oscilloscope. Test and observation: The following is the test result. It shows how FRO frequency varies with FREQTRIM increasing from 0-255. Test result of first development board:     Test result of second development board:   The following two points can be seen from test results: - There is no linear relationship between the FRO clock frequency and the FREQTRIM register value, and there is no precise formula to express the relationship between them; - Even for chips of the same part number, the internal clock frequency changes are slightly different, with the FREQTRIM register value changing, but the trend is same. Therefore, there is no precise formula to guide internal clock frequency calibration. You can only adjust the FREQTRIM register value repeatedly, just like adjusting the focus of a projector. Use an oscilloscope to check the frequency of the internal clock pin to find the most suitable FREQTRIM register value. There is same solution for FRO clock frequency calibration about other LPC chips.   2. LPC51U68: Software calibration USB transmission when using internal clock source The Full Speed USB module of LPC51U68 has a unique FRO automatic calibration function, which automatically adjusts the FREQTRIM value to achieve FRO calibration by measuring the USB SOF bit. Once FRO is calibrated, the corresponding system clock and peripheral clock are calibrated. This solution is only applicable to LPC51U68, please refer to the user manual for other chips. The following is the FRO clock accuracy described in LPC51U68 User Manual, which is ±1%:   For Full Speed USB, the USB data transmission accuracy requirement is ±0.25%, and the FRO clock accuracy is not satisfied. NXP provides a software solution to calibrate FRO by measuring the first packet of frame (SOF), which can meet the transmission accuracy in Full Speed mode.   The solution download link is as follows: https://www.nxp.com/docs/en/application-note/TN00035.zip  
記事全体を表示
Hello Community! This document is provided as a hands-on lab guide.  The intent of the lab is to demonstrate how to program the LPCXpresso804 board with the MCUXpresso IDE making use of the SDK examples and the PLU module drivers. The PLU configuration tool will be used to create a new schematic design that will be programmed to the PLU. Setup The following items need to be installed on your computer to complete the lab: Software: •    SDK_2.4.1_LPCXpresso804: -    Copy link into browser: https://mcuxpresso.nxp.com/en/select?device=LPCXpresso804 -    Select ‘MCUXpresso IDE’ or ‘All Toolchains’ in the Toolchain IDE drop-down -    Select ‘Download SDK’ •    MCUXpresso IDE version 10.2.1: -    Can be installed at following link: https://www.nxp.com/mcuxpresso/ide •    PLU configuration tool -    Can be installed at this link: https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/i.mx-applications-processors/i.mx-rt-series/i.mx-rt1060-crossover-processor-with-arm-cortex-m7-core:i.MX-RT1060?tab=Design_Tools_Tab   Hardware: •    LPCXpresso804 Development Board (OM40001): https://www.nxp.com/support/developer-resources/evaluation-and-development-boards/lpcxpresso-boards/lpcxpresso804-for-the-lpc804-family-of-mcus:OM40001?tab=Design_Tools_Tab •    PLU Shield Board •    1 Micro USB cable Hope this guide is helpful! Any comments are welcome. Best Regards, Carlos Mendoza Technical Support Engineer
記事全体を表示
For the LPC8xx family, the peripheral module input or output signals are not connected to external pads fixedly as most processor does . With SWM module, the peripheral module input or output signals can be routed to any external GPIO pins via software configuration There is special requirement that one peripheral output signal functions as the input signal of another peripheral, in the case, the peripheral output signal and the peripheral input signal can be routed to the same pad via SWM so that the input and output signals are connected internally without external cable. The LPC802 has ACOMP module, CTimer module and SWM module, per customer requirement, the ACOMP output signal and CTimer0 capture 0 input signal can be routed to the same GPIO pin without external connection so that the ACOMP output signal can trigger CTimer0 capture 0 event internally. In the doc, I give the code to configure the CTimer, ACOMP and the SWM, explain the configuration,introduce the tools, board and result.  
記事全体を表示
The documentation is only valid for the LPC55xx and LPC55Sxx families. In power down mode, some of peripherals for LPC55xx are power off, which means that the peripherals lose it’s power in power-down mode, so it is required to reinitialize the peripherals after waking-up from  power down mode. The DOC lists the peripherals which lose power in power down mode and are required to initialize, introduces the procedure to enter the power down mode, and  the procedure to reinitialize the peripherals after waking-up from power down mode. The doc is attached and power scheme is also attached.
記事全体を表示
The article introduces the RSA theory, how to get the RSA parameter, how to encrypt/decrypt with the RSA algorithms. RSA is an asymmetric cryptographic algorithm and widely used in encryption/decryption application and signature application. It completes encryption and decryption operations by encrypting the message with the public key and decrypting with the private key. In order to support security requirements, it is also used in many places in the LPC55 series, such as: -  RSA digitally signs the application code with the private key, and verifies the authenticity of the code through RSA signature verification in secure boot. This is implemented in LPC55 secure boot. For the LPC family, the mbedtls library is used to implement the RSA algorithms with software.
記事全体を表示