Examples for current KSDK 1.3 are located under C:\Freescale\KSDK_1.3.0\examples
examples for middleware (tcpip, filesystem) under C:\Freescale\KSDK_1.3.0\middleware
There are more examples, which were created:
KSDK 1.3
Rainbow color using FTM PWM with KSDK 1.3
How to use printf() to print string to UART in KDS3.0 + KSDK1.3
Driving 16x2 LCD using KSDK drivers
Integrating NFC Controller library with KSDK
KL43Z support for sLCD and Touch sense using KDS3.0 +KSDK1.3.0 + Processor expert
KSDK 1.2
Using DMA to Emulate ADC Flexible Scan Mode with KSDK
Writing my first KSDK1.2 Application in KDS3.0 - Hello World and Toggle LED with GPIO Interrupt
Controlling speed in DC motors and position in servomotors with KSDK [FTM + GPIO]
Line scan camera with KSDK [ADC + PIT + GPIO]
A simple way to detect the track's center for the Freescale Cup Smart Race
FatFs + SDHC data logger with KSDK in Kinetis Design Studio
KSDK GPIO driver with Processor Expert
DAC Sinus Demo (using PEx + KSDK 1.2 + KDS 3.0)
How to start customized KSDK project based on KSDK demo code
KSDK 1.1
An example project for FIR function implement on KV31 with SDK and CMSIS
How to toggle LED in KDS 2.0 with KSDK 1.1.0 and Processor Expert
KSDK SPI Master-Slave with FRDM-K64F
Configuring Kinetis Software Development Kit (KSDK) to measure distance with ultrasonic transducers
A demo project of USB HID bi-directional generic device for Kinetis SDK 1.1.0
Configuring Kinetis Software Development Kit (SDK) to measure distance with infrared (IR) sensor
Writing my first KSDK Application in KDS - Hello World and GPIO Interrupt
KSDK 1.0
Are these examples going to be updated for KSDK 2.0 - These examples are for obsolete KSDK versions, no?
Also, Processor Expert is apparently obsolete and will not be further developed?
Thanks,
Best Regards, Dave