This patch adds Segment LCD (SLCD) examples for the Kinetis Tower boards with the TWRPI-SLCD module. It reuses the SLCD driver included in the "Kinetis SDK 1.2.0 Standalone for KL33Z for the FRDM-KL43Z", and ports the example to boards using the TWRPI-SLCD module.
The patch was written for KSDK v1.2.0, found at www.freescale.com/KSDK. To install the patch, unzip to the KSDK installation directory, by default it is C:\Freescale\KSDK_1.2.0. Only the Debug Build Configurations in the libraries and example applications were updated for these examples. The Release Build Configurations will need to be updated before using. The boards supported with these examples are:
TWR-KL46Z48M
TWR-KL43Z48M
TWR-KL46Z48M board example is provided with a project for Kinetis Development Studio (KDS) toolchain, and tested with KDS v3.0.0. The path for this example is at \KSDK_1.2.0\examples\twrkl46z48m\demo_apps\slcd_low_power_demo\kds. The example also includes the KDS .WSD working set file. When this is imported to KDS, it imports both the platform library and example application. The example is written to display time on the TWRPI-SLCD, and will display mm:ss.
TWR-KL43Z48M board example is provided with a project for Kinetis Development Studio (KDS) toolchain, and tested with KDS v3.0.0. The path for this example is at
\KSDK_1.2.0\examples\twrkl43z48m\demo_apps\slcd_low_power_demo\kds. The example also includes the KDS .WSD working set file. When this is imported to KDS, it imports both the platform library and example application. The example is written to display time on the TWRPI-SLCD, and will display mm:ss.
How to have the fsl_slcd component into processor expert ?