Kinetis Microcontrollers Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis Microcontrollers Knowledge Base

Discussions

Sort by:
Freescale's Jeff Bock highlights the awesome features of the Kinetis 32-bit microcontrollers based on the ARM Cortex-M4 core
View full article
The ARM Cortex-M4 Kinetis K50 MCU integrates an analog measurement engine consisting of integrated operational and transimpedance amplifiers and high-resolution ADC and DAC modules that make it ideal for portable healthcare and medical applications. For more information visit www.freescale.com/kinetis
View full article
Hi team :      I would like to share an experience to you . Any comments would be welcome .      The RTC 32.7668KHz clock can only be sourced from an external crystal that is challenged of some space restricted case . The internal reference clock will be required to support RTC at this moment . Of cause , the IRC accuracy maybe not compete with external crystal , but in this case space is the major concern . However , Kinetis RTC not support clock sourced from IRC . We make a workaround to enable RTC reference to IRC . The detail please refer to attachment . The sample code is build with KDS V3.0 for FRDM-K64F . Best regards, David
View full article
unexplained secured, unexplained locked and unexplained link error.
View full article
The Kinetis K70 MCU family includes 512KB-1MB of flash memory, a single precision floating point unit, Graphic LCD Controller, IEEE 1588 Ethernet, full- and high-speed USB 2.0 On-The-Go with device charge detect, hardware encryption, tamper detection capabilities and a NAND flash controller. 256-pin devices include a DRAM controller for system expansion. The Kinetis K70 family is available in 196 and 256 pin MAPBGA packages. For more information visit www.freescale.com/kinetis
View full article
Hello Community fellows! This time I would like to thank BlackNight for giving us great material to work on. There have been several posts inquiring the uses of USB stack and Processor Expert. The examples he has worked on and now shares with all of us, include this and many more useful concepts that you'll find interesting with the use of boards. For this issue he turns his FRDM-KL25Z into a generic USB keyboard device. With a simple button press he is able to send any keyboard actions to his laptop, making such as ‘print screen’ a single button press...isn't that amazing? :smileygrin: Well, I'll say no more, you better check it out yourself!  MCU on Eclipse by Erich Styger
View full article
I’m using the NXP FRDM-K64F board in several projects.One issue I have faced several times is that the board works fine while debugging and connected and powered by a host machine, but does not startup sometimes if powered by a battery or started without a debugger attached. I have found that the EzPort on the microcontroller is causing startup issues. The EzPort is a special serial interface present on some Kinetis, ColdFire+ and ColdFire V2 devices. The issue is that if the EzPort chip select (EZP_CS) is LOW during reset of the microcontroller, it enters the special EzPort mode. The problem is that a pull-up on the EZP_CS line might not pulled up fast enough due capacitance on the line. The commance is if something is not used, disable it! So the solution is to disable the EzPort functionality. That setting is part of the FOPT (flash option register).
View full article
Some early TWR-K64F120M Revision B boards were shipped with incorrect jumper configurations and demo application. Jumper settings should be: J39 shunt 1-2 J16 shunt 1-2 J29 shunt 1-2 J10 shunt 2-3 J15 shunt 2-3 Updated application demo code and Quick Start Guide can be found at https://www.nxp.com/TWR-K64F120M   TWR-K64F120M boards with updated jumper configurations and demo code will be tagged with a label marked TDA4906 on the bottom side of the board.
View full article
En México, el 5.1% de la población vive con algún tipo de discapacidad, de los cuales 23% poseen discapacidades del tipo motriz en extremidades inferiores y superiores (INEGI, 2011). Los métodos que actualmente se utilizan en el proceso de rehabilitación no poseen características integrales en las que el usuario pueda aprovechar la terapia para ejecutar diferentes acciones. El objetivo de este proyecto es el de diseñar y construir una herramienta que permita al usuario no solo hacer ejercicios de rehabilitación, sino que también le ayude a realizar tareas cognitivas o a interactuar con algún medio electrónico (i. e. navegar por internet, realizar trabajos a través de una computadora con Rehab Glove como mouse y/o teclado). Rehab Glove es una herramienta en forma de guante que posee sensores de flexión en las articulaciones de los dedos y de fuerza en las yemas, ubicados estratégicamente con el fin de obtener diferentes valores arrojados mientras el usuario realiza ejercicios de rehabilitación como cerrar el puño o tocar las yemas de los dedos con el pulgar. Estos valores serán convertidos en instrucciones diversas que van desde mover un  carro a control remoto, pasando por el control de videojuegos educativos, hasta llegar a tareas más complejas como escribir o controlar el cursor de una computadora sin la necesidad de un mouse o un teclado. La terapia comenzará con el usuario portando RehabGlove frente al elemento que desea controlar, pidiéndole que realice movimientos específicos con la mano para que pueda lograr el objetivo final. Se espera que el nivel de complejidad vaya aumentando en cuanto al tipo de movimientos, rapidez, precisión y fuerza aplicada en cada acción. Con el uso de RehabGlove se espera que las terapias de rehabilitación posean niveles de cognición mayores y que tengan un avance progresivo aumentando el nivel de complejidad en cada ejercicio.   Video de prototipo<<<<< Rehab Glove Kinetis - YouTube Original Attachment has been moved to: Codigo-Fuente-Rehab-Glove.txt.zip
View full article
Anis Jarrar, Freescale design engineer, explains how his team developed Kinetis and how the result of their "chasing nanowatts" concept resulted in a highly scalable, ultra low power MCU. 32-bit Kinetis MCUs represent the most scalable portfolio of ARM® Cortex™-M4 MCUs in the industry. The first phase of the portfolio consists of five MCU families with over 200 pin-, peripheral- and software compatible devices with outstanding performance, memory and feature scalability. Enabled by innovative 90nM Thin Film Storage (TFS) flash technologu with unique FlexMemory (configurable embedded EEPROM), Kinetis features the latest low-power innovations and high performance, high precision mixed-signal capability. Kinetis MCUs are supported by a market-leading enablement bundle from Freescale and ARM 3rd party ecosystem partners. http://www.freescale.com/kinetis
View full article
20141030    Release the Alpha version by [email protected]         a) Support FRDM-KL25Z and TWR-K60D100M.         b) Support X-modem 256 and 1K, and test by Teraterm, http://ttssh2.sourceforge.jp/
View full article
Hi All: when someone program FSL MCU  by theirself program tool, and the flash size is over 64KByte , please reference the document. the document is chinese version Br Felix
View full article
Latest published errata for ISF 2.1
View full article
Printer extruders and recyclers use Motors that benefit from torque control that can be obtained by using Kinetis V, a BLDC motor  and the Freescale Motor control algorithms. A plastic waste extruder for RepRap 3D printer filament.  Image: RepRapWiki See this link for more details: How recycled plastic for 3D printing will drive sustainability and improve social consciousness - TechRepublic "Durable, shiny, new plastic -- it's what makes most 3D printers run. And as 3D printing grows in popularity and we begin to scale projects in every industry, the world is going to use a lot more of it. If the industry goal is to have 3D printers in most homes and businesses with lots of other 3D printers running constantly in manufacturing centers, we'll naturally add even more to the 33.6 million tons of plastic Americans toss each year, only 6.5% of which is recycled. It's estimated that 100 million tons of plastic is floating in the world's oceans. Each piece can take anywhere from 500 to 1,000 years to decompose."
View full article
  (para español continua mas abajo) Blind deaf-mute comunication system   Materials Used : A Freedom- KL25Z card A USB Cable A 16x2 LCD Display Three buttons A breadboard A USB cable   Project description Thinking about the difficulties a blind, deaf-mute person has to convey a message, we designed a device to facilitate their communication. Using the Morse key system, the disabled person can write a short message on a LCD screen. For this, you need to press three buttons, and depending on the duration, a function will be performed. 1. If you short-press the button on the left, this will erase the last character typed, however, if you long-press, this will erase everything written. 2. If the middle button with the green label is short-pressed, this will print a dot at the bottom of the screen. If you long press the button, it will print a dash. In Morse code, the dot represents a single signal and the dash represents a triple signal. 3. If the button on the right, with the yellow label is short pressed, the LCD display space will be added to the message. But if he was held down with a longer duration, the set of ¨ Short ¨ and ¨ Long ¨ will be transformed in to a letter in the alphabet and it will be printed on the screen. Note: * If the set of Short and Long does not match any sequence in the matrix, no character is added to the message. **The system to display and write the message on the LCD display are separate.     Modifications for the second stage of the prototype 1. Delete button on the right, the yellow label, Send and Space. a. It is intended that the third button is eliminated by increasing the code efficiency. Instead of sending the sequence of short and long pressing a button, they are sent after a desired time interval. b. Wanted to enter the space with a sequence of short and long. 2. Currently the project is divided into two boxes, one that displays the buttons and other writing. The goal is to have a single box which can write and display the message. 3. With a potentiometer seek to change the time it takes to push a button to be recognized among one short and one long signal.   Modifications for the third stage of the prototype 1. Perform the division again in two boxes , interconnected by Bluetooth modules , as the system is designed to generate a communication between two people, using a system of sending data to harvest deaf -mute person in the future by Braille .       Sistema de Comunicación para Persona Ciega, Sorda y Muda   Materiales Utilizados: Una tarjeta Freedom-KL25Z Un Cable Una Pantalla LCD 16x2 Tres botones Una placa de pruebas (protoboard) Un cable USB   Descripción de Proyecto             Pensando en las dificultades que una persona ciega, sorda y muda tiene para transmitir un mensaje, se ha diseñado un aparato para facilitar su comunicación. Utilizando el sistema de clave morse, la persona con discapacidad puede escribir un mensaje corto en una pantalla LCD. Para esto, se deben presionar tres botones que dependiendo la duración del toque, será la función que efectuará. 1. Si al botón de la izquierda, con la etiqueta azul, apenas se le presiona este borrará el ultimo carácter escrito; sin embargo, si se le presiona con una mayor duración este borrará todo lo escrito. 2. Si al botón del medio, con la etiqueta verde, apenas se le presiona este imprimirá en la parte inferior de la pantalla un punto. El punto representa, un corto en el sistema de clave morse. Sin embargo, si se le mantiene presionado por un momento mas largo, este imprimirá un guión. El guión representa un comando largo en el sistema de clave morse. 3. Si al botón de la derecha, con la etiqueta amarilla, apenas se le presiona, en la pantalla LCD se agregará un espacio al mensaje. Sin embargo si se le mantiene presionado con una mayor duración, se enviará el conjunto de ¨Cortos¨ y ¨Largos¨ a una matriz para que la secuencia se busque y cuando esta se haya, en la LCD se agrega la letra deseada al mensaje. Nota: *Si el conjunto de Cortos y Largos no coincide con ninguna secuencia en la matriz, ningún carácter se agregará al mensaje. ** El sistema para mostrar el mensaje con la LCD esta separado a los botones para escribirlo.     Modificaciones para la segunda etapa del prototipo 1.      Eliminar el botón de la derecha, con etiqueta amarilla,  de Enviar y Espacio. a.       Se pretende que el tercer botón sea eliminado mediante el aumento en la eficiencia del código. En vez de enviar la secuencia de Cortos y Largos al presionar un botón, estos se enviarían después de un intervalo de tiempo deseado. b.      Se busca que el espacio se introduzca con una secuencia de cortos y largos. 2.      Actualmente el proyecto está dividido en dos cajas, una que muestra el mensaje y otra con los botones para escribir. El objetivo es tener una sola caja con el que se pueda escribir y mostrar el mensaje. 3.      Con un potenciómetro se busca cambiar el tiempo que se necesita apretar un botón para que se reconozca entre un toque corto y uno largo.   Modificaciones para la tercera etapa del prototipo 1.      Realizar de nuevo la división en dos cajas, comunicadas entre sí por módulos bluetooth, ya que el sistema está pensado para poder generar una comunicación entre ambas personas, utilizando en un futuro, un sistema de envío de datos a la persona siega sordo-muda mediante el sistema braille.
View full article
当芯片被加密后,在Keil或IAR中下载或者调试时,会弹出以下提示信息: 这时如果点击Yes,那么将会对Flash进行一次mass erase,这样就可以重新下载或者调试程序了。 如果把Do not show this message again复选框勾选上的话,那么以后将不再弹出此提示框,并且会自动进行一次mass erase。 实际使用中,不建议勾选Do not show this message again这一复选框,因为勾上之后就无法直观的看到芯片被锁的提示了。 如果不小心把这一复选框勾上了的话,想要恢复到原来的设置,只能通过修改注册表的方法来实现,具体步骤如下 1) 在CMD窗口下,输入regedit,打开注册表    2)设置 HKEY_CURRENT_USER => Software => SEGGER => J-Link => DontShowAgainUnlockKinetis 为0   
View full article
Kinetis M0+ FAQ文档的版本更新历史: Version 1: Basic structure; Version 2: Add 2 items Top highlights, 7 items Common and 7 items Tools; Version 3: add "Cyclone Max 使用步骤及注意事项"; Version 4,5,6: Adjust the FAQ structure; Version 7: Add "Kinetis L 、E、V、M系列选型指南"; Version 8: Add "开源工具"; Version 9: Add "Kinetis SDK"; Version 10,11,12: Add "智能插座"; Version 13: Add “FAQ使用规范” and "Kinetis Bootloader", and Readjust the "参考设计与方案"; Version 14, 15: Add the new motor control solution link into the "参考设计与方案"; Version 16: Add Blogs to "常用网站资料"; Version 17: Push the Kinetis M0+ FAQ Version log histors' information into subpage of "Kinetis M0+ FAQ 版本更新历史"; Version 18: Add "飞思卡尔MAPS开发板资料" into "常用网站资料"; Version 19: Replace "iBeacon" with "BLE"; Version 20, 21: Remove "WIFI" solution, Add "SPI接口读写SD卡"; Version 22: Rename "软件和例程" with "软件和文档", Add "常用的应用笔记" into "软件和文档" list; Click here to return to Kinetis M0+ FAQ main page...​
View full article
Archive file of the Kinetis-M bare-metal drivers and software examples REV 4.1.5 - this version is not yet available @ nxp.com. Release notes 4.1.5 (Apr.22,2016): Added configuration structures for watchdog timer operating in debug mode. Included IAR EWARM 7.60.1 project templates. Modified LLWU Pin Falling Edge Wakeup example. Please refer to How to download and install KM Bare-metal divers
View full article
Project USB: Connecting USB to CAN with K20   In this project, the internal CAN Controller of the K20 is used to monitor the CAN bus. The connection to the PC is realized by the internal USB Controller. The USB stack is implemented as HID device especially for the K20.   The software runs on a self made hardware board. The connection to CAN is visualized with a Qt program, running on every Win7 PC.   Result: K20_CAN2USB.zip Original Attachment has been moved to: K20_CAN2USB.zip
View full article
Agenda Mastering Kinetis-M Microcontrollers Schedule Module Description Duration Presenter 8:00 Registration 0:30 8:30 Introduction & Welcome 0:15 MM 8:45 MKM34Z256 core and peripherals architecture 1:00 Cano 9:45 DSP fractional, Filter, and FFT-based libraries for general signal processing and metering applications 1:00 LV 10:45 Break 0:15 11:00 Power meter & PLC reference design overview (1ph, 2ph (MKM34Z128), 3ph, 3ph shunt based + sensor node) 1:00 RK 12:00 Introduction to TWR-MKM34Z75, bare-metal drivers, SDK 2.0, FreeRTOS and FreeMaster 1:00 Cano+ID 13:00 Launch in the office 1:00 14:00 Workshop - TWR LCD example (preprogrammed, debugging, SW re-flashing) 0:45 Cano 14:45 Workshop - Using serial bootloader example (learn the way of bootloder integration into application) 0:45 PK 15:30 Workshop - LPTMR and GPIO example (LPTIM & GPIO API, programming interrupt, debugging) 0:45 MM 16:15 Break 0:15 16:30 Workshop - FreeRTOS preemptive multitasking example (basics of FreeRTOS programming) 0:30 MM 17:00 Workshop - High-precision waveform measurement example (SD ADC & FreeMaster programming) 0:45 MM 17:45 Workshop - 64-bit math coprocessor example (mastering DSP instruction set the MMAU) 0:45 MM 18:30 Q&A 0:30 19:00 Dinner @ Brasserie restaurant 2:00 21:00
View full article