Blind deaf-mute comunication system

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Blind deaf-mute comunication system

Blind deaf-mute comunication system

 

(para español continua mas abajo)

Blind deaf-mute comunication system

 

Materials Used :

A Freedom- KL25Z card

A USB Cable

A 16x2 LCD Display

Three buttons

A breadboard

A USB cable

 

Project description

Thinking about the difficulties a blind, deaf-mute person has to convey a message, we designed a device to facilitate their communication. Using the Morse key system, the disabled person can write a short message on a LCD screen. For this, you need to press three buttons, and depending on the duration, a function will be performed.

  1. 1. If you short-press the button on the left, this will erase the last character typed, however, if you long-press, this will erase everything written.
  2. 2. If the middle button with the green label is short-pressed, this will print a dot at the bottom of the screen. If you long press the button, it will print a dash. In Morse code, the dot represents a single signal and the dash represents a triple signal.
  3. 3. If the button on the right, with the yellow label is short pressed, the LCD display space will be added to the message. But if he was held down with a longer duration, the set of ¨ Short ¨ and ¨ Long ¨ will be transformed in to a letter in the alphabet and it will be printed on the screen.

Note:

* If the set of Short and Long does not match any sequence in the matrix, no character is added to the message.

**The system to display and write the message on the LCD display are separate.

 

 

Modifications for the second stage of the prototype

  1. 1. Delete button on the right, the yellow label, Send and Space.
  2. a. It is intended that the third button is eliminated by increasing the code efficiency. Instead of sending the sequence of short and long pressing a button, they are sent after a desired time interval.
  3. b. Wanted to enter the space with a sequence of short and long.
  4. 2. Currently the project is divided into two boxes, one that displays the buttons and other writing. The goal is to have a single box which can write and display the message.
  5. 3. With a potentiometer seek to change the time it takes to push a button to be recognized among one short and one long signal.

 

Modifications for the third stage of the prototype

  1. 1. Perform the division again in two boxes , interconnected by Bluetooth modules , as the system is designed to generate a communication between two people, using a system of sending data to harvest deaf -mute person in the future by Braille .

 

 

 

Sistema de Comunicación para Persona Ciega, Sorda y Muda

 

Materiales Utilizados:

Una tarjeta Freedom-KL25Z

Un Cable

Una Pantalla LCD 16x2

Tres botones

Una placa de pruebas (protoboard)

Un cable USB

 

Descripción de Proyecto

            Pensando en las dificultades que una persona ciega, sorda y muda tiene para transmitir un mensaje, se ha diseñado un aparato para facilitar su comunicación. Utilizando el sistema de clave morse, la persona con discapacidad puede escribir un mensaje corto en una pantalla LCD. Para esto, se deben presionar tres botones que dependiendo la duración del toque, será la función que efectuará.

  1. 1. Si al botón de la izquierda, con la etiqueta azul, apenas se le presiona este borrará el ultimo carácter escrito; sin embargo, si se le presiona con una mayor duración este borrará todo lo escrito.
  2. 2. Si al botón del medio, con la etiqueta verde, apenas se le presiona este imprimirá en la parte inferior de la pantalla un punto. El punto representa, un corto en el sistema de clave morse. Sin embargo, si se le mantiene presionado por un momento mas largo, este imprimirá un guión. El guión representa un comando largo en el sistema de clave morse.
  3. 3. Si al botón de la derecha, con la etiqueta amarilla, apenas se le presiona, en la pantalla LCD se agregará un espacio al mensaje. Sin embargo si se le mantiene presionado con una mayor duración, se enviará el conjunto de ¨Cortos¨ y ¨Largos¨ a una matriz para que la secuencia se busque y cuando esta se haya, en la LCD se agrega la letra deseada al mensaje.

Nota:

*Si el conjunto de Cortos y Largos no coincide con ninguna secuencia en la matriz, ningún carácter se agregará al mensaje.

** El sistema para mostrar el mensaje con la LCD esta separado a los botones para escribirlo.

 

 

Modificaciones para la segunda etapa del prototipo

  1. 1.      Eliminar el botón de la derecha, con etiqueta amarilla,  de Enviar y Espacio.
    1. a.       Se pretende que el tercer botón sea eliminado mediante el aumento en la eficiencia del código. En vez de enviar la secuencia de Cortos y Largos al presionar un botón, estos se enviarían después de un intervalo de tiempo deseado.
    2. b.      Se busca que el espacio se introduzca con una secuencia de cortos y largos.
  2. 2.      Actualmente el proyecto está dividido en dos cajas, una que muestra el mensaje y otra con los botones para escribir. El objetivo es tener una sola caja con el que se pueda escribir y mostrar el mensaje.
  3. 3.      Con un potenciómetro se busca cambiar el tiempo que se necesita apretar un botón para que se reconozca entre un toque corto y uno largo.

 

Modificaciones para la tercera etapa del prototipo

  1. 1.      Realizar de nuevo la división en dos cajas, comunicadas entre sí por módulos bluetooth, ya que el sistema está pensado para poder generar una comunicación entre ambas personas, utilizando en un futuro, un sistema de envío de datos a la persona siega sordo-muda mediante el sistema braille.
添付
評価なし
バージョン履歴
最終更新日:
‎11-15-2013 10:44 PM
更新者: