Kinetis M0+ FAQ版本更新历史

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Kinetis M0+ FAQ版本更新历史

Kinetis M0+ FAQ版本更新历史

Kinetis M0+ FAQ文档的版本更新历史:

Version 1: Basic structure;

Version 2: Add 2 items Top highlights, 7 items Common and 7 items Tools;

Version 3: add "Cyclone Max 使用步骤及注意事项";

Version 4,5,6: Adjust the FAQ structure;

Version 7: Add "Kinetis L 、E、V、M系列选型指南";

Version 8: Add "开源工具";

Version 9: Add "Kinetis SDK";

Version 10,11,12: Add "智能插座";

Version 13: Add “FAQ使用规范” and "Kinetis Bootloader", and Readjust the "参考设计与方案";

Version 14, 15: Add the new motor control solution link into the "参考设计与方案";

Version 16: Add Blogs to "常用网站资料";

Version 17: Push the Kinetis M0+ FAQ Version log histors' information into subpage of "Kinetis M0+ FAQ 版本更新历史";

Version 18: Add "飞思卡尔MAPS开发板资料" into "常用网站资料";

Version 19: Replace "iBeacon" with "BLE";

Version 20, 21: Remove "WIFI" solution, Add "SPI接口读写SD卡";

Version 22: Rename "软件和例程" with "软件和文档", Add "常用的应用笔记" into "软件和文档" list;

Click here to return to Kinetis M0+ FAQ main page...

无评分
版本历史
最后更新:
‎11-02-2015 06:13 AM
更新人: