Kinetis Microcontrollers Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis Microcontrollers Knowledge Base

Discussions

Sort by:
The installation file containing MKM34Z256 training examples programmed using Kinetis-M bare metal drivers and compiled using IAR EWARM 7.40.1. These examples explain programming steps for GPIO, Low Power Timer, Sigma Delta ADC, Memory Math Arithmetic Unit, and LCD on-chip peripherals. In addition, you will learn how to create simple FreeRTOS and 1-phase power meter applications. All examples including their handouts will be installed on your PC in c:\Freescale\KM34Z75_EXAMPLES subfolder. For more information about each example, please refer to its handout.
View full article
As general introduction on thread https://community.freescale.com/docs/DOC-328302 , I did a smart LED application with GoKit and FRDM-KL02. In this design, FRDM-KL02 will communicate with GoKit by WIFI, and control LED flash. Code Structure Code Basic Introduction In this project structure, you need to do following items on code. ü Add your functions, such as UART, LED, motor driver code. ü Add function running functions in protocol.c ü Add functions order in main loop. You can find my main.c and protocol.c as attachment. In this document, I would like to detail introduce function MessageHandle(), void MessageHandle(void) {                 pro_headPart    tmp_headPart; //Common command package                 memset(&tmp_headPart, 0, sizeof(pro_headPart));                 if(get_one_package)                 {                                                                              get_one_package = 0;                                 memcpy(&tmp_headPart, uart_buf, sizeof(pro_headPart));                                                                 //CRC error, send back error command                                 if(CheckSum(uart_buf, uart_Count) != uart_buf[uart_Count-1])                                 {                                                 SendErrorCmd(ERROR_CHECKSUM, tmp_headPart.sn);                                                 return ;                                 }                                 So, you can see that only get_one_package=1, we can receive frame completely.                                 switch(tmp_headPart.cmd)                                 {                                                              case       CMD_GET_MCU_INFO:                                                                 CmdGetMcuInfo(tmp_headPart.sn);                                                                                                                                     break;                                                                   case CMD_SEND_HEARTBEAT:                                                                 SendCommonCmd(CMD_SEND_HEARTBEAT_ACK, tmp_headPart.sn);                                                                                 break;                                                 case CMD_REBOOT_MCU:                                                                 SendCommonCmd(CMD_REBOOT_MCU_ACK, tmp_headPart.sn);                                                 case       CMD_SEND_MCU_P0:                                                                 CmdSendMcuP0(uart_buf);                                                                 break;                                                 case       CMD_REPORT_MODULE_STATUS:                                                                 CmdReportModuleStatus(uart_buf);                                                                 break;                                                 default:                                                                 SendErrorCmd(ERROR_CMD, tmp_headPart.sn);                                                                 break;                                 }                              } } After that, you can do operations mentioned in thread https://community.freescale.com/docs/DOC-328302. You can see smart LED device and been found.
View full article
Hello Freedom users I have created another full board review this time for the FRDM-KL05Z always including clear instructions to program and debug your first project. I'm still working on the video version (looking for a better accent :smileyconfused:), but the commands illustrated by screen captures should be easy to follow. Freescale Freedom development platform: [FRDM-K... | element14 Enjoy Greg
View full article
Installation file containing training examples - unpack and run this file to install code examples.
View full article
Este teclado interactivo, esta hecho para ayudar a discapacitados en su desarrollo motriz. El teclado contara con cuatro botones, los cuales tienen un led en la parte superior y un sensor piezoelectrico. El LED superior se enciende, avisando al paciente que debe presionar el boton. El boton al ser presionado, activa al sensor, el cual manda una señal a la tarjeta freedom y prende un LED verde si activo el boton indicado o rojo si se equivoco. Finalmente el resultado de los botones activa un servomotor.   Ficha técnica del proyecto, indicando una descripción breve de su funcionamiento y especificaciones técnicas. Requerimientos técnicos para la exhibición del demo, como conexiones para lap top o conexión de internet.   Ficha tecnica Teclado interactivo para discapacitados Descripcion Este teclado se controla con la computadora. Tiene 4 botones y cada uno tiene un LED en la parte superior. El terapeuta elije que LED prender y el paciente debe presionar el botón correspondiente. Si presiona el botón debido, se prendera un LED verde y girara un servomotor, si se presiona cualquiera de los otros botones, se encenderá un LED rojo y el servomotor no reaccionara. Especificaciones de construcción Construcción: madera, MDF. Microcontrolador: Tarjeta Freedom Servomotor (x1) Capacitores cerámicos: microfaradios (x4) Sensores Piezoelectricos (x4) Leds (x6) Resistencias: 10K (x10) Requerimientos tecnicos Conexión USB a una computadora con programa Realterm para la comunicación serial.           Video final Tapete interactivo video final - YouTube Original Attachment has been moved to: codigo-teclado.txt.zip
View full article
With the HMI developing, touch sensing is more and more popular. The GPIO-based method was developed as a low-cost way to do touch sensing. NXP had developed this sensing method and provide as TSS library (which combines support for GPIO and hardware-based touch sensing).The GPIO method uses the RC charge time in a capacitor (the electrode or touch pad)   Measurement Principles: TSI Method TSI method uses configurable current sources. The current sources are active outputs, making them far more robust against noise. Current sources are configurable, making it possible to configure sampling time. The signal slope depends on the applied current and the capacitance. When a finger approaches the electrode, frequency decreases. Another oscillator, uses a internal unchanging capacitor, this is our reference, we will configure it to oscillate faster than the external one. By comparing how many reference oscillations where counted by the TSI module per external reference scan, we can know when a touch happened.
View full article
¡ FELICIDADES AL GANADOR! El sábado 7 de diciembre se realizó la final del Kinetis L MCU Challenge México en las instalaciones del Centro de Congresos, Tecnológico de Monterrey Campus Guadalajara; donde se eligió al ganador a través de las redes sociales y la herramienta RankTab. La emoción se sintió entre los participantes durante la votación; al finalizar el conteo de votos y calificaciones en Ranktab ¡obtuvimos un ganador! Nos complace presentar a: Andrés Gafford con el proyecto Tablet Braille para Invidentes como el ganador del Kinetis L MCU Challenge México 2013. Quién se irá de viaje con todos los gastos pagados al Freescale Technology Forum (FTF) en Dallas, Texas del 8 al 11 de abril del 2014. Agradecemos a los finalistas por su esfuerzo y participación en el evento;  también agradecemos a todas las personas que nos ayudaron con su calificación y voto a elegir el mejor de los proyectos. Esperamos que esta competencia haya sido un semillero de grandes ideas que se conviertan en las innovaciones del mañana.
View full article
Este proyecto está siendo desarrollado por alumnos del Tecnológico de Monterrey Campus Guadalajara, el cual está orientado para servir como un tipo de terapia para personas discapacitadas. El proyecto en sí consiste en el control de un vehículo de juguete por medio de pulsaciones que serán realizadas con pelotas anti-estrés, de esta forma la persona podrá realizar un ejercicio de fortalecimiento en sus extremidades superiores de una forma más entretenida y menos tediosa que las clásicas terapias. Es importante mencionar que para poder realizar este proyecto es necesario el uso de dos tarjetas Freedom KL25Z de Freescale®, dos módulos Bluetooth®, dos servomotores de rotación continua y dos sensores de presión, los cuales serán incorporados dentro de las pelotas anti-estrés. El vehículo de juguete estará compuesto por los servomotores, que servirán como llantas; un módulo Bluetooth®, el cual recibirá las señales del otro módulo; y una de las tarjetas Freedom KL25Z. Por otro lado una de las tarjetas Freedom KL25Z estará conectada con los sensores integrados en las pelotas anti-estrés y a un módulo cuya función es mandar la información capturada por los sensores al vehículo de juguete. La mecánica del proyecto depende de la pelota que sea presionada, pues si se presiona solamente una pelota, el vehículo avanzará, por otro lado si se presiona la otra pelota, el vehículo girará sobre su propio eje. Este proyecto tiene como fin la implementación de conocimiento prácticos y teóricos en busca de una aportación en beneficio de la sociedad. También es relevante comentar que las visiones a futuro de este proyecto es que pueda ser implementado como una especie de control para una silla de ruedas, con el fin de facilitar la movilidad y aumentar la comodidad al momento de usar este tipo de vehículo. Original Attachment has been moved to: Codigo-tarjetas-freedom.zip
View full article
Man powers his home from local stream with DIY micro-hydro plant - StumbleUpon The above project is amazing. Imagine a Kinetis V as the inverter for a micro-turbine based on a PMSM or BLDC ??
View full article
This project is for neck's physical therapy and for a wheel chair that will move just with two buttons. This project is intended to be for persons who cannot move arms to do stuff.Instead of having a little joystick to move, they will just have to press one button turn around on the wheel chair or press the other button to make it advance. Because of the time we have to present this project, we will for now apply this idea to a toy car that will help children to do physical therapy on the neck.   Silla de Ruedas controlada por movimientos del cuello - YouTube   Facebook Original Attachment has been moved to: Code.zip
View full article
The modularity of the tower system makes it great for prototyping, but for higher speed interfaces, there might be timing/signal integrity issues from having the TWR-MEM. For example, if you run the NFC demo from MQX 4.2: C:\Freescale\Freescale_MQX_4_2\mqx\examples\nandflash\build\iar\nandflash_twrk60f120m, It works well standalone, but with TWR-MEM connected. It failed when trying to read the data from nandflash. Because the NAND flash is on the TWR-K60F120M board, any time you access the NAND flash through NFC the signal will still travel all the way to the MRAM and reflect back which can distort the signals. Checking with the NFC driver code, you may find the high driven strength of NFC IOs has already been enabled. Decreasing the NFC module clock by setting SIM_CLKDIV4_NFCDIV to 31,  the demo still failed. How to fix it? Here we provide a trick/solution for this issue: Enable the internal pull-ups on NFC interface. then you may set a slower NFC clock by setting SIM_CLKDIV4_NFCDIV to 12, this value can be larger to make the communication more stable, but please note if you try to design a custom board, there is no reason it shouldn’t work at max frequency with a better layout. Hope that helps, -Kan
View full article
Update of FreeMASTER component for PE
View full article
There is a popular WIFI platform called “GoKit” in China. This testing kit can be use to do some customized application. Not only WIFI communication, kit also support other functions. You can find interfaces listed as below. GoKit Interfaces: I try to use FRDM-KL02 to communicate with this kit to do a WIFI communication application. Board connection as below. This platform has two running mode. One is AirLink mode, and another is normal running mode. AirLink mode is used to WIFI communication or pair. Go to AirLink mode steps: Power on FRDM-KL02 Long press key1 to reset WIFI module. Wait until RED led on. Short press Key2 to go into configuration mode, wait until RED led flash on WIFI module. Open demo APP, select “adding device”, input SSID password. Waiting for configuration finish. Command Format HOF: 2bytes, value 0xFFFF Length: 2bytes Cmd:1byte SN:1byte Flags:2bytes DATA: Xbytes Checksum:1byte WIFI acquire device information MCU inform WIFI into configure mode MCU reset WIFI WIFI inform MCU status WIFI ask for reset Illegal command For detail code, I will post another thread for your reference.
View full article
The following (after the "- - - - - -" is debugged code for flashing Green, Red, and Blue LEDs on the FRDM-K22F module. - - - - - - - - - - - - - - - - - - - - - - - - - - - - - - - - - - - - - - - #include "fsl_device_registers.h" #include "board.h" static int i = 0; int main(void) {   // LEDs are common-anode, with cathodes connected to port pins.   // Therefore, logic high (1) turns them off, and logic low   // (0) turns them on.   short OFF = 1;   short ON = 0;         hardware_init();           GPIO_DRV_SetPinDir(kGpioLED1, kGpioDigitalOutput); //Green LED      GPIO_DRV_SetPinDir(kGpioLED2, kGpioDigitalOutput); //Red LED      GPIO_DRV_SetPinDir(kGpioLED3, kGpioDigitalOutput); //Blue LED      GPIO_DRV_WritePinOutput(kGpioLED1, OFF); //Green LED initially off      GPIO_DRV_WritePinOutput(kGpioLED2, OFF); //Red LED initially off      GPIO_DRV_WritePinOutput(kGpioLED3, OFF); //Blue LED initially off      while (1)           {           for (i = 0; i<0xFFFFFF; i++)           {           }           GPIO_DRV_WritePinOutput(kGpioLED1, ON); //Green LED on           for (i = 0; i<0xFFFFFF; i++)           {           }           GPIO_DRV_WritePinOutput(kGpioLED1, OFF); //Green LED off           for (i = 0; i<0xFFFFFF; i++)           {           }           GPIO_DRV_WritePinOutput(kGpioLED2, ON); //Red LED on           for (i = 0; i<0xFFFFFF; i++)           {           }           GPIO_DRV_WritePinOutput(kGpioLED2, OFF); //Red LED off           for (i = 0; i<0xFFFFFF; i++)           {           };           GPIO_DRV_WritePinOutput(kGpioLED3, ON); //Blue LED on           for (i = 0; i<0xFFFFFF; i++)           {           }           GPIO_DRV_WritePinOutput(kGpioLED3, OFF); //Blue LED off           }      return 0; }
View full article
¡EL GRAN DÍA HA LLEGADO, PARTICIPA Y ELIGE AL MEJOR! Te esperamos en el Centro de Congresos del Tecnológico de Monterrey Campus Guadalajara, la exhibición de los proyectos estará disponible a partir de las 09:00 hrs. Se nombrará al ganador a las 13:00 hrs. En seguida de la premiación de The Freescale Cup. La votación se abrirá a las 9:00hrs. Y se cerrará a las 12:30hrs, se tomarán en cuenta solo las interacciones realizadas dentro de este horario. Vota y califica tu proyecto favorito, sigue 2 pasos: 1. VOTA Elige solo UNA de estas 2 opciones. Ingresa a tu cuenta Twitter Publica el hashtag del proyecto #KinetisChallenge Ingresa al Facebook de Freescale University Programs Encuentra la liga y contesta la encuesta, o si lo prefieres puedes hacerlo desde el siguiente acceso.: https://es.surveymonkey.com/s/JQY76J9 2. CALIFICA Califica cada uno de los proyectos de acuerdo a los criterios de selección. Ingresa a https://apps.facebook.com/ranktab/rt.php?l=1452 Califica cada proyecto con los 3 criterios. Observa la matriz de burbujas para ver la opinión de los participantes. Comparte tu calificación en tu muro. Se tomarán en cuenta la sumatoria de votos en Twitter y Survey Monkey; así como la calificación en RankTab. ¡LA ELECCIÓN ESTÁ EN TUS MANOS!
View full article
When I developed the software of FSL Air Mouse based on kinetis KL16 , I need read and write more than 1 byte data from or to sensor by i2c. But I don't find any i2c driver which supports mutli-bytes accessing. So I write the i2c driver which supports mutli-bytes accessing. It can run on MCU KL1x series and you can modify it a little for Kinetis K series.
View full article
近期有客户提出需求,要求通过外部Flash编程工具烧写Flash Program Flash IFR区域。 目前P&E Cyclone MAX和Segger J-Flash均无法实现对IFR区域编程。 客户可以使用软件的方式来编程IFR提供的单次烧写区域,存储客户产品信息,例如MAC地址等。 Program Flash单次烧写区域提供了64个字节,只允许烧写一次,通过Program Once和Read Once命令来读写这个区域。 下图为单次烧写区域在Prgoram Flash IFR的具体位置, IFR独立于FTFL Flash空间,可以理解成另外一个Flash模块。 Program Once和Read Once命令每次调用可以读取Program Flash单次烧写区域的4个字节,通过命令参数的数据索引号可以通过多次操作遍历整个64个字节。 附件中的例程使用Program Once命令编写MAC地址到单次烧写区域,之后通过Read Once命令读取MAC地址信息。 例程环境: IAR Workbench + TWR-K60D100M
View full article
Hi everybody, The original document was moved to KSDK subspace. You can find it in the next link: https://community.freescale.com/docs/DOC-102612 Regards, Carlos
View full article
update of the FreeMASTER component
View full article