Kinetis微控制器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Kinetis Microcontrollers Knowledge Base

讨论

排序依据:
What's eCos eCos is a free open source real-time operating system intended for embedded applications. The highly configurable nature of eCos allows the operating system to be customised to precise application requirements, delivering the best possible run-time performance and an optimised hardware resource footprint. With provided configuration tools (configtool and ecosconfig) it is possible to build configurations that scale from minimal that require less than 32KiB memory to reach full featured operating system with networking, file system, serial communication, etc. eCos for Kinetis Currently the Kinetis eCos support includes: UART; Ethernet - with TCP/IP through either lwIP or BSD stack; Flash - program and erase; eDMA library; DSPI - including MMC/SD card support; Real Time Clock. Cache; DDRAM; FlexBus; Following features are available for testing: I2C; CAN; Watchdog. Configuring eCos for Kinetis Start the graphical configuration tool configtool, then from menu select Build->Templates. In Hardware selection box select your board: In our case we select TWR-K70F120M. Save the configuration and select Build->Library. configtool will build a customised eCos library and extract headers for you. Now you are ready for your "Hello world". Further reading You shall find complete eCos documentation at eCos Documentation
查看全文
Project Summary MonkeyListen uses the FRDM-K20D50 board (which has a Cortex M4 core with DSP instructions) with the FRDM-OLED shield so you can  make your very own spectrum analyzer display  The end result will be a functional DSP system that will analyze incoming audio content via an electret microphone on FRDM-OLED board and display the spectral content.   The example code will also show you how to plot time domain data (a simple audio scope!),  Frequency domain data (via an FFT) and a time-frequency plot (spectrogram).  Extra I/O are provided to hack the code and create your own DMM or oscilloscope. The FRDM-OLED shield also has an optional RS-485 interface for doing cool things like driving a DMX lighting system! Skills Developed: Spectral Analysis via FFT OLED display interfacing Electret microphone Interfacing Soldering SOIC8 and 1206 surface mount devices Cortex CMSIS DSP Library Materials: FRDM-K20D50 FRDM-OLED Development Tools Install Codewarrior 10.5 for Microcontrollers (Eclipse) Special Edition to your  machine Example Code Get the latest copy from Github Prerequisite Videos: All of the videos are organized on a Youtube playlist: H.I.T. #2: MonkeyListen - YouTube MonkeyListen WatchMe1st MonkeyListen Demo: Time Domain + FFT Mode MonkeyListen Demo: Spectrogram Mode Spectral Analysis for Embedded Systems Part 1 & Part 2 Getting Started with the ARM CMSIS DSP FFT library Introduction to Fixed Point Math for Embedded Systems Part 1, 2 and 3 The q31_t (Q.31) number format for the CMSIS DSP libraries FRDM-OLED Overview EEVblog #611 - Electret Microphone Design Loading and Configuring the MonkeyListen Example Software Step 1:  Get a FRDM-OLED      You can order raw PCBs yourself from OSHPark or your favorite PCB vendor.      The bill of materials for the FRDM-OLED is included with the build package on the FRDM-OLED page.     Please let us know if you are interested in a pre-assembled version.   If there is enough demand we will get some built via a Kickstarter campaign   Don't be afraid to build it yourself,  Soldering is fun!  There is plenty of good stuff on the web on how to do SMT soldering.   All of the parts on the board are fairly simply once you get the hang of it and everything can be hand soldered  The key is having some decent tools. Step 2: Put it Together Attach  The FRDM-OLED to the FRDM-K20D50.   The FRDM-K20D50 comes with female headers that you can solder on so the boards can be easily separated. Step 3: Download Download the example software.   The video "Loading and Configuring the MonkeyListen Example Software" will step you though downloading the program and doing some basic configuration. Step 4: Say Something Speak, Sing and Yell.... Step 5: Hack! Do something else cool.....  Make a DMM,  or an o-scope....
查看全文
The documentation points out that the Figure 32-1. Multipurpose Clock Generator (MCG) block diagram in KV5xP144M240RM.pdf is incorrect, the  /2 divider is NOT included in the feedback loop. It gives the formula to compute the VCO and MCGPLLCLK clock frequency and corresponding code.
查看全文
近期有客户提出需求,要求通过外部Flash编程工具烧写Flash Program Flash IFR区域。 目前P&E Cyclone MAX和Segger J-Flash均无法实现对IFR区域编程。 客户可以使用软件的方式来编程IFR提供的单次烧写区域,存储客户产品信息,例如MAC地址等。 Program Flash单次烧写区域提供了64个字节,只允许烧写一次,通过Program Once和Read Once命令来读写这个区域。 下图为单次烧写区域在Prgoram Flash IFR的具体位置, IFR独立于FTFL Flash空间,可以理解成另外一个Flash模块。 Program Once和Read Once命令每次调用可以读取Program Flash单次烧写区域的4个字节,通过命令参数的数据索引号可以通过多次操作遍历整个64个字节。 附件中的例程使用Program Once命令编写MAC地址到单次烧写区域,之后通过Read Once命令读取MAC地址信息。 例程环境: IAR Workbench + TWR-K60D100M
查看全文
Hello, The below attachment is the code for UART with the input data as a character..But i need the input data to be a STRING...Can anyone please post the code for UART with input as a string using MK22D5.
查看全文
There with phase shifting when using two different FTM modules to output PWM signals. Although the two FTM modules using the same clock source (bus clock), there still exists the phase shifting status. Please check attached video about phase shifting. FTM Global Time Base(GTB) introduction The global time base (GTB) is a FTM function that allows the synchronization of multiple FTM modules on a chip. The following figure shows an example of the GTB feature used to synchronize two FTM modules. In this case, the FTM A and B channels can behave as if just one FTM module was used, that is, a global time base. K65’s FTM0 provides the only source for the FTM global time base. The other FTM modules can share the time base as shown in the following figure: The code description:    // Configure ftm params with frequency 2MHz for CLK        ftm_pwm_param_t ftmParamCLK = {             .mode                   = kFtmEdgeAlignedPWM,   //PWM mode             .edgeMode               = kFtmLowTrue,           //PWM Low-true pulses (clear Output on match-on)             .uFrequencyHZ           = 200000u,         //2MHz clock frequency             .uDutyCyclePercent      = 50,                //Duty cycle 50%             .uFirstEdgeDelayPercent = 0,                        };    //using FTM0 & FTM3 GTB feature    FTM_HAL_SetClockSource (FTM0, kClock_source_FTM_None);   //disable FTM0 clock source    FTM_HAL_SetClockSource (FTM3, kClock_source_FTM_None);   //disable FTM3 clock source      FTM_HAL_SetGlobalTimeBaseCmd(FTM0, true);   //enable FTM0 GTBEEN    FTM_HAL_SetBdmMode(FTM0, kFtmBdmMode_11);   //enable FTM0 BDMMODE    FTM_HAL_SetGlobalTimeBaseCmd(FTM3, true);   //enable FTM3 GTBEEN    FTM_HAL_SetBdmMode(FTM3, kFtmBdmMode_11);   //enable FTM3 BDMMODE        FTM_HAL_SetClockSource (FTM0, kClock_source_FTM_SystemClk);   //disable FTM0 clock source    FTM_HAL_SetClockSource (FTM3, kClock_source_FTM_SystemClk);   //disable FTM3 clock source      FTM_HAL_SetCounter(FTM0, 0U);        //clear TFM0 counter value to 0    FTM_HAL_SetCounter(FTM3, 0U);        //clear FTM3 counter value to 0      FTM_HAL_SetGlobalTimeBaseOutputCmd(FTM0, true);      //enale FTM0 GTBEOUT Please check attached video about after using GTB feature, the FTM0_CH4 and FTM3_CH1 PWM output signals. How to output two PWM output signals at one FTM module with KSDK? The two PWM output signal will provides the same clock frequency with different duty cycle. The two PWM output signal need use the same PWM mode. Please check below code to enable K65’s FTM0 module output two PWM signals. // Configure ftm params with frequency 2MHz for CLK        ftm_pwm_param_t ftmParamCLK = {             .mode                   = kFtmEdgeAlignedPWM,   //PWM mode             .edgeMode               = kFtmLowTrue,           //PWM Low-true pulses (clear Output on match-on)             .uFrequencyHZ           = 200000u,         //2MHz clock frequency             .uDutyCyclePercent      = 50,                //Duty cycle 50%             .uFirstEdgeDelayPercent = 0,                        }; // Configure ftm params with frequency 2MHz for CLK                ftm_pwm_param_t ftmParamSH =         {              .mode                   = kFtmEdgeAlignedPWM,   //PWM mode              .edgeMode               = kFtmLowTrue,   //PWM Low-true pulses (clear Output on match-on)              .uFrequencyHZ           = 200000u,        //2MHz clock frequency              .uDutyCyclePercent      = 75,     //Duty cycle 75%              .uFirstEdgeDelayPercent = 0,         };     // Initialize FTM module,     // configure for software trigger.     memset(&ftmInfo, 0, sizeof(ftmInfo));     ftmInfo.syncMethod = kFtmUseSoftwareTrig;  //Using software trigger PWM synchronization     FTM_DRV_Init(BOARD_FTM_INSTANCE, &ftmInfo);  //FTM0 initialization     FTM_DRV_SetClock(BOARD_FTM_INSTANCE, kClock_source_FTM_SystemClk, kFtmDividedBy1); //Enable FTM0 counter clock     FTM_DRV_PwmStart(BOARD_FTM_INSTANCE, &ftmParamCLK, BOARD_FTM_CHANNEL); //Enable PWM output at FTM0_CH4     FTM_HAL_SetClockSource(FTM0, kClock_source_FTM_None); //Disable FTM0 counter clock     FTM_DRV_PwmStart(BOARD_FTM_INSTANCE, &ftmParamSH, BOARD_FTM_CHANNEL5);   //Enable PWM output at FTM0_CH5 The tested code also be attached, please using it with KSDK V1.2 software. Wish it helps.
查看全文
     我想“超频”这个词估计大家都不会陌生,很多玩计算机的都会尝试去把自己电脑的CPU超频玩一些高端大型游戏(咳咳,当然玩的high的时候别忘了小心你的主板别烧了),而对我们这些搞嵌入式的人们来说,估计就只能用这样的情怀去折磨MCU了(当然前提得是有PLL或者FLL的MCU)。      在超频之前首先需要澄清几个概念,我们通常所说的主频一般是指内核时钟或者系统时钟(即core_clk或system_clk)。而对K60来说,其内部还有总线时钟(Bus_clk)、外部总线时钟(FlexBus_clk)、flash时钟(Flash_clk),而这几个时钟互相关联且每个都是有其频率限制的(如下图1所示),所以当我们要超频内核时钟的时候还不得不考虑其他时钟承受极限(姑且用这个词吧)。在我们用MCG模块内部的PLL将输入时钟超频到200MHz作为MCGOUTCLK输出的时候还需要一道关卡(如下图2),也就是说虽然这几个时钟属于同宗(都来自MCGOUTCLK),但是也可以通过不同的分频器(OUTDIV[1:4])约束不同的时钟范围,这里想起一个形象的例子。MCGOUTCLK就类似以前的官家大老爷,娶了四房姨太太(OUTDIV[1:4]),分别生了四个少爷(即core_clk、Bus_clk、FlexBus_clk和Flash_clk),每个少爷都是老爷的儿子,不过在家中地位却是由姨太太的排序决定的,其中大房的大少爷(core_clk)地位最高(频率范围最大),四房的小少爷(flash_clk)地位最低(频率范围最小),不过他们的地位最高也不会超过老爷(其他clk<=MCGOUTCLK),呵呵,有点意思~ 图1 图2      经过上面的分析之后,就可以开始着手超频了。经过验证,其实系统频率超不上去就是“小少爷”(flash_clk)拖了后腿,当我们将MCGOUTCLK超到200MHz的时候,OUTDIV1的分频可以设置为1分频,保证内核频率为200MHz,但却要同时保证其他几个时钟不要超过太多,尤其是Flash_clk的限制要严格(建议不要超过30MHz,小少爷有些“娇气”),因为flash_clk过高就代表取指令的频率过高,指令出错就会造成系统程序跑飞。     说到这里,可能有些人会质疑,把主频超的那么高,但取指令的速度上不去有个啥用,岂不是颇有些大马拉小车的感觉吗,其实不然,这里我说两点。一个是通过RAM调试或者将函数声明成RAM执行函数的时候是可以加快执行速度的,另一个就是当做一些数学运算的时候作用就很明显了,因为一般可能会单纯用到CPU内部的ALU和寄存器组,后者数据访问多一些(注意Cortex-M4是哈佛结构,数据与指令总线独立的),自然其运算速度就上去了,所以还是好处多多的。      当然飞思卡尔本身是不建议超频的,数据手册上给出的极限值都是在保证系统可靠性和稳定性的前提下测试出来的,再往上就不敢保证了(跟你的硬件电路设计能力有一定关系),正所谓“超频有风险,用时需谨慎啊”,呵呵,所以我们大多数的应用还是老老实实的按照“规矩”来吧。不过这里需要提的一点是,每家厂商一般会为超频留有余地(为了满足一些客户的超频需要,哎,不容易啊),至于这个余地是多少,不同的半导体厂商也会有不同的标准。对我来说,记得那是2008年的第一场雪,比往年来的稍晚了些…(没收住,开始整词儿了,呵呵),那一年我第一次接触飞思卡尔的9S12 16位的单片机(MC9S12DG128,哎,搞过智能车的都懂的),额定主频是25MHz,我把它超到40MHz,后来又换成了MC9S12XS128,额定主频是40MHz,我又把它超到80MHz(有点超频强迫症了,呵呵),一直到如今的ARM K60,额定主频为100MHz(VLQ100),所以。。。咳咳。。。很自然的我就把它超到200MHz,再往上我就没有测试了,因为基本也用不到那么高的频率,还是要掌握好这个“度”的,想过把超频的瘾的可以试试看,呵呵~
查看全文
介绍通过使用Kinetis KL系列以及K系列通过不同方式驱动液晶。
查看全文
UART Presentation (universal asynchronous receiver/transmitter) by Ali Piña, Freescale TIC. Module Explanation Connection Diagram Hands-On. Polling mode. Interrupt Mode. Presentación de UART  (universal asynchronous receiver/transmitter) by Ali Piña, Freescale TIC. a.       Explicación del modulo. b.      Diagrama de conexión. c.       Hands-On. Modo de Poleo Modo de Interrupción
查看全文
Kinetis M0+ FAQ文档的版本更新历史: Version 1: Basic structure; Version 2: Add 2 items Top highlights, 7 items Common and 7 items Tools; Version 3: add "Cyclone Max 使用步骤及注意事项"; Version 4,5,6: Adjust the FAQ structure; Version 7: Add "Kinetis L 、E、V、M系列选型指南"; Version 8: Add "开源工具"; Version 9: Add "Kinetis SDK"; Version 10,11,12: Add "智能插座"; Version 13: Add “FAQ使用规范” and "Kinetis Bootloader", and Readjust the "参考设计与方案"; Version 14, 15: Add the new motor control solution link into the "参考设计与方案"; Version 16: Add Blogs to "常用网站资料"; Version 17: Push the Kinetis M0+ FAQ Version log histors' information into subpage of "Kinetis M0+ FAQ 版本更新历史"; Version 18: Add "飞思卡尔MAPS开发板资料" into "常用网站资料"; Version 19: Replace "iBeacon" with "BLE"; Version 20, 21: Remove "WIFI" solution, Add "SPI接口读写SD卡"; Version 22: Rename "软件和例程" with "软件和文档", Add "常用的应用笔记" into "软件和文档" list; Click here to return to Kinetis M0+ FAQ main page...​
查看全文
Hi everybody, The original document was moved to KSDK subspace. You can find it in the next link: https://community.freescale.com/docs/DOC-102612 Regards, Carlos
查看全文
There is a popular WIFI platform called “GoKit” in China. This testing kit can be use to do some customized application. Not only WIFI communication, kit also support other functions. You can find interfaces listed as below. GoKit Interfaces: I try to use FRDM-KL02 to communicate with this kit to do a WIFI communication application. Board connection as below. This platform has two running mode. One is AirLink mode, and another is normal running mode. AirLink mode is used to WIFI communication or pair. Go to AirLink mode steps: Power on FRDM-KL02 Long press key1 to reset WIFI module. Wait until RED led on. Short press Key2 to go into configuration mode, wait until RED led flash on WIFI module. Open demo APP, select “adding device”, input SSID password. Waiting for configuration finish. Command Format HOF: 2bytes, value 0xFFFF Length: 2bytes Cmd:1byte SN:1byte Flags:2bytes DATA: Xbytes Checksum:1byte WIFI acquire device information MCU inform WIFI into configure mode MCU reset WIFI WIFI inform MCU status WIFI ask for reset Illegal command For detail code, I will post another thread for your reference.
查看全文
Freescale Semiconductor is to demonstrate its Kinetis L series microcontrollers (MCUs) built on the ARM Cortex-M0+ processor at DESIGN West in San Jose, California, with alpha sampling due to start in the second quarter of 2012. Freescale  says the ability to demonstrate these devices is possible due to its  close partnership between ARM during the Cortex-M0+ core development  process and as a lead partner provided  input that helped ARM define and  develop the processor. The devices are slated for applications  such as domestic appliances, portable medical systems, smart meters,  lighting, power and motor control systems. "Our close partnership  with ARM throughout the design and development of their new core has  positioned us as the first MCU supplier to produce and demonstrate an MCU based on the Cortex-M0+ and continues our strategy of driving to  market new products based on the ARM architecture," said Reza  Kazerounian, senior vice president and general manager of Freescale’s  Automotive, Industrial and Multi-Market Solutions Group. Mike  Inglis, executive vice president and general manager of ARM’s Processor  Division, added "With the addition of the L series to their Kinetis  line, Freescale is creating one of the industry’s broadest, most  scalable ARM Cortex-M MCU portfolios, ranging from very low-cost,  entry-level products based on the ARM Cortex-M0+ processor, up to 4 MB,  200 MHz devices based on the Cortex-M4 processor." Manufactured  using Freescale’s low-leakage, 90 nm thin film storage (TFS) process  technology, the Kinetis L series will have a selection of on-chip flash  memory densities and analog, connectivity and HMI peripheral options. Upward  migration through the Kinetis portfolio is available via compatible Kinetis K series devices (built on the ARM Cortex-M4 processor) that  provide access to DSP performance and advanced feature integration. The  ARM Cortex-M0+ processor includes a reduced two-stage pipeline,  allowing faster branch instruction execution, single-cycle access to I/O  and critical peripherals, optimized access to program memory, linear 4  GB address space that removes the need for paging, reducing software  complexity and ensuring a more 8-bit-like user experience and a micro  trace buffer, providing a low-cost trace solution that allows faster bug  identification and correction without the need for additional I/O  resources. Freescale will demonstrate the ARM Cortex-M0+ core at its exhibition booth #1604 at DESIGN West , March 26-29 at the San Jose McEnery Convention Center.
查看全文
The Technical University in Brasov (Romania) has set up a Medical Teaching lab featuring the Freescale Tower Kit K53 with Oximeter MED-SPO2 and 2 electrode system EKG MED-EKG. Find below the material associated to this lab led by Prof. Sorin-Aurel Moraru from the Faculty of Engineering. He can be contacted at [email protected] The course is in Romanian and include an overview of the hardware and exercises
查看全文
Using a MK70FN1M0VMJ15 processor with MII and ADC2_SE16 enabled. Also using Codewarrior 10.6 and MQX4.022. Anytime I initialize the ADC2_SE16 the webserver stops working. I have delayed the initialization of the ADC2_SE16 and found that webserver works fine till initialization. I have also noticed that when the ADC2_SE16 is initialized first the webserver never gets link active. My question is that even though these are different ports and no pin is shared could the possibly be affecting each other? Hi Lee: I have been looking for information related to this problem but at this moment I have not find anything, In this case I would like to know if you are using a development board from Freescale or if you are using a custom board? Have a nice day, Perla Moncada ----------------------------------------------------------------------------------------------------------------------- Note: If this post answers your question, please click the Correct Answer button. Thank you! ----------------------------------------------------------------------------------------------------------------------- It is a custom board, with MII setup instead of RMII. I am concerned that it may be a chip issue, and have no real way to test that possibility with the Development board. This document was generated from the following discussion: 
查看全文
Here you will find both the code and project files for the USB Mouse project. In this project the USB module is configured as a device, the X and Y coordinates to move the cursor are obtained from the accelerometer measurements. Once the code is loaded it is necessary to disconnect the USB cable from the J26 USB connector and plug it to the K64 USB connector. Once the device enumerates you can use it as an air mouse. The left and right click buttons have not been enabled. To compile the project you must import the following libraries: USBMouse.h FXOS8700Q.h Code: #include "mbed.h" #include "USBMouse.h" #include "FXOS8700Q.h" //I2C lines for FXOS8700Q accelerometer/magnetometer FXOS8700Q_acc acc( PTE25, PTE24, FXOS8700CQ_SLAVE_ADDR1); USBMouse mouse; int main() {     acc.enable();     float faX, faY, faZ;     int16_t x = 0;     int16_t y = 0;       while (1)     {         //acc.getAxis(acc_data);         acc.getX(&faX);         acc.getY(&faY);         x = 10*faX;         y = 10*faY;               mouse.move(x, y);         wait(0.001);     } }
查看全文
To do: Implement a program that lets the 4 LEDs on the Tower toggle all together using the PIT Interrupt. This time, let the program run in the Flash. * toggle period 0.5 s * extract vector table and service routines in 'vector.c' * Change the linker command file 'ldscript_flash' * Take care of the 16 Byte security settings from $400-$410 in the Flash. Do not overwrite!!! Hint: Use the 'arm_cm4.c and 'arm_cm4.h' from the freescale kinetis homepage, which include access functions for the NVIC. For ease of use, these routines are included in the result file. Result: TWR_K60_PIT0_Flash.zip
查看全文
1. 使用J-Link+J-Flash给Kinesis烧写序列号(Program serial number for Kinetis by J-Link + J-Flash) 2. 教你用J-Flash ARM工具单独烧写程序到Kinetis 3. Cyclone Max 使用步骤及注意事项 4. 飞思卡尔常用脱机烧写工具 5. 离线烧写工具Cyclone Max使用方法及单次按键烧写两个image文件的实现方法​ 6.Kinetis 量产注意事项​
查看全文
Este proyecto se hizo teniendo en mente el consumo del agua en un hogar promedio para ayudar a no desperdiciarla; en un caso típico se tiene una cisterna a la que llega el agua directamente de la red de agua potable de la ciudad, también se cuenta con un tinaco y con una bomba de agua para trasladarla desde la cisterna. Tanto el tinaco como la cisterna cuentan con 2 sensores de nivel de agua, un nivel alto y un nivel bajo... Por dar un ejemplo, cuando la cisterna se encuentre totalmente llena y el tinaco vacío, la bomba encenderá para enviar agua al tinaco y continuará subiendo agua hasta que el sensor alto del tinaco detecte que ya está lleno y entonces se apagará la bomba; cuando el tinaco empiece a vaciarse y el nivel alto no detecte agua la bomba no encenderá, lo hará hasta que el nivel bajo del tinaco no detecte agua, de ésta manera se evita que la bomba esté prendiendo y apagando si es que se utiliza solo el sensor alto para encender y apagar la bomba. Un caso parecido será el de la cisterna; la cisterna solo enviará agua al tinaco si ésta se encuentra llena o si tiene un nivel medio de agua (por el hecho de estar mandando el líquido al tinaco) y en caso de estar vacía o aunque el nivel bajo esté detectando agua no prenderá la bomba hasta que el nivel alto detecte que ya está llena de nuevo, ésto para evitar (al igual que en el caso del tinaco) que con el simple cambio de un solo sensor esté prendiendo y apagando la bomba; es aquí donde se aplica la lógica y es el trabajo que hace en éste proyecto la tarjeta de freescale.
查看全文
Hello Freedom users I have created another full board review this time for the FRDM-KL05Z always including clear instructions to program and debug your first project. I'm still working on the video version (looking for a better accent :smileyconfused:), but the commands illustrated by screen captures should be easy to follow. Freescale Freedom development platform: [FRDM-K... | element14 Enjoy Greg
查看全文