Kinetis Microcontrollers Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis Microcontrollers Knowledge Base

Discussions

Sort by:
Installation file containing training examples - unpack and run this file to install code examples.
View full article
Hi, Anybody has sample code for K22 SPI? where shall I get the same? Thank Sarvani
View full article
Kinetis L series MCUs combine the exceptional energy-efficiency and ease-of-use of the new ARM® Cortex™-M0+ processor with the performance, peripheral sets, enablement and scalability of the Kinetis 32-bit MCU portfolio. The Kinetis L series frees power-critical designs from 8- and 16-bit MCU limitations by combining excellent dynamic and stop currents with superior processing performance, a broad selection of on-chip flash memory densities and extensive analog, connectivity and HMI peripheral options. Kinetis L series MCUs are also hardware and software compatible with the ARM Cortex-M4-based Kinetis K series, providing a scalable migration path to more performance, memory and feature integration. The Kinetis L Series MCUs are Energy-Efficient Product Solutions by Freescale. For more information visit Freescale.com\Lseries
View full article
1 Abstract      LIN (Local Interconnect Network) is a concept for low cost automotive networks, which complements the existing portfolio of automotive multiplex networks. LIN is based on the UART/SCT protocol. It can be used in the area of automotive, home appliance, office equipment, etc. The UART module in NXP kinetis L series contains the LIN slave function, it can be used as the LIN slave device in the LIN bus. Because there is few LIN slave KL sample code for the customer’s reference in our website, now this document mainly take KL43 as an example, explain how to use the FRDM-KL43 board as the LIN slave node to communicate with the LIN master device. LIN master use the specific LIN module: PCAN-USB Pro FD. Master send the publisher ID and subscriber ID, slave give the according LIN data response. This document will share the according code, hardware connection and the test result. 2 LIN bus basic knowledge review         For the convenient to understand the LIN bus, this chapter simply describe the basic knowledge for LIN bus. Mainly about the LIN topology and the LIN frame. 2.1 LIN bus topology structure       LIN bus just use the simple low cost single-wire, it uses single master to communicate with multiple slaves. The bus voltage is 12V, the speed can up to 20 kbit/s. LIN network can connect 16 nodes, but in the practical usage, normally use below 12 nodes. Figure 2-1. LIN bus topology 2.2 LIN bus frame structure          LIN Frame consists of a header (provided by the master task) and a response (provided by a slave task).     Master send publisher frame: Master send header+ data +checksum; slave just receive.     Master send subscriber frame: Master send header; slave receive send data +checksum.     The following figure is the structure of a LIN frame: Figure 2-2. LIN frame structure      LIN frame is constructed of one Break field, sync byte field (0X55), PID, data and checksum. 2.2.1 Break filed and break delimiter Break filed is consist of break and break delimiter. Break should at least 13 nominal bit times of dominant value (low voltage). The break delimiter shall be at least one nominal bit time long (high voltage). Figure 2-3. break field 2.2.2 Sync byte field Sync is a byte field with the data value 0X55. The byte field is the standard UART protocol. Figure 2-4. The sync byte field 2.2.3 Protected identifier field A protected identifier field consists of two sub-fields: the frame identifier and the parity. Bits 0 to 5 are the frame identifier and bits 6 and 7 are the parity.     ID value range: 0x00-0x3f, 64 IDs in total. It determine the frame categories and direction. Figure 2-5. The sync byte field P0 = ID0 xor ID1 xor ID2 xor ID4 P1 = -(ID1 xor ID3 xor ID4 xor ID5) -is NOT。  ID can be split in three categories:   Frame categories Frame ID Signal carrying frame Unconditional frame 0x00-0x3B Event triggered frame Sporadic frame Diagnostic frame Master request frame 0x3c Slave response frame 0x3d Reserved frame   0x3e,0x3f     2.2.4 DATA       A frame carries between one and eight bytes of data. The number of data contained in a frame with a specific frame identifier shall be agreed by the publisher and all subscribers.      For data entities longer than one byte, the entity LSB is contained in the byte sent first and the entity MSB in the byte sent last (little-endian). The data fields are labeled data 1, data 2,... up to maximum data 8. 2.2.5 checksum  The checksum contains the inverted eight bits sum with carry over all data bytes or all data bytes and the protected identifier.        Classic checksum: Checksum calculation over the data bytes. Enhanced checksum: Checksum calculation over the data bytes and the protected identifier byte.  Method: eight bits sum with carry is equivalent to sum all values and subtract 255 every time the sum is greater or equal to 256, at last, the sum data do bitwise invert.  In the receive side, do the same sum, but at last, don’t do invert, then add the received checksum data, if the result is 0XFF, it is correct, otherwise, it is wrong. 3 KL43 LIN slave example    This chapter use KL43 as the LIN slave, and communicate with the specific LIN master device, realize the LIN data sending and receiving. 3.1 Hardware prepare Hardware: FRDM-KL43,TRK-KEA8,PCAN-USB Pro FD       LIN bus voltage is 12V, but the FRDM-KL43 don’t have the LIN transceiver, so we need the external LIN transceiver connect the KL43 uart, to realize the LIN voltage switch. Here we use the TRK-KEA8 on board LIN transceiver MC33662LEF for the KL43. The MC33662LEF circuit is like this:    Figure 3-1. LIN transceiver schematic 3.1.1 FRDM-KL43 and TRK-KEA8 connections      FRDM-KL43 need to connect the UART port to the LIN transceiver. The connection shows in this table: No. FRDM-KL43 TRK-KEA8 note 1 J1-2 J10-5 UART0_RX 2 J1-4 J10-6 UART0_TX 3 J3-14 J14-1 GND 3.1.2 TRK-KEA8 and LIN master connections         LIN bus is using the signal wire.  TRK-KEA8 J14_4 is the LIN wire, it should connect with the LIN wire in PCAN-USB Pro FD. GND also need to connect together.        TRK-KEA8 P1 need a 12V DC supplier. Master also need 12V DC supplier. 3.1.3 Object connection picture   Figure 3-2. Object connections 3.2 Software flow chart and code      Now describe how to realize the LIN master and the LIN slave data transfer. LIN master send a publisher frame, the slave will receive the according data. LIN master send a subscriber frame, the slave will send the data to the master. The code is based on the KSDK2.2_FRDM-KL43 lpuart, add the LIN operation code.  3.2.1 Software flow chart         Figure 3-3. Software flow chart   3.2.2 software code     Code is based on KSDK2.2_FRDM-KL43 lpuart project, add the LIN operation code, the added code is list as follows: void LPUART0_IRQHandler(void) {      if(LPUART0->STAT & LPUART_STAT_LBKDIF_MASK)      {        LPUART0->STAT |= LPUART_STAT_LBKDIF_MASK;// clear the bit        Lin_BKflag = 1;        cnt = 0;        state = RECV_SYN;        DisableLinBreak;          }     if(LPUART0->STAT & LPUART_STAT_RDRF_MASK)      {                  rxbuff[cnt] = (uint8_t)((LPUART0->DATA) & 0xff);                  switch(state)          {             case RECV_SYN:                           if(0x55 == rxbuff[cnt])                           {                               state = RECV_PID;                           }                           else                           {                               state = IDLE;                               DisableLinBreak;                           }                           break;             case RECV_PID:                           if(0xAD == rxbuff[cnt])                           {                               state = RECV_DATA;                           }                           else if(0XEC == rxbuff[cnt])                           {                               state = SEND_DATA;                           }                           else                           {                               state = IDLE;                               DisableLinBreak;                           }                           break;             case RECV_DATA:                           recdatacnt++;                           if(recdatacnt >= 4) // 3 Bytes data + 1 Bytes checksum                           {                               recdatacnt=0;                               state = RECV_SYN;                               EnableLinBreak;                           }                           break;          default:break;                                    }                  cnt++;      }     } void uart_LIN_break(void) {     LPUART0->CTRL &= ~(LPUART_CTRL_TE_MASK | LPUART_CTRL_RE_MASK);   //Disable UART0 first     LPUART0->STAT |= LPUART_STAT_BRK13_MASK; //13 bit times LPUART0->STAT |= LPUART_STAT_LBKDE_MASK;//LIN break detection enable LPUART0->BAUD |= LPUART_BAUD_LBKDIE_MASK;         LPUART0->CTRL |= (LPUART_CTRL_TE_MASK | LPUART_CTRL_RE_MASK);     LPUART0->CTRL |= LPUART_CTRL_RIE_MASK;     EnableIRQ(LPUART0_IRQn);    } int main(void) {     uint8_t ch;     lpuart_config_t config;     BOARD_InitPins();     BOARD_BootClockRUN();     CLOCK_SetLpuart0Clock(0x1U);     LPUART_GetDefaultConfig(&config);     config.baudRate_Bps = BOARD_DEBUG_UART_BAUDRATE;     config.enableTx = true;     config.enableRx = true;     LPUART_Init(DEMO_LPUART, &config, DEMO_LPUART_CLK_FREQ);     uart_LIN_break();     while (1)     {        if(state == SEND_DATA)        {           while((LPUART0->STAT & LPUART_STAT_TDRE_MASK) == 0); // hex mode                   LPUART0->DATA = 0X01;           while((LPUART0->STAT & LPUART_STAT_TDRE_MASK) == 0); // hex mode                   LPUART0->DATA = 0X02;           while((LPUART0->STAT & LPUART_STAT_TDRE_MASK) == 0); // hex mode                   LPUART0->DATA = 0X10;//Checksum   0X10 correct, 0xaa is wrong           recdatacnt=0;           state = RECV_SYN;           EnableLinBreak;        }     } }     4 KL43 LIN slave test result   Master defines two frames: Unconditional ID Protected ID Direction Data checksum 0X2C 0XEC subscriber 0x01,0x02 0x10 0X2D 0XAD Publisher 0x01,0x02,0x03 0x4c    Now, master send 0X2C and 0X2D data, give the test result and the according waveform. 4.1 LIN master configuration Uart baud rate is: 9600bps 4.2  Send ID 0X2C and 0X2D frame       From the PC software of LIN master, we can find 0X2D ID can send the data successfully, and 0X2C ID can receive the correct data (0x01, 0x02) and checksum (0x10) from the KL43 LIN slave side. 4.2.1 0X2D ID frame oscilloscope waveform and debug result      From the debug result, we can find the buff can receive the correct ID, data and checksum from the LIN master.    4.2.2 0X2C ID frame oscilloscope waveform 4.2.3 0X2C ID SLAVE send back the wrong checksum     From the PC software, we can find if the KL43 code modify the checksum to the wrong data 0XAA, then the PC software will display the checksum error. This is the according oscilloscope waveform for the wrong checksum data. From all the above test result. We can find, KL43 as the LIN slave, it can receive the correct data from the LIN master, and when LIN master send the subscriber ID, kl43 also can send back the correct LIN data to the master. More detail, please check the attached code project. BTW, LIN spec can be downloaded from this link: http://www.cs-group.de/wp-content/uploads/2016/11/LIN_Specification_Package_2.2A.pdf   Attached is the code and the pdf version of this document:                  
View full article
  (para español continua mas abajo) Blind deaf-mute comunication system   Materials Used : A Freedom- KL25Z card A USB Cable A 16x2 LCD Display Three buttons A breadboard A USB cable   Project description Thinking about the difficulties a blind, deaf-mute person has to convey a message, we designed a device to facilitate their communication. Using the Morse key system, the disabled person can write a short message on a LCD screen. For this, you need to press three buttons, and depending on the duration, a function will be performed. 1. If you short-press the button on the left, this will erase the last character typed, however, if you long-press, this will erase everything written. 2. If the middle button with the green label is short-pressed, this will print a dot at the bottom of the screen. If you long press the button, it will print a dash. In Morse code, the dot represents a single signal and the dash represents a triple signal. 3. If the button on the right, with the yellow label is short pressed, the LCD display space will be added to the message. But if he was held down with a longer duration, the set of ¨ Short ¨ and ¨ Long ¨ will be transformed in to a letter in the alphabet and it will be printed on the screen. Note: * If the set of Short and Long does not match any sequence in the matrix, no character is added to the message. **The system to display and write the message on the LCD display are separate.     Modifications for the second stage of the prototype 1. Delete button on the right, the yellow label, Send and Space. a. It is intended that the third button is eliminated by increasing the code efficiency. Instead of sending the sequence of short and long pressing a button, they are sent after a desired time interval. b. Wanted to enter the space with a sequence of short and long. 2. Currently the project is divided into two boxes, one that displays the buttons and other writing. The goal is to have a single box which can write and display the message. 3. With a potentiometer seek to change the time it takes to push a button to be recognized among one short and one long signal.   Modifications for the third stage of the prototype 1. Perform the division again in two boxes , interconnected by Bluetooth modules , as the system is designed to generate a communication between two people, using a system of sending data to harvest deaf -mute person in the future by Braille .       Sistema de Comunicación para Persona Ciega, Sorda y Muda   Materiales Utilizados: Una tarjeta Freedom-KL25Z Un Cable Una Pantalla LCD 16x2 Tres botones Una placa de pruebas (protoboard) Un cable USB   Descripción de Proyecto             Pensando en las dificultades que una persona ciega, sorda y muda tiene para transmitir un mensaje, se ha diseñado un aparato para facilitar su comunicación. Utilizando el sistema de clave morse, la persona con discapacidad puede escribir un mensaje corto en una pantalla LCD. Para esto, se deben presionar tres botones que dependiendo la duración del toque, será la función que efectuará. 1. Si al botón de la izquierda, con la etiqueta azul, apenas se le presiona este borrará el ultimo carácter escrito; sin embargo, si se le presiona con una mayor duración este borrará todo lo escrito. 2. Si al botón del medio, con la etiqueta verde, apenas se le presiona este imprimirá en la parte inferior de la pantalla un punto. El punto representa, un corto en el sistema de clave morse. Sin embargo, si se le mantiene presionado por un momento mas largo, este imprimirá un guión. El guión representa un comando largo en el sistema de clave morse. 3. Si al botón de la derecha, con la etiqueta amarilla, apenas se le presiona, en la pantalla LCD se agregará un espacio al mensaje. Sin embargo si se le mantiene presionado con una mayor duración, se enviará el conjunto de ¨Cortos¨ y ¨Largos¨ a una matriz para que la secuencia se busque y cuando esta se haya, en la LCD se agrega la letra deseada al mensaje. Nota: *Si el conjunto de Cortos y Largos no coincide con ninguna secuencia en la matriz, ningún carácter se agregará al mensaje. ** El sistema para mostrar el mensaje con la LCD esta separado a los botones para escribirlo.     Modificaciones para la segunda etapa del prototipo 1.      Eliminar el botón de la derecha, con etiqueta amarilla,  de Enviar y Espacio. a.       Se pretende que el tercer botón sea eliminado mediante el aumento en la eficiencia del código. En vez de enviar la secuencia de Cortos y Largos al presionar un botón, estos se enviarían después de un intervalo de tiempo deseado. b.      Se busca que el espacio se introduzca con una secuencia de cortos y largos. 2.      Actualmente el proyecto está dividido en dos cajas, una que muestra el mensaje y otra con los botones para escribir. El objetivo es tener una sola caja con el que se pueda escribir y mostrar el mensaje. 3.      Con un potenciómetro se busca cambiar el tiempo que se necesita apretar un botón para que se reconozca entre un toque corto y uno largo.   Modificaciones para la tercera etapa del prototipo 1.      Realizar de nuevo la división en dos cajas, comunicadas entre sí por módulos bluetooth, ya que el sistema está pensado para poder generar una comunicación entre ambas personas, utilizando en un futuro, un sistema de envío de datos a la persona siega sordo-muda mediante el sistema braille.
View full article
SSD1963驱动4.3寸屏原理图。
View full article
Hello Kinetis community, High accuracy metering is an essential feature of an electronic power meter application. Metering accuracy is a most important attribute because inaccurate metering can result in substantial amounts of lost revenue. Moreover, inaccurate metering can also undesirably result in overcharging to customers.  The common sources of metering inaccuracies, or error sources in a meter, include the sensor devices, the sensor conditioning circuitry, the Analog FrontEnd (AFE), and the metering algorithm executed either in a digital processing engine or a microcontroller In this post you will find the description of the implementation of a Two Phase Power Meter firmware featuring Kinetis KM34 device using a metering algorithm known as Filter Based Algorithm. The showed firmware was implemented on the hardware design described in the Reference Manual DRM149 (the software implementation shown in the DRM149 is using a more complex metering algorithm called Fast Fourier Transform). Firmware Design The firmware implements the basic functions for an e-meter application such as: Power meter calibration: Performs power meter calibration and stores calibration parameters. Data processing: Read digital values form the AFE and performs scaling. Calculation of quantities: Calculates billing and non-billing quantities HMI control: Updates LCD with the new values and transitions to new LCD screen. Powe Meter Calibration The calibration task runs whenever a non-calibrated power meter is connected to the mains. First it checks if the calibration flag is already stored in the microcontroller flash, if not, then it runs the calibration. More detail about the calibration process can be found in the DRM143 document. The function: int16 CONFIG_CalcCalibData (tCONFIG_FLASH_DATA *ptr)‍‍‍ is in charge of calculating the calibration data and store the calibration flag in the flash. You can refer to the next code section for the complete usage and definition.   /* if calibration data were collected then calibration parameters are       */   /* calculated and saved to flash                                            */   if (CONFIG_CalcCalibData ((tCONFIG_FLASH_DATA *)&ramcfg) == TRUE)     CONFIG_SaveFlash ((tCONFIG_FLASH_DATA *)&ramcfg, ramcfg.flag);‍‍‍‍ The calibration task terminates by storing calibration gains, offsets and phase shift into the flash and by resetting the microcontroller device. Data Processing Reading the phase voltage and phase current samples from the analog front-end (AFE) occurs periodically every 166.6 μs. This task runs on the highest priority level (Level 0) and is triggered asynchronously when the AFE result registers receive new samples. The task reads the phase voltage and phase current samples from the AFE result registers, scales the samples to the full fractional range, and writes the values to the temporary variables for use by the calculation task. While kWh values is being calculated every 6000 Hz the remaining quantities: kVARh, QAVG, PAVG, URMS and IRMS are being calculates every 1500 Hz (666.6 μs). This is according to the decimation factor and to reduce the CPU usage since those values are not needed every AFE sample. The meter definition used for this application can be found in the meterlib2ph_cfg.h files, this file was generated using the Filter-Based Metering Algorithms Configuration Tool, for more information on how to use the tool you can refer to the AN4265 document. This is the Meter configuration: Here you can see the expected error behavior against Frequency: The configuration of the AFE module and channels is the following:   /* Current Phase 1                                                          */   AFE_ChInit (CH0,               AFE_CH_SWTRG_CCM_PGAOFF_CONFIG(DEC_OSR1024),                    0,               PRI_LVL1,               (AFE_CH_CALLBACK)NULL);     /* Current Phase 2                                                          */   AFE_ChInit (CH1,               AFE_CH_SWTRG_CCM_PGAOFF_CONFIG(DEC_OSR1024),               0,               PRI_LVL1,               (AFE_CH_CALLBACK)NULL);     /* Voltage Phase 1                                                          */   AFE_ChInit (CH2,               AFE_CH_SWTRG_CCM_PGAOFF_CONFIG(DEC_OSR1024),                    0,               PRI_LVL1,               (AFE_CH_CALLBACK)NULL);     /* Voltage Phase 2                                                          */     AFE_ChInit (CH3,               AFE_CH_SWTRG_CCM_PGAOFF_CONFIG(DEC_OSR1024),               0,               PRI_LVL1,               (AFE_CH_CALLBACK)afech3_callback);     /* AFE Initialization @ 6 KHz                                               */   AFE_Init    (AFE_MODULE_RJFORMAT_CONFIG(AFE_PLL_CLK, AFE_DIV2, 12.288e6));  ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ As you can see only the CH3, which is measuring the Voltage phase 2, is configured with interrupt. During the CH3 callback the remaining channels are sampled to get the 4 values at the same time and performs scaling: /* measurements callback @ 6000 Hz                                            */ static void afech3_callback (AFE_CH_CALLBACK_TYPE type, int32 result) {   static int cnt_1 = 0;     if (type == COC_CALLBACK)   {      /* Current and Voltage reading                                            */     u24_sample[0] = AFE_ChRead (CH2) << U_SCALE;            /* Voltage 1 reading ... */     i24_sample[0] = AFE_ChRead (CH0) << I_SCALE;            /* Current 1 reading ... */     u24_sample[1] = AFE_ChRead (CH3) << U_SCALE;            /* Voltage 2 reading ... */     i24_sample[1] = AFE_ChRead (CH1) << I_SCALE;            /* Current 2 reading ... */     . . . . }‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Calculation of Quantities Within the CH3 interrupt the metering algorithm functions are called to process the data of the active energy, the calculation task scales the samples using calibration offsets and calibration gains obtained during the calibration phase: METERLIB2PH_ProcSamples removes DC bias from phase voltage and phase current samples together with performing an optional sensor phase shift correction. METERLIB2PH_CalcWattHours recalculates active energy using new voltage and current samples. CONFIG_UpdateOffsets updates offset of the phase voltage and current measurements conditionally. The CH3 calls the next software interrupt, auxcalc_callback where non-billing quantities are calculated: METERLIB2PH_CalcVarHours recalculates reactive energy. METERLIB2PH_CalcAuxiliary recalculates URMS, IRMS, PAVG, QAVG and S auxiliary quantities. You can find more information about the Filter-Based Algorithm function in the AN4265 document.   HMI Control The display_callback task is called every 3 Hz by the auxcalc_callback and is executed on the lowest priority. For this application it update the clock data structure, refresh the watchdog timer and call some metering algorithm functions to read the values of the billing and non-billing quantities: METERLIB2PH_ReadResultsPh1 reads URMS, IRMS, PAVG, QAVG and S auxiliary quantities from phase 1. METERLIB2PH_ReadResultsPh2 reads URMS, IRMS, PAVG, QAVG and S auxiliary quantities from phase 2. A timer interrupt is used to update the the LCD content every 1500 ms. static void lptmr_callback (void) {   lcd_all_off();   /* update menu index                                                    */   menu_fcn[menu_idx]();   if ((++menu_idx) >= DIM(menu_fcn))   {     menu_idx = 0;   } }‍‍‍‍‍‍‍‍‍‍ Results The two-phase hardware has been calibrated using the test equipment ELMA8303. During accuracy calibration and testing, the power meter measured electrical quantities generated by the test bench, calculated active and reactive energies, and generated pulses on the output LEDs; each generated pulse was equal to the active and reactive energy amount kWh (kVARh)/imp3. The deviations between pulses generated by the power meter and reference pulses generated by test equipment defined the measurement accuracy.   The next figure shows the calibration protocol of the power meter. The protocol indicates the results of the power meter calibration performed at 25 °C. The accuracy and repeatability of the measurement for various phase currents and angles between phase current and phase voltage are shown in these graphs. The first graph indicates the accuracy of the active and reactive energy measurement after calibration. The x-axis shows variation of the phase current, and the y-axis denotes the average accuracy of the power meter computed from five successive measurements The second graph (on the bottom) shows the measurement repeatability; i.e. standard deviation of error of the measurements at a specific load point.  You will find attached a ZIP file containing the IAR source code of the application and a PDF file showing the complete results of the protocol. I hope the information helps. Regards, Adrian Cano
View full article
Hello Kinetis World, I just wanted to take this opportunity to share the press release for our newly announced WLCSP device.         http://finance.yahoo.com/news/thin-blade-grass-freescale-newest-120000684.html The Ultra Thin CSP, MK22FN512CBP12R, is equivalent to the standard height CSP, MK22FN512CBP12R.  Therefore, from Therefore, from a software enablement perspective, the MK22FN512CAP12 device can be selected as shown in the attached Processor Expert screenshot.  We're looking forward to seeing what amazing things you can accomplish using Kinetis technology!      
View full article
Hi All, NXP provides a software drivers library for Kinetis M devices, the KM bare-metal drivers. It includes support for peripherals and FreeRTOS. Follow the instructions to download and install the software package. Go to the KM3x section in the NXP webpage. Click on the documentation tab In the Application Notes section look for the API reference manual for Kinetis M bare-metal drivers and software examples, download: HTML > Reference Manual and documentation ZIP > Software package Unzip the KMSWDRVAPIRM_SW.zip file into a computer location. Inside the folder you will find several .exe files, select the appropriate file for your application and follow the installation instructions. By default a folder named KMxxxSWDRV_Rx_x_x is created. You can see the folder structure like this build: Build examples project files for the selected IDE. refman: Source files of the HTML Reference Manual src: Source files for drivers: common – common files for projects: device headers, startup routines, etc. drivers – peripheral drivers source code. freemaster – Freemaster source files for communication functions with Freemaster software. freertos – FreeRTOS files, kernel and RTOS support. projects – example projects demonstrating peripherals and modes. toolchain – toolchain support. template – Base projects for supported IDEs and make_project.exe file to create new project for different supported IDEs. If you need support for a different IDE or KM device you just need to extract the appropriate .exe file from the SW package. Hope information helps! Happy Downloading and installing! Regards, Adrian Cano NXP FAE
View full article
Latest published errata for ISF 2.1
View full article
VREF module provide one input pin VREF, this pin can provide reference voltage for both external circuit but also for internal Sigma Delta ADCs, AFE and DAC.  Also it includes trim function in it. In this document, I would like to use my testing to do a linearity analysis. From figure1 and 2, you can find how to make VREF as reference voltage of different analog module. For example, you can find when S1 switches down, S0 closes and S2 select VREF, VREF will be voltage resource of SAR ADC.                                               Figure 1: Voltage reference function configuration                                   Figure 2: Voltage reference module diagramming I do a testing for VREF trim value linear analysis. The process is connecting the voltmeter to VREFH pin, then record measure result for each setting of VREF trim. There will be 64 records for every different setting. Testing chip is MKM34Z256. Please find my testing result from testing data table. From testing result, you can get the formula that y = kx + x0, where k is about 0.005 (5mV) and x0 is about 1.1881, x is trim value.  You can find there is only a little offset from offset curve.                                         Table 1: Trim voltage testing date                                                                 Figure 3: Offset curve
View full article
Abstract MK60 is a popular MCU in Kinetis K family. NXP has prepared some kinds of bootloader for TWR-K60D100. But as we all know, MCUBoot2.0.0 is the most update bootloader for Kinetis family. It is a configurable flash programming utility that operates over a serial connection on Kinetis MCUs. It enables quick and easy programming of Kinetis MCUs through the entire product life cycle, including application development, final product manufacturing, and beyond. But sinceTWR-K60D100 is a relatively old platform compare to K22 and K64/K65/K66, MCUBoot2.0.0 did not add MK60 to its target board. If customer don’t like those old bootloader, they have to port it by themselves. This article tries to guide user to port MCUBoot to TWR-K60D100 base on Chapter 10 in Kinetis Bootloader v2.0.0 Reference Manual. This time we use KDS. Software requirement: Kinetis Design Studio 3.2 MCUBootloader 2.0.0 (KBoot 2.0.0) MCUXpresso Config Tools v4.0 SDK_2.2_TWR-K60D100M Porting flow Step 1: First I copy NXP_Kinetis_Bootloader_2_0_0\targets\MK64F12 to NXP_Kinetis_Bootloader_2_0_0\targets\MK60D100. The reason I select MK64 is more likely to MK60 than other target, especially in clock distribution, system integration module and signal multiplexing. In mk60d100\src directory, rename the following files: clock_config_mk64f12.c —> clock_config_mk60d100.c hardware_init_mk64f12.c —> hardware_init _ mk60d100.c memory_map_mk64f12.c —> memory_map _ mk60d100.c peripherals_ mk64f12.c —> peripherals _ mk60d100.c Then copy system_MK60D10.c and system_MK60D10.h from SDK_2.2_TWR-K60D100M to mk60d100\src\startup, copy startup_MK60D10.S from SDK_2.2_TWR-K60D100M to mk60d100\src\startup\gcc. Step 3: Then I copy \src\platform\devices\MK64F12 to \src\platform\devices\mk60d100, copy SDK_2.2_TWR-K60D100M\devices\MK60D10\fsl_device_registers.h, MK60D10.h, and MK60D10_features.h to this new directory. Step 4: Open the KDS project in MK60D100 and replace above old file with new file. After that, I change some setting. Figure 1. Target Processor change   K64 has hardware FPU, but K60D100 hasn’t. So, Float ABI must be changed to software. There is a C/C++ preprocessor define that is used by the bootloader source to configure the bootloader based on the target MCU. This define must be updated to reference the correct set of device-specific header files. Figure 2. Preprocessor change   As to the link file, it needn’t to be change. We can use K64’s link file. TWR-K60D100 use an old version PE debugger. So, the debugger setting must be changed. Figure 3. Debug setting Step 5: MK60’s clock distribution structure is different with MK64. We must modify this part. As it is very complex, use MCUXpresso Config Tools to generate this config code is a sensible choice. Open the tools and step clock structure as below: Figure 4. clock setting After that, generate the code and save them to \src\platform\devices\mk60d100. Since MCUBoot2.0.0 is not base on SDK2.x, we must copy some related driver file from SDK2.x package, include fsl_smc.c, fsl_smc.h, fsl_rtc.c, fsl_rtc.h. Then add them to project. In clock_config_mk60d100.c line 168, the code is clock_mode_switch(s_currentClockMode, kClockMode_FEI_48MHz); Replace it with:      BOARD_BootClockUSB(); // this function was generated by MCUXpresso Config Tool Then add the head file of “clock_config.h”.   Step 6: TWR-K60D100 use UART5 as the debug UART port. Please refer to https://community.nxp.com/docs/DOC-340954 for detail. MCUBootloader2.0.0 do not support UART5. User must add its code in pinmux_utility_common.c.   Step 7: Modify usb_clock_init() in hardware_init_MK60D100.c as below bool usb_clock_init(void) {    SIM->SCGC4 &= ~SIM_SCGC4_USBOTG_MASK;      SIM->CLKDIV2 = (uint32_t)0x00L;    SIM->SOPT2 |= SIM_SOPT2_USBSRC_MASK | SIM_SOPT2_PLLFLLSEL(0x01);     //k60 PLLFLLSEL change from 3 to 1      SIM->SCGC4 |= SIM_SCGC4_USBOTG_MASK;   //   USB0->CLK_RECOVER_IRC_EN = 0x03; //   USB0->CLK_RECOVER_CTRL |= USB_CLK_RECOVER_CTRL_CLOCK_RECOVER_EN_MASK;   //   USB0->CLK_RECOVER_CTRL |= 0x20;      return true; }   Modify memory_map_MK60D100.c as below: memory_map_entry_t g_memoryMap[] = {    { 0x00000000, 0x0007ffff, kMemoryIsExecutable, &g_flashMemoryInterface },   // Flash array (512KB)    { 0x1fff0000, 0x2000ffff, kMemoryIsExecutable, &g_normalMemoryInterface }, // SRAM (256KB) { 0x40000000, 0x4007ffff, kMemoryNotExecutable, &g_deviceMemoryInterface }, // AIPS peripherals      { 0x400ff000, 0x400fffff, kMemoryNotExecutable, &g_deviceMemoryInterface }, // GPIO    { 0xe0000000, 0xe00fffff, kMemoryNotExecutable, &g_deviceMemoryInterface }, // M4 private peripherals    { 0 }                 // Terminator };   Modify bl_uart_irq_config_common.c as below: void UART_SetSystemIRQ(uint32_t instance, PeripheralSystemIRQSetting set) {    switch (instance)    {        case 0: #if (FSL_FEATURE_SOC_UART_COUNT > 1)        case 1: #endif // #if (FSL_FEATURE_SOC_UART_COUNT > 1) #if (FSL_FEATURE_SOC_UART_COUNT > 2)        case 2: #endif // #if (FSL_FEATURE_SOC_UART_COUNT > 2) #if (FSL_FEATURE_SOC_UART_COUNT > 3)        case 3: #endif // #if (FSL_FEATURE_SOC_UART_COUNT > 3) #if (FSL_FEATURE_SOC_UART_COUNT > 4)        case 4: #endif // #if (FSL_FEATURE_SOC_UART_COUNT > 4) #if (FSL_FEATURE_SOC_UART_COUNT > 5)          // add UART5 support        case 5: #endif // #if (FSL_FEATURE_SOC_UART_COUNT > 5)              if (set == kPeripheralEnableIRQ)            {                NVIC_EnableIRQ(uart_irqs[instance]);            }            else            {                NVIC_DisableIRQ(uart_irqs[instance]);            }            break;    } }   In target_config.h, modify kMaxCoreClock value to 100.   Step 8: After all of the above work, compile the project and download to TWR-K60D100 board. You’ll find KinetisFlashTool.exe can recognize the device by UART. If you establish a Tower system with TWR-SER board, KinetisFlashTool can also recognize the device by USB.   Conclusion: K60 is the base of many Kinetis K series MCU, include K10, K20, K61, K70. If you want to port MCUBoot2.0.0 to these MCU, you just want to update the clock_config file.
View full article
Hi everyone,      I have got customer queries on unavailability of complementary mode PWM on KL25Z . So, I thought let me experiment something and post it onto the community.      The timer module on KL25 is TPM, not FTM!. There are 3 TPMs, TPM0 with 6 channels, TPM1 and TPM2 with 2 channels each. To generate a PWM signal, PWM component can be used. But the PWM bean doesnot provide option to generate complementary PWM. So, we need to configure different channels to get the complementary PWM. Again, there is a limitation for this. PWM component doesn't allow to generate initial polarity high. It says "the inherited component doesnot support this feature". But in run time can set or clear value on the PWM output pin using the SetValue() and ClrValue(). But again the inherited component"TimerUnit_LDD" doesn't support generating SetValue() and ClrValue().      So, I came to a conclusion 'not to use PWM component' and started using Init_TPM. Using this component, 2 channels are configured to have opposite polarity during initialization. They are configured to have the same period. Deadtime is also inserted by configuring different duty cycle on each channel. But methods are not available since the component only provides the initialization function which is good enough to start . Dynamically if dutycycle needs to be changed, methods have to be written explicitly     Project and oscilloscope captures are attached for reference. Hi Note that this is also supported in the uTasker project - see http://www.utasker.com/docs/uTasker/uTaskerHWTimers.PDF See specifically the final page - this is compatible for K and KL processors. Regards Mark http://www.utasker.com/kinetis.html This document was generated from the following discussion: Complementary PWM on FRDM-KL25Z using processor expert
View full article
The following (after the "- - - - - -" is debugged code for flashing Green, Red, and Blue LEDs on the FRDM-K22F module. - - - - - - - - - - - - - - - - - - - - - - - - - - - - - - - - - - - - - - - #include "fsl_device_registers.h" #include "board.h" static int i = 0; int main(void) {   // LEDs are common-anode, with cathodes connected to port pins.   // Therefore, logic high (1) turns them off, and logic low   // (0) turns them on.   short OFF = 1;   short ON = 0;         hardware_init();           GPIO_DRV_SetPinDir(kGpioLED1, kGpioDigitalOutput); //Green LED      GPIO_DRV_SetPinDir(kGpioLED2, kGpioDigitalOutput); //Red LED      GPIO_DRV_SetPinDir(kGpioLED3, kGpioDigitalOutput); //Blue LED      GPIO_DRV_WritePinOutput(kGpioLED1, OFF); //Green LED initially off      GPIO_DRV_WritePinOutput(kGpioLED2, OFF); //Red LED initially off      GPIO_DRV_WritePinOutput(kGpioLED3, OFF); //Blue LED initially off      while (1)           {           for (i = 0; i<0xFFFFFF; i++)           {           }           GPIO_DRV_WritePinOutput(kGpioLED1, ON); //Green LED on           for (i = 0; i<0xFFFFFF; i++)           {           }           GPIO_DRV_WritePinOutput(kGpioLED1, OFF); //Green LED off           for (i = 0; i<0xFFFFFF; i++)           {           }           GPIO_DRV_WritePinOutput(kGpioLED2, ON); //Red LED on           for (i = 0; i<0xFFFFFF; i++)           {           }           GPIO_DRV_WritePinOutput(kGpioLED2, OFF); //Red LED off           for (i = 0; i<0xFFFFFF; i++)           {           };           GPIO_DRV_WritePinOutput(kGpioLED3, ON); //Blue LED on           for (i = 0; i<0xFFFFFF; i++)           {           }           GPIO_DRV_WritePinOutput(kGpioLED3, OFF); //Blue LED off           }      return 0; }
View full article
This manual explains how to create a project in CW and add components to Processor Expert. It also includes a couple of examples to print and get data with the printf and scanf functions from the stdio library by using Serial component (UART).
View full article
Recently I have received a report which said the customers met compiling issue when they imported the an2295sw CW project file and started to build it, the error message is like the following: When I looked into this issue, I found it was mainly due to some asm source file which was dedicated for Keil wrongly included in the CW project , so there would syntax error during compiling, and the linker issue was due to the path of linker file was wrongly defined, fix them would solve most of the compiling. 1. Fix source file issue: deselect the bootloader.asm file. 2. Fix linker file issue: redefine the correct path for linker file There is also an exception when you try to compile with the configuration for K70 120MHz part, it is due to some files can not be opened because the including path are missing: so besides the above changes, you have to add the paths below to solve this issue for Kinetis 120MHz part.    BTW, during debugging, I also found it is not convenient to switch between different configurations because users have to choose the proper header file for different platforms manually, so I add the following changes to support automatic switching platform according to the configuration but just with an exception for Kinetis K-1M 100MHz part, which still have to choose the proper platform manually. Customers who have downloaded an2295sw may directly replace the following files with that I attached in this document, which have included all above changes mentioned. an2295sw\src\Kinetis\CW_10.3\AN2295_Kinetis\.project an2295sw\src\Kinetis\CW_10.3\AN2295_Kinetis\.cproject an2295sw\src\Kinetis\CommonSource\bootloader_cfg.h Hope that helps, Kan
View full article
In this document we are going to see how to use the attached code which implements the configuration of the FRDM-KL25 board as a USB HOST interfacing with a Numeric Keyboard and a 16x2 LCD. The project is compiled in the CodeWarrior IDE using Processor Expert and the Components to support the USB module of the USB Stack 4.1.1. How to add the Processor Expert USB components. The instructions to install the USB components to use them with Processor Expert are in the documentation of the USB Stack 4.1.1; here you can see the steps as well: Download the USB Stack 4.1.1 from the Freescale’s Website (USB Stack 4.1.1) Run the .exe file and install it in the default location. Open CodeWarrior and select Import Components in the Processor Expert button in menu bar. An Open windows will pop up, there you need to go to the path: <install folder>\Freescale USB Stack v4.1.1\ProcessorExpert\Components. To have the complete components and support for the USB module add each PEupd file repeating this step. Close CodeWarrior and open it again to ensure correct installation of the components. Check that the new components are available in the Components Library. About this Project. This project is based in the example code for Processor Expert in the USB Stack 4.1.1 USB_HID_MOUSE_HOST_MKL25Z128_PEx which implements the use of the FRDM-BOARD KL25 and a HID Mouse Device to interface with. In this project the HID Device is a Numeric Keyboard and the HOST Device (FRDM-KL25) is handling the data and printing them in a 16x2 LCD used in 8 bits mode (The LCDHTA component used here was created by Erich Styger; find the component an all the information about it here: http://mcuoneclipse.com/2012/12/22/hd44780-2x16-character-display-for-kinetis-and-freedom-board/ and say Thank you Erich: “Thank you Erich”). Here you can find a video of the implementation of this application: HID HOST WITH FRDM-KL25 The hardware components are: FRMD-KL25 Rev.E Adafruit Prototype Shield v.5 LCD JHD-162A Numeric USB Keyboard (Product Name: Numpad i110, Model No. GK-100010) USB _host Inside the project you can see there is a folder called USB_Host an it contains two important folders with source files: App_keyboard: Contains the specific function for the Keyboard configuration: in use, attached detached, callbacks and more; contain how to handle the data coming from the device. The function process_kdb_buffer is where the data is transmitted to the LCD and use it for the application. Classes: contain the necessary function to handle a hid as the device. Handle all the functions necessary for the USB protocol. Note: The usb_classes.c and usb_classes.h files are generated by processor expert. I attach these two files as well to have a reference how these files must look like. This is because sometimes during the code generation process Processor Expert erases part of the code. I hope this project is useful for you. Best Regards, Adrian.
View full article
The document describes how to port yaffs2 file system for MQX. The detailed porting user guide can refer to the attached doc which use TWR-K70F120M as example. The reference code can be found in the attached source code package. Now, the yaffs2 for MQX can support NFC and non-NFC at the same time, the only difference is NAND driver. For NFC, you should use NFC driver and for non-NFC, you should use softnand driver. In yaffs2 porting package, include the files which should be modified in MQX release package. user_config.h should be placed at \config\platform name\ init_nandflash.c should be placed at \mqx\source\bsp\platform name\ \nandflash is the NAND driver, should be at \mqx\source\io\ \yaffs2 is the yaffs2 porting codes should be at the root directory of MQX release package softnand2K.c is the NAND driver for non-NFC(simulated by flexbus).
View full article
Abstract         Kinetis M series MCU is Freescale’s Metrology microcontrollers based on ARM Cortex M0+ cores. The SPI module of KM provides for full-duplex, synchronous, serial communication between the MCU and peripheral devices, it also has programmable 8 or 16 bit data transmission length, 64bit FIFO mode for data transfers, DMA transmit and receive features, single wire bidirectional mode, etc. This document is mainly use the KM34Z256VLQ7 SPI module realize the erase, program and read operation in external flash MX25L6404EM2I, it also gives sample code of the detail command external flash operation, and at last, print the testing code via UART. 1.SPI pin assignment and basic code (1) SPI pin assignment SPI signal Pin name Description SPI_SS PTD1 Slave select SPI_SCK PTD2 SPI serial clock SPI_MOSI PTD3 Master data out, slave data in SPI_MISO PTD4 Master data in, slave data out External flash MX25L6404EM2I circuit: (2) SPI initialization   SPI initialization configuration the SPI pin, SPI module baud, master or slave mode, module enable, etc. the code just as following: SIM_SCGC4 |= SIM_SCGC4_SPI0_MASK|SIM_SCGC4_SPI1_MASK;                             SIM_SCGC5 |= SIM_SCGC5_PORTD_MASK; void serial_flash_init(void) {     PORTD_PCR1 &= ~PORT_PCR_MUX_MASK;            PORTD_PCR1 |= PORT_PCR_MUX(1) |0X03;                                           //Use PTD1 as SPI0_SS  // configure it as the GPIO     PORTD_PCR2 &= ~PORT_PCR_MUX_MASK;     PORTD_PCR2 |= PORT_PCR_MUX(3) |0X03;                                           //Use PTD2 as SPI0_SCK     PORTD_PCR3 &= ~PORT_PCR_MUX_MASK;     PORTD_PCR3 |= PORT_PCR_MUX(3) |0X03;                                           //Use PTD3 as SPI0_MOSI      PORTD_PCR4 &= ~PORT_PCR_MUX_MASK;     PORTD_PCR4 = PORT_PCR_MUX(3) |0X03;                                            //Use PTD4 as SPI0_MISO     GPIOD_PDDR |=  0X02; // SS pin output     GPIOD_PDOR |=  0X02; //  SS pin high     SPI0_C1 |= SPI_C1_MSTR_MASK; // SPI0 master mode                             SPI0_BR = 0x43;  //SPPR = 4, SPR = 3, bps div = (SPPR+1)*2^(SPR+1) = 80, baudrate= 24Mhz/80=300khz     SPI0_C1 |= SPI_C1_SSOE_MASK;                              SPI0_C1 &= (~SPI_C1_CPHA_MASK);  // clock polarity     SPI0_C1 &= (~SPI_C1_CPOL_MASK);  //clock phase     SPI0_C1 &= (~SPI_C1_LSBFE_MASK);  // LSB:most significant     SPI0_C1 &= (~SPI_C1_SPIE_MASK);                  //Disable RX interrrupt      SPI0_C1 &= (~SPI_C1_SPTIE_MASK);         //Disable the transmit interrupt     SPI0_C2 |= SPI_C2_MODFEN_MASK;             SPI0_C1 |= SPI_C1_SPE_MASK;  // enable SPI module } (3) One byte transfer code uint8 hal_spi_transfer_one_byte(uint8 v) {    int dummy =0;    char buff=0;    while ((SPI0_S & SPI_S_SPTEF_MASK) == 0)  // wait for transmit buffer empty    {                 dummy++;     }    dummy = SPI0_S;    SPI0_DL = v;   // send one byte to transmit buffer    while ((SPI0_S & SPI_S_SPRF_MASK) == 0); // wait ready buffer full    buff = SPI0_DL;  // read one received byte    return buff;         // return the received byte   } 3 Code realization for external flash operation command     At first, refer to the external flash program / erase flow, then I will give the according command code realization one by one. Take flash sector erase flow as an example, the according code is : void hal_spi_dev_flash_erase_sector(uint8 addr) { write_enable();      // WREN command spi_wait(WEL);     // RDSR command and wait WEL=1 hal_spi_transfe_start();    // enable CS pin , CS=0 hal_spi_transfer_one_byte(CMD_SECTOR_ERASE);   // erase one sector (4KByte)command hal_spi_transfer_one_byte(addr>>16);  // address hal_spi_transfer_one_byte(addr>>8); hal_spi_transfer_one_byte(addr>>0); hal_spi_transfe_stop();  // disable CS pin, CS=1 spi_wait(WIP);    // RDSR command and wait WIP=0;   } (1)Write enable (WREN) command : 0X06 static void write_enable(void) {     hal_spi_transfe_start();  // enable CS pin , CS=0     hal_spi_transfer_one_byte(CMD_WRITE_EN);  // Send WREN command     hal_spi_transfe_stop();  // disable CS pin, CS=1   } (2)Read status register (RDSR) sequence: 0X05 static void spi_wait(uint8 CMD) { if(CMD == WEL) while(get_sr()&0x02 != 0x02); // wait until WEL bit =1 else if(CMD == WIP) while(get_sr()&0x01 != 0x00); // wait until WIP bit =0 } static uint8 get_sr(void) {     uint8 v;     hal_spi_transfe_start(); // enable CS pin , CS=0     hal_spi_transfer_one_byte(CMD_GET_SR);  // Send RDSR command     v = hal_spi_transfer_one_byte(0x00); // read states register data     hal_spi_transfe_stop();    // disable CS pin, CS=1     return v;   } (3) Sector erase (SE) sequence: 0X20 hal_spi_transfe_start();    // enable CS pin , CS=0 hal_spi_transfer_one_byte(CMD_SECTOR_ERASE);   // erase one sector (4KByte)command hal_spi_transfer_one_byte(addr>>16);  // address hal_spi_transfer_one_byte(addr>>8); hal_spi_transfer_one_byte(addr>>0);   hal_spi_transfe_stop();  // disable CS pin, CS=1 (4) Page program (PP) sequence : 0x02 #define PAGE_SIZE 256       hal_spi_transfe_start();// enable CS pin , CS=0 hal_spi_transfer_one_byte(CMD_PROGRAM); //send flash program command hal_spi_transfer_one_byte(addr>>16); // flash page base address hal_spi_transfer_one_byte(addr>>8); hal_spi_transfer_one_byte(addr>>0); for(i=0;i<(PAGE_SIZE-1);i++) // send program data to the flash page hal_spi_transfer_one_byte(buf[i]); hal_spi_transfer_one_byte(buf[i]);   hal_spi_transfe_stop();// disable CS pin, CS=1 (5) Read at higher Speed(FAST_READ) Sequence: 0X0B void hal_spi_dev_flash_read_page(uint8 addr, char *buf) { int i; hal_spi_transfe_start();  // enable CS pin , CS=0 hal_spi_transfer_one_byte(CMD_READ); // read command hal_spi_transfer_one_byte(addr>>16);  // base address hal_spi_transfer_one_byte(addr>>8); hal_spi_transfer_one_byte(addr>>0); hal_spi_transfer_one_byte(0x00); // dummy byte for(i=0;i<(PAGE_SIZE-1);i++)    // read data back from the flash buf[i] = hal_spi_transfer_one_byte(0x00); buf[i] = hal_spi_transfer_one_byte(0x00); hal_spi_transfe_stop();  // disable CS pin, CS=1   } 4 Experimental result The test code function is to realize one sector (4KB) erasing, then read one page (256Byte) and print it out, after that, program one page , read and print it out to check the data. (1)The main function code is : static char buf[256]; int i; serial_flash_init();  // SPI initialization hal_spi_dev_flash_erase_sector(0); // erase one sector(4KByte) printf("reading page...\n"); hal_spi_dev_flash_read_page(0,buf); // read one page(256Byte) print_buf(buf,PAGE_SIZE);  // print the read data out printf("programing a page...\n"); for(i=0;i<256;i++) buf[i] = i;     // define the data which will write to the flash hal_spi_dev_flash_program_page(0,buf); // write 256BYTE to the flash page0 printf("clearing buffer..\n"); for(i=0;i<256;i++)    // clear buff buf[i] = 0; printf("reading page...\n"); hal_spi_dev_flash_read_page(0,buf); // read the page0 data out print_buf(buf,PAGE_SIZE);  // print the read data out   printf("demo end.\n"); (2) print test data reading page... 0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  0xFF,0xFF,0xFF,0xFF,  programing a page... clearing buffer.. reading page... 0x0,0x1,0x2,0x3,  0x4,0x5,0x6,0x7,  0x8,0x9,0xA,0xB,  0xC,0xD,0xE,0xF,  0x10,0x11,0x12,0x13,  0x14,0x15,0x16,0x17,  0x18,0x19,0x1A,0x1B,  0x1C,0x1D,0x1E,0x1F,  0x20,0x21,0x22,0x23,  0x24,0x25,0x26,0x27,  0x28,0x29,0x2A,0x2B,  0x2C,0x2D,0x2E,0x2F,  0x30,0x31,0x32,0x33,  0x34,0x35,0x36,0x37,  0x38,0x39,0x3A,0x3B,  0x3C,0x3D,0x3E,0x3F,  0x40,0x41,0x42,0x43,  0x44,0x45,0x46,0x47,  0x48,0x49,0x4A,0x4B,  0x4C,0x4D,0x4E,0x4F,  0x50,0x51,0x52,0x53,  0x54,0x55,0x56,0x57,  0x58,0x59,0x5A,0x5B,  0x5C,0x5D,0x5E,0x5F,  0x60,0x61,0x62,0x63,  0x64,0x65,0x66,0x67,  0x68,0x69,0x6A,0x6B,  0x6C,0x6D,0x6E,0x6F,  0x70,0x71,0x72,0x73,  0x74,0x75,0x76,0x77,  0x78,0x79,0x7A,0x7B,  0x7C,0x7D,0x7E,0x7F,  0x80,0x81,0x82,0x83,  0x84,0x85,0x86,0x87,  0x88,0x89,0x8A,0x8B,  0x8C,0x8D,0x8E,0x8F,  0x90,0x91,0x92,0x93,  0x94,0x95,0x96,0x97,  0x98,0x99,0x9A,0x9B,  0x9C,0x9D,0x9E,0x9F,  0xA0,0xA1,0xA2,0xA3,  0xA4,0xA5,0xA6,0xA7,  0xA8,0xA9,0xAA,0xAB,  0xAC,0xAD,0xAE,0xAF,  0xB0,0xB1,0xB2,0xB3,  0xB4,0xB5,0xB6,0xB7,  0xB8,0xB9,0xBA,0xBB,  0xBC,0xBD,0xBE,0xBF,  0xC0,0xC1,0xC2,0xC3,  0xC4,0xC5,0xC6,0xC7,  0xC8,0xC9,0xCA,0xCB,  0xCC,0xCD,0xCE,0xCF,  0xD0,0xD1,0xD2,0xD3,  0xD4,0xD5,0xD6,0xD7,  0xD8,0xD9,0xDA,0xDB,  0xDC,0xDD,0xDE,0xDF,  0xE0,0xE1,0xE2,0xE3,  0xE4,0xE5,0xE6,0xE7,  0xE8,0xE9,0xEA,0xEB,  0xEC,0xED,0xEE,0xEF,  0xF0,0xF1,0xF2,0xF3,  0xF4,0xF5,0xF6,0xF7,  0xF8,0xF9,0xFA,0xFB,  0xFC,0xFD,0xFE,0xFF,    demo end From the print data, we can find the code can realize flash sector erasing , flash program and flash data read out, and the test result is correct. The following wave is the page read data out after flash page program. The attachment is the testing code.
View full article