Kinetis微控制器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Kinetis Microcontrollers Knowledge Base

讨论

排序依据:
Hello Kinetis fans, This time I bring to you a document which explains what is and how to configure scatter/gather feature which is present in the Enhanced Direct Memory Access (eDMA). This document includes an example project for the Kinetis Design Studio (KDS) which works in the FRDM-K64F board but the configuration is the same for any MCU which includes the eDMA peripheral. If you are interested in the channel linking feature, please take a look into the document What is and how to configure the eDMA channel linking feature​. I hope you find this document useful. Best regards, Earl Orlando Ramírez-Sánchez Technical Support Engineer NXP Semiconductors
查看全文
for M68HC08, HCS08, ColdFire and Kinetis MCUs by: Pavel Lajsner, Pavel Krenek, Petr Gargulak Freescale Czech System Center Roznov p.R., Czech Republic The developer's serial bootloader offers to user easiest possible way how to update existing firmware on most of Freescale microcontrollers in-circuit. In-circuit programming is not intended to replace any of debuging and developing tool but it serves only as simple option of embedded system reprograming via serial asynchronous port or USB. The developer’s serial bootloader supported microcotrollers includes 8-bit families HC08, HCS08 and 32-bit families ColdFire, Kinetis. New Kinetis families include support for K series and L series. This application note is for embedded-software developers interested in alternative reprogramming tools. Because of its ability to modify MCU memory in-circuit, the serial bootloader is a utility that may be useful in developing applications. The developer’s serial bootloader is a complementary utility for either demo purposes or applications originally developed using MMDS and requiring minor modifications to be done in-circuit. The serial bootloader offers a zero-cost solution to applications already equipped with a serial interface and SCI pins available on a connector. This document also describes other programming techniques: FLASH reprogramming using ROM routines Simple software SCI Software for USB (HC08JW, HCS08JM and MCF51JM MCUs) Use of the internal clock generator PLL clock programming EEPROM programming (AS/AZ HC08 families) CRC protection of serial protocol option NOTE: QUICK LINKS The Master applications user guides: Section 10, Master applications user guides. The description of Kinetis version of protocol including the changes in user application: Section 7, FC Protocol, Version 5, Kinetis. The quick start guide how to modify the user Kinetis application to be ready for AN2295 bootloader: Section 7.8, Quick guide: How to prepare the user Kinetis application for AN2295 bootloader. Full application note and  software attached.
查看全文
The AOI and Crossbar modules are inregrated in DSC, Kinetics KV and i.mxrt families, user can use them to generate complicated trigger signal for the on-chip peripherals. The DOC discusses the AOI function, crossbar fuction based on KV58. It gives the example, the example demos how to implement AND operation of two signals via crossbar switch A and B and AOI modules. The two logic signals are connected to the pads of KV58, and routed to AOI inputs via Crossbar switch B, the AOI sub-module0 implements the AND operation of the two signals, and output the AND output signal Event0  to pad of KV58 via crossbar switch A. Connect input pads and output pad of KV58 to oscilloscope, from the waveform of the three signals on scope, we can see that the AND logic  is implemented.
查看全文
Project USB: Connecting USB to CAN with K20   In this project, the internal CAN Controller of the K20 is used to monitor the CAN bus. The connection to the PC is realized by the internal USB Controller. The USB stack is implemented as HID device especially for the K20.   The software runs on a self made hardware board. The connection to CAN is visualized with a Qt program, running on every Win7 PC.   Result: K20_CAN2USB.zip Original Attachment has been moved to: K20_CAN2USB.zip
查看全文
This is an example for the Kinetis KE02Z devices, showing how to program the EEPROM with initial values when the flash is programmed.  The example works on the FRDM-KE02Z40M board, and was written with Kinetis Design Studio (KDS) v3.0.0.  The example also uses Processor Expert (PEx) to configure the UART and erase/program the EEPROM.  The EEPROM programming works with the P&E Micro Multilink Universal debugger, as well as the P&E Micro OpenSDA debugger app for the FRDM-KE02Z40M board. To program the EEPROM with initial values, the application declares constants for the EEPROM locations, and initializes these in the source code in eeprom.c. Compiler pragmas/attributes are used to force the linker to place these constants in EEPROM, using the m_eeprom memory section defined in the linker command file \Project_Settings\Linker_Files\ProcessorExpert.ld.  The P&E Micro flash programming algorithms initialize the EEPROM in 4Byte words. Therefore, any initialized EEPROM locations should be in aligned 4Byte words. This example initializes the first 4Bytes in the EEPROM as 0, 64, 128, 192. The example uses a terminal program to display EEPROM information.  It connects to the OpenSDA COM port on the FRDM-KE02Z40M board using UART1 from the KE02Z. The terminal settings are:   Baud Rate: 38,400   Data: 8bit   Parity: None   Stop: 1bit   Flow Control: None The example prints 5 bytes of EEPROM to the terminal after reset: the 4 initialized bytes, plus the following EEPROM byte which was not initialized. Then the example increments the first byte, and decrements the second byte, and writes the new values back to EEPROM.  The other 3 bytes are not changed. Then the application prints the new EEPROM values of all 5 bytes.  Everytime the MCU is reset, it will print the existing EEPROM data and then the changed data.  Below is the example output from the terminal after initially programming the KE02Z, and then doing a single reset: Terminal output:   KE02Z EEPROM example   EEPROM values after reset = 0 64 128 192 255   EEPROM values after updating = 1 63 128 192 255   KE02Z EEPROM example   EEPROM values after reset = 1 63 128 192 255   EEPROM values after updating = 2 62 128 192 255
查看全文
  MCU Bootloader2.0.0 enables quick and easy programming of Kinetis MCUs through the entire product life cycle, including application development, final product manufacturing, and beyond. It supports many kinds of peripherals, include UART, I2C, SPI, USB, CAN and so on. Among these peripherals, UART is most common used. In reference manual, it only says that feature can be turned on or off by using #define statement in bootloader_config.h. In fact, you can use UART0 by default. But if you want to use other UART port, change TERM_PORT_NUM to other value is useless. If you traced this value, you’ll find it is not used at all, nor the TERMINAL_BAUD. Here we use FRDM-KV31F512 as the example. We want to download image by UART2. First, we should modify peripherals_pinmux.h. #define BL_ENABLE_PINMUX_UART2 (BL_CONFIG_SCUART)     //line 38   //! UART pinmux configurations #define UART2_RX_PORT_BASE PORTE #define UART2_RX_GPIO_BASE PTE #define UART2_RX_GPIO_PIN_NUM 17               // PIN 16 in the PTB group #define UART2_RX_FUNC_ALT_MODE kPORT_MuxAlt3   // ALT mode for UART0 RX #define UART2_RX_GPIO_ALT_MODE kPORT_MuxAsGpio // ALT mode for GPIO functionality #define UART2_RX_GPIO_IRQn PORTE_IRQn #define UART2_RX_GPIO_IRQHandler PORTE_IRQHandler #define UART2_TX_PORT_BASE PORTE #define UART2_TX_GPIO_PIN_NUM 16             // PIN 17 in the PTB group #define UART2_TX_FUNC_ALT_MODE kPORT_MuxAlt3 // ALT mode for UART0 TX   The original define is UART0, here we change it to UART2. It is strongly recommended to do so. Otherwise you’ll find that UART can’t work at all. Another comment here is PTE16 and PTE17 is conflict with SPI. You must disable SPI or change SPI function to other pins.   Next we must modify peripherals_KV31F512.h. const peripheral_descriptor_t g_peripherals[] = { #if BL_CONFIG_SCUART    // UART0    {.typeMask = kPeripheralType_UART,      .instance = 2, // change this value from 0 to 2      .pinmuxConfig = uart_pinmux_config,      .controlInterface = &g_scuartControlInterface,      .byteInterface = &g_scuartByteInterface,      .packetInterface = &g_framingPacketInterface },   Although there is a baud rate definition TERMINAL_BAUD, but it is never used too. MCU bootloader2.0.0 use auto baud rate detection. When power on, bootloader will go to autobaud detection mode. KinetisFlashTool sends ‘0x ’ every second. Bootloader check this byte and calculate baud rate.   After getting this value, bootloader will change to normal communication mode. Baud rate will not change until reset. If blhost is used, subsequent blhost invocations must specify the same baud rate as was used for the initial invocation unless the bootloader is reset. If the baud rate is not specified using the -p COMx, <baudrate> option, the UART baud rate will be set to 57600. Since Kinetis MCU UART module don’t have auto frequency detect function, the bootloader detects frequcny by software. It uses GPIO interrupt and timer to measure frequency. But in bootloader, there is only code for UART0, there isn’t code for other UART port. We must add the code. In hardware_init_KV31F512.c, modify the function get_uart_clock()   uint32_t get_uart_clock(uint32_t instance) {    switch (instance)    {        case 0:        case 1:            // UART0 and UART1 always use the system clock            return SystemCoreClock;        case 2:            return get_bus_clock();        default:            return 0;    } }   KV31 has 4 UART, include three UART modules and one low-power UART. They have different clock source. UART0 and UART1 use System clock while UART2 and LPUART0 use Bus clock. Thus, we finished the work. UART2 can work as the download port now.
查看全文
       FreeRTOS is a high quality, risk free, supported, free RTOS, and now it is already successful to porting more 35 architectures. As a popular RTOS, more and more embedded engineers considering it for their next project.        Next, I’m going to show you the steps of creating a MAPS-K22 FreeRTOS demo by IAR and I’ve also attached a template demo and FreeRTOS source code (Fig 1). Fig 1 FreeRTOS source code directories and files     1. Copy the FreeRTOS source code to ~\MAPSK22_SC\Libraries     2. Create FreeRTOS_Source group in the workspace, then add the source code (Fig 2) Fig 2 3. Add an application code in the main.c This is a very simple configuration. It creates two tasks, one software timer, and also uses a button interrupt. The two tasks communicate via a queue. The receiving task toggles the LED3 each time a value is received. Pressing user button K5 generates an interrupt. The interrupt service routine for which resets a software timer, then turn the LED1 on. The software timer has a five second period. The timer will expire when K5 has not been pressed again for a full five seconds. The callback function that executes when the timer expires simply turn the LED1 on again. Therefore, pressing K5 will turn the LED1 on, and the LED1 will remain on until a full five seconds pass without the button being pressed again. 4. Modify the Include Directories 5. Run the FreeRTOS demo After build the modified application code, then run it on MAPS-K22 board (Fig 3) Fig 3 IMPORTANT! Cortex-M FreeRTOS port specific configuration Configuration items specific to this demo are contained in ~\MAPSK22_SC\Libraries\RTOS\config\K22F51212\iar. The constants defined in this file can be edited to suit your application. In particular configTICK_RATE_HZ This sets the frequency of the RTOS tick interrupt. The supplied value of 1000Hz is useful for testing the RTOS kernel functionality but is faster than most applications require. Lowering this value will improve efficiency. configKERNEL_INTERRUPT_PRIORITY and configMAX_SYSCALL_INTERRUPT_PRIORITY See the RTOS kernel configuration documentation for full information on these configuration constants. configLIBRARY_LOWEST_INTERRUPT_PRIORITY and configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITY These are equivalents to configKERNEL_INTERRUPT_PRIORITY and configMAX_SYSCALL_INTERRUPT_PRIORITY, but presented in a form suitable for passing into the Freescale NVIC_SetPriority() library function. The NVIC_SetPriority() function expects priorities to be in the range of 0 to 15 - 0 being the highest priority and 15 being the lowest priority.
查看全文
Introduction Even with the prevalence of universal asynchronous receiver/transmitter (UART) peripherals on microcontrollers (MCUs), bit banged UART algorithms are still used.  The reasons for this vary from application to application.  Sometimes it is simply because more UARTs are needed than the selected device provides.  Maybe application or layout restrictions require certain pins to be used for the UART functions but the device does not route UART pins to the required package pins.  Maybe the application requires a non-standard or proprietary UART scheme. Whatever the reason, there are applications where a bit banged UART is used and is typically a pure software implementation (a timer is used and the MCU core controls a GPIO pin directly).  A better alternative may be to use Flextimer (FTM) or Timer/PWM Module (TPM) to take advantage of the features of these peripherals and possibly offload the CPU.  This document will explain and provide a sample application of how to emulate a UART using the FTM or TPM peripheral.  A Kinetis SDK example (for the TWR-K22F120M and FRDM-K22F platforms) and a baremetal legacy code example (for the FRDM-KL26Z) are provided here. UART protocol Before creating an application to emulate a UART, the UART protocol and encoding must be understood. The UART protocol is an asynchronous protocol that typically includes a start bit, payload (of 7-10 data bits), and a stop bit but does allow for many variations on the number of stop bits and what/how to transfer the data.  For this document and application example, the focus will be UART transmission that follows 1 start bit, 8 data bits, 1 stop bit, no parity, and no flow control.  The data will be transmitted least significant bit (LSB) first.  The following image is a block diagram of this transmission. However, this doesn't specify what the transmission looks like electrically. The figure below shows a screenshot of an oscilloscope capture of a UART transmission.  The data transmitted is 0x55 or a "U" in the ASCII representation. Notice that the transmission line is initially a logic high, and then transitions low to signal the start of the transmission.  The transmission line must stay low for one bit width for the receiver to detect it.  Then there are 8 data bits, followed by 1 stop bit.  In the case shown above, the data bits are 0x55 or 0b0101_0101.  Remember that the transmissions are sent LSB first, so the screenshot shows 1-0-1-0-1-0-1-0.  The last transition high marks the beginning of the stop bit and the line remains in that state until the start of the next transmission.  The receiver, being asynchronous, does not require any type of identifying transition to mark the end of the stop bit. FTM/TPM configuration The first question many may ask when beginning a project like this is "How do I configure the FTM/TPM when emulating a UART".  The answer to this depends on the aspect of this problem you are trying to solve.  Transmitting and receiving characters require two different configurations.  Transmission requires a configuration that manipulates the output pin at specific points in time.  Receiving characters requires a configuration that samples the receive pin and measures the time between pin transitions.  The FTM and TPM have the modes listed in the following table: The FTM and TPM have four different modes that manipulate an output:  Output compare (no pulse), Output compare (with pulse), Edge-aligned PWM, and Center-aligned PWM.  Neither PWM mode is ideal for the requirements of the application.  This is because the PWM modes are designed to produce a continuous waveform and are always going to return to the initialized state once during the cycle of the waveform.  However, the UART protocol may have continuous 1's or 0's in the data without pin transitions between them. The output compare mode (high-true or low-true pulse modes) is designed to only manipulate the pin once, and only produces pulses that are one FTM/TPM clock cycle in duration.  So this is obviously not desirable for the application.  The output compare mode (Set/Clear/Toggle on match) is promising.  This mode manipulates the output pin every cycle.  There are three different options:  clear output on match, set output on match, and toggle output on match.  Neither "clear output on match" nor "set output on match" are ideal as either would require configuration changes during the transmission of a character.  The "toggle output on match", however, can be used and is the selected configuration mode for this sample application. To receive characters, there is only one mode that is intuitive:  "the input capture mode".  This mode records the timer count value on an edge transition of the selected input pin.  Similar to the output compare mode chosen for the transmit functionality, the input capture mode has three sub-modes:  capture on rising edge, capture of falling edge, and capture on either edge.  It is clear from the descriptions that capture on either edge should be selected. Transmit encoding The selection of the FTM/TPM mode is moderately intuitive, but using this mode to emulate a UART transmission is not.  There are two issues that make this a little tricky. 1) The output pin is initialized low. However, the UART protocol needs the pin to begin in a logical high state. 2) The pin transitions on every cycle provided the channel value is less than the value of the MOD register. Due to continuous strings of 1's or 0's, it is necessary to have periods where the pin does not transition. Both of these points have workarounds. Output pin initialization For the first issue, the channel interrupt is first enabled and the channel value register is loaded with a value much less than the value in the MOD register.  Then in the channel interrupt service routine, the pin is sampled to ensure that it is in the logic high state and the channel interrupt is disabled (and will not be re-enabled throughout the life of the application).  The code for this interrupt service routine is as follows. Output pin control For the second issue, a method of not transitioning the pin value while allowing the timer to continue counting normally is necessary.  The Output Compare mode uses the channel value register to determine when the pin transition occurs.  If a value greater than MOD is written to the channel value register, the channel value will never match the count register and thus, a pin transition will never occur.  So, when a series of continuous 1's or 0's need to be transmitted, a value greater than the value in the MOD register can be written to the channel value register to keep the output pin in its current state. However, when a value greater than MOD is written to the channel value register, no channel match will occur (which means channel interrupts will not occur).  So the timer overflow interrupt must be used to continue writing values.  This requires the updates to be output pin to be planned ahead of time and makes the transmission algorithm a little tricky.  The following diagram displays when which values should be written to the channel value register at which points in time to generate the appropriate pulses. Writing a function to translate a number into the appropriate series of MOD/2 and MOD+1 values can be a little tricky. To do this, we must first notice that MOD/2 needs to be written when changes on the transmission pin are need and MOD+1 needs to be written when pin transmissions are not desired.   So, what logical function can we use to determine when a change has happened?  XOR is the correct answer.  So what two values need to be XOR'd together?  One value is obviously the value that we want to send.  But what is the second value?  It turns out that the second value is a shifted version of the value that we want to send.  Specifically, the second value is the desired value to send shifted to the left by one.  (You can think of it as sort of a "future" value of the desired value).  The following pictures show how to determine the queue to use for the transmission. Receive decoding The receive functionality has an advantage over the transmit functions in that it is possible to use DMA for the reception of characters.  This is because the receive function takes advantage of the input capture functionality of the FTM / TPM and therefore can use the channel match interrupt.  The example application provided with this document implements a DMA method and a non-DMA method for reception. First, the non-DMA method will be discussed. Before discussing the specifics of gathering the input pulse widths, some details of the receive pin need to be discussed. Detecting the start bit The receive pin needs to be able to determine when the start of the packet transmission begins.  To do this, the receive pin is configured as an FTM / TPM pin. At the same time, the GPIO interrupt functionality is configured on the same pin for a falling edge interrupt.  The GPIO interrupt capabilities are enabled in any digital mode, so the GPIO interrupt will still be able to be routed to the Nested Vector Interrupt Controller (NVIC).  The pin interrupt is used to start the FTM / TPM clock when a new character reception begins. In the GPIO interrupt for this pin, the FTM / TPM counter register is reset and the clock to the FTM / TPM is turned on.  The code for the GPIO interrupt service routine is shown below.  Receiving characters without DMA Now, when receiving characters and not using DMA, the first thing to understand is that the Interrupt Service Routine (ISR) will be used and it will mainly be used to record the captured count values.  The interrupt service routine also tracks the current receive character length and resets the counter register.  This is so that the values in the receive queue reflect the time since the last pin transition.  The interrupt function for the non-DMA application is shown below. Notice that the first two actions in the ISR are resetting the count register, and clearing the channel event interrupt flag.  Then the channel value is stored in the receive pulse width array (this is simply an array that holds the receive pulse widths of the current character being received).  Next, recvQueueLength, the variable which holds the current length of the character being received, is updated to reflect the latest character length.  The next step is to determine if the full character has been received.  This is determined by comparing recvQueueLength to the RECV_QUEUE_THRESH, which is the threshold as determined by multiplying the number of expected bits by the expected bit width plus another bit width (for the start bit).  If the recvQueueLength is greater than the RECV_QUEUE_THRESH, then a semaphore is set, recvdChar, to indicate that a full character has been received.  The FTM / TPM clock is turned off, and the pin interrupt functionality of the receive pin is enabled.  The final step in the interrupt routine is to increment the receive queue index, recvQueueIndex.  This variable points to the current entry in the receive queue array. Using DMA to receive characters When using DMA, the receive FTM / TPM interrupt is much different. The interrupt routine simply needs to clear the channel interrupt flag, stop the FTM / TPM timer, disable the DMA channel, and set the received character semaphore.  The character is then decoded outside of the interrupt routine.  The interrupt function when using DMA is shown below: Decoding the received pulse widths Once the array of pulse widths has been populated, the received character needs to be translated into a single number.  This varies slightly when using DMA and when not using DMA. However, the basic principle is the same.  The number of bits in a single entry is determined by dividing by the expected bit width and this is translated into a temporary array that contains 1's and 0's, and then that is used to shift in the appropriate number of 1's and 0's into the returned char variable.  A temporary array is needed because the values are shifted into the UART LSB first, so the bit must be physically flipped from the first entry to the last.  There is no logical operation that will do this automatically. The algorithm to perform this translation is shown below.  In this algorithm, note that recvPulseWidth is the array that contains the raw count value of the pulse width.  The array tempRxChar holds the decoded character in reverse order and rxChar is a char variable that holds the received character. Conclusion This document provides an overview of the UART protocol and describes a method for creating a software UART using the timing features of the FTM or TPM peripheral.  This method allows for accurate timing and while not relying entirely on the CPU and the latency associated with the interrupt and the GPIO pins.  The receive function is open to further optimization by using DMA, which can provide further unloading of the CPU.
查看全文
For Remote Control means, that is needed two computers - Server Computer and User Computer, which will be in connection. There are two types of connection, which can be used - HTTP or DCOM. There are two different ways how to set up the remote control in Windows. I made the tutorial, which describes both types of Remote Control. Ok - so, let´s start! HTTP Settings On the Server Computer side: 1. Plug the board to the Server Computer 2. Go to Remote Communication Server 3. Set HTTP connection and choose the right COM Port according the plugged board If the plugged board is on e.g. COM23, it is possible to edit number of Port in Device Manager On the User PC side: 1. Open FreeMASTER,  go to Project -> Options 2. Choose Plug-in Module: FreeMASTER CommPlugin for Remote Server (HTTP) and type the IP address of the server, do not forget join to IP address :8080 3. And start communication by STOP button to successful connection DCOM Settings On the Server Computer side: 1. Plug board to the Server Computer 2. Launch DCOM in FreeMASTER Remote Server Choose COM according plugged board or edit COM according to step 2 - Server Computer in HTTP Connection (up). 3. Setting permissions for the user, User PC. Right click on Computer -> Manage. In Computer Management click to Distributed COM Users. In Distributed COM Users Properties add the user, User Computer. After that, set the permissions in Component Services. In cmd type dcomcnfg.exe In Component Services go to Computers -> My Computer -> DCOM Config -> MCB FreeMASTER Remote Server Application Right click on MCB FreeMASTER Remote Server Application and go to Properties. In Security Tab is possible to add the permissions. There are 3 types of permissions. First permission - Launch and Activation Permissions. There are 4 permission options. Local Launch and Remote Launch means, that user, User Computer can launch e.g. FM Remote Server Application. But for success communication is needed allowing Local Activation and Remote Activation. Second permission - Access Permissions. Click to Edit and Allow Local Access and Remote Access for the user. Do not forget that if there is a change of permissions, specifically allowing, it is necessary for User to log out and log in. On the User Computer side: 1. Open Freemaster, go to Project -> Options 2. Choose Plug-in Module: FreeMASTER CommPlugin for Remote Server (DCOM) and for filling Connect string is possible to use Configure. Definitely, type the IP address of the server and ;Port Name. 3. And start communication by STOP button in FreeMASTER to successful connection And now.. you can do anything 🙂
查看全文
The attached zip file contains software that accompanies the document UART Emulation Using the FTM or TPM.  It contains two sample applications:  one that uses the TPM, and one that uses the FTM. The TPM example targets the FRDM-KL26Z development board and is written in baremetal code.  The FTM example targets the TWR-K22F120M and FRDM-K22F and is written using the Kinetis SDK 1.0 release.  Installation instructions are contained within the zip package. Unzip the package to an empty folder and then copy the appropriate folders to the the appropriate locations on your PC per the instructions located in the zip file. 
查看全文
The SysTick is a part of the Cortex-M0+ core and so is not chip specific - for details of the Cortex core you generally need to use ARM documents. For SysTick: http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.dai0179b/ar01s02s08.html By summary, the SysTick is configured through four registers: 1. SysTick Control and Status(CSR): basic control of SysTick e.g. enable, clock source, interrupt or poll COUNTFLAG: count-down flag, if down to 0, then this bit will be set to 1, otherwise, it will be 0. CLKSOURCE:  when using internal core clock, it will be 1. If using external clock, it will be 0. TICKINT: interrupt enabled when setting to 1. ENABLE: counter enabled when setting to 1. 2. SysTick Reload Value(RVR): value to load Current Value register when 0 is reached. 3. SysTick Current Value (CVR): the current value of the count down. 4.SysTick Calibration Value(CALIB): contain the number of ticks to generate a 10ms interval and other information, depending on the implementation. TENMS: tick value for 10 ms. To configure the SysTick you need to load the SysTick Reload Value register with the interval required between SysTick events. The timer interrupt or COUNTFLAG bit is activated on the transition from 1 to 0, therefore it activates every n+1 clock ticks. If a period of 100 is required 99 should be written to the SysTick Reload Value register. See attached code on how to generate microsecond delay.
查看全文
在KE系列MCU中提供了多种寄存器用于实现GPIO的控制:    -PDOR寄存器,用于写入或读取IO的输出状态    -PSOR寄存器,用于置位IO口    -PCOR寄存器,用于清零IO口    -PTOR寄存器,用于翻转IO口    -PDIR寄存器,用于读取IO口的输入状态 当我们想要将PTA0置1时,有多种方法可以选择:    1. 直接操作寄存器,PDOR或PSOR都可以实现:          GPIOA->PDOR |= 0x0001;          GPIOA->PSOR |= 0x0001;          直接操作寄存器的效率更高,但可读性较差。    2. 使用官方的库函数操作       GPIO_PinSet(GPIOA, GPIO_PTA0);       库函数的可读性很好,但显得有些啰嗦,字符较多。 通过KE的BME来实现GPIO的操作能够很好的解决上面的问题,只用将附件中的头文件gpio_bitdef.h包含到工程里,再调用里边的宏定义就可以了。 对PTA0置位和清零可以使用下面的语句: POUTA0 = -1; POUTA0 = 0; 读取PTA0的输入状态则可以使用: tmp = PINA0; 上面的语句是不是看上去简洁了很多呢。 实际上上面GPIO的读写指令,是通过BME的BFI(位域插入)和BFX(位域提取)指令来实现的。 -其中ADDR是存储空间内的地址,我们最终操作的还是GPIO的寄存器,因此在两个指令中分别取GPIOA的PDOR寄存器地址和PDIR寄存器地址。 -bit则表示需要插入或提取位域的起始位置,由于这里是PTA0,PTA0位于寄存器的最低位,因此这里填入了0。 -width则表示需要插入或提取位域的宽度,我们只对单个管脚进行操作,也就是单个位进行操作,宽度自然就是1了。 需要注意的是,BFI(位域插入)指令在插入时,是将对应位插入到目的地址。因此,如果直接为POUTxx赋值为1的话,有可能出现错误。 POUTA0 = 0x01;//正确 POUTA1 = 0x02;//正确 POUTA2 = 0x04;//正确 POUTA1 = 0x01;//错误 为了避免这种情况,我们可以在IO口需要置位时,直接将POUTxx赋值为-1,即0xFFFF FFFF,这样保证了每一位的值都为1。 #define BME_BFI(ADDR,bit,width)        (*(volatile uint32_t *)((((uint32_t)ADDR&0xFFFF))   \                                   | (5 <<28)  \                                   | ((bit)<<23) | ((width-1))<<19)) #define BME_BFX(ADDR,bit,width)        (*(volatile uint32_t *)(((uint32_t)ADDR&0xFFFF)    \                                   | (5 <<28)  \                                   | ((bit)<<23) | ((width-1))<<19))  #define POUTA0 BME_BFI(&GPIOA->PDOR,0,1) #define PINA0 BME_BFX(&GPIOA->PDIR,0,1) ‍‍‍‍‍‍‍‍‍‍
查看全文
浙江地区去年下半年开始到现在,在一些电机控制客户中推广KE02,主要是低功率风机,BLDC,交流异步电机等。 总结了一些KE02在做电机控制方面的不足。 增加一点: (1) KE02 FTM PWM输出与NMI Pin 复用,上电容易烧管子
查看全文
http://dorkbotpdx.org/blog/paul/teensy_audio_library_gets_spdif_support Digital optical audio output from kinetis based teensy 3.1
查看全文
New 32-bit MCUs designed to transform consumer and industrial applications currently using legacy 8- and 16-bit architectures SAN ANTONIO, Jun 19, 2012 (BUSINESS WIRE) -- Freescale Semiconductor FSL +0.80% is now offering alpha samples of its Kinetis L series, the industry's first microcontrollers (MCUs) built on the  ARM(R) Cortex(TM)-M0+ processor. Kinetis L series devices are on display this week at the Freescale        Technology Forum (FTF) Americas and were demonstrated during the event's opening keynote address. As machine-to-machine communication expands and network connectivity  becomes ubiquitous, many of today's standalone, entry-level applications will require more intelligence and functionality. With the Kinetis  L series , Freescale provides the ideal opportunity for users of legacy 8- and 16-bit architectures to migrate to 32-bit platforms and bring additional intelligence to everyday devices without increasing power  consumption and cost or sacrificing space. Applications, such as small  appliances, gaming accessories, portable medical systems, audio systems, smart meters, lighting and power control, can now leverage 32-bit capabilities and the scalability needed to expand future product lines -- all at 8- and 16-bit price and power consumption levels. "In our view, 8- and 16-bit development has reached the end of the road. Those architectures simply can't keep up as the Internet of Things gains traction," said Geoff Lees, vice president and general manager of Freescale's Industrial & Multi-Market MCU business. "Kinetis L series MCUs are ideal for the new wave of connected applications, combining the required energy efficiency, low price, development ease and small  footprint with the enhanced performance, peripherals, enablement and scalability of the Kinetis 32-bit portfolio." Extreme energy efficiency The ARM Cortex-M0+ processor consumes approximately one-third of the energy of any 8- or 16-bit processor available today, while delivering  between two to 40 times more performance. The Kinetis L series supplements the energy efficiency of the core with the latest in  low-power MCU platform design, operating modes and energy-saving peripherals. The result is an MCU that consumes just 50 uA/MHz* in very-low-power run (VLPR) mode and can rapidly wake from a reduced power state, process data and return to sleep, extending application battery life. These advantages are demonstrated in the FTF demo, which compares the energy-efficiency characteristics of the Kinetis L series against solutions from Freescale competitors in a CoreMark benchmark analysis.        The Kinetis L series is also part of the Freescale Energy-Efficient Solutions program. Kinetis L series energy-saving peripherals do more with less power by maintaining functionality even when the MCU is in deep sleep modes. In traditional MCUs, the main clock and processor core must be activated to perform even trivial tasks such as sending or receiving data, capturing or generating waveforms or sampling analog signals. Kinetis L series peripherals are able to perform these functions without involving the core or main system, drastically reducing power consumption and improving battery life. Built using Freescale's innovative, award-winning flash memory technology, the Kinetis L series offers the industry's lowest-power flash memory implementation. This improves upon the conventional silicon-based charge storage approach by creating nano-scale silicon islands to store charge instead of using continuous film, improving the flash memory's immunity to typical sources of data loss. "The Internet of Things needs very low-cost, low-power processors that        can deliver good performance," said Tom R. Halfhill, a senior analyst        with The Linley Group and senior editor of Microprocessor Report. "As  the first 32-bit microcontrollers to use ARM's Cortex-M0+ processor core, Freescale's Kinetis L-series MCUs will bring the energy efficiency and prices typically associated with 8- and 16-bit MCUs to a broad range of consumer and industrial applications." Development simplicity The Kinetis L series addresses the ease-of-use requirement critical for entry-level developers through innovations including: -- The Freescale Freedom development platform, a small, low-power, cost-efficient evaluation and development system for quick application prototyping and demonstration. It combines an industry-standard form factor with a rich set of third-party expansion board options. An integrated USB debug interface offers an easy-to-use mass-storage device mode flash programmer, a virtual serial port and classic programming and run-control capabilities. -- Processor Expert software, a GUI-based, device-aware software generation tool that eliminates the need to write peripheral start-up code or device drivers. Helps developers easily migrate from 8- and 16-bit to 32-bit solutions by simplifying the software architecture and  dramatically reducing application development time. --  The Kinetis MCU Solution Advisor, a web-based application with an interactive MCU product selector that helps identify the best-suited MCU by applying dynamic filters based on operating characteristics, packaging options, memory configuration and peripheral hardware library. Integration and scalability Each Kinetis L series family includes scalable flash memory options, pin-counts and analog, communication, timing and control peripherals, providing easy migration paths for end product line expansion. Features common to the Kinetis L series families include: --         48 MHz ARM Cortex-M0+ core --         High-speed 12/16-bit analog-to-digital converters --         12-bit digital-to-analog converters --         High-speed analog comparators --         Low-power touch sensing with wake-up on touch from reduced power states --         Powerful timers for a broad range of applications including motor control The first three Kinetis L series families: --         Kinetis L0 family -- the entry point into the Kinetis L series. Includes eight to 32 KB of flash memory and ultra-small 4mm x 4mm QFN packages. Pin-compatible with the Freescale 8-bit S08P family. Software- and tool-compatible with all other Kinetis L series families. --         Kinetis L1 family -- with 32 to 256 KB of flash memory and  additional communications and analog peripheral options. Compatible with the Kinetis K10 family. --         Kinetis L2 family -- adds USB 2.0 full-speed host/device/OTG. Compatible with the Kinetis K20 family. The Kinetis L series is pin- and software-compatible with the Kinetis  K series (built on the ARM Cortex-M4 processor), providing a migration path to DSP performance and advanced feature integration. Availability and pricing Kinetis L series alpha samples are available now, with broad market sample and tool availability planned for Q3. Pricing starts at a suggested resale price of 49 cents (USD) in 10,000-unit quantities. The Freescale Freedom development platform is planned for Q3 availability at  a suggested resale price of $12.95 (USD). For more information about Kinetis L series MCUs, visit   www.freescale.com/Kinetis/Lseries    . *Typical current at 25C, 3V supply, for Very Low Power Run at 4MHz core  frequency, 1MHz bus frequency running code from flash with all peripherals off. About the Freescale Technology Forum Created to drive innovation and collaboration, the Freescale Technology Forum (FTF) has become one of the developer events of the year for the embedded systems industry. The Forum has drawn more than 48,000 attendees at FTF events worldwide since its inception in 2005. Our annual flagship event, FTF Americas, takes place June 18-21, 2012, in San Antonio, Texas. About Freescale Semiconductor Freescale Semiconductor  FSL +0.80% is a global leader in embedded processing solutions, providing industry leading products that are advancing the automotive, consumer, industrial and networking markets. From microprocessors and microcontrollers to sensors, analog integrated  circuits and connectivity -- our technologies are the foundation for the innovations that make our world greener, safer, healthier and more connected. Some of our key applications and end-markets include automotive safety, hybrid and all-electric vehicles, next generation wireless infrastructure, smart energy management, portable medical  devices, consumer appliances and smart mobile devices. The company is  based in Austin, Texas, and has design, research and development,        manufacturing and sales operations around the world.   www.freescale.com Freescale, the Freescale logo, Energy Efficient Solutions logo, Kinetis  and Processor Expert are trademarks of Freescale Semiconductor, Inc.,  Reg. U.S. Pat. & Tm. Off. ARM is the registered trademark of ARM  Limited. Cortex is the trademark of ARM Limited. All other product or  service names are the property of their respective owners. (C) 2012   Freescale Semiconductor, Inc. Photos/Multimedia Gallery Available:   http://www.businesswire.com/cgi-bin/mmg.cgi?eid=50313420&lang=en SOURCE: Freescale Semiconductor
查看全文
Heart rate monitors measure the heart rate during exercise or vigorous activity and gauge how hard the patient is working. Newer heart rate monitors consist of two main components: a signal acquisition sensor/transmitter and a receiver (wrist watch or smart phone). In some cases, the signal acquisition is integrated into fabric worn by the user or patient. MCUs analyze the ECG signal and determine the heat rate, while an 8-bit MCU can suffice for a simple heart rate monitor. For more complex analysis, such as heart rate variability, activity level and breathing rate, a high-end 32-bit MCU may be used. Furthermore, low power wireless technologies are used to allow the sensor to communicate to the receiver. Freescale offers 8-bit and 32-bit MCUs that are applicable across the entire spectrum of heart rate monitors. In addition, the Freescale portfolio includes inertial sensors or accelerometers for activity monitoring and ZigBee® and proprietary wireless solutions to enable communication between the sensors and the receiver. For more information go to freescale.com/APLHRM
查看全文
FINALISTAS Después de un profundo análisis de todos los proyectos, nuestros jueces realizaron la difícil selección de los finalistas del Kinetis L MCU Challenge México entre los que el público elegirá al ganador; gracias a la excelente respuesta decidimos nombrar 16 finalistas.  Ellos son: Project Name Contestan Name Description Video Sistema de monitoreo de la contaminación acústica #MonitoreoAcustico Lucio Canche Diseño de una placa para monitoreo de niveles de ruido utilizando un sensor de sonido. Permite el estudio detallado de los patrones de propagación del sonido. Movimiento de un carro controlado #CarroPelotasAntiestres Emilio Jiménez Auto de juguete controlado por medio de pulsaciones realizadas con 2 pelotas anti-estrés, el presionar una pelota hará que el vehículo avance hacia adelante y la otra hará que gire sobre su propio eje. Viking lever #VikingLever Ma. Fernanda Gutierrez Consiste en un sistema de una palanca con contrapeso; tendrá en la punta una pelota con una led que indicará cuando el usuario tiene que golpearla. Controlador para el suministro de agua de una vivienda #ControladorAgua Rogelio Rosales El objetivo es el ahorro de agua. En un tinaco se colocan 2 sensores, uno a nivel alto y el otro a nivel bajo de agua. Dependiendo del nivel del agua los sensores mandan la señal a la bomba para que se encienda o apague. Rehab glove #RehabGlove Alexis Castañón Guante que posee sensores de flexión en las articulaciones de los dedos y de fuerza en las yemas, con el fin de enviar instrucciones a algún aparato, mientras el usuario realiza ejercicios como cerrar el puño o tocar las yemas de los dedos con el pulgar. Tablet braile para invidentes #TabletBraille Andres Gafford Tableta para leer ebooks braile con botones para cambiar de página, apagar y encender, que sean fáciles de percatar por un invidente; así como botones interactivos que desplieguen opciones del menú. Tapete interactivo para discapacitados #TapeteInteractivo Angel Campoy Este tapete interactivo, contribuye al desarrollo motriz. El teclado cuenta con cuatro botones, los cuales tienen un led que se enciende indicando al paciente que debe presionar el boton. Si activo el boton indicado,se enciende un LED verde o rojo si se equivocó. Neck remote control wheel chair #NeckControl Francisco Javier Pérez Corona Silla de ruedas controlada moviendo el cuello a la izquierda o derecha, presionando un botón con la cabeza, que a su vez haga avanzar o girar. Control de sensores infrarrojos para silla de ruedas #SensoresSilla Jesús Lizárraga Silla de ruedas diseñado para personas con parálisis cerebral. El usuario debe colocar las dos manos al ifgual que los codos por encima de los espacios indicados, los sensores se activarán haciendo que la silla avance o gire hacia el lado en que la persona posicionó la mano. N-drid uleta #NdridRuleta Jorge Rodriguez Rodriguez Juego de ruleta de leds de 4 colores, el usuario acumulará puntos cada vez que logre presionar el botón del color en donde parará la ruleta. KMA #KMA Luis Castellanos Prototipo para silla de ruedas que será controlada con un dispositivo de fácil manejo,  comunicado a la silla por bluethooth. Sensilla #Sensilla Miguel Rogel Silla móvil manipulada por sensores y con esto lograr desplazarse de una manera más accesible a sus capacidades. Pest control using Freescale #PestControl Pablo Yerena Este proyecto consiste en el control de plagas de manera ecológica, con la implementación de un aparato electrónico que emite frecuencias ultrasónicas evitando que animales e insectos invadan espacios físicos. Tren de colores musical #TrenColores Ricardo Villaseñor Juguete donde se utiliza un sensor óptico para la lectura de pequeños cubos de colores, donde cada color es una nota musical. Al colocar el lector sobre el cubo de color se emitirá la nota correspondiente. Morse deaf-mute communication system #MorseDeafMute Roberto Vite Ruiz Dispositivo de escritura basado en el código morse. Se muestra un código morse para cada letra del alfabeto permitiendo a una persona sorda o muda darse a entender de manera escrita.       Casco acelerómetro #CascoAcelerometro José Ramón Rodriguez Dispositivo  para silla de ruedas que  permite al paciente transportarse autónomamente mediante una especie de casco que detecte la dirección deseada, además de que sea una manera recreativa de trasladarse Podrás participar calificando cada proyecto a través de redes sociales y la herramienta RankTab; la votación se abrirá el día del evento a partir de las 9:00am, espera las instrucciones a través de la Comunidad Freescale,  Facebook y durante el evento. A todos los finalistas los esperamos el 07 de Diciembre a las 8:00hrs en el Centro de Congresos del Tecnológico de Monterrey Campus Guadalajara, donde se develará el misterio y conoceremos al ganador del viaje al Freescale Technology Forum (FTF) en Dallas, Texas del 08 al 11 de Abril del 2014. Para solicitar mayor información, favor de enviar un correo a [email protected]
查看全文
Hi Team :      We are working on KSDK project recently . I would like to share an experience to migrate a project to a new device that is not listed in KSDK . I hope that helpful . Best regards, David
查看全文
    Curve22519 is a Montgomery elliptic-curve. Such as Apple HomeKit, most of network and IoT software use it in Diffie-Hellman algorithm for key exchanging.     On the Security Kinets MCU chip,if we use just the software algorithm (base on mbedTLS), Curve25519 will spend 180ms for calculation of the shared security.     It is faster than other 256bit elliptic-curve with software algorithm, Because of the shared security calculation will take more than 1200ms with a Weierstrass’s BP256R1curve when use software algorithm.     With LTC ECC HW acceleration, it take only 16ms to calculate the shared security on 256bit elliptic-curve. Whatever you do, the speed of hardware acceleration always faster than the software algorithm.     Now that we should also want to use the LTC to accelerate the Curve22519. The LTC, however, only supported Weierstrass form curve, but Curve22519 is a Montgomery curve…     Although, we can't use LTC in Curve22519 directly, we can use it by mapping it to a Weierstrass form to use it.  As below, we gave parameters of these curves, transform formulas, example code and test result to show how and why to do it. 1. Curve parameter:    Cuvre22519 in Montgomery form:    Y^2 = X^3 + A*X^2 + X    Fp = 0x7fffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffed    A= 486662    Gx = 9    Gy = 0x20ae19a1b8a086b4e01edd2c7748d14c923d4d7e6d7c61b229e9c5a27eced3d9    Order of G point  =  0x1000000000000000000000000000000014def9dea2f79cd65812631a5cf5d3ed      Cuvre22519 in Weierstrass form :    Y^2 = X^3 + a*X + b    Fp = 0x7fffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffed    a  =  0x2aaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaa984914a144L    b  =  0x7b425ed097b425ed097b425ed097b425ed097b425ed097b4260b5e9c7710c864L    Gx = 0x2aaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaad245a    Gy = 0x20ae19a1b8a086b4e01edd2c7748d14c923d4d7e6d7c61b229e9c5a27eced3d9    Order of G point  =  0x1000000000000000000000000000000014def9dea2f79cd65812631a5cf5d3ed    2. Calculation formula:   x_w –  x-coordinate value in  Weierstrass form   y_w –  y-coordinate value in  Weierstrass form   x_m - x-coordinate value in  Montgomory form   y_m -  we don’t care y-coordinate value in  Weierstrass mode   a_m – a coefficient of Montgomery equation (   Y^2 = X^3 + a_m * X^2 + X)   a_w – a coefficient of Weierstrass equation (   Y^2 = X^3 + a*X + b )   b_w – a coefficient of Weierstrass equation (   Y^2 = X^3 + a*X + b )     a)  x_w = (x_m + a_m/3)  %  p     b)  y_w ^2 = x_w ^ 3 + a_w*x_w + b_w c)   x_m = (x_w - a_m/3) % p You could reference these document as below: https://en.wikipedia.org/wiki/Curve25519 https://en.wikipedia.org/wiki/Montgomery_curve 3. example code: // public and private at Montgomery end #define M255_d      "0x7178DAC11D42AA5F39B10A62A8584DB0C8864564ADC9DF84EC0B13D9AEC220F8" #define M255_Qx     "0x3BA5048381744348D84E754B9944ABE080B37F7D4158DCE60CD79F66B98AB89E" // public and private at Weierstrass end #define WTS255_d    "0x09CC5CCF43C656C1309EE5A3491D5A8361607CEEB0C9B2B31A575E0FEF2B8835" #define WTS255_Qx   "0x3F4BDE110EE7AF71EF428D1018D188E35BAFB019F34F84E6465C5194B363DC2D" #define WTS255_Qy   "0x7540577CE6F920354E2A9D38CE88847D7447E66FA4D188AC75CB63C17210B718" #define WTS255_Qx_TO_M255_Qx     "0x14A13366643D04C74497E2656E26DE38B105056F48A4DA3B9BB1A6EA08B6B7DC" #define AM_INV3                  "0x2aaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaad2451" int ecdh_wts_curve_end( ) {     unsigned int ticks;     int ret = 0;     size_t blen = 0, blen_peer = 0;     ecdh_context ecdh;     ecdh_context ecdh_peer;   // to_wts255     ecdh_context ecdh_peer_m255;     mpi R;     mpi_init(&R);     ecdh_init( &ecdh);     ecdh_init( &ecdh_peer);     ecdh_init( &ecdh_peer_m255);     MPI_CHK(ecp_use_known_dp( &ecdh.grp, ECP_DP_WTS25519 ));     MPI_CHK(ecp_use_known_dp( &ecdh_peer.grp, ECP_DP_WTS25519 ));     MPI_CHK(ecp_use_known_dp( &ecdh_peer_m255.grp, ECP_DP_M255 ));     blen = set_hash_buff(/*TEST_ECP_GRP_ID*/ECP_DP_WTS25519, &secret_buf, ecp_name);     if(blen == 0) {         ret = -1;         goto cleanup;     }     mpi_read_string(&ecdh.d, 16,  WTS255_d);     mpi_read_string(&ecdh.Q.X, 16,  WTS255_Qx);     mpi_read_string(&ecdh.Q.Y, 16,  WTS255_Qy);     mpi_lset(&ecdh.Q.Z, 1);     mpi_read_string(&ecdh_peer_m255.d, 16, M255_d);     mpi_read_string(&ecdh_peer_m255.Q.X, 16, M255_Qx);     mpi_init(&ecdh_peer_m255.Q.Y);     mpi_lset(&ecdh_peer_m255.Q.Z, 1);     // map M255 point to WTS255 point     my_timer_start();     mpi_read_string(&R, 16, AM_INV3);         mpi_add_mpi(&ecdh_peer.Q.X, &ecdh_peer_m255.Q.X, &R);     mpi_mod_mpi(&ecdh_peer.Q.X, &ecdh_peer.Q.X, &ecdh_peer_m255.grp.P);        mpi_lset(&R, 3);     mpi_exp_mod (&ecdh_peer_m255.Q.Y , &ecdh_peer.Q.X, &R, &ecdh_peer_m255.grp.P, NULL);     mpi_mul_mpi(&R, &ecdh_peer.grp.A, &ecdh_peer.Q.X);     mpi_mod_mpi(&R, &R, &ecdh_peer.grp.P);          mpi_add_mpi(&ecdh_peer_m255.Q.Y, &ecdh_peer_m255.Q.Y, &R);     mpi_add_mpi(&ecdh_peer_m255.Q.Y, &ecdh_peer_m255.Q.Y, &ecdh_peer.grp.B);     mpi_mod_mpi(&ecdh_peer_m255.Q.Y, &ecdh_peer_m255.Q.Y, &ecdh_peer.grp.P);     mpi_mod_sqrt(&ecdh_peer.Q.Y, &ecdh_peer_m255.Q.Y, &ecdh_peer_m255.grp.P);     // z = 1     mpi_lset(&ecdh_peer.Q.Z, 1);     MPI_CHK(ecp_copy(&ecdh.Qp,  &ecdh_peer.Q));     MPI_CHK(ecdh_calc_secret_wts2mont( &ecdh, &blen, secret_buf, blen, myrand, NULL));     mpi_read_string(&R, 16, AM_INV3);         mpi_sub_mpi(&ecdh_peer_m255.Q.X, &ecdh.Q.X, &R);     mpi_mod_mpi(&ecdh_peer_m255.Q.X, &ecdh_peer_m255.Q.X, &ecdh_peer_m255.grp.P);     ticks = my_timer_stop();     // print out message     polarssl_printf("Weierstrass curve shared secutiy:\n");     mpi_printf_string( &ecdh.z, 16);     polarssl_printf("%s ecdh peer to peer: %lu ticks, %d ms (%d) \n", ecp_name , ticks, ticks / (CLOCK_SYS_GetPitFreq(0) / 1000),CLOCK_SYS_GetPitFreq(0) );     cleanup:     if( ret !=0 )         polarssl_printf( "%s test Unexpected error, return code = %08X\n", ecp_name, ret );     mpi_free(&R);     ecdh_free( &ecdh);     ecdh_free( &ecdh_peer);     ecdh_free( &ecdh_peer_m255);         return( 0 );    } int ecdh_mont_curve_end( ) {     int verbose = 1;     unsigned int ticks;     int ret = 0;     size_t blen = 0, blen_peer = 0;     ecdh_context ecdh;     ecp_point Q_peer;          // peer public point     ecdh_init( &ecdh);     ecp_point_init( &Q_peer);     MPI_CHK(ecp_use_known_dp( &ecdh.grp, ECP_DP_M255 ));     blen_peer = set_hash_buff(ECP_DP_M255, &secret_buf_peer, ecp_name);     if(blen_peer == 0) {         ret = -1;         goto cleanup;     }     mpi_read_string(&ecdh.d, 16,  M255_d);     mpi_read_string(&ecdh.Q.X, 16,  M255_Qx);     mpi_init(&ecdh.Q.Y);   // don't care Y, only init it     mpi_lset(&ecdh.Q.Z, 1);     mpi_read_string(&Q_peer.X, 16, WTS255_Qx_TO_M255_Qx);     mpi_init(&Q_peer.Y);     mpi_lset(&Q_peer.Z, 1);        MPI_CHK(ecp_copy(&ecdh.Qp,  &Q_peer));     my_timer_start();     MPI_CHK(ecdh_calc_secret( &ecdh, &blen_peer, secret_buf_peer, blen_peer, myrand, NULL));     ticks = my_timer_stop();     polarssl_printf("%s ecdh peer to peer: %lu ticks, %d ms (%d) \n", ecp_name , ticks, ticks / (CLOCK_SYS_GetPitFreq(0) / 1000),CLOCK_SYS_GetPitFreq(0) );     polarssl_printf("Montogemory curve shared secutiy:\n");     mpi_printf_string( &ecdh.z, 16);     polarssl_printf( "passed\n" );     cleanup:     if( ret !=0 && verbose != 0 )         polarssl_printf( "%s test Unexpected error, return code = %08X\n", ecp_name, ret );     ecdh_free( &ecdh);     ecp_point_free( &Q_peer);     if( verbose != 0 )         polarssl_printf( "\n" );         return( 0 );    } ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ 4. Test result: Test result of curv25519 in  Weierstrass form with LTC:     2. Test result of curve25519 in Montgomery form with software algorithm:      We could see that the shared security both in Weierstrass form with LTC and Montgomery form are “0x1454BDCD6A94D6336AA5A76F3CB40BBE12B65A2CDC9DA6B478948906638896D1”. But the calculation speed with LTC was ten times faster than other one.
查看全文
Intro to Cortex-M0+ main features presented by Alejandro Lozano, Freescale, TIC. Intro to Cortex M0+. Kinetis L series description. Introducción al Cortex-M0+. Principales características presentadas por Alejandro Lozano, Freescale TIC. Introducción al Cortex-M0+ Descripción de la familia Kinetis L.
查看全文