Kinetisマイクロコントローラ・ナレッジ・ベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis Microcontrollers Knowledge Base

ディスカッション

ソート順:
Latest version of the AN2295 universal bootloader includes support for IAR 7.6 IDE. - added support for Kinetis E MCUs - Kinetis K,L,M,E,W,V support
記事全体を表示
Background: NXP SC18IS602B I2C bus to SPI bridge chip is using TSSOP16 package, which is 16 leads; 0.65 mm pitch; 5 mm x 4.4 mm x 1.1 mm body. Customer requires to use a smaller package to emulate the SC18IS602B function. Kinetis L series MKL03Z16VFK4R product uses QFN24 package with 4 mm x 4 mm x 0.58 mm body. Demo Overview The I2C to SPI Bridge demo provides a replacement solution demo of SC18IS602B chip. The demo is based on FRDM-KL03Z board using I2C0 module as I2C slave and SPI0 module as SPI master. Provided data buffer size is 400bytes. The demo software is based on KSDK V2.0 for FRDM-KL03Z software. I2C slave interface: Pin number                 Function              FRDM-KL03Z jumper PTB3                          I2C0_SCL           J2-10 PTB4                          I2C0_SDA           J2-9   SPI master interface: Pin number                 Function              FRDM-KL03Z jumper PTA5                           SPI0_SS             J2_3 PTA6                           SPI0_MISO         J2_5 PTA7                           SPI0_MOSI         J2_4 PTB0                           SPI0_SCK           J2_6   INT pin (indicates if I2C to SPI Bridge allows i2c master start a new i2c transfer, low is active) Pin number                 Function              FRDM-KL03Z jumper PTB11                        GPIO output         J2_2   Connect I2C master with FRDM-KL03Z I2C slave interface and connect SPI slave with FRDM-KL03Z SPI master interface; Connect FRDM-KL03Z GND to I2C master and SPI slave before add power to those boards.  Below is the hardware platform connection way: I2C to SPI Bridge Demo Function For the KL03 chip with one SPI0_PCS0 chip select pin, I2C to SPI Bridge demo only supports function ID 0x01 as SPI write command. For example: if i2c master want to write 8bytes (0x21,0x22...0x28) to SPI slave, the i2c master needs to send below data to FRDM-KL03Z board:   [START] + [I2C Slave address+/W] + [0x01](Function ID) + [0x21](data 1) + [0x22](data 2) + ... +[0x28](data 😎 + [STOP]     I2C to SPI bridge demo supports Function ID 0xF0 to configure SPI interface: There provides four SPI baud rate: 6Mbps/3Mbps/1.5Mbps/1Mbps. More detailed info, please check below picture (picture abstracted from SC18IS602B datasheet): For example: customer could configure SPI baud rate to 3Mbps with send below data to FRDM-KL03Z board:        [START] + [I2C Slave address+/W] + [0Xf0](Function ID) + [0x01](data 1) + [STOP] Hardware Platform The demo is based on FRDM-KL03Z board, using internal IRC48M clock as system and bus clock source. There doesn’t need external clock source. Toolchain supported - IAR embedded Workbench 7.60.1  (Tested) - Keil MDK 5.18a - GCC ARM Embedded 2015-4.9-q3 - Kinetis Development Studio IDE 3.2.0 Running the Demo Connect a USB cable between the host PC and the USB port on the target board. Open a serial terminal with the following settings:     - 9600 baud rate     - 8 data bits     - No parity     - One stop bit     - No flow control Download the program to the target board. I2C master start to configure SPI interface      I2C to SPI bridge board I2C address is 0x7E. I2C master write data to SPI slave    I2C master write 10bytes to SPI slave, it will send 11bytes (includes one function ID 0x01). The first data is 0xAA and the last data is 0x22.    After I2C to SPI Bridge receive the data, it will send 10bytes to SPI slave.        I2C to SPI Bridge receive 10 bytes     I2C to SPI Bridge send 10bytes to SPI slave I2C master read data from SPI slave    I2C master read 10bytes(0x10 to 0x19) from SPI slave need to write data to SPI slave at first, then read data from I2C to SPI bridge data buffer directly.    Here just shows read 10bytes from I2C to SPI bridge data buffer. Attached I2C to SPI Bridge demo software default location is: ..\SDK_2.0_FRDM-KL03Z\boards\frdmkl03z\user_apps\i2c_to_spi
記事全体を表示
Kinetis Programming using PE multilink Connect All the VDD to +3.3V and all VSS to GND. Connect 10K pullup resistor to RESET_b pin of the controller. If the controller have the option of JTAG/SWD/EZport make sure to connect 10K pullup resistor to NMI_b or EZP_CS_b pin. NMI_b pins selects the interrupt to highest priority so the controller won't enter into programming mode and EZP_CS_b pin is used for selecting Ezport programming method.   At factory reset condition, all the controller is in the continuous watchdog enabled mode and constantly resetting and the voltage level on the reset pin will be approx 1.64V after adding the pullup resistor as mentioned in point 2. Do not add any filter capacitor on the reset pin while programming the controller for the first time. As it will not let the logic level go low while programming. Which is essential. On probing the reset pin to the oscilloscope the following will be the pattern Before programming we need to mass erase the controller otherwise it will be in continuous reset mode. And to do that we need to configure SWD/JTAG mode. The following configurations for K20P48 LQFP in SWD mode. For mass erase following steps we need to follow. Search for thunderbolt icon in code warrior ie flash programmer and click on the drop-down menu on the icon.     Click on edit then      After configuring the above settings then click on the erase whole device option shown on step 9. If the microcontroller have JTAG/SWD and EZPORT then connect the microcontroller to JTAG port using PORT B of multilink with 20 pin headder. Try avoiding jumpers instead connect the 20 pin cable provided with PE multilink programmer. As all GND pins need to be connected on board's GND.   If the problem still persist then refer to this link Freescale community programmer
記事全体を表示
This years annual hacker security conference known as DEFCON used a couple of NXP devices for this years electronic badge. This document is to explain how to program the device and add extra components. The badge was developed by Grand Idea Studio, with engineering help from NXP, and this presentation has details about the development of the badge. I'm the NXP systems engineer that was helping people get started with reprogramming their badge at Defcon, and wanted to create something that gives all the details on how to do that yourself.  Full schematics and firmware source code can be found at: http://www.grandideastudio.com/defcon-27-badge/   The badge has these two NXP devices:  KL27  - MKL27Z64VDA4 - 48Mhz ARM Cortex M0+ microcontroller w/ 64KB flash (Datasheet and Reference Manual) NXH2261UK- Near Field Magnetic Induction (NFMI) chip for the wireless communication. Has a range on the badge of about 6 inches (15cm), but the technology can work a bit further. It's often found in high end headphones because BLE waves are disrupted by your head but these waves aren't. Also less power consumption. Using the serial port: There's a serial interface which prints out helpful information and there's some "secrets" available if you have a completely leveled up badge. It'll also be really helpful if you're writing new code to hack your badge for printf debugging. Note that you cannot program the board by default over the serial port. This particular chip doesn't support that, though some of our other chips do. It of course would be possible to write a serial bootloader for it, but that's definitely not beginner level. You'll need two pieces of hardware: 1) Header Pins 3) Serial-to-USB converter Header Pin: You can solder on a header to the PCB footprint. Because of the quartz, the leads would need to be flat on the PCB. A Harwin M20-8770442 will fit the footprint and is what was provided at the soldering village and what you see in the photos below. You could also try creating your own header.  Serial to USB Converter: Since almost no computer today comes with a serial port, a serial to USB converter dongle is needed. It'll have four pins: GND, Power, TX, and RX. The DEFCON badge runs at 1.8V, but the chip itself is rated up to 3.6V, so a 3.3V dongle can be used *as long as you do not connect the power pin on the serial header*. You only need to connect GND, RX, and TX. In a production design you would not want an IO voltage above VCC, but for hacking purposes it'll work, and I've used it all week without an issue on multiple boards.  There's a lot of options. Here's a 1.8V one if you want to be extra cautious or a 3.3V one that already comes with connectors for $8. Anything that transmits at 1.8V or 3.3V will work so you may already have one, but again, just don't connect the power pin.    Software: You'll need to install a serial terminal program like TeraTerm or Putty.  1) Plug the 3.3V or 1.8V USB converter dongle into your computer and it should enumerate as a COM port.  2) Connect the GND line on the dongle to GND on the header 3) Connect the TX pin on the dongle to the RX pin on the header 4) Connect the RX pin on the dongle to the TX pin on the header (it is not RX to RX, I spent 2 whole days tearing my hair out over that during my robotics project in college) 5) DO NOT CONNECT THE POWER PIN  5) Should look like the following when finished 6) In your serial terminal program, connect to the COM port your dongle enumerated as 7) Find the serial port settings menu (in TeraTerm it's in Setup->Serial Port from the menu bar) , and set the baud rate to 115200. The other settings should not need to be changed (8 data bits, no parity, 1 stop bit).  😎 In the terminal, press enter. You should get a > prompt 9) In the terminal, press the '?' key on your keyboard, and hit enter, you'll see the menu.         10) Note that the key you press won't show up in the terminal, but just press Enter and then the command will be run 11) Hit Ctrl+x to exit interactive mode and turn back on the radio.  12) While not in interactive mode, the terminal will display the transmit packet of any badge you bring close to it.  Reprogramming Your Badge: Hardware:  There's two pieces of hardware needed: 1) Programmer/debugger 2) Programming cable Program Debugger: Most any ARM Cortex M debug programmer can be used, as the KL27 chip has a ARM M0+ core. I'd recommend the LPC-Link2 as it's only $20 and can be bought directly from NXP or from most distributors (like Mouser or DIgikey). Search for "OM13054". But you could also use a J-Link, PEMicro, or others if you already have an ARM programmer. Cable: The DEFCON badge has the footprint for a Tag Connect TC2050-IDC-NL-050-ALL. Because this cable is meant for manufacture programming and not day-to-day debugging, if you plan on stepping through code, you'll also want to pop off the the quartz front and get some retainer clips to keep the programmer connected to the board. If you just simply want to reprogram the board, you can just snip off the 3 long guide clips, and press the cable against the PCB while holding your hand steady for the ~5 seconds it takes to flash it each time.  Alternatively if you already have a JTAG/SWD cable and have soldering skills, you can use some fine gauge wire and hack up your own converter to your board like /u/videlen did with some true hacker soldering. However as /u/int23h pointed out, because it's using Single Wire Debug (SWD) you only need to really solder 2 of the pins, SWDIO and SWDCLK. However nRESET is also recommended as it'll let you take control of the device if it's in sleep mode (which it is most of the time). Power (which is needed so the programmer knows what voltage to send the signals at) and GND you can get from the serial header. Software There's three pieces of software you'll need:  1) Compiler 2) MCUXpresso SDK for the KL27  3) Badge source code Compiler: Recommended Option: Latest version of MCUXpresso IDE - available for Windows, Mac, and Linux Second Option: Download older version of MCUXpresso IDE for Windows from the DEFCON media server  Third Option: If you use the latest SDK, you can easily use ARM-GCC, IAR, or Keil tool chains as well.  MCUXpresso SDK: Recommend Option: Download latest SDK version for KL27 - includes setup for MCUXpresso IDE, ARM-GCC, IAR, and Keil compilers Other option: Download the older 2.4.2 SDK version on the DEFCON server which only has MCUXpresso IDE compiler support.  Badge Source: Recommended Option: Download zip off Joe Grand Website: http://www.grandideastudio.com/wp-content/uploads/dc27_bdg_source.zip  Other option: Download from DEFCON media server. However the .project and .cproject files do not show up by default, so you must make sure to explicitly download them as well and put them in the main firmware folder (at the same level as the .mex file). These are the exact same files as in the zip.  wget -r -np -R "index.html*" https://media.defcon.org/DEF%20CON%2027/DEF%20CON%2027%20badge/Firmware/ wget  https://media.defcon.org/DEF%20CON%2027/DEF%20CON%2027%20badge/Firmware/.cproject wget  https://media.defcon.org/DEF%20CON%2027/DEF%20CON%2027%20badge/Firmware/.project  Getting Started with MCUXpresso IDE:      1) Open up MCUXpresso IDE. When it asks for a workspace directory to use, select (or make) a new empty directory that is in a different location than where you          downloaded the firmware source.       2) Drag and drop the SDK .zip file from your file system into the MCUXpresso IDE "Installed SDKs" window. This is how the compiler learns about the KL27 device and the flash algorithms.  3) Drag and drop the badge firmware folder from a file explorer window into the MCUXpresso IDE "Project Explorer" window 4) In the Quickstart panel hit Build 5) In the Console tab, you should see the message that it compiled successfully 7) In the Quickstart panel hit Debug.  If you're not using a LPC Link2 for programming, you'll need to hold Shift when clicking this the first time so it'll rescan for your debugger.  If using the latest MCUXpresso IDE, you'll see a dialog box that the launch configuration needs to be updated. Click on "Yes".    7) A dialog box will come up confirming your debug probe. 😎 Connect the programming cable to the board and press to make a good connection. Make sure the alignment pins match up with the alignment holes on the PCB, and that pin 1 (the red stripe) matches the photo below. You may hear the badge beep, as it's being reset. 9) Then hit OK in the dialog box to start programming. Make sure to keep the probe held there until the programming is finished - about 5 seconds. 10) You should see it program successfully and hear the board beep as it reboots.  Programming Troubleshooting/Tips: If you're not using a LPC Link2, hold down the Shift key when you hit the Debug button, and it'll re-search for new probes. Also make sure your debug settings and probe is using SWD mode and not JTAG mode.  If you have the programming cable not lined up with the pads, you'll see this error. Re-align your probe and try again. Also you must have power from the battery as the MCU needs to be turned on while programming. You can hit the GUI flash programmer at the top for a quicker download experience since it won't load the debug view. Useful if just flashing the device without wanting to step through code.  Finally, some of the game state variables are stored in the non-volitale internal flash, and may not automatically get erased when reprogramming the firmware as the programmer doesn't realize that area of flash memory is being used and thus to save time, doesn't bother to erase it. You can force a complete erase of the flash to wipe all the game variables by setting the mass erase option. Double click on the dc27_badge LinkServer Debug.launch file which contains the debug settings, and go to GUI Flash Tool->Program and set Program (mass erase first).  Getting Started with ARM-GCC: To make this easier, you'll need to download the latest SDK from the NXP website first.  Follow the instructions in Section 6 of the MCUXpresso SDK User Guide for how to setup the environment and test it out on Hello World. You can then use that project for copying the badge source code into. I'm sure someone can put together a Makefile for the badge specifically. See this series of blog posts on how to use the SDK (compiling/debugging) with arm-gcc in Linux. My badge isn't working: First thing to try is power cycling the badge by gently prying the battery out (with a butter knife or something) and putting it back in. A couple of things might happen: If nothing at all happens, you battery might be dead. Try replacing the battery.  If nothing at all happens still, the battery holder might be loose. Use a multimeter ot measure the voltage between GND and VCC on the serial header, it should read 1.8V. If it does not, check the battery holder. If you hear beeps, all 6 LEDs light up, and then 4 LEDs (2 on each side) flash in sync a few times, it means there was an issue communicating with the NFMI device. This could be due to a loose solder joint on one of the chips or the I2C pull up resistors (SCL and SDA on the pinout image). You could also do a reflow if you have the equipment, but it may not be fixable. Also could see if see any I2C communication on those SCL/SDA pins. If you hear a normal startup beep, the lights flash, and then it goes back to the startup beep, and so on, forever, something is causing the MCU to keep resetting. Could be a short or ESD damage. Check soldering. Connecting your board to a serial terminal and see how far it gets in the boot process to help narrow down the cause.  Sometimes the flags don't get saved properly. A power cycle usually works, and could also try reflashing the badge.  If your badge isn't responding to other badges with the NFMI, it could be one of two things: Your copper antenna is loose/broken/missing. This happened a lot. Solder it back on. If missing, it's a Sunlord MTNF6040FS3R7JTFY01 but it's not available online anywhere at the moment. Datasheet is here. See this post for more details on possible alternatives. If you were previously in interactive mode, you have to explicitly exit it with Ctrl+X to receive packets again.  Further hacking: For basic hacking of the code, try changing your game flags to trick it to giving you a fully unlocked badge. From there, you could try to make your own chameleon badge like others have done (https://github.com/japd06/defcon27_badge and https://github.com/nkaminski/DC27-badge-CFW and https://github.com/NickEngmann/Jackp0t among others if you want ideas). Or make your own songs with the piezo. Or some ASCII art on the terminal. For more advanced hacking on the badge, PTE22 and PTE23, the TX and RX pins on the serial header, could be programmed to be ADC input pins instead. Or timer inputs or outputs for PWM or input capture.  And with some good soldering, you could even add an additional I2C device by soldering to the resistor points. t.   Finally if you want a more flexible platform for exploring embedded development, you can pick up a FRDM-KL27Z dev kit for $20 which has the same chip as the badge. You can buy it direct or all major distributors online. The programmer and serial interface are built into the board so you only need to use a USB cable to do all the programming. The KL27 SDK also includes dozens of example programs that show how to use all the features of the chip and there's some getting started videos (mostly what I covered already in this post though). While it does not have a NFMI chip on it, it does have USB support, as well as an Arduino hardware footprint on it so it can be easily expanded with extra boards. You can find the example programs by going to "Import SDK examples" from the Quickstart panel window.  If you have any more questions about the badge, post a response! 
記事全体を表示
The DOC introduces the nano-edge placement  feature for KV4x family, it gives the application for the nano-edge placement feature, in other words, it's target is to increase the PWM signal resolution. It gives the example code and PWM waveform for the nano-edge placement feature.
記事全体を表示
  当我们在使用Keil 时,经常会遇到无法下载程序的问题,以下对两种常见的情况进行总结:    1. 在我们需要将某工程代码移植到同系列其他型号器件上使用时,如果只是更改了器件型号,这时可能会导致无法正确下载。需要注意的是不仅要在Device中更换型号,还需要在Flash Download栏中选择正确的flash loader 并且设置正确的RAM起始地址。   举个例子:假设我们需要将FRDM_KL26的Sample code中的hello_world工程移植到256K flash的KL26上使用。打开FRDM_KL26的Sample code中hello_world工程,我们可以看到Device中器件为MKL26Z128xxx4,        在Target中可以看到Flash和RAM的起始地址和大小信息。          如果使用Jlink调试接口,选择J-LINK/J-TRACE Cortex  ,之后选择Setting,可以看到flash loader的相关信息。         将此工程移植到到256K flash的器件上,我们需要做的事情是:      在device中进行修改,选择MKL26Z256xxx4               在Target中可以看到这时flash和RAM的起始地址和大小信息已经自动做了更改。不需要再手动修改了。         但是在Flash Download中的设置还是之前的设置,并没有改变。           所以这时是无法正确下载程序的,需要我们手动去修改这里的两处配置。     一是 RAM for Algorithm中的Start应该设置为0x1FFFE000(从Target栏中可以获取该值),Size不用更改。      二是Program Algorithm 删除掉128k的flash loader ,添加256K的flash loader。       2.第二种可能遇到的情况是:本来可以正常下载的程序当复制到另外一台电脑时就无法正常下载了。遇到这种现象时,需要检查一下Flash Download中的相关配置是否正确,很可能会遇到 Program Algorithm中flashloder为空的情况,发生这种情况的原因可能是两个电脑的Keil版本不同,所以flash loader所在路径就会不同,这样flash loader就会变成空白,这时需要自己手动添加一下即可。
記事全体を表示
Hello Kinetis fans, This time I bring to you a document which explains what is and how to configure scatter/gather feature which is present in the Enhanced Direct Memory Access (eDMA). This document includes an example project for the Kinetis Design Studio (KDS) which works in the FRDM-K64F board but the configuration is the same for any MCU which includes the eDMA peripheral. If you are interested in the channel linking feature, please take a look into the document What is and how to configure the eDMA channel linking feature​. I hope you find this document useful. Best regards, Earl Orlando Ramírez-Sánchez Technical Support Engineer NXP Semiconductors
記事全体を表示
Explore the Features of MCU-Link Pro MCU-Link Pro is the latest ARM Cortex-M series core debugger tool from NXP. Some of its features are inherited from the past LPC-LINK2. But overall it was redesigned and introduced and many new features. These additional functions make the MCU-Link Pro a very powerful debugging tool. This article will explore these features and highlight interesting and useful ones. These functions mainly include the following aspects. SWD+SWO Measurement of current and power consumption MCU-Link pro is supported by new blhost LIBUSBSIO library for windows, Ubuntu Linux and MacOS A secondary chip LPC804 on the board   SWD+SWO MCU-Link Pro support SWD only. It doesn’t support JTAG. The main controller in the board is LPC55S69. There is level shifter circuit between the port and LPC55S69. It makes the board can debug the target board work at 1.2V to 5V. It has reference voltage trace circuit which is use to trace the target board voltage. It can trace the port automatically, needn’t any settings. The MCU-Link Pro also can supply 1.8V/3.3V to target board. The maximum current is 350mA. This is done by connecting J6 and selecting by J5. The maximum speed of SWO is 9.6Mbit/s. Same as <PC-Link, MCU-Link Pro support CMSIS-DAP and Jlink firmware. These firmware are kept updating. The latest firmware of CMSIS-DAP is 2.25. If the firmware version is old, there will be a message jump out telling customer to update it when connecting to computer. We can see that the new version gives two VCOM while the original version only have one. The new VCOM use J26-4 and J26-5. jingpan_0-1664529871686.png   Measurement of current and power consumption MCU-Link pro provides a very interesting real-time function of current and voltage measurement. It can capture a burst of samples of target current usage, the target supply voltage, the shield current, the analog input, the debug interface reference voltage, or target power consumption at up to 100ksps. This information is displayed in a graph and can also be exported for further analysis. The average value of the collected data can also be displayed. And based on the current and voltage data, the power consumption can also be calculated and displayed in the graph. The place where the red line is drawn in the figure below is the real-time voltage at the time point of the mouse. jingpan_1-1664529871909.png     What's more interesting is that the energy measurement function does not need to activate the debug to capture the data, it is offline and has a separate data channel. But it can also be linked to a session if such a debug session exists. This is very useful in debugging various low-power applications. Not only can you see the power consumption change under each step of the command, but you can also check the power change rule for a long period of time when the system is running. Since there is a separate data channel, you can even debug the program in KEIL and watch the current change in MCUXpresso. The MCU Link Pro has two current measurement configurations, each with a maximum measurable current. This is to achieve maximum measurement accuracy for a variety of different objectives. There are two automatically controlled ranges in each configuration to provide greater precision. The automatic switching from low current measurement to high current measurement is completely controlled by hardware. jingpan_2-1664529871937.png   Each time the MCU Link Pro is powered up, the measurement circuit calibrates itself. There is no need to disconnect/reconnect the MCU Link Pro before calibration due to transistors are used to isolate the sensing circuit from the target power supply to avoid contention and to ensure a known voltage is applied to the system during calibration. At high sample rates, the MCUXpresso IDE may not capture all data, so the sample rate may need to be adjusted using the configuration options in the energy measurement configuration settings in the tool. If the target current exceeds the maximum current in the selected range, the measurement will saturate and cut off and will therefore be inaccurate. Blhost and MCU-Link Pro The most noteworthy feature of MCU Link Pro is its USB to SPI and I2C bridge functions. This enables the computer to send I2C and SPI signals directly through USB. This powerful function is not ignored by blhost. The new version of blhost can support this function and adds a new command parameter '- L'. Specifically, '- L SPI' refers to the SPI interface and '- L I2C' refers to the I2C interface. The following figure shows the test results on frdm-k64f. It can be clearly seen in the figure that the SPI interface of MCU Link Pro can communicate with mcuboot firmware on k64 and download the encryption program to flash. jingpan_3-1664529872017.png     In addition to KINETIS, this function is most suitable for i.mxrt600 and I mxRT500。 These two chips have serial ISP mode. User can download the program to ram through SPI or I2C port, and then directly let it run. Many users have this usage. In the previous examples in SDK, a board of twr-kv46 or twr-k65 or frdm-kl25 was required to receive command and data from UART and translate them to SPI and I2C command. Since there is no direct interface on these boards, flying wires are required, which is very troublesome. Moreover, NXP only provides firmware for these three boards. If you want to use other chips or boards, you must also transplant firmware. It's also very troublesome. But with MCU Link Pro, it's all very easy and pleasant.   LIBUSBSIO library In order to better expand the use of bridge functions, NXP has provided libusbsio library. By calling this library, you can realize the USB to SPI \ I2C \ GPIO function in your own application. I also made the upper computer tools for writing kinetis ezport and flash according to the libusbsio library provided by NXP. I introduced this point in detail in my last article. Interested friends can read my article. It is not enough to provide libraries based on windows and Linux. NXP also provides a python library. This library is based on python3 and can be installed through the following command >pip install libusbsio Its usage is not described in detail in the libusbsio documentation. Here is a general introduction. The following is an initialization procedure of libusbsio. import logging import logging.config from libusbsio import * # enable basic console logging logging.basicConfig() # load DLL from default directory sio = LIBUSBSIO(loglevel=logging.DEBUG) # the main code # calling GetNumPorts is mandatory as it also scans for all connected USBSIO devices numports = sio.GetNumPorts() print("SIO ports = %d" % numports) if numports > 0 and sio.Open(0): print("LIB version = '%s'" % sio.GetVersion()) print("SPI ports = %d" % sio.GetNumSPIPorts()) print("Max data size = %d" % sio.GetMaxDataSize()) if(sio.GetNumSPIPorts() > 0): spi = sio.SPI_Open(1000000, portNum=0, dataSize=8, preDelay=100) if spi: data, ret = spi.Transfer(spi_ssel[0], spi_ssel[1], b"Hello World") sio.Close() else: print("No USBSIO device found") ​ Line 9 is to open an instance of libusbsio library; Line 14: get the number of usbsio ports of all USB bridges; Lines 18, 19 and 20 are the read version information, the number of SPI ports and the maximum size of SPI cache; Line 22: open an SPI interface; Line 24, start transmitting data. It can be seen from the above that the use process is relatively simple. And these commands are very similar to those of the C language library.   A secondary controller LPC804 on the board There is also an lpc804 on the MCU Link Pro board. This chip is confusing here. What is it for? Its UART, SPI and I2C ports are all connected for external use. But what's the use? One conceivable application is that the UART port is connected to the newly added vcom2, and then the SPI or I2C works in the slave mode. As a listener, it monitors the SPI or I2C bus to be debugged and displays it on the computer terminal. The LPC804 debug interface is the same as the debugging port of MCU Link Pro. Maybe the board itself is a development board, so that users can develop lpc804 programs? In addition, its UART-ISP port is connected to a UART port of LPC55S69. It seems that in the future, it can communicate with each other through the new version of CMSIS-DAP firmware. Let's look forward to new ways of playing in the future.
記事全体を表示
中文版本:     相信很多博友在调试ARM代码的时候,尤其是涉及到操作底层的时候,由于一些误操作常常会遇到Hard fault错误或者程序跑飞的情况,这些bug采用正常的方法是比较难定位的,往往需要我们逐行去排查测试,最后看的眼花缭乱,永远给人以苦逼程序员的印象,呵呵。此篇内容致力于节省广大程序员的精力,以崭新的一种方法角度或者说是手段来定位跟踪bug(仅限于支持Coresight技术的ARM处理器,本篇只讲针对M0+内核的),故冠之以“原创猛料”之称号,希望能名副其实,好了,闲话不多说,呵呵,开整……     ARM的Coresight技术估计大家有所耳闻(没听过的可以参考我之前的一篇介绍类文章http://blog.chinaaet.com/detail/29770.html),它实际上包括了ARM嵌入到其处理器内核的片上跟踪调试组件和相关的配套系统软件标准之类的,方便我们开发调试ARM产品。可能单说Coresight技术有点太泛了,把它具体化的话就不得不提到ETB(Embeded Trace Buffer)和MTB(Micro Trace Buffer)这两个经典的模块,其中ETB模块是Cortex-M3/M4内核的片上跟踪单元,而MTB模块则是Cortex-M0/M0+内核的跟踪单元。不过估计很多人没有用过,所以我就本着“吃螃蟹”的态度去尝试了一番,结果还是挺让我惊喜的,灰常好用,所以下面我就把使用方法分享给大家供大家评估,本文以MTB模块调试飞思卡尔基于Cortex-M0+内核的Kinetis L系列为例:     在介绍使用方法之前需要提一下,目前我测试的结果是J-link暂不支持MTB模块(但是支持ETB模块),所以我使用了OpenSDA平台的CMSIS-DAP固件来调用MTB模块,所以如果你手中有Kinetis L系列的Freedom板的话就直接可以跟我做了,其中CMSIS-DAP固件在本博客附件中,使用方法仍旧是类似更新OpenSDA的应用,不过换过CMSIS-DAP固件之后OpenSDA的小灯可能不亮,这个纯属正常,不要惊慌,哈哈。 测试环境:IAR6.6 + Freedom OpenSDA(CMSIS-DAP firmware) 测试目标芯片:Kinetis MKL25Z128     1)打开一个KL25的demo例程,然后右键工程Options->Debugger,选择“CMSIS-DAP”调试器,然后其他默认即可,设置完毕,点击“OK”,如下图所示:     2)点击调试按钮,进入调试界面,此时菜单栏会出现CMSIS-DAP选项,选择CMSIS-DAP->ETM Trace,调用MTB模块,弹出跟踪窗口,如下图所示。默认情况下跟踪功能是禁止的,此时点击跟踪窗口ETM Trace左上角的“电源符号”,打开跟踪功能,此时调试界面的左上角的ETM显示绿色,表示已经打开;     3)此时MTB功能已经打开,我们可以点击“全速运行”,然后再点击“暂停”,此时就可以在ETM Trace跟踪窗口看到从运行到断点停止这段时间所有的指令执行情况了,非常直观,如下图所示,此外可以选择同时查看汇编和C语言,也可以保存跟踪的结果,进而分析程序执行情况。     说到这,我们就该想到这种方式的好处了吧,如果遇到Hardfault或者程序跑飞的时候,通过设置断点或者点击暂停,然后就可以捕捉到出现hardfault或者程序跑飞的之前的程序执行情况从而帮助我们快速定位到bug的地方,非常方便实用。此外,实用CMSIS-DAP调试工具还有一个好处是,可以使用很多插件了,比如Timeline等等,灰常不错,哈哈~ English Version:     As we know, ARM Coresight, the ARM debug and trace technology, is the most complete on-chip debug and real-time trace solution for the entire System-On-Chip(SoC), making the ARM processor-based SoCs the easiest to debug and optimize. In this technology, the ETB in  Cortex-M3/M4 and MTB in Cortex-M0/M0+ are representative two units, which can effectively help us to monitor the process of software executing or focus on some hard faults by tracing the instructions.     In the article, I wanna introduce the MTB useage in our product Kineits L series, which may be helpful to some customers using KL chip. But, before that, a CMSIS-DAP firmware for OpenSDA platform is needed, which you can find in the attachment of this article. So far as I know, it seems that J-Link don't support MTB yet, but do support ETB of Cortex-M4. Testing Platform:     IAR EWARM6.6 + FRDM KL25 (OpenSDA with CMSIS-DAP fimware) Testing steps:     1) firstly, update the OpenSDA with CMSIS-DAP fimware, just like other OpenSDA applications;     2) open any KL25 demo with IAR, access project setting "Options->Debugger", and select the "CMSIS-DAP" adapter as the screenshot shown below;     3) click the debug button to access thw debug window, then click the CMSIS-DAP->ETM Trace from the menu bar,  and the ETM trace window will appear. Note that, the trace function is disabled in default, so another step is needed to click the "power port" at the top left corner to enable the trace function. The screenshot shows it below;     4) Now, the MTB is working. We can try it by click "run" and wait a while to click "pause", then the instructions from run to pause are shown in the trace window, it is really convenient. Besides, we can save, clear or zoom the trace results. Conclution:    Through the above method, some painstaking issues like hardfault or program fleet can be captured simply by setting breakpoints or mannuly pause, which can help to positioning the source of the problem. Beyong that, the CMSIS-DAP can support plugs like timeline tool. BTW, it is a pity that MTB unit in the new Kinetis E series is cut out.         Happy Tracing!
記事全体を表示
The Freescale Freedom development platform is a low-cost evaluation and development platform featuring Freescale's newest ARM® Cortex™-M0+ based Kinetis KL25Z MCUs NEW! Quick Start Guide Features: KL25Z128VLK4--Cortex-M0+ MCU with:   - 128KB flash, 16KB SRAM - Up to 48MHz operation  - USB full-speed controller OpenSDA--sophisticated USB debug interface Tri-color LED Capacitive touch "slider" Freescale MMA8451Q accelerometer Flexible power supply options   - Power from either on-board USB connector - Coin cell battery holder (optional population option)  - 5V-9V Vin from optional IO header - 5V provided to optional IO header - 3.3V to or from optional IO header Reset button Expansion IO form factor accepts peripherals designed for Arduino™-compatible hardware
記事全体を表示
The 5V Kinetis E series MCUs are designed to maintain high robustness for complex electrical noise environments and high-reliability applications. Kinetis EA series MCUs using the same architecture with automotive level operation temperature range, are various used for auto body electrical application. There was a reality customer requirement to let KEA core running the application (light a LED) within 20ms from power up. It need to know the whole startup processing for KE/KEA product. Please check below picture to get more info about boot sequence: During the power up phase, after VDD rising to VPOR voltage threshold, there with about 15us delay before internal IRC start oscillating. T2 interval is FLL acquisition time to make FLL generating clock. The Reset_b pin is released and then the system is released from reset. After that, the NVM starts internal initialization. Flash Controller is released from reset and begins initialization operations while the core is still halted before the flash initialization completes. When the flash Initialization completes (16 μs) , the core sets up the stack, program counter (PC), and link register (LR). The processor reads the start SP (SP_main) from vector-table offset 0. The core reads the start PC from vector-table offset 4. LR is set to 0xFFFF_FFFF. The CPU begin to execute the first instruction. Overview the whole power up processing, FLL acquisition time is the longest time interval almost 1ms, then following power up time about 0.1ms (using 17KV/sec VDD ramp-up slew rate). There seems a lot of time left to run the chip initialization code and application code. Customer requirement (power up to light a led within 20ms) should be matched without any problem. While, during customer test, there seems it need to take more than 30ms to find the LED be lighten after power up. In order to check the issue, we get the customer test code and find there with below clock initialization code: void Clk_Init() {                 ICS_C1|=ICS_C1_IRCLKEN_MASK; /* Enable the internal reference clock*/                 ICS_C3= 0x90;                                    /* Reference clock frequency = 31.25 KHz*/                       while(!(ICS_S & ICS_S_LOCK_MASK));  /* Wait for FLL lock, now running at 40 MHz (1280 * 31.25Khz) */                                               ICS_C2|=ICS_C2_BDIV(1)  ;                    /*BDIV=2, Bus clock = 20 MHz*/                 ICS_S |= ICS_S_LOCK_MASK ;              /* Clear Loss of lock sticky bit */      } We do a test to check the Clk_init() function execution time and find it will take almost 25ms. We toggle a GPIO pin and almost 25ms for checking ICS status register [LOCK] be asserted. KE/KEA product using ICS module as clock source, which default mode is FEI. In general, during the chip initialization, using ICS status register [LOCK] bit to check if the FLL cock is stable or not. From KE/KEA product datasheet, the Max. FLL acquisition time is 2ms. Why the ICS_S[LOCK] bit be asserted need take more than 25ms? After double check with ICS IP owner, we get below info: The FLL_S[LOCK] bit act as “LOCK detection”, the LOCK bit will be set if FLL clock frequency stays within the tolerance 6% for 20ms~30ms. After acquisition time (max. 2ms) FLL achieved clock accuracy as same as LOCK bit be asserted. After ICS configuration modified, customer can call a 2ms delay routine to make sure FLL acquisition clock successfully before executing the application code. 
記事全体を表示
For motor control and swich mode power supply application, it is required that the ADC sampling is synchronized with PWM signal. In general, most Kinetis sub-family provides FTM, PDB and ADC, it provides a mechanism for ADC converter is synchronizedc with PWM signal. But the KEA family does not have PDB module, instead, the KEA family provides a simple mechanism which enables PWM signal the FTM module generate can synchronize the ADC converter. The DOC introduces the mechanism, give the register configuration description, code and scope screenshot on how the PWM signal synchronizes the ADC.
記事全体を表示
A vulnerability (CVE-2022-22819) has been identified on select NXP processors by which a malformed SB2 file header sent to the device as part of an update or recovery boot can be used to create a buffer overflow. The buffer overflow can then be used to launch various exploits. Refer to the attached bulletin for more information.   09/26/2022 - Bulletin updated to include fix datecode information. 11/01/2022 - Bulletin updated with clarification that mixed datecodes are RT600 only.    
記事全体を表示
客户要求:K60 100MHz芯片作为SPI主机读取片外SPI Flash存储器内容(SPI Flash器件数据准备完成会触发K60 GPIO中断),要求在130~150微秒之间读取九个不连续地址上的数据,每个地址需要读取4个字节,SPI波特率为5MHz。读取SPI Flash存储器,需要使用读取命令(1个字节)外加地址(2个字节)。换言之,每读取一次K60需要发送7个字节(1字节读取命令+2字节地址+4字节空读数据)。同时要求减少内核负担。 Customer requirement: Use K60 100MHz product as SPI master communicate with external SPI Flash device (When data ready, SPI Flash device will trigger K60 GPIO interrupt), it need to read data from 9 discontinuous address, each address read 4 bytes within 130~150us. SPI  baud rate is 5MHz. Read data from SPI Flash, it need SPI master send 1byte read command and 2bytes address. In another word, K60 need to send 7bytes(1byte read command+2bytes address+4bytes dummy read) 9times within 130us. SPI communication baud rate is 5MHz. It also require to reduce core work load. 实现方法:使用DMA模块,其中一个DMA通道1用来装载SPI传输TX数据(触发源为SPI TFFF符号,SPI FIFO可装载),另外一个DMA通道0用来接收SPI数据(触发源为SPI RFDF符号,SPI 接收FIFO非空)。通过使用DMA引擎可以自动发起SPI传输,减少内核在SPI传输过程中的干预,达到降低内核工作负荷的效果。SPI模块采用中断方式。 Reality way: Use DMA module, DMA CH0 loads data for SPI transmit, DMA CH1 stores data for SPI receive.  DMA triggered by SPI module and SPI module works in interrupt way. 测试平台:TWR-K60D100M, TWR-MEM, IAR ARM Workbench V6.60 TWR-MEM板子提供SPI Flash设备(AT26DF081A),可以通过TWR-K60D100M SPI2模块进行访问。 Test platform: TWR-K60D100M ,TWR-MEM , IAR ARM Workbench V6.60 SPI Flash AT26DF081A on TWR-MEM board, which could be accessed by TWR-K60D100M via SPI2 module. 测试场景一:读取AT26DF081A设备ID信息 Test scenario 1:  Read device ID AT26DF081A设备提供查询设备ID命令0x9F,返回4个字节设备ID信息(0x1F,0x45,0x01,0x00)。K60作为SPI主机发出查询命令,之后执行4次空写入操作用来读出设备ID信息。测试中SPI传输/接收数据帧大小设定为1个字节(8bit)。由于DSPI模块传输接收均提供4级FIFO,测试中使用两种方式进行SPI数据发送,一种方式使用DMA通道发送读取设备ID查询命令和4次空写入数据,另一种方式通过执行代码(需要内核干预)发送读取设备ID查询命令和4次空写入数据。SPI数据接收均使用DMA完成。为了便于测试使用DMA模块是否降低内核负荷,在DSPI通信同时,主程序在While循环中不停翻转GPIO引脚(PTD7)。 SPI Flash AT26DF081A provides read device ID command(0x9f), will feedback 4 bytes device ID info(0x1F,0x45,0x01,0x00)。K60 works as SPI master send read ID command, then send 4 dummy write data to read back device ID info. During test, SPI data frame size setting to 1byte(8 bit). For DSPI module TX/RX FIFO is 4 entries, so there using two ways do SPI data transfer, one is using DMA CH1 send data, the other way using software code send data. SPI RX using DMA CH0 and in main while loop it will toggle PTD7 pin to show if using DMA module will reduce core work load. 测试流程图(方法一: 使用DMA CH1发送SPI数据): Test flow chart (Way1: Using DMA CH1 do SPI TX): 测试结果(Test Result): 执行一次读ID信息操作,需要花费12.96us,其中内核处理中断的时间为(2.56+2.72)= 5.28us。 根据客户要求,依照此方法每次发送3个字节,接收4个字节,SPI通信过程中内核负荷时间比率为 (5.28/16.16) =32.7% SPI read ID operation once, it will take 12.96us, includes core deal with interrupt time 5.28us. According to this way, customer want to TX 3bytes then RX 4bytes, during SPI communication core work load rate is 32.7% 测试流程图(方法二: 使用软件代码发送SPI数据): Test flow chart (Way2: Using software code do SPI TX): 测试结果(Test Result): 执行一次读ID信息操作,需要花费11.6us,其中内核处理中断的时间为(2.48+1.40)= 3.88us。 根据客户要求,依照此方法每次发送3个字节,接收4个字节,SPI通信过程中内核负荷时间比率为 (3.88/14.80) =26.2% SPI read ID operation once, it will take 11.6us, includes core deal with interrupt time 3.88us. According to this way, customer want to TX 3bytes then RX 4bytes, during SPI communication core work load rate is 26.2% 测试场景二:读取AT26DF081A设备9处不连续地址数据 Test scenario 2: Read 9 discontinue address data from AT26DF081A AT26DF081A设备提供读阵列命令(0x0B),可以连续读取多个字节数据。根据客户要求,测试读取9处不连续地址数据,每处读取4个字节。根据AT26DF081A设备要求,读阵列命令后需要再发送3个字节地址信息外加1个字节空写入数据,之后K60将会收到数据。即如果要读取4个字节数据,K60作为SPI主机需要发送9个字节数据(1个字节读阵列命令+3个字节地址+1个字节空写入+4个字节空写入)。测试中使用两个DMA通道进行SPI数据收发,两个DMA通道交替工作,DMA通道0(SPI接收)优先级高于DMA通道1(SPI发送)。完成9处数据采集后进入SPI中断,清除EOQ标志并且修正DMA通道配置,进行新的一轮9处数据读取测试。为了便于测试使用DMA模块是否降低内核负荷,在DSPI通信同时,主程序在While循环中不停翻转GPIO引脚(PTD7)。 SPI Flash AT26DF081A provides read array command (0x0B) to sequentially read a continuous stream of data out. With customer requirement, the test will read 9 discontinue address data, each address read 4 bytes data. AT26DF081A datasheet shows read array command with 3 bytes address and 1 dummy byte, then following will be data. In order to read 4 bytes data out, K60 as SPI master need TX 9 bytes data (1byte read array command + 3bytes address + 1byte dummy data + 4bytes dummy data). During the test, it using two DMA channels do SPI TX/RX, each channel alternatively work, DMA CH0(SPI RX) with higher priority than DMA CH1(SPI TX). When finish 9 discontinue address data receive, it will clear EOQ flag and refresh DMA CH0/1 setting in SPI interrupt for next round read 9 discontinue address data test. In main while loop it will toggle PTD7 pin to show if using DMA module will reduce core work load. 测试流程图(Test flow chart): 测试结果(Test Result): 读取AT26DF081A设备9处不连续地址数据,需要花费132.32us,其中内核处理中断的时间为2.6us。 根据客户要求,依照此方法每次发送3个字节,接收4个字节,重复9次。SPI通信过程中内核负荷时间比率为 (2.6/103.52) =2.5% SPI read ID operation once, it will take  132.32us , includes core deal with interrupt time 2.6us. According to this way, customer want to TX 3bytes then RX 4bytes, 9times,during SPI communication core work load rate is 2.5% DMA模块提供动态加载DMA传输控制描述符(TCD)功能,当需要连续多次执行SPI传输时,使用这种功能可以进一步减少内核负荷。 DMA module provides dynamic scatter/gather feature, which supports automatically loading a new TCD into a DMA channel. Using this feature will reduce core work load in SPI transfer continuously. 测试结果(使用DMA动态加载功能): Test Result(Using DMA dynamic scatter/gather feature ): 读取AT26DF081A设备9处不连续地址数据,需要花费130.68us,其中内核处理中断的时间为0.76us。 根据客户要求,依照此方法每次发送3个字节,接收4个字节,重复9次。SPI通信过程中内核负荷时间比率为 (0.76/101.88) =0.75% SPI read ID operation once, it will take 130.68 us , includes core deal with interrupt time 0.76us. According to this way, customer want to TX 3bytes then RX 4bytes, 9times,during SPI communication core work load rate is 0.75% 测试结论(Test conclusion) SPI通信过程中DMA模块使用方式不同对于减轻内核负荷作用差异明显。通常SPI进行大量数据传输接收,使用DMA模块能有效减少内核负荷。鉴于客户需求,使用测试场景二的方法可以有效降低内核负荷。 How to use DMA module to reduce core work load, different way lead to different result. In general, using DMA module do amounts of SPI data transfer will reduce core work load . According customer requirement, using test scenario 2 way reduce core work load dramatically。 为什么每次读操作之间需要SPI片选无效 (Why need deassert CS signal between each read operation)? 根据AT26DF081A手册要求,读ID命令和读阵列命令都需要使片选信号无效用以结束当前的读操作,换言之如果要开始新的读操作,需要结束之前的通信(使片选信号无效)。 AT26DF081A datasheet indicates deasserting the CS pin will terminate the read operation and put the SO pin into a high-impedance state. In order to start new read command operation, it need deassert the CS pin. 计算客户要求每次读命令间隔时间为SPI实际通信时间(以5MHz波特率发送7个字节重复9次 100.8us)加上内核处理中断时间。 According customer requirement SPI each read command interval time is SPI communication time (TX 7bytes 9times with 5MHz baud rate take 100.8us) add core deal with interrupt time. 测试代码(Test source code) 测试代码基于Kientis 100MHz Rev2例程中的[spi_demo]工程,将测试代码替换<spi_demo.c>和<isr.h>文件即可。 Test source code is based on KINETIS512_V2_SC (Kientis 100MHz Rev2 Example Project) [spi_demo] project, using test code instead of orignial <spi_demo.c>&<isr.h> files.
記事全体を表示
RNN on FRDM_K64 to denoise 1 Introduction Ordinary MCUs are limited by resources, and it is difficult to do some complex deep learning. But although it is difficult, it can still be done. Last time we used CNN for handwritten recognition. This time ,we use RNN for audio noise reduction. This audio noise reduction uses fixed-point noise reduction. MFCC and gain are used as input parameters for training. MFCC, Mel frequency cepstrum, is often used for audio feature extraction. RNN achieves the effect of noise reduction by adjusting the gain of different frequencies.        2 Experiment 2.1 Required tools: frdm-k64, python 3.7, Pip, IAR   2.2 Download the source code of deep learning framework, https://github.com/majianjia/nnom This is a pure C framework that does not   rely on hardware structure. Transplantation is very convenient     2.3 we select the example ‘bubble’ to add the Inc, port and Src folders in NNoM to the project, as shown in the figure nxf56274_0-1615450961299.png                        Figure 1 Open the file ‘port.h’ . The definitation of NNOM_LOG is changed to PRINTF (__ VA_ ARGS__ ), Open the ICF file, and change the heap size to 0x5000, define symbol__ size_ heap__ = 0x5000; Malloc, which is used in this library, allocates memory from here. If it is small, it can't run the network   2.4 Transplant fatfs file system to bubble project nxf56274_1-1615450975431.png   Figure 2   2.5 In the bubble.c file, add the following header file        #include "nnom_port.h" #include "nnom.h" #include "weights.h" #include "denoise_weights.h" #include "mfcc.h" #include "wav.h" #include "equalizer_coeff.h"   2.6 Find main.c under ‘examples\rnn-denoise’ in the framework, ‘main_arm.c’ is used for stm32. Main.c is provided for windows running routines. This code is used to open the audio file, then run the network, and finally generate noise reduction. Use this code to facilitate experiments. The APIs for file operations in this file need to be manually changed to MCU APIs. I added a progress bar display. You can refer the attachment.   2.7 This example also uses DSP, so DSP support needs to be turned on, as shown in the figure nxf56274_2-1615450986521.png                                                           Figure 3 2.8 Add macro nxf56274_3-1615450994191.png                                             Figure 4   2.9 After the compilation is passed, download the program. The tested wav needs to be named ‘sample.wav’, and the mcu will reduce noise for it. Finnally mcu will generate ‘filtered_sample.wav’. Plug the SD card into the computer to listen to the noise-reduced audio. This is serial message. nxf56274_4-1615451004815.png     Figure 5 This is the audio analyzed by the audio analysis software. The upper part is the noise reduced, and the lower part is the original sound. You can see that a lot of noise has been suppressed. nxf56274_5-1615451012178.png                                                    Figure 6 3 training Through the above steps, we have achieved audio noise reduction, so how is this data trained? You need to install tensorflow, and keras. How to train is written in the README_CN.md file. This tensorflow needs to install the gpu version, and needs to install cuda. Please check the installation yourself. 3.1 Download the voice data https://github.com/microsoft/MS-SNSD and put it under the MS-SNSD folder 3.2 Use pip3 to install the tools in requirements.txt 3.3 Run ‘noisyspeech_synthesizer.py’ directly, this will report an error. You need to change the 15-line float to int type. 3.4 Run the script gen_dataset.py to generate mfcc and gain 3.5 Run main.py, this will generate the noise file of the sample, which can be used for testing and also generated ‘weights.h,denoise_weights.h,equalizer_coeff.h’ PS: Put the code in directory 'boards/frdmk64f/demo_app'. 'sample.zip' has the noise wave.
記事全体を表示
There is new amazing feature in FreeMaster ver 1.4 ( www.freescale.com/freemaster ) - you can do the debugging and visualization of your application in FreeMASTER without adding any code in there (you do not need a serial driver of any kind to achieve the connection), just using the communication plug-in to OSDA embedded in new version of Freemaster connected instead of the debugger from IDE. The driverless use of Freemaster use is easy to use, just open the FreeMaster, assuming you have your own application, without any Freemaster driver in it. Load the application into flash memory of the KL device and close debugging session from IDE. Open FreeMaster and  go to Project/Options/Comm, use setup from picture below Choose Plug-in - use the FreeMASTER BDM Communication Plug-in, hit configure and take P&E Kinetis. you can test the connection there too. The next step is to go to Options/MAP files, navigate to *.ELF file of your project and set file format to ELF/DWARF (I have chosen .elf from some usb demo project just to show the way how to do so) well, the connection is established, now there is need to choose variables for display and visualization. Go to project/Variables and choose variables you want to follow (hit Generate.. to do so, list of variables available in your project will appear and you can choose the desired one and hit generate - it will check and generate the variable connection, you can do it for single variable, array or more variables - it is intuitive ) When desired variables are generated, close the dialog. You can make a scope or add variables to watch. To add variable to variable watch window click by right mouse button in watch area go to watch properties, Watch tab and hit Add---->> to add it between watched wariables and hit OK and value appears in the Variable Watch window. To create scope, go to project tree window and use right mouse button on NewProject, choose Create Scope... In scope properties chose the name for this scope and go to  Setup tab. You can add your variable to the scope here by choosing in drop down menu Hit OK and start the session (Ctrl+K) or hitting Stop icon in the menu, the variable is displayed in the window. The value in my case stays 0 however displays correctly... Pavel
記事全体を表示
    作者 Shaozhong Liang     YAFFS(Yet Another Flash File System)文件系统是专门针对NAND闪存设计的嵌入式文件系统。在YAFFS中,文件是以固定大小的数据块进行存储的,块的大小可以是512字节、1024字节或者2048字节。这种实现依赖于它能够将一个数据块头和每个数据块关联起来。每个文件(包括目录)都有一个数据块头与之相对应,数据块头中保存了ECC(Error Correction Code)和文件系统的组织信息,用于错误检测和坏块处理。     YAFFS在文件进行改写时总是先写入新的数据块,然后删除旧的数据块,这样即使意外掉电,丢失的也只是这一次修改数据的最小写入单位,从而实现了掉电保护,保证了数据完整性。 YAFFS是为NAND FLASH设计的,它作了以下的假设或定义。     NAND Flash是基于块(block)的,每一个Block大小相同,由整数个chunk组成。每一个Block可单独擦除。一页(page,或chunk)为Flash的分配单元。所有的访问(读或者写)都是基于页(或chunk)的。     当对NAND Flash编程时,只有二进制中的0被编程,而1则“不关心”。比如,一个字节包含的二进制数为1010,那么当编程1001,会导致这两个数的位与操作。结果为1000.这和NOR FLASH不同。     YAFFS 分别用块号和 chunk id 标示块和 chunk 。它将空块(填满0xFF)当作空闲块或者已擦除块。这样,格式化一个YAFFS分区等价于擦除所有未损坏的块。 因此YAFFS最少需要一些函数能够擦除块,读一个页,写一个页。 1. 直接接口(Direct Interface)的相关文件     仅需要提取少量文件。使用yaffs的直接接口,你不需要所有的文件。你实际需要的文件列在下面,其余文件不需要编译。 direct/yaffsfs.c yaffs_guts.c direct/yaffscfg.c yaffs_nand.c yaffs_tagsvalidity.c yaffs_checkptrw.c yaffs_qsort.c yaffs_tagscompat.c yaffs_ecc.c yaffs_packedtags2.c 2. YAFFS  存储设备     YAFFS对文件系统上的所有内容(比如正常文件,目录,链接,设备文件等等)都统一当作文件来处理,每个文件都有一个页面专门存放文件头,文件头保存了文件的模式、所有者id、组id、长度、文件名、Parent Object ID等信息。因为需要在一页内放下这些内容,所以对文件名的长度,符号链接对象的路径名等长度都有限制。前面说到对于NAND FLASH上的每一页数据,都有额外的空间用来存储附加信息,通常NAND驱动只使用了这些空间的一部分,YAFFS正是利用了这部分空间中剩余的部分来存储文件系统相关的内容。以512+16B为一个PAGE的NAND FLASH芯片为例,Yaffs文件系统数据的存储布局如下所示: 0 to 511 数据区域 512 to 515 YAFFS TAG 516 Data status byte 517 Block status byte 坏块标志位 518 to 519 YAFFS TAG 520 to 522 后256字节数据的ECC校验结果 523 to 524 YAFFS TAG 525 to 527 前256字节数据的ECC校验结果     可以看到在这里YAFFS一共使用了8个BYTE用来存放文件系统相关的信息(yaffs_Tags)。这8个Byte的具体使用情况按顺序如下: Bits Content 20 ChunkID,该page在一个文件内的索引号,所以文件大小被限制在2^20 PAGE 即512Mb 2 2 bits serial number 10 ByteCount 该page内的有效字节数 18 ObjectID 对象ID号,用来唯一标示一个文件 12 Ecc, Yaffs_Tags本身的ECC校验和 2 Unused     其中Serial Number在文件系统创建时都为0,以后每次写具有同一ObjectID和ChunkID的page的时候都加一,因为YAFFS在更新一个PAGE的时候总是在一个新的物理Page上写入数据,再将原先的物理Page删除,所以该serial number可以在断电等特殊情况下,当新的page已经写入但老的page还没有被删除的时候用来识别正确的Page,保证数据的正确性。 ObjectID号为18bit,所以文件的总数限制在256K即26万个左右。     由于文件系统的基本组织信息保存在页面的备份空间中,因此,在文件系统加载时只需要扫描各个页面的备份空间,即可建立起整个文件系统的结构,而不需要像JFFS1/2 那样扫描整个介质,从而大大加快了文件系统的加载速度。     一个YAFFS设备是一个逻辑设备,它代表了一个物理设备的部分或整体。你可以认为它是一个Nand上的一个“分区”。比如,该分区可能覆盖整个NAND,也许只是一半,而另外一半就是另一个Yaffs_Device.它也可以用于你使用一个非flash设备(比如RAM)来测试的情况下。 一个Yaffs_Device记录了起始和结束块。通过改变它的起始和结束块,你就可以在同一个物理设备上使用不止一个的Yaffs_Device。 这里将需要你自己建立的Yaffs_Device结构的数据域列出,其他数据域由Yaffs自动创建。 int nDataBytesPerChunk     如其名,这是每一个chunk的字节数,还记得吧,在yaffs术语中,一个页就是一个chunk,因而它也是一页的字节数。它是数据字节数,即不包含OOB的数据。比如一页时2048字节+64字节的OOB,那么数值nDataBytesPerChunk为2048。 int nChunksPerBlock     物理Nand设备中每页包含的chunk(就是Nand上的页)的数目,最少是2。 int spareBytesPerChunk     空闲域(spare area)大小,比如:每个chunk(页)的OOB字节数。 int startBlock     该逻辑Yaffs_Device设备第一个块的块号(而字节地址),注意,yaffs需要第一个块是空闲的,因此你不可以设置该变量为0,如果设置为0,Yaffs会给它加1,并且会在结束块号上也加1,在你设置设备从块0开始,到最后一个块结束,这意味着yaffs试图写一个不存在的块,从而出现错误。 int endBlock     该逻辑Yaffs_Device设备的最后一个块号。如果startBlock为0,那么yaffs会使用endBlock+1,至少使startBlock+nReservedBlocks+2 int nReservedBlocks     这是YAFFS必须保留,用于垃圾回收和块错误恢复的可擦除块的数目。至少是2,但是5更好。如果你使用一个不会损坏的介质,比如RAM或者RAM盘,或者主机文件系统模拟,那么可以是2。 int nShortOpCaches     配置当前设备YAFFS Cache项的数目。0值表示不使用cache。对于大多数系统,推荐使用10到20之间的一个数值。不能大于YAFFS_MAX_SHORT_OP_CACHES定义的数值。 int useNANDECC     这是一个标志,用于指示是由yaffs执行ECC计算,还是由NAND驱动程序来执行ECC计算。(译者注:此数值取0,则使用yaffs来执行ECC计算,软件ECC计算。如果想要使用硬件ECC校验时,应该设置为1,并且在NAND驱动程序中加入硬件ECC校验的代码。) void *genericDevice     这是一个指针,它应该指向任何数据,底层NAND驱动程序需要知道以从物理设备读、写。 int isYaffs2     我们使用的是否YAFFS2版本? int inbandTags     是否为OOB区,如果不是,那么它为真,仅用于yaffs2 u32 totalBytesPerChunk     这个名字可能有点误导人,它应该等于nDataBytesPerChunk ,而非其名字暗示的nDataBytesPerChunk + spareBytesPerChunk。如果inbandTags为真,那么yaffs设置nDataBytesPerChunk,因此有足够的空闲空间存储数据,yaffs会在空闲域中正常存储。 write/readChunkWithTagsFromNAND, markNANDBlockBad queryNANDBlock 这些都是函数指针,你需要提供这些函数来给YAFFS,读写nand flash。 3.NAND Flash 访问函数 int (*writeChunkWithTagsToNAND) (struct yaffs_DeviceStruct * dev, int chunkInNAND, const u8 * data, const yaffs_ExtendedTags * tags);   dev: 要写入的yaffs_Device逻辑设备. chunkInNAND: 将chunk写入的页 Data: 指向需要写入的数据的指针 tags: 未压缩(打包)的OOB数据 Return: YAFFS_OK / YAFFS_FAIL 该函数将页(chunk)写入nand中,向nand中写入数据。数据和标签(tags)永远不应为 NULL. chunkInNand 是将要写入的页的页号,而不是需要转换的地址。 int (*readChunkWithTagsFromNAND) (struct yaffs_DeviceStruct * dev, int chunkInNAND, u8 * data, yaffs_ExtendedTags * tags);  dev: 要写入的yaffs_Device逻辑设备. chunkInNAND: 将chunk读入的页 Data: 指向需要读入的数据的缓冲区指针 tags: 指向未压缩(打包)的OOB数据的缓冲区指针 Return: YAFFS_OK / YAFFS_FAIL 该函数执行上一个函数的相反的功能,首先,读取数据和OOB字节,接着将这些输入放在一个由参数data指向的缓冲区中 int (*markNANDBlockBad) (struct yaffs_DeviceStruct * dev, int blockNo);   dev: 要写入的yaffs_Device逻辑设备. blockNo: 要标记的块. Return: YAFFS_OK / YAFFS_FAIL int (*queryNANDBlock) (struct yaffs_DeviceStruct * dev, int blockNo, yaffs_BlockState * state, u32 *sequenceNumber);   dev: 要写入的Yaffs_Device逻辑设备. blockNo: 要标记的块. state: Upon returning this should be set to the relevant state of this particular block. Sequance number: 该块的顺序号(The Sequence number),为0表示此块未使用 Return: YAFFS_OK / YAFFS_FAIL     它应检查一个块是否是有效的。如果在OOB中设置了坏块标记,那么*state应该被赋值为YAFFS_BLOCK_STATE_DEAD,*sequenceNumber赋值为0,然后返回YAFFS_FAIL。     如果该块没坏,那么应解压缩标签。标签解压缩后,若发现chunk已使用(查看tags.chunkUsed),则*sequenceNumber应赋值为tags.sequenceNumber,*state赋值为YAFFS_BLOCK_STATE_NEEDS_SCANNING,否则该块未使用,则*sequenceNumber赋值为0,*state赋值为YAFFS_BLOCK_STATE_EMPTY 4. YAFFS的缓存机制     由于NandFlash是有一定的读写次数的,所以在对一个文件进行操作的时候往往是先通过缓冲进行,对最后一次性写入NandFlash,这有效的减少了用户对NandFlash的频繁操作,延长了NandFlash的寿命。下面大致说一下YAFFS的缓存机制: 4.1.首先在yaffs_mount的时候会对yaffs_dev这个结构体进行注册,和缓冲部分相关的有: dev->nShortOpCaches//这个变量决定了有多少个缓冲,因为缓冲会大量的占用堆栈的空间,所以在yaffs不建议缓冲的数量很大,即使你填一个很大的数,系统也不会超过YAFFS_MAX_SHORT_OP_CACHES的总数。 yaffs_ChunkCache *srCache;//缓冲区的首地址,dev->srCache = YMALLOC( dev->nShortOpCaches * sizeof(yaffs_ChunkCache));下面介绍一下缓冲区这个结构体的组成: typedef struct { struct yaffs_ObjectStruct *object;//一个缓冲区对应一个文件 int chunkId; int lastUse; //通过lastUse来 int dirty; //标志了这一个缓冲区是否被使用 int nBytes; __u8 data[YAFFS_BYTES_PER_CHUNK];//数据区 } yaffs_ChunkCache; 4.2.什么时候用到缓冲区?        用到缓冲区最多的地方显而易见是对已经创建的文件进行写操作。而且是需要写的大小和512不一致的时候,这是因为如果是刚好512的话,系统会直接写入NandFlash中。对于小于512的系统首先会调用yaffs_FindChunkCache(in,chunk)这个函数来判断in这个object是否在缓冲区中存在。如果存在会调用已有缓冲区进行操作。当然如果是第一次对一个object进行操作,肯定在缓冲区中是不存在对应它的空间的,因此系统会调用yaffs_GrabChunkCache函数为此次操作分配一个缓冲区。 5. 应用层接口     YAFFS为连接的应用程序提供了一组函数。大部分跟标准C库函数,如open/close一致,只是增加了yaffs_前缀,如 yaffs_open. 这些函数定义在direct/yaffsfs.h中。     初始化yaffs来完成读写,你必须在每个你要使用的yaffs设备上调用yaffs_mount。比如yaffs_mount(”/boot”)。这可以在系统启动的时候执行,如果存在一个操作系统,那么程序需要考虑这点。在你完成使用的时候,你也需要调用yaffs_umount函数,这样yaffs就会将它需要状态写入磁盘。 如果读写文件的应用层接口已经存在,你可以根据相关的操作系统调用来封装相关的函数调用。 1 yaffs_mount( ) 功能说明:加载指定器件。 输入参数:path    要加载的器件。 输出参数:无。 返回值: 表明加载的状态。 调用的函数:yaffsfs_FindDevice( )、yaffs_GutsInitialise( )。 2 yaffs_open( ) 功能说明:按照指定方式打开文件。 输入参数:path    文件的绝对路径;           Oflag   打开的方式;           Mode    文件许可模式。 输出参数:无。 返回值:句柄。 调用的函数:yaffsfs_GetHandle( )、yaffsfs_FindDirectory( )、yaffs_MknodFile( )、yaffsfs_PutHandle( )、yaffs_ResizeFile( )、yaffsfs_FindObject( )。 3 yaffs_write( ) 功能说明:根据打开文件的句柄,从指定数组处读指定字节写入文件中。 输入参数:fd      要写入的文件的句柄;           Buf     要写入的数据的首地址;           Nbyte   要写入的字节数。 输出参数:无。 返回值: 写入了的字节数。 调用的函数:yaffs_WriteDataToFile( )、yaffsfs_GetHandlePointer( )、yaffsfs_GetHandleObject( ) 4 yaffs_read( ) 功能说明:根据打开文件的句柄,从文件中读出指定字节数据存入指定地址。 输入参数:fd       要读出的文件的句柄;           Buf      读出文件后要存入的数据的首地址;           Nbyte    要读出的字节数。 输出参数:无。 返回值: 读出了的字节数。 调用的函数:yaffs_ReadDataFromFile( )、yaffsfs_GetHandlePointer( ) 5 yaffs_close( ) 功能说明:关闭已经打开的文件句柄,yaffs 有缓冲机制,当调用yaffs_close()关闭文件之后能够保证将内容写入nandflash。 输入参数:fd    需要关闭的文件的句柄; 输出参数:无。 返回值:无。 6. YAFFS在MQX的应用案例     YAFFS提供了直接调用模式,可以方便移植到 none-OS或者light-weighted OS中。附件是将YAFFS移植到Freescale MQX实时操作系统的源代码和工程,可以在II型集中器的Demo Board上运行。     初步的测试表明YAFFS工作正常,能够完成创建目录,创建/删除文件,读/写文件操作等。 YAFFS非常适合none-OS或者是light-weighted OS,使用YAFFS需要关注的是RAM的消耗,适合小量文件(<20)。 如果不想使用MQX默认的MFS(FAT32文件系统),YAFFS可以作为一个文件系统的备选方案。
記事全体を表示
This is an update to the KE0x Driver Library package with the example projects ported to Kinetis Design Studio (KDS).  These examples support the following boards: FRDM-KE02 FRDM-KE04 FRDM-KE06 The examples were tested with KDS v3.0.0
記事全体を表示
[EEPROM emulation driver for KEA128 and KEA8] software used for Kinetis EA family product (without integrated EEPROM memory), which using the sector-erasable Flash memory be used to emulate the EEPROM through EEPROM emulation software.  The software could downloaded from here: This document will interpret EEPROM emulation driver demo for KEA128 product and shows how the EEPROM emulation driver works and related API function introduction. 1> EEPROM emulation driver feature The EEPROM emulation driver for SGF/FTM flash family implements the fix-length data record scheme. Several sectors shall be involved in emulation with a round robin scheduling scheme. The EEPROM functionalities to be emulated include initializing, de-initializing, reading, writing records. The EEPROM emulation driver is more complicated than general Flash program data application with following features: User configurable emulated EEPROM size. Larger life for the flash memory used for EEPROM emulation. Unique feature of Cache Table which makes data retrieval fast. Support fix length record scheme only. Support synchronous model which can be run from both RAM and FLASH. When running from FLASH, user needs to relocate flash launch command routine to RAM to avoid Read While Write error. If any operation fails during EEPROM emulation, the driver will try to repeat that operation until successfully for several times (which is defined by user). If that operation still fails, the driver will make the related sector to DEAD to eliminate it from round robin sequence and continue other tasks without stopping driver. Concurrency support via callback. Release in C source code format. Ready-to-use demos illustrating the usage of the driver with different compilers. 2> Demo interpretation The demo routine located at default installation path: ..\\KEA EEPROM Emulation Driver\KEA_SGF180\Demos\build\TRK_KEAZ128\iar\Normal_demo folder. For the demo runs in Flash memory, avoiding Read While Write error happened, Eed_FlashLauchnCommand and g_EECallBack must be relocated to or placed in RAM when the main routine start. Then it will disable the cache and initialize Flash clock(KEA128 ICS module default clock mode is FEI, the default system/core clock is 21MHz, the Flash clock divider value set to 20 to make Flash clock to be 1MHz).   After flash clock initialized, it will initialize EEPROM configuration start address. The status of each sector with five value, which means Blanked, Alternative, Active, Dead and Invalid. The EE_ALLOTED_SECTORS macro will calculate the total number of sectors, which includes Active sectors and Alternative sectors. #define EE_ALLOTED_SECTORS              (EE_ACTIVE_SECTORS + EE_READY_SECTORS) The EE_ACTIVE_SECTORS value is 1 and EE_READY_SECTORS value is 2, so the EE_ALLOTED_SECTORS value is 3. Then there with three allotted sector, and allocated at below address:      eepromConfig.startSecAddr[0] = 0x1A00;      eepromConfig.startSecAddr[1] = 0x1C00;      eepromConfig.startSecAddr[2] = 0x1E00; After initialize start address for EEPROM configuration, following to call Eed_DeinitEeprom() function to erase all sectors used for emulation. Then it will initialize EEPROM emulation, includes to remove dead sector from EEPROM system and determine maximum valid index in array of start sector address after that; also includes initialize all sectors by erasing the “possible-error-sector”; and initialize and update cache table if enabled. It call Eed_InitAllSectors() function to initialize all sectors and allocate the current active sector to base sector. The Eed_ShiftIdxToBase() function will be called to shift the current index to base index of 0. After that, the EEPROM configuration startSecAddr array will change to :      eepromConfig.startSecAddr[0] = 0x1E00;      eepromConfig.startSecAddr[1] = 0x1A00;      eepromConfig.startSecAddr[2] = 0x1C00; The active sector start address at 0x1E00. Then it will program erase cycle value to each sector start address, the erase cycle value will occupy 4 bytes with sector start address offset 0: Then make the base sector to be active and program the active indicator at sector start address offset 8. Here the base sector start address is 0x1E00, the active indicator will be programmed at 0x1E08 with active indicator value 0x55555555: Then it will call Eed_SearchBlankSpace () function to find blank space of EEPROM system, in this demo, the blank space start address at 0x1e0c. If enable the Flash cache, the cache will be cleared and updated during EEPROM emulation initialize phase. The demo will write eight group data to EEPROM system, each group with 16 bytes data, total data number is 128 bytes. The data located at Flash start address is 0x1e0c. After each group data programming, it will following with the data ID info and program the status. With all data was written, the all 128 bytes data was programed at 0x1e00 start EEPROM sector. When the write data exceed the active EEPROM sector, the swapping will occur. The swapped EEPROM sector will record previous data and current write data. If there exist sector erase action, it will also update the erase cycle value. The data is full and the new data written will make swap happens: After swap happens: At the end of demo, it will read EEPROM data back and make sure all valid record ID are written to EEPROM emulation.
記事全体を表示
        在我们嵌入式工程应用中,中断作为最常用的异步手段是必不可少的,而且在一个应用程序中,一个中断往往是不够用的,多个中断混合使用甚至多级中断嵌套也经常会使用到,而这样就涉及到一个中断优先级的问题。         以我们最熟悉的Cortex-M系列为例,我们知道ARM从Cortex-M系列开始引入了NVIC的概念(Nested Vectors Interrupts Controller),即嵌套向量中断控制器,以它为核心通过一张中断向量表来控制系统中断功能,NVIC可以提供以下几个功能: 1)可嵌套中断支持; 2)向量中断支持; 3)动态优先级调整支持; 4)中断可屏蔽。         抛开其他不谈,这里我们只说说中断优先级的问题。我们知道NVIC的核心工作原理即是对一张中断向量表的维护上,其中M4最多支持240+16个中断向量,M0+则最多支持32+16个中断向量,而这些中断向量默认的优先级则是向量号越小的优先级越高,即从小到大,优先级是递减的。但是我们肯定不会满足于默认的状态(人往往不满足于约束,换句俗话说就是不喜欢按套路出牌,呵呵),而NVIC则恰恰提供了这种灵活性,即支持动态优先级调整,无论是M0+还是M4除了3个中断向量之外(复位、NMI和HardFault,他们的中断优先级为负数,它们3个的优先级是最高的且不可更改),其他中断向量都是可以动态调整的。         不过需要注意的是,中断向量表的前16个为内核级中断,之后的为外部中断,而内核级中断和外部中断的优先级则是由两套不同的寄存器组来控制的,其中内核级中断由SCB_SHPRx寄存器来控制(M0+为SCB_SHPR[2:3],M4为SCB_SHPR[1:3]),外部中断则由NVIC_IPRx来控制(M0+为NVIC_IPR[0:7],M4为NVIC_IPR[0:59]),如下图所示: M0+中断优先级寄存器: M4中断优先级寄存器:         其中M4所支持的动态优先级范围为0~15(8位中只有高四位[7:4]才有效),而M0+所支持的动态优先级范围则为0~3(8位中只有高两位[7:6]才有效),而且秉承着号越小优先级越高的原则(0最高,15或3为最小),同时也间接解释了为什么复位(-3)、NMI(-2)和HardFault(-1)优先级最高的原因,很简单,人家都是负的了,谁还能比他们高,呵呵,而且这三位中复位优先级最高,NMI其次,HardFault最低(这个最低仅限于这三者)。 下面给出个ARM CMSIS库中关于M0+和M4中断优先级设置的API函数NVIC_SetPriority(IRQn_Type IRQn, uint32_t priority)实现供大家来参考: M0+: NVIC_SetPriority(IRQn_Type IRQn, uint32_t priority) {   if(IRQn < 0) {     SCB->SHP[_SHP_IDX(IRQn)] = (SCB->SHP[_SHP_IDX(IRQn)] & ~(0xFF << _BIT_SHIFT(IRQn))) |         (((priority << (8 - __NVIC_PRIO_BITS)) & 0xFF) << _BIT_SHIFT(IRQn)); }  /* set Priority for Cortex-M  System Interrupts */   else {     NVIC->IP[_IP_IDX(IRQn)] = (NVIC->IP[_IP_IDX(IRQn)] & ~(0xFF << _BIT_SHIFT(IRQn))) |         (((priority << (8 - __NVIC_PRIO_BITS)) & 0xFF) << _BIT_SHIFT(IRQn)); }   /* set Priority for device specific Interrupts  */ } M4: void NVIC_SetPriority(IRQn_Type IRQn, uint32_t priority) {   if(IRQn < 0) {     SCB->SHP[((uint32_t)(IRQn) & 0xF)-4] = ((priority << (8 - __NVIC_PRIO_BITS)) & 0xff); } /* set Priority for Cortex-M  System Interrupts */   else {     NVIC->IP[(uint32_t)(IRQn)] = ((priority << (8 - __NVIC_PRIO_BITS)) & 0xff);    }        /* set Priority for device specific Interrupts  */ }
記事全体を表示