GPIO based method to do touch sensing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

GPIO based method to do touch sensing

GPIO based method to do touch sensing

With the HMI developing, touch sensing is more and more popular. The GPIO-based method was developed as a low-cost way to do touch sensing. NXP had developed this sensing method and provide as TSS library (which combines support for GPIO and hardware-based touch sensing).The GPIO method uses the RC charge time in a capacitor (the electrode or touch pad)

图片1.png

图片2.png

 

Measurement Principles: TSI Method

TSI method uses configurable current sources. The current sources are active outputs, making them far more robust against noise. Current sources are configurable, making it possible to configure sampling time. The signal slope depends on the applied current and the capacitance. When a finger approaches the electrode, frequency decreases.

Another oscillator, uses a internal unchanging capacitor, this is our reference, we will configure it to oscillate faster than the external one. By comparing how many reference oscillations where counted by the TSI module per external reference scan, we can know when a touch happened.

无评分
版本历史
最后更新:
‎10-10-2016 09:24 PM
更新人: