UUU issues on IMX6SX

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

UUU issues on IMX6SX

857 次查看
mabar52
Contributor III

Trying to build write and boot u-boot with uuu utility. 
Our board is based on the sabresd reference with IMX6SX and qspi-flash.

 

 

SO-AP-SE-19:uuu root# ./uuu -lsusb
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.125-5-g1a9d927

Connected Known USB Devices
Path Chip Pro Vid Pid BcdVersion
==================================================
2:11 MX6SX SDP: 0x15A2 0x0071 0x0001



SO-AP-SE-19:uuu root# ./uuu -s
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.125-5-g1a9d927

Build in config:
Pctl Chip Vid Pid BcdVersion
==================================================
SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff]
SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff]
SDPS: MX8DXL 0x1fc9 0x0147
SDPS: MX28 0x15a2 0x004f
SDPS: MX815 0x1fc9 0x013e
SDPS: MX865 0x1fc9 0x0146
SDPS: MX8ULP 0x1fc9 0x014a
SDPS: MX8ULP 0x1fc9 0x014b
SDPS: MX93 0x1fc9 0x014e
SDP: MX7D 0x15a2 0x0076
SDP: MX6Q 0x15a2 0x0054
SDP: MX6D 0x15a2 0x0061
SDP: MX6SL 0x15a2 0x0063
SDP: MX6SX 0x15a2 0x0071
SDP: MX6UL 0x15a2 0x007d
SDP: MX6ULL 0x15a2 0x0080
SDP: MX6SLL 0x1fc9 0x0128
SDP: MX7ULP 0x1fc9 0x0126
SDP: MXRT106X 0x1fc9 0x0135
SDP: MX8MM 0x1fc9 0x0134
SDP: MX8MQ 0x1fc9 0x012b
SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff]
SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998]
SDPV: SPL1 0x1fc9 0x0151 [0x0500..0x9998]
SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999]
SDPU: SPL 0x3016 0x1001 [0x0000..0x04ff]
SDPV: SPL1 0x3016 0x1001 [0x0500..0x9998]
FBK: 0x066f 0x9afe
FBK: 0x066f 0x9bff
FBK: 0x1fc9 0x0153
FB: 0x0525 0xa4a5
FB: 0x18d1 0x0d02
FB: 0x3016 0x0001
FB: 0x1fc9 0x0152
FB: 0x0483 0x0afb

Please input command:
U>SDP: dcd -f files/u-boot-smartoptics-dcp.imx-memtest
>Start Cmd:SDP: dcd -f files/u-boot-smartoptics-dcp.imx-memtest
New USB Device Attached at 2:11
100%2:11>Okay (0.009s)
Okay
U>SDP: write -f files/u-boot-smartoptics-dcp.imx-memtest
2:11>Start Cmd:SDP: write -f files/u-boot-smartoptics-dcp.imx-memtest
New USB Device Attached at 2:11
0%2:11>Fail HID(W):LIBUSB_ERROR_IO(0.004s)
HID(W):LIBUSB_ERROR_IO

 

 


Is there a way to further debug this to know why the error occurs.
With another build u-boot configutation:

 

 

SDP: dcd -f files/u-boot-memtest-DCP-R8.0-r0.imx
SDP: write -f files/u-boot-memtest-DCP-R8.0-r0.imx -ivt 0
SDP: jump -f files/u-boot-memtest-DCP-R8.0-r0.imx -ivt 0
SO-AP-SE-19:uuu root#
SO-AP-SE-19:uuu root#
(reverse-i-search)`-s': cat dcp-start-u-boot.lst.memtest
SO-AP-SE-19:uuu root# ./uuu -s
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.125-5-g1a9d927

Build in config:
        Pctl     Chip            Vid     Pid     BcdVersion
        ==================================================
        SDPS:    MX8QXP          0x1fc9  0x012f  [0x0002..0xffff]
        SDPS:    MX8QM           0x1fc9  0x0129  [0x0002..0xffff]
        SDPS:    MX8DXL          0x1fc9  0x0147
        SDPS:    MX28            0x15a2  0x004f
        SDPS:    MX815           0x1fc9  0x013e
        SDPS:    MX865           0x1fc9  0x0146
        SDPS:    MX8ULP          0x1fc9  0x014a
        SDPS:    MX8ULP          0x1fc9  0x014b
        SDPS:    MX93            0x1fc9  0x014e
        SDP:     MX7D            0x15a2  0x0076
        SDP:     MX6Q            0x15a2  0x0054
        SDP:     MX6D            0x15a2  0x0061
        SDP:     MX6SL           0x15a2  0x0063
        SDP:     MX6SX           0x15a2  0x0071
        SDP:     MX6UL           0x15a2  0x007d
        SDP:     MX6ULL          0x15a2  0x0080
        SDP:     MX6SLL          0x1fc9  0x0128
        SDP:     MX7ULP          0x1fc9  0x0126
        SDP:     MXRT106X        0x1fc9  0x0135
        SDP:     MX8MM           0x1fc9  0x0134
        SDP:     MX8MQ           0x1fc9  0x012b
        SDPU:    SPL             0x0525  0xb4a4  [0x0000..0x04ff]
        SDPV:    SPL1            0x0525  0xb4a4  [0x0500..0x9998]
        SDPV:    SPL1            0x1fc9  0x0151  [0x0500..0x9998]
        SDPU:    SPL             0x0525  0xb4a4  [0x9999..0x9999]
        SDPU:    SPL             0x3016  0x1001  [0x0000..0x04ff]
        SDPV:    SPL1            0x3016  0x1001  [0x0500..0x9998]
        FBK:                     0x066f  0x9afe
        FBK:                     0x066f  0x9bff
        FBK:                     0x1fc9  0x0153
        FB:                      0x0525  0xa4a5
        FB:                      0x18d1  0x0d02
        FB:                      0x3016  0x0001
        FB:                      0x1fc9  0x0152
        FB:                      0x0483  0x0afb

Please input command:
U>SDP: dcd -f files/u-boot-memtest-DCP-R8.0-r0.imx
>Start Cmd:SDP: dcd -f files/u-boot-memtest-DCP-R8.0-r0.imx
New USB Device Attached at 2:11
2:11>Okay (0.004s)
Okay
U>SDP: write -f files/u-boot-memtest-DCP-R8.0-r0.imx -ivt 0
2:11>Start Cmd:SDP: write -f files/u-boot-memtest-DCP-R8.0-r0.imx -ivt 0
New USB Device Attached at 2:11
2:11>Fail HID(W):LIBUSB_ERROR_TIMEOUT(2.157s)

 

 

We use several u-boot compilations that serve different purposes and we have recently upgrade our yocto environment from 2.7 to 4. We have several patches and separate defconfigs that are applied depending on what kind of u-boot configuration that is built.

I suspect that I miss some kCONFIG to u-boot, not sure how to check that, though.

This is an old build that works and I can see through the console that u-boot is started:

 

 

U>SDP: dcd -f files/u-boot-qspi2-DCP-R7.0-r0.imx
>Start Cmd:SDP: dcd -f files/u-boot-qspi2-DCP-R7.0-r0.imx
New USB Device Attached at 2:11
100%2:11>Okay (0.008s)
Okay
U>SDP: write -f files/u-boot-qspi2-DCP-R7.0-r0.imx -ivt 0
2:11>Start Cmd:SDP: write -f files/u-boot-qspi2-DCP-R7.0-r0.imx -ivt 0
New USB Device Attached at 2:11
100%2:11>Okay (0.178s)
Okay
U>SDP: jump -f files/u-boot-qspi2-DCP-R7.0-r0.imx -ivt 0
2:11>Start Cmd:SDP: jump -f files/u-boot-qspi2-DCP-R7.0-r0.imx -ivt 0
New USB Device Attached at 2:11
100%2:11>Okay (7.03s)
Okay
U>

 

 



Any help is most welcome, of course.

0 项奖励
回复
0 回复数