IMX6UL ethernet issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6UL ethernet issue

1,308 次查看
dineshsehrawat
Contributor I

Hi,

i am using the customized board based on imx6UL using Linux. While i ma booting my board with sdcard then ethernet is working fine on u-boot, i am able to ping b/w board and laptop. But when i am booting my board using imx6 usb loader then ethernet is not working on u-boot.

In both cases u-boot.imx is same.

Below are the logs:-

board_mmc_init...
switch to partitions #0, OK
mmc1 is current device
Net: Phy 1 not found
PHY reset timed out
FEC0
Boot from USB for mfgtools
Use default environment for mfgtools
Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};
Hit any key to stop autoboot: 0
Bad Linux ARM zImage magic! 

Thanks-

Dinesh

标记 (3)
0 项奖励
回复
0 回复数