Instead to use gst-launch to play your audio/video media you can create an application do to that. This application was tested in iMX27ADS but should to work on iMX27PDK First execute LTIB (./ltib -c) and select these packages: all gstreamer plugin, alsa-utils and libmad. Create your file code (i.e.: playvideo.c): #include <gst/gst.h>
#include <glib.h> #include <string.h>
static GstElement *source, *demuxer, *vdqueue, *adqueue, *vdsink, *adsink, *decvd, *decad; void on_pad_added (GstElement *element, GstPad *pad) { g_debug ("Signal: pad-added"); GstCaps *caps; GstStructure *str; caps = gst_pad_get_caps (pad); g_assert (caps != NULL); str = gst_caps_get_structure (caps, 0); g_assert (str != NULL); if (g_strrstr (gst_structure_get_name (str), "video")) { g_debug ("Linking video pad to dec_vd"); // Link it actually GstPad *targetsink = gst_element_get_pad (decvd, "sink"); g_assert (targetsink != NULL); gst_pad_link (pad, targetsink); gst_object_unref (targetsink); } if (g_strrstr (gst_structure_get_name (str), "audio")) { g_debug ("Linking audio pad to dec_ad"); // Link it actually GstPad *targetsink = gst_element_get_pad (decad, "sink"); g_assert (targetsink != NULL); gst_pad_link (pad, targetsink); gst_object_unref (targetsink); } gst_caps_unref (caps); } static gboolean bus_call (GstBus *bus, GstMessage *msg, gpointer data) { GMainLoop *loop = (GMainLoop *) data; switch (GST_MESSAGE_TYPE (msg)) { case GST_MESSAGE_EOS: g_print ("End of stream\n"); g_main_loop_quit (loop); break; case GST_MESSAGE_ERROR: { gchar *debug; GError *error; gst_message_parse_error (msg, &error, &debug); g_free (debug); g_printerr ("Error: %s\n", error->message); g_error_free (error); g_main_loop_quit (loop); break; } default: break; } return TRUE; } int main (int argc, char *argv[]) { GMainLoop *loop; GstElement *pipeline; GstBus *bus; /* Initialisation */ gst_init (&argc, &argv); loop = g_main_loop_new (NULL, FALSE); /* Check input arguments */ if (argc != 2) { g_printerr ("Usage: %s <Video H264 filename>\n", argv[0]); return -1; } /* Create gstreamer elements */ pipeline = gst_pipeline_new ("media-player"); source = gst_element_factory_make ("filesrc","file-source"); demuxer = gst_element_factory_make ("mfw_mp4demuxer","avi-demuxer"); decvd = gst_element_factory_make ("mfw_vpudecoder", "video-decoder"); decad = gst_element_factory_make ("mad", "mp3-decoder"); vdsink = gst_element_factory_make ("mfw_v4lsink", "video-sink"); vdqueue = gst_element_factory_make ("queue", "video-queue"); adqueue = gst_element_factory_make ("queue", "audio-queue"); adsink = gst_element_factory_make ("fakesink", "audio-sink"); g_object_set (decvd, "codec-type", "std_avc", NULL); if (!pipeline || !source || !demuxer || !decvd || !decad || !vdsink || !vdqueue || !adqueue || !adsink) { g_printerr ("One element could not be created. Exiting.\n"); return -1; } /* Set up the pipeline */ /* we set the input filename to the source element */ g_object_set (G_OBJECT (source), "location", argv[1], NULL); /* we add a message handler */ bus = gst_pipeline_get_bus (GST_PIPELINE (pipeline)); gst_bus_add_watch (bus, bus_call, loop); gst_object_unref (bus); /* we add all elements into the pipeline */ /* file-source | ogg-demuxer | vorbis-decoder | converter | alsa-output */ gst_bin_add_many (GST_BIN (pipeline), source, demuxer, decvd, decad, adqueue, vdqueue, vdsink, adsink, NULL); /* we link the elements together */ /* file-source -> ogg-demuxer ~> vorbis-decoder -> converter -> alsa-output */ gst_element_link (source, demuxer); gst_element_link (decvd, vdqueue); gst_element_link (vdqueue, vdsink); //gst_element_link (decad, adqueue); gst_element_link (adqueue, adsink); g_signal_connect (demuxer, "pad-added", G_CALLBACK (on_pad_added), NULL); /* note that the demuxer will be linked to the decoder dynamically. The reason is that Ogg may contain various streams (for example audio and video). The source pad(s) will be created at run time, by the demuxer when it detects the amount and nature of streams. Therefore we connect a callback function which will be executed when the "pad-added" is emitted.*/ /* Set the pipeline to "playing" state*/ g_print ("Now playing: %s\n", argv[1]); gst_element_set_state (pipeline, GST_STATE_PLAYING); /* Iterate */ g_print ("Running...\n"); g_main_loop_run (loop); /* Out of the main loop, clean up nicely */ g_print ("Returned, stopping playback\n"); gst_element_set_state (pipeline, GST_STATE_NULL); g_print ("Deleting pipeline\n"); gst_object_unref (GST_OBJECT (pipeline)); return 0; }
Create a directory inside your ltib directory to compile your source code: $ mkdir ~/your-ltib-dir/rpm/BUILD/gst Enter on LTIB shell mode: $ ./ltib -m shell Entering ltib shell mode, type 'exit' to quit LTIB> Enter in your application dir: LTIB> cd rpm/BUILD/gst/ Compile your application: LTIB> gcc -Wall $(pkg-config --cflags --libs gstreamer-0.10) playvideo.c -o playvideo If everything worked file you will get a "playvideo" arm binary: LTIB> file playvideo playvideo: ELF 32-bit LSB executable, ARM, version 1 (SYSV), for GNU/Linux 2.6.14, dynamically linked (uses shared libs), not stripped Now just copy it to ~/your-ltib-dir/rootfs/home. Start your board using this rootfs and execute: root@freescale ~$ cd /home/ root@freescale /home$ ./playvideo your-file-h264-mp3.avi Now playing: your-file-h264-mp3.avi Running...
View full article