NXP wireless solutions build upon decades of Wi-Fi, Bluetooth®, multiprotocol silicon, software and system design expertise, including 802.15.4 in the latest tri-radio architectures. NXP is committed to driving large-scale deployment across multiple markets by a broad array of power- and cost-optimized Wi-Fi, Bluetooth and 802.15.4 transceivers, enabling products with advanced Wi-Fi and multiradio capabilities including Wi-Fi 4, Wi-Fi 5 and Wi-Fi 6 chips.
Market
Product
Wi-Fi Spec
Wi-Fi Support
Summary
IoT
IW623
802.11ax (Wi-Fi 6E)
2x2 Tri-band (2.4G/5/7 GHz)
+ 1x1 Single Band (2.4 GHz)
supports Wi-Fi 6E, with a high-performance 2x2 tri-band module for fast and flexible connectivity, plus an extra 1x1 2.4 GHz module likely for compatibility or low-power tasks
IoT
IW693
802.11ax (Wi-Fi 6/6E)
CDW 2x2 Dual Band (5-7 GHz)
+ 1x1 Single Band (2.4 GHz)
High-speed, low-latency connectivity on modern bands (5 and 6 GHz). Compatibility with older devices via 2.4 GHz A 2x2 MIMO setup for better performance, plus a 1x1 fallback for basic connections
IoT
IW610
802.11ax
(Wi-Fi 6)
1x1 DB
(2.4/5 GHz)
IoT
IW612
802.11ax
(Wi-Fi 6)
1x1 DB
(2.4/5 GHz)
IoT
IW611
802.11ax
(Wi-Fi 6)
1x1 DB
(2.4/5 GHz)
IoT
IW620
802.11ax
(Wi-Fi 6)
2x2 DB
(2.4/5 GHz)
IoT
IW416
802.11n
(Wi-Fi 4)
1x1 DB
(2.4/5 GHz)
Markets
Product
Wi-Fi Spec
Wi-Fi Support
Summary
Wireless MCU Hostless
RW612
802.11ax (Wi-Fi 6)
1x1 DB
(2.4/5 GHz)
supports Wi-Fi 6, has a single antenna (1x1), and can connect to both 2.4 GHz and 5 GHz networks.
Wireless MCU Hostless
RW610
802.11ax (Wi-Fi 6)
1x1 DB
(2.4/5 GHz)
supports Wi-Fi 6, has a single antenna (1x1), and can connect to both 2.4 GHz and 5 GHz networks.
Markets
Product
Wi-Fi Spec
Wi-Fi Support
Automotive
AW692
802.11ax
(Wi-Fi 6)
2x2 + 1x1 CDW DB
(2.4/5GHz + 2.4Ghz)
Automotive
AW693
802.11ax
(Wi-Fi 6E)
2x2 + 1x1 CDW TB
(2.4/5/6Ghz + 2.4Ghz)
Automotive
AW611
802.11ax
(Wi-Fi 6)
1x1 DB
(2.4/5 GHz)
Automotive
AW690
802.11ax
(Wi-Fi 6)
1x1 CDW DB
(2.4/5 GHz)
Wireless Module Partners
Leading wireless connectivity solution providers offer NXP wireless modules in their wireless connectivity solutions. Module manufacturers develop Wi-Fi modules using NXP’s broad portfolio of Wi-Fi chips (system-on-chip (SoC)), including Wi-Fi 6 chips, Wi-Fi and Bluetooth® combo integrated circuits (ICs) and tri-radio SoCs with 802.15.4. NXP enables a broad range of wireless applications with an ecosystem of wireless module partners.
Why Use a Module Vendor?
Accelerate time-to-market
Avoid the complexity of RF design and testing
Ensure regulatory compliance more easily (e.g. FCC, CE, ISED)
Focus on the host product’s functionality while relying on the vendor for wireless performance
Useful Links
Wi-Fi Basic concepts: This post provides information about the different terms used in Wi-Fi, 802.11 standards and the three types of 802.11 MAC frames.
Wi-Fi Security Concepts: This post covers the security and authentication processes
Wi-Fi Connection/Disconnection process: In 802.11 standards, the connection procedure includes three major steps that shall be performed to make the device part of the Wi-Fi network and communicate in the network.
Wi-Fi Software Drivers Locations: NXP Recommends using Wi-Fi source code drivers
WiFi_BT_Integretation-(Linux_BSP_compilation_for_iMX_platform): This article describes how to compile the Linux BSP of the i.MX platform under ubuntu 18.04, 20.04 LTS and debian-10. This is a necessary step to integrate WIFI/BT to the I.MX platform. See the attachment for detailed steps.
Enabling i.MX8MP-EVK uSDHC1 M.2 for Wi-Fi on Android-11.0.0_2.6.0: Detailed steps on enabling usdhc1
NXP Wi-Fi and Bluetooth Product: The article will introduce how to build Wi-Fi Mass Market Driver
Wi-Fi Firmware Automatic Recovery on RW61x: This article introduces the Wi-Fi automatic recovery feature as well as how to enable and verify it on RW61x SDK.
Access Point Wi-Fi configuration on i.MX8 Family: This guide explains how to achieve that, using the i.MX8M Plus EVK (8MP) as the AP device and the i.MX8M Mini EVK (8MM) as the connected device.
How to connect to a Wi-Fi network on i.MX8MP: this article guides you step by step how to connect to a Wi-Fi network
NXP Wi-Fi/Bluetooth firmware on the i.MX8M series: steps to replace Wi-Fi/Bluetooth firmware on the i.MX8M series on Linux
Enabling Wi-Fi on Zephyr projects with the FRDM-RW612: In this guide, we'll modify the mqtt_publisher example—originally designed for Ethernet—to work with Wi-Fi instead
Training
FRDM-iMX91 connectivity Wi-Fi Basic Hands-on
FRDM-iMX91 connectivity Wi-Fi Bluetooth LE and OT COEX
RW612/MCXW71 - Wi-Fi and thread border router Training
FRDM-RW612 Getting Started, Wi-Fi CLI on VScode
Community Support
If you have questions regarding this training, please leave your comments in our Wireless MCU Community! here
記事全体を表示