无线连接知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Wireless Connectivity Knowledge Base

讨论

排序依据:
This document and the attached files are maintained up to date in collaboration with Dragos Musoiu. This document is a supplement for USB MSC device bootloader revision for FRDM-KL25Z (IAR) written by Kai Liu and describes the bootloader support for USB-KW24D512. How to use 1) Connect the USB-KW24D512 to the PC USB port; 2) Download the attached file ‘USB_KW24D512_MSD_Bootloader.bin’ to the flash memory of the MKW24D512 SiP following the next steps: Connect a J-Link programmer to the PC USB port (other than the one used for the USB-KW24D512 dongle); Navigate to your J-Link driver folder using a command console and type ‘jlink.exe’ followed by enter; After the apparition of the J-Link prompter, type ‘unlock kinetis’ followed by enter; Wait for the unlock command confirmation and after, type ‘device mkw24d512xxx5’ followed by enter; After the J-Link prompter appears type ‘loadbin USB_KW24D512_MSD_Bootloader.bin 0’ followed by enter; (Be sure you copied the ‘USB_KW24D512_MSD_Bootloader.bin’ file in the same directory with jlink.exe otherwise, type the command specifying the full path of the binary file); After the flashing process successfully finished type ‘exit’ followed by enter. 3) Reset or reconnect the USB-KW24D512; 4) The OS will prompt MSD device connecting and then BOOTLOADER drive will appear. The bootloader software was tested on Microsoft Windows 10, Microsoft Windows 8.1, Microsoft Windows 7, Ubuntu 14.04 and MAC operating systems. 5) Copy and paste any user application .SREC or .bin file into BOOTLOADER drive; 6) If a valid .SREC or .bin file was given, the board restarts and starts to run the user application. Please refer to the Notes section in order to create valid .SREC or .bin files. Note:            The bootloader has conditional jump to user application. The condition is the state of the SW1 button (PTC4). If the button is pressed (PTC4 grounded) during reset, the bootloader sequence will start, installing BOOTLOADER drive, as described before. Else if the button is released during reset, the SP and PC will be updated from address 0xC000. This means, the user application has to use a linker file which forces the application start address to 0xC000. If a valid SP and PC value is found at address 0xC000, the user application is launched. The bootloader application is located in the flash memory of the MKW24D512 SiP, from address 0x0000 to 0xBFFF, so the user application should not put any code in this memory region. Avoid using .SREC or .bin files having program bytes or fill patterns in the bootloader section. Attached files: USB_KW24D512_MSD_Bootloader.bin – bootloader binary file for USB-KW24D512; Pflash_512KB_0xC000.icf – IAR linker file for user application development; 802.15.4SnifferOnUSB.bin – user application demo binary file for KW24D512-USB. Be aware that the file ‘802.15.4SnifferOnUSB.srec’ is linked according to the above memory restrictions and is working only with the bootloader presented in this document.
查看全文
1. Introduction of ZigBee and popular solutions in the market. 2. Introduction of Freescale ZigBee solution
查看全文
MyWirelessAPP Demo Beacon(End device) code for RTS development
查看全文
This project is for Kinets L MCU Brazil challenge.Actually we don´t know if the project was registered. The goal of this project is to make Bluetooth communication between an android and  Freescale Freedom development kit FRDM-KL25Z. We will show the FRDM-KL25Z accelerometer status and the internal temperature sensor on android app. The android app requires version 4.x or above. Bluetooth module is connected to UART1.The embeddec code was created on CodeWarrior and exported to Keil MDK ARM.   http://youtu.be/-waEkfIuZCw
查看全文
This patch fix the issue in hdmi dongle JB4.2.2_1.1.0-GA release that wifi((STA+P2P)/AP) cann't be enabled properly. In the root directory of Android Source Code, use the following command to apply the patch: $ git apply hdmi_dongle_wifi_jb4.2.2_1.1.0.patch
查看全文
Development environment Hardware: i.MX6Q SabreSD connecting rtl8188cus or rtl8192cus wifi dongle Software: FSL JB 4.2.2-1.1.0-GA release   Advantage brought by JB4.2.2 As we may know that in JB4.0.x, Wifi-Direct is exclusive to normal Wifi access AP, so means that you have to turn off  Wifi normal AP access, then turn on Wifi-Direct. But in JB4.2.x, it can support the following topologies in use scene as following: So that means you can keep p2p connection meanwhile access internet throught AP.     Feature verified 1. Wifi connection support internet surf, and DLNA. 2. Wifi-Direct can support files transmission like Gallery sharing based on Wifi-Direct Demo.apk from FSL. 3. Particial support Wifi-Display, but due to unavailability of Wifi-Display sink module, so cannot be verified fully.   Usage: untar the attached file, then "patch -p1 <" in corresponding subdirectories. It would be better to untar the file in an empty directory, so you can understand which subdirectories are newly created (ex. hardware/realtek is newly created), then within these newly created subdirectoies, you need to "git init" first, then do "patch -p1<" to adopt all newly added files and subdirectories. Original Attachment has been moved to: WiFiDirectDemo.apk.zip Original Attachment has been moved to: patch4rtl8188_8192_on_jb4_2_2-ga.tar.gz
查看全文
There are two patches for HDMI Dongle JB4.2, one is remove the warning message, the other is fix to that sleep will not recover. Jack Mao
查看全文