ワイヤレス接続に関するナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Wireless Connectivity Knowledge Base

ディスカッション

ソート順:
Matter support in Visual Studio Code (VS Code) is now open to all developers. MCUXpresso extension for VS Code v24.12.71 integrates the Matter toolchain for development on Windows, macOS and Linux.  It can be installed by visiting Microsoft’s Marketplace for VS Code. The following steps will set up your Windows system to develop Matter on NXP devices. This Getting Started process takes ~1 hour.  This is similar time it takes with flawless CLI setup. Import Matter repo takes ~30 minutes (Clone Matter repo; run bootstrap setup script)  Import first project for a board takes @~10 minutes (SDK repo download - 1st time every board) Additional projects can then be quickly imported/built. 1. Install Pigweed Project Automation Tool Pigweed is used for easier automation of building, testing, and linting GN and CMake projects.  Matter uses GN, so Pigweed is used by the maintainers of the project.  Complete the following to allow the Matter Bootstrap to properly modify/install the repository. Launch a Terminal in Administrator mode to allow operations to complete successfully. Ensure that Developer Mode is enabled. This can also be done by running the following command as an administrator: REG ADD HKLM\Software\Microsoft\Windows\CurrentVersion\AppModelUnlock /t REG_DWORD /v AllowDevelopmentWithoutDevLicense /d 1 /f\"" Enable long file paths. This can be done using  regedit  or by running the following command as an administrator: REG ADD HKEY_LOCAL_MACHINE\SYSTEM\CurrentControlSet\Control\FileSystem /v LongPathsEnabled /t REG_DWORD /d 1 /f  Enable Git symlinks: git config --global core.symlinks true For more information on these settings visit Get started with Pigweed - Pigweed  2. Install Visual Studio Code (VS Code) Microsoft allows users to quickly install VS Code from https://code.visualstudio.com/download. The link allows the user to select the appropriate download for their OS.  The following instructions are for a Windows installation.  However, most of the following steps also apply to Mac and Linux users. It can be helpful for new users to directly install VS Code and the NXP extension.  This can be done by sharing one of two links:  vscode:extension/NXPSemiconductors.mcuxpresso https://marketplace.visualstudio.com/items?itemName=NXPSemiconductors.mcuxpresso  If VS Code exists on the system, the user will be taken to the NXP MCUXpresso for VS Code extension in the Microsoft Marketplace.  If VS Code is NOT installed on the system the user will be guided through the install of VS Code.  At this point the VS Code application should be installed on the laptop. 3. Install MCUXpresso for VS Code Extension The user can install or update the MCUXpresso for VS Code extension from within VS Code.  The following steps outline how.  A short clip is included to show the steps. Open VS Code.  Launch program from desktop. Open the Extensions Marketplace.  Click on Icon of 4 blocks in left navigation  or use Ctrl-Shft-X. Search "NXP" or "Mcuxpresso" in the Extension search window at the top left. MCUXpresso for VS Code extension will be displayed.  Click on listing. Click on blue Install button in the Extension Overview that is opened in the editor. The Extension is properly installed when the following NXP icon is shown in left navigation.  At this point the VS Code application now includes the NXP MCUXpresso extension. 4. Run MCUXpresso Installer for Tool Dependencies It is now necessary to install other tool dependencies to properly use VS Code for MCUXpresso, Zephyr and/or Matter. NXP provides the MCUXpresso Installer utility to simplify properly meeting these tool dependencies.  The following steps list how to use the installer for a Matter system.  A short clip is included to show the steps. Click on "Open MCUXpresso Installer" found under Quickstart Panel in upper left. The MCUXpresso Installer will launch if already installed.  NOTE: If the Installer is not found, the user should select the blue "Download" button in the bottom right notification. Select the following from the MCUXpresso Installer list of available tools: Matter Developer Arm GNU Toolchain Standalone Toolchain Add-ons LinkServer Click the blue "Install" button and wait until installation progress shows complete Restart VS Code so that new settings are active At this point the VS Code application now includes the NXP MCUXpresso extension, and the laptop has any other tools required to begin Matter installation. 5. Import NXP Matter Repository The MCUXpresso for VS Code extension simplifies how the user can add Matter to their workspace.  The repository import wizard automates most of the steps required for a user to get started with Matter. The following steps show how to add Matter Repository.  2 short clips are included to show the steps. Click on "Import Repository" found under Quickstart Panel in upper left. Click Repository found in the wizard's Remote tab. Select "NXP Matter".  This automatically targets the NXP/Matter repo found on GitHub. Enter a desired location to clone/store the NXP Matter repository.  Closer to C:/ is better. Select "release/v1.4.0" listed as an available version under Revision: Click Import The import process can take ~30 minutes depending on network bandwidth and IT software. NOTE: This is similar amount of time when using CLI in a terminal.   After the repo is cloned, the Matter Bootstrap script is used to setup matter environment. At this point the user laptop has a valid Matter workspace.  The workspace is now capable of importing and building Matter projects. 6. Import First Matter Project The MCUXpresso for VS Code extension includes an Import Example wizard that simplifies adding Matter projects to a workspace.  The following instructions show how to import a project from the NXP Matter repository.   A short clip is included to show the steps. Click "Import Example from Repository" from the Quickstart Panel in the upper left. Select the Matter Repository from the drop-down options for Repository. Select the desired Toolchain from the drop-down options for Toolchain.  A GNU Toolchain should be available from previous MCUXpresso Installer steps. Select the target board from the drop-down options for Board.  The listed boards are supported in the NXP Matter repo. Select the desired project from the Template drop-down options.  Currently there are "contact-sensor-app" and "lighting-app". Click Create blue button. At this point there is a Matter project in the workspace.  The project can be explored with the provided project properties and file explorer views. 7. Build Matter Project Building the project is the final step for Getting Started with a Matter project in VS Code.  The extension has properly setup the project toolchain and will build successfully.  The NXP extension reduces the setup time by not importing the SDK for all supported boards.  The board SDK is automatically imported/cloned when it is not located on the 1st build for a board.  Successive projects for the same board will not require this additional step/delay. The following steps show how to build a matter project in the workspace.  A short clip is included to show the steps.  Select the Matter project listed under the Projects pane located in the primary left sidebar.  When selected, project control icons are revealed to the left of the project name. Click on the Build icon.   Verify the build was successful by viewing the binary files with File Explorer.  Click the File Explorer icon to the right of project name or in the upper left of the side bar navigation.  The binary is found under the project's \out\debug folder. This exercise on "Getting Started with Matter" is completed.  At this point the Matter project imported to the workspace was successfully built. 
記事全体を表示
The MCX W23 is a family of devices. All devices are Arm Cortex®-M33 based wireless microcontrollers for embedded applications supporting Bluetooth Low Energy 5.3. It can be used to develop IoT solutions. MCX W23xA supports LV_SM mode. MCX W23xB supports HV_SM and XR_SM mode. Building on NXP's strong history of providing industrial edge solutions, the MCX W series offers a wide operating temperature range from -40 °C to 125 °C. The Arm Cortex-M33 provides a security foundation, offering isolation to protect valuable IP and data with Trust Zone technology. It simplifies the design and software development of digital signal control systems with the integrated digital signal processing (DSP) instructions. To support security requirements, the MCX W23 also offers support for SHA-1, SHA2-256, AES, RSA, ECC, UUID, dynamic encryption, and decryption of the flash data using a PRINCE engine, debug authentication, and TBSA-M compliance.   Documents Reference Manual Fact sheet Data Sheet Errata for MCX W23xUIK MCX W23 Hardware Design Guide Secure Reference manual** European Union Declaration of Conformity for FRDM-MCXW23 FRDM-MCXW23 Board User Manual Bluetooth Specifications The MCX W23 is compatible with the Bluetooth Low Energy 5.3 specification: – Bluetooth Low Energy 5.3 controller subsystem (QDID 200592) – Bluetooth Low Energy 5.3 host subsystem (QDID 226395) – Includes a 48-bit unique Bluetooth device address – Up to 4 simultaneous connections supported The MCX W23 supports the following Bluetooth Low Energy features: – Device privacy and network privacy modes (version 5.0) – Advertising extension PDUs (version 5.0) – Anonymous device address type (version 5.0) – Up to 2 Mbps data rate (version 5.0) – Long range (version 5.0) – High-duty cycle, Non connectable advertising (version 5.0) – Channel selection algorithm #2 (version 5.0) – High output power (version 5.0) – Advertising channel index (version 5.1) – Periodic advertising sync transfer (PAST) (version 5.1) – Supports LE power control feature (version 5.2) RF antenna: 50 Ω single-ended RF receiver characteristics: – Sensitivity −94 dBm in Bluetooth Low Energy 2 Mbps – Sensitivity −97 dBm in Bluetooth Low Energy 1 Mbps – Sensitivity −100 dBm in Bluetooth Low Energy 500 kbps – Sensitivity −102 dBm in Bluetooth Low Energy 125 kbps – Accurate RSSI measurement with ±3 dB accuracy Flexible RF transmitter level configurability: – TX mode 1 (TXM1): Range from −31 dBm to +2 dBm when VDD_RF exceeds 1.1 V – TX mode 2 (TXM2): Range from −28 dBm to +6 dBm when VDD_RF exceeds 1.7   Bluetooth_5.0_Feature_Overview Bluetooth_5.1_Feature_Overview  Bluetooth_5.2_Feature_Overview Bluetooth_5.3_Feature_Overview   Training MCX W Series Training - NXP Community   Equipment Wireless Equipment: This article provides the links to the Equipment that helps to the project development    Application Notes Power Management: AN14660: Power Management for MCX W23: This App Note provides information about the power manager software component. The application uses this component and the operating system to achieve optimal low-power states, based on the requirements of the application. RF: AN14575: MCX W23 Health Care IoT Peripheral Software Architecture: This App Note provides an overview of the software architecture for the MCX W23 Health care IoT Peripheral application. Designed as a model implementation, this application showcases the key features of the MCX W23 platform and serves as a foundation for developing product-quality applications. AN14659: MCX W23 Bluetooth Low Energy Power Consumption Analysis: This App Note describes the power consumption of the MCX W23 Bluetooth Low Energy (LE) device and the procedure to measure the current consumption using the MCXW23_EVK_BB and MCXW236B_RDM boards. AN2731: Compact Planar Antennas for 2.4 GHz Communication: This App Note is not an exhaustive inquiry into antenna design. It is instead focused on helping the customers understand enough board layout and antenna basics to select a correct antenna type for their application, as well as avoiding typical layout mistakes that cause performance issues that lead to delays Security: AN14657: Getting Started with Secure Boot on MCX W23: This application note covers the design of the bootloader ROM code that NXP has developed on the MCX W23, and how to use all its features. Useful Links Bluetooth LE FSCI Host Application running on FRDM-MCXN947 and MCXW23B-Click Board: The Bluetooth LE FSCI Host application demonstrates a host-side implementation for the Health Thermometer use case. It is designed to work alongside the FSCI Blackbox application, which runs on platforms such as the MCXW236 Click Board, FRDM-MCXW236, or other compatible Bluetooth LE wireless MCUs. Transmitter Maximum Output Power Override Application Note   Kinetis (../45/47/43;MCX W71/72/70) & MCX W23 Power Profile Tools (including Localization):  This page is dedicated to the Kinetis (KW35/KW38/KW45/KW47/KW43) and MCX W7x (MCX W71/W72/W70) Power Profile Tools. It will help you to estimate the power consumption in your application (Automotive or IIoT) and evaluate the battery lifetime of your solution. Development Tools    VSCode: MCUXpresso for Visual Studio Code (VS Code) provides an optimized embedded developer experience for code editing and development. Zephyr RTOs  NXP Application Code Hub: Application Code Hub (ACH) repository enables engineers to easily find microcontroller software examples, code snippets, application software packs and demos developed by our in-house experts. This space provides a quick, easy and consistent way to find microcontroller applications. NXP SPSDK: Is a unified, reliable, and easy to use Python SDK library working across the NXP MCU portfolio providing a strong foundation from quick customer prototyping up to production deployment. NXP SEC Tool: The MCUXpresso Secure Provisioning Tool us a GUI-based application provided to simplify generation and provisioning of bootable executables on NCP MCU devices. NXP OTAP Tool: Is an application that helps the user to perform an over the air firmware update of an NXP development board.
記事全体を表示
Board pictures (KW47-M2) Connectors (KW47-M2) Part Identifier Connector Type Description J3 2x5 pin header SWD DNP J8 1x6 pin header UART1 – FTDI DNP J9 1x6 pin header Power connector DNP Jumpers (KW47-M2) Part Identifier Connector Type Description JP5 2x3 pin header supply power source selection jumper: 1-2 shorted (default configuration): Use this configuration to set target MCU in DCDC mode.  3-4 shorted: Use this configuration to set target MCU in LDO/Bypass mode. All MCU power domains are supplied by P3V3_DUT.  JP4 1x2 pin header Target MCU boot configuration enable jumper: • Open (default setting): ISP mode is disabled • Shorted: ISP mode is enabled Push Buttons (KW47-M2) Part Identifier Switch name Description SW1 Reset button Resets the target MCU. This causes peripherals to reset to their default state. After this, MCU ROM bootloader will be executed. LED D1 turns on at SW1 press. SW2 User PB General purpose input. This pin supports low-power wakeup capabilities through Wake-Up Unit (WUU). LEDs (KW47-M2) Part Identifier Switch name Description D1 Reset LED Indicates a system reset event. When reset is triggered—such as by pressing the SW1 reset button—the D1 LED turns ON. D2 Led Green User indicator, indicates system activity   Power Configurations (KW47-M2) Populate J9 PWR connector. To run KW47 M2 as standalone, supply 3.3V to P3V3_DUT power rail Figure 1 J9 M10 Configuration (KW47-M2)   To get the KW47 M2 up and running, you need to select a power configuration through JP5 jumper. For more information on KW47 power configurations, refer to RM: Part Identifier pin Description JP5 1-2 1-2 shorted (default setting): Sets target MCU to DCDC mode. This mode is the recommended configuration. JP5 3-4 3-4 shorted: Sets target MCU to LDO mode.     External power configuration (KW47-M2) Enable KW47-M2 by supplying power through J9 connector: Note: When using DCDC or LDO mode, it is recommended to supply P3V3_DUT power rail only. Part Identifier pin Description J9 5 Use this pin to supply P3V3_DUT power rail with 3.3V. To get KW47-M2 up and running, it is recommended to set KW47 to DCDC mode and supply P3V3_DUT only. J9 3 Use this pin to supply P1V8_LDO power rail with 1.8V. This power rail is intended for an accurate control of VDD_RF power domain, but it is not necessary. J9 1 Use this pin to supply P1V1_EXT power rail with 1.1V. This power rail is intended for an accurate control of VDD_CORE power domain, but it is not necessary.     Programming the NBU in the KW47-M2 board The following steps guide you to program the NBU software for the KW47-M2 Place a jumper on the JP4 header while holding down the reset button (SW) on the module board. Then, connect the USB cable to the J8 connector (USB-to-serial bridge) and plug it into your computer. After the USB cable is connected, release the reset button.   Verify what COM Port was assigned to your KW47-M2 board. You can check the COM Port assigned in the Windows “Device Manager” program. Search for “Ports (COM & LPT)” and save the COM Port number. In this example the COM Port assigned was “COM19”   Navigate to your computer to the MCU-Link installation folder. The default installation path is located at “C:\nxp\LinkServer_25.3.31\MCU-LINK_installer Locate the “bin” folder and open it. Run the script “blhost” within a windows command prompt.   Type “blhost.exe -p COMX write-memory 0x48800000”, drag and drop the NBU binary file. When the process is ready you will see the response status "success"  
記事全体を表示
This post will cover how to install the CMSIS-DAP/SEGGER J-link firmware for the KW47-EVK and FRDM-MCXW72 using NXP’s MCU-LINK installer. CMSIS-DAP Installation for KW47-EVK Place a jumper on JP20 1-2 while the board is disconnected  Connect the board using a USB-A to USB-C cable between the host PC and the KW47-EVK board’s J14 connector, the D13 red LED should turn ON, indicating that the board is in ISP mode.                         Double click the script called program_CMSIS or program_JLINK  to execute the script. These scripts are found on the following path: C:\NXP\MCU-LINK_installer_3.167\scripts​ ​Note: MCU-Link installer version may vary. Press any key to execute the script, if the board entered ISP mode correctly, the board will be programmed with the selected debug probe firmware:    for FRDM-MCXW72  Place a jumper on JP5 1-2 while the board is disconnected    Connect the board using a USB-A to USB-C cable between the host PC and the FRDM-MCXW72 board’s J10 connector, the ISP_EN_ML INK red LED should turn ON, indicating that the board is in ISP mode.                                                              Double click the script called program_CMSIS to open the command window. This script is found on the following path:  C:\NXP\MCU-LINK_installer_3.167\scripts​​​  Note: MCU-Link installer version may vary.   Press any key to execute the script, if the board entered ISP mode correctly, the board will be programmed with the CMISIS-DAP firmware:                              Once the sequence finishes, the command window will display a completion message like the example below:    Remove the ISP jumper (JP5). Then reboot the board by disconnecting it from the host PC and reconnecting it again. After reconnecting, the ISP_EN_MLINK red LED should be OFF, and the USB_ACT green LED should be ON.    
記事全体を表示
As mentionned in the KW47/MCXW72 errata, a DCDC failure can occur infrequently during a drive strength change to low, and the DCDC output voltage becomes greater than or equal to the current output voltage. To avoid this particular case from happening, a software workaround can be implemented to make the voltage level at the low-power low drive-strength mode lower than the current output voltage of the DCDC. We will take the low power peripheral reference design demo application as example to show the workaround implementation. First of all, the default DCDC configuration in this demo project will never trigger this DCDC failure, because the DCDC is always in low drive-strength mode. To force it to the failure condition, we have to change the DCDC setting in board_dcdc.c. The DCDC configuration should be set to Normal drive strength mode, and the output voltage to 1.25V. BOARD_DCDC_config(kSPC_DCDC_NormalDriveStrength, kSPC_DCDC_LowUnderVoltage, false); The workaround requires the SPC high power mode to be enabled. SPC0->HP_CNFG_CTRL |= SPC_HP_CNFG_CTRL_HP_REQ_EN_MASK; The DCDC output voltage during high power mode is to set to 1.35V (higher than that of the active mode and low power mode): RF_CMC1->SPC_HP_CTRL |= 0x2U;   The SPC_HP mode is to be enabled just at the moment before going into low power mode. To do this, the nbu_ble project needs to be modified, and the NBU needs to be reprogrammed with this change. In the nbu_ble project, please modify the file fwk_platform_lowpower.c. The function PLATFORM_HandleLowPowerEntry manages the low power mode entry, thus we can add here: RF_CMC1->SPC_HP_CTRL |= 0x1U; //enable HP mode while ((RF_CMC1->SPC_HP_STAT && RF_CMC1_SPC_HP_STAT_SPC_HP_ACK_MASH) == 0); //wait for HP mode requested to be ackownledged RF_CMC1->SPC_HP_CTRL &= 0x0U; //disable HP mode while ((RF_CMC1->SPC_HP_STAT && RF_CMC1_SPC_HP_STAT_SPC_HP_ACK_MASH) == 0); //wait for HP mode requested to be ackownledged /* WFI will trigger low power entry procedure */ __DSB(); __WFI(); __ISB();   Please note that this workaround is valid for all wireless connectivity examples where low power mode is used. It does not apply to non-connectivity examples.    
記事全体を表示