大学项目知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

University Programs Knowledge Base

讨论

排序依据:
Instructions There are several main hardware configuration steps. Once the USB cable has been connected between the evaluation board and PC, it may be necessary to update the chip firmware which requires moving a jumper pin on the evaluation board. Then, connect one end of the USB cable to the PC and the other end to the Power/OSJTAG mini-B connector on the TWRK60N512 module. Allow the PC to automatically configure the USB drivers if needed. Before updating the firmware, it is necessary to start a CodeWarrior Project. In this case, the easiest way to do this is to actually navigate to the sample project and click on the Sample.mcp file. This will open CodeWarior 2.8. Selection Project->Build Configurations->MK40X256VMD100_INTERNAL_FLASH Project-»Build All Run->Debug Configurations—> Use the Codewarrior download Filter and Select "PROJECTNAME_MK40XD256VMD100_INTERNAL_FLASH_PnE_OSJTAG" Additional step is required if the firmware is out of date: Firmware Upgrade Instructions (if needed)   Firmware may change after an evaluation board has been manufactured and shipped. As a result, an alert will be displayed during the first attempt to download software to the board. Follow the instructions carefully. 1.     Unplug the USB cable.   2.     Look for the jumper (On the REV B Board) labeled "OSBDM_IRQ" - it is jumper 35. It will be found between the on/off switch and to the right of the the white "Lin" connectors. Remove one of the "LED Enable" jumpers for this if you don't have a   header jumper handy and put the jumper on the OSBDM_IRQ header These LED Jumpers are just above the blue potentiometer knob and marked as "J27."   3.    Reconnect the USB cable and click OK.   4.     Wait for the new firmware to download. 5.     A new dialog will appear when the process is complete.  6.    Unplug the cable, remove the jumper, return it to the location it was "borrowed from" and reconnect the cable. 7.    Then click OK.
查看全文
The first step of starting your TFC project is to get to know your microcontroller. This article serves you as an introduction of Qorivva MPC560xB microcontroller. Qorivva MPC5604B Summary The Qorivva MPC560xB/C/D family of 32-bit microcontrollers (MCUs) includes the latest in integrated devices for automotive electronics applications. These scalable Power Architecture® devices are supported by an enablement ecosystem that includes software drivers, operating systems and configuration code to help you quickly implement your designs.  For the Freescale Cup Challenge, we have provided Tutorials, example code and projects which are based on the trk-mpc5604b StarterTRAK evaluation board. Which Chip do you have? The chipset mounted on the boards for the Freescale Cup can vary. Always validate your chipset to know it's full capabilities. MPC560xB Product Information Page Difference's At-a-Glance: 5604B = 512MB Flash; no DMA 5606B = 1MB Flash; Has 16-Channel DMA 5607B = 1.5Mb Flash; Has 16-Channel DMA Getting Started Presentation Getting Started with MPC5600B.pptx (2Mb) Important Resources: e200z0 Core Reference Manual TRK-MPC5604B User's Manual TRK-MPC5604BQuick Reference Guide TRK-MPC5604B Schematics Reference manual Freescale's Qorivva MPC560xB Page Power.Org
查看全文
In this video we will look at the example code provided for the FRDM-TFC for use with Codewarrior.  
查看全文
Using the logic described in part 2 of the linescan camera tutorial, the actual implementation of the interface will be showed. The example code for the FRDM-TFC shield will be used as a reference implementation of a completely interrupt driven camera interface.
查看全文
Continue showing how to start a project from scratch.  In this second part,  we will see how to import new files into a CodeWarrior project to build a project. View Video Link : 1458
查看全文
Using Header(.h) files provided by Freescale inside CodeWarrior - Blinking an LED
查看全文
Continue discussion on the line scan camera. A completely interrupt driven approach to the interface will be illustrated.
查看全文
A examination of RC servos and their interface. Pulse width modulation will be reviews and a example configuration will be shown. View Video Link : 1465
查看全文
Summary   This page contains the technical information for the FRDM-OLED shield.    This includes the schematics, bill of materials (BOM),  gerber files and raw design files.   Main features: Newhaven NHD-2.7-12864UCY3 128x64 pixel graphic OLED Display Electret microphone interface with gain control RS-485 Interface for doing cool things like driving a DMX lighting system. General purpose I/O (I/O is shared with A/D pins so you could make your own scope!)       Example software, video tutorials tutorials, cool demos, etc are location on the page for MonkeyListen project page located here.     Notes:   You can order PCBs through OSHPark or your favorite board house.   There is a special .zip file with files ready to go for OSHPark  (using their preferred naming convention). There is a complete design package which has the raw design files (Altium Designer Format) as well as gerbers,  a bill of materials,  assembly plots etc.  Look in the "BUILD_PACKAGE" folder for the stuff needed to make the board. A PDF Schematic is also provided for easy reference.   If you are interested in a low cost pre-fabbed board or a fully assembled version,  please leave a comment.  A kickstarter project may follow to get a bunch built!
查看全文
Instructions There are several main hardware configuration steps. After installing the battery, once the USB cable has been connected between the evaluation board and PC, it may be necessary to update the chip firmware which requires moving a jumper pin on the evaluation board. Install the included battery into the VBAT (RTC) battery holder. Then, connect one end of the USB cable to the PC and the other end to the Power/OSJTAG mini-B connector on the TWRK40x256 module. Allow the PC to automatically configure the USB drivers if needed. Before updating the firmware, it is necessary to start a CodeWarrior Project. Open Codewarrior Navigate to File-> New ->Bareboard Project Select Kinetis K40->MK40X256VMD100 , P&E Open Source Jtag, C Language, No Rapid Application Development ,Finish Click on the main.c To get project focus Selection Project->Build Configurations->MK40X256VMD100_INTERNAL_FLASH Project-»Build All Run->Debug Configurations—> Use the Codewarrior download Filter and Select "PROJECTNAME_MK40XD256VMD100_INTERNAL_FLASH_PnE_OSJTAG" Additional step is required if the firmware is out of date: Firmware Upgrade Instructions (if needed) Firmware may change after an evaluation board has been manufactured and shipped. As a result, an alert will be displayed during the first attempt to download software to the board. Follow the instructions carefully. Unplug the USB cable. Look for the two pins labeled JM60 Boot and put a jumper on those pins Note: As it comes from the factory, the K40 board has a free jumper on the board. . Jumper J13 is labeled "JM60 BOOT." It connects two header pins which set the evaluation board in the firmware programming mode. This jumper is behind the LCD screen, and right next to LED/Touch Sensor "E3". Remove the LCD creen to gain access to the jumper. Reconnect the USB cable and click OK. Wait for the new firmware to download. A new dialog will appear when the process is complete. Unplug the cable, remove the jumper, and reconnect the cable. Then click OK. (You can store the jumper on the board, just set it so that it does not connect pins.) You may or may not encounter the firmware issue, or the multiple configurations issue. Once resolved, you should not see them again. With propertly set up hardware, users can return to Step 3: Import the LED Project of the Blink a LED on Kinetis Tutorial
查看全文
Model provided by the Mathworks Academic support team to manage wide angle lenses on the default Freescale Cup car camera.
查看全文
This document is addressed to the participants and visitors that will join us for The Freescale Cup 2015 Worldwide Finals 2015 The Freescale Cup 2015 Worldwide Finals will be held on 14-15 September 2015 at the Fraunhofer Institute for Integrated Circuits (Fraunhofer IIS) in Erlangen, Germany. Full address is: Fraunhofer IIS Am Wolfsmantel 33 91058 Erlangen Germany Google Maps location The attendees official guide is now online at https://community.nxp.com/docs/DOC-106164 Agenda of the event for the participants (subject to change): Sunday September 13th: Arrival at Hotels Get together in the evening (approximate time 18:00) at A&O Hostel Monday September 14th: 8:30: Departure from Hotel for City Tour 11:30: Prepare for departure for Fraunhofer IIS 12:00: Buses depart for Fraunhofer IIS 13:00: Lunch 14:00: Opening session 15:00: Start of Practice 17:30: High School and Innovation Challenge Demos 18:00: End of Practice - Start of the evening event 21:00: End of evening event - boarding buses for return to hotel Tuesday September 15th: 8:00: Buses depart for Fraunhofer IIS 9:00: Practice 13:00: Technical Inspection & Lunch 14:30: Final Race 16:00: Awards Ceremony 17:30: Buses depart for Awards Dinner 20:30: Buses depart for Hotel The event will be presented via LiveCast by the Fraunhofer IIS. URL is http://www2.iis.fraunhofer.de/freescale/  Hotel information: Students Hotel: Nuremberg Hostel - Stay at the A&O Hostel & Hotel Nuremberg  Google Maps Location Professors and Press Hotel: NH Nürnberg City Center hotel in Nuremberg Bahnhofstr. 17-19 | NH Hotel Group Google Maps Location Freescale will cover the cost of travel, accommodation and meals for the event for all Freescale Cup qualified teams and one faculty advisor per the rules in place. For Visa invitation letters, please contact [email protected] or [email protected] Travel booking will be organized by your regional Freescale University Program contact. Please have your faculty advisor get in touch with them for more information
查看全文
This video will examine how can design speed sensing into their vehicle platform.   An example of magnet and sensor placement is shown.
查看全文
Lab exercise supporting the i.MX53QSB for Master Student level student prepared by massimoviolante from the Politecnico of Torino. Complete course file(s) restricted to verified faculty only.  Available for download in the Faculty-Portal
查看全文
A simple demo code for TWR-K60D100
查看全文
Freescale S12 C-Family Specific Device Used = APS12C128SLK Courses Developed by Fredrick M. Cady Related Textbook: Oxford University Press: Software and Hardware Engineering: Fredrick M. Cady Files: All files related to this course are at bottom of this page. Summary: Introductory level course.  Covers basic microcontroller concepts and exercises in both assembly and C programming language.  Instructor editions of the laboratory include answers to questions and additional commentary by author especially for instructors. The following is a laboratory short courses developed applying the Process Oriented Guided Inquiry Learning (POGIL) pedagogy.  POGIL uses guided inquiry – a learning cycle of exploration, concept invention and application – as the basis for many of the carefully designed materials that students use to guide them to construct new knowledge.  POGIL is a student-centered strategy; students work in small groups with individual roles to ensure that all students are fully engaged in the learning process. POGIL activities focus on core concepts and encourage a deep understanding of the course material while developing higher-order thinking skills. POGIL develops process skills such as critical thinking, problem solving, and communication through cooperation and reflection, helping students become lifelong learners and preparing them to be more competitive in a global market. Course Contents: Title Topic Document Name Objective S/W Required H/W Required The Microcontroller - General Principles General Principles – The MCU LABSS12CINTRO01.pdf Show architecture of typical microcontroller; define terms. None None Software Development General Principles – S/W Development LABS12CINTRO02.pdf Show S/W/firmware development tools and process. None None Introduction to CodeWarrior - Simluating the Microcontroller in Assembly Language Introduction to the Laboratory – I LABSS12CINTRO03.pdf Introduce the S/W development system used in the lab. CW Introduction to CodeWarrior - Running Assembly Programs on the Microcontroller Introduction to the Laboratory – II LABSS12CINTRO04.pdf Continue above and introduce hardware used in the lab. CW SLK The Assembler Assembler Program LABSS12CINTRO05.pdf Learn the fundamentals of the assembler. CW Exploring Embedded C Programming The C Compiler LABS12CINTRO06.pdf Learn about using C in embedded systems. CW Introduction to CodeWarrior - Simulating the Microcontroller in C Intro to uC Hardware LABSS12CINTRO07.pdf Learn programmer's model and addressing modes None None Introduction to Your Microcontroller Hardware Intro to uC Hardware LABS12CINTRO08.pdf Learn programmer's model and addressing modes None None The Microcontroller Instruction Set I Instructions – I LABSS12CINTRO09.pdf Start to learn the instruction set; memory addressing; conditional branching. None None The Microcontroller Instruction Set II Instructions – II LABS12CINTRO10.pdf Continue ". CW SLK The Bouncing Switch in Assembly Switch Debouncing in Assembly LABS12CINTRO27.pdf Demonstrate switch debouncing and solutions CW SLK The Timer – Introduction to Timer Overflows With C Timers – I LABSS12CINTRO11.pdf Generating a delay using the timer overflow. CW SLK Digital Input and Output Digital Input and Output LABSS12CINTRO12.pdf Input from switches, output to LEDs. CW SLK Digital Input and Output With C Digital Input and Output LABS12CINTRO13.pdf Input from switches, output to LEDs. CW SLK I/O Software Synchronization Digital I/O software LABSS12CINTRO14.pdf I/O software synchronization CW SLK Introduction to Interrupts Using C Interrupts – I LABS12CINTRO15.pdf Learn fundamentals of interrupt vectors, etc. CW SLK The Bouncing Switch in C Switch Debouncing in C LABS12CINTRO28.pdf Demonstrate switch debouncing and solutions CW SLK Introduction to Interrupts Interrupts – I LABS12CINTRO16.pdf Learn fundamentals of interrupt vectors, etc. CW SLK Sources of Multiple Interrupts Interrupts – II LABS12CINTRO32.pdf Multiple sources of interrupts. CW SLK and scope The Timer – Introduction to Timer Overflows The Timer – Intro to Timer Overflows LABS12CINTRO17.pdf Generating a delay by polling the timer overflow. CW SLK The Timer – Timer Overflow Interrupts The Timer – Timer Overflow Interrupts LABS12CINTRO18.pdf Generating a delay using timer overflow interrupts CW SLK The Timer – Output Compare The Timer – Output Compare LABS12CINTRO19.pdf Waveform generation using output compare and interrupts. CW SLK and scope The Timer – Input Capture The Timer – Input Capture LABS12CINTRO20.pdf Using input capture to measure pulse width CW SLK The Timer – Pulse Accumulator The Timer – Pulse Accumulator LABS12CINTRO21.pdf Using pulse accumulator in event counting and gated time mode CW SLK and signal generator Analog Input using Assembly ATD – I LABSS12CINTRO22.pdf Introduce analog-to-digital conversion CW SLK Analog Input using C ATD – I LABSS12CINTRO26.pdf Introduce analog-to-digital conversion CW SLK Sampling and Resolution for Analog Input ATD- II LABS12CINTRO23.pdf ATD Sampling None None HCS12 A/D Digital I/O ATD – III LABSS12CINTRO24.pdf Digital I/O using the ATD CW SLK COP Coming Soon Using the COP CW SLK MSCAN Coming Soon Using the CAN module CW SLK SERIAL I/O – SCI SCI LABS12CINTRO29.pdf Introduction to SCI CW SLK and terminal SERIAL I/O INTERFACES – RS-232-C SCI-II LABS12CINTRO30.pdf Creating an RS-232-C communication Interface SERIAL I/O – The Serial Peripheral Interface SPI – I LABSS12CINTRO31.pdf Introduction to the SPI CW SLK, scope, SPI device SPI – II Coming Soon LCD CW SLK, LCD Register Listing HCS12C Family Register Listing HCS12C Family LABS12CINTRO25.pdf Complete course files restricted to verified faculty only.  Available for download in the Faculty-Portal
查看全文
Freescale Cup shield introduction for use with the FRDM-KL25Z or similar development board. Steps through the schematic of the FRDM-TFC shield and explain it's interfaces, logic, and use.
查看全文
Entrenamiento acerca de Code Warrior 10.4 presentado por Carlos Musich.
查看全文
Photos Videos
查看全文
First and foremost, be creative!! Below are just a few inspirational ideas. Option #1 - I cut-down (miter saw) a 4-position TWR-ELEVATOR to make this 2-position design. With the intent of having two boards mounted 1) TWR-PROTO and 2) MCU of choice (K40). If cutting PCB's with power tools is not your thing, you can buy a 2-position Tower Elevator here: http://wavenumber.net/twr-elev-2/ I just marked the holes on the back supportand drilled holes into the TWR-PROTO, a few stand-offs and viola! Option #2 - This option requires the removal of the rear spring. I am not sure how much value that spring honestly provides since most of the track is nice and flat. If you have a newer TWR-ELEVATOR you usually find some way to mount it to the screw holes with some form of L-Bracket. If you have an older TWR-ELEVATOR you can drill a hole in the Secondary Elevator (less PCB traces to worry about) and then mount it to the chassis with a L-Bracket. Option #3 - Check out this gallery of images: https://plus.google.com/u/0/photos/106056936857240793028/albums/5598207628299505201
查看全文