大学项目知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

University Programs Knowledge Base

讨论

排序依据:
On this page you will find additional notes to chassis assembly you may find useful. Examples of components used are obtained from the http://www.soselectronic.com/ distributor. Cables To connect battery you will need cable shown at the image top right. You can use the cable provided with the car and add an appropriate connector to its end. This usually requires special crimping tool, so it may be more appropriate to buy the "Tamyia charging cable" (shown on the bottom left side of the image above), cut the banana ends and attach the connector to the board. If you search for the appropriate type of the connector, it is called usually Tamiya charging connector, Tamiya jack 6,3 mm (SOS code 70479) or similar. Another cable you have to assemble is a power supply cable for the microprocessor board. You will need approx. 10-15 cm long cable with the barrel jack (SOS code 3834) or similar on one end and 2-pin 2.54mm connector (e.g. SOS code 4934 + 4937) on the other end. NOTE: Never power the microprocessor board and interface boards from different power supplies! In such case the grounds on both boards are not connected and you can damage the board. The grey flat ribbon cable that interconnects the boards is for signals only, there is no common GND connection! Battery You may find (as we did) the provided cable strips too weak to hold the battery on the place. Replace them with the classic electricians cable strips (e.g. SOS code 67504). Also do not forget that the batteries need to be charged fully the first time you charge them or they will not be able to fully charge in the future. If you jump the gun because you want to test your code as soon as you can you will hurt yourself later as we found our battery was absolutely shot in later stages of our build. Motor wires To attach the motor to the interface board you may find (as we did) the cables too short. Then remove 6 screws on the bottom (see image on the left), open the motor box and desolder the short wires. Replace with approx. 15 cm long silicon cables at least 1mm2. End of the cables should be connected to the 3-pin connectors with the 3,9mm pitch (e.g. SOS order code 5914 ) - see image on the right. Again, the contacts should be attached using a special crimp tool. Camera To attach the camera we found useful to prepare two metal L-shaped pieces made from aluminium. With the help of black plastic distance posts (already available in the kit) and these metal stands, you may freely change the position of the camera over the surface. You may use following files to cut the required shapes (drawing was made using the QCad program): Preview (.pdf) CAD file (.dxf)   Base board There was no motherboard in the kit, so you will need to provide your own. To make life easier, we offer you our CAD files created with QCad program. You may use it to produce your board. We use plexiglass for ours, but any other plastic material is appropriate. The large hole in the middle is for cables from the servo. We attach the board to the car using the plastic standoffs (you will need them 55 mm long, so in our case, we used the combination of 40 + 15 mm) - see an example (SOS code 10260). To attach both the processor and interface boards the simillar 5mm plastic standoffs were used. Preview (.pdf) CAD file (.dxf) Getting all together Please, notice the orientation of cables, especially the power supplies. You may find useful following connection diagram. Enlarged Schematic (.png) NOTE: Never power the microprocessor board and interface boards from different power supplies! In such case the grounds on both boards are not connected and you can damage the board. The grey flat ribbon cable that interconnects the boards is for signals only, there is no common GND connection! Servo Motor connectors The parts provided are extremely flimsy and if you snap them in and the wheels are not perfectly straight the wheels will align wrong when the servo first turns on. First off just concentrate on one wheel at a time and we found it useful to have one person hold the wheel straight while the arm was in the proper position and then we used needle nose pliers to quickly and precisely snap the pieces into the wheel. Don't be afraid to use some muscle we hesitated a few times at first because it didn't look good but it was fine.
查看全文
In this training video we will decompose an NTSC video signal to gaining understanding of how to capture video data from a "analog" camera.
查看全文
This tutorial covers the details of Turning A Servo on the Kinetis K40 using TWR-K40x256-KIT evaluation board. Overview In this exercise you will build a “bare metal” (no RTOS) application which turns a servo, targeting a Freescale K40 board. You will: Create the Servo code in CodeWarrior Build the Servo project Download and run the code on a Kinetis K40 Tower System board Learn how to utilize the FlexTimer module to control a Servo   To successfully complete this exercise you need the following board and development environment. The K40 Tower card, TWR-K40x256 Tower Elevator Panels Servo Prototyping Board Power to your servo - either utilize the 7.2v Nicad Battery or a DC power supply CodeWarrior for Microcontrollers 1. Hardware 2. Create a New CodeWarrior Project 3. Build the Code 4. Download/Debug/Run 5. Learning Step: Servo Code Description Example Code Variables Init_PWM_Servo PWM_Servo PWM_Servo_Angle Set Up a Look-Up Table for Servo Angles Other K40 Tutorials: Links 1. Hardware   The first step of this tutorial requires you read the Turn A Servo article for background information on servo's, timer modules, PWM signals and counters. You will need to connect your servo to the microcontroller and also to a separate power source. 2. Create a New CodeWarrior Project The next step is to create a new project (or add this code to an existing project). 3. Build the Code If you have more than one project in your project view, make sure the proper project is the focus. The most reliable way to do this is to right click the project and choose Build Project as shown below. You can also go to the Project menu and choose the same command. If you encounter errors, look in the Problems view and resolve them. You can ignore any warnings. 4. Download/Debug/Run This link shows a video of the servo turning the wheels from left to right in small increments http://www.youtube.com/watch?v=QgwASk9DHvU&feature=relmfu 5. Learning Step: Servo Code Description Your code will sweep your servo from max to minimum angular position, and then back again continuously. Example Code This code sets up the Pulse Width Modulation Timer Module for use by a servo. It is set to utilize Edge-Aligned PWM, and this file properly configures the period, and pulse width for use by the other modules Several important functions are contained in this file: 1. Init_PWM_Servo () - initializes the timer module 2. PWM_Servo (double duty_Cycle) - enter the desired duty cycle setting for the servo 3. PWM_Servo_Angle (int Angle) - enter the desired angle for the servo Straight forward - PWM_Servo_Angle (45) Full left - PWM_Servo_Angle (90)Full right - PWM_Servo_Angle (0)   4. Servo_Tick - interrupt routine which executes once/servo period PWM_Servo (double duty_Cycle) Init_PWM_Servo () PWM_Servo_Angle (float Angle) void ServoTick() Variables FTM0_CLK_PRESCALE TM0_OVERFLOW_FREQUENCY Pulse_Width_Low Pulse_Width_High Total_Count Low_Count Scale_Factor Angle Init_PWM_Servo Void Init_PWM_Servo () { //Enable the Clock to the FTM0 Module SIM_SCGC6 |= SIM_SCGC6_FTM0_MASK;  //Pin control Register (MUX allowing user to route the desired signal to the pin.  PORTC_PCR4  = PORT_PCR_MUX(4)  | PORT_PCR_DSE_MASK; //FTM0_MODE[WPDIS] = 1; //Disable Write Protection - enables changes to QUADEN, DECAPEN, etc.  FTM0_MODE |= FTM_MODE_WPDIS_MASK; //FTMEN is bit 0, need to set to zero so DECAPEN can be set to 0 FTM0_MODE &= ~1; //Set Edge Aligned PWM FTM0_QDCTRL &=~FTM_QDCTRL_QUADEN_MASK;  //QUADEN is Bit 1, Set Quadrature Decoder Mode (QUADEN) Enable to 0,   (disabled) // Also need to setup the FTM0C0SC channel control register FTM0_CNT = 0x0; //FTM Counter Value - reset counter to zero FTM0_MOD = (PERIPHERAL_BUS_CLOCK/(1<<FTM0_CLK_PRESCALE))/FTM0_OVERFLOW_FREQUENCY ;  // Count value of full duty cycle FTM0_CNTIN = 0; //Set the Counter Initial Value to 0 // FTMx_CnSC - contains the channel-interrupt status flag control bits FTM0_C3SC |= FTM_CnSC_ELSB_MASK; //Edge or level select FTM0_C3SC &= ~FTM_CnSC_ELSA_MASK; //Edge or level Select FTM0_C3SC |= FTM_CnSC_MSB_MASK; //Channel Mode select //Edit registers when no clock is fed to timer so the MOD value, gets pushed in immediately FTM0_SC = 0; //Make sure its Off! //FTMx_CnV contains the captured FTM counter value, this value determines the pulse width FTM0_C3V = FTM0_MOD; //Status and Control bits FTM0_SC =  FTM_SC_CLKS(1); // Selects Clock source to be "system clock" or (01) //sets pre-scale value see details below FTM0_SC |= FTM_SC_PS(FTM0_CLK_PRESCALE); /******begin FTM_SC_PS details **************************** * Sets the Prescale value for the Flex Timer Module which divides the * Peripheral bus clock -> 48Mhz by the set amount * Peripheral bus clock set up in clock.h *  * The value of the prescaler is selected by the PS[2:0] bits.  * (FTMx_SC field bits 0-2 are Prescale bits -  set above in FTM_SC Setting) *  *  000 - 0 - No divide *  001 - 1 - Divide by 2 *  010 - 2 - Divide by 4 *  011 - 3 - Divide by 8 *  100 - 4 - Divide by 16 *  101 - 5 - Divide by 32 *  110 - 6 - Divide by 64 - *  111 - 7 - Divide by 128 *  ******end FTM_SC_PS details*****************************/ // Interrupts FTM0_SC |= FTM_SC_TOIE_MASK; //Enable the interrupt mask.  timer overflow interrupt.. enables interrupt signal to come out of the module itself...  (have to enable 2x, one in the peripheral and once in the NVIC enable_irq(62);  // Set NVIC location, but you still have to change/check NVIC file sysinit.c under Project Settings Folder } PWM_Servo Void PWM_Servo (double duty_Cycle) {          FTM0_C3V =  FTM0_MOD*(duty_Cycle*.01); } PWM_Servo_Angle //PWM_Servo_Angle is an integer value between 0 and 90 //where 0 sets servo to full right, 45 sets servo to middle, 90 sets servo to full left void PWM_Servo_Angle (float Angle) {    High_Count = FTM0_MOD*(Pulse_Width_High)*FTM0_OVERFLOW_FREQUENCY;    Low_Count = FTM0_MOD*(Pulse_Width_Low)*FTM0_OVERFLOW_FREQUENCY;    Total_Count = High_Count - Low_Count;    Scale_Factor = High_Count -Total_Count*(Angle/90);     FTM0_C3V = Scale_Factor; //sets count to scaled value based on above calculations } Set Up a Look-Up Table for Servo Angles int main(void) {   //Servo angles can be stored in a look-up table for steering the car.   float table[n] = { steering_angle_0;    steering_angle_1;    steering_angle_2;   ……    steering_angle_n-1    };   Steering_Angle = table[x];   PWM_Servo_Angle (Steering_Angle); // Call PWM_Servo_Angle function. } Other K40 Tutorials: K40 Blink LED Tutorial K40 DC Motor Tutorial Kinetis K40: Turning A Servo K40 Line Scan Camera Tutorial Links Kinetis K40 TWR-K40X256-KIT
查看全文
Academic Textbooks Collection of textbooks related to or using Freescale processors and/or covering general embedded engineering concepts. Additional resources including lab manuals, sample projects and more are available in the Faculty Portal.  These resources are only available to to verified faculty partners. 32-bit Microprocessor and Microcontrollers Kinetis (ARM Cortex-M) Title: uC/OS-III The Real Time Kernel for the Kinetis Cortex M4 Author: Jean Labrosse ISBN:9780982337523 Publisher: Micrium Press Released: 2011 ColdFire™ (MC51xx, MC52xx, MC53xx, MC54xx) Title: ColdFire Microprocessors and Microcontrollers Author: Munir Bannoura, Rudan Bettelheim, Richard Soja ISBN: 0976297302 Publisher URL: www.amtpublishing.com Released: 2006 Power™ Architectures (MC5xx, MC55xx) Title: MPC5554/MPC5553 Revealed Author: Munir Bannoura, Richard Soja ISBN: 0976297353 Publisher URL: www.amtpublishing.com Released: 2005 Title: eTPU Programming Made Easy  **Now Available in Japanese Author: Munir Bannoura, Margaret Frances ISBN: 0976297310 Publisher URL: www.amtpublishing.com Released: 2004 Title: TPU Microcoding for Beginners Author: Amy Dyson, Munir Bannoura ISBN: Publisher URL: www.amtpublishing.com Released: 1999 Digital Signal Processing Title: DSP for Embedded and Real-Time Systems Author: Robert Oshana ISBN: 9780123865359 Publiser: Elsevier Released: 2012 Title: DSP Filter Cookbook (Electronics Cookbook Series) Author: John Lane, Jayant Datta, Brent Karley, Jay Norwood ISBN: 0790612046 Publisher URL:  No Data Released: 2004 Title: Digital Signal Processing Fundamentals Author: Ashfaq Khan ISBN: 1584502819 Publisher URL: www.oup.com/us/he Released: 2000 Title: Digital Signal Processing Applications with Motorola's DSP56002 Processor Author: Mohammed El-Sharkawy ISBN: 0135694760 Publisher URL:  No Data Available www.oup.com/us/he Released: 1996 Title: Foundations of Digital Signal Processing: Theory, Algorithms and Hardware Design Author: Patrick Gaydecki ISBN-10: 0852964315 ISBN-13: 978-0852964316 Publisher: IEE; General 32-bit topics Title: Modern Micoprocessors 3rd Edition Author: V. Korneev / A.Kiselev ISBN: 1584503688 Publisher URL: www.charlesriver.com Released: 2004 Title: Micrcontrollers and Microcomputers: Principles of Software and Hardware Engineering Author: Fredrick M. Cady ISBN: 0195110080 Publisher URL: www.oup.com/us/he Released: 1997 Title: Programming Microcontrollers in C Author: Ted Van Sickle ISBN: 1878707140 Publisher URL: Released: 1994 Title: Real-Time Programming: A Guide to 32-bit Embedded Development Author: Rick Grehan, Ingo Cyliax, Robert Moote ISBN: 0201485400 Publisher URL:  www.aw.com Released: 1998 Title: Embedded Systems Design: A Unified Hardware/Software Introduction Author: Frank Vahid, Tony D. Givargis ISBN: 0471386782 Publisher URL:  No Data Available Released: 2001 Title: Microcontrollers in Practice Author: Marian Mitescu ISBN: 3540253017 Publisher URL:  No Data Available Released: 2005 Title: Embedded Systems Architecture: A Comprehensive Guide for Engineers and Programmers Author: Tammy Noergaard ISBN: 0750677929 Publisher URL:  books.elsevier.com/newnes/ Released: 2005 Title: MEMS: Applications Author: Mohamed Gad-el-Hak ISBN: 0849391393 Publisher URL:  crcpress.com Released: 2005 Title: High-Performance Embedded Computing: Architectures, Applications, and Methodologies Author: Wayne Wolf ISBN: 012369485X Publisher URL:  No Data Available Released: 2006 Title: Hardware and Computer Organization Author: Arnold S. Berger ISBN: 0750678860 Publisher URL:  www.elsevier.com Released: 2005 8- and 16-bit Microcontrollers HCS12 Title:  Microcontroller Programming For Engineers Author: Harlan Talley ISBN-13: 978-0-557-09570-4 Publisher URL: http://lulu.com Released: 2009 Title:  Learning by Example Using C – Programming the DRAGON12-Plus Author: Richard E. Haskell and Darrin M. Hanna ISBN: Publisher URL: http://www.lbebooks.com Released: Title:  Learning by Example Using C – Programming the mini DRAGON12 Author: Richard E. Haskell and Darrin M. Hanna ISBN: Publisher URL: http://www.lbebooks.com Released: Title:  HCS12 Microcontrollers and Embedded Systems Author: Muhammad Ali Mazidi, Danny Causey, Janice Mazidi ISBN: 978013672294 Publisher URL: http://www.pearsonhighered.com Released: 2008 Title: Assembly and C Programming for the Freescale HCS12 Microcontroller Second Edition Author: Fredrick M. Cady ISBN: 9780195308266 Publisher URL: www.oup.com/us/he Released: 2007 Title: The HCS12/9S12, An Introduction to Hardware and Software Interfacing Author: Han-Way Huang ISBN: 1401898122 Publisher URL: http://www.delmarlearning.com/electronics/ Released: 2006 Title: Embedded Microcomputer Systems: Real Time Interfacing 2nd Edition Author: Jonathan W. Valvano ISBN: 0534551629 Publisher URL: http://engineering.thomsonlearning.com/ Released: 2006 Title: MicroC/OS-II: The Real-Time Kernel Author: Jean J. Labrosse ISBN: 1578201039 Publisher URL: www.cmpbooks.com Released: 2002 HCS08 Title: Microcomputer Architecture - Low Level Programming Methods and Applications of the M68HC908GP32 Author: Dimosthenis E. Bolanakis, Euripidis Glavas, Georgios A. Evangelakis, Konstantinos T. Kotsis, Theodore Laopoulos ISBN: 978-960-93-4536-1 (English version of the book) ISBN: 978-960-357-101-8 (Greek version of the book: delivered with an educational board) Title: HCS08 Unleashed: Designer's Guide To the HCS08 Microcontrollers Author: Fabio Pereira ISBN-10: 1419685929 Publisher URL: http://www.booksurge.com/ Released: March 24, 2008 Title: Using Microprocessors and Microcomputers: The Motorola Family 4th Edition Author: William Wray, Joseph Greenfield, Ross Bannatyne ISBN: 0138404062 Publisher URL:  www.prenhall.com Released: 1998 Title: The Official Robosapien Hacker's Guide Author: Dave Prochnow ISBN: 0071463097 Publisher URL:  /www.mhprofessional.com Released: 2005 Title: Robot Building for Beginners Author: Dave Cook ISBN: 1893115445 Publisher URL:  http://www.robotroom.com Released: 2002 Title: Intermediate Robot Building Author: Dave Cook ISBN: 1590593731 Publisher URL:  http://www.robotroom.com Released: 2004 HC11/HC12 (Legacy Devices) Title: Software and Hardware Engineering Motorola M68HC12 Author: Fredrick M. Cady, James M. Sibigtroth ISBN: 0195110463 Publisher URL: www.oup.com/us/he Released: 2000 Title: Software and Hardware Engineering Motorola M68HC11 Author: Fredrick M. Cady ISBN: 0195110463 Publisher URL: www.oup.com/us/he Released: 1997 Title: MC68HC12 An Introduction: Software and Hardware Interfacing Author: Han-Way Huang ISBN: 0766834484 Publisher URL: http://www.delmarlearning.com/electronics/ Released: 2002 Title: MC68HC11 An Introduction: Software and Hardware Interfacing 2nd Edition Author: Han-Way Huang ISBN: 0766816001 Publisher URL: http://www.delmarlearning.com/electronics/ Released: 2002 Title: Programming the Motorola M68HC12 Family Author: Gordon Doughman ISBN: 0929392671 Publisher URL:  No Data Available Released: 2000 Title: Embedded Systems: Design and Applications with the 68HC12 and HCS12 Author: Steven F. Barrett, Daniel J. Pack ISBN: 0131401416 Publisher URL:  www.prenhall.com Released: 2004 Title: Introduction to Microcontrollers Architecture, Programming, and Interfacing for the Freescale 68HC12 Author: G. Jack Lipovski ISBN: 0124518389 Publisher URL:  books.elsevier.com Released: 2004 Title: Single and Multiple Chip Microcomputer Interfacing Author: G. Jack Lipovski ISBN: 0138105731 Publisher URL:  No Data Available Released:  No Data Available Title: Microcomputer Engineering, Third Edition Author: Gene H. Miller ISBN: 0131428047 Publisher URL: www.prenhall.com Released:  2003
查看全文
INTRODUCTION Hi everyone, Making/Developing/Porting a Bootloader is a tedious task for newbies (even for professionals) and inexperienced hobbyists who wish to use them on their custom hardware for rapid prototyping. After searching a lot on different forums I came to a conclusion that I cant develop a bootloader just like that so my next option was porting ,that too wasnt easy if you are going with old bootloaders with limited support. I then found a very easy and efficient way of rapid software development platform that can be used on almost any IDE (Keil,Codewarrior,KDS,etc.) and can be used to develop softwares like USB MSD Bootloaders,Serial Bootloaders and other applications for almost all Freedom Development Boards ,Freescale Kinetis MCUs (on a Custom Development Board ) with minimal ARM Programming Knowledge, which is perfect for newbies like me who are just starting with ARM Development using freescale or other boards.See Welcome to the homepage of the µTasker operating system with integrated TCP/IP stack, USB and target device simulator Now my project was to make custom board using MK22DX256VLF5 (48 LQFP) MCU ,my board is a rather a simple one using basic filtering circuits for powering the MCU and almost all the pinouts given as hardware pins on the dev board.Somehow I was able to flash my first blink code using Keil IDE using the OpenSDA circuitry of FRDM-KL25Z (J-11 trace cut ) with CMSIS-DAP firmware (OpenSDA app ) loaded on to it using SWD Programming. With the steps mentioned below I'll show you how to port a Mass Storage Device (MSD) Bootloader using uTasker project from scratch. REQUIREMENTS Programmer(Hardware) or Emulated Programmer(OpenSDA apps): Segger Jlink, P&E Multilink ,OpenSDA Emulators (Jlink-SDA, CMSIS-DAP,USBDM ) IDE :Keil,Codewarrior, Kinetis Design Studio etc. (I prefer CW 10.6 ) Target MCU: Choose any MCU between Kinetis,Coldfire V2,STM32  (I am using Freescale Kinetis MK22DX256VLF5 ,48 LQFP ) refer - http://www.utasker.com/ PROCEDURE 1. Lets start by downloading the uTasker project/framwork (for Kinetis ) from µTasker Kinetis Developer's Page . Then extract and copy the folder to your CW workspace ,import the project to CodeWarrior IDE, It should look like this. (I am using version 14-9-2015)   2.Next Select "uTaskerSerialLoader_Flash" from the Five build configurations (refer http://www.utasker.com/docs/uTasker/uTaskerSerialLoader.PDF  ).uTaskerBM_Loader is described in http://www.utasker.com/docs/uTasker/uTasker_BM_Loader.pdf This is a very small loader alternative that works together with an initial application. uTaskerV1.4_BM_FLASH is the application to build so that it can be loaded to a loader (including the USB-MSD one). uTaskerV1.4 is a 'stand-alone' version of the application that doesn't work together with a loader (and doesn't need a loader).If you want to build application to load using the USB-MSD loader you need to use uTaskerV1.4_BM_FLASH. after that find the files config.h and ap_hw_kinetis.h.These files define the type of MCU you use. 3.In config.h Select your board or MCU type or the closest MCU resembling the architecture of your own MCU. My MCU  MK22DX256VLF5 was not there so with a little help from mjbcswitzerland  I chose TWR_K21D50M Board settings as TWR-K21D50M module is a development board for the Freescale Kinetis K11, K12, K21 and K22 MCUs. (Note : Be sure to remove or comment any other defined boards ) After Selecting the Board/MCU scroll down to find USB_INTERFACE and USB_MSD_LOADER and make sure that these two are defined (not commented ).This is necessary to enable USB enumeration as Mass storage device. Also comment the following if already defined : HID_LOADER KBOOT_HID_LOADER USB_MSD_HOST This is necessary as we are using our Bootloader in MSD Device Mode not in MSD Host Mode. Also we arent using HID_LOADER and KBOOT. Now open  ap_hw_kinetis.h and Find your selected MCU (in my case its TWR_K21D50M ) So, Find the String "TWR_K21D50M" (or whatever your MCU is ) and see if the follwing lines are defined. #define OSC_LOW_GAIN_MODE #define CRYSTAL_FREQUENCY    8000000  #define _EXTERNAL_CLOCK      CRYSTAL_FREQUENCY #define CLOCK_DIV            4                                      or    #if(..........)         #define CLOCK_MUL        48                                            #define SYSTEM_CLOCK_DIVIDE 2                                      #else         #define CLOCK_MUL        24 #endif     #define USB_CLOCK_GENERATED_INTERNALLY Here comes an integral part of USB MSD Bootloading/Programming.You must be wondering about CRYSTAL_FREQUENCY  8000000 and  CLOCK_DIV   4  .This is the frequency of an external crystal oscillator  (8mhz) connected between EXTAL0 and XTAL0 pins of the Target MCU.If your MCU has an internal oscillator then check whether the latter is defined. refer- https://cache.freescale.com/files/microcontrollers/doc/app_note/AN4905.pdf          http://www.utasker.com/kinetis/MCG.html There are two ways to be able to use USB: 1. Use a crystal between EXTAL0 and XTAL0 - usually 8MHz is used. (with or without load capacitor -both worked for me ) 2. Use a 48MHz oscillator on the USB-CLKIN pin. First one is easier and it worked for me.Since my MCU doesnt have an internal oscillator I have used and External 8Mhz crystal. If you want to use a 16Mhz crystal then just make the following changes : #define CRYSTAL_FREQUENCY    8000000 #define _EXTERNAL_CLOCK      CRYSTAL_FREQUENCY #define CLOCK_DIV            4                                 TO #define CRYSTAL_FREQUENCY    16000000 #define _EXTERNAL_CLOCK      CRYSTAL_FREQUENCY #define CLOCK_DIV            8 Note: The CLOCK_DIV should be such that it prescales the crystal frequency to range of 2-4MHz. Here is the clocking diagram of My MCU.The next diagram shows an oscillator crystal connected externally to my dev board. Next search for "PIN_COUNT" under your corresponding MCU/Board (mine is TWR_K21D50M).My MCU is 48 LQFP with 256kb flash and 32kb SRAM (you have to change them according to your MCU ).So I have changed the following lines                              from   #define PIN_COUNT           PIN_COUNT_121_PIN                         #define SIZE_OF_FLASH       (512 * 1024)                          #define SIZE_OF_RAM          (64 * 1024)                              to   #define PIN_COUNT           PIN_COUNT_48_PIN                      #define SIZE_OF_FLASH       (256 * 1024)                              #define SIZE_OF_RAM          (32 * 1024)  Next if you search for your MCU/Board (in this case TWR_K21D50M) ,you will find this line : #define UART2_ON_E This defines the alternative port for UART2,since many boards doesnt have PORTE ,it can be chaned to other ports. [its not important though] Note : When building the serial loader for a device with small RAM size reduce the define #define TX_BUFFER_SIZE (5512) to 512 bytes so the buffer can be allocated (the large size was used only for some debugging output on a larger device) [loader version :14.9.2015] Now search for the String "BLINK_LED" under your corresponding MCU/Board ( mine is TWR_K21D50M ) .The uTasker Bootloader has a special function ,whenever it is in MSD/LOADER mode it blinks a test LED on the board.This is not important but it can be used for debugging purposes.I have a test LED on my board at PORTB16 .You can also specify hardare pins to force bootloader mode and to stop watchdog timer if you pull SWITCH_3 and SWITCH_2 down to ground respectively.I am setting SWITCH_3 and SWITCH_2 as PORTD7 and PORTD6 respectively. Now on the toolbars go to Project > Properties > C/C++ Build > Settings > Tool Settings > Target Processor :Change it to your MCU type (mine is cortex-m4 ) .Next go to Linker >General and change the linker script file to match your MCU's flash,RAM,Type.I have set mine to K_256_32.ld (Kinetis K type processor with 256kb flash and 32 kb RAM) Apply your changes.Now you are ready to go. 4.  Build your project under SerialLoader_FLASH configuration .If there are no compilation errors then you have done it! (if there are then recheck everything with this guide ) Now Click the Flash programmer icon a and Select Flash File to Target. (if your not getting the icon switch to "DEBUG" perspective view ) Now you may choose your Programmer (or emulated programmer )[connection tab] ,select the correct Flash configuration file ,then browse for the binary file that has been generated under C:\Users\<computer user>\workspace\Kinetis_14-9-2015\Applications\uTaskerSerialBoot\KinetisCodeWarrior\uTaskerSerialBoot_FLASH\uTaskerSerialBoot.bin and Click on "Erase and Program". You may skip Step 5 and go to Step 6. 5.I am using the OpenSDA circuitry of my FRDM-KL25Z (J-11 trace cut ) as a programmer using J-link OpenSDA app. Download the app from SEGGER - The Embedded Experts for RTOS and Middleware, Debug Probes and Production Programmers - OpenSDA / OpenSDA V2 depending on your OpenSDA version (FRDM KL25Z has OpenSDAv1). Refer - Using the Freedom Board as SWD Programmer | MCU on Eclipse 5.1.First Enter bootloader mode and Flash the Jlink sda app into it.Connect the SWD wires from the board to your  Target MCU/Board ,also connect the target board        to the external oscillator.Also connect the FRDM's OpenSDA through USB. (A drive with the name JLINK Should come )                                          5.2. Go to Flash File to target and under connections tab click new. give any name and click new under Target Tab.Then select the target type (your target MCU ,mine is                      K22DX256M5).Then check Execute Reset under Initialization Tab. Click finish.    Now you'll get the option to select connection type ,then choose J-Link/J-Trace for ARM and change the Debug port interface to SWD .If you get the error :connection name is not        unique then just change the name (I have used jlink1).Click Finish.     Now I have set up my connections so I can flash the MCU with Jlink app on my OpenSDA circuitry. 6. Now to verify USB Enumeration of your Custom Board ,connect it to PC using USB and you should get a drive with the name UPLOAD_DISK.
查看全文
How to install a servo horn.  More specifically for the Freescale Cup kit. [no audio]
查看全文
MathWorks is a proud global sponsor of The NXP Cup If you are a member of a NXP Cup team, you have access to a complimentary Software License for MATLAB / Simulink. Visit the NXP Cup - MathWorks Deutschland website to learn more about the Software offering.  Examples for using Simulink in the NXP Cup are packaged with the Simulink Coder Support Package for  FRDM-KL25Z available from the Hardware Support Page.  Additional examples for reading and analyzing live data from the Line Scan Camera are available in the NXP Cup Companion App available on the MATLAB File Exchange.  Additionally, there is an example which uses the Simulink Coder product from MathWorks to target the FRDM-KL25Z. Feel free to use the forum on MATLAB Answers or here below to ask your questions about MATLAB use with The NXP Cup.  You can also email [email protected] with any questions.
查看全文
Recommend accessories or post your own designs.  For the community by the community! Add your contributions in the comments section below.  As I filter through them I will move them up into this main document, so it is easier to browse. TFC Camera Mounts Designed by Wave Number Print these on demand via Shapeways.com Base Board Hinge Two Position Tower Elevator TWR-ELEV-2 — Wavenumber LLC - Link to the Store
查看全文
Depending on which MCU Devlopment board you have chosen, you will need to figure out a way to mount this to the chassis. I have seen everything from cardboard, to aluminum, to wood. Below is a template complete with CAD drawings to mount the Qorivva TRK-MPC5604B board and the Motor Board onto the chassis. We use plexiglass for ours, but any other millable material is appropriate. The large hole in the middle is for cables from the servo. We attach the board to the car using the plastic standoffs (you will need them 55 mm long, so in our case, we used the combination of 40 + 15 mm) - see an example (SOS code 10260). To attach both the processor and interface boards the simillar 5mm plastic standoffs were used. Preview (.pdf) CAD file (.dxf)
查看全文
One option for mounting the camera on the Freescale Cup car.  The only additional components you need are two zip ties. [no audio]
查看全文
This video will examine how can design speed sensing into their vehicle platform.   An example of magnet and sensor placement is shown.
查看全文
ARM University Programs Lab-in-a-Box (LiB) Freescale and ARM University Programs have teamed up to provide you the Lab in a Box.  If you are interested in adopting the Lab-in-a-Box (LiB) in your course please contact the ARM University Program to request a donation! Development Boards The FRDM-KL25Z is an ultra-low-cost development platform enabled by Kinetis L Series KL1x and KL2x MCUs families built on ARM® Cortex™-M0+ processor. Features include easy access to MCU I/O, battery-ready, low-power operation, a standard-based form factor with expansion board options and a built-in debug interface for flash programming and run-control. The FRDM-KL25Z is supported by a range of Freescale and third-party development software. Freedom Development Platform Lab Exercise for Freescale Freedom KL25Z Board Software Tools ARM offers the Keil Microcontroller Development Kit (MDK-ARM) for ARM powered microcontrollers. It features the industry-standard compiler from ARM, the Keil µVision IDE, and sophisticated debug and data trace capabilities. MDK-ARM offers tailored support for all Cortex-M processor-based devices, and is the recommended solution for students working with standard ARM-based MCU devices. We suggest that students and universities download the free evaluation version of the tools, which offers all the features of the standard version, but with a 32 KByte object code/data limit. Keil Microcontroller Development Kit (MDK-ARM) Textbooks The Definitive Guide to the ARM Cortex-M0 In English, by Joseph Yiu Published by Newnes ISBN-10: 0123854776 ISBN-978-0123854773 C Programming for Embedded Microcontrollers In English, by Warwick A. Smith Published by Elektor ISBN: 978-0-905705-80-4Other ARM-related Books Teaching Materials Teaching Slides ARM Processors and Architectures Comprehensive Overiew - 2012 ARM Processors and Architectures Fundamentals Lab Manuals and Exercises Lab Exercises for Cortex-M4 Freescale Kinetis using Keil MDK Lab Exercises for Cortex-M0+ Freescale Freedom KL25Z Board Application Notes for Students and Faculty AN234: Migrating from PIC Microcontrollers to Cortex-M Other Projects and Resources Variety of Resources and Middleware from onARM Projects-Lab.com - Ideas for Design Projects Other ARM Projects
查看全文
The file contains the rules for The NXP Cup EMEA 2016-2017 edition of the challenge. Revision 1 dated 13-Jul-2016 For any question : [email protected]
查看全文
What is a microcontroller (MCU)? A microcontroller includes a microprocessor (CPU) as well as a number of other components like RAM, flash and EEPROM to store your programs and constants. While a microprocessor requires external devices to control things like input/output, or timers to implement periodic tasks, and digital to analog converters, a microcontroller is all inclusive. Contrast this all-in-one approach with a typical personal computer which contains an INTEL or AMD CPU, as well as separate chips for RAM, a separate video card, a dedicated hard drive, silicon chips or PCI circuit boards to enable the processor to access USB, serial and video card signals Microcontroller pins are general purpose, whereas CPU pins are specific. This means that each pin is tied to a multiplexer which you must set to choose the particular use for the pin. For example, in a microcontroller, one pin pin might be re-purposed for the following tasks 1. The output of a timer 2. Send a signal to a motor 3. Receive an input from a sensor or analog device
查看全文
Which Platform to use?  Qorivva or Kinetis? Both are 32-bit devices. The Qorivva products, a Power architecture, are used widely in the automotive industry.  It has specialized peripherals such as CAN and LIN.  Automotive products are built tough, to high industry standards. The Kinetis products, ARM M4 architecture, are widely used.  You will find it in lots of everyday devices and industrial automation (such as robotics). It can support a lot of consumer peripherals such as USB, WiFi, and Graphical Displays. Which platform is more powerful or easy to use? Both supported processors are powerful 32 bit microcontrollers with similar software peripherals. Take an hour or two to research the evaluation boards on the Freescale sites and their underlying technologies. Think through the design and implementation process of connecting various components like the motor, battery and servo, to the evaluation board. The Tower System provides a modular prototyping platform, and the TRK evaluation board has many features. What level of support does a technology have? For the Cup Challenge, you may use any Freescale microcontroller. There are reference designs here on the wiki and TONS of code and examples on the Freescale site. Students should speak with their professor, and check out their respective documentation and software examples to make a choice. Having on campus support is invaluable in this case. There are online communities for the respective technologies as well. Research which technologies are have more active user communities which best complement the teams design approach? Obviously the Freescale Cup Wiki itself is a resource, and provides details on how to use two different microcontrollers - so it might be best to limit choices to one of these two supported platforms.
查看全文
A microcontroller includes a microprocessor (CPU) as well as a number of other components like RAM, flash and EEPROM to store your programs and constants. While a microprocessor requires external devices to control things like input/output, or timers to implement periodic tasks, and digital to analog converters, a microcontroller is all inclusive. Contrast this all-in-one approach with a typical personal computer which contains an INTEL or AMD CPU, as well as separate chips for RAM, a separate video card, a dedicated hard drive, silicon chips or PCI circuit boards to enable the processor to access USB, serial and video card signals Microcontroller pins are general purpose, whereas CPU pins are specific. This means that each pin is tied to a multiplexer which you must set to choose the particular use for the pin. For example, in a microcontroller, one pin pin might be re-purposed for the following tasks 1. The output of a timer 2. Send a signal to a motor 3. Receive an input from a sensor or analog device Basic Concepts Covered Thus far: Blink an LED - overview of GPIO and setting up the microcontroller Drive a Motor - using the Timer and PWM modules of the microcontroller Turn a Servo - More details on using timer modules and PWM to control a servo Obtain Data from the Line Scan Camera - ADC Setup and GPIO Bit Blasting to create clock and pulse signals controlling the line scan camera I2C tutorial - Using I 2 C to communicate with various sensors using the K40 Button - An overview of how to implement a simple button Additional Concepts we would like to add to the Wiki: Timer Modules PWM watchdog-timer memory
查看全文
As a maker and a professional engineer I always try to keep up with new tools to tinker with.  Being a Freescaler I get especially jazzed about ones using our chips.  But, with so many fish in the sea it's hard to get the word out about all the options out there.  So for your viewing pleasure below is a list of up and coming "development boards" for both Makers and Professionals.  All of these boards use Freescale silicon, but the actual board/product is not made by Freescale.  Add comments below with anything I should be made aware of and any reviews or comments of the ones I mentioned. In the microcontrollers corner... Teensy 3.1 -Weighing in at 2.95 grams, don't be fooled by this one's size; it really packs a punch.  But the board is just the beginning, you can program the board using Arduino Sketch, and Paul has cooked up some cool new audio and video libraries that take advantage of the extra horsepower in the Kinetis K20 chip. WunderBar -This one wins the award for creative naming and packaging.  Basically, you have a main board and several sensor boards.  You snap off the sensor boards (like breaking off a piece of chocolate) and attach them to your desired application.  Out of the box, basic board level stuff is taken care of so you can spend more time working on your tablet/smartphone application. Enter the hybrid cross-overs These two boards have both MCU and MPU's onboard for the best of both worlds.  Generally speaking the MPU handles more multimedia rich tasks, while the MCU handles real-time operations such as controlling motors, monitoring sensors and other various functions. UDOO - After coming off a very successful Kickstarter campaign the UDOO board is gaining some serious traction. You can pick from a dual or quad core Freescale i.MX6 processor with the Atmel SAM32 (aka the Arduino chip) and let the fun begin.  UDoo has a thriving community and really caters well to the "Maker" community. Freedog -  Combines a Atheros AR9331 and Kinetis KL25Z  The Atheros processor supports Linino, a Linux distribution based on OpenWRT. The board has built-in Ethernet and WiFi support, which is a huge plus! The future of personal computing Things are really heating up in the microprocessor corner with lots of new i.MX enabled development boards.  These boards may not go toe-to-toe with your laptop or desktop PC, but the size to performance ratio is just incredible.  For grins I have listed the boards below from largest to smallest. Riot Board- Another SBC (Single Board Computer) solution featuring a single core i.MX 6 application processor.  This board is capable of many things but the focus is for Android development.  I had Netflix and Pandora running on my home TV in less than 30 minutes.  Cool if used for nothing more than a media center! Wand Board - You can pick between single, dual and quad core flavors.  Under the hood this platform is a SOM (System On Module) allowing you to pop this super small plug into your creation and accessorize!  The dual and quad core flavor comes with built in WiFi  and Bluetooth provides a lot of connectivity options. [NEW: Added 7/2/2014] Hummingboard - Several people contributed this in the comments section and I was notified this is now available for purchase.  On paper it looks pretty sweet, same price as the Rasberry Pi but with a much more powerful from a processor performance and peripheral perspective.  I am going to try to get my hands on one and will update you! CuBox - I would put this in more of the finished products camp and not really a development tool, but it is still VERY cool.  A 2 inch cube mini-computer.  Nicely polished packaging and Android O/S, it makes my desktop PC look like a relic. Warp Board - Aimed squarely at wearables, this thing is so small and oh by the way it runs Android and is cranking away at 1 GHz.  It's slated for a end of summer release, but you can start getting updates now from their website!
查看全文
Harvard Extension School CSCI E-251, Fall 2012: Principles of Operating Systems Final Project Presentations Presentation by Eric Pedersen
查看全文