Freescale Cup - Board Mounting Template for the TRK-MPC5604B

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Freescale Cup - Board Mounting Template for the TRK-MPC5604B

Freescale Cup - Board Mounting Template for the TRK-MPC5604B

Depending on which MCU Devlopment board you have chosen, you will need to figure out a way to mount this to the chassis. I have seen everything from cardboard, to aluminum, to wood.

Below is a template complete with CAD drawings to mount the Qorivva TRK-MPC5604B board and the Motor Board onto the chassis.

TFC_BaseBoard.jpgTFC_BaseBoard2.jpgTFC_BaseBoardMounted.jpg

We use plexiglass for ours, but any other millable material is appropriate. The large hole in the middle is for cables from the servo. We attach the board to the car using the
plastic standoffs (you will need them 55 mm long, so in our case, we used the combination of 40 + 15 mm) - see an example (SOS code 10260).
To attach both the processor and interface boards the simillar 5mm plastic standoffs were used.

ラベル(1)
評価なし
バージョン履歴
最終更新日:
‎07-12-2012 07:59 AM
更新者: