The procedure to restrict JTAG access on the S32K3 MCU depends on whether HSE Firmware (FW) is used:
With HSE FW: This scenario is not covered in this document.
Without HSE FW:
WARNING: ONCE THIS PROCESS IS COMPLETED, HSE CANNOT BE INSTALLED ON THE DEVICE.
Development Environment: All code snippets provided represent the essential parts of the application and were developed using:
Test HW: S32K344 (not EVB)
MCU: S32K344
IDE: S32DS v3.5
Debugger: PEmicro USB Multilink Universal FX (unless otherwise noted)
Drivers: S32K3 Real-Time Drivers v3.0.0 (released March 31, 2023)
Base Project: Modified version of C40_Ip_Example_S32K344
Step 1: Program the CUST_DB_PSWD_A Field
The UTEST Sector is an OTP (One Time Programmable), meaning erase operations are not allowed. You can only append or read data.
Memory Range: 0x1B00_0080 to 0x1B00_009
Only the first 16 bytes (0x1B00_0080 to 0x1B00_008F) are usable.
The rest is reserved (see Table 202 in the S32K3xx Reference Manual, Rev. 11).
Programming Steps:
I. Unlock the UTEST sector using PFCBLKU_SPELOCK[SLCK].
II. Write the 16-byte password to address 0x1B00_0080.
Code Adjustments:
/*============================================================================
* LOCAL MACROS
============================================================================*/
#define FLS_MASTER_ID 0U
#define FLS_BUF_SIZE 16U
#define FLS_SECTOR_ADDR 0x1B000080U
#define FLS_SECTOR_TEST C40_UTEST_ARRAY_0_S000
NOTE: Ensure FLS_MAX_VIRTUAL_SECTOR and C40_SECTOR_ERROR are correctly defined in C40_Ip_Cfg.h:
Instead of:
#define FLS_MAX_VIRTUAL_SECTOR (527U)
…
#define C40_SECTOR_ERROR (528U)
Use:
#define FLS_MAX_VIRTUAL_SECTOR (528U)
…
#define C40_SECTOR_ERROR (529U)
/*============================================================================
* GLOBAL CONSTANTS
============================================================================*/
uint8 TxBuffer[FLS_BUF_SIZE] = {0x01,0x02,0x03,0x04,0x05,0x06,0x07,0x08,0x09,0x0A,0x0B,0x0C,0x0D,0x0E,0x0F}; /* Password */
VaneB_0-1696631634239.png
You can verify the password using the Memory Viewer (not covered here).
VaneB_1-1696631672308.png
Step 2: Advance the MCU Lifecycle
I. Set the lifecycle configuration word address in the IVT/boot header. Refer to sections 32.5 and 32.5.3 of the Reference Manual.
NOTE: Ensure the structure of the boot_header (located in Project_Settings → Startup_Code → startup_cm7.s) is defined as follows:
VaneB_2-1696631885135.png
#define LF_CONFIG_ADDR (0x007D2000) /* The LC word can be at any flash address, taking care that does not interfere with HSE */
II. Write the LC word to the defined address:
Life cycle stage
Valid Values for LC Advancement
OEM_PROD
DADA_DADAh
IN_FIELD
BABA_BABAh
Code Adjustments:
/*===========================================================================
* LOCAL MACROS
===========================================================================*/
#define FLS_MASTER_ID 0U
#define FLS_BUF_SIZE 8U
#define FLS_SECTOR_ADDR 0x007D2000U
#define FLS_SECTOR_TEST C40_CODE_ARRAY_0_BLOCK_3_S489 /* Look into C40_Ip_Cfg.h file to find the corresponding sector */
/*===========================================================================
* GLOBAL CONSTANTS
===========================================================================*/
uint8 LC_TxBuffer[FLS_LC_SIZE] = {0xDA, 0xDA, 0xDA, 0xDA, 0x0, 0x0, 0x0, 0x0}; /* Minimum data length 8 bytes */
VaneB_3-1696632329064.png
Confirm the LC word using the Memory Viewer.
VaneB_4-1696632360649.png
III. Reset the MCU using the RESET_B pin, not the debugger.
If the procedure was done correctly, you should see the following message:
VaneB_5-1696632423439.png
Step 3: Debugger Authentication
To unlock the MCU, PEmicro provides Python scripts (PEmicro support files package) to facilitate debugger authentication when the password is set.
In summary:
I. Ensure Python 3.5 or later is installed. II. Open Command Prompt. III. Use cd to navigate to the directory containing the file package. IV. Run the script: py authenticate_password_mode.py -hardwareid=USB1 -password=…
hardwareid: Debug hardware IP, name, serial number, or port
password: 16-byte hexadecimal password
NOTE: This must be done every time the MCU is reset or power cycled.
VaneB_6-1696632573362.png
Step 4: Secure Debugging in S32DS
In S32DS, when configuring the Debug Configurations of a project, change the Target to "SECUREDEBUG". This is necessary because during debug entry, a hard reset is toggled, which clears the authentication.
VaneB_7-1696632658751.png
VaneB_8-1696632678698.png
Once authenticated, you can securely debug the device in S32DS.
*Additional Resources
iSystem: How to unlock secure debug on NXP S32G2/3xx, S32R45x, and S32K3
Segger: NXP S32K3xx - Debug Authentication
Any support, information, and technology (“Materials”) provided by NXP are provided AS IS, without any warranty express or implied, and NXP disclaims all direct and indirect liability and damages in connection with the Material to the maximum extent permitted by the applicable law. NXP accepts no liability for any assistance with applications or product design. Materials may only be used in connection with NXP products. Any feedback provided to NXP regarding the Materials may be used by NXP without restriction.
查看全文