[RTD600 MCAL & IP] S32K3 Low Power Management AN and demos

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[RTD600 MCAL & IP] S32K3 Low Power Management AN and demos

[RTD600 MCAL & IP] S32K3 Low Power Management AN and demos

This is a continuation of the already existing S32K3 Low Power Management AN and demos - NXP Community.

This article provides a software package with additional example projects for wakeup use case using RTD 6.0.0. All the wakeup example projects mentioned in this page are developed based on IP and MCAL layers.

 ------------------------------------------------------------------------------
* Test HW: S32K3X4EVB-T172, S32K312EVB-Q172, S32K396-BGA-DC1
* MCU: S32K344, S32K312, S32K396
* Compiler: S32DS v3.5 & S32DS v3.6.x
* SDK release: RTD 6.0.0
* Debugger: PEMicro
* Target: internal_FLASH
 ------------------------------------------------------------------------------

 

IP/Low-Level Drivers (LLD)

 

MCAL/High-Level Drivers (HLD)

 

These examples are provided as is with no guarantees and no support.

No ratings
Version history
Last update:
‎03-11-2026 11:41 AM
Updated by: