problem while install IAR plugin into S32DS ARM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

problem while install IAR plugin into S32DS ARM

Jump to solution
9,719 Views
steven_zhang
Contributor V

i tried to install IAR plugin into S32DS but get the following errors ,

steven_zhang_1-1606787528700.png

 

Operation details
Cannot complete the install because one or more required items could not be found.
Software being installed: IAR Common Components 3.0.0.202011101213 (com.iar.common.feature.feature.group 3.0.0.202011101213)
Missing requirement: EMF Ecore 2.13.0.v20170609-0707 (org.eclipse.emf.ecore 2.13.0.v20170609-0707) requires 'bundle org.eclipse.emf.common [2.13.0,3.0.0)' but it could not be found
Cannot satisfy dependency:
From: IAR Common Components 3.0.0.202011101213 (com.iar.common.feature.feature.group 3.0.0.202011101213)
To: org.eclipse.emf.ecore.feature.group [2.13.0,3.0.0)
Cannot satisfy dependency:
From: EMF - Eclipse Modeling Framework Core Runtime 2.13.0.v20170609-0707 (org.eclipse.emf.ecore.feature.group 2.13.0.v20170609-0707)
To: org.eclipse.emf.ecore [2.13.0.v20170609-0707

1 Solution
9,305 Views
jwkang
Contributor III

I don't know if it solved the problem, but there is no answer, so I answer.
In my opinion, what I used to do in the past seems to have changed some dependencies.
After seeing the missing EMF message, I accessed the Eclipse site and received the version of the emf package that caused the problem and installed it directly from S32DS.

Get the EMF-Updates-2.13 file from http://download.eclipse.org/modeling/emf/emf/builds/release/2.13/index.html

Select the compressed file downloaded from Install New Software -> Add -> Archive and install all EMF related files. So I solved this problem.

I hope you have good results too.

View solution in original post

11 Replies
9,306 Views
jwkang
Contributor III

I don't know if it solved the problem, but there is no answer, so I answer.
In my opinion, what I used to do in the past seems to have changed some dependencies.
After seeing the missing EMF message, I accessed the Eclipse site and received the version of the emf package that caused the problem and installed it directly from S32DS.

Get the EMF-Updates-2.13 file from http://download.eclipse.org/modeling/emf/emf/builds/release/2.13/index.html

Select the compressed file downloaded from Install New Software -> Add -> Archive and install all EMF related files. So I solved this problem.

I hope you have good results too.

9,242 Views
steven_zhang
Contributor V

it works ,thanks.

Tags (1)
0 Kudos
Reply
9,330 Views
jwkang
Contributor III

I 

0 Kudos
Reply
9,362 Views
jwkang
Contributor III

I have the same issue. Is this a fixed?

0 Kudos
Reply
9,541 Views
stephen_humphre
Contributor II

Was there ever a solution to this?  I am facing the same issue while trying to install S32DS Version 2018.R1 and IAR Embedded Workbench 8.30.1.  They worked great together on my previous laptop, but installing them on my new one using the same installers is producing the issue described above...  (and shown below in the snapshot.)

stephen_humphre_0-1610727426920.png

 

9,709 Views
steven_zhang
Contributor V

S32DS for ARM 2018.R1

0 Kudos
Reply
9,704 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

you are probably trying install unsupported IAR version - https://community.nxp.com/t5/S32-Design-Studio/IAR-Plugin-Issue-for-S32K-Design-Studio/m-p/1190948#M... 

 

Jiri

0 Kudos
Reply
9,695 Views
steven_zhang
Contributor V

I tried the S32DS 2.2 get the same error.

0 Kudos
Reply
9,658 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

here is step by step guide how to install lAR plugin - https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Install-IAR-Eclipse-plug-in-into... 

 

Hope it helps. 

Jiri 

0 Kudos
Reply
9,715 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

same question as on the other IAR thread - what is your S3DS Version?

 

BR, 

Jiri 

0 Kudos
Reply
9,708 Views
steven_zhang
Contributor V

it‘s S32DS FOR ARM 2018.R1.

0 Kudos
Reply