problem while install IAR plugin into S32DS ARM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

problem while install IAR plugin into S32DS ARM

ソリューションへジャンプ
9,539件の閲覧回数
steven_zhang
Contributor V

i tried to install IAR plugin into S32DS but get the following errors ,

steven_zhang_1-1606787528700.pngsteven_zhang_1-1606787528700.png

 

Operation details
Cannot complete the install because one or more required items could not be found.
Software being installed: IAR Common Components 3.0.0.202011101213 (com.iar.common.feature.feature.group 3.0.0.202011101213)
Missing requirement: EMF Ecore 2.13.0.v20170609-0707 (org.eclipse.emf.ecore 2.13.0.v20170609-0707) requires 'bundle org.eclipse.emf.common [2.13.0,3.0.0)' but it could not be found
Cannot satisfy dependency:
From: IAR Common Components 3.0.0.202011101213 (com.iar.common.feature.feature.group 3.0.0.202011101213)
To: org.eclipse.emf.ecore.feature.group [2.13.0,3.0.0)
Cannot satisfy dependency:
From: EMF - Eclipse Modeling Framework Core Runtime 2.13.0.v20170609-0707 (org.eclipse.emf.ecore.feature.group 2.13.0.v20170609-0707)
To: org.eclipse.emf.ecore [2.13.0.v20170609-0707

1 解決策
9,125件の閲覧回数
jwkang
Contributor III

I don't know if it solved the problem, but there is no answer, so I answer.
In my opinion, what I used to do in the past seems to have changed some dependencies.
After seeing the missing EMF message, I accessed the Eclipse site and received the version of the emf package that caused the problem and installed it directly from S32DS.

Get the EMF-Updates-2.13 file from http://download.eclipse.org/modeling/emf/emf/builds/release/2.13/index.html

Select the compressed file downloaded from Install New Software -> Add -> Archive and install all EMF related files. So I solved this problem.

I hope you have good results too.

元の投稿で解決策を見る

11 返答(返信)
9,126件の閲覧回数
jwkang
Contributor III

I don't know if it solved the problem, but there is no answer, so I answer.
In my opinion, what I used to do in the past seems to have changed some dependencies.
After seeing the missing EMF message, I accessed the Eclipse site and received the version of the emf package that caused the problem and installed it directly from S32DS.

Get the EMF-Updates-2.13 file from http://download.eclipse.org/modeling/emf/emf/builds/release/2.13/index.html

Select the compressed file downloaded from Install New Software -> Add -> Archive and install all EMF related files. So I solved this problem.

I hope you have good results too.

9,062件の閲覧回数
steven_zhang
Contributor V

it works ,thanks.

タグ(1)
0 件の賞賛
返信
9,150件の閲覧回数
jwkang
Contributor III

0 件の賞賛
返信
9,182件の閲覧回数
jwkang
Contributor III

I have the same issue. Is this a fixed?

0 件の賞賛
返信
9,361件の閲覧回数
stephen_humphre
Contributor II

Was there ever a solution to this?  I am facing the same issue while trying to install S32DS Version 2018.R1 and IAR Embedded Workbench 8.30.1.  They worked great together on my previous laptop, but installing them on my new one using the same installers is producing the issue described above...  (and shown below in the snapshot.)

stephen_humphre_0-1610727426920.pngstephen_humphre_0-1610727426920.png

 

9,529件の閲覧回数
steven_zhang
Contributor V

S32DS for ARM 2018.R1

0 件の賞賛
返信
9,524件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

you are probably trying install unsupported IAR version - https://community.nxp.com/t5/S32-Design-Studio/IAR-Plugin-Issue-for-S32K-Design-Studio/m-p/1190948#M... 

 

Jiri

0 件の賞賛
返信
9,515件の閲覧回数
steven_zhang
Contributor V

I tried the S32DS 2.2 get the same error.

0 件の賞賛
返信
9,478件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

here is step by step guide how to install lAR plugin - https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Install-IAR-Eclipse-plug-in-into... 

 

Hope it helps. 

Jiri 

0 件の賞賛
返信
9,535件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

same question as on the other IAR thread - what is your S3DS Version?

 

BR, 

Jiri 

0 件の賞賛
返信
9,528件の閲覧回数
steven_zhang
Contributor V

it‘s S32DS FOR ARM 2018.R1.

0 件の賞賛
返信